i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
When using SSI Slave Mode for ASRC_P2P function (https://community.freescale.com/docs/DOC-95342), the waveform of the converted 24bit data is abnormal(have some values between 0 and 1). When using SSI Master Mode, these abnormal data disappear. This patch shows how to enable SSI Master Mode based on ASRC_P2P patches. Because SSI Master Mode uses fixed data width for LRCLK(32bits for each L or R), and the SSI Dual FIFO Mode is not supported for ASRC_P2P, the converted 16bit data is not well supported in this patch. Suggestions: If you want to convert the audio data to 16bit, you can use SSI Slave Mode; if you want to convert the audio data to 24bit, you can use SSI Master Mode.
查看全文
The following are a couple of recommendations for setting up a Host machine for building the Android Nougat 7.1.1_1.0.0 BSP. Some of these recommendations are not exclusive of the Nougat release and may help in other scenarios. These also apply to using Virtual Machines as Host. Installing Open JDK 8 on Ubuntu 14.04 As mentioned on the Android guide for Establishing a Build Environment (http://source.android.com/source/initializing.html) there are no available supported OpenJDK 8 packages for Ubuntu 14.04, which is the version recommended and tested on the Nougat Android BSP. An alternative is downloading the Ubuntu 15.04 Open JDK 8 packages and installing them manually, which can be done by following this procedure: Download the .deb packages for 64-bit architecture from archive.ubuntu.com: openjdk-8-jre-headless_8u45-b14-1_amd64.deb with SHA256 0f5aba8db39088283b51e00054813063173a4d8809f70033976f83e214ab56c0 http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jre-headless_8u45-b14-1_amd64.deb  openjdk-8-jre_8u45-b14-1_amd64.deb with SHA256 9ef76c4562d39432b69baf6c18f199707c5c56a5b4566847df908b7d74e15849 http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jre_8u45-b14-1_amd64.deb  openjdk-8-jdk_8u45-b14-1_amd64.deb with SHA256 6e47215cf6205aa829e6a0a64985075bd29d1f428a4006a80c9db371c2fc3c4c http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jdk_8u45-b14-1_amd64.deb  Once you have downloaded these three packages and checked the checksum for them install the packages (optional) install them by running: $ sudo apt-get update $ sudo dpkg -i openjdk-8-jre-headless_8u45-b14-1_amd64.deb $ sudo dpkg -i openjdk-8-jre_8u45-b14-1_amd64.deb $ sudo dpkg -i openjdk-8-jdk_8u45-b14-1_amd64.deb‍‍‍‍   Increasing SWAP to compensate for the lack of RAM Having insufficient RAM especially on the linking part of the image build may cause a number of issues that are difficult to troubleshoot. In these cases it’s good to take a look at the resource monitor to see if indeed the RAM was depleted. One way to make up for the limited RAM is using a bigger swap. Google recommends at least 16GB of RAM/swap so it’s not uncommon to create a 10GB swap when working in VM, to do this please use the following commands.    $ sudo fallocate -l 10g /mnt/10GB.swap $ sudo chmod 600 /mnt/10GB.swap $ sudo mkswap /mnt/10GB.swap $ sudo swapon /mnt/10GB.swap‍‍‍‍   Increasing heap size to avoid out of memory errors It is possible to encounter an out of memory error with the recommendation “try increasing heap size witj java option ‘-Xmx<size>’. If you encounter this error or would like to proactively avoid it you may run the following commands that will increase heap size to four gigabytes and then reset the Jack Server by killing it and starting it again. With the android environment initialized: $ cd my android $ export JACK_SERVER_VM_ARGUMENTS="-Dfile.encoding=UTF-8 -XX:+TieredCompilation -Xmx4g" $ jack-admin kill-server && jack-admin start-server‍‍‍‍‍‍  Fixing Jack Servers errors due to multiple users on the Host Android Nougat uses Jack Server as mono-user by default. If this is not the case for your host you would need to choose different port numbers for each user and adjust SERVER_NB_COMPILE accordingly. You can also disable the Jack server by setting SERVER=false in your $HOME/.jack. Alternatively, you may also use the patch available on the following link to myandroid/prebuilts/sdk. It will help to fix the mono-user build restriction. When installing the jack-server, it will detect if Jack server is running in the same build machine and then generate a random ports for my build instead of using the default one. https://groups.google.com/forum/#!topic/android-building/UWhJrXH8Vig
查看全文
i.mx8x启动代码定制文档   目录 1    i.MX8X 板级开发包镜像结构... 2 2    创建 i.MX8QXP Linux 4.14.78_ga 板级开发包编译环境... 2 2.1  下载板级开发包... 2 2.2  创建yocto编译环境: 3 3    i.MX8X SC firmware. 11 3.1  SC firmware 目录结构... 11 3.2  SC firmware 启动流程... 12 3.3  SC firmware定制... 12 4    i.MX8X ATF. 18 5    FSL Uboot 定制... 20 5.1  FDT支持... 21 5.2  DM(driver model)支持... 27 5.3  Uboot目录 结构... 40 5.4  Uboot编译... 42 5.5  Uboot初始化流程... 43 5.6  uboot 定制... 53 5.7  uboot debug信息... 60
查看全文
Video, bad performance gst-launch filesrc location=test.mp4 typefind=true ! aiurdemux ! vpudec ! mfw_v4lsink Video, better performance gst-launch filesrc location=sample.mp4 typefind=true ! aiurdemux ! queue max-size-time=0 ! vpudec ! mfw_v4lsink # typefind=true allows to 'type find' the source file before negotiating # max-size-time=0 indicates to ignore possible blocking issues # In case of ASF files gst-launch filesrc location=sample.asf typefind=true ! aiurdemux ! queue max-size-time=0 ! mfw_wmvdecoder ! mfw_v4lsink Audio gst-launch filesrc location=sample.mp3  typefind=true ! beepdec ! audioconvert  ! 'audio/x-raw-int, channels=2' ! alsasink Audio with visualization gst-launch filesrc location=sample.mp3 typefind=true ! beepdec ! tee name=t ! queue ! audioconvert  ! 'audio/x-raw-int, channels=2' ! alsasink t. ! queue ! audioconvert ! goom ! autovideoconvert ! autovideosink Video/Audio long version gst-launch filesrc location=sample.avi typefind=true ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! mfw_v4lsink demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! audioconvert ! 'audio/x-raw-int, channels=2' ! alsasink # queue properties, max-size-buffers=0 and max-size-time=0, allows a smoother playback; type 'gst-inspect queue' for more info VA short version gplay sample.avi VA short version gst-launch playbin2 uri=file://<full path to sample file>
查看全文
$ ~/dylan/sources$ find -name *image*.bb ./meta-fsl-demos/recipes-fsl/images/fsl-image-gui-sdk.bb ./meta-fsl-demos/recipes-fsl/images/fsl-image-test.bb ./meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb ./meta-fsl-demos/recipes-qt/images/qt-in-use-image.bb ./meta-fsl-demos/recipes-qt/images/qte-in-use-image.bb ./meta-openembedded/meta-initramfs/recipes-bsp/images/initramfs-kexecboot-klibc-image.bb ./meta-openembedded/meta-initramfs/recipes-bsp/images/initramfs-kexecboot-image.bb ./meta-openembedded/meta-oe/recipes-support/imagemagick/imagemagick_6.7.5.bb ./meta-openembedded/meta-oe/recipes-multimedia/libsdl-image/libsdl-image_1.2.12.bb ./poky/meta-hob/recipes-core/images/hob-image.bb ./poky/meta-skeleton/recipes-multilib/images/core-image-multilib-example.bb ./poky/meta/recipes-devtools/mkelfimage/mkelfimage_svn.bb ./poky/meta/recipes-sato/images/core-image-sato-dev.bb ./poky/meta/recipes-sato/images/core-image-sato.bb ./poky/meta/recipes-sato/images/core-image-sato-sdk.bb ./poky/meta/recipes-qt/images/qt4e-demo-image.bb ./poky/meta/recipes-core/images/core-image-minimal.bb ./poky/meta/recipes-core/images/core-image-base.bb ./poky/meta/recipes-core/images/core-image-minimal-dev.bb ./poky/meta/recipes-core/images/core-image-minimal-initramfs.bb ./poky/meta/recipes-core/images/build-appliance-image.bb ./poky/meta/recipes-core/images/core-image-minimal-mtdutils.bb ./poky/meta/recipes-extended/images/core-image-lsb-sdk.bb ./poky/meta/recipes-extended/images/core-image-basic.bb ./poky/meta/recipes-extended/images/core-image-lsb-dev.bb ./poky/meta/recipes-extended/images/core-image-lsb.bb ./poky/meta/recipes-graphics/images/core-image-directfb.bb ./poky/meta/recipes-graphics/images/core-image-x11.bb ./poky/meta/recipes-graphics/images/core-image-clutter.bb ./poky/meta/recipes-graphics/xcb/xcb-util-image_0.3.9.bb ./poky/meta/recipes-bsp/u-boot/u-boot-mkimage_2013.01.01.bb ./poky/meta/recipes-bsp/u-boot/u-boot-mkimage_2011.06.bb ./poky/meta/recipes-bsp/u-boot/u-boot-mkimage_2011.03.bb ./poky/meta/recipes-rt/images/core-image-rt-sdk.bb ./poky/meta/recipes-rt/images/core-image-rt.bb Those are all available images. And note that, available images from poky and meta-fsl-arm only. As you may imagine, several other layers can be included, and any new layer can provide new images. If you look line by line, you can see that some of that files are not images, for example u-boot-mkimage_2011.06.bb but you got the message. Yocto Project (and meta-fsl-demos) provides some "pre baked" images. In my point of view, those images are not to be used on your product. They are examples and quick starting points. When you desire a pie, you can go to supermarket and buy a frozen chocolate pie. But when you´re developing a pie to be the Apple Salted Caramel with Dark Chocolate Cinnamon Topping you need to decide every piece of this pie. What is the base, which type of apple to use. How much salt on caramel. This is your product, your pie, not a frozen standard pie. I know the analogy is kind of dumb. But it´s important to understand that the "pre baked" images provided by Yocto Project, or meta-fsl-demos are not supposed to become a product image! You can (and maybe should) base your image on some of those images, but they are not good enough to your product. I highly recommend you to have your own image file. The pre-baked images I´m used with are core-image-minimal I use to image name I use it when/for Formal description core-image-minimal testing machine support; uboot support/upgrade; kernel support/upgrade A small image just capable of allowing a device to boot. core-image-base when I need to add something like ssh/dropbear or evtest or usb utils. I always configure this on local.conf to add the desired package. A console-only image that fully supports the target device hardware. core-image-x11 when I need to test X11 accelerated by GPU, or I need to have X11 for any test. A very basic X11 image with a terminal core-image-direcftb when I debug directfb GPU support An image that uses DirectFB instead of X11. core-image-weston when I debug Wayland GPU support A very basic Wayland image with a terminal fsl-image-test when I need to test VPU with and without gstreamer. - fsl-image-gui when I need to have QT, or I want to build everything altogether. Although I´ve been preferring the smaller images instead. - meta-toolchain To have the crosscompiler installed on my machine to manually build u-boot and kernel, when I´m changing it Meta package for building a installable toolchain All those images DO NOT include -dev packages or native build. If you want it you MUST configure your local.conf. Although, you can find special images that provides the header files or the native compiler. The images with -dev sufix include the header files (and development files) from all packages. For example: core-image-minimal-dev ( A small image just capable of allowing a device to boot and is suitable for development work. ) The images with -sdk sufix include the native build tools. For example core-image-sato-sdk ( Image with Sato support that includes everything within core-image-sato plus meta-toolchain, development headers and libraries to form a standalone SDK. ) *all formal description was copied from poky source code (poky - Poky Build Tool and Metadata) Please, go back to Yocto Training - HOME
查看全文
Ramdisk is unnecessary thing for some embedded systems, but it's required for Android . You can develop an Android system with no ramdisk (initrd/initramfs), just follow these steps: 1) Remove RAMDISK support from kernel: General setup  --->             [ ] Initial RAM filesystem and RAM disk (initramfs/initrd) support Create a single rootfs: cd myandroid/out/target/product/imx51_BBG mkdir rootfs sudo cp -a system rootfs/ sudo cp -a root/* rootfs/ sudo cp -a recovery rootfs/ Since you are using a single filesystem, then comment out these lines from rootfs/init.rc: #mount ext3 /dev/block/mmcblk0p2 /system #mount ext3 /dev/block/mmcblk0p2 /system ro remount #mount ext3 /dev/block/mmcblk0p5 /data nosuid nodev #mount ext3 /dev/block/mmcblk0p6 /cache nosuid nodev Create just one partition into your MMC or Flash memory: Partition 1: 200MB+ as EXT3 will be used as system(rootfs). Remember to skip 4MB to save kernel. It is a good idea to create a second partition (VFAT) to mount as /data to save user files. Mount that "system" partition and copy all content of rootfs: sudo mount /dev/sdb1 -t ext3 /mnt sudo cp -a .../target/product/imx51_BBG/rootfs/* /mnt sudo umount /mnt Now just setup your bootloader parameter correctly (i.e. MMC Partition 1): setenv bootargs_base 'setenv bootargs root=/dev/mmcblk0p1 rootfstype=ext3 console=ttymxc0,115200 noinitrd'
查看全文
There are two format system image(ext4): raw and sparse. The raw image is  larger, you can mount it to ext4 directly(mount -t ext4 system.img system). The sparse image is supported lp5.0, it is a bit smaller. The below part will take IMX7D SDB board as example. You can change the setting according your platform hardware.   1 generate sparse image   In Lollipop 5.0 and 5.1, both raw image and sparse image will be generated by default. sparse system image is located in: out/target/product/sabresd_7d/system_sparse.img raw system image is located in:out/target/product/sabresd_7d/system.img Below are the steps used in android build system to generate system.img build out sparse image(-s means the building system image is sparse)           make_ext4fs -s -T -1 -S out/target/product/sabresd_7d/root/file_contexts -l 374476800 -a system           out/target/product/sabresd_7d/obj/PACKAGING/systemimage_intermediates/system.img out/target/product/sabresd_7d/system transform sparse image to raw image           simg2img out/target/product/sabresd_7d/system_sparse.img out/target/product/sabresd_7d/system.img   2 burn sparse image to sd/emmc      There are two ways to program the sparse image into android boot storage Transform the sparse image into raw image in host Linux PC. And use the commands dd commands to program the raw image into the boot storage. Program the sparse image with MFG Tool in i.MX Android release package.                Steps: copy system_sparse.img to files/android/sabresd/. copy simg2img binary (in simg2img.zip) to files/android/. You also need update mfgtools-without-rootfs.tar\mfgtools\Profiles\Linux\OS Firmware\ucl2.xml        diff --git a/Profiles/Linux/OS Firmware/ucl2.xml b/Profiles/Linux/OS Firmware/ucl2.xml      index 3b15ddd..3c3d2ae 100755      --- a/Profiles/Linux/OS Firmware/ucl2.xml      +++ b/Profiles/Linux/OS Firmware/ucl2.xml        @@ -621,8 +621,12 @@              <CMD state="Updater" type="push" body="$ mkfs.ext4 /dev/mmcblk%mmc%p6">Formatting cache partition</CMD>                <CMD state="Updater" type="push" body="$ mkfs.ext4 /dev/mmcblk%mmc%p7">Formatting device partition</CMD>      -       <CMD state="Updater" type="push" body="pipe dd of=/dev/mmcblk%mmc%p5 bs=512" file="files/android/sabresd/system.img">Sending and writting system.img</CMD>      -      +       <CMD state="Updater" type="push" body="send" file="files/android/simg2img" ifdev="MX7D">Sending simg2img</CMD>      +       <CMD state="Updater" type="push" body="$ cp $FILE /tmp/simg2img ">cp simg2img</CMD>      +       <CMD state="Updater" type="push" body="$ chmod  777 /tmp/simg2img ">chmod 777</CMD>      +       <CMD state="Updater" type="push" body="$  mount -o remount,size=512M rootfs /">change size of tmpfs</CMD>      +       <CMD state="Updater" type="push" body="send" file="files/android/sabresd/system_sparse.img" ifdev="MX7D">Sending system_sparse.img</CMD>      +       <CMD state="Updater" type="push" body="$ /tmp/simg2img $FILE /dev/mmcblk%mmc%p5">Sending and writting system_sparse.img</CMD>              <!-- Write userdata.img is optional, for some customer this is needed, but it's optional. -->              <!-- Also, userdata.img will have android unit test, you can use this to do some auto test. -->              <!--    <CMD state="Updater" type="push" onError="ignore" body="pipe dd of=/dev/mmcblk0p7" file="file/android/userdate.img"> Sending userdata.   3 Support sparse image in uboot(v2014.04)      Cheery-pick sparse image related patches. Use write_sparse_image to burn sparse system image.      For detail information, Please check the attached file(uboot(v2014.04)which support sparseimage.zip )        The step of apply these patches: cd myandroid/bootable/bootloader/uboot-imx/ copy uboot(v2014.04) which support sparseimage.zip to myandroid/bootable/bootloader/uboot-imx/         unzip uboot(v2014.04) which support sparseimage.zip git am 0001-add-header-for-Android-sparse-image-format.patch         git am 0002-add-code-to-handle-Android-sparse-image-format.patch         git am 0003-update-code-which-handles-Android-sparse-image-forma.patch         git am 0004-cleanup-code-which-handles-the-Android-sparse-image-.patch         git am 0005-implement-the-Android-sparse-image-format.patch         git am 0006-aboot-fix-block-addressing-for-don-t-care-chunk-type.patch         git am 0007-MA-6732-Add-sparse-image-flash-support-for-uboot-s-f.patch            The page will keep updating.   Reference:      How to enable userdata.img and cache.img in lollipop
查看全文
Issue: On i.MX 6Solo designs using LPDD2 memory, the correct settings for two important registries may be confusing to determine. Solution: 1) MMDCx_MDMISC register, LPDDR2_2CH Field: For the i.MX 6Solo processor, this field should always be set to '0'. Reason: Two channel mode is not possible on this processor. Only channel MMDC0 is connected to external pins. 2) IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET register, DDR_SEL Field: For the i.MX 6Solo processor, this field should always be set to "00". Reason: A DRAM Warm Reset requires a response from MMDC1, which is not connected externally on the 6Solo processor, so a Warm Reset never complets. These two issues will be clarified in a subsequent revision of the MCIMX6SDL Reference Manual.
查看全文
The document in attachment describes how to learn System Boot Flow of Linux by code using Trace32. The hardware platform is i.MX6Q SABRE and the software in PC is Trace32. Contents 1. Introduction 2. Hardware Connection 3. Serial Connection Setup 4. U-boot Directory Setup 5. Trace32 Installation & U-boot Debugging
查看全文
This document provides the steps to patch and build a fastboot Linux System. This document assumes the BSP 3.0.35_1.1.0 and a  i.MX6Q platform. For more information about what the patches do, please check this link. Install LTIB and move to the ltib folder Download the ltib patch from this document and patch it (patch -p1 < 0001-set-imx6_ssd_lite_defconfig-as-default-kernel-config.patch) Go to the LTIB configuration menu (./ltib -m config), select mx6q platform and min profile Select mx6q_sabresd as u-boot board Fetch and Patch: u-boot: Prepare u-boot source code (./ltib -m prep -p u-boot) Move to u-boot folder (cd rpm/BUILD/u-boot-2009.08) Download u-boot attached patches Patch code (for p in *.patch; do patch -p1 < $p;done) kernel: Prepare kernel source code (./ltib -m prep -p kernel) Move to kernel folder (cd rpm/BUILD/linux) Download attached kernel patches Patch code (for p in *.patch; do patch -p1 < $p;done) Build  (./ltib) Add  an application to run first after boot in rootfs/etc/inittab (see example inittab file, it captures data from the MIPI Camera) Create necessary devices nodes under rootfs/dev. For example terminal: sudo mknod ttymxc0 c 207 16 video capture nodes: sudo mknod video0 c 81 5; sudo mknod video1 c 81 6 video display nodes: sudo mknod video16 c 81 0; sudo mknod video17 c 81 1 frame-buffers: for i in 0 1 2 3 4; do sudo mknod fb$i c 29 $i; done Package rootfs (cd rootfs; sudo tar --numeric-owner -cvfj ../rootfs.tar.bz2 *; cd ..) On a windows machine, download latest Manufacturing tool and uncompress it. Move rootfs.tar.bz2, rootfs/boot/uImage and rootfs/boot/u-boot.bin into the corresponding Manufacturing folder (Profiles\MX6Q Linux Update\OS Firmware\files) Choose a sabresd-eMMC profile and flash the board Boot the board using the eMMC
查看全文
There are two ways: 1. BitBake. Append the package into the IMAGE_INSTALL variable. But In case you want the package in every image,  add a line to your conf/local.conf file IMAGE_INSTALL_append = " package"           Make sure to include the space BEFORE the package name. You can add other packages, just place spaces in-between. In case you want the package in a particular image, e.g. fsl-image-gui,, add it on meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb IMAGE_INSTALL += " \     ${SOC_IMAGE_INSTALL} \     cpufrequtils \     nano \     packagegroup-fsl-gstreamer \     packagegroup-fsl-tools-testapps \     packagegroup-fsl-tools-benchmark \     packagegroup-qt-in-use-demos \     qt4-plugin-phonon-backend-gstreamer \     qt4-demos \     qt4-examples \     fsl-gui-extrafiles \     package \     " 2. Hob. Due to its graphical nature, adding more packages to a base image is easier than the bitbake way. Run the hob app under the build folder, select your machine and image, then edit the later (click on the Edit image button) In case the package is not available, you need to create it. As a starting point take a look at this example. In case you consider is good enough to be present on the mainstream repos, send the patch to the meta-freescale mailing list.
查看全文
In Chinese Twitter: Sino Weibo, one famous distributor mentioned “i.MX28 is the best choice in ARM9 core-based processor, no ‘one of’”. With high integration of analog module and digital module, i.MX28 is attracting more and more engineers in various applications. Despite its advantage, there are some mistakes one may commit or issues they may meet. The note records a number of issues/mistakes. Each case in the note comes from a real story. I hope the note will help you in your development work. And It is definitely welcomed for everyone to add your own content to the note.The more you share, the more you get.
查看全文
Boundary Devices has a tool to load directly a U-boot binary file, all using the USB OTG port. Assuming that you have connected your i.MX board to your Linux Host through an USB cable, board is power-on  with dip switches configure to 'Serial Download Mode' (this configuration depends on the board you are booting),  clone the imx_usb_loader repo, generate the tool then boot as indicate below: $ git clone https://github.com/boundarydevices/imx_usb_loader.git $ cd imx_usb_loader $ make $ ./ imx_usb   ../ tmp/deploy/images/ u-boot.imx On the console terminal, you should see the booting kernel logs and at the end reaching the login prompt. Useful Links: [1] Unbricking a Nitrogen6X or Sabre Lite i.MX6 board [2] Boundary Devices Repos [3] Boundary Devices Main page
查看全文
  Just sharing some experiences during the development and studying.   Although, it appears some hardwares, it focuses on software to speed up your developing on your  hardware.     杂记共享一下在开发和学习过程中的经验。    虽然涉及一些硬件,但其本身关注软件,希望这些能加速您在自己硬件上的开发。   12/16/2025 iMX8MN DDR3 Frequency Shifting iMX8MN DDR3 Frequency Shifting - NXP Community   3/4/2025 GPIO USB ID GPIO USB ID - NXP Community   1/20/2025 MDIO on GPIOs MDIO on GPIOs - NXP Community   12/09/2024 GPIO LEDs https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/GPIO-LEDs/ta-p/2009743     10/22/2024 iMX93-EVK PWM LED https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX93-EVK-PWM-LED/ta-p/1978047   07/25/2024 iMX secondary boot collection https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-secondary-boot-collection/ta-p/1916915   07/25/2024 HSM Code-Signing Journey https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244 25JUL2024 - add pkcs11 proxy                         HSM Code-Signing Journey_25JUL2024.pdf                          HSM Code-Signing Journey_25JUL2024.txt   06/06/2024 HSM Code-Signing Journey https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244     02/07/2024 Device Tree Standalone Compile under Windows https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Device-Tree-Standalone-Compile-under-Windows/ta-p/1855271   02/07/2024 i.MX8X security overview and AHAB deep dive i.MX8X security overview and AHAB deep dive - NXP Community   11/23/2023 “Standalone” Compile Device Tree https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Standalone-Compile-Device-Tree/ta-p/1762373     10/26/2023 Linux Dynamic Debug https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Dynamic-Debug/ta-p/1746611   08/10/2023 u-boot environment preset for sdcard mirror u-boot environment preset for sdcard mirror - NXP Community   06/06/2023 all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek all(bootloader, device tree, Linux kernel, rootfs)... - NXP Community     09/26/2022 parseIVT - a script to help i.MX6 Code Signing parseIVT - a script to help i.MX6 Code Signing - NXP Community   Provide  run under windows   09/16/2022   create sdcard mirror under windows create sdcard mirror under windows - NXP Community     08/03/2022   i.MX8MM SDCARD Secondary Boot Demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011     02/16/2022 mx8_ddr_stress_test without UI   https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/mx8-ddr-stress-test-without-UI/ta-p/1414090   12/23/2021 i.MX8 i.MX8X Board Reset https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-i-MX8X-Board-Reset/ta-p/1391130       12/21/2021 regulator userspace-consumer https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/regulator-userspace-consumer/ta-p/1389948     11/24/2021 crypto af_alg blackkey demo crypto af_alg blackkey demo - NXP Community   09/28/2021 u-boot runtime modify Linux device tree(dtb) u-boot runtime modify Linux device tree(dtb) - NXP Community     08/17/2021 gpio-poweroff demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/gpio-poweroff-demo/ta-p/1324306         08/04/2021 How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709       07/14/2021 SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416     04/07/2021 i.MX8QXP eMMC Secondary Boot https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45       03/25/2021 sc_misc_board_ioctl to access the M4 partition from A core side sc_misc_board_ioctl to access the M4 partition fr... - NXP Community     03/17/2021 How to Changei.MX8X MEK+Base Board  Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8X-MEK-Base-Board-Linux-Debug-UART/ba-p/1246779#M43     03/16/2021 How to Change i.MX8MM evk Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938#M40       05/06/2020 Linux fw_printenv fw_setenv to access U-Boot's environment variables Linux fw_printenv fw_setenv to access U-Boot's env... - NXP Community     03/30/2020 i.MX6 DDR calibration/stress for Mass Production https://community.nxp.com/docs/DOC-346065     03/25/2020 parseIVT - a script to help i.MX6 Code Signing https://community.nxp.com/docs/DOC-345998     02/17/2020 Start your machine learning journey from tensorflow playground Start your machine learning journey from tensorflow playground      01/15/2020 How to add  iMX8QXP PAD(GPIO) Wakeup How to add iMX8QXP PAD(GPIO) Wakeup    01/09/2020 Understand iMX8QX Hardware Partitioning By Making M4 Hello world Running Correctly https://community.nxp.com/docs/DOC-345359   09/29/2019 Docker On i.MX6UL With Ubuntu16.04 https://community.nxp.com/docs/DOC-344462   09/25/2019 Docker On i.MX8MM With Ubuntu https://community.nxp.com/docs/DOC-344473 Docker On i.MX8QXP With Ubuntu https://community.nxp.com/docs/DOC-344474     08/28/2019 eMMC5.0 vs eMMC5.1 https://community.nxp.com/docs/DOC-344265     05/24/2019 How to upgrade  Linux Kernel and dtb on eMMC without UUU How to upgrade Linux Kernel and dtb on eMMC without UUU     04/12/2019 eMMC RPMB Enhance and GP https://community.nxp.com/docs/DOC-343116   04/04/2019 How to Dump a GPT SDCard Mirror(Android O SDCard Mirror) https://community.nxp.com/docs/DOC-343079   04/04/2019 i.MX Create Android SDCard Mirror https://community.nxp.com/docs/DOC-343078   04/02/2019: i.MX Linux Binary_Demo Files Tips  https://community.nxp.com/docs/DOC-343075   04/02/2019:       Update Set fast boot        eMMC_RPMB_Enhance_and_GP.pdf   02/28/2019: imx_builder --- standalone build without Yocto https://community.nxp.com/docs/DOC-342702   08/10/2018: i.MX6SX M4 MPU Settings For RPMSG update    Update slide CMA Arrangement Consideration i.MX6SX_M4_MPU_Settings_For_RPMSG_08102018.pdf   07/26/2018 Understand ML With Simplest Code https://community.nxp.com/docs/DOC-341099     04/23/2018:     i.MX8M Standalone Build     i.MX8M Standalone Build.pdf     04/13/2018:      i.MX6SX M4 MPU Settings For RPMSG  update            Add slide CMA Arrangement  Consideration     i.MX6SX_M4_MPU_Settings_For_RPMSG_04132018.pdf   09/05/2017:       Update eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 09/01/2017:       eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 08/30/2017:     Dual LVDS for High Resolution Display(For i.MX6DQ/DLS)     Dual LVDS for High Resolution Display.pdf 08/27/2017:  L3.14.28 Ottbox Porting Notes:         L3.14.28_Ottbox_Porting_Notes-20150805-2.pdf MFGTool Uboot Share With the Normal Run One:        MFGTool_Uboot_share_with_NormalRun_sourceCode.pdf Mass Production with programmer        Mass_Production_with_NAND_programmer.pdf        Mass_Production_with_emmc_programmer.pdf AndroidSDCARDMirrorCreator https://community.nxp.com/docs/DOC-329596 L3.10.53 PianoPI Porting Note        L3.10.53_PianoPI_PortingNote_151102.pdf Audio Codec WM8960 Porting L3.10.53 PianoPI        AudioCodec_WM8960_Porting_L3.10.53_PianoPI_151012.pdf TouchScreen PianoPI Porting Note         TouchScreen_PianoPI_PortingNote_151103.pdf Accessing GPIO From UserSpace        Accessing_GPIO_From_UserSpace.pdf        https://community.nxp.com/docs/DOC-343344 FreeRTOS for i.MX6SX        FreeRTOS for i.MX6SX.pdf i.MX6SX M4 fastup        i.MX6SX M4 fastup.pdf i.MX6 SDCARD Secondary Boot Demo        i.MX6_SDCARD_Secondary_Boot_Demo.pdf i.MX6SX M4 MPU Settings For RPMSG        i.MX6SX_M4_MPU_Settings_For_RPMSG_10082016.pdf Security        Security03172017.pdf    NOT related to i.MX, only a short memo
查看全文
bitbaked meta-toolchain-qt Install it  with ~/yocto/build/tmp/deploy/sdk$ poky-eglibc-x86_64-arm-toolchain-qt-1.4.1.sh Download Qtcreator from here http://qt-project.org/downloads and Install it to Your home directory edit the bin/qtcreator.sh source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi #! /bin/sh makeAbsolute() {     case $1 in         /*)             # already absolute, return it             echo "$1"             ;;         *)             # relative, prepend $2 made absolute             echo `makeAbsolute "$2" "$PWD"`/"$1" | sed 's,/\.$,,'             ;;     esac } .... To do it before "#! /bin/sh" is IMPORTANT!!!! In QtCreator i set Compiler as                /opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/armv7a-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++ Qt version as                               /opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/qmake sysroot as                     /opt/poky/1.4.1/sysroots/armv7a-vfp-neon-poky-linux-gnueabi Put them in a Kit For connection to Your Board click on  Device  --->    Manage Build a new project and add some to the .pro file Building the image for Your Board: add         EXTRA_IMAGE_FEATURES = "debug-tweaks ssh-server-openssh" to Your localconfig bitbake core-image-sato-sdk set a password to root  via ssh root@[boardip] passwd test connection via sftp  root@[boardip] start qtcreator ./qtcreator.sh Message was edited by: Joerg Boge Good Video to get more Information about Programming are this Beaglebone: LCD Touchscreen GUI Applications for Embedded Linux - YouTube Beaglebone: Qt Creator for C++ ARM Embedded Linux Development - YouTube Beaglebone: Example Qt Embedded Linux Application - YouTube It is for Beagelbone but for programming Qt it is a good start. Dieses Dokument wurde aus folgender Diskussion erzeugt: Setup QT Creator with Yocto Build
查看全文
Here is the explaination of relationship of SD-CAN, SD-MAN, 6233, 6003, 3002: AR6003 + AR3002 = AR6233 AR6233 + RF Components = SX-SDMAN-2830S SX-SDMAN-2830S + SDIO CONN = SX-SDCAN-2830BT SX-SDCAN-2830BT card is inserted into SD3 slot. BT adaptor board (attached files) is inserted into SD1 slot. SX-SDCAN-2830BT card is connected with BT adaptor board via 20-pin FFC. Software: signals of SD1 are muxed into UART4 and GPIO for BT application. Below is the description of IO mux on SD1:
查看全文
Since LF_v5.10.52-2.1.0 crypto_af_alg blackkey demo “caam-decrypt” becomes default in release. You can try it with binary demo release image. The demo is using black key to decrypt data. This document goes more detail based on BSP release document i.MX Linux® User's Guide, Rev. LF5.10.52_2.1.0, 15 October 2021 10.6 crypto_af_alg application support   HW: i.MX8MM EVK SW: LF_v5.10.52-2.1.0_images_IMX8MMEVK binary demo image PC side: 1. generate key and iv by openssl echo 12345 | openssl enc -aes-256-cbc -k - -P -md sha1 -pbkdf2 salt=1982686A7BACEE4D key=D84041EC14BB28543E8545BEB094FE643B5BC1345C31CD576BC708A1559FBD2D iv =F950CACE80F76F0AC00D9C8762B3A5C9 2. encrption by openssl echo "For test caam-decrypt" | openssl enc -e -aes-256-cbc -in - -out test.txt.enc -K D84041EC14BB28543E8545BEB094FE643B5BC1345C31CD576BC708A1559FBD2D -iv F950CACE80F76F0AC00D9C8762B3A5C9 3. decryption by openssl openssl enc -d -aes-256-cbc -in test.txt.enc -out - -K D84041EC14BB28543E8545BEB094FE643B5BC1345C31CD576BC708A1559FBD2D -iv F950CACE80F76F0AC00D9C8762B3A5C9 4. convert key and iv to plian txt for caam-decrypt. echo F950CACE80F76F0AC00D9C8762B3A5C9| xxd -r -p > fromopenssl.iv.txt echo D84041EC14BB28543E8545BEB094FE643B5BC1345C31CD576BC708A1559FBD2D| xxd -r -p > fromopenssl.key.txt 5. prepare data for caam-decrypt cat fromopenssl.iv.txt test.txt.enc > data.caam-decrypt.enc note: the format for with blackkey AES Encrypted file format 16 Octets - Initialization Vector (IV) is an input to encryption algorithm. nn Octets - Encrypted message (for AES-256-CBC, it must be multiple of 16) 6. send fromopenssl.key.txt and data.caam-decrypt.enc to the board on i.MX8MM evk board 1. generate blackkey blob caam-keygen create blackkey ecb -t $(cat fromopenssl.key.txt) 2. delete fromopenssl.key.txt 3. test decryption by caam-decrypt with blackkey caam-decrypt /data/caam/blackkey.bb AES-256-CBC data.caam-decrypt.enc data.caam-decrypt.dec root@imx8mmevk:/# cat data.caam-decrypt.dec For test caam-decrypt  
查看全文
-BACKGROUND       Since the release of i.MX8MQ and i.MX8M Mini, some customers have submitted questions about the design of USB2.0 for these two processors: due to the needs of the project, there is no need to use USB3.0 and USB TYPE-C. Therefore, these applications need to use a conventional USB2.0 interface design similar to i.MX6Q.       In order for customers with similar needs to complete the design smoothly, this document summarizes the answers to previous customer responses and draws two USB2.0 design schematics. At the same time, the i.MX expert hardware team member helped review these two drawings, and the i.MX Expert software team gave suggestions on software adjustments. -BEGIN       i.MX8MQ supports USB3.0 and is compatible with USB2.0, i.MX8M Mini only supports USB2.0, not USB3.0. In both development boards, the USB TYPE-C design scheme is used. We must remove the USB TYPE-C, PD chip and logic chip. At the same time, change the connector to MicroUSB and USB TYPE-A-F. No.1 Hardware Design 1. IOMUX list 2 、USB circuit design (1) USB Power & OC control I.MX8MM i.MX8MQ                                                 i.MX8MQ                                              i.MX8MQ [Comment] For i.MX8MQ -USB1 is configured as Dual Role Mode, USB1 OTG ID is used for detection -USB2 is configured as fixed Host mode, USB2 OTG ID is used for detection -i.MX8M Mini USB2.0                                        i.MX8M Mini                                     i.MX8M Mini [Comment] For i.MX8M Mini -USB1 is configured as Dual Role Mode, USB1 OTG ID is used for detection -USB2 is configured as fixed Host mode, USB2 OTG ID is used for detection (3) Additional description --About USB1_VBUS & USB2_VBUS of i.MX8M Mini          According to i.MX8M Mini datasheet, USB1_VBUS & USB2_VBUS allows 0~3.9V input. See below, please! Therefore, some customers have questioned the USB1_VBUS on the I.MX8M Mini-EVK. From the drawings, the external input voltage exceeds this range.          In fact, customers do not need to worry about this problem. There are internal voltage-dividing resistors on the USB1_VBUS and USB2_VBUS pins. As long as the customer refers to the design method on the I.MX8M Mini-EVK, the input voltage of these 2 pins can be guaranteed Inside. --About USBx OTG ID & USBx_ID (1) USBx_OTG_ID          USBx OTG ID is also called GPIO ID, which is the same as that of i.MX6Q. During the work process, the software changes the role between device and host according to the level of the ID pin from high to low or from low to high. (2)USBx_ID          USBx_ID is called USB PHY ID, which can also perform the same function as USBx OTG ID. (3)Using USBx_OTG_ID or USBx_ID          USBx_OTG_ID is recommended. But if customer wants to use USBx_ID, for i.MX8MQ, she can configure USB_CTL0_ADDR[utmiotg_iddig_sel] register. And for I.MX8M Mini, USBNC_n_CTRL2[DIG_ID_SEL] register. [Comment]          The configuration is got from reference manual of these 2 processors, due to no suitable board, this configuration is not validated on board. Customers can try it. (4) About Flashing Images to the Storage of Board          For an empty board or a board that requires an update image, we need to use the USB interface to program the image. At this time, we need the USB interface to work in device mode. For this, the ROM CODE inside the CPU will ensure that the USB works in device mode. No.2 Tuning Software 1.IOMUX According to the actual application, the signals to be used are multiplexed in the dts file. This step is relatively simple and will not be described here 2. Tuning USB configuration in u-boot / device tree For i.MX8M Mini & i.MX8MQ, i.MX Expert softer team gives the following suggestions, I quote their suggestions here:       Customer can try it by removing CONFIG_USB_TCPC in imx8mm_evk_defconfi and well as removing the typec_ptn5110_1/2 dependencies in the fsl-imx8mm-evk.dts. The uboot does check the state of the Type C ICs and crash or gets stuck if they are removed. --i.MX8M Mini U-BOOT:  CONFIG_USB_TCPC=n Device Tree: &usbotg1 {     status = "okay"; }; &usbotg2 {     status = "okay"; --------------------------------------------------------- --i.MX8MQ --u-boot CONFIG_USB_TCPC=n --Node of Device tree &usb_dwc3_0 {              status = "okay";              /*extcon = <&typec_ptn5100>;*/              dr_mode = "otg";              hnp-disable;              srp-disable;              adp-disable;              maximum-speed = "high-speed"; }; ---------------------------------------------- -END [Comment] If you encounter problems while using this document, please submit a ticket to me. Here are the steps to submit a ticket: 1. Open below SUPPORT site, click blue "Go to Tickets" in the middle. http://www.nxp.com/support/support:SUPPORTHOME 2.Then you will be requested to Login, if you have no an account, please first Register with your business email. 3.After login, please "Create New Cases" button in the middle, then you can submit your question. NXP TIC team Weidong Sun 2020/3/30
查看全文
1  Introduction   This document explains how to configure a cross compiler running in iMX6Q. The target is the Kinetis L family.  For the iMX6Q, Yocto is used to generate the iMX6Q image. 2 Requirements   Basic knowledge of Yocto and Linux is required. The steps explained were performed for the iMX6Q SABRE-SD and the Freedom KL25.  Installation of Yocto in your host system is needed too. 3 Procedure   The chosen method to configure the cross compiler for the Kinetis L, needs a native compiler that will run in the iMX6Q. Below are the general steps:   Generate native compiler for the iMX6Q and adding the needed packages for the configuration. Get and extract the source packages of the compiler. Configure, build and install the packages Test the generated cross compiler   3.1 Generating packages and native compiler for the iMX6Q   The iMX6Q image needs certain packages in order to configure and generate correctly the cross-compiler. After setting up the environment and chose the MACHINE the below lines added in the local.conf file to install those packages in our rootfs:   IMAGE_INSTALL_append = " gcc g++ binutils libgcc libgcc-dev libstdc++ libstdc++-dev libstdc++-staticdev gawk gzip perl autoconf automake libtool gettext gperf tcl guile gmp mpfr make m4 texinfo flex bison git"   The image to generate is the core-image-minimal:   bitbake core-image-minimal   Once the building is finished, a native compiler for the iMX6 and other packages needed to configure the Kinetis Compiler should be added to the Yocto image. 3.2 Getting and Extracting the Kinetis L compiler   The arm cross compiler version was gotten from CodeSourcery. arm-2011.03-42-arm-none-eabi is used in this document. You can get the source code by:   wget https://sourcery.mentor.com/sgpp/lite/arm/portal/package8736/public/arm-none-eabi/arm-2011.03-42-arm-none-eabi.src.tar.bz2   Once the image was built, boot the imx6 board with this image. Copy the source code (arm-2011.03-42-arm-none-eabi.src.tar.bz) in your target that is running Linux and extract the files.   For example, a new folder was created in /home/root directory:   $ mkdir gcc_test $ cd gcc_test   And extract the files in this folder:   $ tar –jxvf  arm-2011.03-42-arm-none-eabi.src.tar.bz2 $ cd arm-2011.03-42-arm-none-eabi   Create a source and a build folder:   $ mkdir source build   Move all the files to the source folder:   $ mv *.tar.bz2 source/   Create a new folder in /opt where the kinetis cross compiler will be installed   $ cd /opt              $ mkdir arm-none-eabi   3.3 Configure, Build and Install Kinetis Compiler on the iMX6   To configure, build and install the compiler these general steps are followed for certain packages:   Extract the package Configure the package Build and Install the package   Create an environment variable that will specify where the cross compiler will be installed:   $ export INSTALL_PREFIX=/opt/arm-none-eabi   3.3.1 GMP Package   Extract the gmp files: $ cd ~/gcc_test/arm-2011.03-42-arm-none-eabi/source $ tar –jxvf gmp-2011.03-42.tar.bz2   Create a new folder in build directory. This folder will contain a generated Makefile that will be used to build and install the package:   $ cd ../build $ mkdir gmp $cd gmp   Configure the package: $ ../../source/gmp-2011.03/configure --prefix=$INSTALL_PREFIX --build=arm-poky-linux-gnueabi CC=arm-poky-linux-gnueabi-gcc CXX=arm-poky-linux-gnueabi-g++  --disable-newlib-supplied-syscalls --disable-libgloss --disable-nls --disable-shared   Build and Install the package $make $make install 3.3.2 MPFR Package   Extract the mpfr files: $ cd ~/gcc_test/arm-2011.03-42-arm-none-eabi/source $ tar –jxvf mpfr-2011.03-42.tar.bz2   Create a new folder in build directory. This folder will contain a generated Makefile that will be used to build and install the package:   $ cd ../build $ mkdir mpfr $cd mpfr   Configure the package: $ ../../source/mpfr-2011.03/configure --prefix=$INSTALL_PREFIX  --build=arm-poky-linux-gnueabi --target=arm-none-eabi CC=arm-poky-linux-gnueabi-gcc CXX=arm-poky-linux-gnueabi-g++ --with-gmp=$INSTALL_PREFIX --disable-shared   Build and Install the package $make $make install   3.3.3 MPC Package   Extract the mpc files: $ cd ~/gcc_test/arm-2011.03-42-arm-none-eabi/source $ tar –jxvf mpc-2011.03-42.tar.bz2   Create a new folder in build directory. This folder will contain a generated Makefile that will be used to build and install the package:   $ cd ../build $ mkdir mpc $cd mpc   Configure the package: $ ../../source/mpc-0.8.1/configure --prefix=$INSTALL_PREFIX --target=arm-none-eabi --build=arm-poky-linux-gnueabi CC=arm-poky-linux-gnueabi-gcc CXX=arm-poky-linux-gnueabi-g++ --with-gmp=$INSTALL_PREFIX --with-mpfr=$INSTALL_PREFIX --disable-shared   Build and Install the package $make $make install   3.3.4 Binutils Package                                                                                 Extract the binutils files: $ cd ~/gcc_test/arm-2011.03-42-arm-none-eabi/source $ tar –jxvf binutils--2011.03-42.tar.bz2   Create a new folder in build directory. This folder will contain configure the package:   $ cd ../build $ mkdir binutils $cd binutils   Configure the package: $ ../../source/binutils-2011.03/configure --prefix=$INSTALL_PREFIX --target=arm-none-eabi --build=arm-poky-linux-gnueabi CC=arm-poky-linux-gnueabi-gcc CXX=arm-poky-linux-gnueabi-g++ --with-gmp=$INSTALL_PREFIX --with-mpfr=$INSTALL_PREFIX --with-mpc=$INSTALL_PREFIX --disable-nls --disable-werror   Build and Install the package $make MAKEINFO=true $make install MAKEINFO=true   3.3.5 GCC Package   Extract the gcc files: $ cd ~/gcc_test/arm-2011.03-42-arm-none-eabi/source $ tar –jxvf    Create a new folder in build directory. This folder will contain configure the package:   $ cd ../build $ mkdir gcc $cd gcc   Configure the package: $ ../../source/gcc-4.5-2011.03/configure --prefix=$INSTALL_PREFIX --target=arm-none-eabi   --build=arm-poky-linux-gnueabi  --host=arm-poky-linux-gnueabi  CC=arm-poky-linux-gnueabi-gcc CXX=arm-poky-linux-gnueabi-g++ --enable-languages="c" --with-gnu-ld --with-gnu-as --with-newlib --disable-nls --disable-libssp --with-newlib --without-headers --disable-shared --disable-threads  --disable-libmudflap --disable-libgomp --disable-libstdcxx-pch --disable-libunwind-exceptions --disable-libffi  --enable-extra-sgxxlite-multilibs  --with-gmp=$INSTALL_PREFIX --with-mpfr=$INSTALL_PREFIX --with-mpc=$INSTALL_PREFIX   Build and Install the package $make $make install     3.4 Testing the Cross Compiler   To test the Cross compiler it is necessary to add the path of the installation to the PATH variable.   $ export PATH=/opt/arm-none-eabi/bin/:$PATH   To check the version of the cross compiler:   $ arm-none-eabi-gcc –version arm-none-eabi-gcc (GCC) 4.5.2 Copyright (C) 2010 Free Software Foundation, Inc. This is free software; see the source for copying conditions.  There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE   Attached you can find a folder that contains a simple KL25 example that can be compiled in the iMX6 and then flash the Freedom KL25 with the OpenSDA. This means that you have to attach the USB OpenSDA to the OTG port of the iMX6 board.   Type the next in the hello folder (/Kinetis  GNU/KL25_TEST/KL25/hello)   $make clean $make   This will generate a main.srec file that can be copied to the USB MSD device featured by the OpenSDA.   $cp main.srec /meida/sda1 $sync   After this, the RGB LED in the Freedom KL25 will toggle. Original Attachment has been moved to: KL25.tar.zip
查看全文
NOTE: Please suggest bitbake commands you find it useful! bitbake command Description bitbake <image> Bake an image (add -k to continue building even errors are found in the tasks execution) bitbake <package> -c <task> Execute a particular package's task. Default Tasks names: fetch, unpack , patch , configure , compile , install , package , package_write , and build. Example: To (force) compiling a kernel and then build, type: $ bitbake  linux-imx -f -c compile $ bitbake linux-imx bitbake <image > -g -u depexp Show the package dependency for image. Example: To show all packages included on fsl-image-gui $ bitbake fsl-image-gui -g -u depexp NOTE: This command will open a UI window, so it must be execute on a console inside the host machine (either virtual or native). bitbake <package> -c  devshell Open a new shell where with neccesary system values already defined for package hob bitbake frontend/GUI. bitbake <package> -c listtasks List all tasks for package bitbake virtual/kernel -c menuconfig Interactive kernel configuration bitbake <image> -c fetchall Fetch sources for a particular image bitbake-layers show-layers Show layers bitbake-layers show-recipes "*-image-*" Show possible images to bake. Without "*-images-*", it shows ALL recipes bitbake -g <image> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq Show image's packages bitbake -g <pkg> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq Show package's dependencies bitbake –v <image> 2>&1 | tee image_build.log Print (on console) and store verbose baking bitbake -s | grep <pkg> Check if certain package is present on current Yocto Setup
查看全文