i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
This article describes how to enable the GPIO support in SPL for i.MX 93 and how to use the associated library. Available GPIO banks Bank Registers' Base Address GPIO1 0x47400000 GPIO2 0x43810000 GPIO3 0x43820000 GPIO4 0x43830000   Software Tests performed using the LF6.12.20-2.0.0 BSP, but should work similarly in other versions.   Enable the GPIO support in SPL Enable the CONFIG_SPL_GPIO through menuconfig. Configure the GPIO pin Make sure the chosen GPIO pin is not used by any other peripheral, by checking U-Boot's device tree (example: imx93-11x11-evk.dts and its included files). If used, disable the conflicting peripheral in the device tree. To identify the exact macro associated to the GPIO functionality, please check the arch/arm/dts/imx93-pinfunc.h file.  Example 1: Use an available GPIO pin (e.g. GPIO2_IO05) This pin is not used by other peripheral, so there is nothing to disable.  To use the pin with the GPIO functionality, the following pin muxing must be added in the iomux node of the imx93-11x11-evk.dts file (located in dts/upstream/src/arm64/freescale/😞 😞 pinctrl_hog: hoggrp { fsl,pins = < MX93_PAD_GPIO_IO05__GPIO2_IO05 0x51e >; }; Note: 0x51e represents the value you want in the PAD register (SW_PAD_CTL_PAD_GPIO_IO05). You may configure it as you want.  Example 2: Use the XSPI1_TXC pin as GPIO (GPIO1_IO12) In our BSP, by default, this pin is used by the SAI1 peripheral. To use this pin as GPIO, SAI1 must be disabled in device tree. &sai1 { status = "disabled"; }; To use the XSPI1_TXC pin with the GPIO functionality, the following pin muxing must be added in the iomux node of the imx93-11x11-evk.dts file (located in dts/upstream/src/arm64/freescale/😞😞 pinctrl_hog: hoggrp { fsl,pins = < MX93_PAD_SAI1_TXC__GPIO1_IO12 0x51e >; }; Include the correct header files In the file you want to use the GPIO, include the following headers: #include <asm/arch-mx7ulp/gpio.h> #include <asm-generic/gpio.h> Define the GPIO To define the GPIO's handle, use the IMX_GPIO_NR(bank, index) macro. index = The pin number within the bank. bank = The GPIO bank number, mapped as follows (due to the way they are placed in memory): GPIO Bank bank value for IMX_GPIO_NR GPIO1 4 GPIO2 1 GPIO3 2 GPIO4 3 Example 1: Compute the handle for GPIO2_IO05 #define TIMED_GPIO IMX_GPIO_NR(1, 5) Example 2: Compute the handle for XSPI1_TXC (GPIO1_IO12) #define TIMED_GPIO IMX_GPIO_NR(4, 12)   Read the GPIO pin gpio_request(TIMED_GPIO, "timed_gpio"); gpio_direction_input(TIMED_GPIO); int val = gpio_get_value(TIMED_GPIO); printf("GPIO value is %d\n", val);   Write the GPIO pin gpio_request(TIMED_GPIO, "timed_gpio"); // set the pin as output and make it high gpio_direction_output(TIMED_GPIO, 1);   The driver used is drivers/gpio/gpio-uclass.c.
記事全体を表示
Background : Some customer wants to know the DRAM's MR register value. But, For now, we do not have any documentation or binary to complete this. So, this article aim to show how to read this register.   Hardware environment : i.MX8ULP EVK board Software environment : uboot-imx : lf_v2024.04   1. The related registers information are as following:   DENALI CTL 165 [READ MODEREG[24:8]] Read the specified memory mode register from specified chip when start bit set. Bits (7:0) define the memory mode register and bits (15:8) define the chip select. Set bit (16) to 1 to trigger.   DENALI CTL 166 [PERIPHERAL MRR - DATA[31:0]] Data and chip returned from memory mode register read requested by the READ MODEREG parameter. Bits (7:0) indicate the read data and bits (15:8) indicate the chip. READ-ONLY   2. Test result :         Type the below command: mrr <chip_select MR_register>  Like the below picture, when type the mrr 0 c, it means the chip select is 1 and the MR register is MR12, then the value of MR12 register can be output , is 0x1c.   pengyong_zhang_1-1761115918403.png   Note : When read the MR register, must make sure the register has read right. Because most of MR register only have write right. you can check about it on JDEC spec document.   If you want to get the test binary file, please contact to me, i will send it to you.
記事全体を表示
i.MX8MP and i.MX95 both support USB3.0. In EVK board, USB download pin is USB3.0 with Type-C.  While in other boards, they may delete CC logic design PTN5110, or use USB2.0 signals instead. This document describes how to modify U-Boot to support a design without PTN5110 when using the uuu tool to download.
記事全体を表示
This document explains how to enable and test Bluetooth 6LoWPAN (IPv6 over Low-power Wireless Personal Area Networks) in the i.MX Linux BSP.   Environment   i.MX Linux BSP 6.6.52-2.2.0 (based on Yocto scrathgap) i.MX 93 EVK (2 units) An Embedded Artists 2EL M.2 module with the Murata LBES5PL2EL module (containing NXP IW612) is inserted into the i.MX 93 EVK's M.2 slot and connected to the onboard Wi-Fi/BT antenna. One i.MX 93 EVK will serve as the Peripheral device, while the other will act as the Central device. It should also work with i.MX 8 and 9 series evaluation kit equipped with Bluetooth LE modules.   Configurations   Although the Linux kernel includes a Bluetooth 6LoWPAN driver, it is disabled in the i.MX Linux BSP. Therefore, we will modify the kernel configuration to enable it. Add 2 settings below in kernel configuration file (imx_v8_defconfig) to build the required drivers as modules: CONFIG_6LOWPAN=m CONFIG_BT_6LOWPAN=m These settings can be found in the following section of the Linux kernel menuconfig. CONFIG_6LOWPAN: Depends on: NET [=y] && IPV6 [=y] Location: -> Networking support (NET [=y]) -> Networking options -> 6LoWPAN Support (6LOWPAN [=m]) CONFIG_6LOWPAN  CONFIG_BT_6LOWPAN: Depends on: NET [=y] && BT_LE [=y] && 6LOWPAN [=y] Location: -> Networking support (NET [=y]) -> Bluetooth subsystem support (BT [=y]) -> Bluetooth Low Energy (LE) features (BT_LE [=y]) -> Bluetooth 6LoWPAN support (BT_6LOWPAN [=m]) config-bt-6lowpan.png Rebuild the image containing the Linux kernel and make sure that the required drivers are present in the following paths. /lib/modules/6.6.52-ge0f9e2afd4cf-dirty/kernel/net/6lowpan/6lowpan.ko /lib/modules/6.6.52-ge0f9e2afd4cf-dirty/kernel/net/bluetooth/bluetooth_6lowpan.ko   Operations for Peripheral device   Boot the Peripheral device EVK and log in as the root user. NXP i.MX Release Distro 6.6-scarthgap imx93-11x11-lpddr4x-evk ttyLP0 imx93-11x11-lpddr4x-evk login: root Load the NXP Bluetooth UART driver to enable Bluetooth. # modprobe btnxpuart Start the Bluetooth hci0 interface with the hciconfig command. # hciconfig hci0 up Type hciconfig command to check the BD Address of the Bluetooth hci0 interface and confirm that its status is "UP RUNNING". # hciconfig -a hci0: Type: Primary Bus: UART BD Address: D0:17:69:12:34:56 ACL MTU: 1021:7 SCO MTU: 120:6 UP RUNNING RX bytes:862 acl:0 sco:0 events:59 errors:0 TX bytes:1085 acl:0 sco:0 commands:58 errors:0 Features: 0xbf 0xfe 0x8f 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: PERIPHERAL ACCEPT Name: 'imx93-11x11-lpddr4x-evk' Class: 0x200000 Service Classes: Audio Device Class: Miscellaneous, HCI Version: 5.4 (0xd) Revision: 0x8300 LMP Version: 5.4 (0xd) Subversion: 0x1015 Manufacturer: NXP Semiconductors (formerly Philips Semiconductors) (37) Load the Bluetooth 6LoWPAN driver. # modprobe bluetooth_6lowpan Enable Bluetooth 6LoWPAN. # echo 1 > /sys/kernel/debug/bluetooth/6lowpan_enable Start Bluetooth advertising and waits for a connection request from the Central device. # bluetoothctl advertise on   Operations for Central device   Boot the Central device EVK and log in as the root user. NXP i.MX Release Distro 6.6-scarthgap imx93-11x11-lpddr4x-evk ttyLP0 imx93-11x11-lpddr4x-evk login: root Load the NXP Bluetooth UART driver to enable Bluetooth. # modprobe btnxpuart Start the Bluetooth hci0 interface with the hciconfig command. # hciconfig hci0 up Type hciconfig command to check the BD Address of the Bluetooth hci0 interface and confirm that its status is "UP RUNNING". # hciconfig -a hci0: Type: Primary Bus: UART BD Address: D0:17:69:AB:CD:EF ACL MTU: 1021:7 SCO MTU: 120:6 UP RUNNING RX bytes:862 acl:0 sco:0 events:59 errors:0 TX bytes:1085 acl:0 sco:0 commands:58 errors:0 Features: 0xbf 0xfe 0x8f 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: PERIPHERAL ACCEPT Name: 'imx93-11x11-lpddr4x-evk' Class: 0x200000 Service Classes: Audio Device Class: Miscellaneous, HCI Version: 5.4 (0xd) Revision: 0x8300 LMP Version: 5.4 (0xd) Subversion: 0x1015 Manufacturer: NXP Semiconductors (formerly Philips Semiconductors) (37) Load the Bluetooth 6LoWPAN driver. # modprobe bluetooth_6lowpan Enable Bluetooth 6LoWPAN. # echo 1 > /sys/kernel/debug/bluetooth/6lowpan_enable Send a connection request to the Peripheral device. (In this example, the BD address of the Peripheral device is D0:17:69:12:34:56.) # echo "connect D0:17:69:12:34:56 1" > /sys/kernel/debug/bluetooth/6lowpan_control After waiting for a few tens of seconds, the bt0 network interface will appear. (At the same time, the bt0 network interface will appear on the Peripheral device that accepted the connection.) # ifconfig bt0 bt0: flags=4161<UP,RUNNING,MULTICAST> mtu 1280 inet6 fe80::d017:69ff:feab:cdef prefixlen 64 scopeid 0x20<link> unspec D0-17-69-AB-CD-EF-00-00-00-00-00-00-00-00-00-00 txqueuelen 1000 (UNSPEC) RX packets 9 bytes 884 (884.0 B) RX errors 0 dropped 4 overruns 0 frame 0 TX packets 13 bytes 1069 (1.0 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 The Central device and Peripheral device are now connected via Bluetooth 6LoWPAN.   Testing Send a ping from the Central device to the Peripheral device. (In this example, the IPV6 address of the Peripheral device is fe80::d017:69ff:fe12:3456.) # ping6 fe80::d017:69ff:fe12:3456%bt0 PING fe80::d017:69ff:fe12:3456%bt0 (fe80::d017:69ff:fe12:3456%bt0) 56 data bytes 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=1 ttl=64 time=181 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=2 ttl=64 time=125 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=3 ttl=64 time=67.7 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=4 ttl=64 time=56.1 ms ...   Benchmarking   Run the iperf3 server on the Peripheral device. # iperf3 -s Run the iperf3 benchmark on the Central device. For example, check the TCP connections. # iperf3 -V -c fe80::d017:69ff:fe12:3456%bt0 You can also check UDP connections. For example, the following example sends UDP 200Kbps bandwidth. # iperf3 -V -c fe80::d017:69ff:fe12:3456%bt0 -u -b 200K   Disclaimer   This document is provided as a reference for utilizing NXP products. Please refer to the official product manuals and application notes for formal specifications. Due to differences in software versions and other conditions, actual behavior may differ from the descriptions provided. This document does not verify all functions, so please be sure to conduct appropriate validation and testing to ensure suitability for your intended use.  
記事全体を表示
Streaming different use case pipelines between i.MX 95 and i.MX 8M Plus LF-6.12.20
記事全体を表示
We are pleased to announce that Config Tools for i.MX v25.09 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) • The Release Notes format is updated from plain text to markdown. • The newly generated configuration includes the default NXP copyright notice and is licensed under the BSD-3-Clause license. • DDR tool – ODT and Driver Strength Updates for LP4/LP5 on i.MX 943 and i.MX 95 – Improved DRAM Configuration for i. MX 9x devices – Multicore support is enabled for DDR tests on i.MX 943 and i.MX 95 – Linux support for the DDR tool – Vref DQ Setting now available in the GUI – Board-agnostic SM Support for i.MX 943 and i.MX 95 – DDR part number entry is supported in the GUI – Enhanced logging from the target application – Stress test repetition option is enabled – Updated ODT shmoo scenario values on i.MX 943 and i.MX 95 – Support for SNPS FW and PHY Init 2024.09 SP2 on i.MX 943 and i.MX 95 – AHAB image update to align with BSP for CES parts on i.MX 943 and i.MX 95 – New configuration support for 15x15 on i.MX 943 – Improved bus configuration for single-channel setups – LP4/LP5 CS signal configuration now exposed in the GUI for i.MX 943 and i.MX 95 • Clocks – Supported input frequency setting • System Manager – Initial version of the tool
記事全体を表示
This article describe some bring up tips during i.MX95 board debug, including HW and SW aspects.  
記事全体を表示
based on customer's issue when use PTF pins of imx8ulp as GPIO or gpio hog
記事全体を表示
  This document shows how to use the open source gstreamer1.0-rtsp-server package on i.MX6QDS and i.MX8x to stream video files and camera using RTP protocol.  The i.MX 6ULL and i.MX 7 doesn't have Video Processing Unit (VPU). Real time protocol (RTP) is a very common network protocol for delivering media over IP networks. On the board, you will need a GStreamer pipeline that encodes the raw video, adds the RTP payload, and sends over a network sink. A generic pipeline would look as follows: video source ! video encoder ! RTP payload ! network sink Video source: often it is a camera, but it can be a video from a file or a test pattern, for example. Video encoder: a video encoder as H.264, H.265, VP8, JPEG and others. RTP payload: an RTP payload that matches the video encoder. Network sink: a video sync that streams over the network, often via UDP. Pre-Requisites: MX6x o MX8x board with the L6.6.52 BSP installed. A host PC with either Gstreamer or VLC player installed.   Receiving h264 / h.265 Encoded RTP Video Stream on a Host Using GStreamer: GStreamer is a low-latency method for receiving RTP video. On your host machine, install Gstreamer and send the following command: $ gst-launch-1.0 -v udpsrc port=5000 caps = "application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" ! rtph264depay ! decodebin ! videoconvert ! autovideosink sync=false   Using HOST PC: VLC Player Optionally, you can use VLC player to receive RTP video on a PC. First, in your PC, create a sdp file with the following content:  stream.sdpv=0m=video 5000 RTP/AVP 96c=IN IP4 127.0.0.1a=rtpmap:96 H264/90000 After this, with the GStreamer pipepline on the device running, open this .sdp file with VLC Player on the host PC.   Sending h.264 and h.265 Encoded RTP video stream GStreamer provides an h.264 encoding element by software named x264enc. Use this plugin if your board does not support h.264 encoding by hardware or if you want to use the same pipeline on different modules. Note that the video performance will be lower compared with the plugins with encoding accelerated by hardware. # gst-launch-1.0 videotestsrc ! videoconvert ! x264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Note: Replace <host-machine-ip> by the IP of the host machine. In all examples you can replace videotestsrc by v4l2src element to collect a stream from a camera   i.MX8X # gst-launch-1.0 videotestsrc ! videoconvert ! v4l2h264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000   i.MX8M Mini Quad / 8M Plus # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 i.MX6X The i.MX6QDS does not support h.265 so the h.264 can work: # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Using other video Encoders While examples of streaming video with other encoders are not provided, you may try it yourself. Use the gst-inspect tool to find available encoders and RTP payloaders on the board: # gst-inspect-1.0 | grep -e "encoder"# gst-inspect-1.0 | grep -e "rtp" -e " payloader" Then browse the results and replace the elements in the original pipelines. On the receiving end, you will have to use a corresponding payload. Inspect the payloader element to find the corresponding values. For example: # gst-inspect-1.0 rtph264pay   Install rtp in your yocto different form L6.6.52 BSP, to install gstreamer1.0-rtsp-server in any Yocto Project image, please follow the steps below: Enable meta-multimedia layer: Add the following on your build/conf/bblayers.conf: BBLAYERS += "$"${BSPDIR}/sources/meta-openembedded/meta-multimedia" Include gstreamer1.0-rtsp-server into the image: Add the following on your build/conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server" Run bitbake and mount your sdcard. Copy the binaries: Access the gstreamer1.0-rtsp-server examples folder: $ cd /build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0-rtsp-server/$version/build/examples/.libs Copy the test-uri and test-launch to the rootfs /usr/bin folder. $ sudo cp test-uri test-launch /media/USER/ROOTFS_PATH/usr/bin Be sure that the IPs are correctly set: SERVER: => ifconfig eth0 $SERVERIP CLIENT: => ifconfig eth0 $CLIENTIP Video file example SERVER: => test-uri file:///home/root/video_file.mp4 CLIENT: => gst-launch-1.0 playbin uri=rtsp://$SERVERIP:8554/test You can try to improve the framerate performance using manual pipelines in the CLIENT with the rtspsrc plugin instead of playbin. Follow an example: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test caps = 'application/x-rtp'  ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! queue max-size-buffers=0 ! imxv4l2sink sync=false   Camera example SERVER: => test-launch "( imxv4l2src device=/dev/video0 ! capsfilter caps='video/x-raw, width=1280, height=720, framerate=30/1, mapping=/test' ! vpuenc_h264 ! rtph264pay name=pay0 pt=96 )" CLIENT: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test ! decodebin ! autovideosink sync=false The rtspsrc has two properties very useful for RTSP streaming: Latency: Useful for low-latency RTSP stream playback (default 200 ms); Buffer-mode: Used to control buffer mode. The slave mode is recommended for low-latency communications. Using these properties, the example below gets 29 FPS without a sync=false property in the sink plugin. The key achievement here is the fact that there is no dropped frame: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test latency=100 buffer-mode=slave ! queue max-size-buffers=0 ! rtph264depay ! vpudec ! imxv4l2sink    
記事全体を表示
  This article shows how to use the i.MX6DL/Q to transcode and stream videos on 1080i/p @ 24fps and 720p @ 30fps. For this test, we used one i.MX6DL as server and an i.MX6DL and i.MX6Q as clients. The video is streamed by the server, playing the sound at the same time, while the clients show the video in the HDMI output, as the image below:   Bio_TICFSL_0-1756400346080.jpeg   This test depends on some GStreamer plugins. To check that the right GStreamer plugins are installed type the following commands: $ gst-inspect-1.0 | grep h264 To return all the H.264 related plugins, or: $ gst-inspect-1.0 decodebin To check directly the command. To connect more than one board to the minicom, open it with the command: $ sudo minicom –s This way, you open the configuration menu. Enter in the “Serial port setup” option and press “A” to set or change the PORTNUMBER, in “ttyUSB$PORTNUMBER”. To set the HDMI output, run the commands below from the U-Boot prompt: => setenv mmcargs 'setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 consoleblank=0' => saveenv Be sure that the IPs are correctly setted: SERVER: => ifconfig eth0 $SERVERIP CLIENTS: => ifconfig eth0 $CLIENTSIP Streaming transcoded video only SERVER: => gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 CLIENTS: => gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, payload=(int)96' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false Streaming transcoded video + audio SERVER: => gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin name=demux demux. ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 demux. ! alsasink CLIENTS: => gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, encoding-name=(string)H264' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false   You can check the results with the 1080p@24fps.
記事全体を表示
Overview The purpose of this document is to provide guidance for FlexIO 8080 display capability. Generally, the 8080 bus interface consists of one chip-select line (CS), one writing-latch line (WR), one reading-latch line (RD), one data/command-select line (RS, also called D/C), and 8 or 16 bidirectional data lines (Data Bus). Since The FlexIO instance of i.MX 943 support only 16 pins, the demo can only support 8 bit 8080 mode(two pin should be used as WR and RD signal. winteri_wang_0-1756800337092.png   Below are pins used in the 8 bit 8080 display. winteri_wang_1-1756282634017.png Panel Setup The panel in the example is X-LCD-PAR-S035. To use 8 bit 8080 mode, need ser IM[2:0] to be 011. Connection and Software i.MX 943 Need pull down SPI8_SEL1 and SPI8_SEL3 of PCA6416 in SW to select Arduino for 8080 pins D[7:4]. imx943_flexio_8080_connection.png Here is the patch for system manager. For quick verification, use flash_m70 when building bootloader. diff --git a/configs/mx94evk.cfg b/configs/mx94evk.cfg index 9d46976..90bf089 100755 --- a/configs/mx94evk.cfg +++ b/configs/mx94evk.cfg @@ -499,6 +499,9 @@ ENC_PLL OWNER ENDAT2_1 OWNER ENDAT2_2 OWNER ENDAT3_1 OWNER +GPIO2 OWNER +GPIO3 OWNER +FLEXIO1 OWNER FLEXIO3 OWNER FLEXIO4 OWNER FLEXPWM1 OWNER @@ -515,6 +518,7 @@ HIPERFACE_SAFE1_2 OWNER HIPERFACE_SAFE2_1 OWNER HIPERFACE_SAFE2_2 OWNER IRQSTEER_M7_0 OWNER +LPI2C6 OWNER LPIT1 OWNER LPTMR1 OWNER LPTMR2 OWNER @@ -557,6 +561,25 @@ XBAR_DSC3 OWNER PIN_GPIO_IO24 OWNER PIN_GPIO_IO25 OWNER +# 8080 +PIN_GPIO_IO00 OWNER +PIN_GPIO_IO01 OWNER +PIN_GPIO_IO02 OWNER +PIN_GPIO_IO03 OWNER +PIN_GPIO_IO08 OWNER +PIN_GPIO_IO09 OWNER +PIN_GPIO_IO10 OWNER +PIN_GPIO_IO11 OWNER +PIN_GPIO_IO12 OWNER +PIN_GPIO_IO13 OWNER +PIN_GPIO_IO14 OWNER +PIN_GPIO_IO15 OWNER +PIN_GPIO_IO38 OWNER + +# I2C6 +PIN_GPIO_IO28 OWNER   Attached imx943_flexio_8080_8bit.zip is patch for m70 demo based on SDK_25_06_00_MCIMX943-EVK.   i.MX 93 Need pull up EXP_SEL(pin4 R4) of ADP5585 in SW to route some pins. imx93_flexio_8080_connection.png Attached imx93_flexio_8080_8bit.zip is patch for m33 demo based on SDK_25_06_00_MCIMX93-EVK. The running status is similar as i.MX943.
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX8MP-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX8MP-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX8MP-EVK SDK Chavira_0-1756151575498.png   Import "hello world" example Chavira_1-1756151657646.png Ensure that we are compiling a debug binary Chavira_0-1755709033328.png Build Project Chavira_2-1756151706391.png Flash the Binary using UUU Tool Connect the IMX8MP-EVK Board to your Host PC via USB   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write hello_world.bin mmc X:1 hello_world_debug.bin Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card Chavira_5-1755701729711.png   Connect MCU-LINK Pro to the Target Chavira_0-1756153231712.jpeg   IMX8MP-EVK Debug connection: Chavira_1-1756153245680.jpeg     Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 0x48000000 hello_world_debug.bin; cp.b 0x48000000 0x7e0000 0x20000; => bootaux 0x7e0000 Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card Chavira_3-1755701674202.png   Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso: Chavira_1-1756153109266.png     Chavira_0-1756153065481.png      With the MCU-LINK Pro configured, the IMX8MP-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX8MP based projects.   References: AN14120.pdf 
記事全体を表示
The documentation is to provide steps for single secure boot for BSP Android 14.0.0_2.0.0. More details related to secure boot for Android BSP can be found from IMX ANDROID SECURE BOOT. However, the steps in this document facilitate some helps signing an Android boot image in the aspects of - First, the Android build process for signing the image, and second, the FDT signing process must be performed after the SPL/FIT of the signing process. The second one of which is crucial.   Best regards Harvey
記事全体を表示
This slides firstly introduce the xSPI NOR devices related industry standards:JESD251 and JESD216, and i.MX95 FlexSPI controller. Based on these background knowledge, how to configure the FlexSPI Configuration Block(FCB) for FlexSPI boot in i.MX95 is introduced as well. Finally, some examples in Uboot to deal with the FCB are list.
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX8MN-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX8MN-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX8MN-EVK SDK Chavira_0-1755698330924.png   Import "hello world" example Chavira_1-1755698515769.png Ensure that we are compiling a debug binary Chavira_0-1755709033328.png Build Project Chavira_0-1755708251783.png   Flash the Binary using UUU Tool Connect the IMX8MN-EVK Board to your Host PC via USB   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write hello_world.bin mmc X:1 hello_world_debug.bin Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card Chavira_5-1755701729711.png   Connect MCU-LINK Pro to the Target Chavira_0-1755708638687.jpeg   IMX8MN-EVK Debug connection: Chavira_1-1755708652859.jpeg   Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 0x48000000 hello_world_debug.bin; cp.b 0x48000000 0x7e0000 0x20000; => bootaux 0x7e0000 Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card Chavira_3-1755701674202.png   Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso: Chavira_0-1755708802524.png   Chavira_1-1755702026549.png    With the MCU-LINK Pro configured, the IMX8MN-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX8MN based projects.   References: AN14120.pdf 
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX8MM-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX8MM-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX8MM-EVK SDK Chavira_0-1755698330924.png   Import "hello world" example Chavira_1-1755698515769.png Ensure that we are compiling a debug binary Chavira_0-1755709077404.png Build Project Chavira_2-1755698624814.png   Flash the Binary using UUU Tool Connect the IMX8MM-EVK Board to your Host PC via USB Chavira_0-1755701104573.jpeg   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write hello_world.bin mmc X:1 hello_world_debug.bin Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card Chavira_5-1755701729711.png Connect MCU-LINK Pro to the Target Chavira_1-1755701131673.jpeg     IMX8MM-EVK Debug connection: Chavira_2-1755701139996.jpeg   Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 0x48000000 hello_world_debug.bin; cp.b 0x48000000 0x7e0000 0x20000; => bootaux 0x7e0000 Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card Chavira_3-1755701674202.png     Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso: Chavira_0-1755701976656.png   Chavira_1-1755702026549.png    With the MCU-LINK Pro configured, the IMX8MM-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX8MM based projects.   References: AN14120.pdf 
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX93-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX93-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX93-EVK SDK Chavira_0-1755621430498.jpeg     Import "hello world" example Chavira_1-1755621430541.jpeg   Ensure that we are compiling a debug binary Chavira_2-1755621430505.jpeg Build Project Chavira_3-1755621430500.jpeg   Flash the Binary using UUU Tool Connect the IMX93-EVK Board to your Host PC via USB Chavira_2-1755697061118.jpeg       Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write sdk20-app.bin mmc X:1 hello_world.bin Note: replace the X with 0 if you are booting from eMMC or 1 if you are booting from SD Card Chavira_4-1755621484546.png     Connect MCU-LINK Pro to the Target   Chavira_8-1755621967816.jpeg   IMX93-EVK Debug connection:   Chavira_1-1755697045386.jpeg     Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 80000000 hello_world.bin; cp.b 0x80000000 0x201e0000 0x10000; => bootaux 0x1ffe0000 0 Note: replace the X with 0 if you are booting from eMMC or 1 if you are booting from SD Card Chavira_5-1755621576326.png     Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso: Chavira_6-1755621576151.png     Chavira_7-1755621576273.png    With the MCU-LINK Pro configured, the IMX93-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX93-based projects.   References: AN14120.pdf 
記事全体を表示
Running Zephyr on i.MX9 A55 core brings a high performance, real-time (short interrupt, scheduler latency, etc.) OS experiences as well as the fast boot, small memory footprint features. This article provide all the information on how to run the Zephyr v4.1 on Cortex-A55 cores to support below features: Supported Features FRDM-IMX93 FRDM-IMX91 Description Zephyr RTOS code base     Based on Zephyr v4.1 FRDM-IMX93 board configure Yes   Board configuration, build, device tree files FRDM-IMX91 board configure   Yes Board configuration, build, device tree files Hello world Yes Yes   Dual Ethernet Yes   TY8521 Ethernet PHY support Display Yes   LCDIF, MIPI DSI, Waveshare 1024x600 7inch DSI LCD(C) Camera Yes   MIPI-CSI, ISI, AP1302 sensor Audio Yes   I2S with eDMA (Driver only) uSDHC Yes   SD card only USB Yes   USB CDC device class   The code has been release on github: Zephyr samples/drivers: https://github.com/nxp-zephyr/zephyr Zephyr HAL: https://github.com/nxp-zephyr/hal_nxp Tag: FRDM-IMX93-v4.1 How to doc is attached.  
記事全体を表示
Hello! In this post, we’ll cross-compile a kernel module for Linux 6.12.    This can be done either using a standalone kernel or a Yocto-built kernel.    Requirements:  A compiled Linux kernel 6.12.  A board running the same kernel version (Linux 6.12 in this case).  A cross-compiler toolchain.    This process applies to any i.MX processor, including i.MX8, i.MX8M, i.MX8MM, i.MX8MN, i.MX8MP, i.MX93, i.MX91, i.MX95, as well as the i.MX6 and i.MX7 families.    Step 1: Compile the Linux Kernel and get the Toolchain    First, you need to compile the Linux kernel (6.12 in this case).    You can do this in a standalone environment or using Yocto.     If you are using a Standalone environment, please refer to the Chapter 4.5.12 How to build U-Boot and Kernel in standalone environment of i.MX Linux User's Guide.  Also, in that document section, you will see how to obtain the cross-compiler toolchain.    NOTE: To get the toolchain you need use Yocto at least once (for more information please refer to i.MX Yocto Project User's Guide😞  $ DISTRO=fsl-imx-xwayland MACHINE=Target-Machine bitbake core-image-minimal -c populate_sdk   At the end of the building, you can install your toolchain populated under:    yocto-bsp/build/tmp/deploy/sdk     There you will find a file called:    fsl-imx-wayland-glibc-x86_64-imx-image-core-armv8a-your-machine-name-toolchain-6.12-walnascar.sh    Execute with:  $ sudo ./fsl-imx-wayland-glibc-x86_64-imx-image-core-armv8a-your-machine-name-toolchain-6.12-walnascar.sh   If you use the default installation, you will have your toolchain under /opt in your host machine.      (If you will use the compiled kernel from Yocto, you can avoid below step)  Download Standalone Kernel source by cloning with:  $ git clone https://github.com/nxp-imx/linux-imx -b lf-6.12.y $ cd linux-imx   To build the kernel in the standalone environment for i.MX 6 and i.MX 7, execute the following commands:    $ make imx_v7_defconfig $ Make   To build the kernel in the standalone environment for i.MX 8 and i.MX 9, execute the following commands:  $ make imx_v8_defconfig $ make   The full kernel compilation is required to generate headers and symbol files required for external module compilation, even if you don't plan to boot this kernel directly.      Step 2: Write a simple Kernel Module to test    Now that your kernel is compiled, you can write a basic kernel module for testing.    Create a new directory. It will have our hello.c and Makefile.    We will create the file hello.c:  #include <linux/init.h> #include <linux/module.h> #include <linux/kernel.h> MODULE_LICENSE("GPL"); MODULE_AUTHOR("Salas"); MODULE_DESCRIPTION("A simple kernel module example for cross-compilation."); MODULE_VERSION("0.1"); static int __init hello_init(void) { printk(KERN_INFO "Hello from the kernel module!\n"); return 0; } static void __exit hello_exit(void) { printk(KERN_INFO "Goodbye from the kernel module!\n"); } module_init(hello_init); module_exit(hello_exit);   Then, create a basic Makefile to compile the modules:    # Module name obj-m += hello.o # Build flags ldflags-y += --strip-debug # Kernel source directory (provided by Yocto) KERNEL_SRC ?= /path/to/your/compiled/kernel # Build target all: $(MAKE) -C $(KERNEL_SRC) M=$(PWD) modules # Clean target clean: $(MAKE) -C $(KERNEL_SRC) M=$(PWD) clean # Install target modules_install: $(MAKE) -C $(KERNEL_SRC) M=$(PWD) modules_install   KERNEL_SRC should be your compiled kernel from your Yocto build:   yocto-bsp/build/tmp/work/your-machine-poky-linux/linux-imx/6.12.20+git/build   Or the Standalone : path/to/linux-imx/     Step 3: Set the toolchain and compile the kernel module    Finally, we can compile the kernel module.    First, set the toolchain (in my case):  $ source /opt/fsl-imx-wayland/6.12-walnascar/environment-setup-armv8a-poky-linux   Then, compile using the makefile:  $ make   f everything goes well, at final you will have the generated files:    hello.ko hello.mod hello.mod.c hello.mod.o hello.o Makefile modules.order Module.symvers   The one we need is the hello.ko (Kernel Object).    We can check if the file was created correctly using:    $ readelf -h hello.ko ELF Header: Magic: 7f 45 4c 46 02 01 01 00 00 00 00 00 00 00 00 00 Class: ELF64 Data: 2's complement, little endian Version: 1 (current) OS/ABI: UNIX - System V ABI Version: 0 Type: REL (Relocatable file) Machine: AArch64 Version: 0x1 Entry point address: 0x0 Start of program headers: 0 (bytes into file) Start of section headers: 33992 (bytes into file) Flags: 0x0 Size of this header: 64 (bytes) Size of program headers: 0 (bytes) Number of program headers: 0 Size of section headers: 64 (bytes) Number of section headers: 41 Section header string table index: 40   We can see the Machine is AArch64 and the Type is a Relocatable file.      Step 4: Running the Kernel Object/Module in the board    Transfer the generated hello.ko file from your host machine to your board.    Then, In your board you can run with:    root@imx93evk:~# ls hello.ko root@imx93evk:~# insmod hello.ko root@imx93evk:~# dmesg | tail [ 5140.547447] Hello world from kernel! root@imx93evk:~# rmmod hello.ko root@imx93evk:~# dmesg | tail [ 5140.547447] Hello world from kernel! [ 5153.415215] Goodbye world from kernel!   I hope this can helps to you.    Best regards,  Salas. 
記事全体を表示
  Background : Some customer want to test the LPDDR4/X ECC feature based on the i.MX93 chip, But, for now, Our DDR Config Tool do not release this test chosen. And our ECC guide only tell the ECC feature function, does not tell the customer how to test it. So in this article, Will show you more details about ECC feature and how to run the ECC test use uboot command. But I won't put the source code of the test here, You can download the binary run the test on the i.MX93 EVK board.   HW : i.MX93 EVK board with 2GB LPDDR4 SW : 6.1.1-1.0.0   ECC Introduce what is ECC?       ECC is the abbreviation of Error Correction Code. Its function is to automatically detect and repair some minor errors in the memory to prevent data errors. How does ECC work? We can think of it as an "automatic proofreader", and its workflow is roughly as follows:  When writing data: The memory controller generates a "check code" (similar to the fingerprint of the data) for each piece of data. This check code will be stored together with the data. When reading data: The memory controller will recalculate the "fingerprint". Then compare the previously stored check code to see if there is any difference. If a difference is found: If it is just a 1-bit error, ECC can automatically correct it. But, If there are multiple errors, ECC can at least detect them and issue a warning.   ECC test step: 1. Flash the attachment file to the imx93 board. 2. Enter the uboot, run the "ecc --help" command, you will see the below help output message   pengyong_zhang_2-1752117144449.png 3. For example : ecc 0x80000000 0x90000000, it will test the ecc feature with on bit error detect and correct , 2 bits errors detect with 256MB DRM size. pengyong_zhang_3-1752117148095.png   if you need this ECC_ test binary file, please contact me, i will share it to you        
記事全体を表示