i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Wireless HW module on i.MX 6 DQ HDMI dongle board is bcm4330 that is SDIO interface. Modprobe  default configuration will only insmod bcm4330.ko without any kernel module parameter, while bcm4330,ko needs extra firmware binary and nvram configuration file absolute path/filename  as parameter like firmware_path=/lib/firmware/bcm4330/fw_bcm4330.bin nvram_path=/lib/firmware/bcm4330/nvram_bcm4330.txt. To auto insmod bcm4330 kernel module with those parameters by modprobe we need a modprobe configuration file. Now create this file at /etc/modprobe.d/bc4330.conf, it's content as below: #For BCM4330 special install requirement options bcm4330 firmware_path=/lib/firmware/bcm4330/fw_bcm4330.bin nvram_path=/lib/firmware/bcm4330/nvram_bcm4330.txt Of course we need copy correct firmware and nvram configuration file to directory as /etc/modprobe.d/bc4330.conf set.
View full article
The Register Programming Aid (RPA) provides a default DRAM PLL setting (DRAM frequency) based on the default setting supported in u-boot.  It is highly recommended to use the default DRAM frequency settings in the RPA for ease of use and to align with u-boot.  Otherwise, in addition to updating the RPA for the new DRAM frequency, the u-boot SPL code itself will need to be manually updated with the new DRAM PLL setting.   Should the user wish to change the DRAM frequency, the following steps are required:   First, the user needs to update the RPA Register Configuration worksheet tab Device Information table “Clock Cycle Freq (MHz)“ setting to the desired DRAM frequency       2. Next, in the RPA DDR stress test file worksheet tab search for “memory set 0x30360054”.  The address “0x30360054” is for the DRAM PLL register address and its setting needs to be updated to the desired frequency.        Note that there is another place where the DRAM frequency is also updated “freq0 set 0x30360054” but it is automatically updated based on the setting above.    Below is a table of various frequencies to choose from.  For frequencies not listed in the table below, it is up to the user to calculate a new register setting based on the formula:     (24MHz x m)/(p x 2^s)   Where “m” represents the PLL_MAIN_DIV, “p” represents the PLL_PRE_DIV, and “s” represents the PLL_POST_DIV.  NOTE:  The DRAM frequency is double the DRAM PLL frequency DRAM_freq = DRAM_PLL x 2   The DRAM PLL register and bit settings are shown below:          The following table provides examples of the various settings to create the desired frequency:       For example, in the i.MX 8M Mini LPDDR4 RPA where the default DRAM frequency is 1500MHz, let’s assume that the user instead wants 1200MHz.    First, the user changes the RPA Register Configuration worksheet tab Device Information table “Clock Cycle Freq (MHz)“ setting to 1200.   Next, in the RPA DDR stress test file worksheet tab search for “memory set 0x30360054” and replace “0xFA080” (original setting from DRAM frequency 1500MHz) with “0x000C8022” (updated for DRAM frequency 1200MHz).  Note that for a DRAM frequency of 1200MHz, the DRAM PLL is configured for 600MHz, as the DRAM frequency is double the DRAM_PLL.   The steps outlined above are sufficient in order to create a DDR script for use with the DDR stress test tool to run the calibration and execute the DDR stress test.  However, to deploy the generated code in SPL, more steps are needed as the u-boot SPL DDR driver does not automatically change the DRAM PLL according to the generated code. Hence the user will need to manually modify related code in u-boot.  It is highly recommended to work with a software engineer familiar with u-boot when making the following modifications.    3. Modify DRAM PLL configuration in uboot-imx/drivers/ddr/imx8m.c, specifically the code highlighted below (function call dram_pll_init).  Note that the files and file paths in u-boot change frequently, so if this particular file (or file path) does not exist in the current u-boot, simply search for dram_pll_init or ddr_init.   void ddr_init(struct dram_timing_info *dram_timing) { ……    debug("DDRINFO: cfg clk\n");      if (is_imx8mq())           dram_pll_init(DRAM_PLL_OUT_800M);      else          dram_pll_init(DRAM_PLL_OUT_750M); ……  }   In the above code, the user should update the macro “DRAM_PLL_OUT_750M” with the new DRAM PLL value.  Note that the default DRAM_PLL_OUT_750M results in the DRAM frequency of 1500MHz, where the DRAM frequency is double the DRAM PLL (as previously stated above).   For example, if the user desires to run the DRAM at 1200MHz, they would change the above to: dram_pll_init(DRAM_PLL_OUT_600M);   Note that DRAM_PLL_OUT_600M is a supported macro in the dram_pll_init() API.  If the desired DRAM PLL configuration does not exist in dram_pll_init(), you will need to add support in uboot-imx/arch/arm/mach-imx/imx8m.c  (as stated above, if this file path does not exist in the current u-boot simply search for dram_pll_init):   void dram_pll_init(enum dram_pll_out_val pll_val) { …… }   Related Links i.MX8 MSCALE SERIES DDR Tool Release (V3.10) 
View full article
Pre-requisites: An TFTP server U-boot with TFTP capabilities If you need to run a script (for example, running multiple setenv's commands) in U-boot for many boards, you can instead create a U-boot script (called script image), place it into your tftp folder, then ask U-boot to fetch it and run it. For example, you want to run the following setenv instructions setenv loadaddr 0x10800000 setenv bootargs_base 'setenv bootargs console=ttymxc0,115200' setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666' setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev 3;mmc read ${loadaddr} 0x800 0x2000;bootm' run bootcmd_mmc save it into a file, I choose the name 'myscript'; under your <U-boot folder>/tools, execute $ mkimage -T script -C none -n 'My Script' -d myscript myscript.img and copy myscript.img file into your TFTP folder. On the target, set the following two variables (serverip and bootcmd) # Set the Server IP, where the TFTP server is running setenv serverip <the server IP> # In case the server IP is static, you can place this line into the U-boot script setenv scriptaddr 0x10700000 setenv scriptname myscript.img # You can use either TFTP or DHCP setenv tftpcmd tftp # or 'dhcp'  in case you want to use dhcp U-boot command # Not needed for dhcp setenv ipaddr <the target IP> # needed in case the command tftp is used setenv gatewayip <the Gateway IP> # needed in case the command tftp is used setenv bootcmd '${tftpcmd} ${scriptaddr} ${scriptname}; source ${scriptaddr}' saveenv reset That is all you need to do. Enjoy U-booting!
View full article
Introduction There are four boot logos in kk4.4.3_2.0.0-beta  system at first: uboot logo\linux logo\android init logo\android animation. We plan to use uboot logo to cover linux logo and android init logo so that we  can combine first three logoes into one logo.This guide provides a step by step explanation of how to transfer uboot UI to  linux kernel and android init smoothly on board sasbresd_6dq sabresd_6dl. The core ideas of the patch: need to  keep display clock from uboot to kernel. When kernel boot up , we do not break the frambuffer for that it stores uboot logo data. need to disable show android init logo. what do the patch do in uboot 1、 can not shut down video after uboot is over.The patch delete releted code in function  arch_preboot_os() 2、 keep hsp clock (ipu clock) the same with linux 3.10 the below is the setting in sabrasd DQ board: osc(24MHz) -> pll2(528MHz) -> mmdc_ch0(528MHz) -> ipu1_hsp_clk(264MHz) the below is the setting in sabrasd DL board: osc(24MHz) -> pll3(480MHz) -> pll3_pdf1(540MHz) -> ipu1_hsp_clk(270MHz) 3、 keep pixel clock the same with linux 3.10 the below is the setting in sabrasd DQ board: osc(24MHz) -> pll2(528MHz) -> pll2_pfd0(452.57MHz) -> ldb_di1(64.65MHz) -> ipu1_di1(64.65MHz) -> ipu1_pixel(64.65MHz) the below is the setting in sabrasd DL board: osc(24MHz) -> pll2(528MHz) -> pll2_pfd0(452.57MHz) -> ldb_di1(64.65MHz) -> ipu1_di1(64.65MHz) -> ipu1_pixel(64.65MHz) 4、 keep pwm clock In kernel,there is a 100% duty pwm to drive lvds panel.So the patch set the pad SD1_DATA3 to a 100% duty pwm pin. 5、 add fbbase and fbmem to bootargs the fbbase is the uboot logo’s phy addr. So the patch pass the parament to kernel through cmdline.we should allocate address aligned 1M for linux 3.10 reserve address aligned by 1 M. what do the patch do in linux 3.10 1、 reserve the address which come from fbbase 2、 keep  ipu related clock when system init the clock in clk-imx6q.c The patch  enable ldb_di1_clk、ipu1_di1_clk、ipu1_clk、pwm1_clk.  Do not disable pll2 and pll3 related clock for the clock may be the source of  ipu clock. Although we enable ldb_di1_clk、ipu1_di1_clk and so on in register, we need to use the function clk_prepare_enable(). Because  the system may close some clocks for their user count is 0(if we use clk_prepare_enable(),it and it’s parent  user count will add 1 ) 3、 disable cabc which will light the panel according the content. Change cabc_enable in dts file. 4、 Move global alpha and color key setting in probe  after framebuffer is registered. Delay       register IPU interrupts used by framebuffer  until IPU hsp clock is enabled.Because global alpha and color key setting and register IPU interrupts may disable hsp clock. disable show android init logo android init logo is the text"android_". we need disable to show it so that the former three logos looks the same logo.The patch 92-system_core solve this problem. The environment of the patch: Hardware: SABRASD DQ&DL Soft ware: kk4.4.3_2.0.0-beta on linux 3.10 How to use the patch: $ cd my_android/kernel_imx/ $ patch -p1 < ./92-kernel_v2 $ cd my_android/bootable/bootloader/uboot-imx/ $ patch -p1 < ./92-uboot_v2     $ cd my_android/system/core $ patch -p1 < 92-system_core Note:      1、 If you want to have this feature on sabraSD dq&dl board,this patch is OK .After you use this patch, you want to change to  other board such as sx, you may meet this problem that the kernel logo penguin don’t appear. You may change this file: arch/arm/configs/imx_v7_android_defconfig                 CONFIG_LOGO=y                 CONFIG_FRAMEBUFFER_CONSOLE=y                 CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY=y                 #CONFIG_MX6_CLK_FOR_BOOTUI_TRANS=y                 #CONFIG_MX6_CLK_FOR_BOOTUI_TRANS_LVDS_IPU1_DI1=y
View full article
本文档主要包括两个部分: 1:如何将一首超过两声道的多声道音乐放到多个双声道声卡上播放,来模拟原音乐文件的多声道输出。 2:如何将多个双声道音乐文件同时放到一个8声道的声卡的不同channel上播放。 涉及的文件:etc/asound.conf 1:如何将一首超过两声道的多声道音乐放到多个双声道声卡上播放,来模拟原音乐文件的多声道输出。 1):Sabresd板子 按设计来讲,sabresd板子最多只能播双声道的音乐,但是如果一个音乐文件是四声道,该如何用sabresd板子来播放呢? 可以让前两个声道通过WM8962来播放,后两个声道通过HDMI来播放: 33 pcm.multi { 34         type multi 35 36         slaves.a.pcm "hw:0,0" 37         slaves.a.channels 2 38         slaves.b.pcm "hw:1,0" 39         slaves.b.channels 2 40 41         bindings.0.slave a 42         bindings.0.channel 0 43         bindings.1.slave a 44         bindings.1.channel 1 45         bindings.2.slave b 46         bindings.2.channel 0 47         bindings.3.slave b 48         bindings.3.channel 1 49 } 273 pcm.asymed{ 274 type asym 275 playback.pcm "multi" 276 capture.pcm "dsnoop_44100" 277 } 278 279 ctl.multi{ 280         type hw; 281         card 0; 282 } 289 pcm.!default{ 290 type plug 291 route_policy "average" 292 slave.pcm "asymed" 293 } 可以通过以下命令来测试: speaker-test -c 4 -t sine speaker-test -c 4 -t sine -D multi 2):ARD板子 ARD板子,6声道的audio文件,用ESAI来播放前四个channel,后两个channel用HDMI来播放: 33 pcm.multi { 34         type multi 35 36         slaves.a.pcm "hw:0,0" 37         slaves.a.channels 4 38         slaves.b.pcm "hw:2,0" 39         slaves.b.channels 2 40 41         bindings.0.slave a 42         bindings.0.channel 0 43         bindings.1.slave a 44         bindings.1.channel 1 45         bindings.2.slave a 46         bindings.2.channel 2 47         bindings.3.slave a 48         bindings.3.channel 3 49         bindings.4.slave b 50         bindings.4.channel 0 51         bindings.5.slave b 52         bindings.5.channel 1 53 } 273 pcm.asymed{ 274 type asym 275 playback.pcm "multi" 276 capture.pcm "dsnoop_44100" 277 } 278 279 ctl.multi{ 280         type hw; 281         card 0; 282 } 289 pcm.!default{ 290 type plug 291 route_policy "average" 292 slave.pcm "asymed" 293 } 可以用下面命令来测试: 播源文件是6声道的音乐: aplay 48kHz16bit-six-channel.wav aplay -D multi 48kHz16bit-six-channel.wav speaker-test -c 6 -t sine speaker-test -c 6 -t sine -D multi 播源文件是双声道的音乐,ESAI的四个channel和HDMI的两个声道都是该音乐: aplay heart.wav 2:如何将多个双声道音乐文件同时放到一个8声道的声卡的不同channel上播放。 我们ARD的板子,ESAI是8声道的,大部分音乐都是双声道的,ESAI的6个channel会被浪费掉。如何将其余的6个声道也应用起来? alsa lib有dshare这个plugin,可以将4个双声道的音乐文件当成一个8声道的音乐来处理。 28  pcm_slave.nforce { 29        pcm "hw:0,0” 30        channels 8 31        rate 48000        # fixed, because all dshare devices must use the same samplerate. 32        buffer_size 4096  # make these sizes smaller for lower latency 33        period_size 1024 34        periods 4 35        period_time 0 36    } 37 39  pcm.ch12 { 40        type dshare 41        ipc_key 47110815 42        slave nforce 43        bindings.0 0 44        bindings.1 1 45    } 46 47  pcm.ch34 { 48        type dshare 49        ipc_key 47110815 50        slave nforce 51        bindings.0 2 52        bindings.1 3 53    } 54 55   pcm.ch56 { 56        type dshare 57        ipc_key 47110815 58        slave nforce 59        bindings.0 4 60        bindings.1 5 61    } 62 63   pcm.ch78 { 64        type dshare 65        ipc_key 47110815 66        slave nforce 67        bindings.0 6 68        bindings.1 7 69    } 可以通过下面的命令来测试: (aplay -Dplug:ch12 XX.wav &) (aplay -Dplug:ch34 XXX.wav &) (aplay -Dplug:ch56 XXXX.wav &) (aplay -Dplug:ch78 XXXXX.wav &) 四首音乐会分配到ESAI的8个channel上。
View full article
Quaestion: What does exactly the RNG_TRIM after burning the SRK hash table? There is no such thing on the former i.MX HAB procedure. What would a random generator stuff bring here? Additionnally, there is the possibility to lock the SRK shadow register via an OTP bit. Is it recommeneded to lock it? if not, is it really possible to change the SRK hash value by modofying the shadow register value before performing the SRK hash key check in a HAB boot process? One last question: the PKI requires the user to enter a certificate lifetime. Does that really mean that openssl will refuse generating new signatures once the certificates lifetime is expired? Answer: 1. The intent of the of the RNG_TRIM fuses is for Freescale to essentially extendthe amount of time the RNG4 in CAAM has to generate entropy.  The longer this period the more likely it is that RNG4 will generate entropy that will pass its internal statistical tests.  The reason for the fuses is HAB (in the Closed configuration only) instantiates the RNG by default and needs some external indication on how to progran the RNG4 in CAAM to ensure the internal HW statistical tests will pass.  This was to allow the RNG to be useable by application code after execution has left the ROM.  However this requires that the RNG_TRIM fuse value be fully characterized across numerous conditions temperature, voltage etc.  This effort is still on going.  For customers performing secure boot (in Closed configuration) we recommend they follow Section 6.3 of http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf.  In this case the RNG4 can be instantiated by CAAM driver code which can be easily changed if required. 2. Yes, once the SRK hash is provisioned to the SRK_HASH field it is recommended to blow the corresponding SRK_LOCK fuse.  If the SRK_LOCK fuse is not blown then additional fuses in the SRK_HASH field can be blown.  This will cause devices in the closed configuration to fail to boot.  i.e. "bricking" the device. 3. Please see https://community.freescale.com/message/334186#334186 for the answer to your question on the certificate validity period.
View full article
http://freescale.eefocus.com/bbs/article_175_179914.html Freescale i.mx53 i.mx6x series solution to speed up the progress of your product 深圳市优创科技有限公司 Josephwang 王伟 深圳市南山区高新技术产业园南区创维大厦C15 Tel:0755-26017990  13128865181        Mail:[email protected]        QQ:[email protected]
View full article
i.MX6 4.0.0 BSP release doesn't support ASRC_P2P function. This patch provides the reference codes to enable ASRC_P2P function for SSI. It can convert input sample rate to 44.1K_16bit/44.1K_24bit and 48K_16bit/48K_24bit. You can modify the configurations in the Board file. By the way, the SSI controler works at slave mode. Known limitations for the patch: -- The SDMA doesn't support SSI Dual FIFO when using ASRC_P2P function. -- From the waveform, the converted 24bit data have some abnormal data(values between 0 and 1) , but can't hear any abnormal sound from headphone. One suggestion is given under https://community.freescale.com/docs/DOC-95340
View full article
Wayland:   Wayland is a display SERVER and COMPOSITION protocol. It is relatively new, as its first release was in 2012. The protocol enables applications to allocate their own off-screen buffers and render their window contents directly, using hardware accelerated libraries like OpenGL ES, or high quality software implementations like Cairo. Wayland is ONLY a display server protocol, not a display server itself. Weston is the reference Wayland protocol implementation.   YOCTO Setup . $ mkdir ~/bin $ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo $ export PATH=~/bin:$PATH $ git config --global user.name "Your Name" $ git config --global user.email "Your Email" $ git config –list $ mkdir fsl-release-bsp $ cd fsl-release-bsp $ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga $ repo sync     you will be able to build Yocto and also have all the recipes to do so, we need to add WAYLAND, then execute the following steps: $ DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-wayland $ bitbake fsl-image-gui After these steps, you will have a wayland based i.MX6Q image where you will be able to play with all the knowledge we provided here.   Once your image has been properly generated, you will find the Weston source codes in: <YOUR YOCTODIR>/build-wayland/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/weston/1.9.0-r0/weston-1.9.0     Wayland application for extended desktop: This functionality is only supported using the GAL2D blitter, in order to enable a multiple desktop approach, you need to pass the following parameters to your weston command: /etc/init.d/weston stop echo 0 > /sys/class/graphics/fb4/blank weston --tty=1 --use-gal2d=1 --use-gl=0 --device=/dev/fb0,/dev/fb4 &     Xwayland: Wayland is a complete window system in itself, but even so, if we're migrating away from X, it makes sense to have a good backwards compatibility story. With a few changes, the Xorg server can be modified to use wayland input devices for input and forward either the root window or individual top-level windows as wayland surfaces.   DISTRO=fsl-imx-xwayland MACHINE=imx6qsabresd source ./fsl-setup-release.sh -b build-xwayland bitbake fsl-image-gui Once you have the image your Wayland/Weston image will be able to run X11 applications   Excepting X11 applications that use EGL, we don’t support that, if you plan to use EGL apps, please use the Wayland provided functions to create the buffer.   Application for rotation: Weston allows rotating windows with super-key + middle mouse button. As this works for Wayland clients only, you can run Xwayland in weston, run your X application on Xwayland, and rotate the Xwayland display. For another option: Create a file ~/.config/weston.ini with this content: [core] modules=xwayland.so shell=desktop-shell.so idle-time=0 [shell] background-color=0xff002244 locking=false # panel-location=none    [launcher] icon=/usr/share/icons/gnome/24x24/apps/utilities-terminal.png path=/usr/bin/weston-terminal [launcher] icon=/usr/share/icons/hicolor/48x48/apps/firefox.png path=/usr/bin/firefox [output] name=X1 mode=640x800 transform=90 # wanna get mad? use: transform=flipped-270 scale=1 This weston.ini enables a rootless xwayland.so in weston. The [output] section with name=X1 defines weston's appearance as X client. transform=90 rotates the weston display.   the [launcher] sections can be used to create custom panel starters for your X applications. See  /usr/share/doc/weston/examples/weston.ini for more detailed information for further cases, I will attach in the future.
View full article
Brief introduction on the aarch64 linux kernel memory mapping layout and basic management stuffs.  Contents include: Kernel's virtual memory layout and mapping after running i.MX8QM/QXP kernel reserved memory layout Kernel memory allocation method and technology (Buddy, cma, ION...) DMA buffer management, SWIOTLB, IOMMU GPU memory management How to customize the memory for different use cases How to avoid using CMA for a better stability and performance
View full article
These questions and answers are about interrupt generation at a dedicated (configurable) video output port. The i.MX6D manual (Rev. 0) Image Processing Unit (IPU) chapter mentions: Every DI has 10 timing generator counters. The IPU Interrupt Generator has 10 DI0 counters (1...10) and just 2 DI1 counters (3 & 😎 as interrupt sources. The Interrupt Control Register lists 11 DI0 counters (0...10) Q1. Are the DI timing-generator counters linked to the counters in the interrupt controller, or are they different counters? A1. Yes, the DI timing generator counters are linked to the counters in the interrupt controller. Q2. Why are there 11 counters listed in the interrupt controller, but just 10 counters in the timing generator? A2. There is disp_clk_en_pre in the interrupt controller. Thus the 11 counters: 10 timing generator counters and 1 disp clock generator counter. Q3. Is configurable timing feasible for DI0 by using the timing generator counters? A3. Yes, using the 10 internal timing counters you can generate various timing relationships. In addition, you can detect any of the interrupt counters. For example, if you use counter 8, then you can detect the interrupt associated with counter 8. Q4. Explain the impact of the DI1 counter access of only channels 3 and 8. A4. DI1 also has 10 timing generator counters and 1 disp clock generator counter, which you can use to generate desired waveforms. This is similar to DI0. The difference is only 2 of the 10 counters (plus another disp_clk) are connected to the interrupt controller for DI1. Therefore, there is a restriction for detection. If you use counter 7, read out the counter 7 interrupt of DI1 is not possible. However, 2 channels should be sufficient. These interrupts are usually used to indicate a frame start or a frame end. We usually use counter 3 to represent Vsync. So normally we only use counter 3 interrupt. DI1 has only 3 accesses because this covers the anticipated use case and the desire was to restrict register size. The extra counters facilitate flexible DI1 timing generation.
View full article
Overview The first in the series, the i.MX53 Quick Start board is a low cost development platform. Integrated with an ARM® CortexTM-A8 1 GHz processor, the Quick Start board includes a display controller, hardware-accelerated graphics, 1080p video decode and 720p encode as well as numerous connectivity options ideally suited for applications such as human machine interface in embedded consumer, industrial and medical markets. Go to http://www.freescale.com/iMXQuickStart and visit the official Quick Start Board page Hardware Features Processor • i.MX53 1 GHz ARM Cortex-A8 Processor • Power management IC • 1 GB DDR3 memory Display • LVDS connector • VGA connector • Parallel LCD add-on card (via expansion connector) • HDMI add-on card (via expansion connector) Audio • SPDIF output via HDMI add-on card • Freescale SGTL5000 audio codec • Microphone jack • Headphone jack Expansion Connector • Enables parallel LCD or HDMI output • Camera CSI port signals • I2C, SSI, SPI signals Connectivity • Full-size SD/MMC card slot • microSD card slot • 7-pin SATA data connector • 10/100 Base-T Ethernet port • Two High-Speed USB host ports • Micro USB device port Debug • JTAG connector • DB-9 UART port Miscellaneous • 3” x 3” 8-layer PCB • 3-axis Freescale accelerometer (MMA8450QT) • 2A, 5V power supply Tutorials, Training Materials and Documentation Android i.MX 53 QSB Enable WiFi Android i.MX 53 QSB Android Recovery Mode Linux i.MX 53 QSB Board Get Started i.MX 53 QSB Ubuntu Dual Display Running Dual Display on i.MX53QSB   
View full article
Wondering how to manage and install the various rpms generated under tmp/deploy/rpm? smart is the application you need on the target to replace apt-get Please set your local.conf with the following: # It is also recommended you use build history, which adds some sanity checks to package versions, in conjunction with the server that # is running the PR Service. To enable build history, add the following to each building system's # It is recommended to activate "buildhistory" for testing the PR service INHERIT += "buildhistory" BUILDHISTORY_COMMIT = "1" PRSERV_HOST = "localhost:0"  # This will set up your host computer as Package Revision Server // PACKAGE_FEED_URIS = "http://10.170.96.7/imx7rpm" #please place any server ip addr, this one is mine. add also the following to enable the package management (smart): EXTRA_IMAGE_FEATURES += "package-management" Setup your own http server, and link the server repository with your tmp/deploy/rpm repo (your are free to use your preferred http server). Since Morty (yocto 2.4), smart has been deprecated, and now the package management is done with dnf (from Debian). Please check dnf document to get more to know about dnf. The dependencies are still poorly controlled. After compiling a pkg the easiest remain: dnf install package.rpm example: root@imx8mmevk:~# dnf install libfuse2-2.9.7-r0.aarch64.rpm Failed to synchronize cache for repo 'oe-remote-repo-imx8m-imx8mqevk-arm', disabling. Dependencies resolved. ===============================================================================================================  Package                  Arch                    Version                   Repository                    Size =============================================================================================================== Installing:  libfuse2                 aarch64                 2.9.7-r0                  @commandline                  56 k Transaction Summary =============================================================================================================== Install  1 Package Total size: 56 k Installed size: 212 k Is this ok [y/N]: y Downloading Packages: Running transaction check Transaction check succeeded. Running transaction test Transaction test succeeded. Running transaction   Preparing        :                                                                                       1/1   Installing       : libfuse2-2.9.7-r0.aarch64                                                             1/1   Running scriptlet: libfuse2-2.9.7-r0.aarch64                                                             1/1 /sbin/ldconfig: /usr/lib/libOpenVG.so is not a symbolic link   Verifying        : libfuse2-2.9.7-r0.aarch64                                                             1/1 Installed:   libfuse2.aarch64 2.9.7-r0 Complete!
View full article
For the board imx8M Quad EVK running the Linux 4.14.78-1.0.0_ga version BSP, the resolutions 3840x2160,1920x1080, 1280x720, 720x480 are support in our default BSP. For the other resolutions how to make it work? This patch used to do support for a non-default resolution on i.MX 8MQ EVK. Basically, the customer needs to change the clocks accordingly to the display requirements,  it to be used as a base to the display support.
View full article
In this doc will show how to adjust display brightness/contrast/saturation by using i.MX8  Display Controller (DC) Subsystem.   HW: i.MX8QXP MEK board SW: Linux 4.14.98_2.0.0 BSP release.   See i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual, Rev. 😧 This kind Matrix total number is 5 , that is 0/1/4/5/9. In this doc using Matrix0 to adjust whole display brightness/contrast/saturation. Matrix0 unit position is located between FramGen unit and Tcon unit, that means using Matrix0 will impact on the whole display contents. Note, this Matrix is applied on RGB color space.    The Matrix is consist of two parts: and  You can program any value into register of A11 to A44 and C1 to C4, Matrix will applied on input RGB data, then output RGB data will changed as you want. In this way, we can change the display brightness/contrast/saturation. The Matrix entry from A11 to A44, their register format is same as below: Each register entry of A11 to A44 , total 13 bit, bit 12 is symbol bit , bit 11 and bit 10 is integer bit, bit 9 to bit 0 is floating point bit. The Matrix entry from C1 to C4, their format is same as below: Each register entry of C1 to C4, total 13 bit, bit 12 is symbol bit, others are integer bit. Now let us choose the matrix that will be used for adjust brightness/contrast/saturation. See this link  https://docs.rainmeter.net/tips/colormatrix-guide/ So we can set matrix as below to change brightness/contrast/saturation   A11=c(sr+s)   A12=c(sg)    A13=c(sb)   A21=c(sb)     A22=c(sg+s)  A23=c(sb)   A31=c(sr)     A32=c(sg)    A33=c(sb+s)   C1=C2=C3=t+b   b as brightness , range[-1.0, 1.0], zero means no change , >0 will increases brightness, <0 will reduce brightness. c as contrast, range [0,2.0) , default is 1.0 , >1.0 is increase , <1.0 is reduce. s is saturation, range [0,1.0], default is 1.0.  Other matrix entry is related to alpha, in this doc not change it, just keep them as zero.     Note here sr,sb,sg value will depend on lumR/ lumG/ lumB constant value you choose, this value may depend on different color standard.   Due to each matrix value is floating point number, and in this doc , i.MX8X run Linux OS. So you can choose do floating point operation in user space program, then pass related register value into kernel space , let driver write them into register. But in this doc, to make Linux kernel driver more simple, I will convert floating point operation into integer operation , then user space app just pass brightness/contrast/saturation value into kernel space, then kernel driver to do left operation in kernel space. So 1024*c and 1024*s is integer number that user space app will passed into kernel space. And in kernel space could be do left integer number operation, then write register value. The kernel patch 8qxp_4.14.98_brightness_contrast_saturation.diff could be used on 4.14.98_2.0.0 BSP release. Test usage, need used one patch that for proptest which from libdrm test case, see 8qxp_prop_test.diff, recompile the proptest case. root@imx8qxpmek:~# ./proptest     //list current drm property CRTC 32         42 bringhtness:                 flags: range                 values: 0 131071                 value:0x0         43 contrast:                 flags: range                 values: 0 2048                 value:0x400         44 saturation:                 flags: range                 values: 0 1024                 value:0x400         45 update:                 flags: range                 values: 0 1                 value:0x0   I add four drm property , brightness, contrast, saturation, update. The “update property” should be set as 1 at last, otherwise kernel space will not update related property. Reference API usage ( in 8qxp_prop_test.diff) +     drmModeObjectSetProperty(fd_rend, obj_id, obj_type, 42, b_int); +     drmModeObjectSetProperty(fd_rend, obj_id, obj_type, 43, c_int); +     drmModeObjectSetProperty(fd_rend, obj_id, obj_type, 44, s_int); +     drmModeObjectSetProperty(fd_rend, obj_id, obj_type, 45, 1);      //run cmd as below , will ask you input related brightness/contrast/saturation value , then will get result in display root@imx8qxpmek:~# ./proptest 32 crtc 45 1   input brightness [-1,1] 0.3 input contrast, >1.0 or <1.0 1.2 input saturation, [0,1] 0.3 brightness 0.300000  0x133 from [-1,1] percent contrast  1.200000  0x4cc >1.0 or <1.0 saturation 0.300000 0x133  from 0.0 to 1.0   Known Issue: For demo this feature , I need run proptest and weston at same time. Due to the set property drm ioctl default allowed by DRM master and DRM control client. But 4.14. kernel, removed the DRM control device node, so I changed to open drm render node fd, and allow DRM render client to using set property drm ioctl.  This is just a workaround, you may not use it. Reference: 1.https://www.nxp.com/docs/en/reference-manual/IMX8DQXPRM.pdf  2.https://docs.rainmeter.net/tips/colormatrix-guide/
View full article
Overview The purpose of this document is to describe how to enable 3G modem in i.MX sabresx board for Android software. Hardware Changes Unlike other boards of I.mx series, in sabresx board  3G modem doesn't share to use PCIE slot any longer. It is not connected with PCIE slot by default. So if you still want to use 3G modem like in sabresd board. You need to do a tiny hardware rework. Like the below, R177 and R178 is DNP. Just add a zero resistor here. Software patches After you have do hardware rework above, then you should git am the attached patch to add software support which will add the dts config of 3G power. In our official release version, we don't include this patch.
View full article
       The document will introduce all steps for poring BCM4330/BCM43362 WIFI module to freescale android4.2.2 BSP, it includes these contents: --Hardware & Software Environment --Hardware Design Based on BCM43362 module --i.MX6 BSP configuration for WIFI module --BCM4330/BCM43362 dirver for linux 3.0.35 --Integrated to Android4.2.2    If customer has some questions with the porting, contact me , please ! my email address: [email protected] Freescale TICS team Weidong.sun 2015-08-20
View full article
After Nokia acquisition of Trolltech, QT has become an even more interesting framework/tool for UI and graphics development. The new release 4.6 can be obtained under LGPL license and comes with a new integrated IDE for software development (QT Creator) with many demos, some of them using OpenGL. In order to create an environment to create, simulate and cross-compile, it's needed to build three versions of QT: Qt/X11, qmake-x11. This is the Qt version that you will be using on your PC. It is also used for building the tools, such as Designer and Linguist. Qt/QVFb, qmake-qvfb. This is an embedded Qt configuration that runs on host, but works with the virtual framebuffer instead of the actual screen. It let’s you emulate the target system, but run your code on your host machine. Qt/target, qmake-target. This is the embedded Qt configuration that runs on your target platform. This is what you use to build an actual application running on your embedded device. On Host you need TO install following package (for Ubuntu distri) to install this QT toolsuit: [X] libx11-dev [X] libpng-dev [X] libjpeg-dev [X] libxext-dev [X] x11proto-xext-dev [X] qt3-dev-tools-embedded [X] libxtst-dev Building Qt/X11 Extract downloaded Qt package (from here) and install it by running: ./configure make sudo make install Qt will be installed on /usr/local/Trolltech/Qt-version directory. We also need to build qvfb tool that will provide virtual framebuffer for X11. To build and install it run: cd tools/qvfb make sudo make install qvfb will be installed on /usr/local/Trolltech/Qt-version/bin directory. Building Qt/QVFb To build Qt/QVFb, will be needed some parameters on configure file. Extract again Qt package on other folder and build as following: ./configure -embedded -qt-gfx-qvfb -qt-kbd-qvfb -qt-mouse-qvfb -prefix /usr/local/Trolltech/Qt-qvfb-version make sudo make install Used parameters: -qt-gfx-qvfb, the graphics driver will be for QVFb, i.e., the virtual framebuffer. -qt-kbd-qvfb, the keyboard input will come from the QVFb. -qt-mouse-qvfb, the mouse input will come from the QVFb. -prefix /usr/local/Trolltech/Qt-qvfb-version, the prefix is used to separate the QVFb version of embedded Qt from the target version. Testing QVFb So far you have two versions of Qt: 1. Qt/X11 built for PC host using X11 and located at /usr/local/Trolltech/Qt-version 2. Qt/QVFb built for PC host using Qt virtual framebuffer and located at /usr/local/Trolltech/Qt-qvfb-version Call qvfb from X11 version cd /usr/local/Trolltech/Qt-version/bin ./qvfb & A simple virtual framebuffer will open. To change screen configuration and add a skin, click in "file -> configure". The following window will open: i.e., choose ClamshellPhone and click ok. A cell phone skin will open. On QVFb version, there are a lot of example applications that can be run using Qt virtual framebuffer. Let's open fluidlauncher demo: cd /usr/local/Trolltech/Qt-qvfb-version/demos/embedded/fluidlauncher ./fluidlauncher -qws The argument -qws is used to inform that the application will run on Qt virtual framebuffer. Building Qt/Target To build Qt for target (i.MX), it's necessary to build Ltib with some required packages. In this example, a kernel and rootfs will be built for i.MX51 EVK with the following extra packages. [x] amd-gpu-bin-mx51 [x] freetype [x] glib2 [x] gstreamer [x] gstreamer-plugins-base [x] gstreamer-plugins-good [x] gstreamer-plugins-bad [x] gstreamer-plugins-ugly [x] libxml2 [x] tslib [x] zlib If you are building for any other i.MX processor, you don't need the "amd-gpu-bin-mx51" option. After build ltib, make a symbolic link /tftpboot/ltib pointing to your rootfs folder. It's needed to make the i.MX libs and incs available to qmake. ln -s <rootfs folder dir> /tftpboot/ltib Restart nfs server. If using Ubuntu, the command is: sudo /etc/init.d/nfs-kernel-server restart Extract downloaded Qt package on a new folder. Export the crosscompiler path. Usually it's located at /opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin: export PATH=$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin If you are building Qt for i.MX51 Download the mkspec package and extract the folder linux-mxc-g++ under <Qt source code folder>/mkspecs/qws Configure, build and install with the following commands: ./configure -embedded arm -xplatform qws/linux-mxc-g++ -release -prefix /usr/local/Trolltech/Qt-target-version -qt-gfx-linuxfb -qt-kbd-tty -qt-mouse-tslib -opengl es2 -little-endian -host-little-endian make sudo make install For targets without 3D engine support If you are building Qt for a target that doesn't support OpenGL, i.e., i.MX25, 233: Download the makespecs_no3D package and extract the folder linux-mxc-g++ under <Qt source code folder>/mkspecs/qws Configure, build and install with the following commands: ./configure -embedded arm -xplatform qws/linux-mxc-g++ -release -prefix /usr/local/Trolltech/Qt-target-version -qt-gfx-linuxfb -qt-kbd-tty -qt-mouse-tslib -little-endian -host-little-endian make sudo make install Copy Cross Qt to target's RFS The crosscompiled version of Qt will be located on your host machine as indicated on -prefix, in this case /usr/local/Trolltech/Qt-target-version Copy Qt-target-version folder to rootfs: cd /tftpboot/usr/local mkdir Trolltech cd Trolltech cp -a /usr/local/Trolltech/Qt-target-version . Now it's ready to use. On target, run: /usr/local/Trolltech/Qt-qvfb-version/demos/embedded/fluidlauncher/fluidlauncher -qws See some pictures of the same application running on host and on EVK: Tips 1. To clean all Qt configuration settings: make confclean 2. To check the current configuration: On Qt source code folder, you can open the file config.status to check the current configuration settings.
View full article
Debugging with JTAG JTAG was created to test populated circuit boards after manufacture. Nowadays, JTAG is primarilly used to access sub-blocks of integrated circuits and useful mechanism for debugging embedded systems. When used as a debugging tool, an in-circuit emulator - which in turn uses JTAG as the transport mechanism - enables a programmer to access an on-chip debug module which is integrated into the CPU, via the JTAG interface. The debug module enables the programmer to debug the software of an embedded system. Besides debugging, the second purpose of the JTAG interface is allowing device programmer hardware to transfer data into internal non-volatile device memory. Some device programmers serve a double purpose for programming as well as debugging the device. [Source: http://en.wikipedia.org] All Boards Hardware Software i.MX27 ADS Board Installing OpenOCD and GDB All Boards Debugging Android All Boards How To Understand JTAG BSDL
View full article