i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
If you already followed the i.MX31ADS Compiling Uboot steps or got a compiled U-boot image, copy u-boot.bin to /tftpboot: $ cp u-boot.bin /tftpboot If you have RedBoot on your board follow the "Installing RedBoot using U-Boot", but if you already have been installed U-Boot and are just installing a new version jump to "Installing U-Boot using U-Boot". Installing U-Boot using RedBoot Load the U-boot image to board RAM: RedBoot> load -v -r -b 0x100000 /tftpboot/u-boot.bin -h 10.29.244.27 Where: 0x100000 is the memory position where the firmware image will be downloaded; 10.29.244.27 is your host IP which is running the TFTP server. Erase the Flash: RedBoot> fis erase -f 0xA0000000 -l 0x00040000 To make sure about what area you should erase, perform the fis list command and compare the areas Write the image to Flash: RedBoot> fis write -f 0xA0000000 -b 0x100000 -l 0x00040000 Reset the board: RedBoot> reset You should see something like this: U-Boot 1.3.3 (May 26 2008 - 11:19:43) CPU: Freescale i.MX31 at 531 MHz Board: MX31ADS DRAM: 128 MB Flash: 32 MB In: serial Out: serial Err: serial Hit any key to stop autoboot: 0 => Installing U-Boot using U-Boot First upload the U-Boot firmware using Network (Transferring file over network ) or Serial (Transferring File Over Serial) This is a common serial transfer output: => loady ## Ready for binary (ymodem) download to 0x80800000 at 115200 bps... CCmode, 1359(SOH)/0(STX)/0(CAN) packets, 9 retries ## Total Size = 0x0002a388 = 172936 Bytes Unprotect the bootloader flash area: protect off A0000000 A003FFFF Erase the flash blocks: erase A0000000 A003FFFF Copy from RAM to Flash: If firmware has been thansfered over serial: cp.b 80800000 A0000000 2a388 If firmware has been transfered over tftp: cp.b 100000 A0000000 2a388 Installing U-Boot using OpenOCD JTAG/GDB To do that you need to compile U-Boot with this define: #define CONFIG_SKIP_LOWLEVEL_INIT 1 Then enter in GDB and execute: (arm-gdb) restore u-boot.bin binary 0x87f00000 Restoring binary file u-boot.bin into memory (0x87f00000 to 0x87f2c790) (arm-gdb) set $pc = 0x87f00000 (arm-gdb) c You will see U-Boot starting in the serial console. Then compile a new U-Boot without the CONFIG_SKIP_LOWLEVEL_INIT and follow the Installing U-Boot using U-Boot to install U-Boot in the flash. Installing U-Boot using LogicLoader losh> ifconfig sm0 dhcp losh> load raw 0x81000000 115764 /tftp/10.29.244.27:u-boot.bin.lite losh> exec 0x81000000 -
View full article
Summary: The i.MX 8M-Mini can boot from QSPI flash using a dedicated boot image. The boot config settings are not correctly documented in the EVK Board Hardware User's Guide Rev 0 from 02/2019. In the document i.MX_Linux_User's_Guide.pdf  in the BSP documentation 4.14.98 the settings are correctly given in Table 38 Details: To generate a bootable file for the QSPI with Yocto, you need to include the following setting into local.conf: UBOOT_CONFIG = "fspi" If you don't want/need to make a complete build, just rebuild u-boot: bitbake -c deploy u-boot-imx Alternatively the file imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi included already in the BSP demo packages will work as well Program the image into QSPI: With UUU:   uuu -b qspi imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi With u-boot: u-boot=> fatls mmc 0:1 14557696   Image    …   1446848   imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi 11 file(s), 0 dir(s) u-boot=> sf probe SF: Detected n25q256a with page size 256 Bytes, erase size 4 KiB, total 32 MiB u-boot=> fatload mmc 0:1 0x40480000 imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi 1446848 bytes read in 79 ms (17.5 MiB/s) u-boot=> sf erase 0x0 0x200000 SF: 2097152 bytes @ 0x0 Erased: OK u-boot=> sf write 0x40480000 0x0 0x200000 device 0 offset 0x0, size 0x200000 SF: 2097152 bytes @ 0x0 Written: OK u-boot=> sf read 0x50000000 0x0 0x200000 device 0 offset 0x0, size 0x200000 SF: 2097152 bytes @ 0x0 Read: OK u-boot=> cmp.b 0x40480000 0x50000000 0x200000 Total of 2097152 byte(s) were the same u-boot=> Set boot config jumpers correctly and power on the board (no SD-card in the slot) 8M-Mini Rev A and Rev B boards:  01xxxxx0 0000x001 8M-Mini Rev C boards: 0110xxxxxx 00100x0010
View full article
The init file is a key component of the Android boot sequence. It is a program to initialize the elements of the Android system.  Unlike Linux, Android uses its own initialization program. This Android init program processes 2 files, and it executes the commands it finds in both programs. These programs are: ‘init.rc’ and ‘init<machine name>.rc’ (this machine name is the name of the hardware that Android is running on). What does each program contain?: init.rc provides the generic initialization instructions init<machine name>.rc provides specific initialization instructions init<machine name>.rc is imported by the init.rc program. What is the syntax of these .rc files? The android init language consists of 4 classes of statements: Actions, Commands, Services and Options. Actions and Services declare new sections. All the commands or options belong to the section most recently declared. Actions and Services have to have unique names. If a second Action or Service has the same name of a previous one, it is ignored. Actions Actions are sequences of commands. They have a trigger which is used to determine when the action should occur. Actions take following form. On <trigger> <command> <command> <command>… Services Services are programs which init launches and (optionally) restart when it exists Services take the following form. Service <name> <patchname>  [argument] <option> <option>… Options Options are modifiers to services. These affect how and when init runs a service. Critical This is a device-critical service. If it exits more than four times in four minutes, the device will reboor into recovery mode. Disabled This service will not automatically start with its class. It must be explicitly started by name. Setenv <name> <value> Set the environment variable <name> to <value> in the launched process. User <username> Change to username before executing this service. Currently defaults to root. Group <groupname> [<groupname>] Change to groupname before executing this service. Oneshot Do not restart the service when it exists Class <name> Specify a class name for the service. All services in a named class may be started or stopped together. Onrestart Execute a command when service restarts Triggers Triggers are strings which can be used to match certain kinds of events and used to cause an action to occur. Boot This is the first trigger that will occur when init starts (after /init.conf is loaded) Commands: Exec <path> [<arguments>] Fork and execute a program (<path>). This will block until the program completes execution. Export <name> <value> Set the environment variable <name> equal to <value> in the global environment. Ifup <interface> Bring the network interface <interface> online. Import <filename> Parse and init config file, extending the current configuration. Hostname <name> Set the host name Chdir <directory> Change working directory Chmod <octal-dmoe> <path> Change file access permissions Chwon <owner> <group> <path> Change file owner and group Chroot <directory> Change process root directory Class_start <serviceclass> Start all services of the specified class if they are not already running. Class_stop <serviceclass> Stop all services of the specified class if they are currently running. Domainname <name> Set the domain name Enable <servicename> Turns a disabled service into an enabled one. Insmod <path> Install the module at <path> Mkdir <path> Create a directory at <path> Mount <type><device><dir> Attempt to mount the named device at the directory. Restorecon <path> Restore the file named by <path> to the security context specified in the file_contexts configuration. Setcon <securitycontext> set the current process security context to the specified string. Setenforce 0|1 Set the SELinux system wide enforcing status. 0 = permissive. 1 = enforcing. Setprop <name><value> Set system property <name> to <value> Setrlimit <resource><cur><max> Set the rlimit for a resource Setsebool <name><value> Set SELinux Boolean <name> to <value> Start <service> Start a service Stop <service> Stop a service Symlink <target><path> Create a symbolic link at <path> with the value <target> Trigger <event> Trigger an event. Used to queue an action from another action Wait <path> Poll for the existence of the given file and return when found. Write <path> <string> Open the file at <path> and write a string to it. Examples How to run a script: service my_service /data/test   class main   oneshot Here we are declaring the service named 'my service' with location in /data/test. It belongs to the main class and will start along with any other service that belongs with that class and we declare that the service wont restart when it exits (oneshot). Change file access permissions: chmod 0660   /sys/fs/cgroup/memory/tasks Here we are changing access permissions in path /sys/fs/cgroup/memory/tasks Write a string to a file in a path: write  /sys/fs/cgroup/memory/memory/memory.move_charge_at_immigrate   1 Create a symbolic link: symlink  /system/etc /etc Here we are creating a symbolic link to /system/etc -> /etc Set a specific density of the display: setprop ro.sf.lcd_density 240 Here we are setting a system property of 240 to ro.sf.lcd_density Set your watchdog timer to 30 seconds: service watchdog /sbin/watchdogd 10 20 class core We are petting the watchdog every 10 seconds to get a 20 second margin Change file owner: chown root system /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq The new owner being 'root' from the group 'system'
View full article
Recipes to include Amazon's Alexa Voice Services in your applications. Step 1 : Get iMX Yocto AVS setup environment Review the steps under Chapter 3 of the i.MX_Yocto_Project_User'sGuide.pdf on the L4.X LINUX_DOCS to prepare your host machine. Including at least the following essential Yocto packages $ sudo apt-get install gawk wget git-core diffstat unzip texinfo \ gcc-multilib build-essential chrpath socat libsdl1.2-dev u-boot-tools Install the i.MX NXP AVS repo Create/Move to a directory where you want to install the AVS yocto build enviroment. Let's call this as <yocto_dir> $ cd <yocto_dir> $ repo init -u https://source.codeaurora.org/external/imxsupport/meta-avs-demos -b master -m imx-alexa-sdk-4.9.51-8mq_ga.xml Download the AVS BSP build environment: $ repo sync Step 2: Setup yocto for Alexa_SDK image with AVS-SETUP-DEMO script: Run the avs-setup-demo script as follows to setup your environment for the imx8mqevk board: $ MACHINE=imx8mqevk DISTRO=fsl-imx-xwayland source avs-setup-demo.sh -b <build_sdk_8M> Where <build_sdk> is the name you will give to your build folder. After acepting the EULA the script will prompt if you want to enable: Sound Card selection The following Sound Cards are supported on the build: 2-Mic Synaptics/Conexant 2-Mic TechNexion Voice Hat (with DSPConcepts SW) The script will prompt to select the soundcard you will be using: Which Sound Card are you going to use? Synaptics/Conexant .................... 1 VoiceHat (for DSPConcepts SW) ......... 2 Type the number of your selection and press Enter... Install Alexa SDK Next option is to select if you want to pre-install the AVS SDK software on the image. Do you want to build/include the AVS_SDK package on this image(Y/N)? If you select YES, then your image will contain the AVS SDK ready to use (after authentication). Note this AVS_SDK will not have WakeWord detection support, but it can be added on runtime. If your selection was NO, then you can always manually fetch and build the AVS_SDK on runtime. All the packages dependencies will be already there, so only fetching the AVS_SDK source code and building it is required. Finish avs-image configuration At the end you will see a text according with the configuration you select for your image build. Next is an example for a Preinstalled AVS_SDK with Synaptics Sound Card support ============================================================ AVS configuration is now ready at conf/local.conf - Sound Card = Synaptics - Alexa SDK 1.7 pre-installed - Wifi supported You are ready to bitbake your AVS demo image now:   bitbake avs-image If you want to use QT5DisplayCards, use then:   bitbake avs-image-qt5 ============================================================ Step 3: Build the AVS image Go to your <build_sdk> directory and start the build of the avs-image There are 2 options Regular Build: $ cd  <yocto_dir>/<build_sdk>   $ bitbake avs-image With QT5 support included: $ cd  <yocto_dir>/<build_sdk>   $ bitbake avs-image-qt5 The image with QT5 is useful if you want to add some GUI for example to render DisplayCards. Step 4 : Deploying the built images to SD/MMC card to boot on target board. After a build has succesfully completed, the created image resides at <build_sdk>/tmp/deploy/images/imx8mqevk/ In this directory, you will find imx8mqevk-avs--.sdcard image or imx8mqevk-avs-qt5--.sdcard, depending on the build you chose on Step3. To Flash the .sdcard image into an SD Card follow the next steps: Extract and copy the .sdcard file to your SD Card $ cd <build_sdk>/tmp/deploy/images/imx8mqevk/ $ cp -v imx8mqevk-avs-synaptics-1.7.sdcard.bz2 <workdir> $ cd <workdir> $ sudo bzip2 -d imx8mqevk-avs-synaptics-1.7.sdcard.bz2 $ sudo dd if=imx8mqevk-avs-synaptics-1.7.sdcard.bz2 of=/dev/sd<part> bs=1M && sync $ sync Properly eject the SD Card: $ sudo eject /dev/sd<part> Insert the flashed SD Card on the 8M EVK and boot. Follow the instructions at startup to setup your AVS and run the SampleApp. NXP Documentation For a more comprehensive understanding of Yocto, its features and setup; more image build and deployment options and customization, please take a look at the i.MX_Yocto_Project_User's_Guide.pdf document from the Linux documents bundle mentioned at the beginning of this document. For a more detailed description of the Linux BSP, u-boot use and configuration, please take a look at the i.MX_Linux_User's_Guide.pdf document from the Linux documents bundle mentioned at the beginning of this document.
View full article
Question: The code signing tool(CST) of i.MX6 with "CST -h" command just for viewing help message took about 22 minutes. On other system, it was shorter but still took about 2 minutes. CST version is BLN_CST_MAIN_02.00.00. More test results: 1. Print help message => 4 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --help && date Fri Oct 18 14:10:52 KST 2013 Fri Oct 18 14:15:01 KST 2013 2. Signing 512MB file => 11 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_system.csf" < "example_system.csf" && date Fri Oct 18 14:15:01 KST 2013 CSF Processed successfully and signed data available in out_system.csf Fri Oct 18 14:25:47 KST 2013 3. Signing 3MB file => 17 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_kernel.csf" < "example_kernel.csf" && date Fri Oct 18 14:25:47 KST 2013 CSF Processed successfully and signed data available in out_kernel.csf Fri Oct 18 14:42:39 KST 2013 4. Signing 160KB file => 2 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_uboot.csf" < "example_uboot.csf" && date Fri Oct 18 14:42:39 KST 2013 CSF Processed successfully and signed data available in out_uboot.csf Fri Oct 18 14:45:05 KST 2013 Answer: The slow performance is caused by lack of entropy source and it takes long time to initialize random number generator. Check amount of entropy  "cat /proc/sys/kernel/random/entropy_avail" Tried to install package rng-tools. 1. $sudo apt-get install rng-tools 2. add the following settings in /etc/default/rng-tools HRNGDEVICE=/dev/urandom RNGDOPTIONS=”-W 90% -t 1? 3. sudo /etc/init.d/rng-tools restart 4. cat /proc/sys/kernel/random/entropy_avail After rng-tools starts, entropy increases from less than 100 to more than 1000, then command ./cst -h can run very smoothly.
View full article
Whenever possible is always better to avoid Virtual Machines when compiling Android as the building process might take several hours to even a day or two depending on the resources available to the Virtual Machine. Sometimes, however, a VM is the only option available and here are some useful considerations when using a VM as a host for Android builds. This document addresses some of the requirements for the Kit-Kat Freescale Android BSP although some may also apply to the general Android releases. It’s recommended to use Ubuntu 12.04 64-bits as Host OS. As for HDD space, which is often a limited resource when using VM, Google states that at least 30GB of disk space in order to build the Android Tree. In practice, however, it’s recommended to allocate at least 100GB to the VM HDD if possible, as additional packages and larger images can quickly deplete disk space. Installing Java (not VM specific) It’s recommended (albeit not mandatory) to uninstall any version of Java other than the recommended for the specific Android release for which we will build. In the case of Kit-Kat this is Java 6. Another option is to just switch the java alternatives to the ones we want to use for Android. There is a document with the exact instructions on how to install the required JKD on the following link. How to install Sun's JDK in Ubuntu for Android build Starting KitKat, however, it’s also necessary to install javap (Java Class File Dissasembler) so please also add these steps when following this document. $ sudo update-alternatives --install /usr/bin/javac javac /usr/lib/jvm/jdk1.6.0_45/bin/javac 1 $ sudo update-alternatives --config javac Memory considerations when using a Virtual Machine Using a Virtual Machine slows down the image building considerably. Besides that memory system is often also an issue. Having insufficient RAM especially on the linking part of the image build may cause a number of issues that are difficult to troubleshoot. In these cases it’s good to take a look at the resource monitor to see if indeed the RAM was depleted. One way to make up for the limited RAM is using a bigger swap. Google recommends at least 16GB of RAM/swap so it’s not uncommon to create a 10GB swap when working in VM, to do this please use the following commands. $ sudo fallocate -l 10g /mnt/10GB.swap $ sudo chmod 600 /mnt/10GB.swap $ sudo mkswap /mnt/10GB.swap $ sudo swapon /mnt/10GB.swap This will helps with the memory requirements but won’t speed up the build process. Building time with VM, as previously stated, will take several hours or even a couple of days depending on computing power.
View full article
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the  i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. NOTE: Please note that DDR support for the i.MX 8M Family and has also been added in the Config Tools for i.MX Applications Processors | NXP Semiconductors Please consider using this tool with more enhanced features. i.MX 8M Family DDR Tools Overview The i.MX 8M Family DDR Tool is a Windows-based software to help users to do LPDDR4/DDR4/DDR3L training, stress test and DDR initial code generation for u-boot SPL. This page contains the latest releases for the i.MX 8M Family DDR Tools and cover the following SoCs : i.MX 8M Quad and its derivatives i.MX 8M Quadlite and i.MX 8M Dual i.MX 8M Mini Quad and its derivatives i.MX 8M Mini Quadlite/Dual/DualLite/Solo/SoloLite  i.MX 8M Nano Quad and its derivatives i.MX 8M Nano Quadlite/Dual/DualLite/Solo/SoloLite  i.MX 8M Plus   NOTE: For the i.MX 8/8X Family of DDR tools please refer to the: i.MX 8/8X Family DDR Tools Release   The purpose of the i.MX 8M Family DDR Tools is to enable users to generate and test a custom DRAM initialization based on their device configuration (density, number of chip selects, etc.) and board layout (data bus bit swizzling, etc.).  This process equips the user to then proceed with the bring-up of a boot loader and an OS.  Once the OS is brought up, it is recommended to run an OS-based memory test (like Linux memtester) to further verify and test the DDR memory interface.     The i.MX 8M Family DDR Tools consist of: DDR Register Programming Aid (RPA) MSCALE DDR Tool   For more details regarding these DDR tools and their usage, refer to the i.MX 8M DDR Tools User Guide.   i.MX 8M Family DDR Tool    The i.MX 8M Family DDR stress test tool is a Windows-based software tool that is used as a mechanism to verify that the DDR initialization is operational for use with u-boot and OS bring-up. To install the DDR Stress Test, save and extract the zip file mscale_ddr_tool_vXXX_setup.exe.zip   (where 'xxx' is the current version number) and follow the on-screen installation instructions.   i.MX 8M Family DDR Tool Requirements   The tool requires access to the Windows registry, hence users must run it in administrator mode. When users design new i.MX 8M Family boards, please make sure to follow the rules outlined in the respective Hardware Developers Guide and the MSCALE_DDR_Tool_User_Guide, which can help users bring up DDR devices on their respective i.MX 8M boards.   i.MX 8M Family DDR Tool User Guide   The i.MX 8M DDR tool includes the document: MSCALE_DDR_Tool_User_Guide NOTE: Please read the MSCALE_DDR_Tool_User_Guide inside the package carefully before you use this tool.   i.MX8M DDR Tool Revision History   Rev Major Changes* (Features) Comments 3.31 Integration of the workaround for 8MQ ERR051273   3.30 Fix DBI enabled issue for all i.MX 8M series Automatically identify ROHM and PCA9450 PMICs on i.MX 8M Nano board Fix 4GB/8GB memory tester issues   3.20 Add support to i.MX 8M Plus   3.10 Fixe UART communication issues for some specific characters between the PC software and the target board. Fine-tune DDRPHY registers in generated C code.   3.00 Add support to i.MX8M-nano Add support to different PMIC or PMIC configuration Add support to stress test for all DDR frequency points RPA tools for Nano include support for DDR3L, DDR4, and LPDDR4.   Note that the DDR3L and LPDDR4 RPAs contain the name preliminary only to denote that these RPAs are based on internal NXP validation boards where the DDR4 RPA is based on the released EVK.   2.10 Change DDR4 capacity computing method   2.00 Add support to i.MX8M-mini   * Further details available in the release notes   Sample configuration in the .ds script for i.MX 8M debug UART2: ################step 0: configure debug uart port. Assumes use of UART IO Pads.   ##### ##### If using non-UART pads (i.e. using other pads to mux out the UART signals), ##### ##### then it is up to the user to overwrite the following IO register settings   ##### memory set 0x3033023C 32 0x00000000 #IOMUXC_SW_MUX_UART2_RXD memory set 0x30330240 32 0x00000000 #IOMUXC_SW_MUX_UART2_TXD memory set 0x303304A4 32 0x0000000E #IOMUXC_SW_PAD_UART2_RXD memory set 0x303304A8 32 0x0000000E #IOMUXC_SW_PAD_UART2_TXD memory set 0x303304FC 32 0x00000000 #IOMUXC_SW_MUX_UART2_SEL_RXD sysparam set debug_uart   1 #UART index from 0 ('0' = UART1, '1' = UART2, '2' = UART3, '3' = UART4)   Sample configuration in the front of the .ds script for i.MX 8M debug UART3  ################step 0: configure debug uart port. Assumes use of UART IO Pads.   ##### ##### If using non-UART pads (i.e. using other pads to mux out the UART signals), ##### ##### then it is up to the user to overwrite the following IO register settings   ##### memory set 0x30330244 32 0x00000000 #IOMUXC_SW_MUX_UART3_RXD memory set 0x30330248 32 0x00000000 #IOMUXC_SW_MUX_UART3_TXD memory set 0x303304AC 32 0x0000000E #IOMUXC_SW_PAD_UART3_RXD memory set 0x303304B0 32 0x0000000E #IOMUXC_SW_PAD_UART3_TXD memory set 0x30330504 32 0x00000002 #IOMUXC_SW_MUX_UART3_SEL_RXD sysparam set debug_uart   2 #UART index from 0 ('0' = UART1, '1' = UART2, '2' = UART3, '3' = UART4)   Sample configuration in the front of the .ds script for i.MX 8M Mini PMIC configuration: ##############step 0.5: configure I2C port IO pads according to your PCB design.   ##### ########### You can modify the following instructions to adapt to your board PMIC ####### memory set 0x30330214 32 0x00000010  #IOMUXC_SW_MUX_I2C1_SCL memory set 0x30330218 32 0x00000010  #IOMUXC_SW_MUX_I2C1_SDA memory set 0x3033047C 32 0x000000C6 #IOMUXC_SW_PAD_I2C1_SCL memory set 0x30330480 32 0x000000C6  #IOMUXC_SW_PAD_I2C1_SDA sysparam set pmic_cfg 0x004B #bit[7:0] = PMIC addr,bit[15:8]=I2C Bus. Bus index from 0 ('0' = I2C1, '1' = I2C2, '2' = I2C3, '3' = I2C4) sysparam set pmic_set 0x2F01 #bit[7:0] = Reg val, bit[15:8]=Reg addr. #REG(0x2F) = 0x01 sysparam set pmic_set 0x0C02   #REG(0x0C) = 0x02 sysparam set pmic_set 0x171E   #REG(0x17) = 0x1E sysparam set pmic_set 0x0C00   #REG(0x0C) = 0x00 sysparam set pmic_set 0x2F11    #REG(0x2F)=0x11     i.MX 8M Family DDR Register Programming Aid (RPA) The i.MX 8M DDR RPA (or simply RPA) is an Excel spreadsheet tool used to develop DDR initialization for a user’s specific DDR configuration (DDR device type, density, etc.). The RPA generates the DDR initialization(in a separate Excel worksheet tab):   DDR Stress Test Script: This format is used specifically with the DDR stress test by first copying the contents in this worksheet tab and then pasting it to a text file, naming the document with the “.ds” file extension. The user will select this file when executing the DDR stress test. The How to Use Excel worksheet tab provides instructions on using the RPA   i.MX 8M Family DDR Register Programming Aid (RPA): Current Versions To obtain the latest RPAs, please refer to the following links (note, existing RPAs have been removed from this main page and moved to the SoC specific links below): i.MX 8M Quad : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8M-m850D-DDR-Register-Programming-Aid-RPA/ta-p/1172441 i.MX 8M Mini : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443 i.MX 8M Nano: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MNano-m815S-DDR-Register-Programming-Aid-RPA/ta-p/1172444 i.MX 8M Plus: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352   Processor Mask Revisions Memory Supported Latest RPA Version * i.MX 8M Quad & Derivatives All LPDDR4 Rev 33 i.MX 8M Quad & Derivatives All DDR4 Rev 18 i.MX 8M Quad & Derivatives All DDR3L Rev 9 i.MX 8M Mini & Derivatives A0 LPDDR4 Rev 22 i.MX 8M Mini & Derivatives A0 DDR4 Rev 21 i.MX 8M Mini & Derivatives A0 DDR3L Rev 10 i.MX 8M Nano & Derivatives A0 LPDDR4 Rev 9 i.MX 8M Nano & Derivatives A0 DDR4 Rev 12 i.MX 8M Nano & Derivatives A0 DDR3L Rev 6 i.MX 8M Plus & Derivatives A1 LPDDR4 Rev 9 i.MX 8M Plus & Derivatives A1 DDR4 Rev 9 * For the details about the updates, please refer to the Revision History tab of the respective RPA.    To modify the DRAM Frequency for a custom setting refer to iMX 8M Mini Register Programming Aid DRAM PLL setting    Related Resources Links: Config Tools for i.MX Applications Processors | NXP Semiconductors i.MX 8M Mini Register Programming Aid DRAM PLL setting  i.MX 8/8X Series DDR Tool Release  i.MX 6/7 DDR Stress test GUI Tool i.MX 8M Application Processor Related Resources i.MX8M (m850D) DDR Register Programming Aid (RPA)  i.MX8MMini (m845S) DDR Register Programming Aid (RPA)  i.MX8MNano (m815S) DDR Register Programming Aid (RPA) i.MX 8MPlus (m865S) DDR Register Programming Aids (RPA)   i.MX 8ULP DDR tools: i.MX Software and Development Tools | NXP Semiconductors Scroll down to “Other Resources --> Tools --> DDR Tools”  
View full article
The D-PHY PLL (in the red circle in the picture below) is the PLL that drives the MIPI Clock lane. It must be set in accordance with the video to be sent to the display.   Calculating the video bandwidth The video bandwidth is calculated with the following equation: Pixels per second = Horizontal res. x Vertical res. x Frame rate x Bits per pixel Taking as example the 1080p60 OLED display RM67191: Pixels per second = 1920 x 1080 x 60 x 24 Pixels per second = 2985984000 = 2,98Gpixels/sec Pixel clock calculation The Display pixel clock can be obtained on the display driver. In this example for RM67191, the pixel clock is 132Mpixel/sec, see file: panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Line 530: .pixelclock = { 66000000, 132000000, 132000000 }, Or the number can be obtained with the following equation: pixel clock = (hactive + hfront_porch + hsync_len + hback_porch) x (vactive + vfront_porch + vsync_len + vback_porch) x frame rate pixel clock = (1080 + 20 + 2 +34) × (1920 + 10 + 2 + 4) x 60 pixel clock = 132000000 (rounded up) Bit clock calculation (clock lane) The mipi-dphy bit_clk is the output clock and is calculated on file sec-dsim.c (line 1283): sec-dsim.c\bridge\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Bit clock can be calculated with the following equation: bit_clk = Pixel clock * Bits per pixel / Number of lanes In the case of 1980p60 (Raydium display), It is:   bit_clk = pixel clock * bits per pixel / number of lanes bit_clk = 132000000 * 24 / 4 bit_clk = 792000000 Other important timing parameters like 'p', 'm', 's' are obtained on the table in the following header file: sec_mipi_dphy_ln14lpp.h\imx\drm\gpu\drivers - linux-imx - i.MX Linux kernel 
View full article
Instead to use gst-launch to play your audio/video media you can create an application do to that. This application was tested in iMX27ADS but should to work on iMX27PDK First execute LTIB (./ltib -c) and select these packages: all gstreamer plugin, alsa-utils and libmad. Create your file code (i.e.: playvideo.c): #include <gst/gst.h> #include <glib.h> #include <string.h> static GstElement *source, *demuxer, *vdqueue, *adqueue, *vdsink, *adsink, *decvd, *decad; void on_pad_added (GstElement *element, GstPad *pad) {         g_debug ("Signal: pad-added");         GstCaps *caps;         GstStructure *str;         caps = gst_pad_get_caps (pad);         g_assert (caps != NULL);         str = gst_caps_get_structure (caps, 0);         g_assert (str != NULL);         if (g_strrstr (gst_structure_get_name (str), "video")) {                 g_debug ("Linking video pad to dec_vd");                 // Link it actually                 GstPad *targetsink = gst_element_get_pad (decvd, "sink");                 g_assert (targetsink != NULL);                 gst_pad_link (pad, targetsink);                 gst_object_unref (targetsink);         }         if (g_strrstr (gst_structure_get_name (str), "audio")) {                 g_debug ("Linking audio pad to dec_ad");                 // Link it actually                 GstPad *targetsink = gst_element_get_pad (decad, "sink");                 g_assert (targetsink != NULL);                 gst_pad_link (pad, targetsink);                 gst_object_unref (targetsink);         }         gst_caps_unref (caps); } static gboolean bus_call (GstBus    *bus,           GstMessage *msg,           gpointer    data) {   GMainLoop *loop = (GMainLoop *) data;   switch (GST_MESSAGE_TYPE (msg)) {     case GST_MESSAGE_EOS:       g_print ("End of stream\n");       g_main_loop_quit (loop);       break;     case GST_MESSAGE_ERROR: {       gchar  *debug;       GError *error;       gst_message_parse_error (msg, &error, &debug);       g_free (debug);       g_printerr ("Error: %s\n", error->message);       g_error_free (error);       g_main_loop_quit (loop);       break;     }     default:       break;   }   return TRUE; } int main (int  argc,       char *argv[]) {   GMainLoop *loop;   GstElement *pipeline;   GstBus *bus;   /* Initialisation */   gst_init (&argc, &argv);   loop = g_main_loop_new (NULL, FALSE);   /* Check input arguments */   if (argc != 2) {     g_printerr ("Usage: %s <Video H264 filename>\n", argv[0]);     return -1;   }   /* Create gstreamer elements */   pipeline      = gst_pipeline_new ("media-player");   source        = gst_element_factory_make ("filesrc","file-source");   demuxer      = gst_element_factory_make ("mfw_mp4demuxer","avi-demuxer");   decvd        = gst_element_factory_make ("mfw_vpudecoder", "video-decoder");   decad        = gst_element_factory_make ("mad", "mp3-decoder");   vdsink        = gst_element_factory_make ("mfw_v4lsink",    "video-sink");   vdqueue      = gst_element_factory_make ("queue",            "video-queue");   adqueue      = gst_element_factory_make ("queue",            "audio-queue");   adsink        = gst_element_factory_make ("fakesink",        "audio-sink");   g_object_set (decvd, "codec-type", "std_avc", NULL);   if (!pipeline || !source || !demuxer || !decvd || !decad || !vdsink || !vdqueue || !adqueue || !adsink) {     g_printerr ("One element could not be created. Exiting.\n");     return -1;   }   /* Set up the pipeline */   /* we set the input filename to the source element */   g_object_set (G_OBJECT (source), "location", argv[1], NULL);   /* we add a message handler */   bus = gst_pipeline_get_bus (GST_PIPELINE (pipeline));   gst_bus_add_watch (bus, bus_call, loop);   gst_object_unref (bus);   /* we add all elements into the pipeline */   /* file-source | ogg-demuxer | vorbis-decoder | converter | alsa-output */   gst_bin_add_many (GST_BIN (pipeline),                     source, demuxer, decvd, decad, adqueue, vdqueue, vdsink, adsink,  NULL);   /* we link the elements together */   /* file-source -> ogg-demuxer ~> vorbis-decoder -> converter -> alsa-output */   gst_element_link (source, demuxer);   gst_element_link (decvd, vdqueue);   gst_element_link (vdqueue, vdsink);   //gst_element_link (decad, adqueue);   gst_element_link (adqueue, adsink);   g_signal_connect (demuxer, "pad-added", G_CALLBACK (on_pad_added), NULL);   /* note that the demuxer will be linked to the decoder dynamically.     The reason is that Ogg may contain various streams (for example     audio and video). The source pad(s) will be created at run time,     by the demuxer when it detects the amount and nature of streams.     Therefore we connect a callback function which will be executed     when the "pad-added" is emitted.*/   /* Set the pipeline to "playing" state*/   g_print ("Now playing: %s\n", argv[1]);   gst_element_set_state (pipeline, GST_STATE_PLAYING);   /* Iterate */   g_print ("Running...\n");   g_main_loop_run (loop);   /* Out of the main loop, clean up nicely */   g_print ("Returned, stopping playback\n");   gst_element_set_state (pipeline, GST_STATE_NULL);   g_print ("Deleting pipeline\n");   gst_object_unref (GST_OBJECT (pipeline));   return 0; } Create a directory inside your ltib directory to compile your source code: $ mkdir ~/your-ltib-dir/rpm/BUILD/gst Enter on LTIB shell mode: $ ./ltib -m shell Entering ltib shell mode, type 'exit' to quit LTIB> Enter in your application dir: LTIB> cd rpm/BUILD/gst/ Compile your application: LTIB> gcc -Wall $(pkg-config --cflags --libs gstreamer-0.10) playvideo.c -o playvideo If everything worked file you will get a "playvideo" arm binary: LTIB> file playvideo playvideo: ELF 32-bit LSB executable, ARM, version 1 (SYSV), for GNU/Linux 2.6.14, dynamically linked (uses shared libs), not stripped Now just copy it to ~/your-ltib-dir/rootfs/home. Start your board using this rootfs and execute: root@freescale ~$ cd /home/ root@freescale /home$ ./playvideo your-file-h264-mp3.avi Now playing: your-file-h264-mp3.avi Running...
View full article
Here is a BDI3000 config file I used with a SABRE SD board sometimes ago that includes DDR initialization. I had several request on this in the past so I am placing it here in case anyone needs it. Please feel free to comment or update the document according to your own experience and results. Regards Sinan Akman
View full article
L5.4.3_1.0.0 release is now available on IMX_SW landing page: BSP Updates and Releases -> Linux ->Linux L5.4.3_1.0.0. Documentation -> Linux -> Linux 5.4.3_1.0.0 Documentation Files available: # Name Description 1 imx-yocto-LF_L5.4.3_1.0.0.zip i.MX L5.4.3_1.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 LF_v5.4.y-1.0.0_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6Solox Linux Binary Demo Files 3 LF_v5.4.y-1.0.0_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 LF_v5.4.y-1.0.0_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 LF_v5.4.y-1.0.0_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  6 LF_v5.4.y-1.0.0_images_MX8MMEVK.zip i.MX 8M Mini EVK Linux Binary Demo Files  7 LF_v5.4.y-1.0.0_images_MX8MNEVK.zip i.MX 8M Nano EVK Linux Binary Demo Files  8 LF_v5.4.y-1.0.0_images_MX8MQEVK.zip i.MX 8M Quad EVK Linux Binary Demo files 9 LF_v5.4.y-1.0.0_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 LF_v5.4.y-1.0.0_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.10.1.tar.gz System Controller Firmware (SCFW) porting kit v1.2.10.1 for L5.4.3_1.0.0   Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 8M Nano EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board   What’s New/Features: Please consult the Release Notes.   Known Issues: For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-zeus ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-zeus      
View full article
You can create GTK applications manually—this is just like creating Graphics Java Applications. It uses a similar layout idea! Copy this example and save as helloworld.c: /* example-start helloworld helloworld.c */ #include <gtk/gtk.h> /* This is a callback function. The data arguments are ignored * in this example. More on callbacks below. */ void hello( GtkWidget *widget, gpointer   data ) {    g_print ("Hello World\n"); } gint delete_event( GtkWidget *widget, GdkEvent  *event,  gpointer   data ) {    /* If you return FALSE in the "delete_event" signal handler,     * GTK will emit the "destroy" signal. Returning TRUE means     * you don't want the window to be destroyed.     * This is useful for popping up 'are you sure you want to quit?'     * type dialogs. */    g_print ("delete event occurred\n");    /* Change TRUE to FALSE and the main window will be destroyed with     * a "delete_event". */    return(TRUE); } /* Another callback */ void destroy( GtkWidget *widget, gpointer   data ) {    gtk_main_quit(); } int main( int   argc, char *argv[] ) {    /* GtkWidget is the storage type for widgets */    GtkWidget *window;    GtkWidget *button;       /* This is called in all GTK applications. Arguments are parsed     * from the command line and are returned to the application. */    gtk_init(&argc, &argv);       /* create a new window */    window = gtk_window_new (GTK_WINDOW_TOPLEVEL);       /* When the window is given the "delete_event" signal (this is given     * by the window manager, usually by the "close" option, or on the     * titlebar), we ask it to call the delete_event () function     * as defined above. The data passed to the callback     * function is NULL and is ignored in the callback function. */    gtk_signal_connect (GTK_OBJECT (window), "delete_event",                        GTK_SIGNAL_FUNC (delete_event), NULL);       /* Here we connect the "destroy" event to a signal handler.      * This event occurs when we call gtk_widget_destroy() on the window,     * or if we return FALSE in the "delete_event" callback. */    gtk_signal_connect (GTK_OBJECT (window), "destroy",                        GTK_SIGNAL_FUNC (destroy), NULL);       /* Sets the border width of the window. */    gtk_container_set_border_width (GTK_CONTAINER (window), 10);       /* Creates a new button with the label "Hello World". */    button = gtk_button_new_with_label ("Hello World");       /* When the button receives the "clicked" signal, it will call the     * function hello() passing it NULL as its argument.  The hello()     * function is defined above. */    gtk_signal_connect (GTK_OBJECT (button), "clicked",                        GTK_SIGNAL_FUNC (hello), NULL);       /* This will cause the window to be destroyed by calling     * gtk_widget_destroy(window) when "clicked".  Again, the destroy     * signal could come from here, or the window manager. */    gtk_signal_connect_object (GTK_OBJECT (button), "clicked",                               GTK_SIGNAL_FUNC (gtk_widget_destroy),                               GTK_OBJECT (window));       /* This packs the button into the window (a gtk container). */    gtk_container_add (GTK_CONTAINER (window), button);       /* The final step is to display this newly created widget. */    gtk_widget_show (button);       /* and the window */    gtk_widget_show (window);       /* All GTK applications must have a gtk_main(). Control ends here     * and waits for an event to occur (like a key press or     * mouse event). */    gtk_main ();       return(0); } /* example-end */
View full article
Hello i.MX Community. Attached there is a guide on How to Use an Older Uboot version with 3.1x.xx Kernel Version I hope you find the document and Sample provided useful! Regards!
View full article
Video Streaming over Ethernet This section shows how to stream a video over Ethernet using UDP and RTP. Be sure to have the newest gst-plugin-good installed to ensure the best streaming quality. Define the environment variable HOST with the ip address of the receiver machine (that one that will show the video). $ export HOST=XX.XX.XX.XX Do you know how to get caps? i.MX 27 Video GST Caps H264 (MX->PC) in i.MX27: gst-launch-0.10 -v mfw_v4lsrc capture-width=640 capture-height=480 ! mfw_vpuencoder width=640 height=480  /     codec-type=std_avc ! rtph264pay ! udpsink host=$HOST port=5000 in PC: gst-launch-0.10 -v --gst-debug=2 udpsrc port=5000 /   caps ="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, /   profile-level-id=(string)42001e, sprop-parameter-sets=(string)Z0IAHqaAoD2Q, payload=(int)96, /   ssrc=(guint)3296222373, clock-base=(guint)2921390826, seqnum-base=(guint)35161" ! /   rtph264depay  ! ffdec_h264 ! autovideosink MPEG4 (MX->PC) in i.MX27 gst-launch-0.10 -v mfw_v4lsrc capture-width=352 capture-height=288 ! mfw_vpuencoder width=352 height=255 bitrate=64 codec-type=std_mpeg4 ! rtpmp4vpay send-config=true / ! udpsink host=10.29.244.32 port=5000 Set send-config to true to send configuration with the video. Ensures better deconding PC gst-launch-0.10 -v --gst-debug=2 udpsrc port=5000 caps ="application/x-rtp, media=(string)video, clock-rate=(int)90000, / encoding-name=(string)MP4V-ES, profile-level-id=(string)2, config=(string)000001b002000001b59113000001000000012000c888800f50b042414103, / payload=(int)96, ssrc=(guint)4006671474, clock-base=(guint)3714140954, seqnum-base=(guint)29742" / ! rtpmp4vdepay ! ffdec_mpeg4 ! autovideosink MPEG4 (MX->MX) Sender gst-launch-0.10 -v mfw_v4lsrc capture-width=640 capture-height=480 ! mfw_vpuencoder width=640 height=480  codec-type=std_mpeg4 ! rtpmp4vpay send-config=true ! udpsink host=$HOST port=5000 Receiver gst-launch-0.10 -v udpsrc port=5000 caps= "application/x-rtp, media=(string)video, clock-rate=(int)90000, / encoding-name=(string)MP4V-ES, profile-level-id=(string)4, config=(string)000001b004000001b59113000001000000012000c888800f514043c14103, / payload=(int)96, ssrc=(guint)907905085, clock-base=(guint)2029414707, seqnum-base=(guint)22207" ! rtpmp4vdepay ! / mfw_vpudecoder codec-type= std_mpeg4 min_latency=true ! mfw_v4lsink sync=false   Setting min_latency true gives the better latency for the streaming H264 (MX->MX) Sender gst-launch-0.10 -v mfw_v4lsrc capture-width=640 capture-height=480 ! mfw_vpuencoder width=640 height=480  codec-type=std_avc ! rtph264pay ! udpsink host=10.29.240.51 port=5000 Receiver gst-launch-0.10 -v udpsrc port=5000 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000" ! rtph264depay ! mfw_vpudecodr codec-type=std_avc ! mfw_v4lsink sync=false
View full article
Hello Community, Freescale’s MFG Tool Updated for Windows Embedded Compact and i.MX6 Platform TES Electronic Solutions (India) Private Limited has updated Freescale MFG tool for Windows Embedded Compact (7/2013) The Tool is tested on TES Electronic solution’s “MAGIK2 Evaluation Board” And Freescale’s “Saber SD” Evaluation Board www.tes-dst.com Thanks, Misbah
View full article
In our document there is about how to fuse in the u-boot, as follows you can see: Here we can use the mfgtool and these command to download the fuse to u-boot. 1/ Set the BOOT_MODE[1:0] to 00 2/Use the mfgtool to download the u-boot to RAM Use the mfgtool to download only the u-boot, so you have to annotate the code not about u-boot. Only u-boot download code left. As follows:  …………    Loading uboot.  Jumping to OS image. 3/When the u-boot boot up, print and go to the u-boot command line. U-Boot contains a tool, imxotp, which is used for fusing. The commands imxotp read addr and imxotp blow --force addr value read the data of Efuse. The addr is the register address of eFUSE, and the base address of eFUSE is 0x021BC0000, details you can refer to the section 46 of the iMX6DQRM.pdf p4016. And the The exact configuration please refer to the section 5 of the iMX6DQRM.pdf p315. Take the Sabrelite as an example the value of burning : imxotp blow --force 0x5 0x18000030 imxotp blow --force 0x6 0x10 Hope this can do some hope for you. About the efuse you also can refer to : https://community.nxp.com/thread/316232 
View full article
Check memory leakage in media server. Set libc debug level. So libc will record back trace for all memory allocate. setprop libc.debug.malloc 1 Kill mediaserver to let the libc debug take effect. Android will restart mediaserver. busybox killall -HUP mediaserver you will see below log if you setting right. I/libc    ( 3074): /system/bin/mediaserver using MALLOC_DEBUG = 1 (leak checker) Dump all used memory of mediaserver. dumpsys media.player -m Allocation count 297 Total memory 1483423 size   262144, dup    1, 0x401f4c18, 0x400b6152, 0x401a6568, 0x4061a95c, 0x40146cfa, 0x4019639c, 0x40146ec2, 0x4014a1ec, 0x4014a3ca, 0x00008a98, 0x400b67aa size   178192, dup    1, 0x401f4c18, 0x400b6152, 0x4280adae, 0x427ffcee, 0x4280ae6c, 0x427ec75a, 0x427f7e22, 0x42807648, 0x428082ea, 0x415144f0, 0x4151334a, 0x413381d0, 0x401dcbc, 0x401d438c, 0x4014d996, 0x405c3c46, 0x405c7516, 0x405c6ad4, 0x412c02ca, 0x412c0584, 0x4108c64c, 0x4107d622, 0x4107fbf2, 0x4107c19a, 0x400b2eac, 0x400b2a00 Diff two times of memory dump to check if there is any memory leakage. You can playback one video file between the dump. diff 1.txt 2.txt > diff.txt Get maps file of mediaserver. adb pull proc/<pid of mediaserver>/maps . Use attached script to map back trace to function symbols and file line. ./addr2func.py --root-dir=../../ --maps-file=./maps --product=sabresd_6dq diff.txt Notes: should use eng build for the debug.
View full article
Description       This doc explain how to enable the plugin boot on i.MX6Q/6DL and which used for change the pll2 clock and add the spread spectrum support to pass the EMI test. we still list the source codes of 3.0.35 and 4.1.15. to explain the dts/non-dts kernel support.       本文旨在说明如何在i.MX6Q/6DL上实现plugin启动,以支持展频和改变pll2的频率,其目的是为了通过 EMI测试。也附上了基于3.0.35和4.1.15的源代码,以供参考   Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 SabreSDP https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false          Version: MX6Q_PLUGIN_FC_SSC_V7-20200915_chn..pdf(chinese version)add baidou support MX6Q_PLUGIN_FC_SSC_V7-20170504_eng-chapter-imx6dl.doc+MX6Q_PLUGIN_FC_SSC_V3-20170309_eng.doc(english version)      
View full article
Although you can develop your own driver to control GPIOs inside kernel space, there is a much simpler way for accessing GPIOs from user space. When timing requirements are not an issue, you are able to use GPIO-SYSFS. SYSFS is a virtual file system that exports some kernel internal framework functionalities to user space and GPIO is one of the frameworks that can have functionalities exported through SYSFS. The GPIO-SYSFS feature is available in all mainline kernels from 2.6.27 onwards. Configuring Kernel to export GPIO through SYSFS To enable GPIO in SYSFS, select the following kernel option: Device Drivers --->       --- GPIO Support             [*] /sys/class/gpio/... (sysfs interface) If you are using i.MX233 or i.MX28, after recompiling the kernel, do not forget to generate boot streams again, because this is not automatic even in ltib. Be sure that the pins you will try to use are really accessible as GPIO pins and were not requested by the kernel (gpio_request). If pin was gpio_request'ed, you will need to gpio_export the same pin inside the kernel in order to have it accessible through SYSFS. If pin is not set as GPIO by default, you will need to set IO MUX in the proper file inside <kernel>/arch/arm/mach-XXX. Accessing GPIO in user space After enabling GPIO-SYSFS feature, you can boot your device with the new kernel to make some tests. First you need to export the GPIO you want to test to the user space: echo XX > /sys/class/gpio/export XX shall be determined by the following algorithm: GPIOA_[B] is the GPIO you want to export, where "A" is the GPIO bank and "B" is the offset of the pin in the bank. if the first available GPIO bank is 0 // (iMX.28, for example)     XX = A*32 + B; else // first GPIO bank is 1     XX = (A-1)*32 + B; After exporting a GPIO pin, you shall be able to see the GPIO interface exported to: /sys/class/gpio/gpioXX Through this interface, you are now able to do things like: # Reading the pin value cat /sys/class/gpio/gpioXX/value # Changing pin direction echo in > /sys/class/gpio/gpioXX/direction echo out > /sys/class/gpio/gpioXX/direction # Toggling GPIO output level echo 0 > /sys/class/gpio/gpioXX/value echo 1 > /sys/class/gpio/gpioXX/value It is important to note that through the GPIO virtual filesystem it is only possible to deal with one GPIO pin at a time (per command).
View full article
Freescale does not have a specific GStreamer element to do JPEG encoding, so the standard 'jpegenc' should be used. Image Capture With a web camera gst-launch v4l2src num-buffers=1 ! jpegenc ! filesink location=sample.jpeg With an embedded camera gst-launch mfw_v4lsrc num-buffers=1 !  jpegenc ! filesink location=sample.jpeg More pipelines on GStreamer i.MX6 Pipelines
View full article