i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Starting from $52, the VAR-SOM-MX6 sets the bar for unparalleled design flexibility. The VAR-SOM-MX6 ensures scalable and simplified development, while also extending the product lifecycle. Thanks to four CPU core assembly options, customers can apply a single System on Module in a broad range of applications to achieve short time-to-market for their current innovations, while still accommodating potential R&D directions and marketing opportunities.     VAR-SOM-MX6 CPU: Freescale iMX6 Key features include: Freescale i.MX6 1.2GHz Quad / Dual / Single core Cortex-A9       2GB DDR3, 1GB SLC NAND Flash       Full HD 1080p video encoding/decoding capability       Vivante GPU providing 2D/3D acceleration       Simultaneous multiple display support       Gigabit Ethernet       TI WiLink™ 6.0 single-chip connectivity solution (Wi-Fi, Bluetooth®)       PCI-Express 2.0, S-ATA 3.0       Camera interface       USB 2.0: Host, OTG       Audio In/Out       Dual CAN Bus This versatile solution's -40 to 85°C temperature range and Dual CAN support is ideal for industrial applications, while 1080p video and graphics accelerations make it equally suitable for intensive multimedia applications. The impressive scalability of the VAR-SOM-MX6 satisfies the needs of the most demanding future application requirements whether faster processing power, enhanced algorithms or improved graphics and video performance to name just a few. The VAR-SOM-MX6 is an all-round solution with broad connectivity and sophisticated video and acceleration graphic capabilities, delivering a range of middle to high end assembly options all from the same product. For more details, please see VAR-SOM-MX6 CPU: Freescale iMX6
View full article
Hi, The document "How to create ubuntu hardfloat rootfs for imx6d/q" was shared by Junping Mao. https://community.freescale.com/docs/DOC-95185 However, some modification need to be made to build imx-tests on this rootfs. Attached please find the guide for building imx-tests on hf-ubuntu rootfs for imx6d/q. Any problems, pls feel free to let me know. Regards, Alvin zheng
View full article
The NXP i.MX 8M provides industry leading audio, voice and video processing for applications that scale from consumer home audio to industrial building automation and mobile computers. The i.MX 8M Quad supports multiple audio interfaces as listed below: Besides the general audio input/output function, the audio interfaces will supports following features: - SAI-1 supports up to 16-channels TX (8 lanes) and 16-channels RX (8 lanes) at 384KHz/32-bit. - SAI-5 supports up to 8-channels TX (4 lanes) and 8-channels RX (4 lanes) at 384KHz/32-bit. - SAI-2/3/6 supports up to 2-channels TX (1 lanes) and 2-channels RX (1 lanes) at 384KHz/32-bit. - SAI-2/3/6 support up to 2-channels TX (1 lane) and 2-channels RX (1 lane) at 384KHz/32-bit. - SAI-1 supports glue-less switching between PCM & DSD operation for popular audio DACs - SPDIF-1/2 supports raw capture mode that can save all the incoming bits into audio buffer The SAI-1/2/3/5/6 and SPDIF-1 share GPIO pads on the chip through IOMUX. Common use cases supported by the audio interfaces are listed in the table below (many other configurations are possible). The number is the data lanes supported. For the MCLK pin on each SAI module, it can be configured as either input or output. When configured as output, the SAI_CLK_ROOT from CCM will be routed to the pad output. When configured as input, the external input to the pad will be routed to SAI.MCLK, which can be used as master clock for SAI. Below is the diagram showing the both input/output options, by using SAI1 as the example. Each SAI module supports up to 3 master clock inputs. The TX and RX sub-module inside each SAI can independently select one of the clock inputs as its master clock. This allows TX and RX of one SAI to run from different clock source. The master clock inputs have following options: - SAI.MCLK[1] can be selected from SAI_CLK_ROOT from CCM or SAI.MCLK from IOMUX. This is the most straight-forward clock routing in which SAI only use its own clock source from CCM or IO pad. - SAI.MCLK[2] can be selected from following clock sources:       Any of the SAI_CLK_ROOT from CCM;       Any of the SAI.MCLK from IOMUX;       Other clock sources from SPIDF; - SAI.MCLK[3] has exact same clock source options as SAI.MCLK[2]. This allows both TX and RX can have access to all the options without any dependency between each other. The clock options for master clock on SAI are shown in the diagram blow, by using SAI-1 as an example. The options on MCLK[1] is also available on MCLK[2] and MCLK[3]. The reason to keep this options is to provide the similar SAI clock structure as i.MX6/i.MX7 processors. The configuration of the MUX for master clock are controlled by IOMUXC_GPR registers. They should be configured before SAI clock is enabled to avoid glitches on the clock. Note: Because those MUX on clocks are missed during the design, the actual implementation in the silicon is simplified as shown in the following diagram. All the SAI and SPDIF instances have SDMA support. In order to meet the audio data rate, two SDMA modules are used. Because the SAI-2/3 and SPDIF-1/2 do not require high data throughput, they are assigned to SDMA-1, shared with other peripherals such as UART/SPI. SAI-1/4/5/6 need to support high sample rate & multichannel audio, they are assigned to SDMA-2, which is a dedicated SDMA engine for audio. The SDMA-2 frequency is increased to 500/250 instead of 133/66 to make sure it has enough throughput. In order to allow SW tracking the progress of audio DMA, the TX_SYNC and RX_SYNC of SAI modules are routed to GPT as the external clock input. Since there are totally 6 SAI modules, these signals will be MUXed when connection to GPT. - GPT-4/5/6 external clock input can be selected from the TX_SYNC or RX_SYNC of any 6 SAI modules; - The MUX select is controlled by IOMUXC_GPR register; - The MUX select register for GPT-4/5/6 are fully independent of each other.
View full article
This is a copy of the currently posted i.MX 6DQ reference manual, revision 2, published Jun 2014.  This is part 1 of 2, and includes the first 43 chapters.  Go here for part 2: i.MX 6DQ Reference Manual (IMX6DQRM R2, Part 2) This document is to be used to enter community comments.  Please feel free to add inline comments in this reference manual. You can point out where more information is needed or where existing information is incorrect.  You can also enter information in your comment that expands on existing information in the document, based on your experience with the device.  If you are pointing out that more information is needed in a paragraph or a section, please be very specific, not “needs more information”.  Your comments in this manual may help other members and will drive improvements in this and future documentation. Note: The doc viewer does not support going directly to a specified page.  Instead of manually paging through one page at a time, you can do a search on a string on a page such as "types of resets", or you can go to chapter links listed in the inline comments.  To do this, page down to the comments below the doc view, select "Inline Comments", sort the comments by "page", and then select the chapter you want to view. You may find it easier to use this manual by downloading and viewing it in your local Adobe Reader.  Then when you have a comment/question to add to this review copy, navigate to the chapter as described above and then do a search on the text for which you want to add a comment.  This will take you to that page the quickest.
View full article
ADB ADB is a tool for Android debugging. With ADB, you can install applications from you PC, copy files to/from your device, access console. You can access your device using an USB Cable, or through network (using an IP address). You can take ADB from SDK [1] or inside <my_android>/out/host/linux-x86/bin/adb I cannot see my device First checkpoint must be for ADBD. It´s the ADB daemon, and if it´s not running on your device, you will not be able to access it. Install and configure any USB driver [2] [3] Double check connection (USB cable, ethernet) Double check if debugging is on Double check if USB config is right (see how on User Guide) Tips and Tricks Turning on Remember to turn debugging mode on: Settings->Applications->Development->USB debugging No Permission When you get "no permissions" from ADB, you need to start server with your root user: $ sudo /usr/share/android-sdk-linux_86/tools/adb devices List of devices attached ????????????    no permissions $ sudo /usr/share/android-sdk-linux_86/tools/adb shell error: insufficient permissions for device $ sudo /usr/share/android-sdk-linux_86/tools/adb kill-server $ sudo /usr/share/android-sdk-linux_86/tools/adb start-server * daemon not running. starting it now * * daemon started successfully * $ sudo /usr/share/android-sdk-linux_86/tools/adb devices List of devices attached 0123456789ABCDEF    device $ sudo /usr/share/android-sdk-linux_86/tools/adb shell # ls dev etc
View full article
First execute LTIB (./ltib -c) and select these packages: all gstreamer plugin, alsa-utils and libmad. Create your file code (i.e.: playmp3.c): #include <gst/gst.h> #include <glib.h> static gboolean   bus_call (GstBus    *bus,             GstMessage *msg,             gpointer    data) {   GMainLoop *loop = (GMainLoop *) data;   switch (GST_MESSAGE_TYPE (msg)) {           case GST_MESSAGE_EOS:               g_print ("End of stream\n");               g_main_loop_quit (loop);               break;           case GST_MESSAGE_ERROR: {               gchar  *debug;               GError *error;               gst_message_parse_error (msg, &error, &debug);               g_free (debug);               g_printerr ("Error: %s\n", error->message);               g_error_free (error);               g_main_loop_quit (loop);               break;         }         default:           break;     }     return TRUE; } int main (int  argc,               char *argv[]) {       GMainLoop *loop;       GstElement *pipeline, *source, *decoder, *conv, *resample, *sink;       GstBus *bus;       /* Initialisation */       gst_init (&argc, &argv);       loop = g_main_loop_new (NULL, FALSE);       /* Check input arguments */       if (argc != 2) {           g_printerr ("Usage: %s <MP3 filename>\n", argv[0]);           return -1;       }         /* Create gstreamer elements */       pipeline = gst_pipeline_new ("audio-player");       source  = gst_element_factory_make ("filesrc",      "file-source");       decoder  = gst_element_factory_make ("mad",      "mp3-decoder");       conv    = gst_element_factory_make ("audioconvert",  "converter");       resample = gst_element_factory_make ("audioresample", "audio-resample");       sink    = gst_element_factory_make ("autoaudiosink", "audio-output");       if (!pipeline || !source || !decoder || !conv || !resample || !sink) {           g_printerr ("One element could not be created. Exiting.\n");           return -1;       }       /* Set up the pipeline */       /* we set the input filename to the source element */       g_object_set (G_OBJECT (source), "location", argv[1], NULL);         /* we add a message handler */         bus = gst_pipeline_get_bus (GST_PIPELINE (pipeline));         gst_bus_add_watch (bus, bus_call, loop);         gst_object_unref (bus);         /* we add all elements into the pipeline */         /* file-source | mp3-decoder | converter | resample | alsa-output */         gst_bin_add_many (GST_BIN (pipeline),                                                       source, decoder, conv, resample, sink, NULL);           /* we link the elements together */           /* file-source -> mp3-decoder -> converter -> resample -> alsa-output */           gst_element_link_many (source, decoder, conv, sink, NULL);         /* Set the pipeline to "playing" state*/         g_print ("Now playing: %s\n", argv[1]);         gst_element_set_state (pipeline, GST_STATE_PLAYING);         /* Iterate */       g_print ("Running...\n");       g_main_loop_run (loop);         /* Out of the main loop, clean up nicely */         g_print ("Returned, stopping playback\n");       gst_element_set_state (pipeline, GST_STATE_NULL);       g_print ("Deleting pipeline\n");       gst_object_unref (GST_OBJECT (pipeline));           return 0; } Create a directory inside your ltib directory to compile your source code: $ mkdir ~/your-ltib-dir/rpm/BUILD/gst Enter on LTIB shell mode: $ ./ltib -m shell Entering ltib shell mode, type 'exit' to quit LTIB> Enter in your application dir: LTIB> cd rpm/BUILD/gst/ Compile your application: LTIB> gcc -Wall $(pkg-config --cflags --libs gstreamer-0.10) playmp3.c -o playmp3 If everything worked file you will get a "playmp3" arm binary: LTIB> file playmp3 playmp3: ELF 32-bit LSB executable, ARM, version 1 (SYSV), for GNU/Linux 2.6.14, dynamically linked (uses shared libs), not stripped Now just copy it to ~/your-ltib-dir/rootfs/home. Start your board using this rootfs and execute: root@freescale ~$ cd /home/ root@freescale /home$ ./playmp3 your-file.mp3 Now playing: your-file.mp3 Running...
View full article
Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of Tsinghua University. Preparations 1. Installing Ubuntu16.04.2 LTS Customer can download ubuntu-16.04.2-desktop-amd64.iso from https://www.ubuntu.com/download/desktop Then install it to VMware workstation player v12 or PC, after finishing installation, use “Software Update” to update system. In order to compile android9.0.0-2.0.0 BSP, necessary packages should also be installed on Ubuntu 16.04. $ sudo apt-get install gnupg $ sudo apt-get install flex $ sudo apt-get install bison $ sudo apt-get install gperf $ sudo apt-get install build-essential $ sudo apt-get install zip $ sudo apt-get install zlib1g-dev $ sudo apt-get install libc6-dev $ sudo apt-get install lib32ncurses5-dev $ sudo apt-get install x11proto-core-dev $ sudo apt-get install libx11-dev $ sudo apt-get install lib32z1-dev $ sudo apt-get install libgl1-mesa-dev $ sudo apt-get install tofrodos $ sudo apt-get install python-markdown $ sudo apt-get install libxml2-utils $ sudo apt-get install xsltproc $ sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 $ sudo apt-get install gcc-multilib g++-multilib $ sudo apt-get install subversion $ sudo apt-get install openssh-server openssh-client $ sudo apt-get install uuid uuid-dev $ sudo apt-get install zlib1g-dev liblz-dev $ sudo apt-get install liblzo2-2 liblzo2-dev $ sudo apt-get install lzop $ sudo apt-get install git-core curl $ sudo apt-get install u-boot-tools $ sudo apt-get install mtd-utils $ sudo apt-get install android-tools-fsutils $ sudo apt-get install openjdk-8-jdk $ sudo apt-get install device-tree-compiler $ sudo apt-get install gdisk $ sudo apt-get install liblz4-tool $ sudo apt-get install m4 $ sudo apt-get install libz-dev More detail, see Android_User’s_Guide.pdf ( android 9.0.0-2.0.0 BSP documents) 2. Downloading and unpacking Android release package [ For android 9.0.0_2.2.0, see commemts, please!] https://www.nxp.com/support/developer-resources/evaluation-and-developmentboards/ sabre-development-system/android-os-for-i.mx-applicationsprocessors: IMXANDROID?tab=Design_Tools_Tab -- P9.0.0_2.0.0_GA_ANDROID_SOURCE File name is imx-p9.0.0_2.0.0-ga.tar.gz # cd ~ # tar xzvf imx-p9.0.0_2.0.0-ga.tar.gz Downloading Android 9.0.0-2.0.0 source code 1. Getting repo # cd ~ # mkdir bin # cd bin # curl https://mirrors.tuna.tsinghua.edu.cn/git/git-repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin 2. Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL = ' https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/ ' 3、Setting email address # git config --global user.email "[email protected]" # git config --global user.name "xxxx" [ Email & Name should be yours] 4、Modifying android setup script and Running it Open ~/imx-p9.0.0_2.0.0-ga/imx_android_setup.sh and add a line like below: ... ... if [ "$rc" != 0 ]; then echo "---------------------------------------------------" echo "-----Repo Init failure" echo "---------------------------------------------------" return 1 fi find -name 'aosp-p9.0.0_2.0.0-ga.xml'| \ xargs perl -pi -e 's|https://android.googlesource.com/|https://aosp.tuna.tsinghua.edu.cn/|g' fi ... ... Then save it and exit. # cd ~/ # source ~/imx-p9.0.0_2.0.0-ga/imx_android_setup.sh Then android_build directory is created at ~/ If fetching errors occur, like below, run “repo sync” again. # repo sync # export MY_ANDROID=~/android_build [Note] imx_android_setup.sh will be in charge of downloading all android source code. 5.Begin to compile android 9.0.0-2.0.0 BSP $ export ARCH=arm64 $ export CROSS_COMPILE=${MY_ANDROID}/prebuilts/gcc/linuxx86/aarch64/aarch64-linuxandroid-4.9/bin/aarch64-linux-android- $ cd ~/android_build/vendor $ cp -r ~/imx-p9.0.0_2.0.0-ga/vendor/* ./ $ cd ~/android_build $ source build/envsetup.sh $ lunch evk_8mm-userdebug $ make –j4 NXP TIC team Weidong sun 2019-05-05
View full article
Structures to be modified The main table that needs to be modified is in C:\WINCE600\PLATFORM\COMMON\SRC\SOC\COMMON_FSL_V2_PDK1_9\NAND\INC\NANDTYPES.h. Add the Nand specific information to the following structure. typedef struct _NandChipInfo { FlashInfo fi; //@<<info> FlashInfo structure BYTE NANDCode[NANDID_LENGTH];//@<<info> NAND full ID BYTE NumBlockCycles; //@<<info> flash erase address cycle BYTE ChipAddrCycleNum; //@<<info> flash access address cycle BYTE DataWidth; //@<<info> 8/16 bits data width BYTE BBMarkNum; //@<<info> MAX_MARK_NUM = 4 BYTE BBMarkPage[MAX_MARK_NUM];//@<<info> MAX_MARK_NUM = 4 BYTE StatusBusyBit; //@<<info> interleave mode support BYTE StatusErrorBit; //@<<info> interleave mode support WORD SpareDataLength; //@<<info> spare area size BYTE CmdReadStatus; //@<<command> read status BYTE CmdRead1; //@<<command> read first 256 bytes data BYTE CmdRead2; //@<<command> read last 256 bytes data BYTE CmdReadId; //@<<command> read device ID BYTE CmdReset; //@<<command> reset nand flash BYTE CmdWrite1; //@<<command> sequence data input BYTE CmdWrite2; //@<<command> page program BYTE CmdErase1; //@<<command> block erase BYTE CmdErase2; //@<<command> block erase NANDTiming timings; //@<<info> NAND timing parameters }NandChipInfo, *pNandChipInfo; All information from NANDCode to CmdErase2, can be obtained from the Nand Datasheet. The structure FlashInfo, is filled in with data obtained from the Nand Analysis sheet. Please check this link to see how to create this spreadsheet from Nand Datasheets. typedef struct _FlashInfo { FLASH_TYPE flashType; DWORD dwNumBlocks; DWORD dwBytesPerBlock; WORD wSectorsPerBlock; WORD wDataBytesPerSector; }FlashInfo, *PFlashInfo; In the similar way the Nand timings calculated from the spreadsheet are add into this structure. typedef struct _NANDTiming { BYTE DataSetup; BYTE DataHold; BYTE AddressSetup; BYTE DataSample; }NANDTiming, *PNANDTiming; Remember to do a clean sysgen and build.
View full article
Hi All, The new i.MX 6 Q/D/DL/S/SL L3.0.35_4.1.0 GA release is now available on the http://www.freescale.com/site. ·         Files available                                   # Name Description 1 L3.0.35_4.1.0_LINUX_DOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP   Documentation. Includes Release Notes, Reference Manual, User guide. API   Documentation 2 L3.0.35_4.1.0_LINUX_MMDOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Multimedia Codecs Documentation.   Includes CODECs Release Notes and User's Guide 3 L3.0.35_4.1.0_SOURCE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP   Source Code Files 4 L3.0.35_4.1.0_MM_CODECS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Multimedia Codecs Sources 5 L3.0.35_4.1.0_AACP_CODECS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux AAC Plus Codec 6 L3.0.35_4.1.0_DEMO_IMAGE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Binary Demo Files 7 L3.0.35_4.1.0_UBUNTU_RFS_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux File System for the Ubuntu Images 8 i.MX_6D/Q_Vivante_VDK_146_Tools Set   of applications for the Linux L3.0.35_4.1.0 BSP, designed to be used by   graphics application developers to rapidly develop and port graphics   applications. Includes applications, GPU Driver with vprofiler enabled and   documentation. 9 IMX_6DL_6S_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6DualLite and i.MX   6Solo. 10 IMX_6DQ_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6Quad and i.MX 6Dual. 11 IMX_6SL_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6Sololite. ·         Target HW boards o   i.MX 6Quad SABRE-SDP o   i.MX 6Quad SABRE-SDB o   i.MX 6Quad SABRE-AI o   i.MX 6DualLite SABRE-SDP o   i.MX 6DualLite SABRE-AI o   i.MX 6SL EVK ·         New features o   BSP New Features on i.MX 6D/Q, i.MX 6DL/S and MX 6SL: §  HDCP §  CEC §  GPU4.6.9p12 §  Audio playback IRAM/SDMA §  V4L capture resize on MX6SL §  MX6DQ disable the double line fill feature of PL310 ·         Known issues o   For known issues and limitations please consult the release notes.
View full article
Descriptions on the issue: running “uuu uuu-android-mx8mq-evk-emmc.lst” No any problem, downloading images is OK. running “uuu_imx_android_flash.bat -f imx8mq -a -e” Below lines will be showed on windows console: flash the file of u-boot-imx8mq.imx to the partition of bootloader0 <waiting for any devices>             Then downloading operation stopped. ------------------------------------------------------------------------                 In order to help uses save development time, I tested above 2 commands for downloading images on windows 7 64bit and windows 10 64bit respectively.                 Below is detailed steps for the operation: Hardware Preparations (1) Switch SW802 on i.MX8MQ EMEK, set 1-4 off, 2-3 on i.MX8MQ is at usb serial download mode. (2) Connecting J1701 to PC USB by a USB OTG cable. (3) Connecting J901(usb type c) to PC USB by a USB 3.0 cable. (4) Plugging [email protected] adapter into Power Jack (J902) (5) Power on I.MX8MQ board via SW701 Switch Software Preparations (1) Related windows drivers for i.MX8MQ MEK                 Windows 7 64bit or windows 10 64bit will find new devices and begin to search and install corresponding drivers, like below:                 Probably windows 10 64bit can’t automatically install CP2105 driver from official website of manufacture: https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers                 Then installed it manually. (2) Power off i.MX8MQ MEK (3) Installing winusb driver by zadig                 According to method described in uuu.pdf, download zadig tool from https://zadig.akeo.ie/, and install it to windows 7 64bit . [Note] windows 10 64bit doesn’t need to install winusb driver. Press “Install WCID Driver” Button (4) Downloading Android SDK Manager Download SDK Manager from : http://visualgdb.com/android/install_redir?item=SDK After downloading it, decompress it, and run SDK Manager application: Press OK. Then press “Close” Close SDK Manager Installation Guide . Find the directory of SDK Manager installation, and enter into “platform-tools”, like below: D:\i.MX8-Projects\IMX8MQ-MEK-windows-drivers\android-sdk_r24.4.1-windows\android-sdk-windows\platform-tools Copy items in blue rectangle to C:\windows\system Copy items in red rectangle to C:\windows\system32     Beginning to download android images to I.MX8MQ MEK via UUU Tool (1) Downloading android DEMO images for i.MX8MQ MEK https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/evaluation-kit-for-the-i.mx-8m-applications-processor:MCIMX8M-EVK?tab=Design_Tools_Tab After downloading it, decompress it to a directory.  Like below: (2) Downloading UUU Tool https://github.com/NXPmicro/mfgtools/releases After downloading uuu.exe,  copy it to the directory of android 9.0 demo image , see above. (3) Run command “uuu_imx_android_flash.bat -f imx8mq -a -e” ----Power on i.MX8MQ MEK. ----open a command line window ---open Hyper terminal ( set it 115200 bps) ---run “uuu_imx_android_flash.bat -f imx8mq -a -e”           For windows 10 64bit, downloading images will be done without any errors.    But for windows 7 64bit, downloading images will stop at “ waiting for any devices”.    It means Android ADB driver will be needed. Follow the steps below to solve the problem. Right button, click “update driver” Close it.           Then downloading operations will be automatically continued. OK, done. NXP TIC team Weidong Sun 02-25-2019
View full article
The i.MX 6 D/Q/DL/S/SL Linux 3.10.17_1.0.0 GA release is now available on www.freescale.com Files available Name Description L3.10.17_1.0.0_LINUX_DOCS i.MX 6 D/Q/DL/S/SL Linux 3.10.17_1.0.0 GA BSP documentation. y L3.10.17_1.0.0_iMX6QDLS_Bundle i.MX 6 D/Q/DL/S  Linux 3.10.17_1.0.0 GA BSP Binary Demo Files L3.10.17_1.0.0_iMX6SL_Bundle i.MX 6 SL  Linux 3.10.17_1.0.0 GA BSP Binary Demo Files i.MX_6_Vivante_VDK_150_Tools Vivante VTK 1.5 Codec for the i.MX 6 D/Q/DL/S/SL Linux 3.10.17_1.0.0 GA BSP    y L3.10.17_1.0.0_AACP_CODECS AAC Plus Codec for the i.MX 6 D/Q/DL/S/SL Linux 3.10.17_1.0.0 GA BSP y IMX_6_MFG_L3.10.17_1.0.0_TOOL Manufacturing Tool and Documentation for Linux 3.10.17_1.0.0 GA BSP y Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board New  Features o   Main BSP New Features on MX6DQ, MX6DL and MX6SL from L3.10.9_1.0.0 GA: SD3.0 reset USB HSIC HWRNG security feature on MX6SL VIIM OTP Fuse in uboot Battery charge LED U-boot USB mass storage support USB Camera on host mode X backend: Adaptive HDMI display support backed by XRandR Main Codec New Features on MX6DQ, MX6DL and MX6SL from L3.10.17_1.0.0 Beta: Bug fix Main Codec New Features on MX6DQ, MX6DL and MX6SL from L3.10.17_1.0.0 Beta: Bug fix Other features not supported found during testing: UART: only support some baud rates like 9600, 115200, can't support high to 4000000 Known issues For known issues and limitations please consult the release notes located in the BSP documentation package.
View full article
Enabling Dual Display in Ubuntu with the i.MX53 Quick Start Board Here you will learn how to enable two displays in a Ubuntu system running in an iMX53 Quick Start Board. We assume here that you already have a micro SD card with a valid Ubuntu image (including uboot, Linux kernel and Ubuntu filesystem). You can use the original SD card that comes with the i.MX53 Quick Start Board, which brings an image of Ubuntu or, if you do not have the original SD card, you can reproduce it by downloading Ubuntu binaries package (L2.6.35_MX53_ER_1101_IMAGE) from Freescale iMX53qsb download area. You will also need to update U-boot and kernel binaries in the SD card with more recent images. You can find the most recent binaries (L2.6.35_MX53_ER_1109_IMAGE_) from Freescale iMX53qsb download area as well. Introduction To enable dual display, you need to perform two tasks: Enable two displays at kernel level Configure your Xorg server accordingly Enabling Two Displays at Kernel Level To enable two displays at kernel level means to map one display interface to fb0 device and the other to fb1 device. So first thing is to choose which interface will be the primary one, mapped as fb0. As an example, we consider the VGA interface as primary in this tutorial. Second thing is to choose one of the other available external video interfaces to be secondary, mapped as fb1 device in the system. We consider the 4.3" seiko LCD display in this tutorial as the secondary interface. Once chosen primary and secondary interfaces, we need to configure kernel video arguments accordingly. The arguments are available in specific variables in the U-boot that comes with the Ubuntu binaries. You can see them (HDMI, VGA, etc.) by printing the U-boot environment variables from the U-boot shell, but you will probably not find those variables in other versions of U-boot and their contents will probably need to be adapted to the kernel version in use, as arguments recognized by kernel modules varies considerably between kernel versions. You can always refer to the Linux Release Notes documents for video arguments. It's available for each Linux BSP that can be found on the Freescale website. For the 1109 BSP, we have the following video arguments (extracted from i.MX53_START_Linux_BSP_Release_Note.pdf that comes with L2.6.35_11.09.01_ER_docs.tar.gz downloaded from here - IMX53_1109_LINUXDOCS_BUNDLE😞 VGA: video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga SEIKO LCD: video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary Both are considered primary, because these are the arguments for single display setups. Now that we have video arguments for both desired interfaces, we only need to merge them together removing the primary argument from the one that is the secondary. In our case, we need to pass the following arguments to the kernel: video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga video=mxcdi0fb:RGB24,SEIKO-WVGA For this, we can add these arguments to one of the variables that are used in the boot process. We can add the content to bootarg_base, for instance. In the U-boot command line, execute following commands to setup the environment: setenv vga_and_seiko 'video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga video=mxcdi0fb:RGB24,SEIKO-WVGA' setenv bootargs_base 'setenv bootargs console=ttymxc0,115200 vga_and_seiko' saveenv After applying a reset and booting the board, you shall have both interfaces enabled, but the secondary will not be used by the Xorg server until we complete the next step. Configuring Xorg Server Now that we have two video interfaces properly configured and mapped to /dev/fb0 and /dev/fb1 devices, we need to tell Xorg server how to use them. Here is an example of xorg.conf file that you can use to replace the default one, found at /etc/X11: Section "InputDevice" Identifier     "Generic Keyboard" Driver          "kbd" Option          "XkbRules"     "xorg" Option          "XkbModel"     "pc105" Option          "XkbLayout"     "us" EndSection  Section "InputDevice" Identifier     "Configured Mouse" Driver          "mouse" Option          "CorePointer" EndSection  Section "Device" Identifier     "i.MX Accelerated Framebuffer Device 0" Driver          "imx" Option          "fbdev"               "/dev/fb0"  # This option only recognized when "mxc_epdc_fb" frame buffer driver in # use.  Values are "RGB565" (default, 16-bit RGB), "Y8" (8-bit gray), # and "Y8INV" (8-bit gray inverted). Option          "FormatEPDC"               "Y8INV"  EndSection  Section "Device" Identifier     "i.MX Accelerated Framebuffer Device 1" Driver          "imx" Option          "fbdev"               "/dev/fb1"  EndSection  Section "Monitor" Identifier     "Configured Monitor 0" EndSection  Section "Monitor" Identifier     "Configured Monitor 1" EndSection  Section "Screen" Identifier     "Screen 0" Monitor          "Configured Monitor 0" Device          "i.MX Accelerated Framebuffer Device 0"  # These "Display" SubSection's are needed for working with the # "mxc_epdc_fb" frame buffer driver. SubSection     "Display" Depth     8 Visual     "StaticGray" EndSubSection SubSection     "Display" Depth     16 Visual     "TrueColor" EndSubSection EndSection  Section "Screen" Identifier     "Screen 1" Monitor          "Configured Monitor 1" Device          "i.MX Accelerated Framebuffer Device 1" EndSection  Section "ServerLayout" Identifier     "Xinerama Layout" Screen          "Screen 0" Screen          "Screen 1" RightOf "Screen 0" EndSection  Section "ServerFlags" Option          "Xinerama"          "true" EndSection Results The following picture shows the i.MX 53 QSB running the extended desktop previously configured. You can see the VGA monitor with a Firefox instance and the SEIKO LCD display with a calc instance.
View full article
The lastest iMX28 WinCE 6.0 BSP "WCE600_MX28_SDK1008" has a UART RX DMA data lost issue. Test case to duplicate the issue: Connect iMX28 UART1 and PC with UART cable, then run some UART test application on iMX28 and PC side, PC can send a file to IMX28, file size should bigger than the default RX DMA buffer size 1024 bytes, then from iMX28 side, there will be data lost. The attached "SERIALAPP.zip" is the updated UART driver code to fix this issue, you can unzip and update it to "wince600\platform\common\src\soc\common_fsl_v2_pdk1_9\serialapp" folder, and rebuild the WinCE image. The followed improvement had been implemented in this update for UART RX DMA: 1. Added DMA recover code.     When UART error happens in DMA mode, the driver will re-initialize the DMA for next transfer.. 2. Set UART DMA timeout interrupt to 5ms. "#define SERIAL_DMA_RX_TIMEOUT      5"     After UART DMA interrupt happens, the IST need copy data from DMA buffer to MDD buffer, so it needs time. The default BSP had set this delay to 31 bits transfer time, this is very short, if the PC send "DMA buffer + 1" bytes to iMX28, after first DMA buffer full interrupt happens, the second DMA timeout interrupt will happen in a short time, this interrupt will be lost, because the driver is still processing the pre-interrupt. 3. Updated MDD code to make sure the buffer send to PDD is always bigger than the RX DMA buffer.     This MDD code modification will only active in DMA mode, so there is no impact for PIO mode. 4. Update UART DMA interrupt handler code.     When UART DMA interrupt happens, set up the next DMA transfer at once, so DMA can continue to receive data with another DMA buffer, the same time the IST will copy data from pre-DMA buffer to MDD buffer.
View full article
       Of all the i.MX serials SoC, i.MX28/i.MX6UL/i.MX7D/S use Synchronous Audio Interface(SAI) to support audio applications. SAI supports I2S, AC97, TDM and code/DSP interfaces. The SAI interface consists of these signals: SAI_MCLK         ------------  used to provide working clock for external audio device , such as audio codec. SAI_RX_BCLK  ------------  bit clock for receiving channle. SAI_RX_DATA   ------------  data of receiving channel. SAI_RX_SYNC  ------------  Frame Synchronous signal of Left and right channel for receiving channel. SAI_TX_BCLK  ------------  bit clock for transmitting channel. SAI_TX_DATA   ------------  data of transmitting channel SAI_TX_SYNC  ------------  Frame Synchronous signal of Left and right channel for transmitting channel.         According to above signals, SAI has 2 channels: receive and transmit, and these 2 channels have their own clock: bit clock and frame SYNC, so they can work independently, it means PLAY and CAPTURE can be operated simultaneously, that is to say, SAI works at Asynchronous mode this moment.        In the document, we will discuss several usages of SAI on hardware design when it works at I2S(SYNC) mode. we will take i.MX6UL as an example, and for i.MX7D/S, usages are similar. 1. IOMUX of SAI From i.MX6UL reference manual, there are 3 SAI modules in i.MX6UL: SAI1 , SAI2 & SAI3, see page 2529 in IMX6ULRM.pdf. As common applications, we will use 2 interface of SAIs. 2. Hardware connections for I2S mode Either CPU is Master or Codec is Master, hardware connections are same. (1) Single audio codec or (2) Dual audio codec (3) Audio codec + Bluetooth PCM or (4) Audio codec + Bluetooth PCM + 4G PCM or     [Note]   Attachments are schematics of WM8958 and MAX98089, which are not released by NXP, just for users who are interested in i.MX audio applications reference. If you want to use WM98089 or WM8958, please contact their manufactures and confirm if schematics are correct, so don't use them directly for your solution. NXP China TIC i.MX team Weidong Sun
View full article
When boot from battery, then plug in 5V cable, the actual charging current can't reach the preset charging current. It is because the HEADROOM_ADJ is not correctly set. Please use attached mx28_chargingcurrent_limit_bootfrombattery.patch. Grace
View full article
What is HOB? Hob is a graphical user interface for BitBake. Its primary goal is to enable a user to perform common tasks more easily. It basically runs the Bitbake commands on the background while showing a Graphic User Interface. Hob may not work correctly with Daisy metadata as it is getting deprecated in favor of a new web based interface for Yocto under the name Toaster. Here is what you can do with the current version of Hob on the Freescale Community BSP and BSP Release. - Build images - Edit existing image recipes - Create your own image recipes Note: HOB will write the local.conf file and make modifications which may conflict with baking images outside of HOB. In this case you may need to re-run the environment initialization in order to restore the local.conf file. Starting HOB Once the environment has been initialized (using the setup-environment script on the Freescale Community BSP or the fsl-setup-release on the Freescale BSP Release) use the command below. $ hob & The GUI should then appear: You may then select the MACHINE for which you will build and the Layers of your project. HOB  will take and updated the local.conf and bblayers.conf values so the desired BSP layers will already be selected and available MACHINES on these layers will appear on the drop down menu. Once these options are set HOB will parse the recipes and create a dependency tree in order to show available images for that MACHINE. Image File System Types Advance configuration options include image file system types. Please note that HOB does not support the sdcard format so if it is needed it has to be added manually on the local.conf file and then run bitbake outside of HOB. As HOB changed the local.conf file even if the sdcard format was originally available it may be rewrite and no longer available until the following line is added to local.conf. IMAGE_FSTYPES="tar.bz2 ext3 sdcard" Recipes screen On the recipes screen we can see the recipes included on the image and available recipes, then also package groups. Time to bake! After these configurations you may either build the packages using HOB interface or run Bitbake outside of HOB. (In case you wish to have your image on the sdcard format please see the earlier image types clarification) The resulting image will be stored on <BUILD>/tmp/deploy/images/<MACHINE> You may also save your image recipe with the selected customizations.
View full article
Network File System (NFS) Setting the Host 1 - Install NFS Service on host typing: $sudo apt-get install nfs-kernel-server 2 - Create symbolic link to ltib/rootfs $sudo ln -s <ltib instalation folder>/rootfs /tftpboot/rootfs 3 - Setup exports typing: $sudo gedit /etc/exports and add the following line: /tftpboot/rootfs/ *(rw,no_root_squash,no_subtree_check,async) 4 - Restart the NFS server: $sudo /etc/init.d/nfs-kernel-server restart Now the host is ready to use NFS. Setting Target Linux Image to use NFS 1 - Run LTIB configuration typing: $cd <ltib instalation folder> $./ltib -c 2 - On first page menu, go to "Target Image Generation -> Options" as in the picture below. 3 - Select the option NFS only and exit LTIB configuration to compile with the new configuration. 4 - LTIB should start new compiling and create a new Linux image on /<ltib instalation folder>/rootfs/boot/zImage 5 - Copy the created image on /<ltib instalation folder>/rootfs/boot/zImage to /tftpboot/zImage 6 - The system is ready to run with NFS. The root file system on target will be located on host on /<ltib instalation folder>/rootfs/
View full article
www.nxp.com公网资源 .............................................. 2 1.1 www.nxp.com Documentation ................................ 3 1.2 www.nxp.com Tools&Software ............................... 7 2 nxp share point资源(仅对有访问权限客户开放) ....... 14 2.1 i.MX 8X Family Board, Software POR and How to Purchase ...................................................................... 14 2.2 Development Platforms ........................................ 14 2.3 Device Dcoumentation ......................................... 15 2.4 Security Reference Manual .................................. 16 2.5 Software Documentation ...................................... 16 3 nxp 社区资源 ........................................................... 16
View full article
I've recently done some digging into fstrim feature on sabresd-6q. Here list it below detailed: Background:      When Nexus 7 first came out, many users felt it was speedy and high-performance. But after months of installing applications and using the tablet, things began slowing down.This was a friction point that many hoped would be fixed in the new Nexus 7 (2013) model, which it was. There’s even more to the story though, it turns out Google has fixed that storage I/O aging problem on all Nexus devices with the Android 4.3 update which comes with a little-hyped feature that could be huge for performance in the future – TRIM support via fstrim. Why slowing down?      Remember that deleting a file in software isn't actually communicated to solid state storage (whether SSD or eMMC). The space is freed up from the user's perspective, but the eMMC controller in this case still treats the pages in NAND as having valid data. Let's say you copy a 3GB movie to your internal storage, watch the movie and later delete it. You'd have 3GB free to re-use, but until you re-write those blocks the eMMC controller would treat all 3GB as valid data. There's a data structure used by the eMMC controller that tracks mapping logical locations to physical locations in NAND. I won't go into great detail here but the more complex that mapping becomes, and the more locations that have to be tracked, the slower internal NAND management works. Why SSD has such issue? Root cause is "Flash memory is divided into blocks, which is further divided in pages. The minimum write unit is a page, but the smallest erase unit is a block" which will cause fragments as time goes. Why fstrim?      Fstrim is one mechanism of linux filesystem which derives from TRIM. TRIM is already introduced since linux2.6.33. It is the name of a command that the operating system can send to tell the SSD which blocks are free in the filesystem.The SSD uses this information to internally defragment the blocks and keep free pages available to be written quickly and efficiently. How framework triggers fstrim in android4.3?      Android4.3 introduces a new service IdleMaintenanceService to manage when and how trigger fstrim in right time. Once system satisfies the following conditions, it will send out one "ACTION_IDLE_MAINTENANCE_START" intent which the MountService listens for. Last time  "ACTION_IDLE_MAINTENANCE_START" intent has been sent before 24 hours. The device is either off-charger with 80% battery or on-charger with 30% battery The device can go idle state. User don't use it for 71 minutes. Test fstrim on Imx.6      In order to wait little time to trigger fstrim, I tried to change the following variables not to wait 71 minutes and 24 hours. After changing, it will trigger one time fstrim two minutes after system goes into idle state every 30 minutes. --- a/services/java/com/android/server/IdleMaintenanceService.java +++ b/services/java/com/android/server/IdleMaintenanceService.java -    private static final long MIN_IDLE_MAINTENANCE_INTERVAL_MILLIS = 24 * 60 * 60 * 1000; // 1 day +    private static final long MIN_IDLE_MAINTENANCE_INTERVAL_MILLIS = 30 * 60 * 1000; // 30 minute -    private static final long MIN_USER_INACTIVITY_IDLE_MAINTENANCE_START = 71 * 60 * 1000; // 71 min +    private static final long MIN_USER_INACTIVITY_IDLE_MAINTENANCE_START = 2 * 60 * 1000; // 2 min -    private static final long MAX_IDLE_MAINTENANCE_DURATION = 71 * 60 * 1000; // 71 min +    private static final long MAX_IDLE_MAINTENANCE_DURATION = 2 * 60 * 1000; // 2 min Firstly I  run Quadrant apk to see my I/O performance at beginning, Its score is 3544. During this 30 minutes, you can try to mess your system. Try your best to install most apks. Run monkey test in background. Then I  run Quadrant again to check my I/O performance, its score is only a little decline 3538. After that I run "logcat | busybox grep -i fstrim" in console to wait for the action of fstrim, here is my logcat: 130|root@sabresd_6dq:/ # logcat -d | busybox grep -i fstrim I/fstrim  ( 2344): Starting fstrim work... I/fstrim  ( 2344): Invoking FITRIM ioctl on /data I/fstrim  ( 2344): Trimmed 6367305728 bytes on /data I/fstrim  ( 2344): Invoking FITRIM ioctl on /cache I/fstrim  ( 2344): Trimmed 526355456 bytes on /cache I/fstrim  ( 2344): Finished fstrim work. OK, I checked the I/O information again, its score is restored to 3546: Conclusion      Good, fstrim takes effect. So on imx.6 using android4.3, fstrim will also work automatically. We will also enjoy good performance in I/O memory.Great!
View full article
Network File System (NFS)      Setting the host          1 - Install NFS Service on host typing:        $sudo apt-get install nfs-kernel-server          2 - Create symbolic link to ltib/rootfs        $sudo ln -s <ltib instalation folder>/rootfs /tftpboot/rootfs          3 - Setup exports typing:        $sudo gedit /etc/exports          and add the following line:        /tftpboot/rootfs/ *(rw,no_root_squash,no_subtree_check,async)          4 - Restart the NFS server:        $sudo /etc/init.d/nfs-kernel-server restart          Now the host is ready to use NFS      Setting Target Linux Image to use NFS          1. Run LTIB configuration by typing: $cd <ltib instalation folder>          $./ltib -c          2 . On first page menu, go to "Target Image Generation -> Options"       3. Select the option NFS only and exit LTIB configuration to compile with the new configuration.          4. LTIB should start new compiling and create a new Linux image on /<ltib instalation folder>/rootfs/boot/zImage          5. Copy the created image on /<ltib instalation folder>/rootfs/boot/zImage to /tftpboot/zImage          6. The system is ready to run with NFS. The root file system on target will be located on host on /<ltib instalation folder>/rootfs/         
View full article