i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Question: To connect an FPGA to the i.MX6Q over LVDS.,to connect the 2 LVDS channels in split mode. The datasheet indicates the driver output max skew due to different propagation time of rising and falling edge. For the sake of the design of their FPGA interface, it would be also interesting to get the skew between the 2 LVDSn_CLK (of the 2 channels) as well as the intrachannel- skew. Answer: Backend database are checked. We can provide the result in the view of design. Since we do not check inter-channel skew in production, the following may not be guaranteed.  At the core boundary, we found that, timing skews between every data and clock are within 30ps. Path from core boundary to PAD are matched by analog layout, should produce some skew well below 30ps also. As the result, I think, all LVDS signal can be considered as one single group, and skew in datasheet can apply to any signal.
View full article
Hi All, The new i.MX 6 Q/D/DL/S/SL L3.0.35_4.1.0 GA release is now available on the http://www.freescale.com/site. ·         Files available                                   # Name Description 1 L3.0.35_4.1.0_LINUX_DOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP   Documentation. Includes Release Notes, Reference Manual, User guide. API   Documentation 2 L3.0.35_4.1.0_LINUX_MMDOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Multimedia Codecs Documentation.   Includes CODECs Release Notes and User's Guide 3 L3.0.35_4.1.0_SOURCE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP   Source Code Files 4 L3.0.35_4.1.0_MM_CODECS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Multimedia Codecs Sources 5 L3.0.35_4.1.0_AACP_CODECS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux AAC Plus Codec 6 L3.0.35_4.1.0_DEMO_IMAGE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Binary Demo Files 7 L3.0.35_4.1.0_UBUNTU_RFS_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux File System for the Ubuntu Images 8 i.MX_6D/Q_Vivante_VDK_146_Tools Set   of applications for the Linux L3.0.35_4.1.0 BSP, designed to be used by   graphics application developers to rapidly develop and port graphics   applications. Includes applications, GPU Driver with vprofiler enabled and   documentation. 9 IMX_6DL_6S_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6DualLite and i.MX   6Solo. 10 IMX_6DQ_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6Quad and i.MX 6Dual. 11 IMX_6SL_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6Sololite. ·         Target HW boards o   i.MX 6Quad SABRE-SDP o   i.MX 6Quad SABRE-SDB o   i.MX 6Quad SABRE-AI o   i.MX 6DualLite SABRE-SDP o   i.MX 6DualLite SABRE-AI o   i.MX 6SL EVK ·         New features o   BSP New Features on i.MX 6D/Q, i.MX 6DL/S and MX 6SL: §  HDCP §  CEC §  GPU4.6.9p12 §  Audio playback IRAM/SDMA §  V4L capture resize on MX6SL §  MX6DQ disable the double line fill feature of PL310 ·         Known issues o   For known issues and limitations please consult the release notes.
View full article
Question: On i.MX6 DQ, the ON_TIME and DEBOUNCE bit fields of the SNVS_LPCR register are not readable.  Also in the preliminary (i.MX61) specs bits 31-15 are reserved.  Are ON_TIME and DEBOUNCE bit fields actually in this register for i.MX 6DQ and are these bits writable but not readable? Answer: This is a document issue which will be fixed in the next version of the RM.  The register diagram should read as follows:
View full article
1. User Case: Demo Architecture: Demo Description: A, B, C and Speaker all are i.MX6DQ SabreSD board and running Ubuntu system. A is media server which send out broadcast 30Mbps h264 video and audio stream and running iperf to send out tcp packets via best efforts lane to PC. B and C are clients to get video data only and play in screen.  Speaker is a client to receive audio data only and play to speaker. PC which install ubuntu system is used to received best efforts data from A. Demo Goal: Use Gstreamer playback 30Mbps streaming  "H264_AVC_1080p_30fps_27Mbps_mp3.avi", while running iperf TCP streaming under the following two case: 1. Running the non-CBS kernel 2. Enable the FIQ kernel Validate the Qav (Queue and Forwarding Protocol) which is developed by SW. 2. Resource: FIQ Patch: 0001-GIC-FIQ-EPIT-implement.patch 0002-set-EPIT-priority-to-highest.patch 0003-GIC-support-SMP-4-cores-of-FIQ.patch CBS &Shaper Patch: 0004-Implement-credit-base-shaper-alogrithim-to-schdule-A.patch 0005-enet-avb-CBS-SIRQ-rum-mode-pass-performance-stress-t.patch Others Patch: 0006-Fix-the-61883-sub-type-protocol-check.patch 0007-Add-hrtimer-for-the-sirq.-Talker-transmit-packets-nu.patch 0008-1.-Fix-memory-map-size-issue.patch 0009-Increase-BD-entries-to-reduce-the-full-times.patch 0010-Add-sys-interface-to-log-out-the-video-packet-number.patch 0011-Add-AVB-timestamp-support.patch 0012-GIC-support-SMP-4-cores-of-FIQ.patch Gstreamer UDPAVB Plug-in Library and Source: Library: udp/output/libgstudp.so Source: udp/* 3. Setup the Patch:       - Low level:  kernel enet driver implement CBS and traffic shaper:              1. Apply all the patches in the patch_whole.tar.gz in the attachment               2. Rebuild kernel 3.0.35: Enable "CONFIG_ENET_IMX6_AVB" to support AVB.                        Enable "CONFIG_RUN_IN_FIQ"  in kernel:            let CBS run in FIQ mode.                3. make uImage.                You can also use the uImage-avb-fig in the attachment directly.  Flash to the SD card use dd command, the user gudie refer to the  i.MX_6Dual6Quad SABRE_SD_Linux_User_Guide.pdf.                Note: the uImage_org_nonavb in the attachment is the kernel image without QAV and FIQ. - High level: use Gstreamer as the media input/output interface, encapsulation with IEEE1722 format:         Before the below action, you should already have seutp the Ubuntu Rootfs,  copied all the Freescale *.deb files that come alone with the Release BSP demo image package and copied all the MM codec *.deb files (IMX_MMCODEC_3.0.7.tar) that from Freescale offical website, the user gudie refer to the  i.MX_6Dual6Quad SABRE_SD_Linux_User_Guide.pdf. 1. Add gstreamer setup version as following: - gstreamer core version: 0.10.35 - gst-plugins-good version: 0.10.30 - gst-plugins-bad version: 0.10.11 2. Setup: - tar xvzf udp.tar.gz - cd gst-plugins-good-0.10.30 - ./configure - make - make install - cp ~/udp/* gst/udp/ - cd gst/udp - make - cp  libgstudp.so /usr/lib/gstreamer-0.10/ - gst-inspect | grep avb         //Check whether the avb plugin is installed successfully. If the three avb plugin is printed out in the terminal, the avb plugins are proved to install properly. 4. Run the Demo:       1.  Start the iperf server in PC linux machine by inputting " iperf -s -i 1&".              2.  Power on the A board, ensure the board can get the DHCP IP address, Start the iperf client on the demo board which sends outgoing Audio-Video streaming in the background. Input "iperf -c <iperf server ip> - t 6000&". If the connection is  successful, the iperf log should be able to be seen in the linux machine terminal.              3.  Power on the B and C board, inputting the following command to receive video data:            Run "./startRxVideoAVB.sh"  to start gstreamer video receive process on video display board       4.  Power on the speaker board, inputting the following command to receive audio data:             Run "./startRxAudioAVB.sh" to start gstream audio receive process on audio  playback board 5.  Inputting the following command to send video/audio data to client at the A board terminal windowns:                              Run "./startTxAVB.sh" to start the 1722 streaming traffic                                      (note: H264_AVC_1080p_30fps_27Mbps_mp3.avi located at current directory)               6.  Change to the kernel with QAV and follow the steps 1~5 above 5. Result: Without FIQ Qav,  video play at client B and C serious freeze. It takes 3 minutes to play 1min 40s h264 stream.  iperf speed over 80Mbps. With FIQ Qav, video play at client B and  C is smooth and same as without iperf in background. Iperf show speed is less than 70Mbps.  FIQ Qav correctly reserve necessary bandwidth to AV stream 6. Know issues Failed to request the IP from DHCP         [Solution]  For FIQ, after kernel up, you must run the command: echo 1 > /sys/devices/platform/imx_wfi_issue.0/enable   2.   Kernel is halted or crashed [Solution] In bootloader parameter, add 'nosmp' in bootargs_mmc.
View full article
This document provide an overall guide how to get started with i.MX6 development. There are several chapters: 1. how to get necessary docs from freescale website; 2. how to setup environment and build your own images;3. Hardware design consideration;4. How to get help. I hope the doc will bring you in i.MX world more easily, and hope you all have a fun in it.
View full article
Q:Is there an issue using odd DIV_SELECT values? When setting the CPU clock (maybe others also) in uboot, the code will only use even valuesfor the DIV_SELECT field. There is nothing in the Reference Manual or Errata that indicates only even values can be used for this field. There were 2 SR's that had conflicting answers and we are trying to determine what can be used. The CPU freq setting trying to be achieved is 996MHz. With a 24MHz source, you need 24MHz x 41.5 = 996MHz. Since the DIV_SELECT is x2, a value of 83 would be needed. A: Below is the DIV_SELECT description of ARM PLL, since the Fin is 24MHz, so there is no odd issue of DVI_SELECT, as 24 / 2 = 12MHz. Such as for 996M, this value is 83, that is fine. "This field controls the pll loop divider. Valid range for divider value: 54-108. Fout = Fin * div_select/2.0." This document was generated from the following discussion: mx6Q PLL Setting
View full article
Q: What is latency figures for the VPU to decode Device: i.MX6Q OS: Linux Resolution:                         1920x1080(HD) Frame rate:                        30 FPS Function:                             Overlay messages. Input/Output:                   8 bit / YUV 4:2:0 / NAL stream Profile level:                      4.1. Constrained Baseline. I and P frames support. A: It depend on the syntax in H.264, includes num_reorder_frames,max_dec_frame_buffering,num_ref_frames,MaxDpbSize,etc. for start latency: it cover vpu driver loading, allocate buffers, init, decoding the first frame less than 100ms on iMX6/Linux. This document was generated from the following discussion: VPU Latency i.MX6
View full article
Q: When trying to mount his SDIO WiFi module (an Azurewave module containing a Marvel 88W8790)  in 4 bit mode, and got error wifi module on iMX6 Smart SD dev board using the alpha kernel (3.5.7+3285970). mwifiex_sdio mmc0:0001:1: WLAN FW is active mwifiex_sdio mmc0:0001:1: mwifiex_cmd_timeout_func: Timeout cmd id (2004.239824) = 0xa9, act = 0x0 mwifiex_sdio mmc0:0001:1: num_data_h2c_failure = 0 mwifiex_sdio mmc0:0001:1: num_cmd_h2c_failure = 0 mwifiex_sdio mmc0:0001:1: num_cmd_timeout = 1 mwifiex_sdio mmc0:0001:1: num_tx_timeout = 0 mwifiex_sdio mmc0:0001:1: last_cmd_index = 1 mwifiex_sdio mmc0:0001:1: last_cmd_resp_index = 0 mwifiex_sdio mmc0:0001:1: last_event_index = 0 mwifiex_sdio mmc0:0001:1: data_sent=1 cmd_sent=1 mwifiex_sdio mmc0:0001:1: ps_mode=1 ps_state=0 +++++++++++++++++++++++ There are only two known issues with the SDHC driver as noted in the release notes and these don't seem to match.  The Linux Reference Manual states the operation of the SDIO was veriifed usign the AR6003.  My assumption is that this is the Silex module we have standardized on.  Was 4 bit mode verified using this module? Does anyone have any idea what could be happening here? A: L3.5.7 is an alpha release, and WiFi function is not stable. The test report shows that open WiFi issue exists. Wifi module sometime can't work on mx6q_smd. After insmod ath, ath6kl_core and ath6kl_sdio. Insert the wifi card, sometime(50%) will display -------------------------- ath6kl: unable to read RX_LOOKAHEAD_VALID                                      ath6kl: Unable to recv target info: -84                                        ath6kl: Failed to init ath6kl core                                             ath6kl_sdio: probe of mmc0:0001:1 failed with error -84    -------------------------- reinsert the wifi card may solve the problem. when execute "udhcpc -i wlan0", sometime (30%) will cause program exception. Sometime can't get the wlan0 ip(program hang). Environment(OS,Platform,Driver, etc): HW: MX6Q_SMD Num014 and Num017 MX6Q_ARD don't have this problem SW: Kernel 3.5.7-1.0.0 GNU/Linux Case ID: TGE-LV-WIFI-0043 Reproduce Steps: #modprobe ath #modprobe ath6kl_core #modprobe ath6kl_sdio insert the wifi card # iwconfig wlan0 mode managed # iwlist wlan0 scanning | grep MAD-wifi #iwconfig wlan0 key 00112233445566778899123456 #iwconfig wlan0 essid MAD-wifi #udhcpc -i wlan0 Attached MX6 ARD WiFi issue also. [Kernel3.5.7_MX6QARD]Wifi:wifi card can't work during suspend and resume. 100% -- Bug detailed description: With wifi card inserted in the board. doing system suspend and resume test. wifi card can't work well after the system suspend and resume. Always report : ath6kl: Unable to decrement the command credit count register: -84             ath6kl: Unable to write to the device: -84                                     ath6kl: bmi_write_memory for uart debug failed                                 ath6kl: Failed to boot hw in resume: -5          Environment(OS,Platform,Driver, etc): HW: MX6QARD -023 Only tried on this platform SW: root@imx6qsabreauto:~# uname -a                                                Linux imx6qsabreauto 3.5.7-1.0.0+3285970 #1 SMP PREEMPT Sat Jun 29 10:20:45 CDT 2013 armv7l GNU/Linux Case ID:  TGE-LV-WIFI-1060 and TGE-LV-WIFI-1062 Reproduce Steps: 1. boot the kernel with wif card inserted 2. doing wifi stress test 3. doing suspend and resume
View full article
Hi, the document "how to create ubuntu hardfloat rootfs for imx6d/q" was shared by Junping Mao. https://community.freescale.com/docs/DOC-95387 Here, i build the OpenCV based on the ubuntu hardfloat rootfs for i.MX6Q sabre board. Details about building instruction pls refer to the attachment. Thanks! 
View full article
Hi, The document "How to create ubuntu hardfloat rootfs for imx6d/q" was shared by Junping Mao. https://community.freescale.com/docs/DOC-95185 However, some modification need to be made to build imx-tests on this rootfs. Attached please find the guide for building imx-tests on hf-ubuntu rootfs for imx6d/q. Any problems, pls feel free to let me know. Regards, Alvin zheng
View full article
We use PCIe to connect Intersil TW6865 chip for the surround view solution. This is the connection of PCIe to iMX6Q SabreSD board.   This is the block diagram of the connection: This is the 4 camera surround view:   Code base is L3.0.35_12.10.02 release. You can merge the patch file to the latest Freescale release. Please check the attach file for the patch code.   Note:  It is only a test version. The last code for L3.0.35 BSP: L3.0.35_GA4.1.0 Patches.7z The last code for L3.10.53 BSP: L3.10.53_TW686x_patch.7z Patch for L4.1.15 1.1.0 GA BSP: TW6865 driver for Linux L4.1.15_1.1.0-ga.7z
View full article
In this post we see how to setup a Debian server, to allow booting the i.MX6 sabre sd platform (mostly) from the network. Booting from the network instead of e.g. the SD card is very handy for day to day development and testing, as it eliminates almost all physical interactions with the board and saves much time. Also, fortunately for us, both u-boot and Linux for i.MX6 support network booting out of the box. Boot sequence principles Before we setup the server, here are some more details on the boot sequence we will obtain in the end: i.MX6 boots, loads u-boot from SD card. u-boot starts, loads its environment (boot commands) from SD card. u-boot obtains its network address by DHCP, loads a Linux kernel uImage and a dtb by TFTP. Linux boots; obtains its network address by DHCP (again), mounts its root filesystem on NFS. Setting up DHCP and TFTP One can easily setup a Debian server to act as DHCP and TFTP server with Dnsmasq; just install the dnsmasq package. The default configuration is mostly empty; so we need to enhance it a bit. For the following we will assume that your Debian server has IP address 192.168.111.1 on the network where it sees the i.MX6 sabre sd platform. You can add some options to a dnsmasq config file such as e.g. /etc/dnsmasq.d/my-custom-config-file:   dhcp-range=192.168.111.50,192.168.111.150,12h   enable-tftp   tftp-root=/var/ftpd This informs dnsmasq to act as a DHCP server for addresses range 192.168.111.50-150 and act as TFTP server, which serves files under /var/ftpd. That means you will need to copy a Linux uImage and an imx6q-sabresd.dtb under /var/ftpd/. See this post for more details about compiling Linux to obtain those two files. Setting up NFS If we want the root filesystem to be mounted on the network we will need to export some folders with NFS from the Debian server. We need to install the nfs-kernel-server package and setup /etc/exports with a line such as:   /tftpboot       192.168.111.*(rw,no_root_squash,subtree_check) This allows clients on the 192.168.111.0 network to access filesystems under the /tftpboot folder. So you will need to create a /tftpboot folder on the server, and install some "filesystem" under there. For this example we assume you will have a busybox installed under a /tftpboot/busybox/ folder. That means we want to have under there all folders such as bin, dev, etc... See this post for details on how to compile busybox to populate this folder. Do not forget to restart the NFS server after configuration, with:   # /etc/init.d/nfs-kernel-server restart We are now setup on the server side. Setting up u-boot At the time of this writing we need to help u-boot a bit when booting the i.MX6 sabre sd platform from the network. Stop at u-boot prompt and configure a few things:   env default -a   setenv netargs $netargs rw   setenv serverip 192.168.111.1   setenv nfsroot /tftpboot/busybox   setenv bootcmd run netboot   saveenv Reset your board; it should now boot from the network:   U-Boot 2013.07-rc1-00210-gc623eb0 (Jun 27 2013 - 21:10:47)   (..)   Hit any key to stop autoboot:  0   Booting from net ...   BOOTP broadcast 1   DHCP client bound to address 192.168.111.121   Using FEC device   TFTP from server 192.168.111.1; our IP address is 192.168.111.121   Filename 'uImage'.   Load address: 0x12000000   Loading: #################################################################            #################################################################            #################################################################            #################################################################            ##########################            4 MiB/s   done   Bytes transferred = 4185600 (3fde00 hex)   BOOTP broadcast 1   DHCP client bound to address 192.168.111.121   Using FEC device   TFTP from server 192.168.111.1; our IP address is 192.168.111.121   Filename 'imx6q-sabresd.dtb'.   Load address: 0x11000000   Loading: ##            2.7 MiB/s   done   Bytes transferred = 22818 (5922 hex)   ## Booting kernel from Legacy Image at 12000000 ...      Image Name:   Linux-3.10.0-rc7   (..)   Starting kernel ...   Booting Linux on physical CPU 0x0   Linux version 3.10.0-rc7 (jenkins@debian) (gcc version 4.7.2 (Debian 4.7.2-5) ) #1 SMP Tue Jun 25 08:28:31 CEST 2013   (..)   Kernel command line: console=ttymxc0,115200 root=/dev/nfs ip=dhcp nfsroot=192.168.111.1:/tftpboot/busybox,v3,tcp rw   (..)   fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)   IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready   libphy: 2188000.ethernet:01 - Link is Up - 1000/Full   IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready   Sending DHCP requests ., OK   IP-Config: Got DHCP answer from 192.168.111.1, my address is 192.168.111.121   IP-Config: Complete:        device=eth0, hwaddr=00:04:9f:02:b7:fd, ipaddr=192.168.111.121, mask=255.255.255.0, gw=192.168.111.1        host=192.168.111.121, domain=, nis-domain=(none)        bootserver=192.168.111.1, rootserver=192.168.111.1, rootpath=        nameserver0=192.168.111.1   ALSA device list:     No soundcards found.   VFS: Mounted root (nfs filesystem) on device 0:11.   devtmpfs: mounted   Freeing unused kernel memory: 292K (806d5000 - 8071e000)   Please press Enter to activate this console. Enjoy! Bonus: updating u-boot by the network One last piece remains on the SD card: u-boot. If you do not want to move your SD card out of its slot any more, here is a method for you to update even u-boot from the network. You will need to copy u-boot.imx under /var/ftpd. See this post for details on how to compile u-boot and obtain u-boot.imx. Then, at u-boot prompt, do:   dhcp $loadaddr u-boot.imx   mmc dev 1   mmc write $loadaddr 2 600 This will download a new u-boot.imx from the network and flash it to your SD card; reboot your board and you are done. Note that we give 600 as the number of SD card blocks to write; this is a rough estimate of ~300KB, which should work in most of the cases as writing a bit "too much" blocks does not harm. If you are very picky, you can compute the exact number of blocks by dividing your u-boot.imx size by 512 and rounding it up. See also... Did you know that dnsmasq primary role is to be used to "relay" the DNS queries? A feature that come very handy when you want to let your i.MX6 platform "see" the internet.
View full article
Here we show how to generate a minimal root filesystem fairly quickly with BusyBox, for the i.MX6 sabre sd platform. This document assumes you are able to boot a Linux kernel on your platform already. See this post for details on how to do it. This implies you already have a "working" Linux development environment with some ARM cross-compilers at hand (e.g. Debian + Emdebian). busybox is so small that we will go for a ramdisk as our main root filesystem. Get busybox sources We will use git to fetch busybox sources:   $ git clone git://git.busybox.net/busybox This should create a busybox directory with all the latest sources. Note that for more stability you might want to checkout a release instead of the latest version; to do so, list the available release tags with e.g. git tag -l, and git checkout <the-desired-tag>. Compile Assuming your cross compiler is called e.g. arm-linux-gnueabihf-gcc, you can compile by doing:   $ cd busybox   $ export ARCH=arm   $ export CROSS_COMPILE=arm-linux-gnueabihf-   $ make defconfig   $ sed -i.orig 's/^#.*CONFIG_STATIC.*/CONFIG_STATIC=y/' .config   $ make   $ make install This should create an _install folder hierarchy containing binaries and links. Note that we force the build of a static binary with the sed command. Configure the root filesystem We need to add some more configuration into the _install folder before we can call it a minimal filesystem. Create some folders We need to create some mountpoints and folders:   $ mkdir _install/dev   $ mkdir _install/proc   $ mkdir _install/sys   $ mkdir -p _install/etc/init.d Add some configuration files and scripts We need to prepare the main init configuration file, _install/etc/inittab, with this contents:   ::sysinit:/etc/init.d/rcS   ::askfirst:/bin/sh   ::ctrlaltdel:/sbin/reboot   ::shutdown:/sbin/swapoff -a   ::shutdown:/bin/umount -a -r   ::restart:/sbin/init This is very close to the default behavior busybox init has with no inittab file. It just suppresses some warnings about missing tty. We need to add some more configuration to mount a few filesystems at boot for convenience. This is done with an _install/etc/fstab file containing:   proc     /proc proc     defaults 0 0   sysfs    /sys  sysfs    defaults 0 0   devtmpfs /dev  devtmpfs defaults 0 0 We also need to actually trigger the mount in the _install/etc/init.d/rcS script, which is called from the inittab. It should contain:   #!/bin/sh   mount -a And we need to make it executable:   $ chmod +x _install/etc/init.d/rcS Generate the ramdisk contents Now that we have adapted the root filesystem contents, we can generate a busybox ramdisk image for u-boot with the following commands:   $ (cd _install ; find |cpio -o -H newc |gzip -c > ../initramfs.cpio.gz)   $ mkimage -A arm -T ramdisk -d initramfs.cpio.gz uInitrd This results in a uInitrd file, suitable for u-boot. Prepare a boot script The default u-boot commands are not sufficient to boot our system, so we need to edit a boot.txt file with the following contents:   run loaduimage   run loadfdt   setenv rdaddr 0x13000000   fatload mmc ${mmcdev}:$mmcpart $rdaddr uInitrd   setenv bootargs console=${console},${baudrate} rdinit=/sbin/init   bootm $loadaddr $rdaddr $fdt_addr Then we generate a boot.scr script, which can be loaded by u-boot with:   $ mkimage -A arm -T script -d boot.txt boot.scr Put on SD card Assuming you have prepared your SD card with u-boot and Linux as explained in this post, you have a single FAT partition on your card with your kernel and dtb. Our boot script and ramdisk image should be copied alongside:   $ mount /dev/<your-sd-card-first-partition> /mnt   $ cp uInitrd boot.scr /mnt/   $ umount /mnt Your SD card first partition is typically something in /dev/sd<X>1 or /dev/mmcblk<X>p1. Note that you need write permissions on the SD card for the command to succeed, so you might need to su - as root, or use sudo, or do achmod a+w as root on the SD card device node to grant permissions to users. Boot! Your SD card is ready for booting. Insert it in the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. Your busybox system should boot to a prompt:   ...   Freeing unused kernel memory: 292K (806d5000 - 8071e000)   Please press Enter to activate this console. After pressing enter you should have a functional busybox shell on the target. Enjoy! See also... For a more featured root filesystem you might want to try a Debian filesystem in a second SD card partition, as explained in this post, or generate your filesystem with Buildroot. If you plan to compile busybox often, you might want to use a C compiler cache; see this post.
View full article
Here we show how to bootstrap the Debian Linux distribution from a PC to the i.MX6 sabre sd platform. While bootstrapping Debian on any architecture "natively" is pretty straightforward, "cross-bootstrapping" requires some techniques that we will explain. This document assumes you are able to boot a Linux kernel on your platform already. See this post for details on how to do it. Also, this document assumes you are using a Debian PC for preparing your SD card. You will require the following packages to be installed: binfmt-support qemu-user-static debootstrap Note: all the commands found in the following steps need to be run as root. Formatting the SD card We need to format the SD card with two partitions; one small FAT partition to contain the Linux kernel and its dtb, and one large ext4 partition, which will contain the root filesystem with the Debian userspace. Also, we need to make sure we leave some space for u-boot starting from offset 1024B. Here is an example SD card layout:   +-----+------+--------+-----+---------------+-----------------   | MBR |  ... | u-boot | ... | FAT partition | Linux partition ...   +-----+------+--------+-----+---------------+-----------------   0     512    1024           1M              ~257M (offsets in bytes) Here is an example SD card layout, as displayed by fdisk:   Device    Boot      Start         End      Blocks   Id  System   /dev/sdc1            2048      526335      262144    c  W95 FAT32 (LBA)   /dev/sdc2          526336     8054783     3764224   83  Linux (units: 512B sectors) You can format and mount the Linux partition with:   # mkfs.ext4 /dev/<your-sd-card-second-partition>   # mount /dev/<your-sd-card-second-partition> /mnt Your SD card second partition is typically something in /dev/sd<X>2 or /dev/mmcblk<X>p2. Do not forget to install u-boot and a Linux kernel as explained in those posts. Bootstrapping Debian First stage The first stage of Debian bootstrapping is done with:   # debootstrap --foreign --arch=armhf testing /mnt This will retrieve the base Debian packages from the internet, and perform a first stage of installation:   I: Retrieving Release   I: Retrieving Release.gpg   I: Checking Release signature   I: Valid Release signature (key id A1BD8E9D78F7FE5C3E65D8AF8B48AD6246925553)   I: Validating Packages   I: Resolving dependencies of required packages...   I: Resolving dependencies of base packages...   I: Found additional required dependencies: insserv libbz2-1.0 libcap2 libdb5.1 libsemanage-common libsemanage1 libslang2 libustr-1.0-1   I: Found additional base dependencies: libee0 libept1.4.12 libestr0 libgcrypt11 libgnutls-openssl27 libgnutls26 libgpg-error0 libidn11 libjson-c2 liblognorm0 libmnl0 libnetfilter-acct1 libnfnetlink0 libp11-kit0 libsqlite3-0 libtasn1-3 libxapian22   I: Checking component main on http://ftp.us.debian.org/debian...   (...)   I: Extracting util-linux...   I: Extracting liblzma5...   I: Extracting zlib1g... At this point, the necessary tools for second stage of installation are under /mnt/debootstrap/. Second stage The second stage needs to run natively; on an arm platform, that is. But we can use the combination of two techniques to perform this stage on the PC anyway:   # cp /usr/bin/qemu-arm-static /mnt/usr/bin/   # chroot /mnt /debootstrap/debootstrap --second-stage Those commands copy an arm emulator on the target filesystem, and use the chroot command to execute the second stage of the installation into the SD card, on the PC, with transparent emulation:   I: Installing core packages...   I: Unpacking required packages...   I: Unpacking libacl1:armhf...   I: Unpacking libattr1:armhf...   I: Unpacking base-files...   (...)   I: Configuring tasksel...   I: Configuring tasksel-data...   I: Configuring libc-bin...   I: Base system installed successfully. You can now remove /mnt/usr/bin/qemu-arm-static, or keep it for later, subsequent chroot under emulation. Finetuning the root filesystem For development it is handy to remove the root password on the target by removing the '*' from /mnt/etc/shadow on the SD card:   root::15880:0:99999:7::: Also, we can add the following line in /mnt/etc/inittab to obtain a login prompt on the UART:   T0:23:respawn:/sbin/getty -L ttymxc0 115200 vt100 You can now unmount the filesystem with:   # umount /mnt Boot! Your SD card is ready for booting. Insert it in the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. At the time of writing u-boot tells the kernel to boot from the wrong partition by default, so we need to interrupt by pressing enter at u-boot prompt for the first boot and setup u-boot environment to fix this:   U-Boot > setenv mmcroot /dev/mmcblk0p2 rootwait rw   U-Boot > saveenv   Saving Environment to MMC...   Writing to MMC(1)... done As this is saved in the SD card it need only to be done once at first boot. You can reboot your board or type boot; your Debian system should boot to a prompt:   (...)   [ ok ] Starting periodic command scheduler: cron.   [ ok ] Running local boot scripts (/etc/rc.local).   Debian GNU/Linux jessie/sid debian ttymxc0   debian login: From there you may login as root. It is recommended to setup the network connection and install an ssh server inside the target for further development. Enjoy! See also... With the amounts of memory we have today in the systems, it is even possible to boot Debian in a ramdisk. See this post about busybox for the ramdisk generation. Another way of generating a root filesystem is by building it with buildroot. See and this post for details.
View full article
ccache is a C compiler cache. ccache can save a large amount of compilation time on recurring builds and builds restarted from a clean repository after make clean or git clean. It is well suited for e.g. u-boot and Linux compilation. Caching the host compiler Caching "native" builds is easily done by adding in the beginning of your $PATH a special directory, which contains links to ccache to override the usual compiler. On e.g. Debian this directory is readily available as /usr/lib/ccache, So you can do:   $ export PATH="/usr/lib/ccache:$PATH" Typical links found in this folder are:   c++ -> ../../bin/ccache   cc -> ../../bin/ccache   g++ -> ../../bin/ccache   gcc -> ../../bin/ccache etc... Caching the cross compiler Caching cross-compiled builds can be done in the same way as native builds, provided you create links of the form e.g. arm-linux-gnueabihf-gcc pointing to ccache. But there is an even more convenient way for those projects, which rely on a $CROSS_COMPILE environment variable (as is the case for e.g. u-boot and Linux). You can prefix the cross compiler with ccache there in e.g. the following way:   $ export CROSS_COMPILE="ccache arm-linux-gnueabihf-" Monitoring efficiency Now that your builds are cached, you might want to see how much is "spared" with this technique. ccache -s will tell you all sorts of statistics, such as:   cache directory                     /home/vstehle/.ccache   cache hit (direct)                 10852   cache hit (preprocessed)            3225   cache miss                         19000   called for link                    33267   called for preprocessing            9463   compile failed                         3   preprocessor error                     1   couldn't find the compiler           117   unsupported source language          921   unsupported compiler option         2167   no input file                      31681   files in cache                     51694   cache size                           1.3 Gbytes   max cache size                       4.0 Gbytes Here you see a somewhat typical 50%/50% hit/miss ratio. Enjoy! See Also ccache is usually supported natively by build systems, such as Buildroot or Yocto.
View full article
Here is a quick summary at booting Linux on the i.MX 6 sabre sd platform. This assumes you already have u-boot working on your platform as described here. This implies you already have a "working" Linux development environment with some ARM cross-compilers at hand (e.g. Debian + Emdebian). Get Linux sources We will use git to fetch Linux sources:   $ git clone git://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git This should create a linux directory with all the latest sources (after a while). Note that for more stability you might want to checkout a release instead of the latest version; to do so, list the available release tags with e.g. git tag -l 'v*', and git checkout <the-desired-tag>. Compile Assuming your cross compiler is called e.g. arm-linux-gnueabihf-gcc, you can compile by doing:   $ cd linux   $ export ARCH=arm   $ export CROSS_COMPILE=arm-linux-gnueabihf-   $ make imx_v6_v7_defconfig   $ make You then need to supply a LOADADDR (as joowonkim pointed out); do:   $ make uImage LOADADDR=0x10008000 This should create a number of files, including arch/arm/boot/uImage and arch/arm/boot/dts/imx6q-sabresd.dtb. Put on SD We need a proper FAT partition on the SD card, from which u-boot will be able to load the kernel and dtb. Also, we need to make sure we leave some space for u-boot starting from offset 1024B. Here is an example SD card layout:   +-----+------+--------+-----+----------------   | MBR |  ... | u-boot | ... | FAT partition ...   +-----+------+--------+-----+----------------   0     512    1024           1M (offsets in bytes) Here is an example SD card layout, as displayed by fdisk:   Device    Boot      Start         End      Blocks   Id  System   /dev/sdc1            2048     8054783     4026368    c  W95 FAT32 (LBA) (units: 512B sectors) You can format the FAT partition, mount, copy and unmount with:   $ mkfs.vfat /dev/<your-sd-card-first-partition>   $ mount /dev/<your-sd-card-first-partition> /mnt   $ cp arch/arm/boot/uImage arch/arm/boot/dts/imx6q-sabresd.dtb /mnt/   $ umount /mnt Your SD card first partition is typically something in /dev/sd<X>1 or /dev/mmcblk<X>p1. Note that you need write permissions on the SD card for the command to succeed, so you might need to su - as root, or use sudo, or do a chmod a+w as root on the SD card device node to grant permissions to users. Also, be sure to have u-boot on the SD card as explained in this post. Boot! That's it; u-boot already knows how to deal with your kernel by default so you are good to go. Insert the SD card into the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. You should see u-boot messages:   U-Boot 2013.07-rc1-00014-g74771f4 (Jun 21 2013 - 16:27:39) u-boot should load the uImage and dtb from SD card and boot the kernel:   (...)   reading uImage   4215344 bytes read in 449 ms (9 MiB/s)   Booting from mmc ...   reading imx6q-sabresd.dtb   22818 bytes read in 22 ms (1012.7 KiB/s)   ## Booting kernel from Legacy Image at 12000000 ...      Image Name:   Linux-3.10.0-rc6      Image Type:   ARM Linux Kernel Image (uncompressed)      Data Size:    4215280 Bytes = 4 MiB      Load Address: 10008000      Entry Point:  10008000      Verifying Checksum ... OK   ## Flattened Device Tree blob at 11000000      Booting using the fdt blob at 0x11000000      Loading Kernel Image ... OK   OK      Using Device Tree in place at 11000000, end 11008921   Starting kernel ... The kernel should boot:   Booting Linux on physical CPU 0x0   Linux version 3.10.0-rc6 (vstehle@debian) (gcc version 4.7.2 (Debian 4.7.2-5) ) #1 SMP Fri Jun 21 18:09:26 CEST 2013 By default, the kernel will try to mount a root filesystem from the SD card second partition, as can be read in the default kernel command line:   (...)   Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw ...but we did not prepare a root filesystem partition, so after a number of boot messages the kernel will wait indefinitely:   (...)   mmc1: new SDHC card at address b368   (...)    mmcblk0: p1   (...)   Waiting for root device /dev/mmcblk1p2... We will see in another post how to prepare this root filesystem on the second SD card partition. Enjoy! See also... If you plan to compile Linux often, you might want to use a C compiler cache; see this post. Once you have Linux booting on your platform the next step is to give it a root filesystem. See this post for a Debian root filesystem, this post for a minimal busybox filesystem and this post for generating a root filesystem with buildroot.
View full article
Here is a quick summary at booting u-boot on the i.MX 6 sabre sd platform. This assumes you already have a "working" Linux development environment with some ARM cross-compilers at hand (e.g. Debian + Emdebian). Get u-boot sources We will use git to fetch the U-Boot sources:   $ git clone git://git.denx.de/u-boot.git This should create a u-boot directory with all the latest sources. Note that for more stability you might want to checkout a release instead of the latest version; to do so, list the available release tags with e.g. git tag -l 'v2*', and git checkout <the-desired-tag>. Compile Assuming your cross compiler is called e.g. arm-linux-gnueabihf-gcc, you can compile by doing:   $ cd u-boot   $ export CROSS_COMPILE=arm-linux-gnueabihf-   $ make mx6qsabresd_config   $ make This should create a number of files, including u-boot.imx. Put on SD U-boot should reside at offset 1024B of your SD card. To put it there, do:   $ dd if=u-boot.imx of=/dev/<your-sd-card> bs=1k seek=1   $ sync Your SD card device is typically something in /dev/sd<X> or /dev/mmcblk<X>. Note that you need write permissions on the SD card for the command to succeed, so you might need to su - as root, or use sudo, or do a chmod a+w as root on the SD card device node to grant permissions to users. Boot! Your SD card is ready for booting. Insert it in the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data, power up the platform and you should see something like:   U-Boot 2013.07-rc1-00014-g74771f4 (Jun 20 2013 - 19:05:09)   CPU:   Freescale i.MX6Q rev1.2 at 792 MHz   Reset cause: POR   Board: MX6Q-SabreSD   DRAM:  1 GiB   MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2   *** Warning - bad CRC, using default environment   In:    serial   Out:   serial   Err:   serial   Net:   FEC [PRIME]   Warning: FEC using MAC address from net device   Hit any key to stop autoboot:  0 Enjoy! See also... u-boot most common mission is to boot the Linux kernel. See this post for details on how to do it. If you plan to compile u-boot often, you might want to use a C compiler cache; see this post. Running a Script in U-boot u-boot on the Vybrid tower board in a few commands
View full article
There is GPU SDK for i.MX6D/Q/DL/S: IMX_GPU_SDK.  This is to share the experience when compiling the example code from the SDK with Linux BSP release: L3.0.35_1.1.0_121218 and  L3.0.35_4.0.0_130424 . Minimal profile is using and have been verified on both i.MX6Q SDP and i.MX6DL SDP. To start: Please make sure “gpu-viv-bin-mx6q” has been selected in the Package list and compiled to your rootfs. After finished the compilation of the rootfs, you should find some newly added libraries for GLES1.0, GLES2.0, OpenVG and EGL in <ltib>/rootfs/usr/lib However, you should find libOpenVG.so is actually copied from libOepnVG_3D.so: vmuser@ubuntu:~/ltib_src/ltib/rootfs/usr/lib$ ls -al libOpen* -rwxr-xr-x 1 root root 115999 2013-06-06 18:31 libOpenCL.so -rwxr-xr-x 1 root root 515174 2013-06-06 18:31 libOpenVG_355.so -rwxr-xr-x 1 root root 272156 2013-06-06 18:31 libOpenVG_3D.so -rwxr-xr-x 1 root root 272156 2013-06-06 18:31 libOpenVG.so So, in this way, i.MX6D/Q will no use libOpenVG_355.so in the build. Also, if you run NFS, the libOpenVG.so will change to symbolic link:           For example, run on i.MX6Q SDP, it will link to /usr/lib/libOpenVG_355.so                          For example, run on i.MX6DL SDP, it will link to /usr/lib/libOpenVG_3D.so                Then, when you compile the OpenVG example code, it is becoming very confusing.  Thus, it needs to pay attention when doing the compilation.  For example, delete the symbolic link and make copy of the corresponding library: For i.MX6D/Q, please do this: $ sudo /bin/rm libOpenVG.so $ sudo cp libOpenVG_355.so libOpenVG.so For i.MX6S/DL, please do this: $ sudo /bin/rm libOpenVG.so $ sudo cp libOpenVG_3D.so libOpenVG.so To compile the sample code in the GPU SDK, you could refer to iMXGraphicsSDK_OpenGLES2.0.pdf or iMXGraphicsSDK_OpenGLES1.1.pdf in ~/gpu_sdk_v1.00.tar/Documentation/Tutorials to set up the cross compilation environment; which is assuming the LTIB and the rootfs is ready. $ export ROOTFS=/home/vmuser/ltib_src/ltib/rootfs $ export CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi- For OpenVG: $ cd ~/gpu_sdk_v1.00/Samples/OpenVG $ make -f Makefile.fbdev clean $ make -f Makefile.fbdev $ make -f Makefile.fbdev install The executable will then be copied to this directory: ~/gpu_sdk_v1.00/Samples/OpenVG/bin/OpenVG_fbdev For GLES2.0 $ cd ~/gpu_sdk_v1.00/Samples/ GLES2.0 $ make -f Makefile.fbdev clean $ make -f Makefile.fbdev $ make -f Makefile.fbdev install The executable will then be copied to this directory: ~/gpu_sdk_v1.00/Samples/ GLES2.0/bin/GLES20_fbdev For GLES1.1, please modify the Makefile.fbdev to remove the compilation of example codes "18_VertexBufferObjects" and "19_Beizer" that are not exist. Then, $ cd ~/gpu_sdk_v1.00/Samples/ GLES1.1 $ make -f Makefile.fbdev clean $ make -f Makefile.fbdev $ make -f Makefile.fbdev install The executable will then be copied to this directory: ~/gpu_sdk_v1.00/Samples/ GLES1.1/bin/GLES11_fbdev Finally, you could copy the executable to the rootfs and test on i.MX6Q SDP/SDB or i.MX6DL SDP board. NOTE: the newly added makefiles.tgz contains Makefile.x11 hacked from GLES2.0 example code to make OpenVG to compile and run on Ubuntu 11.10 rootfs.
View full article
The customer would like to test BT.656 using Test mode. Is it supported? 38.4.3.3 Test mode in RM shows only one CSIx_SENS_CONG setting. Does it mean Test mode support only one as follows? Does Test mode support other settings? CSIx_EXT_VSYNC = 0x1 CSIx_DATA_WIDTH = 0x1 CSIx_SENS_DATA_FORMAT = 0x0 CSIx_PACK_TIGHT = 0x0 CSIx_SENS_PRTCL = 0x1 CSIx_SENS_PIX_CLK_POL = 0x1 CSIx_DATA_POL = 0x0 CSIx_HSYNC_POL = 0x0 CSIx_VSYNC_POL = 0x0 For example, customer want to know if Test mode support  CSIx_SENS_PRTCL=0x2or 0x3 instead of 0x1? customer want to know if Test mode support CSIx_SENS_DATA_FORMAT=0x1or 0x2 instead of 0x0? Answer: CSI CM TEST MODE is working as below: 1,only ungated mode. 2,data width should be configured to 8 3,data format should be configured to rgb888 It cannot be other format such as bt656. It uses CSI1_TST_CTRL register to configure {R,G,B} 24 bit value and taking it as RGB888/YUV444 format for further process.  The generated image size is due to the configured width & height in the registers.
View full article
The i.MX6 Multi-Mode DDR Controller (MMDC) has profiling capabilities to monitor the operation of the controller. The profiling capability counts certain events related to a specified AXI-ID during a profiling period. The events that can be counted are: The number of read accesses during the profiling period (MMDCx_MADPSR2[RD_ACC_COUNT] register field) The number of write accesses during the profiling period (MMDCx_MADPSR3[WR_ACC_COUNT] register field) The number of bytes read during the profiling period (MMDCx_MADPSR4[RD_BYTES_COUNT] register field) The number of bytes written during the profiling period (MMDCx_MADPSR5[WR_BYTES_COUNT] register field) The number of MMDC clock cycles during which the MMDC state machine is busy (MMDCx_MADPSR1[BUSY_COUNT] register field) BUSY_COUNT is the number of MMDC clock cycles during the profiling period in which the MMDC state machine is not idle. So this is the time the MMDC spends doing any activity, not just read or write data transfers. The MMDC state machine is active whenever there are any read or write requests in the read and write FIFOs. The MMDC is active during many operations that are not reading or writing data such as arbitration of requests, control cycles, bank open/close, etc. So BUSY_COUNT represents the number of cycles when the controller is busy, not just the number of cycles when the external bus is busy. The number of bytes read and bytes written can be used to determine data throughput and the BUSY_COUNT can be used to determine what part of the time the controller is active/idle. Together these can be used to determine the controller efficiency for a particular application. For detailed information, see the "MMDC profiling" section of the MMDC chapter in the reference manual for the SoC being used.
View full article