MPC5604B_FLASH.lcf file Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5604B_FLASH.lcf file Configuration

1,536件の閲覧回数
qm1013
Contributor III

hello, I have some problems about how to configure the .lcf file in codewarrior 10.7, bellow is the memmap.h file and MPC5604B_FLASH.lcf file. 

Can you help me to modified the MPC5604B_FLASH.lcf file according to the memmap.h file ?

When I configured ,it encounter many mistakes.

Thank you very much.

memmap.h

#ifdef SBL_START_BEGIN
#pragma push
#pragma section R ".SBL_START"
#ifndef QAC
__declspec(section ".SBL_START")
#endif
#undef SBL_START_BEGIN
#endif

#ifdef SBL_START_END
#pragma pop /* Load the previous state */
#undef SBL_START_END
#endif

/* Section limiters for signature of body of SBL */
#ifdef SBL_BODY_BEGIN
#pragma push /* Save the current state */
#pragma section code_type ".SBL_BODY" code_mode=far_abs
#undef SBL_BODY_BEGIN
#endif

#ifdef SBL_BODY_END
#pragma pop /* Load the previous state */
#undef SBL_BODY_END
#endif

/* Section limiters for signature of end of SBL */
#ifdef SBL_END_BEGIN
#pragma push
#pragma section R ".SBL_END"
#ifndef QAC
__declspec(section ".SBL_END")
#endif
#undef SBL_END_BEGIN
#endif

#ifdef SBL_END_END
#pragma pop /* Load the previous state */
#undef SBL_END_END
#endif

MPC5604_FLASH.lcf

/* Internal FLASH linker command file for MPC5604B */
/* */
/* 512KB Flash, 32KB SRAM */
/* */
/* Intended to be used for the stationary example project. */
/* */
/* VERSION: 1.1 */
/* */

MEMORY
{
/*FLASH: 0x00000000 - 0x00007FFFF*/

/* Fixed location required for RCHW and program entry point. */
resetvector: org = 0x00000000, len = 0x00000008

/* Contains initializations from __ppc_eabi_init.c,
MPC56xx_HWInit.c, MPC56xx_init_*.c and the entry point (__startup).
*/
init: org = 0x00000008, len = 0x00000FF0

/* Contains interrupt branch tables for both core and INTC module
and the ISR handlers code. Note, since the vector base address field
of IVPR is defined within the range [0:19] the table must be loaded
at an address aligned to 4K boundary.
*/
exception_handlers: org = 0x00001000, len = 0x00002000

/* Space allocated for user code and device initialization.
ROM Image address should be set with the start address of this
segment in order to instruct the runtime to initialize the
static variables. All the section above are ignored for this action.
Please see -romaddr linker option.*/
internal_flash: org = 0x00003000, len = 0x0007D000

/* SRAM: 0x40000000 - 0x40007FFF */
internal_ram: org = 0x40000000, len = 0x00006000 /* 24K */
heap : org = 0x40006000, len = 0x00001000 /* 4K */
stack : org = 0x40007000, len = 0x00001000 /* 4K */
}

/* This will ensure the rchw and reset vector are not stripped by the linker */
FORCEACTIVE { "bam_rchw" "bam_resetvector" }

SECTIONS
{
.__bam_bootarea LOAD (ADDR(resetvector)): {} > resetvector

GROUP : {
/* Section used for initialization code: __ppc_eabi_init.c,
MPC56xx_HWInit.c, MPC56xx_init_*.c and the entry point (__startup).
*/
.init LOAD(ADDR(init)) : {}
.init_vle (VLECODE) LOAD(_e_init) : {
*(.init)
*(.init_vle)
}
} > init

GROUP : {
/* Fixed length of 0x800 is required for core interrupt branch table.
Core IVOR branch table entries must be aligned to 16 bytes.
*/
.ivor_branch_table (VLECODE) LOAD(ADDR(exception_handlers)) ALIGN (0x10) : {}

/* Note if intc_hw_branch_table is used it MUST be loaded at the IVPR + 2KB (0x800).
For this device the intc_hw_branch_table should contain entries aligned to 4 bytes.
*/
.intc_hw_branch_table (VLECODE) LOAD(_e_ivor_branch_table) ALIGN(0x800) : {}

/* ISR handlers code.*/
.__exception_handlers (VLECODE) LOAD(_e_intc_hw_branch_table) : {}
} > exception_handlers

GROUP : {
.text : {}
.text_vle (VLECODE) ALIGN(0x08): {
*(.text)
*(.text_vle)
}
.rodata (CONST) : {
*(.rdata)
*(.rodata)
}

.ctors : {}
.dtors : {}
extab : {}
extabindex : {}
} > internal_flash

GROUP : {
/* The INTC module for this device contains up to 221 IRQs.*/
.__uninitialized_intc_handlertable ALIGN(2048) : {}
.data : {}
.sdata : {}
.sbss : {}
.sdata2 : {}
.sbss2 : {}
.bss : {}
} > internal_ram
}

/* Freescale CodeWarrior compiler address designations */

_stack_addr = ADDR(stack)+SIZEOF(stack);
_stack_end = ADDR(stack);
_heap_addr = ADDR(heap);
_heap_end = ADDR(heap)+SIZEOF(heap);


/* Exceptions Handlers Location (used in Exceptions.c IVPR initialization)*/
EXCEPTION_HANDLERS = ADDR(exception_handlers);

/* L2 SRAM Location (used for L2 SRAM initialization) */
L2SRAM_LOCATION = ADDR(internal_ram);

/* How many writes with stmw, 128 bytes each, are needed to cover
the whole L2SRAM (used for L2 SRAM initialization) */
L2SRAM_CNT = 0x8000 / 128;

0 件の賞賛
返信
0 返答(返信)