MPC5777M: XBIC Master/Slave Numbering

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777M: XBIC Master/Slave Numbering

743 Views
D75
Contributor I

Hello,

I am seeking clarification on the numbering used for masters and slaves in XBIC_0 and XBIC_1 on the MPC5777M.

When attempting to inject an error on XBIC_0 during a write transfer from core 2 (the IOP core) to internal SRAM, I followed the XBAR port numbering and selected master 4 and slave 4. However, no error was detected—the write transfer completed normally. If I select master 2 instead — which seems unrelated to the expected data path — an error is detected.

I have observed similar behavior on XBIC_1: using master 4 does not result in the expected error detection, while selecting master 2 does.

Could anyone confirm the correct numbering for masters and slaves in XBIC_0 and XBIC_1? Are the XBIC and XBAR numberings different?

Thank you in advance!

Tags (1)
0 Kudos
Reply
1 Reply

606 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

XBIC chapter uses term 'master ID' what could be logical ID probably as follows:

image.png

 

0 Kudos
Reply