コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
NXP’s latest and most powerful Microprocessor requires the latest and fastest memories to keep it running efficiently. During this session, we will discuss the new memories supported on the new i.MX 8 processor family. For DRAM, this will include DDR4 and Low Power DDR4. For non-volatile memory this will include Octal SPI NOR (XccelaTM Flash) which offers up to 400MB/s as well as the latest eMMC 5.X devices that also support high speeds. These devices are offered with Commercial, Industrial or Automotive temperature and quality ratings. I will include a section on packaging technologies that can provide designers with innovative ways to reduce size. These include Package on Package and Multi-Chip Packages. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8 systems. Micron will be giving away 2-1/2” 120GB SSDs to the first 50 attendees of this session.
記事全体を表示
Explain 3-phase motor control fundamentals with an overview of NXP’s hardware and software enablement solutions for motor control applications.
記事全体を表示
Course will provide an overview of the “Classical Machine Learning Toolbox” developed by the IoT Solutions team, along with an example integration with Microsoft Azure ML.
記事全体を表示
Learn how to move from physical to virtual network functions (VNFs) on ARM QorIQ platforms using KVM virtual machines and Docker containers with native DPAA2 and virtual virtio devices. Leverage packet processing, crypto acceleration and advanced offloads from DPDK/ODP and Linux native guest applications. Connect VNFs through virtual switching either using optimized user space implementations or offloading datapath into DPAA2 Advanced IO Processor. Make use of the switching functions provided by DPAA2 integrated Edge Virtual Bridge and L2 Switch. Leverage OPNFV integration and take advantage of distributed VNFs via Service Function Chaining.
記事全体を表示
This session explores the fast-growing vehicle gateway market and new applications for vehicle network processing. It will identify key use cases and requirements, and provide insights into how gateways will evolve over the next decade.
記事全体を表示
With a number of vehicles being connected to the internet, the need to have a secure environment inside the vehicle is increasing. This session will present secure use cases for edge nodes microcontroller in the vehicle and how the S32K can achieve them. Topics including what is security, NXP 4 layer of automotive security, and S32K CSEc.
記事全体を表示
AMP has been developing new market leading MCU solutions for the safety, electrification and powertrain markets. This presentation will go into the detail of the products and demonstrate their value in the target applications.
記事全体を表示
During that session, attendees will learn how to integrate NFC readers component into an industrial or consumer devices, from PCB layout to FCC certification and covering considerations for antenna design, software development and specific application certification requirements like EMVCo.
記事全体を表示
Many people involved in the electronics industry need a basic knowledge of semiconductor components in order to understand issues like manufacturing cycle time, semiconductor fab consolidation and failure analysis results. This session is geared towards a non-technical audience and gives a high-level overview of semiconductor devices and how they are made. The lecture begins with a brief overview of how semiconductor devices work. The bulk of the presentation describes the generic manufacturing flow for semiconductor devices with an emphasis on the complexity of the equipment/facilities used and the process time required.
記事全体を表示
The number of ECUs in a car is increasing dramatically on a year by year basis. Modern cars are starting to introduce the concept of centralizing multiple domains (Infotainment, ADAS, etc.) in a single ECU and separate them using technologies like virtualization, multicore or multiple SOCs. Although separated, these entities need to communicate and implementing a software communication solution which is scalable, portable, open and easy to program is key to offering a complete software enablement to our customers. This session will present NXP software solution for communication within a domain and between domains controllers in an ECU.
記事全体を表示
Security has never been more critical than it is today. Learn how the QorIQ Trust Architecture can be leveraged to increase the security of your design. Different phases in a product's life cycle can expose different vulnerabilities for attackers to exploit. This session covers secure device life cycle management as a concept, while also providing specific examples of secure implementations using QorIQ Trust Architecture.
記事全体を表示
Ethernet adoption in new OEM platforms is accelerating, as a result of increased media, communication, and ADAS streams between different end points in vehicles. The required Quality of Service and synchronization is typically achieved through the implementation of Audio Video Bridging (AVB) specifications, or derivatives of AVB. NXP has a unique position in the market given our capability to offer a full solution for AVB in the car, from end points (MPUs as well as MCUs), PHYs, switches, plus the needed software stacks. In addition, the software stacks are full featured, including critical but often initially forgotten components such as Media Clock Recovery. Get an introduction to the basis of the AVB technology, and how NXP can help you deploy AVB in your products.
記事全体を表示
Hands-on workshop using the low cost KIT-HGDRONEK66 HoverGames drone reference platform for small autonomous vehicles. Learn about the open source PX4 flight stack vehicle manangement unit, NuttX RTOS, Mavlink, DDS RTPS services, associated Linux companion computer and Qgroundcontrol groundstation for vehicle configuration and flight logging and planning. Learn by example compiling the code and adding new functions within the PX4 modular software framework. Discover interfacing to Rapid-IOT via MAVLINK.
記事全体を表示
Emerging trends in automotive vision processing for ADAS and AV systems. NXP roadmap to meet the requirements.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.
記事全体を表示
In this class, participants will learn how to leverage model-based design technology (MATLAB/Simulink) to quickly develop motor control algorithms for BLDC, ACIM, and PMSM motors using NXP S32K MCUs on the S32K144 automotive reference platform. Learn the basics of the motor control toolbox to generate C-code from simulation models. The toolbox will be utilized demonstrating peripheral driver blocks, optimized automotive math/motor control blocks, software and processor in the loop techniques for algorithm verification, as well as other utilities for MCU profiling and algorithm development.
記事全体を表示
Learn how NXP provides support for ODP and DPDK without sacrificing performance. Learn how we're leveraging specific acceleration advantages of the NXP data plane architectures, such as packet IO, classification, scheduling, crypto, etc. This session will provide a comparative analysis and evolution of both of these open-source, platform independent and vendor-neutral standard APIs for optimized packet processing and traditional networking services in user space. It will help you choose the right API for your project, based on design requirements.   We will also cover how the ODP and DPDK can provide the necessary infrastructure for virtualized environments.
記事全体を表示
In the last 10 years, Green Hills has observed carmaker and Tier 1 customers expand from the traditional segments of powertrain, airbags and braking ECUs into graphics-rich dashboards, open source operating sytems and the secure Connected Car. A leading requirement is ECU consolidation while keeping ASIL safety intact. This requires the run-time architecture to safety and securely run guest operating systems Linux or Android on the same single core (or across multiple cores as SMP) alongside safety or security-critical applications like instrument clusters, gateways, V2X and ADAS. Here, we'll take a closer look at the customer’s pain points and goals, and we’ll summarize various industry solutions, including the INTEGRITY Multivisor secure hypervisor.
記事全体を表示
This course will provide an in-depth system analysis of High Voltage (HV) Electric. We review how the MCU, GDIC and IGBTs function individually and as a system. We will discuss EV and HEV power systems and components for achieving a highly efficient and safe HV motor drive. Using system block diagrams and oscilloscope screen shots of NXP’s new HV IGBT GDIC, the GD3100, and Fuji GEN 7 IGBT modules as we will consider how to achieve smaller, more efficient and lower cost HV inverter designs. We will review SPI interface programmability that enables any IGBT to be tuned for maximum efficiency, thermal design considerations, layout considerations, power budget assessment, power up sequencing, managing short circuit faults, temperature monitoring and advanced features achieve system ASIL level D and ISO26262 certification.
記事全体を表示
Introduction to the ISO26262/EC61508 standard - with emphasis on how to apply it, cross BL designing for advanced functional safety requirements- ASIL B/C/D.
記事全体を表示