コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
NXP provides total USB Type-C AC/DC solutions with higher Power density, security and safety with leading technologies that enables time to market, solving application challenges and complying to key global Power regulations. NXP solution supports USB-PD, BC1.2 and Leader in QC4.0+. Resonant AC/DC supplies have superior efficiency at high power output. The TEA1916+ TEA1995 is a digital controller simplifying the complexity of resonant LLC designs and providing easy tuning. It succeeds the very popular TEA1716 used in many resonant Switch Mode Power Supplies for e.g. PC's & TV's, but the TEA1916 is actually very suitable for any power supply > 75W, e.g. medical, industrial and server power supplies. The TEA1916 uses a new digital cycle-by-cycle architecture (Vcap control) to enable a new type of operation at low-power loads.
記事全体を表示
NXP leads in the ability to integrate the sensing transducers with the algorithmic computations and the wireless communication channels for TPMS solutions. Leading car OEMs, Tier1s and even tire manufacturers have started to consider and use BLE instead of the standard UHF-band RF interface in TPMS applications. Join this training session to learn about the changing dynamics in TPMS wireless connectivity and the relative merits driving these changes. Further learn about NXPs steps to support these changes with the introduction of a BLE enabled TPMS demo.
記事全体を表示
The GD3100 is a  programmable high-voltage gate driver with advanced functional safety (FuSa), control, and protection features, developed for automotive and eMobility applications. This presentation will give a brief review of HV power devices such as Si IGBTs and WBG MOSFETs. Then the talk will focus on key features of the GD3100 that are important for implementation of high traction inverters, DC/DC converters, or on-board chargers (OBCs) using Si IGBTs or SiC MOSFETs.
記事全体を表示
DDR tools overview. Part 1, DDR test tool features and capabilities. Part 2, DDR configuration tool features and capabilities, benefits of each for the end users.
記事全体を表示
Start using UUU i.MX family. An overview of the new firmware download tool called Univeral Update Utility that has replaced the manufacturing tool.
記事全体を表示
Introduction to NXP’s state-of-the-art 1-chip next generation software defined radio(SDR) system solution covering global radio reception standards (Mercury family).
記事全体を表示
i.MX RT has a flexible external SPI Flash interface, which supports all existing SPI protocols. However, Serial Flash products may vary in READ performance due to the number of I/O, command protocols and the maximum frequency. Serial Flash Read performance has a direct impact on the system bootup time as well as code execution efficiency. In an advanced system design where system code is shadowed from Flash to DRAM, the initial boot time depends on the data transfer time from Flash to DRAM. In a cost-efficient system design, DRAM is reduced or eliminated since the processor will be able to fetch execution instructions directly from the Flash to the internal cache. During code fetching, a fixed length of data (typically 32- or 64-Byte) is read out from the flash. Shortening the overall 32-Byte or 64-Byte Read time will greatly reduce processor’s wait cycle, leading to improvement on XiP efficiency.
記事全体を表示
The hottest topic in automotive design today is the concept of the eCockpit -- where all visual functions in the car are controlled across multiple screens and fully integrated for the driver’s convenience. The key technology that enables eCockpit to run on a single processor also offers new capabilities in industrial, embedded and consumer products such as drones, manufacturing HMI interfaces and smart displays. This class will cover the fundamental technologies and architectural techniques in the i.MX 8 processor which enables rich eCockpit functionality, how NXP has implemented the world’s most significant full chip virtualization capabilities in an ARM-based processor and breaks down the eCockpit demo from the Tech Lab.
記事全体を表示
i.MX offers some of the most versatile platforms for multimedia and display applications. Join this session to get an in depth view of how i.MX 8/8X’s multimedia systems, including GPU, Display, Vision, Virtualization and Machine Learning come together to provide customers with a scalable set of powerful media capabilities for auto infotainment.
記事全体を表示
Hands-on: Quick introduction into non-AUTOSAR software solutions based on NXP S32 SDK. How to create an automotive application featuring secure CAN communication. Integration with S32 Design Studio IDE, tips and tricks.
記事全体を表示
This session will go into the detail of the software enablement around the BlueBox v2.0, aka “BlueBox Mini” or “BLBX2”. Suited for level 2/3 autonomous drive. From an engineering perspective topics will include: 1. The BlueBox v2.0 hardware layout. 2. BSP content with middleware; Linux config and Ubuntu rootfs; Linux options between and inter-communication between them; Discussion of middleware options (including ROS versions, and others). 3. How ADAS is supported. 4. Combined to achieve level 2/3 ADAS with AutonomouStuff. 5. Apollo versions ported and benchmarking of the planning module. 6. Future offerings with hardware support and systems-level safety and orchestration. 7. Technical lecture explaining the internals of this enablement.
記事全体を表示
In Automotive, the need for communication between various ECUs has grown as the number of ECU’s have grown as well. Implementing a software solution which is scalable, portable, open and easy to program is key to offering a complete software enablement to our customers. This session will present our software solution for communication between multiple SOCs with different operating systems across  multiple physical areas.
記事全体を表示
The self driving car has a major impact on ECUs power and complexity and the network architecture connecting them together. The sheer fact that the driver is now a mere passenger with potentially limited options of taking back control raises significant functional safety questions that cannot be addressed with conventional approaches. In this presentation, we discuss how autonomous driving is impacting the functional safety requirements for automotive Ethernet switches and PHYs. We will review what functional safety for a component really means, going beyond marketing figures and ticking off feature lists. Finally, we will discuss how NXP is attacking this challenge in our current portfolio with a hint to the products to come.
記事全体を表示
Introduction to A100x secure authenticators including new A1007, as part of overall training authentication protocols, what to look for in security IC and potential use cases.
記事全体を表示
This one hour session will introduce the architecture, block diagrams and products of NXP’s electric vehicles (EV) and hybrid electric vehicles (HEV) portfolio for electric drive trains. Areas of focus include battery management, microprocessors for drive control, system basis chips, IGBT and MOSFET gate drivers and power modules for high voltage and 48V inverters. A leader in functional safety, NXP’s safety case for EV and HEV will be discussed. How we enable the customer design through evaluation boards, software and reference designs will be reviewed.
記事全体を表示
Introduction to new features introduced by AUTOSAR 4.3.0 and an overview of the NXP AUTOSAR portfolio for the NXP microcontrollers and processors. Introduction to the AUTOSAR ADAPTIVE platform.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
This session will address how S12 MagniV mixed-signal MCUs can help customers design more compact and cost-effective electronic control units. The S12 MagniV devices are built on proven S12 technology, enabling software and tool compatibility across the entire portfolio. With the right blend of digital programmability and high-precision analog, plus a portfolio of scalable memory options, the S12 MagniV portfolio streamlines automotive design.
記事全体を表示
In this presentation, we are going to highlight the use of Model-Based Design processes for Vehicle Dynamics and Body Controller that involves electric drives which are typically used by OEM and Tiers 1 for product development. The primary benefit of Model-Based Design is the ability to cover traceability between design artifacts produced as a part of the design process. A traceability path from requirement management tool to software model, code, and finally tests in the hardware-in-the-loop environment is demonstrated. A typical PMSM Field Oriented Control application will be used to demonstrate all the steps shown above using NXP S32K Motor Kit.
記事全体を表示
A guide to using HAB on i.MX family of processors. Learn features and tools available to help deploy signed and encrypted images.
記事全体を表示