i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
New i.mx6Q core board from OpenEmbed.com
查看全文
Hi all, I shared my test results and solutions in attachments. Best regards, Carl
查看全文
NOTES: Empty cells do not mean there is no bitbake parameter for the corresponding ltib one. This is still work in progress. Both engines are completely different and doing a one-to-one comparison is not actually fair. The following tables compare the two core build tools, ltib for LTIB and bitbake for the Yocto Project (YP, hereafter). For YP, there is another important tool called HOB,  when appropriate, we add comments on the Comment's column. There are two main tables, 'ltib modes versus bitbake' 'ltib options versus bitbake'.          We split in two based how ltib splits its parameter, so the order is the same as the one shown when typing './ltib --help'. LTIB comes in every released BSP, follow the User Guide to install it. The command 'ltib' is a script located on the folder with the same name, so all ltib commands should be run with './' as prefix YP can be seen of a series of layers (folders). To download these, including the Freescale layers, follow this link. The command 'bitbake' must be installed independently, you can either use the package manager of you OS (e.g. sudo apt-get install bitbake on Ubuntu) or download the source code and do the setup manually. Both ways should place the bitbake script into a executable path. ltib modes versus bitbake Mode description ltib command bitbake command Comment Just prep the package ltib -m prep -p <package> bitbake <package> -c patch With bitbake when running the patch task, it executes two lower tasks: fetch and unpack. For example, if one wants a untouched (no yocto patches) kernel, one can try: 'bitbake linux-imx -c unpack' and code unpacked code is placed on tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/<version>/git/ rpmbuild -bc --short-circuit ltib -m scbuild -p <package> bitbake <package> -c compile With bitbake running compile also runs a lower task: configure. rpmbuild -bi --short-circuit ltib -m scinstall -p <package> bitbake <package> -c With ltib the install task executes the %Install section of the package's spec. With bitbake the same task executes all related package's recipe install functions, e.g. do_install. Note: with ltib running a higher task (like scinstall) will not execute lower tasks (like scbuild and prep); this is not the case for bitbake: it runs lower tasks automatically. does an scinstall followed by an install to the rootfs ltib -m scdeploy -p <package> bitbake <package> -c build With bitbake, build is the default task, so one can even omit the -c build parameter, e.g. 'bitbake <package>' generate and merge a patch (requires -p <pkg>) ltib -m patchmerge -p <package> NA This is a pretty nice feature from LTIB, unfortunately with bitbake the command does not exit. For example, to patch the Kernel's recipe, take a look at this procedure. In case you follow all these steps to fix a bug, do not forget to send your patch to the community. lean/uninstall target packages ltib -m clean -p <package> NA With bitbake the 'clean' counterpart does not exit. If one needs to remove a specific package from a build, you may remove it from the image configuration file (e.g. file meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, remove item on IMAGE_INSTALL variable); if package is inside a package group (e.g. ./meta-fsl-demos/recipes-fsl/packagegroup/packagegroup-fsl.bb) you may remove it there. After this change, bitbake again and the resulting image won't have the package. With HOB, this is much simpler due to its Graphical User Interface. Just type hob on your build directory, select the machine and the base image, then click on the 'Edit Image'. On that window you can easily deselect packages. Once deselection is done, build the image. full cleanup, removes nearly everything ltib -m distclean NA With bitbake the 'distclean' command does not exit. The way to remove all the built, remove the build/tmp folder. Be careful, next time you run bitbake, all tasks for all packages will be executed, in other words, you will start from scratch. list packages (alphanumeric) ltib -m listpkgs non-GUI: bitbake -g fsl-image-gui && cat pn-depends.dot GUI: bitbake -g -u depexp fsl-image-gui A bit more complex non-GUI: bitbake -g <image> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq list package names and licenses ltib -m listpkgseula NA With HOB, you can see every package name name and its licence. Just type hob, then select the machine and image, and click on the 'Edit Image' button. On the 'All recipes' tab, you get a list of packages with their licenses. list packages in twiki format ltib -m listpkgstw NA list packages in a format for import into spreadsheet ltib -m listpkgscsv NA make a binary release iso image ltib -m release NA make a non-distributable test iso release ltib -m trelease NA configure selected platform (no build) ltib -m config NA There is no way to open a configuration menu with bitbake. Instead, you can use hob. With hob, things are much easier. Just type hob under the build folder and you can select the machine and the image. If the image you want does not fit to the ones already available, you can add packages manually and even store your new tuned image. NOTES: 1. On YP, an image is a similar concept as LTIB's package profile (usually called just profile). There are many predefined images which can be used as starting point, so type 'bitbake <image name>'. 2. In case the kernel needs to be configure, run 'bitbake linux-imx -c menuconfig'. sub-platform selection (no build) ltib -m selectype NA The selectype on LTIB opens two menus: 1. Platform and the Package Profile selection 2. Configuration menu (the same menu as the one shown with -m config). In case one needs to do execute just the first task, just run 'bitbake <image name>'. In case you need to execute both, run hob. enter ltib shell mode (sets up spoofing etc) ltib -m shell bitbake <package name> -c devshell import srpms into ltib (semi-automatic) ltib -m addsrpms ltib options versus bitbake Option Description ltib command bitbake command Comments Root context number (0 is the primary and implicit) ltib --rootn | ltib -R operate on this package only ltib --pkg | ltib -p bitbake <package> With bitbake there is no need to add a '-' parameter, just use the package name without the .bb extension run the interactive configuration and build ltib --configure  | ltib -c NA See the mode -m config for more info run the sub-platform configuration and build ltib --selectype NA See the mode -m selectype for more info configuration file to build from (defaults to .config) ltib --preconfig bitbake <predefined image> With bitbake use any of the predefined images (assuming that these have not been modified), e.g. bitbake core-image-minimal or bitbake fsl-image-gui (it happens to be the smallest and the largest image, in terms of number of packages) profile file.  This is used to select an alternate  set of userspace packages, this is saved and used on later runs of ltib (e.g config/profiles/max.config) ltib --profile use this resource file ltib --rcfile <f> | ltib - r <f> batch mode, assume yes to all questions ltib --batch | ltib -b force rebuilds even if they are up to date ltib --force | ltib -f bitbake --force | bitbake -f For example, to force recompiling the kernel: bitbake linux-imx -c compile -f re-install rpms (but don't force rebuild) ltib --reinstall | ltib -e bitbake <package name> -c install -f remove (erase) rpm ltib --erase | ltib -E turn off install/uninstall dependency checks ltib --nodeps | ltib -n bitbake -b <somepath/somefile.bb> For example, to build just the kernel (no dependencies, just kernel): bitbake -b ../sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.0.35.bb NOTE: ALL dependencies should be already be installed, otherwise the command will fail don't force install rpms that have file conflicts ltib --conflicts | ltib -k keep the srpms after the build (deleted by default) ltib --keepsrpms | ltib -s more output ltib --verbose | ltib -v bitbake --verbose | bitbake -v On YP, the log can be too verbose, so one way to handle the amount of log is to store it and then grep it: bitbake linux-imx | tee log; grep -i <your string to seach> < log mostly a dry run (calls to system are just echos) ltib --dry-run | ltib -d bitbake --dry-run | bitbake -n try to continue on package build errors (autobuilds) ltib --continue | ltib -C bitbake --continue | bitbake -k print the application version and quit ltib --version | ltib -V bitbake --version do not redirect any output ltib --noredir | ltib -N run the deploy scripts even if build is up to date ltib --deploy | ltib -D bitbake <image name> -f disabled deployment (even with -p <pkg>) ltib --no-deploy just download the packages only ltib --dlonly bitbake -c fetchall <image name> E.g. bitbake -c fetchall core-image-minimal test that the BSP's packages are available ltib --dltest check against external staging repositories ltib --external leave the sources unpacked (only valid for pkg mode) ltib --leavesrc | ltib -l NA This is the default mode in YP. All source code can be found on tmp/work. In case you want to remove source code after building (as in LTIB), add INHERIT += "rm_work" to your local.conf. NOTE: If your adding changes to a particular package, these will be lost. In case you want to keep source code of a specific package, include this on the RM_WORK_EXCLUDE variable (e.g. RM_WORK_EXCLUDE += "busybox eglibc"). Make the selected root number sticky --sticky Remove root stickiness --no-sticky (re)configure/build/install the host support package set --hostcf use with package listings --enable use if you really want to ignore any locks (careful!) --ignorelock used with -m release to copy additional content --fullbsp used with -m release to copy specical packages into ISO --distmap don't check sudo, work around for broken sudo (fc9) --no-sudo use git for some package's build where use-git-mode is either: internal    Use fsl internal git external   Use fsl external git --use-git-mode use external git for some package's build --external-git help on usage --help | -h --help | -h
查看全文
Hi All, The new i.MX 6 SL L3.0.35_2.1.0 release is now available on the http://www.freescale.com/site. ·         Files available # Name Description 1 L3.0.35_2.1.0_LINUX_DOCS i.MX   6SoloLite Linux BSP Documentation. Includes Release Notes, Reference Manual,   User guide. API Documentation 2 L3.0.35_2.1.0_LINUX_MMDOCS i.MX 6SoloLite Linux Multimedia Codecs   Documentation. Includes   CODECs Release Notes and User's Guide 3 L3.0.35_2.1.0_ER_SOURCE i.MX   6SoloLite Linux BSP Source Code Files 4 L3.0.35_2.1.0_MM_CODECS i.MX   6SoloLite Linux Multimedia Codecs Sources 5 L3.0.35_2.1.0_AACP_CODECS i.MX   6SoloLite Linux AAC Plus Codec 6 L3.0.35_2.1.0_DEMO_IMAGE i.MX   6SoloLite Linux Binary Demo Files ·         Target HW boards o   i.MX6SL-EVK ·         New features o   Updated thermal equation for i.MX 6SoloLite o   Added Fuse check for all the devices o   Enabled DISPLAY power gating feature on TO1.2 ·         Known issues o   For known issues and limitations please consult the release notes.
查看全文
Share my test procedure in the attachment.
查看全文
When to improve kernel booting using hibernation [1], I found kernel initialized each component [2] took too much time. One solution is to remove unnecessary module to save time. Another approach is to delay those modules until user space up. Then it won’t lost some features just because hopes to gain benefit on booting speed. This is very useful since hibernation’s trigger point is at the late_initcall [3]. Kernel doesn't need do much module initialize since hibernate will restore those module status later. The detailed implementation is in the attached patch. [1]: hibernation is a technique to store system memory content to storage. Then the device can be shutdown and read the content back after power on. [2]: component means subsystem or driver. [3]: Consult kernel/power/hibernate.c, software_resume
查看全文
ERR005723           PCIe: PCIe does not support L2 Power Down   Description: When PCIe works as Root Complex, it can exit L2 mode only through reset. Since PCIe doesn't have a dedicated reset control bit, it cannot exit L2 mode.   Projected Impact: PCIe does not support L2 Power Down   Workarounds: The PCIe can be put in PDDQ mode to save on PCIe PHY power and wakeup only by the OOB (Out of Band) wakeup signal (since wakeup by a beacon from link partner is not supported) driven from the link partner (End Point). This signal could be used as a GPIO interrupt to exit this mode. The limitation of this workaround is that the link partner cannot be put into L2.   Proposed Solution:                 No fix scheduled   Linux BSP Status:                 No software workaround available   SW workaround used to fix ERR005723 in Linux BSP Why the original workarounds can’t be implemented in Linux BSP * PCIe controller doesn’t have the reset mechanism that can be used when re-insmod the PCIe driver without power down/up PCIe module. * During the PCie driver rmmod/insmod operations, the PCIe CLKs would be turned off/on. IC can’t guarantee that the PCIe PHY can work well and re-establish the PCIe link properly. One SIMPLE SW workaround for this errata imx: pcie: toggle bit18 of grp1 fix pcie can't exit L2 issue.   Set bit18 of gpr1 before enter into supend, and clean it after resume, can fix the following errata. Errata ERR005723_PCIe PCIe does not support L2 Power Down. About the details, please refer to the attached patch. "0001-imx-pcie-toggle-bit18-of-grp1-fix-pcie-can-t-exit-L2.patch"   The conception of the other SW workaround (System warm-reset) The procedures of the original suspend/resume. Suspend User suspend command echo mem > /sys/power/state All driver call suspend function SRPG,  ARM save all state to memory Enter Stop mode and Power down ARM   Resume:   GPC receive IRQ Wake up system Power on ARM domain. ROM code running Jump to SRPG point Recovery ARM status from memory Call all devices resume function.   Because PCIe only reset by system reset, we need change above follow. Resume:   GPC receive IRQ Wake up system Power on ARM domain. ROM code running Jump to SRPG point Warm Reset system, memory context will be kept. But all peripheral status lost. ROM code running Jump to SRPG point again. Recovery ARM status from memory Call all devices resume function. Resume function call init to initialize it.  And recover to the status saved before.   Impact: Can’t support usb remote wake up, which required 4ms responsive Longer latency, warm reset need some ms.  The recovery of the device status needs some more ms.   Risk:   Current BSP have not tested above follow Device driver have not supported this follow yet. Need additional work to enable \debug\test it.     Modules enabled in this workaround now: * UART * ENET * PCIe   Tests procedure. HW: one i.MX6Q SD boards, and one INTEL pciex1 1000M CT network card.   SW(The images used by me are attached):   * Apply the attached patches(kernel and uboot) to the kernel/uboot source codes, re-build, get the images. Kernel is based on imx_3.0.35_4.0 release, uboot , is based on imx_v2009.08 # build out SD/MMC and USB driver to make DRAM hibernate work     # build pcie in.   *procedure of the suspend/resume tests;     # unload ep's driver --> suspend/resume --> reload ep's driver.   NOTE: Please make sure that the command line contains “no_console_suspend” The command used to enable the console input wake up after login the consol: echo enabled > /sys/devices/platform/imx-uart.0/tty/ttymxc0/power/wakeup   Log when the INTEL CT 1G network card is used: -------------------------------log--------------------------------------------   PM: Syncing filesystems ... done.                                             start suspend Freezing user space processes ... (elapsed 0.01 seconds) done. Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done. add wake up source irq 101 add wake up source irq 99 add wake up source irq 103 add wake up source irq 51 add wake up source irq 58 PM: suspend of devices complete after 15.482 msecs PM: late suspend of devices complete after 0.823 msecs Disabling non-boot CPUs ... CPU1: shutdown CPU2: shutdown CPU3: shutdown IMX PCIe imx_pcie_pltfm_suspend entering. IMX PCIe imx_pcie_pltfm_suspend exit.          suspended     U-Boot 2009.08-00679-g6ec6783 (May 20 2013 - 14:50:20)     resume   CPU: Freescale i.MX6 family TO1.2 at 792 MHz src 0x92eac8 resume 0x92eac8 jump to resume IMX PCIe imx_pcie_pltfm_resume entering. IMX PCIe imx_pcie_pltfm_resume pcie start re-link. IMX PCIe port imx_pcie_pltfm_resume: re-link up. Enabling non-boot CPUs ... CPU1: Booted secondary processor Calibrating delay loop (skipped) already calibrated this CPU i.MXC CPU frequency driver CPU1 is up CPU2: Booted secondary processor Calibrating delay loop (skipped) already calibrated this CPU i.MXC CPU frequency driver CPU2 is up CPU3: Booted secondary processor Calibrating delay loop (skipped) already calibrated this CPU i.MXC CPU frequency driver CPU3 is up PM: early resume of devices complete after 0.974 msecs remove wake up source irq 58 imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7) imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7) remove wake up source irq 51 remove wake up source irq 103 remove wake up source irq 101 remove wake up source irq 99 PM: resume of devices complete after 54.174 msecs Restarting tasks ... done. PHY: 1:01 - Link is Up - 100/Full                            resume is ok, reload ep’s driver num is 61 e1000e: Intel(R) PRO/1000 Network Driver - 1.3.10-k2 e1000e: Copyright(c) 1999 - 2011 Intel Corporation. e1000e 0000:01:00.0: Disabling ASPM L0s e1000e 0000:01:00.0: (unregistered net_device): Failed to initialize MSI-X interrupts.  Falling back to MSI interrupts. e1000e 0000:01:00.0: (unregistered net_device): Failed to initialize MSI interrupts.  Falling back to legacy interrupts. e1000e 0000:01:00.0: eth1: (PCI Express:2.5GT/s:Width x1) 00:1b:21:3a:18:8b e1000e 0000:01:00.0: eth1: Intel(R) PRO/1000 Network Connection e1000e 0000:01:00.0: eth1: MAC: 3, PHY: 8, PBA No: E42641-005 e1000e: eth1 NIC Link is Up 1000 Mbps Full Duplex, Flow Control: Rx/Tx PING 192.168.0.1 (192.168.0.1): 56 data bytes 64 bytes from 192.168.0.1: seq=0 ttl=64 time=3.126 ms 64 bytes from 192.168.0.1: seq=1 ttl=64 time=0.244 ms 64 bytes from 192.168.0.1: seq=2 ttl=64 time=0.232 ms 64 bytes from 192.168.0.1: seq=3 ttl=64 time=0.206 ms 64 bytes from 192.168.0.1: seq=4 ttl=64 time=0.222 ms 64 bytes from 192.168.0.1: seq=5 ttl=64 time=0.207 ms 64 bytes from 192.168.0.1: seq=6 ttl=64 time=0.250 ms 64 bytes from 192.168.0.1: seq=7 ttl=64 time=0.209 ms 64 bytes from 192.168.0.1: seq=8 ttl=64 time=0.154 ms 64 bytes from 192.168.0.1: seq=9 ttl=64 time=0.211 ms   --- 192.168.0.1 ping statistics --- 10 packets transmitted, 10 packets received, 0% packet loss round-trip min/avg/max = 0.154/0.506/3.126 ms PM: Syncing filesystems ... done.                                   ep’s functions are ok, re-do the suspend/resume tests Freezing user space processes ... (elapsed 0.01 seconds) done. -------------------------------end-------------------------------------------- Original Attachment has been moved to: 0001-imx-pcie-toggle-bit18-of-grp1-fix-pcie-can-t-exit-L2.patch.zip Original Attachment has been moved to: uboot_patch_image.zip Original Attachment has been moved to: kernel_patch_image.zip
查看全文
Development environment: i.MX6Q SabreSD w/ L3.0.35_1.1.0_121218 release. Quoting from Wikipedia about exFAT (exFAT - Wikipedia, the free encyclopedia) as following: exFAT (Extended File Allocation Table) is a Microsoft file system optimized for flash drives. [3] It is proprietary and patent-pending. [1] It is supported in Windows XP and Windows Server 2003 with update KB955704, [2] Windows Embedded CE 6.0, Windows Vista with Service Pack 1, [4] Windows Server 2008, [5] Windows 7, Windows 8, Windows Server 2008 R2 (except Windows Server 2008 Server Core), Mac OS X Snow Leopard starting from 10.6.5, [6] Mac OS X Lion and OS X Mountain Lion. The history of support exFAT in Linux was since from 2.6.x, it involves several parts that will be described followingly. Part 1: Linux Kernel            Enable FUSE (Filesystem in userspace) feature in Kernel Config, then build a new uImage and module if set it to be "M"; Part 2: fuse-2.9.2.tar.gz            Download fuse-2.9.2.tar.gz from http://sourceforge.net/projects/fuse/files/fuse-2.X/, untar it, then build it with following commands: ./configure --prefix=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs/usr --host=`/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc -dumpmachine` --enable-lib --enable-util --enable-example --exec-prefix=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs/usr make sudo make install Part 3: exfat-utils-1.0.1.tar.gz            Download exfat-utils-1.0.1.tar.gz from http://code.google.com/p/exfat/downloads/list, untar it, then build it with following command: sudo scons SYSROOT=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs DESTDIR=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs/sbin CC=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc AR=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-ar RANLIB=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-ranlib STRIP=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-strip install Part 4: fuse-exfat.git git clone git://sources.progress-linux.org/git/releases/baureo-backports/packages/fuse-exfat.git  fuse-exfat.git cd fuse-exfat.git Replace the root SConstruct with the attached one, then execute command: sudo scons SYSROOT=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs DESTDIR=/home/alanz/i.MX6_L3.0.35_121218/ltib/rootfs/sbin CC=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc AR=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-ar RANLIB=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-ranlib STRIP=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-strip install After all above steps done, you can check whether the necessary files under your rootfs like I did as following: http://en.wikipedia.org/wiki/ExFAT#cite_note-uspatent-2alanz@alanz-VirtualBox:~/i.MX6_L3.0.35_121218/ltib$ find ./rootfs/ -name *exfat*./rootfs/sbin/exfatlabel ./rootfs/sbin/mount.exfat ./rootfs/sbin/fsck.exfat ./rootfs/sbin/dumpexfat ./rootfs/sbin/exfatfsck ./rootfs/sbin/mount.exfat-fuse ./rootfs/sbin/mkexfatfs ./rootfs/sbin/mkfs.exfat alanz@alanz-VirtualBox:~/i.MX6_L3.0.35_121218/ltib$ find ./rootfs/ -name *fuse*./rootfs/usr/include/fuse ./rootfs/usr/include/fuse/fuse_common_compat.h ./rootfs/usr/include/fuse/fuse_compat.h ./rootfs/usr/include/fuse/fuse_lowlevel_compat.h ./rootfs/usr/include/fuse/fuse_opt.h ./rootfs/usr/include/fuse/fuse_lowlevel.h ./rootfs/usr/include/fuse/fuse.h ./rootfs/usr/include/fuse/fuse_common.h ./rootfs/usr/include/fuse.h ./rootfs/usr/src/linux/include/linux/fuse.h ./rootfs/usr/lib/libfuse.so ./rootfs/usr/lib/libfuse.a ./rootfs/usr/lib/libfuse.so.2.9.2 ./rootfs/usr/lib/libfuse.la ./rootfs/usr/lib/libfuse.so.2 ./rootfs/sbin/mount.exfat-fuse Check Steps can be referenced by the steps presented on internet. NOTE: The directory name "/home/alanz/i.MX..." should be revised per your self development environment.
查看全文
Change ambient graphic - Ambient Grafic:      Fluxbox (low memory and fast initialization) - Install (root):      apt-get update      apt-get install fluxbox - After instalation, edit file /etc/lightdm/lightdm.conf and change line:      "greeter-session=unity-grreter"  for  "greeter-session=fluxbox"   if, preference auto login comment this line:      "autologin-user=user"  for  "#autologin-user=user" - Reboot and try fluxbox  🙂
查看全文
Based on example code provided in AN4466 I've written a simple memory calibration script for ARM DS-5 that runs same steps and prints out results for DQS, read and write calibration. This script can be run on new boards in order to find optimum calibration settings for the memory controller. Prior to running this script it is necessary to run standard memory initialization script! When bringing up new board: obtain default memory initialization script for memory type you're using (for example from DDR stress tester package) and modify the memory controller settings according to memory device you are going to use. run DDR stress tester with the given configuration on target frequency you're going to use to make memory works with given settings (default values for calibration are  fine in most cases unless there's issues with PCB and/or routing). run memory init script and then the attached script to obtain calibrated values. Re-test Vladan
查看全文
The attached document describes how to integrate the souphttpsrc plugin and make it work.
查看全文
All Boards GTK Manually All Boards GTK Glade All Boards GTK+
查看全文
Hi All, The new Android JB4.2.2_1.0.0-GA release is now available on www.freescale.com ·         Files available Name Description IMX6_JB422_100_ANDROID_DOCS i.MX 6Quad, i.MX 6Dual, and   i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Documentation. Includes Release   Notes, User's Guide, QSG and FAQ Sheet. IMX6_JB422_100_ANDROID_SOURCE i.MX 6Quad, i.MX 6Dual, and   i.MX 6DualLite Android jb4.2.2_1.0.0 BSP, Documentation and Source Code for   BSP and Codecs. IMX6_JB422_100_ANDROID_DEMO i.MX 6Quad, i.MX 6Dual, and   i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Binary Demo Files ·         Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board ·         Release Description i.MX Android jb4.2.2_1.0.0-ga is GA release for Android 4.2.2 Jelly Bean(JB) on i.MX6Q SABRE SD, i.MX6DL SABRE SD and i.MX6Q/DL SABRE AI platform with key features integrated. i.MX Android jb4.2.2_1.0.0-ga release includes all necessary codes, documents and tools to assist users in building and running Android 4.2.2 on i.MX6Q and i.MX6DL hardware board from the scratch. The prebuilt images are also included for a quick trial on Freescale i.MX6Q, i.MX6DL SABRE SD and i.MX6Q/DL SABRE AI boards. Most of deliveries in this release are provided in source code with the exception of some proprietary modules/libraries from third parties. ·         Features Feature i.MX6Q   SABRE SD i.MX6DL   SABRE SD i.MX6   SABRE AI Comments Linux 3.0.35  kernel Y Y Y Based on Linux BSP   L3.0.35_4.0.0 GA release Google JellyBean   4.2.2 release Y Y Y Based on   android-4.2.2_r1 release Bootup with Android Y Y Y Boot source eMMC& External SD eMMC& External SD SD&Nand Default Nand chip   been support is Micron MT29F8G08ABABAWP Splash Screen for   LVDS Y Y N UI (input) Multi-touch on LVDS   panel Multi-touch on LVDS panel Multi-touch on LVDS   panel UI (display) LVDS panel, HDMI   display LVDS panel, HDMI   display LVDS panel, HDMI   display UI (dual display,   LVDS+HDMI, UI mirror displayed on second device) Y Y Y UI (brightness   control) Y Y Y UI (LiveWallpaper) Y Y Y Storage - External   Media Y Y Y SD, External SD and   UDisk Storage - MTP   (Media Transfer Protocol) Y Y Y Connectivity -   Ethernet Y Y Y Connectivity - BT     Y Y     N Hardware: ·           Atheros AR3001 ·           Atheros AR3002 Profiles: ·           A2DP ·           HID ·           OPP ·           PBAP Connectivity - WiFi Y Y     Y Hardware: ·           Atheros AR6103 SDIO card Features: ·           AP mode ·           Wake on Wireless Connectivity -   3G Y Y   N Hardware: ·           HUAWEI EM770W modem ·           Infinion Amazon 1 modem ·           ZTE FM210 modem Connectivity -   GPS Y Y N Connectivity - USB Tethering Y Y Y Support WIFI and   Ethernet as upstream Internet - SIP   voice call N N N Internet - VPN Y Y Y Power - Battery   status report Y Y N/A Known limitations   about the accuracy in some use cases Power - CPU Freq Y Y Y Power - Bus Freq Y Y Y Media - Music Play Y Y Y Media - Sound Record Y Y Y Media - Video Play Y Y Y Media - Camera Y Y N Media - TVIN N/A N/A Y PAL/NTSC Media - Dual Camera Y Y Y Hardware for SABRE SD: ·           Front Camera: OV5642 CSI camera ·           Rear Camera: OV5640 MIPI camera Hardware   for SABRE AI: ·           Front Camera: UVC camera ·           Rear Camera: TV IN Media - Camcorder Y Y N Media - USB Camera Y Y Y Logitech: ·           C250 ·           E3500 Media - USB Micro Y Y Y Media - Movie   Studio Y Y Y Media - HDMI audio output Y Y Y Graphic - HW 3D   acceleration Y Y Y OpenGLES 1.1/2.0   via GC2000 or GC800 3D core Graphic - HW   accelerated UI surface composition Y Y Y Misc - ADB over USB Y Y Y Misc - Fastboot   utility Y Y Y Misc - SW update   and factory reset Y Y Y Sensor - Magmatic Y Y N Sensor -   Accelerometer Y Y N Sensor - Light Y Y N NTFS-3G File System Y Y Y For external   Storage NAND N N Y Tested NAND chip: - Micro 29F8G08ABABA ·         Change List The below section lists the big changes in JellyBean which need the user’s attention when comparing to Freescale ICS version: o   Default Android multiple display implementation in JellyBean o   Display resolution change in Setting is not been supported o   New camera hal implementation based on JellyBean libcamera2 o   Add NTFS file system support for external storage ·         Known issues For known issues and limitations please consult the release notes
查看全文
The refine to TV mode of R10.3.1 causes dual video function fail. The attached patch recovers dual video function. Attached dual_video.patch only work for RGB output (HDMI support). For legacy TVout (YUV output), the extra patch is necessary, see the attached "legacy_tvout.zip". Refer to Dual video with single UI on i.MX53 SMD with Android R10.4  for setup.
查看全文
Issue: On i.MX 6Solo designs using LPDD2 memory, the correct settings for two important registries may be confusing to determine. Solution: 1) MMDCx_MDMISC register, LPDDR2_2CH Field: For the i.MX 6Solo processor, this field should always be set to '0'. Reason: Two channel mode is not possible on this processor. Only channel MMDC0 is connected to external pins. 2) IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET register, DDR_SEL Field: For the i.MX 6Solo processor, this field should always be set to "00". Reason: A DRAM Warm Reset requires a response from MMDC1, which is not connected externally on the 6Solo processor, so a Warm Reset never complets. These two issues will be clarified in a subsequent revision of the MCIMX6SDL Reference Manual.
查看全文
This document provides the steps to patch and build a fastboot Linux System. This document assumes the BSP 3.0.35_1.1.0 and a  i.MX6Q platform. For more information about what the patches do, please check this link. Install LTIB and move to the ltib folder Download the ltib patch from this document and patch it (patch -p1 < 0001-set-imx6_ssd_lite_defconfig-as-default-kernel-config.patch) Go to the LTIB configuration menu (./ltib -m config), select mx6q platform and min profile Select mx6q_sabresd as u-boot board Fetch and Patch: u-boot: Prepare u-boot source code (./ltib -m prep -p u-boot) Move to u-boot folder (cd rpm/BUILD/u-boot-2009.08) Download u-boot attached patches Patch code (for p in *.patch; do patch -p1 < $p;done) kernel: Prepare kernel source code (./ltib -m prep -p kernel) Move to kernel folder (cd rpm/BUILD/linux) Download attached kernel patches Patch code (for p in *.patch; do patch -p1 < $p;done) Build  (./ltib) Add  an application to run first after boot in rootfs/etc/inittab (see example inittab file, it captures data from the MIPI Camera) Create necessary devices nodes under rootfs/dev. For example terminal: sudo mknod ttymxc0 c 207 16 video capture nodes: sudo mknod video0 c 81 5; sudo mknod video1 c 81 6 video display nodes: sudo mknod video16 c 81 0; sudo mknod video17 c 81 1 frame-buffers: for i in 0 1 2 3 4; do sudo mknod fb$i c 29 $i; done Package rootfs (cd rootfs; sudo tar --numeric-owner -cvfj ../rootfs.tar.bz2 *; cd ..) On a windows machine, download latest Manufacturing tool and uncompress it. Move rootfs.tar.bz2, rootfs/boot/uImage and rootfs/boot/u-boot.bin into the corresponding Manufacturing folder (Profiles\MX6Q Linux Update\OS Firmware\files) Choose a sabresd-eMMC profile and flash the board Boot the board using the eMMC
查看全文
FAE Title Date i.MX Device BSP Description Leo Demo uImage for iMX257 does not support EXT3 filesystem 2/May2013 257 L2.6.31_09.12.00_SDK_images_MX25 For some reason the demo uImage does not support EXT3 filesystems (ext2 is not good for SD cards). kernel has to be recompile with this feature. Xisco start-weston command doesn't work when running from SD card. Only from NFS 3/may/2013 6 RC3.0.35.4.0.0 When compiling rootfs with LTIB, there is a problem that /tmp is tmpfs but keeps the size as 512k, far from common program running requirement, and it's full when system boots up.   When executing start-weston script it needs to write to /tmp and it fails. Only happens with LTIB built BSP.   $ mount -t tmpfs /tmp /tmp        Should be run before executing start-weston Xisco Porting OpenGL ES2 cpp apps for i.MX6 7/may/2013 6 RC3.0.35.4.0.0 When porting OpenGL ES2 cpp apps that were written for i.MX53, you will find an error saying that the function :   fbGetDisplay()   needs more arguments.   All that is needed to fix this error is to change the function to:   fbGetDisplayByIndex(0)   And you will be able to compile your app. Leo Stand-alone MFG and Android MFG are not the same Wed May 15 12:15:17 CDT 2013 6 JB4.2.2_1.1.0 In case you want to flash Android, use the MFG inside the source code tarball and not the stand-alone (the one found directly on the SW & Tools tab). Seems that it takes some time for both to be sync (the same) Leo gst-ffmpeg plugins is broken Thu May 16 13:31:44 CDT 2013 6 RC3.0.35.4.0.0 Attached patch should be applied to gst-ffmpeg code Original Attachment has been moved to: 0001-gstffmpegdemux.c-Remove-deprecated-flow-macros.patch.zip
查看全文
Notes: First run the playback pipeline then the streaming pipeline. The above example streams H263 video and AMR audio data. Change codec format to your needs. In case where the iMX is the streaming machine, the audio encoder 'amrnbenc' must be installed before. This scenario has not been tested Shell variables and pipelines Playback machine (receiver) # On playback machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where PC does the playback     AUDIO_DEC_SINK="rtpamrdepay ! amrnbdec ! alsasink "     VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\""     VIDEO_DEC_SINK="rtph263pdepay ! ffdec_h263 ! autovideosink" ## End of IMX2PC Settings ## PC2IMX: Case where iMX does the playback     AUDIO_DEC_SINK="rtpamrdepay ! mfw_amrdecoder ! alsasink "     VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\""     VIDEO_DEC_SINK="rtph263pdepay ! vpudec ! mfw_v4lsink " ## End of PC2IMX Settings PLAYBACK_AUDIO="udpsrc caps=\"application/x-rtp,media=(string)audio,clock-rate=(int)8000,encoding-name=(string)AMR,encoding-params=(string)1,octet-align=(string)1\" \             port=5002 ! rtpbin.recv_rtp_sink_1 \         rtpbin. ! $AUDIO_DEC_SINK \      udpsrc port=5003 ! rtpbin.recv_rtcp_sink_1 \      rtpbin.send_rtcp_src_1 ! udpsink port=5007 sync=false async=false" PLAYBACK_VIDEO="udpsrc caps=$VIDEO_CAPS port=5000 ! rtpbin.recv_rtp_sink_0 \         rtpbin. ! $VIDEO_DEC_SINK \         udpsrc port=5001 ! rtpbin.recv_rtcp_sink_0 \         rtpbin.send_rtcp_src_0 ! udpsink port=5005 sync=false async=false" PLAYBACK_AV="$PLAYBACK_VIDEO $PLAYBACK_AUDIO" # Playback pipeline gst-launch -v gstrtpbin name=rtpbin $PLAYBACK_AV Streaming Machine (sender) # On Streaming machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where iMX does the streaming     IP=x.x.x.x # IP address of the playback machine     VIDEO_SRC="mfw_v4lsrc"     VIDEO_ENC="vpuenc codec=h263 ! rtph263ppay "    AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " ## END IMX2PC settings ## PC2IMX: Case where PC does the streaming     IP=y.y.y.y # IP address of the playback machine     VIDEO_SRC="v4l2src"     VIDEO_ENC="ffenc_h263 ! rtph263ppay "     AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " # END PC2PC settings STREAM_AUDIO="$AUDIO_ENC ! rtpbin.send_rtp_sink_1 \         rtpbin.send_rtp_src_1 ! udpsink host=$IP port=5002 \         rtpbin.send_rtcp_src_1 ! udpsink host=$IP port=5003 sync=false async=false \         udpsrc port=5007 ! rtpbin.recv_rtcp_sink_1" STREAM_VIDEO="$VIDEO_SRC ! $VIDEO_ENC ! rtpbin.send_rtp_sink_0 \         rtpbin.send_rtp_src_0 ! queue ! udpsink host=$IP port=5000 \         rtpbin.send_rtcp_src_0 ! udpsink host=$IP port=5001 sync=false async=false \         udpsrc port=5005 ! rtpbin.recv_rtcp_sink_0" STREAM_AV="$STREAM_VIDEO $STREAM_AUDIO" # Stream pipeline gst-launch -v gstrtpbin name=rtpbin $STREAM_AV
查看全文
Application Note covering how to get the Silex SX-SDCAN working with the Sabre-SD i.MX6 Evaluation kit.
查看全文
Hi all,      I have a problem about usb mass storage driver, that's it can't enumerate my mass storage device.      but it can enumerate my mouse, keyboard...etc hid device.      anyone have idea about it ?      I always get below messages when my mass storage device plugs in.      and below is my dmesg information      My hardware -->      Type A receptacle on otg controller ~
查看全文