i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
This doc show: on i.MX8QXP MEK board, configure ov5640 sensor(parallel interface) output 5MP(2592x1944) RAW(Bayer) data at 15fps, and Parallel Capture Subsystem and Image Sensor Interface capture RAW RGB data, and i.MX8QXP GPU debayer RAW data then display image. HW: i.MX8QXP MEK board, MEK base board (to place the parallel camera), ov5640 sensor. SW: Linux 4.14.98_2.0.0 BSP, and patches in this doc.   Configure at camera sensor side A Bayer filter is a color filter array (CFA) for arranging RGB color filters on a square grid of photosensors. The filter pattern is 50% green, 25% red and 25% blue, hence is also called BGGR, RGBG ,GRGB, or RGGB. The ov5640 has an image array capable of operating at up to 15 fps in 5 megapixel (2592x1944) resolution. OV5640 support output formats: RAW(Bayer), RGB565/555/444,CCIR656, YUV422/420, YCbCr422, and compression. To make ov5640 output 5MP RAW data at 15fps, check my kernel patch imx8-ov5640-raw-capture-driver-4.14.98_2.0.0.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP kernel code. Parallel interface ov5640, use ov5640_raw_setting[] array of drivers/media/platform/imx8/ov5640_v3.c. This register setting is come from ov5640 software application note and data sheet. Configure at i.MX8QXP side The Parallel Capture Subsystem consists of the Parallel Capture Interface (BT 656) and associated peripherals. It interfaces to the Parallel CSI sensor. This allows for up to 24 RGB data bits in parallel or for RGB components on consecutive clocks (up to 10-bit color depth). The formats supported are RGB, RAW and YUV 422. Below is Parallel Capture Subsystem diagram: For RAW format data, CSI_CTRL_REG of Parallel Capture Subsystem need configured as my patch, otherwise found cannot get correct data.   The multiple input sources (MIPI CSI, Parallel Capture) captures the pixel data and feeds it to the ISI. The ISI is responsible for capturing and pre-processing the pixel data from multiple input sources and storing them into the memory. Below is ISI diagram: For RAW format data, it should be bypass any processing pipeline of ISI, just use ISI to save it to memory.   Capture test code To capture the RAW data and save it to file, check my patch imx8_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP unit test code. Note the usage is: ./imx8_cap.out -of -cam 1 -fr 15 -fmt BA81 -ow 2592 -oh 1944 -num 100   Display RAW data The RAW data cannot be displayed directly, debayer process is needed to get complete red, green, blue color for each pixel. The debayer process if run on CPU, will cost much CPU time. To save CPU time, debayer could done by GPU. The method is, captured RAW data upload to GPU as texture , then GPU will do the debayer, then full color of each pixel will be got, then display it. To upload RAW camera data to GPU with zero memory copy, i will use i.MX8QXP GPU extension GL_VIV_direct_texture. It create a texture with direct access support. API glTexDirectVIVMap,  which support mapping a user space memory or a physical address into the texture surface. The API glTexDirectVIVMap need logic and physical address of data buffer, so i will allocate data buffer from g2d lib, it is dma-buffer also get logic/physical address of buffer, then queue it as DMABUF to v4l2 capture driver, after dequeue got RAW camera data, pass it to GPU for debayer. GPU side, I will use OpenGL shader code from "Efficient, High-Quality Bayer Demosaic Filtering on GPUs". Check my patch imx8_debayer-gpusdk-5.3.0.diff which apply on i.MX GPU SDK 5.3.0 code. Note, here i only do is debayer, no extra process.   Known issue One thing is ov5640 output 5MP at 15fps, compare with output 5MP at 5fps, there are more noise of camera data at 15fps case. My debug found is, this noise seems come from ov5640 itself.   Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX8QXP&appType=license c>https://github.com/NXPmicro/gtec-demo-framework d>ov5640 data sheet e>ov5640 software application note f>Efficient, High-Quality Bayer Demosaic Filtering on GPUs https://www.semanticscholar.org/paper/Efficient%2C-High-Quality-Bayer-Demosaic-Filtering-on-McGuire/088a2f47b7ab99c78d41623bdfaf4acdb02358fb
查看全文
This doc show: on i.MX6Q SabreSD board, configure ov5640 sensor(parallel or MIPI) output 5MP(2592x1944) RAW(Bayer) data at 15fps,and i.MX6Q IPU capture RAW RGB data, and i.MX6Q GPU debayer RAW data then display image. HW: i.MX6Q-SabreSD board, ov5640 sensor. SW: Linux 4.14.98_2.0.0 BSP, and patches in this doc. Configure at camera sensor side A Bayer filter is a color filter array (CFA) for arranging RGB color filters on a square grid of photosensors. The filter pattern is 50% green, 25% red and 25% blue, hence is also called BGGR, RGBG ,GRGB, or RGGB. The ov5640 has an image array capable of operating at up to 15 fps in 5 megapixel (2592x1944) resolution. OV5640 support output formats: RAW(Bayer), RGB565/555/444,CCIR656, YUV422/420, YCbCr422, and compression. To make ov5640 output 5MP RAW data at 15fps, check my patch imx6_ov5640_dvp_mipi_raw_capture_driver-4.14.98_2.0.0.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP kernel code: Parallel interface ov5640, use ov5640_raw_setting[] array of drivers/media/platform/mxc/capture/ov5640.c. This register setting is come from ov5640 software application note and data sheet. MIPI interface ov5640, use ov5640_mipi_raw_setting[] array of drivers/media/platform/mxc/capture/ov5640_mipi.c. This register setting is combine setting of original code (remove ISP register setting), plus PLL register setting for MIPI interface, plus some data format register setting. Configure at i.MX6Q side The i.MX6Q IPU camera port(CSI-2 module) support data format include Raw(Bayer), RGB, YUV 4:4:4, YUV 4:2:2 and grayscale, up to 16 bits per value. Below is camera data routing for i.MX6Q:    Below is i.MX6Q IPU block daigram: The CSI-2 of IPU which is responsible for synchronizing and packing the video (or generic data) and sending it to other blocks. The video data received by CSI-2, could be sent to three other blocks: SMFC, VDI, IC. For RAW (Bayer) data capture, should go through path like this: CSI-2-->SMFC-->IDMAC-->DDR memory It means RAW data is received as generic data, see IPU_PIX_FMT_GENERIC in my patch, and IPU cannot process this kind data, it is just received to DDR memory. For MIPI interface camera, need note is i.MX6 side MIPI D-PHY clock must be calibrated to the actual clock range of the camera sensor’s D-PHY clock and the calibrated value must be equal to or greater than the camera sensor clock, detail see  AN5305. Take MIPI ov5640 as example: Pixel clock = 2592x1944x15fpsx(1/2 cycle/pixel)x1.35 blank interval = 51MHZ MIPI data rate = 51MHZ x 16 bit = 816Mb/s so 816/2/2*2 is 408MHZ is i.MX6 side D-PHY clock. Here due to one bayer pixel is 8bit, and i.MX6 MIPI data bus is 16 bit, so above use 1/2 cycle/pixel. And check ov5640_mipi_raw_setting[], you will got the sensor side D-PHY clock is about 672/2 = 336MHZ. And check AN5305, register MIPI_CSI2_PHY_TST_CTRL1 of i.MX6 need set as 0xC, but here i still keep it as default BSP value 0x14.   3.Capture test code I changed unit test mxc_v4l2_capture.c to capture the RAW data and save it to file. Check my patch imx6_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff which apply on i.MX  Linux 4.14.98_2.0.0 BSP unit test code. Note the usage is: ./cap.out -c 1 -i 1 -fr 15 -m 6 -iw 2592 -ih 1944 -ow 2592 -oh 1944 -f BA81 -d /dev/video1 savefile.dmp parameter -i 1 means use CSI to MEM mode /dev/video1 is MIPI ov5640, /dev/video0 is parallel ov5640   4.Display RAW data The RAW data cannot be displayed directly, debayer process is needed to get complete red, green, blue color for each pixel. The debayer process if run on CPU, will cost much CPU time. To save CPU time, debayer could done by GPU. The method is, captured RAW data upload to GPU as texture , then GPU will do the debayer, then full color of each pixel will be got, then display it. To upload RAW camera data to GPU with zero memory copy, i will use i.MX6Q GPU extension GL_VIV_direct_texture. It create a texture with direct access support. API glTexDirectVIVMap,  which support mapping a user space memory or a physical address into the texture surface. The API glTexDirectVIVMap need logic and physical address of data buffer, so i will allocate data buffer from /dev/mxc_ipu, it is dma-buffer also get logic/physical address of buffer, then queue it as USERPTR to ipu v4l2 capture driver, after dequeue got RAW camera data, pass it to GPU for debayer. GPU side, I will use OpenGL shader code from "Efficient, High-Quality Bayer Demosaic Filtering on GPUs". Check my patch imx6-5640-debayer-testcode-gpusdk-5.2.0.diff which apply on i.MX GPU SDK 5.2.0 code. Note, here i only do is debayer, no extra process.   Known issue One thing is ov5640 output 5MP at 15fps, compare with output 5MP at 5fps, there are more noise of camera data at 15fps case. My debug found is , this noise seems come from ov5640 itself.   Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX6DQRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX6QDLSOLOX&appType=license c>https://github.com/NXPmicro/gtec-demo-framework d>https://www.nxp.com/docs/en/application-note/AN5305.pdf e>ov5640 data sheet f>ov5640 software application note g>Efficient, High-Quality Bayer Demosaic Filtering on GPUs https://www.semanticscholar.org/paper/Efficient%2C-High-Quality-Bayer-Demosaic-Filtering-on-McGuire/088a2f47b7ab99c78d41623bdfaf4acdb02358fb
查看全文
The NXP i.MX 8M provides industry leading audio, voice and video processing for applications that scale from consumer home audio to industrial building automation and mobile computers. The i.MX 8M Quad supports multiple audio interfaces as listed below: Besides the general audio input/output function, the audio interfaces will supports following features: - SAI-1 supports up to 16-channels TX (8 lanes) and 16-channels RX (8 lanes) at 384KHz/32-bit. - SAI-5 supports up to 8-channels TX (4 lanes) and 8-channels RX (4 lanes) at 384KHz/32-bit. - SAI-2/3/6 supports up to 2-channels TX (1 lanes) and 2-channels RX (1 lanes) at 384KHz/32-bit. - SAI-2/3/6 support up to 2-channels TX (1 lane) and 2-channels RX (1 lane) at 384KHz/32-bit. - SAI-1 supports glue-less switching between PCM & DSD operation for popular audio DACs - SPDIF-1/2 supports raw capture mode that can save all the incoming bits into audio buffer The SAI-1/2/3/5/6 and SPDIF-1 share GPIO pads on the chip through IOMUX. Common use cases supported by the audio interfaces are listed in the table below (many other configurations are possible). The number is the data lanes supported. For the MCLK pin on each SAI module, it can be configured as either input or output. When configured as output, the SAI_CLK_ROOT from CCM will be routed to the pad output. When configured as input, the external input to the pad will be routed to SAI.MCLK, which can be used as master clock for SAI. Below is the diagram showing the both input/output options, by using SAI1 as the example. Each SAI module supports up to 3 master clock inputs. The TX and RX sub-module inside each SAI can independently select one of the clock inputs as its master clock. This allows TX and RX of one SAI to run from different clock source. The master clock inputs have following options: - SAI.MCLK[1] can be selected from SAI_CLK_ROOT from CCM or SAI.MCLK from IOMUX. This is the most straight-forward clock routing in which SAI only use its own clock source from CCM or IO pad. - SAI.MCLK[2] can be selected from following clock sources:       Any of the SAI_CLK_ROOT from CCM;       Any of the SAI.MCLK from IOMUX;       Other clock sources from SPIDF; - SAI.MCLK[3] has exact same clock source options as SAI.MCLK[2]. This allows both TX and RX can have access to all the options without any dependency between each other. The clock options for master clock on SAI are shown in the diagram blow, by using SAI-1 as an example. The options on MCLK[1] is also available on MCLK[2] and MCLK[3]. The reason to keep this options is to provide the similar SAI clock structure as i.MX6/i.MX7 processors. The configuration of the MUX for master clock are controlled by IOMUXC_GPR registers. They should be configured before SAI clock is enabled to avoid glitches on the clock. Note: Because those MUX on clocks are missed during the design, the actual implementation in the silicon is simplified as shown in the following diagram. All the SAI and SPDIF instances have SDMA support. In order to meet the audio data rate, two SDMA modules are used. Because the SAI-2/3 and SPDIF-1/2 do not require high data throughput, they are assigned to SDMA-1, shared with other peripherals such as UART/SPI. SAI-1/4/5/6 need to support high sample rate & multichannel audio, they are assigned to SDMA-2, which is a dedicated SDMA engine for audio. The SDMA-2 frequency is increased to 500/250 instead of 133/66 to make sure it has enough throughput. In order to allow SW tracking the progress of audio DMA, the TX_SYNC and RX_SYNC of SAI modules are routed to GPT as the external clock input. Since there are totally 6 SAI modules, these signals will be MUXed when connection to GPT. - GPT-4/5/6 external clock input can be selected from the TX_SYNC or RX_SYNC of any 6 SAI modules; - The MUX select is controlled by IOMUXC_GPR register; - The MUX select register for GPT-4/5/6 are fully independent of each other.
查看全文
Platform: i.mx8qm/qxp OS: imx-yocto-L4.14.98_2.0.0_ga Camera: max9286 deserializer <=> max96705 serializer  + ar0144 or: max9286 deserializer <=> max96705 serializer + ov9284 Note that currently only one camera is support and the serializer should be connected to the IN0 of max9286. Data format: ar0144: mono raw 12bit. ov9284: mono raw 10bit. On imx8qm/qxp the data will be recieved as raw 16bit and the valid data bit start from bit[13] to LSB. for mono raw 12bit the valid data bit is 0bxxdd_dddd_dddd_ddxx for mono raw 10bit the valid data bit is 0bxxdd_dddd_dddd_xxxx max9286 and max96705 configuration: dbl bws PXL_CRC/edc hven hibw lccen him should be the same on both sides, this can be achieved by pin or register configurations. The crossbar function of max96705 can be used to fix the reversed data bit. for example, reversed 12bit with dbl to 1. 0x20 0xb 0x21 0xa 0x22 0x9 ....... 0x2b 0x0 0x30 0xb 0x31 0xa .... 0x3b 0x0 0x20 to 0x2b and 0x30 to 0x3b are the registers of max96705. Patch apply: 1. push the kernel-patch to the kernel source and apply it. 2. reconfig the kernel setting, make sure there is only CONFIG_MAX9286_AR0144 or        CONFIG_MAX9286_WISSEN(ov9284) enabled, all other max9286 related are disabled. You can run menuconfig to achieve this. 3. For testing copy the vulkan-v4l2.tar to the board, and run vulkan-v4l2.     the source code is at https://github.com/sheeaza/vulkan-v4l2 branch ar0144 for ar0144, branch ov9284 for ov9284. =========== updated patch for data format.
查看全文
   Recently, some customers encountered the problem that compilation failed when compiling l4.14.98-2.0.0 fsl-imx-waylan + fsl-image-qt5-validation-imx in Ubuntu 18.04 environment. In fact, compiling QT image is a very time-consuming process, especially in the process of compiling, errors need to be handled, which will be more time-consuming. The following compilation took four days to complete. 1. Environment Linux Host : ubuntu 18.04 LTS Virtual Machine: VMware workstatin Player 12 images: fsl-imx-waylan + fsl-image-qt5-validation-imx Hardware: imx8mqevk Linux BSP verison: L4.14.98-2.0.0 2. Steps (1)Installation of Ubuntu 18.04 2.Update software 3. Installing software package for compiling BSP # sudo apt-get install flex # sudo apt-get install bison # sudo apt-get install gperf # sudo apt-get install build-essential # sudo apt-get install zlib1g-dev # sudo apt-get install lib32ncurses5-dev # sudo apt-get install x11proto-core-dev # sudo apt-get install libx11-dev # sudo apt-get install lib32z1-dev # sudo apt-get install libgl1-mesa-dev # sudo apt-get install tofrodos # sudo apt-get install python-markdown # sudo apt-get install libxml2-utils # sudo apt-get install xsltproc          # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 # sudo apt-get install gcc-multilib g++-multilib # sudo apt-get install subversion # sudo apt-get install openssh-server openssh-client # sudo apt-get install uuid uuid-dev # sudo apt-get install zlib1g-dev liblz-dev # sudo apt-get install liblzo2-2 liblzo2-dev # sudo apt-get install lzop # sudo apt-get install git-core curl # sudo apt-get install u-boot-tools # sudo apt-get install mtd-utils # sudo apt-get install android-tools-fsutils # sudo apt-get install openjdk-8-jdk # sudo apt-get install device-tree-compiler # sudo apt-get install aptitude # sudo aptitude install libcurl4-openssl-dev nss-updatedb   From i.MX_Yocto_Project_User's_Guide.pdf: # sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \ build-essential chrpath socat libsdl1.2-dev   4. Downloading Yocto BSP according to steps in i.MX_Yocto_Project_User's_Guide.pdf 5.Compiling L4.14.98-2.0.0 BSP # cd ~/imx-yocto-bsp # DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland # bitbake fsl-image-qt5-validation-imx In the process of compilation, there have been many "fetch errors", which are caused by disconnection or timeout of network connection. We just need to run the bitmake command again in the build Wayland subdirectory to continue the compilation. # bitbake fsl-image-qt5-validation-imx          Fetching errors below were what I encountered:          The following picture is to re-run “bitbake fsl-image-qt5-validation-imx” after fetch errors occurred.          In order to improve the speed of compilation , I re-configured vmware player, assigning 6 CPU cores for Ubuntu.          Compilation is a long and arduous process. It took 4 days to compile normally with error handling. Finally, the compilation was completed. NXP TIC Team Weidong Sun 2019-11-02
查看全文
Most i.MX8QXP/QM customers already work on L4.14.98 GA for their Auto product, like C-V2X TBOX, Car infortainment system. Some customers also want to adopt OP-TEE in their security design, but OP-TEE on i.MX8QXP/QM platform don't support HW cryptography accelerating which base on CAAM module. So I worked on the issue last week and fixed it. The package meta-optee-add-on_4.14.98_2.0.0_ga.tgz is Yocto layer which includes all patches for fixing the issue. Software environments as the belows: Linux kernel: imx_4.14.98_2.0.0_ga HW platform:  i.MX8QM/QXP MEK. How to build: 1, decompress meta-optee-add-on_4.14.98_2.0.0_ga.tgz and copy meta-optee-add-on to folder (Yocto 4.14.98_2.0.0_ga dir)/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-optee and add BBLAYERS += " ${BSPDIR}/sources/meta-optee-add-on " into (Yocto 4.14.98_2.0.0_ga dir)/build-optee/conf/bblayers.conf  3, Run bitbake fsl-image-validation-imx. 4, You can run xtest or xtest -l 1 4007 on your MEK board to test optee crypto feature after completing build image. You can find it only take about one second comparing no CAAM accelerating when test "regression_4007.11 Generate RSA-2048 key".
查看全文
Hello everyone, this document will explain on how to use the UUU (Universal Update Utility) tool to flash Linux to an i.MX device (i.MX 8MM).   Requirements:   MX 8M Mini EVK UUU tool documentation, available here Linux Binary Demo Files - i.MX 8MMini EVK UUU 1.2.135 binary Serial console emulator (tera term or putty)   UUU auto script For this example is used the L4.14.98_2.0.0_ga demo image for the i.MX 8MM, inside the demo image we will find the auto script, which by default flash the eMMC of the board, the structure of the script is as following   /***********************************************************************************/ uuu_version 1.2.39   # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk   # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk   # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -offset 0x57c00 SDPU: jump # }   # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -skipspl SDPV: jump # }   FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd mmc dev ${emmc_dev} FB: flash -raw2sparse all fsl-image-validation-imx-imx8mmevk.sdcard FB: flash bootloader imx-boot-imx8mmevk-sd.bin-flash_evk FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB: done /***********************************************************************************/    In short, when the board goes into serial downloader mode UUU downloads the bootloader to internal RAM, once done and uboot is running, through fastboot utility it will flash .sdcard file and uboot to the eMMC on the board.   More information about the protocol UUU use please refer to the UUU documentation (UUU.pdf) section 5 Supported protocol.   Running the tool In order to run the tool the binary of uuu needs to be downloaded, the binary files can be downloaded from the link above, uuu.exe is for Windows and uuu is for Linux. Once downloaded it can be placed inside the same file as the demo image, this so it is easy to run and cleaner on the shell commands.   Windows In windows OS the tool should be run using the Windows PowerShell in administrator mode, once open we will run the next commands: > .\uuu.exe uuu.auto   Linux >$ sudo ./uuu uuu.auto   The tool will start running and should be waiting for any i.MX device to be detected by host pc   Preparing the board For the board to be flashed it is needed to be in download mode, the switch configuration (i.MX 8MM EVK) is as following: SW1101  -  1010XXXXXX SW1102  -  XXXXXXXXX0   Connect a USB cable from the host pc which will run the tool to the USB OTG/TYPE C port, usually specified as download, on the board.   Connect a USB cable from the host to the OTG-to-UART for console output, usually specified as debug, on the board.   Open terminal emulator program with the following settings: Bits per second - 115200 Data bits - 8 Parity - None Stop bits - 1 Flow control - None   Power on the board, the download will start and the serial prompt will show the progress in uboot, wait until the tool show success.   Finally power off the board and change the switch configuration to boot from the eMMC, power on the board again and it should boot successfully!   Built in scripts One can use the built in scripts using the -b option to burn the bootloader  and the rootfs to the target flash, just type the command accordingly to the target flash device.    SD Write bootloader only: Windows: > .\uuu.exe -b sd <bootloader> Linux: $ sudo ./uuu -b sd <bootloader>   Replace <bootloader> for your .imx/.bin file, example using the i.MX 8MM for Windows and Linux respectively below. > .\uur.exe -b sd imx-boot-imx8mmevk-sd.bin-flash_evk $ sudo ./uuu -b sd imx-boot-imx8mmevk-sd.bin-flash_evk    Write whole Linux image Windows: > .\uuu.exe -b sd_all <bootloader> <rootfs>.sdcard Linux: $ sudo ./uuu -b sd_all <bootloader> <rootfs>.sdcard   Replace <bootloader> and <rootfs> for the name of your .imx/.bin and .sdcard files respectively, example using the i.MX 8MM below. > .\uuu.exe -b sd_all  imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard $ sudo ./uuu -b sd_all  imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard   eMMC Write bootloader only Windows: > .\uuu.exe -b emmc <bootloader> Linux: $ sudo ./uuu -b emmc <bootloader>   Example using i.MX 8MM > .\uuu.exe -b emmc imx-boot-imx8mmevk-sd.bin-flash_evk $ sudo ./uuu -b emmc imx-boot-imx8mmevk-sd.bin-flash_evk   Write whole Linux image Windows: > .\uuu.exe -b emmc_all <bootloader> <rootfs>.sdcard Linux: $ sudo ./uuu -b emmc_all <bootloader> <rootfs>.sdcard   Example using i.MX 8MM > .\uuu.exe -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard $ sudo ./uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard   Hope this will helpful for everyone who is starting to use this flashing tool.
查看全文
For the board imx8M Quad EVK running the Linux 4.14.78-1.0.0_ga version BSP, the resolutions 3840x2160,1920x1080, 1280x720, 720x480 are support in our default BSP. For the other resolutions how to make it work? This patch used to do support for a non-default resolution on i.MX 8MQ EVK. Basically, the customer needs to change the clocks accordingly to the display requirements,  it to be used as a base to the display support.
查看全文
KSZ9031 is a very common PHY used with many ethernet design. This document will show you how to add it in u-boot and kernel. 1. Schematic The MODE[3:0] strap-in pins are sampled and latched at power-up/reset. MODE[3:0]=1111 is RGMII mode - Advertise all capabilities (10/100/1000 speed half-/full-duplex) The PHY address, PHYAD[2:0], is sampled and latched at power-up/reset. Here PHY address is set to 001. In this design example, the ENET_RESET_B is connected to GPIO pin GPIO1_IO03. 2. Source code modification In u-boot source code, add the following code in the <board_name>.c file. - IOMUX setup for the GPIO1_IO03 pin. static iomux_v3_cfg_t const phy_reset_pads[] = {      MX7D_PAD_GPIO1_IO03__GPIO1_IO3 | MUX_PAD_CTRL(NO_PAD_CTRL), }; - In the function setup_fec(int fec_id), add the code for phy reset. imx_iomux_v3_setup_multiple_pads(phy_reset_pads, ARRAY_SIZE(phy_reset_pads)); gpio_request(IMX_GPIO_NR(1, 3), "ENET PHY Reset"); gpio_direction_output(IMX_GPIO_NR(1, 3) , 0); mdelay(20); gpio_set_value(IMX_GPIO_NR(1, 3), 1); - There is a PHY config for the KSZ9031. int board_phy_config(struct phy_device *phydev) {    /*      * Default setting for GMII Clock Pad Skew Register 0x1EF:      * MMD Address 0x2h, Register 0x8h      *      * GTX_CLK Pad Skew 0xF -> 0.9 nsec skew      * RX_CLK Pad Skew 0xF -> 0.9 nsec skew      *      * Adjustment -> write 0x3FF:      * GTX_CLK Pad Skew 0x1F -> 1.8 nsec skew      * RX_CLK Pad Skew 0x1F -> 1.8 nsec skew      *      */     /* control data pad skew - devaddr = 0x02, register = 0x04 */     ksz9031_phy_extended_write(phydev, 0x02,                    MII_KSZ9031_EXT_RGMII_CTRL_SIG_SKEW,                    MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x0000);     /* rx data pad skew - devaddr = 0x02, register = 0x05 */     ksz9031_phy_extended_write(phydev, 0x02,                    MII_KSZ9031_EXT_RGMII_RX_DATA_SKEW,                    MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x0000);     /* tx data pad skew - devaddr = 0x02, register = 0x05 */     ksz9031_phy_extended_write(phydev, 0x02,                    MII_KSZ9031_EXT_RGMII_TX_DATA_SKEW,                    MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x0000);     /* gtx and rx clock pad skew - devaddr = 0x02, register = 0x08 */     ksz9031_phy_extended_write(phydev, 0x02,                    MII_KSZ9031_EXT_RGMII_CLOCK_SKEW,                    MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x03FF);     if (phydev->drv->config)         phydev->drv->config(phydev);     return 0; } The KSZ9031 driver (drivers/net/phy/micrel.c) had already supported in the u-boot source code. Add the following #define in the <board_name>.h file to enable the driver for building. #define CONFIG_PHY_MICREL As the PHY address on the board is 001, change the PHYADDR to 1 in the <board_name>.h file. #define CONFIG_FEC_MXC_PHYADDR          0x1 In the kernel source code, add/modify the PHY setting in dts file like this. &fec1 {     pinctrl-names = "default";     pinctrl-0 = <&pinctrl_enet1 &pinctrl_enet_reset>;     assigned-clocks = <&clks IMX7D_ENET_PHY_REF_ROOT_SRC>,               <&clks IMX7D_ENET_AXI_ROOT_SRC>,               <&clks IMX7D_ENET1_TIME_ROOT_SRC>,               <&clks IMX7D_ENET1_TIME_ROOT_CLK>,               <&clks IMX7D_ENET_AXI_ROOT_CLK>;     assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_25M_CLK>,                  <&clks IMX7D_PLL_ENET_MAIN_250M_CLK>,                  <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;     assigned-clock-rates = <0>, <0>, <0>, <100000000>, <250000000>;     phy-mode = "rgmii";     phy-handle = <&ethphy0>;     phy-reset-gpios = <&gpio1 3 0>;     fsl,magic-packet;     status = "okay";     mdio {         #address-cells = <1>;         #size-cells = <0>;         ethphy0: ethernet-phy@1 {    //here '@1' is the PHY address             compatible = "ethernet-phy-ieee802.3-c22";             reg = <1>;         };     }; }; Add the GPIO pin for the ENET_RESET_B &iomuxc { ... ... pinctrl_enet_reset: enet_resetgrp {             fsl,pins = <                 MX7D_PAD_GPIO1_IO03__GPIO1_IO3      0x14     //ENET_RESET_B             >;         }; } There is a PHY fixup in the arch/arm/mach-imx/<imx_cpu>.c Here is the example in mach-imx7d.c #define PHY_ID_KSZ9031    0x00221620 #define MICREL_PHY_ID_MASK 0x00fffff0 static void mmd_write_reg(struct phy_device *dev, int device, int reg, int val) {     phy_write(dev, 0x0d, device);     phy_write(dev, 0x0e, reg);     phy_write(dev, 0x0d, (1 << 14) | device);     phy_write(dev, 0x0e, val); } static int ksz9031rn_phy_fixup(struct phy_device *dev) {     /*      * min rx data delay, max rx/tx clock delay,      * min rx/tx control delay      */     mmd_write_reg(dev, -1, 0x4, 0);     mmd_write_reg(dev, -1, 0x5, 0);     mmd_write_reg(dev, -1, 0x6, 0);     mmd_write_reg(dev, -1, 0x8, 0x003ff);     return 0; } static void __init imx7d_enet_phy_init(void) {     if (IS_BUILTIN(CONFIG_PHYLIB)) {         phy_register_fixup_for_uid(PHY_ID_AR8031, 0xffffffff,                        ar8031_phy_fixup);         phy_register_fixup_for_uid(PHY_ID_BCM54220, 0xffffffff,                        bcm54220_phy_fixup);         phy_register_fixup_for_uid(PHY_ID_KSZ9031, MICREL_PHY_ID_MASK,                 ksz9031rn_phy_fixup);     } } Now, the PHY is working on your board. Reference: 1.  Create an Ubuntu VM environment to build Yocto BSP  2.  i.MX Software | NXP 
查看全文
imx8mm platform on 4.14.78/98 GA Android  LCD MIPI panel or HDMI display may appear some strange color stride .  This is  one patch for this issue. 
查看全文
恩智浦BSP的内核定制 ........................................... 103 6.1 IO管脚配置与Pinctrl驱动 .................................... 103 6.2 新板bringup ........................................................ 118 6.3 更改调试串口: .................................................. 127 6.4 uSDHC设备定制(eMMC flash,SDcard, SDIOcard) 133 6.5 LVDS LCD 驱动定制 .......................................... 142 6.6 GPIO_Key 驱动定制 .......................................... 145 6.7 GPIO_LED 驱动定制 ......................................... 149 6.8 Fuse nvram驱动 ................................................. 152 6.9 SPI与SPI Slave驱动 ........................................... 153 6.10 USB 3.0 TypeC 改成 USB 3.0 TypeA(未验证) ... 160 6.11 汽车级以太网驱动定制 ....................................... 160
查看全文
Platform: imx8qxp mek b0. OS: android imx-p9.0.0_2.1.0-auto-ga. Hardware block: brief: Android p9 ga enabled the hardware partition, so it is impossible to share dpu between AP and m4, and seamless switching can be achieved by keeping the last m4 ui frame until android ui is ready. To achieve seamless switch between android A core and M4 core on android ga, user needs to modify two parts: Linux kernel: remove init or configure codes of dpu units and lvds used by m4 core M4 code: modify dpu pipes, share memory with android partition.        Switching flow:        M4 release and move camera, dpu to android partition and share the display buffer memory with android, android will not init the dpu subsyses that have been inited by m4 and will keep the m4 last frame ui until android ui is ready. Imx8qxp dpu block: Android and M4 shared dpu path:
查看全文
iMX8QXP/iMX8QM have hardware JPEG decoder: The JPEG-D-X core. This is the example code to use this hw decoder in M4 SDK to decode JPEG files. M4_JPEG_DECODER_SDK_2.5.1.7z The attached "rear_view_camera_jpegdec.tar.bz2" is the updated source code for "SDK\boards\mekmimx8qx\demo_apps\rear_view_camera". It is based on SDK 2.5.1 for iMX8QXP MEK. The "rear_view_camera_jpegdec.patch" is the modified code, it hasn't included the added "fsl_jpeg_dec.c" and "fsl_jpeg_dec.h".   The testing used two 256*256 JPEG files, they are RGB color space. We used followed commands to build them into flash.bin: ./mkimage_imx8 -soc QX -rev B0 -append ahab-container.img -c -scfw scfw_tcm.bin -m4 m4_rear_view_camera.bin 0 0x34FE0000 --data demo_rgb.jpg 0x84000000 --data demo_rgb2.jpg 0x84008000 -out flash.bin   If customer need change the JPEG resoluion, they can change them in file "fsl_jpeg_dec.h", APP_JPEG_SIZE_OF_KB is the JPEG file length in memory, aligned in KB.   #define APP_JPEG_WIDTH (256) #define APP_JPEG_HEIGHT (256) #define APP_JPEG_SIZE_OF_KB (32) #define APP_JPEG_FORMAT JPEG_RGB #define APP_JPEG_BUFFER (0x84000000)   To created RGB format JPEG file from RGB data, the customer can use linux unit test application "/unit_tests/JPEG/encoder_test.out". M4_JPEG_DECODER_WINDOW_MODE_SDK_2.5.1.7z Based on JEPG decoder, added DPU CSC support and render JEPG decoded video in overlay window. The architecture is followed: NXP logo is put in FetchLayer0 with RGB565 format, after LayerBlend0, it will be the prim layer for LayberBlend1 (FetchLayer0 can't be used as prim layer for LayerBlend), the JPEG decoder output is put to FetchDecoder0. RGB888 format, and it will be resize to 640*480, and put to x=100, y=100 of the display. (Only the sec layer of LayerBlend can be window mode). Some limitation for layer selection in LayerBlend:
查看全文
Please join us for a webinar tomorrow - July 30 at 10 AM CDT. Register here: https://info.cranksoftware.com/resources/modernize-embedded-graphics-ultra-low-power-ui-nxpcranksoftware NXP’s i.MX 7ULP applications processor, alongside Crank's Storyboard GUI design and development software, gives embedded teams the best of both worlds – rich 2D/3D performance with MCU-level low power. Join Brian Edmond and Nik Jedrzejewski to get a technical deep dive into the i.MX 7ULP and Storyboard and learn: the latest trends in graphics for battery-powered devices hardware features of the i.MX 7ULP, including the Heterogeneous Domain Computing architecture how to leverage Storyboard's hybrid rendering solution when switching between 2D and 3D graphics to minimize power consumption   PANELLISTS Brian Edmond, President, Crank Software Nik Jedrzejewski, i.MX Product Manager, NXP
查看全文
The Guide is how to use Ubuntu filesystem with i.MX8 series platform.At present, I had try it on i.MX8QXP with 4.14.98 kernel with ubuntu16.04. The Document will be continuously updated with enable VPU, ubuntu18.04. The desktop we can chose Gnome or weston.  Because driver  support issue, gc7000 series gpu not support render Gnome destop but it can render weston destop.  Update 2019/7/31: Ubuntu-i.MX8-weston.pdf   Feature: weston + ubuntu18.04 + 4.14.98 kernel VPU (enable with gplay or gst-play)  GPU (could render desktop and run GPU demo under root privileges on Weston Desktop) I also try ubuntu with gnome desktop, ubuntu18.04 can not run gnome, need use ubuntu19.04. But Gnome Desktop just render by CPU.  ------------------------------------------------------------------------------------- Update 2020/3/6: Ubuntu-i.MX8M.pdf Just a simple guide for IMX8M series, will be  continuously updated. 
查看全文
In this doc will show how to adjust display brightness/contrast/saturation by using i.MX8  Display Controller (DC) Subsystem.   HW: i.MX8QXP MEK board SW: Linux 4.14.98_2.0.0 BSP release.   See i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual, Rev. 😧 This kind Matrix total number is 5 , that is 0/1/4/5/9. In this doc using Matrix0 to adjust whole display brightness/contrast/saturation. Matrix0 unit position is located between FramGen unit and Tcon unit, that means using Matrix0 will impact on the whole display contents. Note, this Matrix is applied on RGB color space.    The Matrix is consist of two parts: and  You can program any value into register of A11 to A44 and C1 to C4, Matrix will applied on input RGB data, then output RGB data will changed as you want. In this way, we can change the display brightness/contrast/saturation. The Matrix entry from A11 to A44, their register format is same as below: Each register entry of A11 to A44 , total 13 bit, bit 12 is symbol bit , bit 11 and bit 10 is integer bit, bit 9 to bit 0 is floating point bit. The Matrix entry from C1 to C4, their format is same as below: Each register entry of C1 to C4, total 13 bit, bit 12 is symbol bit, others are integer bit. Now let us choose the matrix that will be used for adjust brightness/contrast/saturation. See this link  https://docs.rainmeter.net/tips/colormatrix-guide/ So we can set matrix as below to change brightness/contrast/saturation   A11=c(sr+s)   A12=c(sg)    A13=c(sb)   A21=c(sb)     A22=c(sg+s)  A23=c(sb)   A31=c(sr)     A32=c(sg)    A33=c(sb+s)   C1=C2=C3=t+b   b as brightness , range[-1.0, 1.0], zero means no change , >0 will increases brightness, <0 will reduce brightness. c as contrast, range [0,2.0) , default is 1.0 , >1.0 is increase , <1.0 is reduce. s is saturation, range [0,1.0], default is 1.0.  Other matrix entry is related to alpha, in this doc not change it, just keep them as zero.     Note here sr,sb,sg value will depend on lumR/ lumG/ lumB constant value you choose, this value may depend on different color standard.   Due to each matrix value is floating point number, and in this doc , i.MX8X run Linux OS. So you can choose do floating point operation in user space program, then pass related register value into kernel space , let driver write them into register. But in this doc, to make Linux kernel driver more simple, I will convert floating point operation into integer operation , then user space app just pass brightness/contrast/saturation value into kernel space, then kernel driver to do left operation in kernel space. So 1024*c and 1024*s is integer number that user space app will passed into kernel space. And in kernel space could be do left integer number operation, then write register value. The kernel patch 8qxp_4.14.98_brightness_contrast_saturation.diff could be used on 4.14.98_2.0.0 BSP release. Test usage, need used one patch that for proptest which from libdrm test case, see 8qxp_prop_test.diff, recompile the proptest case. root@imx8qxpmek:~# ./proptest     //list current drm property CRTC 32         42 bringhtness:                 flags: range                 values: 0 131071                 value:0x0         43 contrast:                 flags: range                 values: 0 2048                 value:0x400         44 saturation:                 flags: range                 values: 0 1024                 value:0x400         45 update:                 flags: range                 values: 0 1                 value:0x0   I add four drm property , brightness, contrast, saturation, update. The “update property” should be set as 1 at last, otherwise kernel space will not update related property. Reference API usage ( in 8qxp_prop_test.diff) +     drmModeObjectSetProperty(fd_rend, obj_id, obj_type, 42, b_int); +     drmModeObjectSetProperty(fd_rend, obj_id, obj_type, 43, c_int); +     drmModeObjectSetProperty(fd_rend, obj_id, obj_type, 44, s_int); +     drmModeObjectSetProperty(fd_rend, obj_id, obj_type, 45, 1);      //run cmd as below , will ask you input related brightness/contrast/saturation value , then will get result in display root@imx8qxpmek:~# ./proptest 32 crtc 45 1   input brightness [-1,1] 0.3 input contrast, >1.0 or <1.0 1.2 input saturation, [0,1] 0.3 brightness 0.300000  0x133 from [-1,1] percent contrast  1.200000  0x4cc >1.0 or <1.0 saturation 0.300000 0x133  from 0.0 to 1.0   Known Issue: For demo this feature , I need run proptest and weston at same time. Due to the set property drm ioctl default allowed by DRM master and DRM control client. But 4.14. kernel, removed the DRM control device node, so I changed to open drm render node fd, and allow DRM render client to using set property drm ioctl.  This is just a workaround, you may not use it. Reference: 1.https://www.nxp.com/docs/en/reference-manual/IMX8DQXPRM.pdf  2.https://docs.rainmeter.net/tips/colormatrix-guide/
查看全文
Brief introduction on i.MX Android
查看全文