恩智浦BSP的内核定制 ........................................... 103
6.1 IO管脚配置与Pinctrl驱动 .................................... 103
6.2 新板bringup ........................................................ 118
6.3 更改调试串口: .................................................. 127
6.4 uSDHC设备定制(eMMC flash,SDcard, SDIOcard)
133
6.5 LVDS LCD 驱动定制 .......................................... 142
6.6 GPIO_Key 驱动定制 .......................................... 145
6.7 GPIO_LED 驱动定制 ......................................... 149
6.8 Fuse nvram驱动 ................................................. 152
6.9 SPI与SPI Slave驱动 ........................................... 153
6.10 USB 3.0 TypeC 改成 USB 3.0 TypeA(未验证) ... 160
6.11 汽车级以太网驱动定制 ....................................... 160
chipset rm error and need update the emmc support to 5.1, will modify it in next version.
firmware version should be: modify in next version
注意:也可以如下使用wget命令获得mx8qx-ahab-container.img
wget http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.1.bin
chmod +x firmware-imx-8.1.bin && ./ firmware-imx-8.1.bin --auto-accept
mx8qx-ahab-container.img位于firmware-imx-8.1/firmware/seco/mx8qx-ahab-container.img
updated to v3
增加nandflash
支持/DDR 修
改/i.MX8DX
支持