i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Customer is asking high-capacity external storage(for example >64GB) support on i.MX BSP, ext4 is ok for HC storage, but it can’t be supported by Windows. Pls find NFTS and exFAT support status on Linux BSP below: Updated test result on L5.4.70.2.3.0 and L6.1.22: L5.4.70.2.3.0 1.You can enable ntfs support in kernel config as below,  ntfs can be mounted normally, but you can only modify existing file content in disk, you can’t create/delete/rename file on disk. > File systems > DOS/FAT/NT Filesystems Lambert_0-1694955886098.jpeg   Log: root@imx8mpevk:~# mount -t ntfs /dev/sda1 /mnt/fat/ [  662.732869] ntfs: volume version 3.1. root@imx8mpevk:~# cp ntfs-3g /mnt/fat/ cp: cannot create regular file '/mnt/fat/ntfs-3g': Permission denied root@imx8mpevk:~# ls /mnt/fat/ 111.png  Image_org  System Volume Information  gpuinfo.sh root@imx8mpevk:~# vi /mnt/fat/gpuinfo.sh root@imx8mpevk:~# umount /mnt/fat/ root@imx8mpevk:~# ntfs file system can be accessed via ntfs-3g in user space as below //build: wget https://tuxera.com/opensource/ntfs-3g_ntfsprogs-2017.3.23.tgz tar zxvf ntfs-3g_ntfsprogs-2017.3.23.tgz cd ntfs-3g_ntfsprogs-2017.3.23/ source ../../sdk/environment-setup-aarch64-poky-linux   ./configure --host=aarch64-linux --build=aarch64-poky-linux --disable-shared --enable-static   make   ls /src/ntfs-3g   //put it into rootfs cp ntfs-3g /bin   //test log: root@imx8mpevk:/# [ 1058.724471] usb 1-1: USB disconnect, device number 4 [ 1062.058613] usb 1-1: new high-speed USB device number 5 using xhci-hcd [ 1062.214029] usb-storage 1-1:1.0: USB Mass Storage device detected [ 1062.220986] scsi host0: usb-storage 1-1:1.0 [ 1063.235871] scsi 0:0:0:0: Direct-Access     VendorCo ProductCode      2.00 PQ: 0 ANSI: 4 [ 1063.246185] sd 0:0:0:0: [sda] 15728640 512-byte logical blocks: (8.05 GB/7.50 GiB) [ 1063.254023] sd 0:0:0:0: [sda] Write Protect is off [ 1063.259164] sd 0:0:0:0: [sda] No Caching mode page found [ 1063.264540] sd 0:0:0:0: [sda] Assuming drive cache: write through [ 1063.296946]  sda: sda1 [ 1063.300860] sd 0:0:0:0: [sda] Attached SCSI removable disk   root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh root@imx8mpevk:/# cp /unit_tests/memtool /mnt/fat/ root@imx8mpevk:/# umount /mnt/fat/ root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh  memtool root@imx8mpevk:/#   3.exFAT is not supported on this BSP..   L6.1.22(you can check it on L5.15 and above, should be the same) You can enable ntfs support in kernel config as below, full features can be supported. > File systems > DOS/FAT/EXFAT/NT Filesystems Lambert_1-1694955886116.jpeg   Pls use ‘-t ntfs3’ during mounting, otherwise it will be mounted as ‘read-only’ Log: root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information' root@imx8ulpevk:~# root@imx8ulpevk:~# cp gpuinfo.sh /mnt/fat/ root@imx8ulpevk:~# umount /mnt/fat/ root@imx8ulpevk:~# root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information'   gpuinfo.sh root@imx8ulpevk:~#   exFAT has been supported in L6.1.22. > File systems > DOS/FAT/EXFAT/NT Filesystems Lambert_2-1694955886139.jpeg   /dev/sda1 on /run/media/sda1 type exfat (rw,relatime,fmask=0022,dmask=0022,iocharset=utf8,errors=remount-ro) root@imx8ulpevk:~# ls /run/media/sda1 'Certificate of Completion.pdf'             carlife.MP4 Image_org                                  example.tflite L5.4.70_2.3.0                              mx8mp_vpu.txt NXP-5G.mp4                                 sd.mp4 'System Volume Information'                 vela.ini android_p9.0.0_2.1.0-auto-ga_image_8qmek root@imx8ulpevk:~# ls Image_org  gpuinfo.sh root@imx8ulpevk:~# cp gpuinfo.sh /run/media/sda1/ root@imx8ulpevk:~# umount /run/media/sda1 root@imx8ulpevk:~#
查看全文
Platform i.MX8MPlus EVK, Android 13 Background Customer find we have enabled all configs about pstore and ramoops, but they can't get ramoops log in /sys/fs/pstore node on Android 13. Solution The default reboot will reset all hardware including the DDR control, so this will result in the loss of the log stored in RAM. We have include such codes in ATF, the default code will use imx_wdog_restart(true) to reset all hardware. void __dead2 imx_system_reset(void) { #ifdef IMX_WDOG_B_RESET imx_wdog_restart(true); #else imx_wdog_restart(false); #endif }   To avoid DDR reset, we should comment  IMX_WDOG_B_RESET in vendor/nxp-opensource/arm-trusted-firmware/plat/imx/imx8m/imx8mp/include/platform_def.h Zhiming_Liu_0-1693468718652.png   Result evk_8mp:/sys/fs/pstore # ls console-ramoops-0 dmesg-ramoops-0 pmsg-ramoops-0  
查看全文
In the i.MX 8M Plus LPDDR4 EVK board there are two Type-C port design. For the port0 is used to power supply no usb function, for the port1 used for USB function but without PD function. But in customer’s design, customer only use one USB design on their board, how to make the one USB work with the PD and USB function, we need to make the hardware design and software modify. This article only give method to realized it and have tested and realized the port1 PD function. 1 Introduction of the USB interface on i.MX8MP         There are two USB 3.0 TypeC controllers with integrated PHY interface on the i.MX8MP: Backward compatibility with USB 2.0 Spread spectrum clock support b45499_0-1664552067335.png   The USB on the i.MX8MP supports USB3.0 and is compatible with USB2.0 downward. We can see that the upper layer is the universal layer for USB 2.0 and USB 3.0 operations. This is a common interface, buffer management block, list processor, used to schedule and control the status register (CSR) function: USB 2.0 physical layer and MAC layer USB 3.0 physical layer, link layer and MAC layer b45499_1-1664552067341.png   Features of USB 3.0: USB compliant version 3.0 (xHCI compatible) Supports operation as a stand-alone USB host controller USB dual role operation, configurable as host or device Ultra high speed (5Gbit/s), high speed (480Mbit/s), full speed (12Mbit/s) and low speed (1.5Mbit/s) operation. Support independent single port USB operation Support for four programmable bidirectional USB endpoints Support system memory interface with 40 bit addressing capability   2 Design of USB on Development Board         The i.MX 8M Plus processor includes two USB 2.0/3.0 controllers and two integrated USB PHYs. USB supports both running as an independent USB host controller and dual role USB operation, and can be configured as a host or device. Therefore, the design of these two functions is implemented on the development board of i.MX8MP. b45499_2-1664552067507.png   We can see that on the development board, one USB1 is used for the USB Type-C port and the other USB2 is used for the USB 3.0 host port. USB Type-C port 0 (J5) is only used for power supply. It does not support USB data transfer. It is the only power port, so the system must always be powered.   On the CPU side of the schematic diagram, we can also see that USB1 is the port for USB Type-C, and USB2 is the host for USB3.0. b45499_3-1664552067525.png    USB1 is designed as USB Type-C: b45499_4-1664552067554.png   USB2 USB3.0 Host design: b45499_5-1664552067564.png   Power design of the USB Type-C port: b45499_6-1664552067594.png   3 Only one USB interface is used in the design (compatible with both USB PD function and USB dual roles function)         Two USB Type-C ports are used on our development board. One is used to power the board separately, and the other is used as the function of USB Type-C. However, due to the limited design cost and chip layout and space on the board, some customers will use a USB interface to realize the dual role function of power supply and USB. How to achieve this? USB Device(Download mode): b45499_7-1664552067607.png     USB Host mode(power+device Need the hub support PD function): b45499_8-1664552067639.png     The specific implementation and design are as follows: 3.1 Hardware realize PTN5110 To realize the USB Type-C support power supply function, PTN5110 (USB PD TCPC PHY IC) chip is required to realize Type-C data logic and power control and management. The selection of PTN5110 is critical and important.   PTN5110 is a single port USB PD (power supply) PHY IC that conforms to TCPC. It integrates Type-C configuration channel (CC) interface and USB PD physical layer functions into Type-C port manager (TCPM) that handles PD policy management. It complies with USB PD, Type-C and TCPC specifications.   The IC is mainly aimed at applications in system platforms (such as laptops, desktops, Chromebooks, tablets, flip notebooks, etc.). Other application cases may be feasible, depending on the application architecture, such as docking stations, displays, accessories, cable adapters, smartphones, etc.   It can support various Type-C applications: Sink, Source, Sink with accessory support or DRP. It executes Type-C CC simulation part (i.e. Rd/Rp/Ra detection, Rd/Rp indication) and PD Tx/Rx PHY and protocol state machine. PTN5110 supports TCPM in the system implementation of the following PD roles.   PTN5110 integrates VCONN load switch, programmable current limit, reverse leakage current blocking and over temperature protection (OTP). It is equipped with two enable control outputs to control the load switch/FET in the VBUS pull and/or sink path. It can also perform VBUS voltage monitoring/measurement, VBUS forced discharge and discharge discharge.   PTN5110 provides the main IO related functions for the main processor/TCPM, so that Type-C/PD interfaces can be easily controlled and managed through the TCPC interface.   PTN5110 supports a wide range of power input voltages, providing platform integrators with great flexibility. PTN5110 can run on VBUS to support specific system use cases that require no power operation.https://www.nxp.com/products/interfaces/usb-interfaces/usb-type-c/usb-pd-phy-and-cc-logic/usb-pd-tcpc-phy-ic:PTN5110   The design only use the USB1: b45499_9-1664552067666.png   Here, it is required to weld R53 or R54. You can refer to this design completely. 2 Software modify Modify the BPS of the software: Take the newest released Linux 5.15.32_2.0.0​ as example: In the u-boot /board/freescale/imx8mp_evk/imx8mp_evk.c   b45499_10-1664552067672.png   It can be seen that the PD function of the port is turned off, so if you want to use USB1 for power supply, remove the following commands and turn on the PD function of USB1. “-   .disable_pd = true,” Use the above action to enable Port1 PD function. Kernel section modify: Kernel section modify towards to PTN5110. Type-C Configure channel (CC) interface: root/drivers/usb/typec/tcpm/tcpci.c @@ -524,6 +524,7 @@ static int tcpci_vbus_force_discharge(struct tcpc_dev *tcpc, bool enable)  static int tcpci_set_vbus(struct tcpc_dev *tcpc, bool source, bool sink)  {        struct tcpci *tcpci = tcpc_to_tcpci(tcpc); +      unsigned int reg;        int ret;          if (tcpci->data->set_vbus) { @@ -533,16 +534,20 @@ static int tcpci_set_vbus(struct tcpc_dev *tcpc, bool source, bool sink)                         return ret < 0 ? ret : 0;        }   +      ret = regmap_read(tcpci->regmap, TCPC_POWER_STATUS, &reg); +      if (ret < 0) +              return ret; +        /* Disable both source and sink first before enabling anything */   -       if (!source) { +      if (!source && (reg & TCPC_POWER_STATUS_SOURCING_VBUS)) {                 ret = regmap_write(tcpci->regmap, TCPC_COMMAND,                                     TCPC_CMD_DISABLE_SRC_VBUS);                 if (ret < 0)                         return ret;        }   -       if (!sink) { +      if (!sink && (reg & TCPC_POWER_STATUS_SINKING_VBUS)) {                 ret = regmap_write(tcpci->regmap, TCPC_COMMAND,                                     TCPC_CMD_DISABLE_SINK_VBUS);                 if (ret < 0)   Type-C port manager managed by PD (TCPM): root/drivers/usb/typec/tcpm /tcpm.c @@ -340,6 +340,7 @@ struct tcpm_port {         */        bool vbus_vsafe0v;   +      bool vbus_keep;        bool vbus_never_low;        bool vbus_source;        bool vbus_charge; @@ -3662,7 +3663,8 @@ static void tcpm_reset_port(struct tcpm_port *port)        port->rx_msgid = -1;          port->tcpc->set_pd_rx(port->tcpc, false); -       tcpm_init_vbus(port);     /* also disables charging */ +      if (!port->vbus_keep) +              tcpm_init_vbus(port);  /* also disables charging */        tcpm_init_vconn(port);        tcpm_set_current_limit(port, 0, 0);        tcpm_set_polarity(port, TYPEC_POLARITY_CC1); @@ -5834,6 +5836,9 @@ static void tcpm_init(struct tcpm_port *port)          port->tcpc->init(port->tcpc);   +      port->vbus_present = port->tcpc->get_vbus(port->tcpc); +      if (port->vbus_present) +              port->vbus_keep = true;        tcpm_reset_port(port);          /* @@ -5872,7 +5877,10 @@ static void tcpm_init(struct tcpm_port *port)         * Some adapters need a clean slate at startup, and won't recover         * otherwise. So do not try to be fancy and force a clean disconnect.         */ -       tcpm_set_state(port, PORT_RESET, 0); +      if (!port->vbus_keep) +              tcpm_set_state(port, PORT_RESET, 0); + +      port->vbus_keep = false;  }    static int tcpm_port_type_set(struct typec_port *p, enum typec_port_type type) Note: The software just needs to modify these two parts. You also need to mention to the proper the I2C port use, if not proper the driver of the PTN5110 can not driver. 4 Test         In our i. MX8MP EVK development board show that R53 and R54 in the USB1 part of our development board are in DNP status, so VBUS_ IN is disconnected and no power comes in. Here, connect R53 or R54 with solder, so that VBUS_ IN, the power comes in again. After the power is connected. The board can be powered through USB1. 4.1 Download images to the emmc on the Board: Power from the USB1, set the boot mode to serial download mode, then go to download images finished. 4.2 Boot up the board from the EMMC Change the boot mode to boot up from EMMC,the board boot up, the log file is as following show: b45499_11-1664552067688.png   It will stop at the TCPC for the section of PTN5110 driver. By default, the PD function of port1 in the u-boot is turned off, so if you want to use USB1 for power supply, remove the following commands and turn on the PD function of USB1. “-   .disable_pd = true,” After the PD function is turned on, the board can be started normally, but the whole part running to the kernel will be powered down, so the kernel part of PTN5110 still needs to be modified. After the patch modification of the above kernel part, the board can run normally.         I also did the same experiment on the i.MX8MM EVK development board. The same phenomenon occurs when the kernel starts. Therefore, similar modifications to the above i. MX8MP can work normally. Summary: In one word i.MX8MP and i.MX8M series can realize the role of using a USB for power supply and USB Dual. The hardware design refers to our development board, and we must use the logic chip PTN5110. For software, refer to the above code modification.  
查看全文
Hello everyone! In this quick example its focused on how to customize uboot code to generate an uboot image with a silent console so its speed up the flash and boot time, this may provide helpful for customers who have a bigger images or just want to have a silent console. Note: this should not be enabled if the image is still being under test, since this will disable all communication with the debug terminal and there won't be boot messages. Requirements: I.MX 8M Nano DDR4 EVK i.MX 8M Nano EVK Prebuilt image (6.1.1-1.0.0) UUU tool First clone the code from the uboot repository: $ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.1.1-1.0.0 $ cd uboot-imx After we get the code, then proceed to enable the silent console in the uboot defconfig: $ nano configs/imx8mn_ddr4_evk_defconfig CONFIG_SILENT_CONSOLE=y CONFIG_SILENT_U_BOOT_ONLY=y For this to actually work we need to create the silent environmental variable and give it a value different from "0": $ nano include/configs/imx8mn_evk.h "silent=1\0"      \ As specified in our Linux porting guide: Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command, set Target-Machine to the machine you are building for. See Section "Build configurations" in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG) Set up the host terminal window toolchain environment: $ source/opt/fsl-imx-xwayland/6.1.1/environment-setup-aarch64-poky-linux $ export ARCH=arm64 Build uboot binary: $ make distclean $ make imx8mn_ddr4_evk_defconfig $ make Build ARM Trusted Firmware (ATF) $ cd .. $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.1.1-1.0.0 $ cd imx-atf/ $ make PLAT=imx8mn bl31 In case you get the error aarch64-poky-linux-ld.bfd: unrecognized option '-Wl,-O1' $ unset LDFLAGS Download the DDR training & HDMI binaries $ cd .. $ mkdir firmware-imx $ cd firmware-imx $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.19.bin $ chmod a+x firmware-imx-8.19.bin $ ./firmware-imx-8.19.bin Accept EULA and the firmware will be deployed. Download imx-mkimage and build the boot image $ cd .. $ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.1.1-1.0.0 $ cd imx-mkimage $ cp ../uboot-imx/spl/u-boot-spl.bin iMX8M/ $ cp ../uboot-imx/u-boot-nodtb.bin iMX8M/ $ cp ../uboot-imx/arch/arm/dts/imx8mn-ddr4-evk.dtb iMX8M/ $ cp ../imx-atf/build/imx8mn/release/bl31.bin iMX8M/ $ cp ../firmware-imx/firmware-imx-8.19/firmware/ddr/synopsys/ddr4_* iMX8M/ $ cp ../uboot-imx/tools/mkimage iMX8M/mkimage_uboot $ make SOC=iMX8MN flash_ddr4_evk After this we can download our uboot image to our board, we can either use the uboot image for boot or for flashing purpose only. We can compare the time it takes using UUU with a standard pre-built image uuu -V -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-full-imx8mnevk.wic AldoG_0-1692908409933.png It takes 485.5 seconds using normal uboot with debug console enabled. uuu -V -b emmc_all flash.bin imx-image-full-imx8mnevk.wic AldoG_1-1692908409934.png It takes 477.5 seconds using silent uboot console. Even if the speed is not greatly improved (~8 seconds), in larger files it could help to speed up flashing, even if wants to have the console silent is a good option. Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
查看全文
1.Test environment Board: i.MX8MPlus, RM67199 BSP: uboot 2022.04, linux-6.1.1-1.0.1 2.Modification of uboot  In uboot, you need comment the video_link_shut_down and dm_remove_devices_flags in announce_and_cleanup function. #if defined(CONFIG_VIDEO_LINK) //video_link_shut_down(); #endif board_quiesce_devices(); printf("\nStarting kernel ...%s\n\n", fake ? "(fake run for tracing)" : ""); /* * Call remove function of all devices with a removal flag set. * This may be useful for last-stage operations, like cancelling * of DMA operation or releasing device internal buffers. */ // #ifndef CONFIG_POWER_DOMAIN // dm_remove_devices_flags(DM_REMOVE_ACTIVE_ALL | DM_REMOVE_NON_VITAL); // /* Remove all active vital devices next */ // dm_remove_devices_flags(DM_REMOVE_ACTIVE_ALL); // #endif cleanup_before_linux(); }  After doing this, the uboot logo will not be cleaned before Linux PM framework. 3.Modification of Linux You need add  CONFIG_LOGO=n into defconfig file to disable kernel logo.  3.1 Disable the power down of mediamix and mipi-dphy in gpcv2.c Please add below code into the beginning of  imx_pgc_power_down function if ((strcmp(genpd->name, "mipi-phy1") == 0) || (strcmp(genpd->name, "mediamix") == 0)) { return 0; }  3.2 Only reset lcdif in the last call of drm framework Please modify imx_lcdifv3_runtime_resume function like this. The imx_lcdifv3_runtime_resume function will be called two times, thus the lcdif will be reset two times.We can let it only reset last time,which before the rootfs mount. bool rst = false; ////////////////////////////// static int imx_lcdifv3_runtime_resume(struct device *dev) { int ret = 0; struct lcdifv3_soc *lcdifv3 = dev_get_drvdata(dev); if (unlikely(!atomic_read(&lcdifv3->rpm_suspended))) { dev_warn(lcdifv3->dev, "Unbalanced %s!\n", __func__); return 0; } if (!atomic_dec_and_test(&lcdifv3->rpm_suspended)) return 0; /* set LCDIF QoS and cache */ if (of_device_is_compatible(dev->of_node, "fsl,imx93-lcdif")) regmap_write(lcdifv3->gpr, 0xc, 0x3712); request_bus_freq(BUS_FREQ_HIGH); ret = lcdifv3_enable_clocks(lcdifv3); if (ret) { release_bus_freq(BUS_FREQ_HIGH); return ret; } ////////////////////////////// if (rst) { /* clear sw_reset */ writel(CTRL_SW_RESET, lcdifv3->base + LCDIFV3_CTRL_CLR); rst = false; } rst = true; ////////////////////////////// /* enable plane FIFO panic */ lcdifv3_enable_plane_panic(lcdifv3); return ret; } 4.Conclusion The uboot logo will be cleaned at log "imx-drm 1.0.0 20120507 for display-subsystem on minor 1". The boot time of  systemd service on evk is very long. For weston.service, it needs 3 seconds. From log here we test, the pcie and ethernet probe after drm system also cost about 1 second. If you want to reduce the boot time of other modules, you can try to reduce the system service and disable pcie/ethernet drivers if you don't need them. [ 2.505616] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1 [ 2.620324] imx6q-pcie 33800000.pcie: iATU unroll: enabled [ 2.620335] imx6q-pcie 33800000.pcie: iATU regions: 4 ob, 4 ib, align 64K, limit 16G [ 2.720689] imx6q-pcie 33800000.pcie: PCIe Gen.1 x1 link up [ 2.820996] imx6q-pcie 33800000.pcie: PCIe Gen.2 x1 link up [ 2.821003] imx6q-pcie 33800000.pcie: Link up, Gen2 [ 2.821010] imx6q-pcie 33800000.pcie: PCIe Gen.2 x1 link up [ 2.821112] imx6q-pcie 33800000.pcie: PCI host bridge to bus 0000:00 [ 2.821119] pci_bus 0000:00: root bus resource [bus 00-ff] [ 2.821126] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] [ 2.821133] pci_bus 0000:00: root bus resource [mem 0x18000000-0x1fefffff] [ 2.821161] pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400 [ 2.821176] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff] [ 2.821187] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref] [ 2.821232] pci 0000:00:00.0: supports D1 [ 2.821237] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold [ 2.824664] pci 0000:01:00.0: [1b4b:2b42] type 00 class 0x020000 [ 2.824725] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x000fffff 64bit pref] [ 2.824761] pci 0000:01:00.0: reg 0x18: [mem 0x00000000-0x000fffff 64bit pref] [ 2.825066] pci 0000:01:00.0: supports D1 D2 [ 2.825072] pci 0000:01:00.0: PME# supported from D0 D1 D3hot D3cold [ 2.835499] pci 0000:00:00.0: BAR 0: assigned [mem 0x18000000-0x180fffff] [ 2.835511] pci 0000:00:00.0: BAR 15: assigned [mem 0x18100000-0x182fffff pref] [ 2.835519] pci 0000:00:00.0: BAR 6: assigned [mem 0x18300000-0x1830ffff pref] [ 2.835530] pci 0000:01:00.0: BAR 0: assigned [mem 0x18100000-0x181fffff 64bit pref] [ 2.835561] pci 0000:01:00.0: BAR 2: assigned [mem 0x18200000-0x182fffff 64bit pref] [ 2.835590] pci 0000:00:00.0: PCI bridge to [bus 01-ff] [ 2.835598] pci 0000:00:00.0: bridge window [mem 0x18100000-0x182fffff pref] [ 2.835899] pcieport 0000:00:00.0: PME: Signaling with IRQ 218 [ 2.897767] Console: switching to colour frame buffer device 135x120 [ 3.098361] imx-drm display-subsystem: [drm] fb0: imx-drmdrmfb frame buffer device [ 3.111239] pps pps0: new PPS source ptp0 [ 3.316650] fec 30be0000.ethernet eth0: registered PHC device 0 [ 3.323645] imx-dwmac 30bf0000.ethernet: IRQ eth_lpi not found [ 3.329593] imx-dwmac 30bf0000.ethernet: force_sf_dma_mode is ignored if force_thresh_dma_mode is set. [ 3.340074] imx-dwmac 30bf0000.ethernet: User ID: 0x10, Synopsys ID: 0x51 [ 3.346883] imx-dwmac 30bf0000.ethernet: DWMAC4/5 [ 3.351684] imx-dwmac 30bf0000.ethernet: DMA HW capability register supported [ 3.358825] imx-dwmac 30bf0000.ethernet: RX Checksum Offload Engine supported [ 3.365966] imx-dwmac 30bf0000.ethernet: Wake-Up On Lan supported [ 3.372113] imx-dwmac 30bf0000.ethernet: Enable RX Mitigation via HW Watchdog Timer [ 3.379778] imx-dwmac 30bf0000.ethernet: Enabled L3L4 Flow TC (entries=8) [ 3.386573] imx-dwmac 30bf0000.ethernet: Enabled RFS Flow TC (entries=10) [ 3.393373] imx-dwmac 30bf0000.ethernet: Enabling HW TC (entries=256, max_off=256) [ 3.400950] imx-dwmac 30bf0000.ethernet: Using 34 bits DMA width [ 3.608045] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 3.613580] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1 [ 3.621621] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220fe6d hci version 0x110 quirks 0x0000002001010010 [ 3.631059] xhci-hcd xhci-hcd.1.auto: irq 226, io mem 0x38200000 [ 3.637197] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 3.642698] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2 [ 3.650365] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed [ 3.657695] hub 1-0:1.0: USB hub found [ 3.661473] hub 1-0:1.0: 1 port detected [ 3.665669] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 3.674445] hub 2-0:1.0: USB hub found [ 3.678220] hub 2-0:1.0: 1 port detected [ 3.683428] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 7 mkt segment 2 supported-hw 0x80 0x4 [ 3.693184] Hot alarm is canceled. GPU3D clock will return to 64/64 [ 3.702683] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO [ 3.703346] mxc-mipi-csi2-sam 32e40000.csi: supply mipi-phy not found, using dummy regulator [ 3.716645] : mipi_csis_imx8mp_phy_reset, No remote pad found! [ 3.722602] mxc-mipi-csi2-sam 32e40000.csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 500000000 [ 3.739353] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA [ 3.752018] isi-m2m 32e00000.isi:m2m_device: Register m2m success for ISI.0 [ 3.759172] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 3.768303] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 3.787598] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [ 3.795171] ALSA device list: [ 3.796227] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db [ 3.799186] No soundcards found. [ 3.819630] EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Quota mode: none. [ 3.828212] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 3.834944] devtmpfs: mounted
查看全文
  Introduction   Prior to 6.1.22_2.0.0 BSP release, Bluetooth interface are based on the tty line discipline framework, so we need to use hciattach tool to enable it in the user space. From 6.1.22_2.0.0 BSP, the nxp bluetooth driver no longer needs the help of the userspace hciattach tool, and the tty port bound by bluetooth also won't be exported to the user space, so you cannot find the corresponding tty device anymore. So, you won't see the (/dev/ttymxcX), for the Bluetooth interface. All jobs has been done in the new NXP Bluetooth driver. New Method   The new NXP Bluetooth UART Driver is based on a server driver for the NXP BT serial protocol, which can enable the built-in Bluetooth device inside an NXP BT chip. This driver has a Power Save feature that will put the chip into a sleep state whenever there is no activity for 2000ms and will be woken up when any activity is to be initiated over UART.  Device Tree support The new BT framework requires adding a "bluetooth" sub node with a device compatibility string to the attached UART node in the dts file &uart1 { bluetooth { compatibility = "nxp,88w8987-bt"; fw-init-baudrate = <3000000>; #Optional. Default is considered 115200 if this parameter not defined. }; };   Note: The parameter ‘compatibility = “nxp,88w8987-bt”’ will use for 88W8987, IW416, 88Q9098, IW612 chipsets and need to change for 88W8997 with parameter ‘compatibility = “nxp,88w8997-bt”’.   Note: ’fw-init-baudrate’ parameter depends on the module vendor. The Murata and Azuere wifi modules support in BSP release uses the default value -- 115200. We strongly recommend looking at the module vendor-specific baud rate parameter. Note: For the old 88Q9098 Murata 1XL module that uses the 3Mbps by default, please add the fw-init-baudrate = <3000000> property in dts files to make it work. Enable Guide   Use wifi interface to load combo (wifi & bt) firmware and enable BT Need to load wifi driver first, then load the BT driver, otherwise, BT driver suspend/resume test will fail. This is a HW limitation, since NXP wifi and BT module use the same power control pin(W_DISABLE1#), if we don't load the wifi driver, SDIO bus will power down the wifi chip during suspend resume, which may cause the BT chip also been powered down and cannot work after resume back. So we need to load the wifi driver to make sure SDIO bus won't power down the BT chip to make sure BT functions can work during suspend resume. modprobe moal mod_para=nxp/wifi_mod_para.conf modprobe btnxpuart or insmod mlan.ko insmod moal.ko mod_para=nxp/wifi_mod_para.conf insmod btnxpuart btnxpuart.png   Unload UART Driver modprobe moal Make sure run hciconfig hci0 up or hciconfig hci0 reset or bluetootctl power on before unload btnxpuart driver. If we don't open hci0 interface, the driver cannot send change to 115200 baud rate command to BT chip, which causes the host and BT chip baud rate mismatch, the host still uses 115200bps talk to the BT chip which now use 3Mbps, it cannot work anymore. So we need to make sure open the hci0 interface before unload btnxpuart driver.   mod_para=nxp/wifi_mod_para.conf modprobe btnxpuart sleep 3 hciconfig hci0 up #Note: Need to up hci interface before unload the BT module hcitool -i hci0 cmd 3F 23 02 00 00 modprobe -r btnxpuart modprobe -r moal sleep 3​ For better reference: Please find the I.MX 8MQ Linux getting started user guide, UM11483, Chapter "7.1 Bring-up using NXP Bluetooth UART driver"  Bluetooth Deep Sleep Feature App Note AN13920, Chapter 6 Load NXP UART driver module NOTE: Please do not run the power save feature for Murata IW612 2EL Module Regards, Mario
查看全文
In the i.MX8MP support 3 SDIO interface, and in the reference board i.MX 8M Plus LPDDR4 EVK design default use the eMMC connect to the USDHC3 to boot up from emmc,use the SD card connect to the USDHC2 port. When the U-Boot starts, it will detect the starting slot and automatically set mmcdev and mmcroot, for the USDHC3 in the default Linux set is mmc dev 2. But some customer need to change to the mmc dev 0, make the mmc0 work, see the following introduction.   1 For the EMMC         MMC (multiMedia card) is a communication protocol that supports two modes, SPI and MMC. EMMC is a chip that supports MMC protocol. Both eMMC and SD card package the flash controller and NAND Flash together, but their interfaces are different. eMMC is generally BGA packaged and soldered on PCB. b45499_0-1664554199176.png   EMMC includes 11 signals, namely CLK, CMD, DATA0-7 and Data Strobe. The specific signals are as follows: CLK: It is used to output clock signal from the host side, synchronize data transmission and drive device operation. Each cycle can be transmitted on the rising or falling edge, or both CMD: The signal is mainly used by the host to send a command to the eMMC and the eMMC to send a response to the host. DAT0-7: DAT0-7 signal is mainly used for data transmission between Host and eMMC. After the eMMC is powered on or soft reset, only DAT0 can transmit data. After initialization, DAT0-3 or DAT0-7 can be configured for data transmission, that is, the data bus can be configured as 4 bits or 8 bits. Data Strobe: The clock signal is sent to the host by eMMC with the same frequency as the CLK signal. It is used for synchronization of data reception at the host side. The Data Strobe signal can only be configured and enabled in the HS400 mode. After being enabled, the stability of data transmission can be improved and the bus tuning process can be omitted. 2 For the EMMC design on the i.MX8MP LPDDR4 EVK 2.1 The i.MX8MP The i.MX8MP there is 3 SDIO interface,and the i.MX8MP has 3 USDHC ports:USDHC1, USDHC2 and USDHC3. b45499_1-1664554199192.png   At i MX8MP supports SD/MMC/eSD/eMMC/SDXC, and starts and boots using the USDHC port based on setting of the BOOT_MODE[3:0] pins. b45499_2-1664554199198.png   b45499_3-1664554199200.png   b45499_4-1664554199215.png   In the reference design, eMMC is connected to USDHC3, and SD card is connected to USDHC2. USDHC3 is used as the eMMC boot device by default on the development board. We can see the detailed definitions of the three USDHC interfaces in the reference manual. Among them, USDHC1 and USDHC3 are 8 bits and support 8-bit data, while USDHC2 only supports 4-bit data. b45499_5-1664554199245.png   2.2 Hardware and software design b45499_6-1664554199281.png   The hardware design is as shown above. The eMMC is connected to the SD3 interface, and the software is configured in this way by default. 2.3 The port number of the default BSP In the i.MX 8M Plus LPDDR4 EVK development board design, the eMMC is connected to the USDHC3 as the default boot device When the U-Boot starts, it will detect the starting slot, and automatically set mmcdev and mmcroot. For USDHC3, the default is mmc dev 2. b45499_7-1664554199283.png   The device structure of SD/MMC cards is similar. MMC should be the predecessor of SD, but the design of MMC at that time was half that of SD. Therefore, the SD/MMC driver is universal, and the device node of Linux continues the name of MMC.   Meaning of blk: blk is a block device, and the number after ⾯ is the serial number of the device   Meaning of p: p indicates partition, and p1 is the first partition   We can see the correspondence between the USDHC interface and the mmc under Linux. The kernel MMC module now uses a fixed mmcblk index for the uSDHC slot. The default BSP is "mmc2=&usdhc3":   In the design of the MX 8M Plus LPDDR4 EVK development board, by default, the eMMC is connected to the USDHC3, SD3 is used, and mmcblk2 is used in the SD3 slot. When setting the kernel parameters in the u-boot, you can see that: ### select mmc dev 2 (USDHC3) on the i.MX 8M Mini EVK, i.MX 8M Nano EVK, and i.MX 8M Plus EVK: U-Boot > mmc dev 2 0 For the emmc the related port is :mmcblk2 By default, the flash target is MMC: 2 after the Demo images burning of the development board is started. b45499_8-1664554199308.png   3 mmc0 work as emmc device and boot up We need to modify the device, u-boot, kernel related part for the mmc0 work on the android BSP, 3.1 Software modify 2.2.1 u-boot: Dts section root/arch/arm/dts/imx8mp-evk.dts: memory@40000000 {                  device_type = "memory";                  reg = <0x0 0x40000000 0 0xc0000000>,                        <0x1 0x00000000 0 0xc0000000>;         }; aliases { /* SD/MMC: eMMC/SD slot numbering fix */        mmc0 = &usdhc3; /*Modify the usdhc3 and mmc0, default is mmc2*/        mmc1 = &usdhc2; /* usdhc2 and mmc0 do not change*/        mmc2 = &usdhc1; /*Modify the usdhc1 to mmc2, make the usdhc1 work*/         }; reg_can1_stby: regulator-can1-stby {…..} Board secton: root/board/freescale/imx8mp_evk/imx8mp_evk.c int board_init(void) {         struct arm_smccc_res res; } int board_mmc_get_env_dev(int devno) {        if(devno == 0)         return devno + 2;           else if (devno == 2)         return devno - 2;           else         return devno; }   int mmc_map_to_kernel_blk(int devno) {         return devno; } int board_late_init(void) {         board_late_mmc_env_init(); } SPL: root/common/spl/spl_mmc.c int spl_mmc_load_image(struct spl_image_info *spl_image,                         struct spl_boot_device *bootdev) {…..} Default settings: b45499_9-1664554199311.png     2.2.2 kernel section: In the kernel section need to change all the related mmcblk2 to mmcblk0.                   2.2.3 device section modify: Change all the related mmcblk2 to mmcblk0. Change the uuu_imx_android_flash.bat /android_build/device/nxp/common/tools/fastboot_imx_flashall.bat if not [%soc_name:imx8mp=%] == [%soc_name%] (  set vid=0x1fc9& set pid=00x0146& set chip=MX8MP  set uboot_env_start=0x2000& set uboot_env_len=0x8  - set emmc_num=2& set sd_num=1 + set emmc_num=0& set sd_num=1  set board=evk  goto :device_info_end   All the modify see the Patch in the attachment.
查看全文
In some cases, such as mass production or preparing a demo. We need u-boot environment stored in demo sdcard mirror image.  Here is a way: HW:  i.MX8MP evk SW:  LF_v5.15.52-2.1.0_images_IMX8MPEVK.zip The idea is to use fw_setenv to set the sdcard mirror as the operation on a real emmc/sdcard. Add test=ABCD in u-boot-initial-env for test purpose. And use fw_printenv to check and use hexdump to double confirm it. The uboot env is already written into sdcard mirror(imx-image-multimedia-imx8mpevk.wic). All those operations are on the host x86/x64 PC. ./fw_setenv -c fw_env.config -f u-boot-initial-env Environment WRONG, copy 0 Cannot read environment, using default ./fw_printenv -c fw_env.config Environment OK, copy 0 jh_root_dtb=imx8mp-evk-root.dtb loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script}; mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi arch=arm baudrate=115200 ...... ...... ...... splashimage=0x50000000 test=ABCD usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi vendor=freescale hexdump -s 0x400000 -n 2000 -C imx-image-multimedia-imx8mpevk.wic 00400000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................| hexdump -s 0x400000 -n 10000 -C imx-image-multimedia-imx8mpevk.wic 00400000 5f a4 9b 97 20 6a 68 5f 72 6f 6f 74 5f 64 74 62 |_... jh_root_dtb| 00400010 3d 69 6d 78 38 6d 70 2d 65 76 6b 2d 72 6f 6f 74 |=imx8mp-evk-root| 00400020 2e 64 74 62 00 20 6c 6f 61 64 62 6f 6f 74 73 63 |.dtb. loadbootsc| 00400030 72 69 70 74 3d 66 61 74 6c 6f 61 64 20 6d 6d 63 |ript=fatload mmc| 00400040 20 24 7b 6d 6d 63 64 65 76 7d 3a 24 7b 6d 6d 63 | ${mmcdev}:${mmc| 00400050 70 61 72 74 7d 20 24 7b 6c 6f 61 64 61 64 64 72 |part} ${loadaddr| 00400060 7d 20 24 7b 62 73 70 5f 73 63 72 69 70 74 7d 3b |} ${bsp_script};| 00400070 00 20 6d 6d 63 5f 62 6f 6f 74 3d 69 66 20 6d 6d |. mmc_boot=if mm| ...... ...... ...... 00401390 76 3d 31 00 73 6f 63 3d 69 6d 78 38 6d 00 73 70 |v=1.soc=imx8m.sp| 004013a0 6c 61 73 68 69 6d 61 67 65 3d 30 78 35 30 30 30 |lashimage=0x5000| 004013b0 30 30 30 30 00 74 65 73 74 3d 41 42 43 44 00 75 |0000.test=ABCD.u| 004013c0 73 62 5f 62 6f 6f 74 3d 75 73 62 20 73 74 61 72 |sb_boot=usb star| 004013d0 74 3b 20 69 66 20 75 73 62 20 64 65 76 20 24 7b |t; if usb dev ${| 004013e0 64 65 76 6e 75 6d 7d 3b 20 74 68 65 6e 20 64 65 |devnum}; then de| flash the sdcard mirror into i.MX8MP evk board emmc to check uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mpevk.wic  The first time boot, the enviroment is already there. Untitled.png  How to achieve that: a. fw_setenv/fw_printenv: https://github.com/sbabic/libubootenv.git Note: Please do not use uboot fw_setenv/fw_printenv Compile it on the host x86/x64 PC. It is used on host. b. u-boot-initial-env Under uboot, make u-boot-initial-env Note: Yocto deploys u-boot-initial-env by default c. fw_env.config  imx-image-multimedia-imx8mpevk.wic 0x400000 0x4000 0x400000 0x4000 are from uboot-imx\configs\imx8mp_evk_defconfig CONFIG_ENV_SIZE=0x4000 CONFIG_ENV_OFFSET=0x400000 Now, you can run  ./fw_setenv -c fw_env.config -f u-boot-initial-env
查看全文
Introduction ARM SoC+FPGA/CPLD is widely used in some application like industry control and data acquisition system, there were many customers adopted i.MX6 EIM (a memory parallel interface) to access FPGA/CPLD, and archived good data throughput, but EIM is removed from i.MX8M and i.MX9, some customers is asking for such a compatible solution for i.MX8/8M and coming i.MX9 family.  FlexSPI is designed for connecting storage devices like NOR Flash, integrated in most of i.MXRT/i.MX8/LS products and provides flexible configuration for 4-wire/8wire working mode, this article provides a low-cost and efficiency demo to show how  to support CPLD/FPGA  via FlexSPI, as a replacement of EIM for EP i.MX8/9/LS products. key features Implement a  new kernel driver for FlexSPI to support read/write access to FPGA/CPLD. Support two type connections: Support 4-wire(QSPI) and 8-wire(HypeBUS, OctalSPI) Deliverables A new kernel driver for FlexSPI to support read/write access to FPGA/CPLD by AHB command A kernel patch to disable the QSPI Flash in kernel A test program shows how to do read/write performance test. Hardware Hardware Prepare: i.MX8MM-LPDDR4-EVK Lattice LFE5U EVK fuzhenlin_0-1690194268371.png Figure1 4-wire SPI HW Block diagram fuzhenlin_1-1690194328119.png Figure2 8-wire OctalSPI   Hardware Rework on i.MX8MM-EVK     1 Need to remove the SPI-Flash(U5, MT25QU256ABA) on the i.MX8MM-EVK board, and wire below signals: QSPI_DATA0 QSPI_DATA1 QSPI_DATA2 QSPI_DATA3 QSPI_SCLK QSPI_nSS0 VDD_1V8 GND fuzhenlin_2-1690195893230.jpeg Figure3 QPSI signals for FPGA/CPLD fuzhenlin_4-1690196152847.png Figure4 Hardware rework on i.MX8MM-EVK board Note that, i.MX8MM-EVK QSPI power rails is 1.8v, so be careful that the FPGA/CPLD side IO should be 1.8V. Software BSP version 1 Linux BSP version: L5.10.52 Software Change  Apply 0001-FlexSPI-FPGA-need-to-disable-flexspi-for-fpga-usage.patch in Linux kernel and generate the new dtb extract the flexspi-fpga driver compile the flexspi-fpga driver with the kernel$ $make -C $(YOUR_KDIR) M=$(FlexSPI_FPGAW_DIVER_DIR) modules ARCH=arm64 CROSS_COMPILE=$(CROSS_COMPILE) Deployment  upload new generated i.mx8mm-evk.dtb to the target board(the 1st partition) upload the flex-spi driver and fpga/cpld test program to the target board   Test Test1: Set the flexspi working at 40Mhz   $insmod imx_flexspi_fpga.ko pre_div=2 post_div=5 Read/write FPGA/CPLD test .$/flexspi_fpga_test -p 0x08000000 -s 768 Test2: Set the FlexSPI working at 100MHz   $ insmod imx_flexspi_fpga.ko pre_div=1 post_div=4 Read/write FPGA/CPLD test $./flexspi_fpga_test -p 0x08000000 -s 768   Limitation FPGA and Flash devices can’t work at the same time due to just one FlexSPI controller. Due to the IO assignment conflict in i.MX8M EVK design, this demo just tested 4-wire(QSPI) mode at 50MHz and got data throughput as expected. Disclaimer: − “Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.”
查看全文
Environment BSP: L6.1.22_2.0.0​ Platform: i.MX93 Links:  https://github.com/NXP/swupdate-scripts https://github.com/nxp-imx-support/meta-swupdate-imx   The AN13872 provides us the swupdate yocto layer, swupdate-scripts and test steps, but there is still much to add. The purpose of this knowledge base is to provide customized advice. 1.How to port meta-swupdate-imx to any yocto version you want? As meta-swupdate-imx only provide kirkstone version, we can upgrade or degrade it based on this version. We will take L6.1.22_2.0.0​ porting steps as an example. 1.1 Download Yocto layer  cd imx-yocto-bsp/sources git clone https://github.com/sbabic/meta-swupdate.git -b mickledore git clone https://github.com/nxp-imx-support/meta-swupdate-imx.git 1.2 Modify  Yocto layer  imx-yocto-bsp/sources/meta-swupdate-imx/conf/layer.conf Zhiming_Liu_0-1691565490091.png   You can find swupdate version in imx-yocto-bsp/sources/meta-swupdate/recipes-support/swupdate/ Zhiming_Liu_1-1691565520029.png 1.3 Handle patches in meta-swupdate-imx/recipes-bsp/u-boot/files/ About patchs in sources/meta-swupdate-imx/recipes-bsp/u-boot/files/ and imx-yocto-bsp/sources/meta-swupdate-imx/recipes-support/swupdate/files/, you need use devtool to unpack uboot and swupdate into workspace and add changes manunally for development. CONFIG_ENV_OFFSET_REDUND=CONFIG_ENV_OFFSET+CONFIG_ENV_SIZE Zhiming_Liu_2-1691565664319.png   sources/meta-swupdate-imx/recipes-bsp/u-boot/u-boot-imx_%.bbappend Zhiming_Liu_3-1691565694894.png 2.How to flash base image? Use uuu or dd command, just like common imx-image-xxx 3.swupdate-scripts porting suggestions 3.1 Partition table You can modify partition table refer the size of images. For different soc, the first offset is different. If you are porting i.MX8MP based on iMX8MM, the offset should be 32K. Zhiming_Liu_4-1691565894626.png   3.2 Some errors 3.2.1 This error indicates that you need enlarge size of rootfs. e2fsck 1.45.5 (07-Jan-2020) The filesystem size (according to the superblock) is 887599 blocks The physical size of the device is 768000 blocks Either the superblock or the partition table is likely to be corrupt! Abort<y>?    3.2.2 You need upgrade e2fsck verison. e2fsck 1.46.5 (30-Dec-2021) /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4 has unsupported feature(s): FEATURE_C12 e2fsck: Get a newer version of e2fsck! /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4: ********** WARNING: Filesystem still has errors ********** resize2fs 1.46.5 (30-Dec-2021) resize2fs: Filesystem has unsupported feature(s) (/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_ass  solution: wget https://mirrors.edge.kernel.org/pub/linux/kernel/people/tytso/e2fsprogs/v1.47.0/e2fsprogs-1.47.0.tar.xz tar -xf e2fsprogs-1.47.0.tar.xz cd e2fsprogs-1.47.0/ ./configure make -j16 sudo make install   3.2.3 mtools /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 58: mdir: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 68: mdir: command not found solution: sudo apt-get install mtools
查看全文
We are pleased to announce that Config Tools for i.MX v14.0 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) The product is based on Eclipse 2022-12 Open JDK 17 is updated. Batch processing on command line is supported. Support for SDK 2.14 in Project cloner and Detect toolchain project is added. Quick fix for errors allows setting the "Called by the default initialization function" flag when it would fix an error. Search functionality to Code Preview is added. TEE Export TEE registers via wizard or command line is available. Boot ROM hiding feature is supported. Tier mode for TRDC is supported. Domain ambivalence for RDC masters is added. Master-specific memory alias Validation for A28 bit of MPU region address is added. Memory map filters are aligned with Arm terminology. Status bar is united with other tools. Pins Labels defined for Expansion header pins can be set as identifiers of the routed pin. Expansion headers can be locked for editing. Expansion headers and boards are added to the HTML and CSV reports. Pins filtering is added into the expansion header pin routing dialogs. Columns from Routing Details can be added to the External User Signals view. New External User Signals can be created for all routed pins that are missing in the signals table. Clocks Support for the same frequencies settings from different source for internal clocks is added.
查看全文
Issue description: ZQ calibration issue with LPDDR2 memory with two chip selects    Micron has verified it on my customer's board with i.MX6Q. (ECT-SYT-1163 for FIC.pdf) The patch is made based on lp 5.1, see attachment.
查看全文
On customer design, they may need to fine tune LVDS driver strength for different case, for example, PCB impedance does not match, or the value of terminal resistor in panel side is lower or bigger. In IMX8MPRM.pdf, it has reg for this feature: Lambert_0-1690979359195.png   Lambert_1-1690979359199.png       LVDS is constant current source, when voltage on terminal or panel side is lower than spec, you need to increase output current to get higher voltage to meet spec. otherwise ,you need to reduce it There is no detail description for these bits, pls refer to below: CC_ADJ = 000b => 3.5mA as default CC_ADJ = 001b => 3.5mA + 0.215mA x 1 CC_ADJ = 010b => 3.5mA + 0.215mA x 2 CC_ADJ = 011b => 3.5mA + 0.215mA x 4 CC_ADJ = 100b => 3.5mA - 0.215mA x 4 CC_ADJ = 101b => 3.5mA - 0.215mA x 3 CC_ADJ = 110b => 3.5mA - 0.215mA x 2 CC_ADJ = 111b => 3.5mA - 0.215mA x 1   Thanks, Lambert
查看全文
  Solution weiping_liu_0-1690964187350.png     weiping_liu_1-1690262928368.png weiping_liu_2-1690262966158.png       
查看全文
Hello everyone, this document will share an step by step guide of the configuration needed in a Linux PC to compile the SDK examples we provide, as well as how to download them in an easy way. Requirements: I.MX 8M Mini EVK SDK package (for i.MX8MM) UUU tool First step would be to get the SDK package, this include documentation and code, which is available at the MCUXpresso builder webpage: https://mcuxpresso.nxp.com/en/welcome Click on the select a development board and select the package for your development kit or the i.MX MPU MCUXpresso builder.png   Select SDK.png This guide is focused on Linux build so will select GCC package and Linux host PC as the environment. Select Linux.png Select GCC.png Click on build and wait for the SDK package to be ready for download. Note1: Click on select all if the whole middleware package is desired Note2: it is possible to select each middleware that are desired. Select middleware & download.png On new window select download SDK download sdk.png Select on new pop-up window download both SDK and documentation SDK archive and docs.png Read and accept EULA so the download start accept EULA.png Decompress the package using the following command: $ tar -xvzf ~/SDK_2_13_0_EVK-MIMX8MM.tar.gz -C ~/SDK_2_13_0_EVK-MIMX8MM Next will be to download the GCC from the ARM webpage, gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 https://developer.arm.com/downloads/-/gnu-rm Note that the GCC version used is based on the minimum version required, since this was tested and supported, this could be found within the SDK documentation (~/SDK_2_13_0_EVK-MIMX8MM/docs/MCUXpresso SDK Release Notes for EVK-MIMX8MM) GCC version.png Once downloaded we can decompress and configure the environment: $ tar -xf gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ sudo apt-get install cmake  Check the version >= 3.0.x $ cmake --version Once this is done we enter the path of the example of our choice and compile using the script, as necessary using debug, release or all. $ cd ~/SDK_2_13_0_EVK-MIMX8MM/boards/evkmimx8mm/demo_apps/hello_world/armgcc $./build_release.sh The binary (elf and bin) will be found inside the folder according to whether we use debug or release script. For this example we used release script: $ cd release Once builded we can move/download the binaries from the Linux host PC to the board by using the UUU tool with the command fat_write #### we put the board in fastboot mode by entering the command in the uboot terminal fastboot 0 #### From the Linux terminal introduce the UUU command to  download to the FAT partition of the eMMC of the baord: ## For rproc it is needed the .elf binary ## $ uuu -v -b fat_write hello_world.elf mmc 0:1 hello_world.elf ## For bootaux it is needed the .bin binary ## $  uuu -v -b fat_write hello_world.bin mmc 0:1 hello_world.bin Once with the binaries in the FAT partition of the SD/eMMC of our board we can make the necessary modifications (device tree/bootargs) to test the Cortex-M examples. For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
查看全文
  Platform: i.MX8MP EVK , L6.1.22-2.0.0 LT9211 is a chip that can realize the conversion of MIPI DSI signals to LVDS signals. This patch is based on this mainline driver:https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/gpu/drm/bridge/lontium-lt9211.c Keypoint Move lt9211_host_attach function to lt9211_attach to skip bridge attach error.  
查看全文
1.Compile full aosp or only kernel Build full aosp: source build/envsetup.sh lunch evk_8mm-userdebug ./imx-make.sh -j8  Only build kernel: ./imx-make.sh kernel -j8 2.Build GKI locally Download GKI outside of android_build. mkdir gki && cd gki (Make sure folder gki is not inside of ${MY_ANDROID}) repo init -u https://android.googlesource.com/kernel/manifest -b commonandroid13-5.15 repo sync Build GKI locally. BUILD_CONFIG=common/build.config.gki.aarch64 build/build.sh 3. Export symbols After building GKI locally, you can copy linux-imx from /vendor/nxp-opensource/kernel_imx into common. cd common rm -r ./* cp ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/* ./ ln -s ${MY_ANDROID}/vendor/nxp-opensource/verisilicon_sw_isp_vvcam verisilicon_sw_isp_vvcam ln -s ${MY_ANDROID}/vendor/nxp-opensource/nxp-mwifiex nxp-mwifiex  Build GKI about i.MX: BUILD_FOR_GKI=yes BUILD_CONFIG=common/build.config.imx EXT_MODULES_MAKEFILE="verisilicon_sw_isp_vvcam/vvcam/v4l2/Kbuild" EXT_MODULES="nxp-mwifiex/mxm_wifiex/wlan_src" build/build_abi.sh --update-symbol-list -j8 Then the  common/android/abi_gki_aarch64_imx will be generated. cd gki cp common/android/abi_gki_aarch64_imx /tmp/abi_gki_aarch64_imx   Update GKI kernel rm -r common/* # delete imx kernel repo sync # recover aosp kernel cp /tmp/abi_gki_aarch64_imx android/abi_gki_aarch64_imx cd .. BUILD_CONFIG=common/build.config.gki.aarch64 build/build_abi.sh LTO=thin --update -j8  Then, common/android/abi_gki_aarch64.xml is updated.  
查看全文
  Introduction   Platform: i.MX93 EVK Uboot: origin/lf_v2022.04(lf-6.1.1-1.0.0) The LVDS design and media block control in i.MX93 is very similiar with i.MX8MPlus.This article implements the LVDS driver in uboot. You need apply 0001-Add-fake-adp5585-pwm-driver.patch which implements the adp5585 pwm driver in uboot. This is a fake pwm driver only implement the pwm driver framework. You can't use pwm value to adjust brightness for the moment, but this is enough to enable the backlight. Then please apply 0002-Add-imx93-lvds-and-panel-driver.patch, you will see nxp logo with this panel: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/dy1212w-4856:DY1212W-4856   Porting suggestions   1. Modify panel timing in drivers/video/simple_panel.c /* define your panel timing here and * copy it in simple_panel_get_display_timing */ static const struct display_timing boe_ev121wxm_n10_1850_timing = { .pixelclock.typ = 71143000, .hactive.typ = 1280, .hfront_porch.typ = 32, .hback_porch.typ = 80, .hsync_len.typ = 48, .vactive.typ = 800, .vfront_porch.typ = 6, .vback_porch.typ = 14, .vsync_len.typ = 3, }; static int simple_panel_get_display_timing(struct udevice *dev, struct display_timing *timings) { memcpy(timings, &boe_ev121wxm_n10_1850_timing, sizeof(*timings)); return 0; }   2.Modify VIDEO_PLL The VIDEO_PLL = pixel clock * 7. For default panel, the pixel clock is 71.143MHz and VIDEO_PLL  is 498MHz. static struct imx_fracpll_rate_table imx9_fracpll_tbl[] = { FRAC_PLL_RATE(1000000000U, 1, 166, 4, 2, 3), /* 1000Mhz */ FRAC_PLL_RATE(933000000U, 1, 155, 4, 1, 2), /* 933Mhz */ FRAC_PLL_RATE(700000000U, 1, 145, 5, 5, 6), /* 700Mhz */ FRAC_PLL_RATE(498000000U, 1, 166, 8, 0, 1),/* rate, rdiv, mfi, odiv, mfn, mfd */ FRAC_PLL_RATE(484000000U, 1, 121, 6, 0, 1), FRAC_PLL_RATE(445333333U, 1, 167, 9, 0, 1), FRAC_PLL_RATE(466000000U, 1, 155, 8, 1, 3), /* 466Mhz */ FRAC_PLL_RATE(400000000U, 1, 200, 12, 0, 1), /* 400Mhz */ FRAC_PLL_RATE(300000000U, 1, 150, 12, 0, 1), }; 3. Modify lcdif node in dts <498000000>, <71142857>, <400000000>, <133333333>; <VIDEO PLL>,<PIX CLK>, <MEDIA_AXI>,<MEDIA_APB> &lcdif { status = "okay"; - assigned-clock-rates = <484000000>, <121000000>, <400000000>, <133333333>; + assigned-clock-rates = <498000000>, <71142857>, <400000000>, <133333333>; };  
查看全文
The following setup is done on i.MX 93. For i.MX 8M the same steps are valid and can be followed. Prerequisites Prepare the Yocto environment. $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-langdale -m imx-6.1.1-1.0.0.xml $ repo sync  Set the build environment. $ DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk source imx-setup-release.sh -b build-imx93 Add the 32-bit support to the image For i.MX 8M / i.MX 93, building 32-bit applications on 64-bit OS can be supported using the multilib configuration. Multilib offers the ability to build libraries with different target optimizations or architecture formats and combine these together into one system image.  Building a 32-bit application requires the following statements in conf/local.conf. The configuration specifies a 64-bit machine as the main machine type and adds multilib:lib32, where those libraries are compiled with the armv7athf-neon tune, and then includes to the image the lib32 packages. # Define multilib target require conf/multilib.conf MULTILIBS = "multilib:lib32" DEFAULTTUNE:virtclass-multilib-lib32 = "armv7athf-neon" # Add the multilib packages to the image IMAGE_INSTALL:append = " lib32-glibc lib32-libgcc lib32-libstdc++" Multilib is not supported with the debian package management. It requires the RPM system. Check and comment out the two package management lines in conf/local.conf to go to the default RPM. PACKAGE_CLASSES = "package_deb" EXTRA_IMAGE_FEATURES += "package-management" Build the image. bitbake imx-image-core Cross-compile a 32-bit application This section shows how to use the Linux SDK to cross-compile a simple C application into a 32-bit binary. Generate the SDK, which includes the tools, toolchain, and small rootfs to compile against to put on host machine: DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk bitbake core-image-minimal -c populate_sdk Set the SDK environment with the following command before building: source /opt/fsl-imx-wayland/6.1-langdale/environment-setup-armv7at2hf-neon-pokymllib32-linux-gnueabi Implement a simple hello world application: cat hello_world_32.c #include <stdio.h> int main() { printf("Hello, World!"); return 0; } $CC hello_world_32.c -o hello_world_32 Check the file's type: $ file hello_world_32 hello_world_32: ELF 32-bit LSB shared object, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, BuildID[sha1]=0a5042a0309858e0b10b12175a155cfbfb4c6a80, for GNU/Linux 3.2.0, with debug_info, not stripped Copy the binary to the Linux rootfs. Run the application on i.MX 93 Boot the board and run the application: root@imx93-11x11-lpddr4x-evk:~# ./hello_world_32 Hello, World!  
查看全文