The purpose of this document is to specify the maximum LPDDR3, LPDDR4, & LPDDR4X densities that are supported by i.MX 8ULP processor along with a running list of tested memories to aid project feasibility assessment capabilities of customers that are evaluating the SoCs for usage in their products.
It is strongly recommended to consult with NXP and the memory vendor the final choice of the memory part number to ensure that the device meets all the compatibility, availability, longevity and pricing requirements.
In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs.
For any questions related to specific DRAM part numbers please contact the respective DRAM vendor. For any questions regarding the i.MX SoC please contact your support representative or enter a support ticket.
LPDDR4/LPDDR4X Maximum Support Density
Please note that the SoC limits the addressable DDR memory map range to 2GB.
SoC
Max data bus width
Maximum density
Assumed memory organization
Notes
i.MX 8ULP
32-bit
16Gb/2GB
single-rank, dual-channel device with 16-row addresses (R0-R15)
1, 2, 6,11
LPDDR4 - list of validated memories
The validation process is an ongoing effort - regular updates of the table are expected.
SoC
Density
Memory Vendor
Validated Memory Part#
Notes
i.MX 8ULP
16Gb/2GB
Micron
MT53D512M32D2DS-053 WT:D
10
16Gb/2GB
Micron
MT53E512M32D1ZW-046 WT:B
8
64Gb/8GB
Micron
MT53E2G32D4DE-046 WT:A
3, 4, 8
32Gb/4GB
Micron
MT53E1G32D2FW-046 AUT:B
3, 4, 10
16Gb/2GB
Nanya
NT6AN512T32AV-J2
3, 7, 8
8Gb/1GB
Forsee
FL4C2001G-D9
3, 10
LPDDR4x - list of validated memories
The validation process is an ongoing effort - regular updates of the table are expected.
SoC
Density
Mamory Vendor
Validated Memory Part#
Notes
i.MX 8ULP
16Gb/ 2GB
Nanya
NT6AP512T32AV-J2
3, 7, 8
2Gb/ 256MB
Fidelix
FMF2D32VAC-4CDIR
3
4Gb/ 512MB
Winbond
W66CQ2NQUAFJ
3, 8
8Gb/1GB
Alliance
Memory
AS4C256M32MD4V-062BAN
3, 8
32Gb/4GB
Micron
MT53E1G32D2FW-046 AUT:B (Z42M)
3, 4, 10
16Gb/ 2GB
Micron
MT53D512M32D2DS-053 WT:D
10
16Gb/ 2GB
Micron
MT53E512M32D1ZW-046 WT:B
9
LPDDR3 Maximum Support Density
Please note that the SoC limits the addressable DDR memory map range to 2GB.
SoC
Max data bus width
Maximum density
Assumed memory organization
Notes
i.MX 8ULP
32-bit
16Gb/2GB
Single Channel, Dual Chip Select
5,11
LPDDR3 - list of validated memories
The validation process is an ongoing effort - regular updates of the table are expected.
SoC
Density
Memory Vendor
Validated Memory Part#
Notes
i.MX 8ULP
16Gb/2GB
Micron
MT52L512M32D2PF-107 WT:B
8
Note 1:
The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC and on the memory device used on NXP evaluation boards, and on the JEDEC standards JESD209-4/JESD209-4B (LPDDR4/4X). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk.
Note 2:
Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification).
Note 3:
The memory part number did not undergo full JEDEC verification however, it passed all functional testing items.
Note 4:
As the i.MX 8ULP DDR memory map is limited to 2GB, only up to 2GB of the device can be utilized even though the device density exceeds the 2GB range.
Note 5:
The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC and on the memory device used on NXP evaluation boards, and on the JEDEC standards JESD209-3C (LPDDR3). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk.
Note 6:
The SoC supports also LPDDR4/4X devices with 17-row address bits however, given the SoC's memory map constraints (see Note 4), full density of those devices cannot be utilized since the dual channel (x32) 17-row address memory devices have the density of 4GB and higher.
Note 7:
By default, LPDDR4/4X devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity. Please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured.
Note 8:
Part is active. Reviewed Jan 2026
Note 9:
Part is active as MT53E512M32D1ZW-046BWT:B.
Note 10:
Part is obsolete.
Note 11:
i.MX 8ULP does not support Non-Power of 2 Memory densities (e.g. 3,6,12 Gb).
記事全体を表示