i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
An i.MX50 customer encountered such kernel bug recently. Android UI has no response, because the suspend work queue is blocked:     suspend       pm_suspend         enter_state           suspend_prepare / suspend_finish             pm_prepare_console / pm_restore_console               vt_move_to_console                 vt_waitactive                   vt_event_wait                     wait_event_interruptible Confimed the same bug can also happen on imx6SL which is running linux 3.0.35. e.g. by echo standby/mem > /sys/power/state It takes over thousand suspend/resume cycles to reproduce the problem. The bug fix has been merged since linux 3.6: commit a7b12929be6cc55eab2dac3330fa9f5984e12dda
記事全体を表示
The attached patch enables HDMI overscan for Android JB, and tested by MX6Q SabreSD with Android_4.2.2_1.0.0-ga. The bootargs includes "video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off".
記事全体を表示
Tested on imx28 EVK Rev. D. When plug-in or plug-out cable on eth0 port, eth1 port (and vice versa) will also be reset and the communication will be interrupted. Reason: Both Ethernet PHYs on EVK board share the same GPIO as their reset pin, in software the function name is mx28evk_enet_gpio_init. So any call to pdata->init() in fec.c will reset both PHY at the same time. In order to avoid such problem, you have to use 2 individual GPIO for the PHY reset.
記事全体を表示
Add the above line to conf/local.conf file: PREFERRED_PROVIDER_virtual/kernel = "linux-fslc" Check this page to see what the mainline Linux kernel supports for a particular Freescale board.
記事全体を表示
You can but building times will take much longer (approximately 2 times longer for the core-image-minimal) compared to a build done on a native machine. In case you can not do the build on a native machine, make sure your virtual has enough hard-disk room (at least 50GB). For example, these are the build folders sizes after baking core-image-minimal: build$ du -h --max-depth=1 1.3G    ./sstate-cache 3.2M    ./cache 12K    ./.hob 32K    ./conf 22G    ./tmp 23G    . The tmp folder is by far the largest (containing building statistics, source code, deployed images, etc.) build/tmp$ tree -L 2 -d . ├── buildstats │   ├── cogl-imx6qsabresd │   ├── fsl-image-gui-imx6qsabresd │   ├── fsl-image-gui-sdk-imx6qsabresd │   ├── mesa-dri-imx6qsabresd │   ├── mesa-imx6qsabresd │   └── pseudo-native-imx6qsabresd ├── cache │   └── default-eglibc ├── deploy │   ├── images │   ├── licenses │   └── rpm ├── log │   ├── cleanlogs │   └── cooker ├── pkgdata │   ├── all-poky-linux │   ├── all-poky-linux-gnueabi │   ├── armv7a-vfp-neon-poky-linux-gnueabi │   ├── imx6qsabresd-poky-linux │   └── imx6qsabresd-poky-linux-gnueabi ├── sstate-control ├── stamps │   ├── all-poky-linux │   ├── all-poky-linux-gnueabi │   ├── armv7a-vfp-neon-poky-linux-gnueabi │   ├── imx6qsabresd-poky-linux │   ├── imx6qsabresd-poky-linux-gnueabi │   ├── work-shared │   └── x86_64-linux ├── sysroots │   ├── imx6qsabresd │   ├── imx6qsabresd-tcbootstrap │   └── x86_64-linux ├── work │   ├── all-poky-linux │   ├── all-poky-linux-gnueabi │   ├── armv7a-vfp-neon-poky-linux-gnueabi │   ├── imx6qsabresd-poky-linux │   ├── imx6qsabresd-poky-linux-gnueabi │   └── x86_64-linux └── work-shared     └── gcc-4.7.2-r13
記事全体を表示
There are two ways: 1. BitBake. Append the package into the IMAGE_INSTALL variable. But In case you want the package in every image,  add a line to your conf/local.conf file IMAGE_INSTALL_append = " package"           Make sure to include the space BEFORE the package name. You can add other packages, just place spaces in-between. In case you want the package in a particular image, e.g. fsl-image-gui,, add it on meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb IMAGE_INSTALL += " \     ${SOC_IMAGE_INSTALL} \     cpufrequtils \     nano \     packagegroup-fsl-gstreamer \     packagegroup-fsl-tools-testapps \     packagegroup-fsl-tools-benchmark \     packagegroup-qt-in-use-demos \     qt4-plugin-phonon-backend-gstreamer \     qt4-demos \     qt4-examples \     fsl-gui-extrafiles \     package \     " 2. Hob. Due to its graphical nature, adding more packages to a base image is easier than the bitbake way. Run the hob app under the build folder, select your machine and image, then edit the later (click on the Edit image button) In case the package is not available, you need to create it. As a starting point take a look at this example. In case you consider is good enough to be present on the mainstream repos, send the patch to the meta-freescale mailing list.
記事全体を表示
There are two optionsou 1. Remove all source code after building: You can indicate bitbake to remove all source code after a build adding this line INHERIT += "rm_work" our to your conf/local.conf file. Of course, when baking another image, ALL source code has to be fetched again and it can take a lot of time, specially on machines with low connections to the Internet. The smallest image you can build is core-image-minimal, containing the minimal set of packages to board a particular machine. The largest is fsl-image-gui (in fact, there is one bigger 'fsl-image-gui-sdk' used for developing purposes inside the target). Between these two, there are a lot of images you can choose. You can even create your own image using hob. In case you do not want to build anything, there are some pre-built images on this site, just download the sdcard file and flash it to an SD card. 2. Select only those  IMAGE_FSTYPES you need. There is a variable named IMAGE_FSTYPES  which indicates the output formats you want for the resulting root file system images, by default is has this value: IMAGE_FSTYPES ?= "tar.bz2 ext3 sdcard" and it is located on /sources/meta-fsl-arm/conf/machine/include/imx-base.inc machine's header file. If you want to change it, place this variable on the build/conf/local.conf file. In case you have NFS mounting, remove the 'sdcard' (and either 'ext3' or 'tar.bz2') string, resulting in IMAGE_FSTYPES = "tar.bz2"
記事全体を表示
1. Follow all instructions from Freescale's github repo except the last bitbake command 2. Run hob under the build folder build$ hob & 3. On the GUI, select machine and image, then build 4. In case you need to flash an SD Card, hob does not produce an .sdcard image, so as a workaround, close hob and on the same console run build$ bitbake <image>     where image must be the same as the one you choose with hob 5. Flash your SD card build$ sudo dd if=tmp/deploy/images/fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=4M NOTES: In case of building issues, please follow this link In case of booting issues, make sure: 1. board DIP switches are set correctly 2. you have chosen the correct machine before baking If issues persist, report it to the community
記事全体を表示
Downloading and building the IPU examples IPU examples - v0.1 are available at https://github.com/rogeriorps/ipu-examples To download, just clone the project: $ git clone https://github.com/rogeriorps/ipu-examples.git Follow the README.md on the project root folder to build and install it. Available demos Alpha Blending Basic Combining Cropping Color Space Conversion Deinterlacing Resizing Rotation i.MX5 basic_ex1 rot_ex1 i.MX6 alpha_ex1 alpha_ex2 crop_ex1 csc_ex1 dint_ex1 res_ex1 rot_ex1 i.MX5 Basic examples basic_ex1: Prints all information from all framebuffers. It uses only the framebuffer device /dev/fb*. Rotation examples rot_ex1: Rotate an image a show on display. This example uses the ipu library instead using directly the /dev/mxc_ipu. i.MX6 Alpha blending examples alpha_ex1: This example shows how to use global alpha blending. It fills layer 1 with white color, an overlay layer with 4 color strips and varies the global alpha blending, showing on display 2 planes at the same time with different transparency rates. alpha_ex2: This example shows how to use local alpha blending. This example uses 3 buffers: 1 - Input buffer: Used as layer 1 (background). 2 - Overlay buffer: Used as layer 2 (foreground). 3 - Alpha buffer: Used as alpha buffer, where each pixel will correspond to the transparency value between input and overlay buffers. When running it will fill input and overlay buffers with solid colors, alpha buffer with 4 different alpha strips and will turn on and off the local alpha blending. Color space conversion examples csc_ex1: This example shows how to use color space conversion. It reads 4 different formats images (RGB565, RGBA32, NV12 and YUYV422) and show them on background framebuffer on a RGB565 format. Crop example crop_ex1: This example shows how to crop an image using "output crop". It fills the input buffer with a solid color and crop the output buffer. The result will be a solid block on the display. De-interlace example dint_ex1: This example shows how to de-interlace a single interlaced frame. The example loads an 320x240 interlaced NV12 image and show on display turning on and off the de-interlace feature. Resize examples res_ex1: This example resizes the image freescale_1024x768.raw (1024x768 RGB565 format) to an 800x480 RGB24 format image, storing into a local file output_file.raw. Rotation examples rot_ex1: This example rotates the image freescale_1024x768.raw (1024x768 RGB565 format) and displays using all rotation modes: 0 - No rotation 1 - Vertical flip 2 - Horizontal flip 3 - 180 degrees 4 - 90 degrees right 5 - 90 degrees right with vertical flip 6 - 90 degrees right with horizontal flip 7 - 90 degrees left Known issues
記事全体を表示
You already know. Your source code is one week old now, so please, update it! $ repo sync What was the changes? Please, read the output and determinate what file was changed. Directory tree This is what I have under fsl-community-bsp directory: $ tree -d -L 2 -A . ├── build_mx53 │   ├── conf │   ├── sstate-cache │   └── tmp ├── build_mx6 │   ├── conf │   ├── sstate-cache │   └── tmp ├── downloads │   └── git2 └── sources     ├── base     ├── meta-fsl-arm     ├── meta-fsl-arm-extra     ├── meta-fsl-demos     ├── meta-openembedded     └── poky Sstate-cache keeps the pre-build packages cache so once one package is built, and it´s not changes, no need to re-build it again. If a team shares the same build environment, the sstate-cache folder can be shared as well. I´m not personally used to configure it, so, please, follow the doc: Yocto Project Reference Manual The downloads folder is shared for any build folder. It holds every package´s source code. For example, the ssh source code (and this source code can be built for any architecture) In addition, you may want to share the download folder with your team (one download folder for the complete team), so please, go to Yocto Project Reference Manual and look for DL_DIR. Build_mx6 tree .../build_mx6$ tree -d -L 2 -A . ├── conf ├── sstate-cache └── tmp     ├── buildstats     ├── cache     ├── deploy     ├── log     ├── pkgdata     ├── sstate-control     ├── stamps     ├── sysroots     ├── work     └── work-shared Inside tmp folder you will find images and build results. Images is placed inside deploy. Build statistics like initial and final time for each package/task are under buildstats The complete log for any 'bitbake' you did is under log. Take a look, for example, on the file  log/cooker/imx6qsabresd/11111111111.log. Please, notice that 111111111 is the PID number, so every time you run bitbake you have a different one. The source code, the patches, and the logs for the last bitbake, for each package is under work. Take a look on the files under tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/ for example, for the kernel. .../build_mx6$ tree -d -L 1 -A tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/ tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/ ├── deploy-linux-imx ├── deploy-rpms ├── git ├── image ├── license-destdir ├── package ├── packages-split ├── pkgdata ├── pseudo ├── sysroot-destdir └── temp Go under temp, and see a lot of log.* and run.*: .../build_mx6$ ls tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/temp/ log.do_bundle_initramfs             log.do_uboot_mkimage                run.do_package_write_rpm.28992      run.perform_packagecopy.16364 log.do_bundle_initramfs.28986       log.do_uboot_mkimage.2325           run.do_patch                        run.populate_packages.16364 log.do_compile                      log.do_unpack                       run.do_patch.2556                   run.read_shlibdeps.16364 log.do_compile.3483                 log.do_unpack.1155                  run.do_populate_lic                 run.read_subpackage_metadata.28992 log.do_compile_kernelmodules        log.task_order                      run.do_populate_lic.10988           run.split_and_strip_files.16364 log.do_compile_kernelmodules.29051  run.base_do_fetch.28859             run.do_populate_sysroot             run.split_kernel_module_packages.16364 log.do_configure                    run.base_do_unpack.1155             run.do_populate_sysroot.17692       run.split_kernel_packages.16364 log.do_configure.3048               run.BUILDSPEC.28992                 run.do_qa_configure.3048            run.sstate_create_package.10988 log.do_deploy                       run.debian_package_name_hook.16364  run.do_qa_staging.17692             run.sstate_create_package.16364 log.do_deploy.617                   run.do_bundle_initramfs             run.do_sizecheck                    run.sstate_create_package.17692 log.do_fetch                        run.do_bundle_initramfs.28986       run.do_sizecheck.2323               run.sstate_create_package.2724 log.do_fetch.28859                  run.do_compile                      run.do_strip                        run.sstate_create_package.28992 log.do_install                      run.do_compile.3483                 run.do_strip.2321                   run.sstate_create_package.617 log.do_install.2327                 run.do_compile_kernelmodules        run.do_uboot_mkimage                run.sstate_task_postfunc.10988 log.do_package                      run.do_compile_kernelmodules.29051  run.do_uboot_mkimage.2325           run.sstate_task_postfunc.16364 log.do_package.16364                run.do_configure                    run.do_unpack                       run.sstate_task_postfunc.17692 log.do_packagedata                  run.do_configure.3048               run.do_unpack.1155                  run.sstate_task_postfunc.2724 log.do_packagedata.2724             run.do_deploy                       run.emit_pkgdata.16364              run.sstate_task_postfunc.28992 log.do_package_write_rpm            run.do_deploy.617                   run.fixup_perms.16364               run.sstate_task_postfunc.617 log.do_package_write_rpm.28992      run.do_fetch                        run.package_depchains.16364         run.sstate_task_prefunc.10988 log.do_patch                        run.do_fetch.28859                  run.package_do_filedeps.16364       run.sstate_task_prefunc.16364 log.do_patch.2556                   run.do_install                      run.package_do_pkgconfig.16364      run.sstate_task_prefunc.17692 log.do_populate_lic                 run.do_install.2327                 run.package_do_shlibs.16364         run.sstate_task_prefunc.2724 log.do_populate_lic.10988           run.do_package                      run.package_do_split_locales.16364  run.sstate_task_prefunc.28992 log.do_populate_sysroot             run.do_package.16364                run.package_fixsymlinks.16364       run.sstate_task_prefunc.617 log.do_populate_sysroot.17692       run.do_packagedata                  run.package_get_auto_pr.16364       run.sysroot_cleansstate.3048 log.do_sizecheck                    run.do_packagedata.2724             run.package_get_auto_pr.2327        run.sysroot_stage_all.17692 log.do_sizecheck.2323               run.do_package_qa.16364             run.package_get_auto_pr.617         run.write_specfile.28992 log.do_strip                        run.do_package_rpm.28992            run.package_name_hook.16364 log.do_strip.2321                   run.do_package_write_rpm            run.patch_do_patch.2556 For each package, you will be able to see the log for the latest task, and what was done on the latest task. For example: log.do_compile - shows the log output from latest do_compile made for kernel run.do_compile - shows the compile command line log.do_compile.111111 - shows the log output from 1111111 time of do_compile In order to know the tasks and the task sequence, take a look to log.taskorder file For the images generated, you will find something like that: .../build_mx6$ ls -la tmp/deploy/images/imx6qsabresd/ total 146260 drwxr-xr-x 2 user user     4096 Mar  6 21:21 . drwxrwxr-x 3 user user     4096 Mar  6 21:12 .. -rw-r--r-- 1 user user 67108864 Mar  6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.ext3 -rw-r--r-- 1 user user 83886080 Mar  6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.sdcard -rw-r--r-- 1 user user 18782361 Mar  6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.tar.bz2 lrwxrwxrwx 1 user user       55 Mar  6 21:21 core-image-base-imx6qsabresd.ext3 -> core-image-base-imx6qsabresd-20140306173758.rootfs.ext3 lrwxrwxrwx 1 user user       57 Mar  6 21:21 core-image-base-imx6qsabresd.sdcard -> core-image-base-imx6qsabresd-20140306173758.rootfs.sdcard lrwxrwxrwx 1 user user       58 Mar  6 21:21 core-image-base-imx6qsabresd.tar.bz2 -> core-image-base-imx6qsabresd-20140306173758.rootfs.tar.bz2 -rw-rw-r-- 2 user user   439697 Mar  6 21:12 modules--3.0.35-r37.14-imx6qsabresd-20140306173758.tgz lrwxrwxrwx 2 user user       54 Mar  6 21:12 modules-imx6qsabresd.tgz -> modules--3.0.35-r37.14-imx6qsabresd-20140306173758.tgz -rw-rw-r-- 2 user user      294 Mar  6 21:20 README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt lrwxrwxrwx 2 user user       35 Mar  6 21:16 u-boot.imx -> u-boot-imx6qsabresd-v2013.10-r0.imx lrwxrwxrwx 2 user user       35 Mar  6 21:16 u-boot-imx6qsabresd.imx -> u-boot-imx6qsabresd-v2013.10-r0.imx -rwxr-xr-x 2 user user   297984 Mar  6 21:16 u-boot-imx6qsabresd-v2013.10-r0.imx lrwxrwxrwx 2 user user       53 Mar  6 21:12 uImage -> uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin -rw-r--r-- 2 user user  4042496 Mar  6 21:12 uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin lrwxrwxrwx 2 user user       53 Mar  6 21:12 uImage-imx6qsabresd.bin -> uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin You can access any generated image, the image name ending with the yearmothdaypid (long number) is the real image, and every time your bitbake complete, it generate a new image. The symbolic link points to the latest created image. The .ext3 file is the EXT3 image for the rootfs. (you can copy it directly to SD card using dd: $sudo dd if=core-image-base.ext3 of=/dev/sdb2 ) The .sdcard file is the complete image to be copied to sdcard. It´s u-boot+uImage+rootfs The .tar.bz2 file is the tarball for the rootfs, you can extract it on your PC. uImage is the latest kernel image u-boot is the latest u-boot image. and so on. Play around with generated files. A lot of them I don´t know. And a lot of them I don´t use. For a standard image generation you only need to know where the final images is placed. Any question, comment, issue, please let me know. Before you go, let your bitbake creates the biggest image ever: $ bitbake fsl-image-gui Note (24Feb2014): Required disk space for build image is ~44GB Start it and let it finish while you do something else. Go HOME Go to Task #2 Go to Task#4
記事全体を表示
USB Certification report of i.Mx6
記事全体を表示
NOTE: Please suggest bitbake commands you find it useful! bitbake command Description bitbake <image> Bake an image (add -k to continue building even errors are found in the tasks execution) bitbake <package> -c <task> Execute a particular package's task. Default Tasks names: fetch, unpack , patch , configure , compile , install , package , package_write , and build. Example: To (force) compiling a kernel and then build, type: $ bitbake  linux-imx -f -c compile $ bitbake linux-imx bitbake <image > -g -u depexp Show the package dependency for image. Example: To show all packages included on fsl-image-gui $ bitbake fsl-image-gui -g -u depexp NOTE: This command will open a UI window, so it must be execute on a console inside the host machine (either virtual or native). bitbake <package> -c  devshell Open a new shell where with neccesary system values already defined for package hob bitbake frontend/GUI. bitbake <package> -c listtasks List all tasks for package bitbake virtual/kernel -c menuconfig Interactive kernel configuration bitbake <image> -c fetchall Fetch sources for a particular image bitbake-layers show-layers Show layers bitbake-layers show-recipes "*-image-*" Show possible images to bake. Without "*-images-*", it shows ALL recipes bitbake -g <image> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq Show image's packages bitbake -g <pkg> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq Show package's dependencies bitbake –v <image> 2>&1 | tee image_build.log Print (on console) and store verbose baking bitbake -s | grep <pkg> Check if certain package is present on current Yocto Setup
記事全体を表示
The customer would like to test BT.656 using Test mode. Is it supported? 38.4.3.3 Test mode in RM shows only one CSIx_SENS_CONG setting. Does it mean Test mode support only one as follows? Does Test mode support other settings? CSIx_EXT_VSYNC = 0x1 CSIx_DATA_WIDTH = 0x1 CSIx_SENS_DATA_FORMAT = 0x0 CSIx_PACK_TIGHT = 0x0 CSIx_SENS_PRTCL = 0x1 CSIx_SENS_PIX_CLK_POL = 0x1 CSIx_DATA_POL = 0x0 CSIx_HSYNC_POL = 0x0 CSIx_VSYNC_POL = 0x0 For example, customer want to know if Test mode support  CSIx_SENS_PRTCL=0x2or 0x3 instead of 0x1? customer want to know if Test mode support CSIx_SENS_DATA_FORMAT=0x1or 0x2 instead of 0x0? Answer: CSI CM TEST MODE is working as below: 1,only ungated mode. 2,data width should be configured to 8 3,data format should be configured to rgb888 It cannot be other format such as bt656. It uses CSI1_TST_CTRL register to configure {R,G,B} 24 bit value and taking it as RGB888/YUV444 format for further process.  The generated image size is due to the configured width & height in the registers.
記事全体を表示
This patch release is target for LPDDR2 ( dual channels in interleave mode ) support on i.MX6DL platform. Two patches are prepared to modify u-boot and kernel in order to have correct DRAM init sequence, 400MHz & 24MHz frequency switching and suspend/resume support. The patches are not fully verified. It is provided as reference for customer to enable their i.MX6DL board with LPDDR2. Customization and Testing is needed by customer. We need to remind some points here: MMDC_MDCFG3LP in 24MHz need to increase the margin ( 0x40222 -> 0x80555 ) in order to pass the OS frequency switch stress test. We are identifying the reason but this workaround is working fine and included to the patch. Code changes in kernel is prepared so that it is compatible to DDR3. In other words, the DDR type will be detected and a correct handling will be done for LPDDR2 and DDR3. In LPDDR2 system, we can't put SDQ pin into LPM during suspend. Otherwise, the system cannot resume. Dual channels in fix mapping mode is not recommended to use.
記事全体を表示
           This application note shows how to get i.MX6X development resources from Freescale website. Contents           We can enter Freescale i.MX website by the follow link http://www.freescale.com/imx, and after we input it into the IE address, it will remap to the new address of http://www.freescale.com/webapp/sps/site/homepage.jsp?code=IMX_HOME&tid=vanIMX. And the website page will have all the i.MX chipsets access web link like the follows:       And if we enter the i.MX6 serials Processors web link http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=IMX6X_SERIES , we will get the page like the follows:        Which have all the i.MX6 serials processors feature lists and website links. 1       i.MX6Q/D website guide. We enter the i.MX6D/Q web link http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&webpageId=129226228141673454B24A&nodeId=018rH3ZrDRB24A&fromPage=tax its main page as follows:    The Documentation and Software&Tools items is very important to get the design resource, and the Buy/Parametrics item will have the development board and chipset order information 1.1    i.MX6Q/D Documentation      We enter the Documentation item link: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Documentation_Tab, which will have our documentation materials include the Datasheet, Errata, Application Notes, Reference manual, User guides, Fact Sheets and related supporting information. 1.1.1  i.MX6Q/D DataSheet          We have i.MX6Q/D datasheets of automotive, consumer and industrial, the datasheet will have the chipset mark number, electrical, thermal and package information. IMX6DQAEC i.MX 6Dual/6Quad Automotive and Infotainment Applications Processors IMX6DQCEC i.MX 6Dual/6Quad Applications Processors for Consumer Products IMX6DQIEC i.MX 6Dual/6Quad Applications Processors for Industrial Products 1.1.2  i.MX6Q/D Errata       Chipset Errata will show us our current version chipset bugs and rework method. IMX6DQCE Chip Errata for the i.MX 6Dual/6Quad 1.1.3  i.MX6Q/D  Application Notes AN4724 i.MX 6Dual/6Quad Product Usage Lifetime Estimates AN4629 Fast Image Processing with i.MX 6 Series AN4671 i.MX 6 Series HDMI Test Method for Eye Pattern and Electrical Characteristics AN4397      //all the i.MX6 Serial can use the same PCB, this doc descript the hardware design difference Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite AN4581 Secure Boot on i.MX50, i.MX53, and i.MX 6 Series using HABv4 AN4509   //explan the i.MX6D/Q power consumption in every working features. i.MX 6Dual/6Quad Power Consumption Measurement AN4589 Configuring USB on i.MX 6 Series Processors AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors AN4467 //explain the ddr calibration method, need check with FSL FAE for DDR test calibration tools i.MX 6 Series DDR Calibration AN4579 // explain the thermal design i.MX 6 Series Thermal Management Guidelines 1.1.4  i.MX6Q/D Chipset reference manual IMX6DQRM //i.MX6DQ reference manual for all the internal module description and registers define. i.MX 6Dual/6Quad Applications Processor Reference Manual IMX6DQ6SDLSRM   // i.MX6DQ security related reference manual, need NDA approve. Security Reference Manual for i.MX 6 1.1.5  i.MX6Q/D User guide IMX6DQ6SDLHDG //i.MX6DQ hardware design user guide, include the schematic layout check points, hardware bring up… Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications EB792 i.MX 6 Series Standardized Signal Name Map EB793 MISRA Compliance in Freescale Automotive C Language Header Files - Engineering Bulletin 1.1.6  i.MX6Q/D Fact Sheet IMX6SRSFS i.MX 6 Series of Applications Processors - Fact Sheet 1.1.7  i.MX6Q/D BSP/Codec Software Document L3.0.35_4.0.0_LINUX_DOCS   i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Documentation. Includes Release Notes, Reference Manual,... MX6 folder include the BSP release notes, reference manual, user guide and other APIs doc. L3.0.35_4.0.0_LINUX_MMDOCS   i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Multimedia Codecs Documentation. Includes CODECs Release... IMX6_JB422_100_ANDROID_DOCS   i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Documentation. Includes Release Notes, User's... 1.1.8  i.MX6Q/D InfoCTR IMX_INFOCTR //TIC support center i.MX Infocenter—Online Documentation 1.2    i.MX6Q/D  Software&Tools We enter into the Software&Tools item page: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Design_Tools_Tab 1.2.1  i.MX6Q/D  Reference Designs SABRE Platform for Smart Devices Based on the i.MX 6 Series  The Smart Application Blueprint for Rapid Engineering (SABRE) platform for smart devices allows you to hold in your hands and evaluate the full multimedia performance capabilities of i.MX 6 series applications processors based on ARM® Cortex™-A9 technology.  Targeted for any device ... Enter it: Press Buy: SABRE Board for Smart Devices Based on the i.MX 6 Series  Freescale's Smart Application Blueprint for Rapid Engineering (SABRE) board for smart devices introduces developers to quad-core processing, low-power consumption and leading-edge multimedia and graphics applications on the i.MX 6Quad ARM ® Cortex™ -A9 applications processor. The SABRE board for smart devices ... Enter it: Press Buy:   SDB board share the same PCB with SDP, but have no camera, LVDS and GPS moduel. SABRE for Automotive Infotainment Based on the i.MX 6 Series  The Smart Application Blueprint for Rapid Engineering (SABRE) for automotive infotainment offers a solid foundation for next-generation converged telematics and infotainment platform designs. Based on i.MX 6 series of applications processors, Freescale's most scalable implementation of the ARM® Cortex™-A9 CPU ... Enter it: Press Buy:    Which have the CPU board and automotive base board, And if need the automotive board LVDS display panel, we can enter the i.MX53 automotive board link to get the order name. SABRE Lite Development Kit: The SABRE Lite Development Kit includes one SABRE Lite board, one 5V power adapter, one customized serial cable, one cross serial cable (DB9-DB9), one USB cable, one net cable and one 4GByte micro SD... Format: html    Saber Lite board a mini system board which use the separate power design, which launch by 3 rd party. 1.2.2  i.MX6Q/D  PCB and Schematic i.MX6_SABRE_AI_DESIGNFILES   : Design files, including hardware schematics, layout files and BOM. Size (K): 39164 Format: zip Rev #: 1.0.2 Modified: 2/27/2013 i.MX6_SABRE_SDP_DESIGNFILES   : Design files, including hardware schematics, Gerbers, and OrCAD files.. Size (K): 11631 Format: zip Rev #: C3 Modified: 3/21/2013 iMX6_SABRE_SDB_DESIGNFILES   : Design files, including hardware schematics, Gerbers, and OrCAD files.. Size (K): 9541 Format: zip Rev #: C3 Modified: 3/21/2013 1.2.3  i.MX6Q/D  Programmers Tools IMX_6DQ_MFG_TOOL   : Tool and documentation for downloading OS images to the i.MX 6Quad and i.MX6Dual. Size (K): 69444 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 IMX_MFG_TOOL_V2_SOURCE   : Source Code for the i.MX manufacturing tool used for downloading OS images to the i.MX 6 Processors. Size (K): 955 Format: zip Rev #: 2.1.1 Modified: 12/19/2012 1.2.4  i.MX6Q/D  Software IMX_6D_Q_VIVANTE_VDK_145_TOOLS   : Set of applications for the Linux L3.0.35_4.0.0 BSP, designed to be used by graphics application developers to rapidly develop and port graphics applications. Includes applications, GPU Driver with vprofiler enabled and documentation.. Size (K): 40113 Format: zip Rev #: 1.4.5 Modified: 5/13/2013 IMX6_GPU_SDK   : i.MX6 Graphics SDK – Includes sample, demo code, and documentation for working with the i.MX6X family graphics cores. Includes OpenVG, OpenGL ES, and GAL2D reference files. Size (K): 21065 Format: gz Rev #: 1.0.0 Modified: 1/25/2013 i.MX 6Series Platform SDK   : Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license. Size (K): 29865 Format: tgz Rev #: 1.1 Modified: 2/11/2013      A non-OS i.MX6X driver test codes.  1.2.5  i.MX6Q/D  Tools IMX_CST_TOOL   : Freescale Code Signing Tool for the High Assurance Boot library. Provides software code signing support designed for use with i.MX processors that integrate the HAB library in the internal boot ROM. Size (K): 3855 Format: tgz Rev #: 2.0 Modified: 11/16/2012      Please still refer the document of i.MX6Q/D security RM and HAB application notes. IMX6_IOMUX_TOOL   : Interactive i.MX Pin Mux Tool.. Size (K): 5313 Format: zip Rev #: 3.4.0.3 Modified: 2/14/2013      Please still refer the document of i.MX6Q/D iomux table. 1.2.6  i.MX6Q/D  BSDL IMX6_DQ_BSDL   : i.MX 6Quad and i.MX 6Dual BSDL File. Size (K): 64 Format: zip Rev #: 2 Modified: 1/15/2013        A Boundary scan file for manufacture ICT test. 1.2.7  i.MX6Q/D  IBIS IMX6_DQ_IBIS   : i.MX 6Quad and i.MX 6Dual IBIS File. Size (K): 19173 Format: zip Rev #: 1 Modified: 11/9/2012       Use for signals simulation. 1.2.8  i.MX6Q/D  BSP IMX6_DQ_SABRE_AI_SD_DEMO_IMAGE   : Demo Image Flashed on the i.MX 6Quad SABRE AI SD Cards. Size (K): 1789607 Format: exe Rev #: L3.0.35_1.1.1 Modified: 4/23/2013 IMX6_DQ_SDB_SD_DEMO_IMAGE   : Demo Image Flashed on the i.MX 6Quad SDB SD Cards. Size (K): 1670416 Format: exe Rev #: R13.4.1 Modified: 4/24/2013 IMX6_DQ_SDP_SD_DEMO_IMAGE   : Demo Image Flashed on the i.MX 6Quad SDP SD Cards. Size (K): 1670892 Format: exe Rev #: R13.4.1 Modified: 4/24/2013 L3.0.35_4.0.0_DEMO_IMAGE   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Binary Demo Files. Size (K): 359441 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 IMX6_JB422_100_ANDROID_DEMO   : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Binary Demo Files. Size (K): 836432 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/8/2013 Demo image for customer to evaluate on Freescale’s board. IMX6_JB422_100_ANDROID_SOURCE   : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP, Documentation and Source Code for BSP and Codecs.. Size (K): 235533 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/9/2013 Android JB422 source codes, still have the R13.41 android source codes in the same web folder. L3.0.35_4.0.0_ER_SOURCE   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Source Code Files. Size (K): 1064236 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 Linux LTIB source codes package. L3.0.35_4.0.0_UBUNTU_RFS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux File System for the Ubuntu Images. Size (K): 820076 Format: tgz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 Ubuntu rootfs working on our linux BSP. 1.2.9  i.MX6Q/D  Software Codecs IMX6_JB422_100_AACP_CODEC   : AAC Plus Codec for i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0. Size (K): 84 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/15/2013    Android have no codec package except AACP, have include in the BSP release codes. L3.0.35_4.0.0_AACP_CODECS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux AAC Plus Codec. Size (K): 1377 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 L3.0.35_4.0.0_MM_CODECS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Multimedia Codecs Sources. Size (K): 79197 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013    Linux have MM codec package. 1.2.10              i.MX6Q/D  Updates and Patches   Which have the older patch on L3.0.35 elder version, and Android R13.4/13.4.1. 2       i.MX6DL/S website guide. We enter the i.MX6DL/S web link http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&webpageId=129226228141673454B24A&nodeId=018rH3ZrDRB24A&fromPage=tax    its main page as follows: 2.1    i.MX6DL/S Documentation http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Documentation_Tab 2.1.1  i.MX6DL/S DataSheet IMX6SDLAEC i.MX 6Solo/6DualLite Automotive and Infotainment Applications Processors IMX6SDLCEC i.MX 6Solo/6DualLite Applications Processors for Consumer Products IMX6SDLIEC i.MX 6Solo/6DualLite Applications Processors for Industrial Products 2.1.2  i.MX6DL/S Errata IMX6SDLCE Chip Errata for the i.MX 6Solo/6DualLite 2.1.3  i.MX6DL/S D  Application Notes IMX6SDLIEC i.MX 6Solo/6DualLite Applications Processors for Industrial Products AN4576 i.MX 6DualLite Power Consumption Measurement 2.1.4  i.MX6DL/S Chipset reference manual IMX6SDLRM i.MX 6Solo/6DualLite Applications Processor Reference Manual IMX6DQ6SDLSRM   Security Reference Manual for i.MX 6 2.1.5  i.MX6DL/S User Guide IMX6DQ6SDLHDG Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications EB793 MISRA Compliance in Freescale Automotive C Language Header Files - Engineering Bulletin 2.1.6  i.MX6DL/S Fact Sheet IMX6SRSFS i.MX 6 Series of Applications Processors - Fact Sheet 2.1.7  i.MX6DL/S BSP/Codec Software Document L3.0.35_4.0.0_LINUX_DOCS   i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Documentation. Includes Release Notes, Reference Manual,... L3.0.35_4.0.0_LINUX_MMDOCS   i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Multimedia Codecs Documentation. Includes CODECs Release... IMX6_JB422_100_ANDROID_DOCS   i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Documentation. Includes Release Notes, User's... 2.1.8  i.MX6DL/S InfoCTR IMX_INFOCTR i.MX Infocenter—Online Documentation 2.2    i.MX6DL/S Software&Tools http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Design_Tools_Tab 2.2.1  i.MX6DL/S Reference Designs SABRE Platform for Smart Devices Based on the i.MX 6 Series  The Smart Application Blueprint for Rapid Engineering (SABRE) platform for smart devices allows you to hold in your hands and evaluate the full multimedia performance capabilities of i.MX 6 series applications processors based on ARM® Cortex™-A9 technology.  Targeted for any device ... SABRE for Automotive Infotainment Based on the i.MX 6 Series  The Smart Application Blueprint for Rapid Engineering (SABRE) for automotive infotainment offers a solid foundation for next-generation converged telematics and infotainment platform designs. Based on i.MX 6 series of applications processors, Freescale's most scalable implementation of the ARM® Cortex™-A9 CPU ... 2.2.2  i.MX6DL/S PCB and Schematic i.MX6_SABRE_AI_DESIGNFILES   : Design files, including hardware schematics, layout files and BOM. Size (K): 39164 Format: zip Rev #: 1.0.2 Modified: 2/27/2013 I.MX_6DL_S_VIVANTE_VDK_TOOLS   : i.MX6DL and i.MX6S Vivante VDK Tools. Size (K): 39752 Format: zip Rev #: 1.4.1 Modified: 1/4/2013 i.MX 6Series Platform SDK   : Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license. Size (K): 29865 Format: tgz Rev #: 1.1 Modified: 2/11/2013 2.2.3  i.MX6DL/S Programmers Tools IMX_6DL_6S_MFG_TOOL   : Tool and documentation for downloading OS images to the i.MX 6DualLite and i.MX6Solo. Size (K): 67584 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 2.2.4  i.MX6DL/S  Software 2.2.5  i.MX6DL/S BSDL IMX6_DL_S_BSDL   : i.MX 6DualLite and i.MX 6Solo BSDL File. Size (K): 81 Format: html Rev #: 1 Modified: 11/9/2012 2.2.6  i.MX6DL/S IBIS IMX6_DL_S_IBIS   : i.MX 6DualLIte and i.MX 6Solo IBIS File. Size (K): 15450 Format: zip Rev #: 1 Modified: 11/9/2012 2.2.7  i.MX6DL/S BSP IMX6_DL_SDP_SD_DEMO_IMAGE   : Demo Image Flashed on the i.MX 6DualLiteSDP SD Cards. Size (K): 367806 Format: zip Rev #: R13.4.1 Modified: 12/10/2012 IMX6_JB422_100_ANDROID_DEMO   : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Binary Demo Files. Size (K): 836432 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/8/2013 L3.0.35_4.0.0_DEMO_IMAGE   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Binary Demo Files. Size (K): 359441 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 IMX6_JB422_100_ANDROID_SOURCE   : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP, Documentation and Source Code for BSP and Codecs.. Size (K): 235533 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/9/2013 L3.0.35_4.0.0_ER_SOURCE   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Source Code Files. Size (K): 1064236 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 L3.0.35_4.0.0_UBUNTU_RFS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux File System for the Ubuntu Images. Size (K): 820076 Format: tgz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 2.2.8  i.MX6DL/S Software Codecs IMX6_JB422_100_AACP_CODEC   : AAC Plus Codec for i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0. Size (K): 84 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/15/2013 L3.0.35_4.0.0_AACP_CODECS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux AAC Plus Codec. Size (K): 1377 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 L3.0.35_4.0.0_MM_CODECS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Multimedia Codecs Sources. Size (K): 79197 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 2.2.9  i.MX6Q/D  Updates and Patches Which have the older patch on L3.0.35 elder version, and Android R13.4/13.4.1. 3       i.MX6SL website guide. http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&webpageId=129226228141673454B24A&nodeId=018rH3ZrDRB24A&fromPage=tax 3.1    i.MX6SL Documentation http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Documentation_Tab 3.1.1  i.MX6SL DataSheet IMX6SLCEC i.MX 6SoloLite Applications Processors for Consumer Products 3.1.2  i.MX6SL Errata IMX6SLCE Chip Errata for the i.MX 6SoloLite 3.1.3  i.MX6SL Application Notes AN4726 i.MX 6SoloLite Product Usage Lifetime Estimates AN4580 i.MX 6SoloLite Power Consumption Measurement 3.1.4  i.MX6SL Chipset reference manual IMX6SLRM i.MX 6SoloLite Applications Processor Reference Manual 3.1.5  i.MX6SL User guide IMX6SLHDG Hardware Development Guide for i.MX 6SoloLite Applications Processors - User Guide 3.1.6  i.MX6SL Fact  Sheet IMX6SRSFS i.MX 6 Series of Applications Processors - Fact Sheet IMX6SLEVKFS i.MX 6SoloLite Evaluation Kit - Fact Sheet 3.1.7  i.MX6SL BSP/Codec Software Document L3.0.35_2.1.0_LINUX_DOCS   i.MX 6SoloLite Linux BSP Documentation. Includes Release Notes, Reference Manual, User guide. API Documentation L3.0.35_2.1.0_LINUX_MMDOCS   i.MX 6SoloLite Linux Multimedia Codecs Documentation. Includes CODECs Release Notes and User's Guide IMX6_R13.5_ANDROID_DOCS_BUNDLE   i.MX 6 Sololite Android GA BSP Documentation. 3.1.8  i.MX6SL INFOCTR IMX_INFOCTR i.MX Infocenter—Online Documentation 3.2    i.MX6SL Software&Tools http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Design_Tools_Tab 3.2.1  i.MX6SL Reference Designs IMX6SLEVK: i.MX 6SoloLite Evaluation Kit. Freescale delivers the next installment in a line of highly-flexible, market-focused development tools with an Evaluation Kit (EVK) based on the i.MX 6SoloLite applications processor. The i.MX 6SoloLite is the first... Format: html Modified: 6/4/2013 3.2.2  i.MX6SL PCB and Schematics iMX6SL_EVK_DESIGNFILES   : Design files, including hardware schematics, Gerbers, and OrCAD files.. Size (K): 6034 Format: zip Rev #: 1 Modified: 11/12/2012 3.2.3  i.MX6SL Programmers Tools IMX_6SL_MFG_TOOL   : Tool and documentation for downloading OS images to the i.MX 6SoloLite. Size (K): 46502 Format: gz Rev #: L3.0.35_2.1.0 Modified: 5/24/2013 3.2.4  i.MX6SL Tools IMX_CST_TOOL   : Freescale Code Signing Tool for the High Assurance Boot library. Provides software code signing support designed for use with i.MX processors that integrate the HAB library in the internal boot ROM. Size (K): 3855 Format: tgz Rev #: 2.0 Modified: 11/16/2012 IMX6_IOMUX_TOOL   : Interactive i.MX Pin Mux Tool.. Size (K): 5313 Format: zip Rev #: 3.4.0.3 Modified: 2/14/2013 3.2.5  i.MX6SL Software i.MX 6Series Platform SDK   : Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license. Size (K): 29865 Format: tgz Rev #: 1.1 Modified: 2/11/2013 3.2.6  i.MX6SL BSDL IMX6_SL_BSDL   : i.MX 6SoloLite BSDL File. Size (K): 54 Format: html Rev #: 1 Modified: 11/9/2012 3.2.7  i.MX6SL IBIS IMX6_SL_IBIS   : i.MX 6SoloLite IBIS File. Size (K): 25706 Format: zip Rev #: 1 Modified: 11/9/2012 3.2.8  i.MX6SL BSP IMX6_R13.5_ANDROID_DEMO_IMAGE   : i.MX 6Sololite GA BSP Binary Demo Files. Size (K): 372634 Format: gz Rev #: R13.5 Modified: 11/16/2012 L3.0.35_12.10.02_DEMO_IMAGE   : Linux Binary Demo Files for i.MX 6SoloLite Linux GA BSP. Size (K): 434356 Format: gz Rev #: 12.10.02 Modified: 11/9/2012 L3.0.35_2.1.0_DEMO_IMAGE   : i.MX 6SoloLite Linux Binary Demo Files. Size (K): 464844 Format: gz Rev #: L3.0.35_2.1.0. Modified: 6/4/2013 IMX6_R13.5_ANDROID_SOURCE_CODE   : i.MX 6 Sololite Android GA BSP Documentation and Source Code for BSP and Codecs.. Size (K): 100683 Format: gz Rev #: R13.5 Modified: 11/16/2012 L3.0.35_12.10.02_ER_SOURCE   : i.MX 6SoloLite Linux GA BSP 3.0.35 Source Code Files.. Size (K): 872027 Format: gz Rev #: 12.10.02 Modified: 11/9/2012 L3.0.35_12.10.02_UBUNTU_RFS   : File System for the Ubuntu Imagea for i.MX 6SoloLite Linux GA BSP. Size (K): 810816 Format: tgz Rev #: 12.10.02 Modified: 11/9/2012 L3.0.35_2.1.0_ER_SOURCE   : i.MX 6SoloLite Linux BSP Source Code Files. Size (K): 1064541 Format: gz Rev #: L3.0.35_2.1.0. Modified: 6/4/2013 3.2.9  i.MX6SL Software Codecs L3.0.35_2.1.0_AACP_CODECS   : i.MX 6SoloLite Linux AAC Plus Codec. Size (K): 1374 Format: gz Rev #: L3.0.35_2.1.0 Modified: 5/24/2013 L3.0.35_2.1.0_MM_CODECS   : i.MX 6SoloLite Linux Multimedia Codecs Sources. Size (K): 45883 Format: gz Rev #: L3.0.35_2.1.0 Modified: 5/24/2013 3.2.10              i.MX6SL Updates and Patches IMX6_R13.5_01_ANDROID_PATCHES   : Android 13.5.0-GA.01 patch release. It adds camera support (USB and CSI camera), provides some bug fixes, and includes some regular updates. The 13.5.0-GA.01 patch release is based on 13.5.0-GA.. Size (K): 186882 Format: gz Rev #: R13.5-GA.01 Modified: 1/4/2013 Which have the older patch on L3.0.35 elder version, and Android R13.5.         
記事全体を表示
The i.MX6 Multi-Mode DDR Controller (MMDC) has profiling capabilities to monitor the operation of the controller. The profiling capability counts certain events related to a specified AXI-ID during a profiling period. The events that can be counted are: The number of read accesses during the profiling period (MMDCx_MADPSR2[RD_ACC_COUNT] register field) The number of write accesses during the profiling period (MMDCx_MADPSR3[WR_ACC_COUNT] register field) The number of bytes read during the profiling period (MMDCx_MADPSR4[RD_BYTES_COUNT] register field) The number of bytes written during the profiling period (MMDCx_MADPSR5[WR_BYTES_COUNT] register field) The number of MMDC clock cycles during which the MMDC state machine is busy (MMDCx_MADPSR1[BUSY_COUNT] register field) BUSY_COUNT is the number of MMDC clock cycles during the profiling period in which the MMDC state machine is not idle. So this is the time the MMDC spends doing any activity, not just read or write data transfers. The MMDC state machine is active whenever there are any read or write requests in the read and write FIFOs. The MMDC is active during many operations that are not reading or writing data such as arbitration of requests, control cycles, bank open/close, etc. So BUSY_COUNT represents the number of cycles when the controller is busy, not just the number of cycles when the external bus is busy. The number of bytes read and bytes written can be used to determine data throughput and the BUSY_COUNT can be used to determine what part of the time the controller is active/idle. Together these can be used to determine the controller efficiency for a particular application. For detailed information, see the "MMDC profiling" section of the MMDC chapter in the reference manual for the SoC being used.
記事全体を表示
Issue: During DDR3 Burst Write, the DQS strobe signal must be driven low for a minimum of 0.3 x cycle period on the last data clock cycle before it is released. This ensures sufficient time for the write to be strobed correctly. When measuring this timing parameter, it has often been found to be too short. This may be contributing to write errors on customer boards, depending on the signal layout used by the board. Root Cause: The internal DQS strobe enable signal is controlled by the MMDC, which is tied to the SDCLK clock signal. But the DQS strobe signal can be delayed in the MMDC to match different SDCLK trace lengths by using Write Leveling parameters to ensure the the DQS strobe edge reaches the DDR3 device at the same time the SDCLK edges reaches the device. If the write level delay is too long, the MMDC can crop the end of the DQS strobe signal too short, causing a violation of the Write Post Amble Delay timing specification and potentially leading to  write errors. How much delay in the Write Leveling parameter would cause this problem? The Reference Manual states that a delay around half a cycle may cause problems, but testing on some boards indicates that delays even as short as 1/4 a cycle could cause violations of the Write Post Amble Delay. Solution: The MMDC was designed with the ability to add extra time to the strobe enable period during write procedures. This parameter is referred to as Write Additional Latency. It is found in the MMDCx_MDMISC register and the field is labeled as WALAT. Incrementing the value of this register field by one adds a full clock cycle delay to the Write Post Amble period, and ensures enough time at the end of a burst write to guarantee a correct write. There is no maximum value to Write Post Amble Delay. Setting WALAT = 1 (or larger if WL parameters are larger) will cause a small hit in overall performance, but will add to the reliability of write operations, particularly on boards that require larger WL parameter settings.
記事全体を表示
Overview This document introduces how to setup i.MX6Dual/Quad and i.MX6Solo/DualLite Linux software for PCIe compliance test. Software Baselines i.MX6Dual/Quad: Linux BSP L2.6.35_1.0.0 i.MX6Solo/DualLite: Linux BSP L2.6.35_2.0.0 Software Changes To enable PCIe compliance test, PCIe software driver should not turn off PCIe clock and power in the tests. So the following changes are required: diff --git a/arch/arm/mach-mx6/pcie.c b/arch/arm/mach-mx6/pcie.c index 26d26f2..ad71085 100644 --- a/arch/arm/mach-mx6/pcie.c +++ b/arch/arm/mach-mx6/pcie.c @@ -801,6 +801,7 @@ static void __init add_pcie_port(void __iomem *base, void __iomem *dbi_base,      } else {          pr_info("IMX PCIe port: link down!\n"); +#if 0          /* Release the clocks, and disable the power */          pcie_clk = clk_get(NULL, "pcie_clk");          if (IS_ERR(pcie_clk)) @@ -820,6 +821,7 @@ static void __init add_pcie_port(void __iomem *base, void __iomem *dbi_base,          imx_pcie_clrset(IOMUXC_GPR1_TEST_POWERDOWN, 1 << 18,                  IOMUXC_GPR1); +#endif      } } Software Build Integrate the patch to the baseline code and recompile the kernel by following the instructions in Linux BSP user guide. Before recompile, please ensure the following configuration is enabled by selecting " System Type -> Freescale MXC Implementations -> PCI Express support" as "*": # MX6 Options: # CONFIG_IMX_PCIE=y
記事全体を表示
New i.mx6Q core board from OpenEmbed.comNew i.mx6Q core board from OpenEmbed.com
記事全体を表示