i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
JAVA on i.MX Sun Microsystems has pre-built versions of Java Virtual Machine for ARM Processors. It's possible to download them at: http://java.sun.com/javase/downloads/embedded.jsp All pre-built software mentioned on site above are distributed as evaluation software. For more information about use and license, please contact Sun Microsystems i.MX31 PDK will be used as an example to describe installation, compilation and execution procedures. It can be easily done for other i.MX platforms Installing Sun Java on i.MX For i.MX31, i.MX35, download the following version: Usage Headful Binary Version Non-Graphical Applications ARMv6 Linux - Headless (Early Access) EABI, glibc 2.5, Hard Float (VFP), Little Endian Graphical Applications ARMv6 Linux - Headful (Early Access) EABI, glibc 2.5, Hard Float (VFP), Little Endian For i.MX21, i.MX25, i.MX27, download the following version: Usage Headful Binary Version Non-Graphical Applications ARMv5 Linux - Headless (Early Access) EABI, glibc 2.5, Soft Float, Little Endian Graphical Applications ARMv5 Linux - Headful (Early Access) EABI, glibc 2.5, Soft Float, Little Endian On following example, a graphical application will be compiled, the headful version will be used. This example uses X11 as graphical server. On LTIB, select X11 and also the package libXtst and libXi. Extract the downloaded package (in this case "ejre-1_6_0_10-ea-b39-linux-armv6-vfp-eabi-min-eval-30_jul_2009.tar.gz") tar xzvf ejre-1_6_0_10-ea-b39-linux-armv6-vfp-eabi-min-eval-30_jul_2009.tar.gz Create a new folder on <LTIB Directory>/rootfs/ called ejre1.6.0_10 cd rootfs sudo mkdir ejre1.6.0_10 Copy all files and folders located inside the extracted package to <LTIB Directory>/rootfs/ejre1.6.0_10/ cd rootfs/ejre1.6.0_10 cp -a ../../ejre1.6.0_10/* . Include the bin folder to the PATH: export PATH=$PATH:/ejre1.6.0_10/bin/ In this example the X11 will be used as graphical server. Add the display environment variable: export DISPLAY=:0 Running a simple program Compiling and testing on Host PC Let's first compile and test a simple program on Host Machine (PC). Create a file called Example1.java and add the following code: import java.awt.*;   public class Example1 extends java.applet.Applet {    public void init()    {         add(new Button("One"));         add(new Button("Two"));    }     public Dimension preferredSize()    {         return new Dimension(480, 640);    }        public static void main(String [] args)    {         Frame f = new Frame("Example 1");          Example1 ex = new Example1();          ex.init();          f.add("Center", ex);                  f.pack();         f.show();    } } On terminal, compile the source code using ecj: $ ecj Example1.java ecj Java Compiler is needed to compile this example. To install ecj on Debian based OS, install the packages: sudo apt-get install ecj ecj-gcj libecj-java libecj-java-gcj Now it's possible to test the compiled program. Just type on host: $ java Example1 The following window will be shown: Running on i.MX Copy the file Example1.class to <LTIB Directory>/rootfs/home cp Example1.class rootfs/home On i.MX Linux, start Xfbdev in background: $ Xfbdev & Run Example1: $ java Example1 The following screen will be shown on LCD:
記事全体を表示
Hi, The document "How to create ubuntu hardfloat rootfs for imx6d/q" was shared by Junping Mao. https://community.freescale.com/docs/DOC-95185 However, some modification need to be made to build imx-tests on this rootfs. Attached please find the guide for building imx-tests on hf-ubuntu rootfs for imx6d/q. Any problems, pls feel free to let me know. Regards, Alvin zheng
記事全体を表示
Question: When working with v1.6.0.55 using the standard profile for i.MX35 the tool fails most of the time when transferring the target root file system, on v1.6.0.42 it works just fine. The tags on the internal git don’t clearly mention a tool version, but a BSP. Wwhat are the differences between v1.6.0.55 and v1.6.0.42? Or to which tag(or commit) they correspond on git? Answer: 1.6.042 commit by looking at "Apps/MfgTool.exe/docs/changelog.txt": 1ca2a16df736ac51979a67423fef6a09bed6b7e2 And 1.6.055: "06a4f9190e34297b7273fc4bb4a92737e5bc837f"
記事全体を表示
///////////////////////////create device node /dev/galcore///////////////////////////// $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/Kbuild MODULE_NAME ?= galcore /* define node name*/ $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h define DEVICE_NAME "galcore" $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_probe.c drv_init call ret = register_chrdev(major, DEVICE_NAME, &driver_fops); ///////////////////////////////opengles2 functios/////////////////////////////////////////// myandroid/device/fsl-proprietary/gpu-viv/lib/egl/libGLESv2_VIVANTE.so glActiveTexture glBindBuffer ... ... ... //those glxxxxxx call into sub_D40C int __fastcall sub_D40C(int a1, int a2, int a3) //address 0x0000D40C { int result; // r0@1 int v4; int v5; v4 = a2;   v5 = a3;   gcoOS_GetTLS(&v4);  //------------> goto libGAL.so   result = v4;   if ( v4 )     result = *(_DWORD *)(v4 + 36);   return result; } and $home/myandroid/device/fsl-proprietary/gpu-viv/lib/libGAL.so //export function signed int __fastcall gcoOS_GetTLS(void **a1) { ... ... gcoOS_GetTLS v4 = open("/dev/galcore", 2); ... ... } and device node /dev/galcore pass command into module galcore $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel.c gckKERNEL_Dispatch This document was generated from the following discussion: Share Vivante 3d gc2000 work flow
記事全体を表示
  Some our customers want to use the mfgtool to download the images to QSPI and boot up. When download the demo images on our website (Linux 4.1.15) to the QSPI-NOR on IMX7D SABRE-SDB. The error occurred as follows: Is it able to program the QSPI-NOR on i.MX7D SABRE-SDB by using MFG-Tool? Answer is yes. In the above error message we can see that the system can not find and detect the qspi, so it can not excute the following code,<CMD state="body="$ flash_erase /dev/mtd0 0 20">Erasing Boot partition</CMD>Updater" type="push" when use the mfgtool to download the images to the QSPI-NOR . The board i.MX7D SABRE-SDB and default BSP are boot up from EPDC.  Here customer want to boot up from QSPI, When using QSPI, you need to de-populate R388-R391, R396-R399 and populate R392-R395, R299, R300 in your hardware. QSPI signals are muxed with EPDC_D[7:0]. You can see the schematic, details you can see as follow. After hardware modify, you can use the mfgtool2-yocto-mx-sabresd-qspi-nor-mx25l51245g.vbs to download. And then boot up from qspi, boot mode you can refer to the schematic boot up setting. Both software and mfgtool you can download here http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-software-and-tools:IMXSW_HOME. Demo images can documents you can also get.    
記事全体を表示
The LTC®3676 is a complete power management solution for i.MX6, ARM Cortex processor systems. The LTC3676 features eight independent resistor-programmable voltage rails, with dynamic control and sequencing, in compact QFN and LQFP packages. These rails supply power to the processor core, SDRAM, system memory, PC cards, always on real-time clock (RTC), and a variety of other functions. Quad I 2 C Adjustable High Efficiency Step-Down DC/DC Converters: 2.5A, 2.5A, 1.5A, 1.5A Triple 300mA LDO Regulators (2 Adjustable) DDR Power Solution with VTT and VTTR Reference Pushbutton On/Off Control with System Reset Independent Enable Pin-Strap and I2C Sequencing Programmable Autonomous Power-Down Control Power Good and Reset Functions Dynamic Voltage Scaling Selectable 2.25MHz or 1.12MHz Switching Frequency Always Alive 25mA LDO Regulator 10μA Standby Current 40-Pin 6mm × 6mm × 0.75mm QFN and 48-Pin 7mm × 7mm LQFP Packages Contact Linear Technology for further details (please note that this is a pre-release product; however, data sheets and ES samples are available from Linear Technology) http://www.linear.com/product/LTC3676 or Gerard Velcelean at [email protected] or Steve Knoth at [email protected]
記事全体を表示
Hello i.MX Community. Attached there is a guide on how to install Ubuntu trusty on i.MX7D-SD board Basically it explains all steps to install and to have running ubuntu core 14.04 on the Freescale i.Mx7D-SDB: I hope you find the document and projects useful! Regards!
記事全体を表示
Hardware : i.MX8MNLPDDR4EVK Build Yocto Image [Linux 4.14.98_2.3.1] Yocto Project Setup          $: mkdir imx-yocto-bsp          $: cd imx-yocto-bsp                $: repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.3.1.xml          $: repo sync  copy marvell bb.file into yocto source         $: cp  0001-Porting-mrvl-8987-wifi.patch   imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp         $: git apply 0001-Porting-mrvl-8987-wifi.patch Image Build         $: DISTRO=fsl-imx-xwayland MACHINE=imx8mnlpddr4evk source fsl-setup-release.sh -b build-xwayland         $:bitbake fsl-image-qt5-validation-imx Enable wifi and BT (These operations is on EVK) WiFi $:insmod /lib/modules/4.14.98-2.3.1+g860ec89/extra/sd8xxx.ko fw_name=/mrvl/sduart8987_combo.bin cal_data_cfg=none cfg80211_wext=0xf BT $:hciattach /dev/ttymxc0 any -s 115200 115200 flow dtron $:hciconfig hci0 reset $:hcitool -ihci0 cmd 0x3f 0x0009 0xc0 0xc6 0x2d 0x00 & $:killall hcitool $:killall hciattach $:hciattach /dev/ttymxc0 any -s 3000000 3000000 flow dtron Build  Android Image[Android P9_2.3.4] These patches in  Android-2.3.4-patch. Getting i.MX Android release source code        $: cd ~ (or any other directory you like)        $: tar xzvf imx-p9.0.0_2.3.4.tar.gz        $: mkdir ~/bin        $: curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo        $: chmod a+x ~/bin/repo        $: export PATH=${PATH}:~/bin        $: source ~/imx-p9.0.0_2.3.0/imx_android_setup.sh        # By default, the imx_android_setup.sh script will create the source code build environemnt        in the folder ~/android_build        # ${MY_ANDROID} will be refered as the i.MX Android source code root directory in all i.MX        Andorid release documentation.        $ : export MY_ANDROID=~/android_build Copy 88W8987 firmware and driver into  Android release code        $:copy -r Android-2.3.4-patch/mrvl    android_build/vendor/nxp/fsl-proprietary  Apply these patches.The name of these patches is the patche installation path.            example:  0001-android_build-hardware-marvell-wlan.patch         $: cp 0001-android_build-hardware-marvell-wlan.patch   android_build/hardware/marvell/wlan            (if not exist android_build/hardware/marvell/wlan, mkdir -p android_build/hardware/marvell/wlan)         $: git apply 0001-android_build-hardware-marvell-wlan.patch  Building Android images          $: cd  android_build          $: source build/envsetup.sh          $: lunch evk_8mn-userdebug          $: make 
記事全体を表示
$ git log --pretty=oneline --abbrev-commit 6f0c058 Linux 3.7-rc2 198190a Merge tag 'arm64-fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/cmarinas/linux-aarch64 aeed41a arm64: fix alignment padding in assembly code 31fd84b use clamp_t in UNAME26 fix 8c1bee6 Merge branch 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip 45bff41 perf python: Properly link with libtraceevent
記事全体を表示
Question: Clarify if the delay units, mentioned in  i.MX6 RM in two places are the same : 1. There are delay units for data strobes, that are considered in calibration procedures. 2. There are delay units for clocks SDCLK, mentioned in section 44.12.54 “MMDC PHY CK Control Register (MMDCx_MPSDCTRL)” of the RM. General delay units description states : “ The delay issued by the delay-line (according to the configured value) is absolute and takes into account the operating and temperature conditions. The delay-line has a resolution that may vary from device to device; an increment of 1 delay unit may vary between 20 pSec to 50 pSec.” It may be guessed that the same relates to SDCLK delays, but preliminary i.MX6 specs mention that bit fields SDCLKx_DEL (x=0,1) control SDCLK delay, that can be up to 1 cycle.  This means SDCLKx_DEL step is 1/4  of the SDCLK. Please clarify SDCLK delays (SDCLKx_DEL) in more details. Answer: "The delay elements in the SDCLK path are similar to those in the data strobes but they are not exactly the same. The delay is on the order of picoseconds, though, not a full SDCLK cycle as might have been interpreted from the older document."
記事全体を表示
Enabling Dual Display in Ubuntu with the i.MX53 Quick Start Board Here you will learn how to enable two displays in a Ubuntu system running in an iMX53 Quick Start Board. We assume here that you already have a micro SD card with a valid Ubuntu image (including uboot, Linux kernel and Ubuntu filesystem). You can use the original SD card that comes with the i.MX53 Quick Start Board, which brings an image of Ubuntu or, if you do not have the original SD card, you can reproduce it by downloading Ubuntu binaries package (L2.6.35_MX53_ER_1101_IMAGE) from Freescale iMX53qsb download area. You will also need to update U-boot and kernel binaries in the SD card with more recent images. You can find the most recent binaries (L2.6.35_MX53_ER_1109_IMAGE_) from Freescale iMX53qsb download area as well. Introduction To enable dual display, you need to perform two tasks: Enable two displays at kernel level Configure your Xorg server accordingly Enabling Two Displays at Kernel Level To enable two displays at kernel level means to map one display interface to fb0 device and the other to fb1 device. So first thing is to choose which interface will be the primary one, mapped as fb0. As an example, we consider the VGA interface as primary in this tutorial. Second thing is to choose one of the other available external video interfaces to be secondary, mapped as fb1 device in the system. We consider the 4.3" seiko LCD display in this tutorial as the secondary interface. Once chosen primary and secondary interfaces, we need to configure kernel video arguments accordingly. The arguments are available in specific variables in the U-boot that comes with the Ubuntu binaries. You can see them (HDMI, VGA, etc.) by printing the U-boot environment variables from the U-boot shell, but you will probably not find those variables in other versions of U-boot and their contents will probably need to be adapted to the kernel version in use, as arguments recognized by kernel modules varies considerably between kernel versions. You can always refer to the Linux Release Notes documents for video arguments. It's available for each Linux BSP that can be found on the Freescale website. For the 1109 BSP, we have the following video arguments (extracted from i.MX53_START_Linux_BSP_Release_Note.pdf that comes with L2.6.35_11.09.01_ER_docs.tar.gz downloaded from here - IMX53_1109_LINUXDOCS_BUNDLE😞 VGA: video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga SEIKO LCD: video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary Both are considered primary, because these are the arguments for single display setups. Now that we have video arguments for both desired interfaces, we only need to merge them together removing the primary argument from the one that is the secondary. In our case, we need to pass the following arguments to the kernel: video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga video=mxcdi0fb:RGB24,SEIKO-WVGA For this, we can add these arguments to one of the variables that are used in the boot process. We can add the content to bootarg_base, for instance. In the U-boot command line, execute following commands to setup the environment: setenv vga_and_seiko 'video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga video=mxcdi0fb:RGB24,SEIKO-WVGA' setenv bootargs_base 'setenv bootargs console=ttymxc0,115200 vga_and_seiko' saveenv After applying a reset and booting the board, you shall have both interfaces enabled, but the secondary will not be used by the Xorg server until we complete the next step. Configuring Xorg Server Now that we have two video interfaces properly configured and mapped to /dev/fb0 and /dev/fb1 devices, we need to tell Xorg server how to use them. Here is an example of xorg.conf file that you can use to replace the default one, found at /etc/X11: Section "InputDevice" Identifier     "Generic Keyboard" Driver          "kbd" Option          "XkbRules"     "xorg" Option          "XkbModel"     "pc105" Option          "XkbLayout"     "us" EndSection  Section "InputDevice" Identifier     "Configured Mouse" Driver          "mouse" Option          "CorePointer" EndSection  Section "Device" Identifier     "i.MX Accelerated Framebuffer Device 0" Driver          "imx" Option          "fbdev"               "/dev/fb0"  # This option only recognized when "mxc_epdc_fb" frame buffer driver in # use.  Values are "RGB565" (default, 16-bit RGB), "Y8" (8-bit gray), # and "Y8INV" (8-bit gray inverted). Option          "FormatEPDC"               "Y8INV"  EndSection  Section "Device" Identifier     "i.MX Accelerated Framebuffer Device 1" Driver          "imx" Option          "fbdev"               "/dev/fb1"  EndSection  Section "Monitor" Identifier     "Configured Monitor 0" EndSection  Section "Monitor" Identifier     "Configured Monitor 1" EndSection  Section "Screen" Identifier     "Screen 0" Monitor          "Configured Monitor 0" Device          "i.MX Accelerated Framebuffer Device 0"  # These "Display" SubSection's are needed for working with the # "mxc_epdc_fb" frame buffer driver. SubSection     "Display" Depth     8 Visual     "StaticGray" EndSubSection SubSection     "Display" Depth     16 Visual     "TrueColor" EndSubSection EndSection  Section "Screen" Identifier     "Screen 1" Monitor          "Configured Monitor 1" Device          "i.MX Accelerated Framebuffer Device 1" EndSection  Section "ServerLayout" Identifier     "Xinerama Layout" Screen          "Screen 0" Screen          "Screen 1" RightOf "Screen 0" EndSection  Section "ServerFlags" Option          "Xinerama"          "true" EndSection Results The following picture shows the i.MX 53 QSB running the extended desktop previously configured. You can see the VGA monitor with a Firefox instance and the SEIKO LCD display with a calc instance.
記事全体を表示
The attached patch applies to iMX6_Platform_SDK for i.MX6 Dual and Quad and brings 2 additional SDMA memory to memory scripts: fixed destination address, increasing source address fixed source address, increasing destination address. With this patch, the new scripts are also integrated in the SDMA Test menu of the Platform SDK. I created these scripts starting from the ROM script ap_to_ap. In order to dump the content of the SDMA ROM, I used mxc_printSDMAcontext function which is also included in the attached patch and can be invoked when needed.
記事全体を表示
MX6X_eMMC_turning_2014.11.11_V2.doc
記事全体を表示
When boot from battery, then plug in 5V cable, the actual charging current can't reach the preset charging current. It is because the HEADROOM_ADJ is not correctly set. Please use attached mx28_chargingcurrent_limit_bootfrombattery.patch. Grace
記事全体を表示
Tested on Android 10 (android_Q10.0.0_1.0.0) After your the first BSP build the kernel sources are at: ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/ For the i.MX8M Mini, You can check the defconfig files being used on: ${MY_ANDROID}/device/fsl/imx8m/evk_8mm/UbootKernelBoardConfig.mk # imx8mm kernel defconfig TARGET_KERNEL_DEFCONFIG := android_defconfig TARGET_KERNEL_ADDITION_DEFCONF := android_addition_defconfig You could change one of them to add the desired configuration. - android_defconfig - is ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/arch/arm64/configs/android_defconfig - android_addition_defconfig - is on the same folder ${MY_ANDROID}/device/fsl/imx8m/evk_8mm/ "merge_config.sh" is called to generate the final defconfig file prior to building the kernel Check out: https://source.android.com/devices/architecture/kernel/config For example, I want to add DEVMEM support on my build: 1. Change the defconfig I add the line below to android_addition_defconfig CONFIG_DEVMEM=y (Or could have added it android_defconfig) 2. Build the kernel ./imx-make.sh kernel -c -j8 3. Verify your change After compiling, you can confirm your change by reading: ${MY_ANDROID}/out/target/product/evk_8mm/obj/KERNEL_OBJ/.config Then rebuild boot.img and reprogram the target.
記事全体を表示
Why raising QoS priority for EPDC Eink has been developing higher resolution panel. With higher resolution, TCE underrun problem is observed more easily. Highest QoS priority can provide obvious improvement. What's TCE underrun TCE is Timing Controller Engine which is responsible for TFT scan frame refreshes. The pixel FIFO (PIX_FIFO) is used to load working buffer pixel data for TCE. When FIFO underrun, TCE_UNDERRUN_IRQ interrupt is triggered, and TCE underrun log pops up in kernel log. The pixel data is processed by TCE to generate TFT voltage control pixels for panel. If an underrun occurs, unknown data is used and that can damage the panel. About the patch The patch raises EPDC reading to highest priority (QoS='f'), so the EPDC reading becomes real time channel in MMDC configuration. The patch is based on L4.1.15 kernel. Stress test of unit test can pass with 1920x1440 configuration.
記事全体を表示
How to add Ethernet UI support in ICS     How to add Ethernet UI support in ICS 1.  Introduction 2.  New feature detail   1.  Introduction   If you want to add Ethernet UI support , you need manually apply the attached patches in this file which is based on Android ICS and i.MX6.        About what the patches do, here is some comments: framework/base-----0001-ENGR00220371-Ethernet-add-support-for-ethernet.patch        By default, Android has no support for Ethernet UI. So if you want to add Ethernet UI , add Ethernet state tracker & Ethernet service & Ethernet manager & Ethernet monitor like WiFi. Meanwhile we need add Ethernet display support in status bar. Here this patch can solve it. Build---0001-ENGR00220371-Ethernet-add-ethernet-support.patch        add package directory compile. packages\apps\Settings---0001-ENGR00220371-Ethernet-add-app-UI-in-setting.patch        add UI logic in setting app. packages\providers\DownloadProvider---0001-ENGR00220371-Ethernet-add-downloadinfo.patch        add ConnectivityManager.TYPE_ETHERNET type support in download provider’s DownloadInfo.   2.  New feature detail   After applying the above patches, you will get the following features: Icon for Ethernet connection status. If on, a green icon will appear in status bar; If off,no icon will appear.     Add “Ethernet configuration” UI.  Choose box is designed for turn on or off Ethernet.      Only Ethernet is turned on, Ethernet configuration can be configured static IP.   First boot, Ethernet device default may not be eth0. So change it from the device list. Use imx6-ics-ethernet-v3.zip. It has updated and fixed the following issues compared with the previous two versions:   1. fix static IP not work issue. 2. fix dns using default 8.8.8.8 issue. 3. eth0 is the default interface, no longer need to choose it from the list. 4. dhcp is default mode. and if you are using static IP. After reboot, it will restore to dhcp again. 5. no need to edit dns again.   List the bug list for update. If using ethernet as upstream type, you need to apply the attached fix-use-ethernet-as-upstream.patch.   For JB4.2.2 and JB4.3, we have written one apk for this. Anyone who is interested in this can get it.
記事全体を表示
I've recently done some digging into fstrim feature on sabresd-6q. Here list it below detailed: Background:      When Nexus 7 first came out, many users felt it was speedy and high-performance. But after months of installing applications and using the tablet, things began slowing down.This was a friction point that many hoped would be fixed in the new Nexus 7 (2013) model, which it was. There’s even more to the story though, it turns out Google has fixed that storage I/O aging problem on all Nexus devices with the Android 4.3 update which comes with a little-hyped feature that could be huge for performance in the future – TRIM support via fstrim. Why slowing down?      Remember that deleting a file in software isn't actually communicated to solid state storage (whether SSD or eMMC). The space is freed up from the user's perspective, but the eMMC controller in this case still treats the pages in NAND as having valid data. Let's say you copy a 3GB movie to your internal storage, watch the movie and later delete it. You'd have 3GB free to re-use, but until you re-write those blocks the eMMC controller would treat all 3GB as valid data. There's a data structure used by the eMMC controller that tracks mapping logical locations to physical locations in NAND. I won't go into great detail here but the more complex that mapping becomes, and the more locations that have to be tracked, the slower internal NAND management works. Why SSD has such issue? Root cause is "Flash memory is divided into blocks, which is further divided in pages. The minimum write unit is a page, but the smallest erase unit is a block" which will cause fragments as time goes. Why fstrim?      Fstrim is one mechanism of linux filesystem which derives from TRIM. TRIM is already introduced since linux2.6.33. It is the name of a command that the operating system can send to tell the SSD which blocks are free in the filesystem.The SSD uses this information to internally defragment the blocks and keep free pages available to be written quickly and efficiently. How framework triggers fstrim in android4.3?      Android4.3 introduces a new service IdleMaintenanceService to manage when and how trigger fstrim in right time. Once system satisfies the following conditions, it will send out one "ACTION_IDLE_MAINTENANCE_START" intent which the MountService listens for. Last time  "ACTION_IDLE_MAINTENANCE_START" intent has been sent before 24 hours. The device is either off-charger with 80% battery or on-charger with 30% battery The device can go idle state. User don't use it for 71 minutes. Test fstrim on Imx.6      In order to wait little time to trigger fstrim, I tried to change the following variables not to wait 71 minutes and 24 hours. After changing, it will trigger one time fstrim two minutes after system goes into idle state every 30 minutes. --- a/services/java/com/android/server/IdleMaintenanceService.java +++ b/services/java/com/android/server/IdleMaintenanceService.java -    private static final long MIN_IDLE_MAINTENANCE_INTERVAL_MILLIS = 24 * 60 * 60 * 1000; // 1 day +    private static final long MIN_IDLE_MAINTENANCE_INTERVAL_MILLIS = 30 * 60 * 1000; // 30 minute -    private static final long MIN_USER_INACTIVITY_IDLE_MAINTENANCE_START = 71 * 60 * 1000; // 71 min +    private static final long MIN_USER_INACTIVITY_IDLE_MAINTENANCE_START = 2 * 60 * 1000; // 2 min -    private static final long MAX_IDLE_MAINTENANCE_DURATION = 71 * 60 * 1000; // 71 min +    private static final long MAX_IDLE_MAINTENANCE_DURATION = 2 * 60 * 1000; // 2 min Firstly I  run Quadrant apk to see my I/O performance at beginning, Its score is 3544. During this 30 minutes, you can try to mess your system. Try your best to install most apks. Run monkey test in background. Then I  run Quadrant again to check my I/O performance, its score is only a little decline 3538. After that I run "logcat | busybox grep -i fstrim" in console to wait for the action of fstrim, here is my logcat: 130|root@sabresd_6dq:/ # logcat -d | busybox grep -i fstrim I/fstrim  ( 2344): Starting fstrim work... I/fstrim  ( 2344): Invoking FITRIM ioctl on /data I/fstrim  ( 2344): Trimmed 6367305728 bytes on /data I/fstrim  ( 2344): Invoking FITRIM ioctl on /cache I/fstrim  ( 2344): Trimmed 526355456 bytes on /cache I/fstrim  ( 2344): Finished fstrim work. OK, I checked the I/O information again, its score is restored to 3546: Conclusion      Good, fstrim takes effect. So on imx.6 using android4.3, fstrim will also work automatically. We will also enjoy good performance in I/O memory.Great!
記事全体を表示
After rework the board, enable two OTG controllers in Linux DTB file and disable VBUS valid comparator when in suspend mode by clear USB_OTGx_PHY_CTL2 bit 16.  Then we get the following power data on suspend mode  Suspend Mode     ****  The page is under internal check ****
記事全体を表示