S32DS for Vision - list of HOWTOs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS for Vision - list of HOWTOs

S32DS for Vision - list of HOWTOs

Installation & Activation

HOWTO: Activate S32 Design Studio 

HOWTO: Install Lauterbach TRACE32 debugger plug-in into S32 Design Studio 

Create a New Project 

HOWTO: Create APEX2 Project From Example in S32DS for Vision 

HOWTO: Create An ISP Project From Example in S32DS for Vision 

HOWTO: Create A53 Linux Project in S32DS for Vision 

HOWTO: Create An ISP Project From Existing VSDK Graph in S32DS for Vision 

HOWTO: Create A New Makefile Project With Existing Code From NXP Vision SDK Example Project  

HOWTO: Build a Project and Setup a Debug Configuration for debugging in S32 Design Studio 

HOWTO: Create A53 APEX2 and/or ISP Linux Project in S32DS for Vision

DDR Configuration & Validation and Stress Test Tools

HOWTO: Use DDR Configuration and Validation Tool 

HOWTO: Use DDR Stress Test Tool 

Hardware Setup

HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP

HOWTO: Prepare and boot S32V234 EVB from eMMC 

HOWTO: Setup static IP address for S32 debug probe 

Debugging

HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP 

HOWTO: S32V234-EVB debugging with Linux and gdbserver on target machine 

HOWTO: Start Debug on an ISP Application Project with S32 Debugger and S32 Debug Probe 

HOWTO: Start Debug on an APEX2 Application Project with S32 Debugger and S32 Debug Probe 

Debugging the Startup Code with Eclipse and GDB | MCU on Eclipse  

VSDK

HOWTO: Change Vision SDK root in S32DS for Vision 

HOWTO: Create A New Makefile Project With Existing Code From NXP Vision SDK Example Project 

HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK 

Linux

HOWTO: S32V234 EVB Linux - Static IP address configuration 

HOWTO: S32V234 EVB Linux - DHCP IP address setup 

HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK 

HOWTO: Access Linux BSP file system on S32V234-EVB from S32DS for Vision

HOWTO: Setup A Remote Linux Connection in S32DS for Vision 

General Usage

HOWTO: S32 Design Studio Command Line Interface 

HOWTO: Add user example into S32DS 

HOWTO: Generate S-Record/Intel HEX/Binary file 

HOWTO: Update S32 Design Studio 

Troubleshooting

Help! I just relaunched S32DS for Vision and my visual graph is collapsed! 

Help! I just updated to new version of S32DS and now my projects have errors and I can't build! 

Troubleshooting: PEmicro Debug Connection: Target Communication Speed 

Troubleshooting: Indexer errors on header file 

S32 Design Studio Offline activation issue hot fix 

https://community.nxp.com/docs/DOC-345238 

标签 (1)
标记 (2)
无评分
版本历史
最后更新:
‎09-14-2017 06:40 AM
更新人: