i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
We have validated Toshiba Smart NAND in our i.MX6SX platform, and boot successfully. The results are as below: 1. chip part number: THGBR2G5D1JTA00,  page_size: 16k+64  pages_per_block: 256 2. test platform: i.MX6SX Some information to take care of: 1. The pin assignment of smart nand is different from common raw nand, that is, Nand pin1 must connect to Vcc, pin2 connects to Vss, pin23 connects to VssQ, pin24 connects to VccQ, pin38 connects to VccQ 2. The ECC layout of FCB page itself must be set according to the i.MX6SX RM, otherwise FCB can't be read correctly. 3. EccBlock0EccType and EccBlockNEccType in FCB must be set as 0, and raw data can be put in DBBT and firmware without any ECC check codes.
查看全文
RidgeRun provides a fully featured Embedded Linux Software Development Kit for Freescale iMX6 based applications processors. Freescale iMX6 platform delivers high performance, power efficient applications processors with a robust support network and software portfolio including open source. The complete platform allows for differentiation and rapid development of applications from wireless handsets to other multimedia-enhanced devices. The i.MX6 series processors are a scalable multicore platform that includes single-, dual- and quad-core families based on the ARM® Cortex™-A9 architecture. This architecture is a robust - cross industry and product platform. Whether your product is targeted at consumer electronics, industrial, automotive or security related, this flexible, scalable architecture combined with RidgeRun's easy-to-use SDK's and extension products allows you to concentrate your effort of differentiating features and not product infrastructure. FEATURES Boot loader 2013.07 Linux kernel 3.0.35-4.0.0 Gstreamer-0.10.36 Freescale gst-plugins 3.0.7 Hardware based audio and video codecs SD and NFS file system support Boot from SD3, SD4 or SPI-NOR with an easy installation (Boundary devices boards only) Toolchain to linaro 2012.03 for software floating point and 2013.03 for hardware floating point support For more info please contact: [email protected] or Please Click -> Contact Us
查看全文
Ridgerun SDK for iMX6 based boards now supports the X11 protocol. The server-client based protocol is now supported by our professional SDK using hardware floating point which enables a high performance and provides all the advantages that comes with X.  In the RidgeRun SDK you'll also find complete integration of Qt4.8.5 using an X-based windowing system. We currently support Matchbox and Enlightenment which is a complete desktop environment. Contact RidgeRun for more details at : [email protected] or Please Click -> Contact Us RidgeRun Home Page : www.ridgerun.com RidgeRun iMX6 based solutions : iMX6 Based Solutions
查看全文
The i.MX 6 D/Q/DL/S/SL  Linux L3.0.101_4.1.1 Patch release is now available on [www.freescale.com]www.freescale.com ·          Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board This patch release is based on the i.MX 6 Linux 3.0.35_4.1.0 release. The purposes of this patch release are as follows: ·         To fix the BSP multimedia GPU bugs ·         To upgrade the Linux kernel to v3.0.101 ·         To upgrade the multimedia library ·         To upgrade the GPU driver and library to 4.6.9p13 Please consult the release notes for more details. ​
查看全文
The i.MX 6 D/Q/DL/S/SL  Linux L3.10.17_1.0.2 Patch release is now available on www.freescale.com ·          Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board This patch release is based on the i.MX 6 Linux L3.10.17_1.0.2 BSP release. ·         Release Description o    Kernel branch: imx_v2013.04_3.10.17_1.0.0_ga o    U-Boot branch: imx_3.10.17_1.0.0_ga o    Graphics: gpu-viv-bin-mx6q, 3.10.17_1.0.2 o    Graphics: gpu-viv-g2d, 3.10.17_1.0.2 o    Graphics: Xorg-driver, 3.10.17_1.0.2 ·         Patch Description Please consult the release notes.
查看全文
As the Voice over IP (VoIP) market grows, the next evolution of the market is Video and Voice over IP (V2IP). iWave’s iW-RainboW-G15S is a Pico-ITX Single Board Computer (SBC) which has a Freescale’s i.MX6 DualLite ARM Cortex-A9 core based CPU which can operate up to 800MHz speed/core with 1GB (expandable) DDR3 RAM. iWave has provided V2IP on iWave’s Pico ITX i.MX6 which gives more quality in video and audio streaming. iWave has expertise in HD video streaming over V2IP. The SIP(Session Initiation Protocol) protocol for connection between i.MX6 PICO ITX board and host PC which is used in the application Linphone through network (Ethernet). Linphone is a comprehensive solution consisting of an extensive set of algorithms and codecs designed for Digital Voice and Video applications. Above design can be utilized for peer to peer communication between i.MX6 PICO ITX single board computer and PC with Android OS. The i.MX6 single board computer and PC are connected to an Ethernet. The Audio CODEC used on the iMX6 PICO ITX dev board is ALC5610 from Realtek with inbuilt Headphone amplifier and MIC which is used to provide a complete audio solution for portable products. The video pixel rates are typically from 25 MHz up to 297 MHz, but HDMI can support higher rates up to 340 MHz’s i.MX6 PICO ITX board supports LVDS connector to connect different LVDS LCDs. It also supports backlight connector with 15V 300mA output for LCD backlight. iWave's i.MX 6 PICO ITX SBC supports 8/10bit CMOS Camera Interface. External clock for camera is provided using on board Oscillator of frequency 26MHz. i.MX6 CPU supports MIPI CSI interface. The V2IP systems use some existing standard video codec and audio codec to reduce the program material to a bit stream and then use an Internet Protocol (IP) network to carry that bit stream encapsulated in stream of IP packets. This is typically accomplished using some variant of the RTP protocol. Freeescale i.MX6 multimedia applications processor provides sufficient power to provide high-quality audio through wideband audio, in-call audio and video recording on flash. Image: V2IP on iWave’s Android i.MX6 Pico ITX Single Board Computer Video Streaming Platform feature: Pico ITX board with i.MX6 dual lite CPU 320X240p camera OS: Android jelly-bean (4.3) MIC HDMI with 1920X1080p display Android NDK and SDK H264 video codec Freescale’s VPU     For further information or enquiries please write to [email protected] or visit www.iwavesystems.com
查看全文
In recovery mode, recovery may update /boot or /system, but it never overwrite itself. The update of /recovery is in the normal bootup. When system boot up, it will execute init.rc which will call install-recovery.sh. The install-recovery.sh is in update.zip. when the system is in recovery mode, updater-script will  unzip update.zip, and the install-recovery.sh will be unzip into /system/etc/. So if you update your image through recovery mode, the install-recovery.sh will be unzip to /system/etc/ automatically. If your update.zip do not include install-recovery.sh. You can edit it and copy it to /system/etc. the below is content in install-recovery.sh. #!/system/bin/sh if ! applypatch -c EMMC:/dev/block/mmcblk3p2:7762488:374c3807940a38d9497a4c5ef64a069e553bc218; then   log -t recovery "Installing new recovery image"   applypatch -b EMMC:/dev/block/mmcblk3p1:7203059:238a297e7e3c7197b2f5af646d0e7e49cef0fd9f EMMC:/dev/block/mmcblk3p2  374c3807940a38d9497a4c5ef64a069e553bc218 7762488 c3c9482c8616805ea4c071ee9184240936f260e5:/system/recovery-from-boot.p else   log -t recovery "Recovery image already installed" fi Explain of the install-recovery.sh: 1、 judge whether the recovery-imx6q.img’s sha1 is the same with mmcblk3p2 on board. 374c3807940a38d9497a4c5ef64a069e553bc218 is the new recovery-imx6q.img’s sha1. 7762488 is the length of recovery-imx6q.img. 2、 if not the same , that mean it was a new recovery-imx6q.img. make a new recovery-imx6q.img through patch recovery-from-boot.p on boot.img. 7203059 and 238a297e7e3c7197b2f5af646d0e7e49cef0fd9f is the length and sha1 of boot.img.     src-file EMMC:/dev/block/mmcblk3p2 is the recovery partition.      tgt-file c3c9482c8616805ea4c071ee9184240936f260e5 is the sha1 of recovery-from-boot.p which is in update.zip. Note: 1、 recovery-from-boot.p is in update.zip. And it is unzip into /system. It is the patch of boot-imx6q.img and recovery-imx6q.img. 2、 for EMMC:/dev/block/mmcblk3p2 is the partition, you can check ./out/target/product/sabresd_6dq/recovery/root/etc/recovery.fstab to see detail partition. Check whether recovery is updated, there are two ways to check: 1、 you can write printf() in file bootable/recovery/recovery.cpp. On the board you can check the file /cache/recovery/last_log. You can find what you printf if the recovery.img was updated. 2、 Also you can use the adb the pull the recovery file system to check whether the recovery was updated.
查看全文
Introduction There are four boot logos in kk4.4.3_2.0.0-beta  system at first: uboot logo\linux logo\android init logo\android animation. We plan to use uboot logo to cover linux logo and android init logo so that we  can combine first three logoes into one logo.This guide provides a step by step explanation of how to transfer uboot UI to  linux kernel and android init smoothly on board sasbresd_6dq sabresd_6dl. The core ideas of the patch: need to  keep display clock from uboot to kernel. When kernel boot up , we do not break the frambuffer for that it stores uboot logo data. need to disable show android init logo. what do the patch do in uboot 1、 can not shut down video after uboot is over.The patch delete releted code in function  arch_preboot_os() 2、 keep hsp clock (ipu clock) the same with linux 3.10 the below is the setting in sabrasd DQ board: osc(24MHz) -> pll2(528MHz) -> mmdc_ch0(528MHz) -> ipu1_hsp_clk(264MHz) the below is the setting in sabrasd DL board: osc(24MHz) -> pll3(480MHz) -> pll3_pdf1(540MHz) -> ipu1_hsp_clk(270MHz) 3、 keep pixel clock the same with linux 3.10 the below is the setting in sabrasd DQ board: osc(24MHz) -> pll2(528MHz) -> pll2_pfd0(452.57MHz) -> ldb_di1(64.65MHz) -> ipu1_di1(64.65MHz) -> ipu1_pixel(64.65MHz) the below is the setting in sabrasd DL board: osc(24MHz) -> pll2(528MHz) -> pll2_pfd0(452.57MHz) -> ldb_di1(64.65MHz) -> ipu1_di1(64.65MHz) -> ipu1_pixel(64.65MHz) 4、 keep pwm clock In kernel,there is a 100% duty pwm to drive lvds panel.So the patch set the pad SD1_DATA3 to a 100% duty pwm pin. 5、 add fbbase and fbmem to bootargs the fbbase is the uboot logo’s phy addr. So the patch pass the parament to kernel through cmdline.we should allocate address aligned 1M for linux 3.10 reserve address aligned by 1 M. what do the patch do in linux 3.10 1、 reserve the address which come from fbbase 2、 keep  ipu related clock when system init the clock in clk-imx6q.c The patch  enable ldb_di1_clk、ipu1_di1_clk、ipu1_clk、pwm1_clk.  Do not disable pll2 and pll3 related clock for the clock may be the source of  ipu clock. Although we enable ldb_di1_clk、ipu1_di1_clk and so on in register, we need to use the function clk_prepare_enable(). Because  the system may close some clocks for their user count is 0(if we use clk_prepare_enable(),it and it’s parent  user count will add 1 ) 3、 disable cabc which will light the panel according the content. Change cabc_enable in dts file. 4、 Move global alpha and color key setting in probe  after framebuffer is registered. Delay       register IPU interrupts used by framebuffer  until IPU hsp clock is enabled.Because global alpha and color key setting and register IPU interrupts may disable hsp clock. disable show android init logo android init logo is the text"android_". we need disable to show it so that the former three logos looks the same logo.The patch 92-system_core solve this problem. The environment of the patch: Hardware: SABRASD DQ&DL Soft ware: kk4.4.3_2.0.0-beta on linux 3.10 How to use the patch: $ cd my_android/kernel_imx/ $ patch -p1 < ./92-kernel_v2 $ cd my_android/bootable/bootloader/uboot-imx/ $ patch -p1 < ./92-uboot_v2     $ cd my_android/system/core $ patch -p1 < 92-system_core Note:      1、 If you want to have this feature on sabraSD dq&dl board,this patch is OK .After you use this patch, you want to change to  other board such as sx, you may meet this problem that the kernel logo penguin don’t appear. You may change this file: arch/arm/configs/imx_v7_android_defconfig                 CONFIG_LOGO=y                 CONFIG_FRAMEBUFFER_CONSOLE=y                 CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY=y                 #CONFIG_MX6_CLK_FOR_BOOTUI_TRANS=y                 #CONFIG_MX6_CLK_FOR_BOOTUI_TRANS_LVDS_IPU1_DI1=y
查看全文
This is an example of QR code encoding using i.MX28. The encoded QR image can show on the LCD display directly using frame buffer and the image saved as a BMP file. Board : i.MX28EVK BSP : L2.6.35_1.1.0_130130_source QR Code Lib:  qrencode-3.4.4.tar.gz Download from https://fukuchi.org/works/qrencode/ Libqrencode is a C library for encoding data in a QR Code symbol. This library is a free software made by Kentaro Fukuchi. Build the QR Code Lib source code into rootfs. 1. Create a new folder in <ltib>/dist/lfs-5.1/.     e.g. <ltib>/dist/lfs-5.1/qrencode 2. Copy the qrencode.spec to this new created folder 3. Build the source code    ./ltib –p qrencode.spec –m prep    ./ltib –p qrencode.spec –m scbuild    ./ltib –p qrencode.spec –m scdeploy Create and build the application in unit_test: - I use the existing unit_test package to build my application code. 1. Extract the source code of unit_test    ./ltib –p imx-test –m prep 2. cd <ltib>/rpm/BUILD/imx-test-2.6.35.3-1.1.0/test 3. mkdir qr_test 4. copy the Makefile and qr_test.c to qr_test folder 5. Build the unit_test     ./ltib –p imx-test  –m scbuild     ./ltib –p imx-test  –m scdeploy After built the code successfully, the qr_test.out will be generated in the unit_test folder. I start the board with NFS, so I can run the qr_test.out on the board directly. The command is : ./qr_test.out   (the default QR encode text is “http://www.freescale.com”) Or input the new text like this : ./qr_test.out –t https://community.freescale.com/community/imx The QR code  show on the display: And the BMP files will be generated in the unit_test folder.
查看全文
The i.MX 6 D/Q/DL/S/SL  Android JB4.3_1.1.1 Patch release is now available on www.freescale.com ·         Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board This patch release is based on the i.MX 6 Android JB 4.3_1.1.0-GA BSP release. ·         Release Description o   To upgrade the GPU kernel and libraries to improve GPU stability o   To handle the Android SDK build failure o   To improve FSL OMX The table below describes the contents of this release.      Release Description Patches Contains the patches included in this release. The patches   are described in “Patch Description”. Documentation Contains the following document: • i.MX 6 Android JB 4.3_1.1.1 Patch Release Notes: This   document. ·         Patch Description Please consult the release notes.
查看全文
Some questions arise when we think about the Android boot sequence. What is the Zygote, init.rc, what is the difference between the linux kernel and the android linux kernel?. This document is intended to explain how the booting process runs. Consider the following graph: Step 1: Power On and System Startup When we press the power button, the Boot ROM code starts executing from a pre-defined location which is hardwired in ROM. It loads the Bootloader into RAM and starts executing. Step 2: Bootloader The bootloader is a small program which runs before Android does. This is NOT part of the Android operating system. The bootloader is the place where manufacturer puts their locks and restrictions. The bootloader executes in two stages. In the first stage it detects external RAM and loads a program which helps in the second stage. In the second stage, the bootloader setups the network, memory, etc, which requires to run kernel. The bootloader is able to provide configuration parameters or inputs to the kernel for specific purposes. The bootloader can be found at: <android source>/bootable/bootloader/legacy/usbloader This legacy loader contains 2 important files: 1- Init.s :: Initializes stacks, zeros the BSS segments and  call_main() in main.c 2- Main.c :: Initializes hardware (clocks, board, keyboard, console) and creates linux tags. Step 3: Kernel The Android kernel starts in a similar way as the linux kernel.  As the kernel launches, is starts to setup cache, protected memory, scheduling and loads drivers. When the kernel finishes the system setup, it looks for “init” in the system files. What is the difference between the linux and android kernels?, here's a list of changes/addons that the Android Project made to the Linux kernel: Binder: It is an Android specific interprocess communication mechanism and remote method invocation system. ashmem:  "Android Shared Memory". It is a new shared memory allocator, similar to POSIX SHM but with a different behavior and sporting a simpler file-based API. pmem: "Process memory allocator": It is used to manage large (1-16+ MB) physically contigous regions of memory shared between userspace and kernel drivers. logger:  This is the kernel support for the logcat command. wakelocks: It is used for power management files. It holds the machine awake on a per-event basis until wakelock is released. oom handling: It kills processes as available memory becomes low. alarm manager: It lets user space tell the kernel when it would like to wake up. RAM_CONSOLE: Allows to save kernel printk messages to a buffer in RAM, so that after a kernel panic they can be viewed in the next kernel invocation. USB gadget driver for ADB yaffs2 flash filesystem Step 4: init process Init is the very first process, we can say it is a root process, or the grandfather of all processes. The init process has two responsibilities.      1- Mounts directories like /sys , /dev    or /proc      2- Runs init.rc script - The init process can be found at /init :: <android source>/system/core/init - Init.rc file can be found at :: <android source>/system/core/rootdir/ Android has specific format and rules for init.rc files. More information about this rules can be found in: What is inside the init.rc and what is it used for. At  this stage, you can finally see the Android logo in your screen. Step 5: Zygote and Dalvik In Java, we know that a separate Virtual Machine instance will popup in memory for separate per app, but in the case of Android, the VM should run as quick as possible for an app. But what happens if you have several apps thus launching several instances of the Dalvik (VM)?, it would consume an immense amount of memory. To overcome this problem, the Android OS has a system called “Zygote”.  The Zygote enables code sharing across the Dalvik VM, achieving a lower memory footprint and minimal startup time.  Zygote is a virtual machine process that starts at system boot. The Zygote preloads and initializes core library classes. The Zygote loading process: Load Zygote Init class: <android source>/frameworks/base/core/java/com/android/internal/os/ZygoteInit.java registerZygoteSocket() :: It registers a server socket for zygote command connections. preloadClasses() :: Is a simple text file that contains a list of classes that need to be preloaded, you can find the file at <android source>/framework/base preloadResources()  :: Everything that is included in the android.R file will be loaded with this method (themes and layouts). At this time, you can see the boot animation. Step 6: System service After the above steps are completed,  Zygote launches the system services.  The Zygote forks a new process to launch the system services. Core services: Starting power manager Creating the Activity Manager Starting telephony registry Starting package manager Set activity manager service as system process Starting context manager Starting system contact providers Starting battery service Starting alarm manager Starting sensor service Starting window manager Starting Bluetooth service Starting mount service Other services: Starting status bar service Starting hardware service Starting NetStat service Starting connectivity service Starting Notification Manager Starting DeviceStorageMonitor service Starting Location Manager Starting Search Service Starting Clipboard Service Starting checkin service Starting Wallpaper service Starting Audio Service Starting HeadsetObserver Starting AdbSettingsObserver Now we have finally completed the booting process (system service are up and running in memory). Need to analyze the Android Bootup? The logcat ::  Use adb to get the booting process events from the logcat. ‘adb logcat –d –b events | grep “boot” ‘adb logcat –d | grep preload’ More information about ADB can be found here: Using ADB with your Sabre Board
查看全文
The init file is a key component of the Android boot sequence. It is a program to initialize the elements of the Android system.  Unlike Linux, Android uses its own initialization program. This Android init program processes 2 files, and it executes the commands it finds in both programs. These programs are: ‘init.rc’ and ‘init<machine name>.rc’ (this machine name is the name of the hardware that Android is running on). What does each program contain?: init.rc provides the generic initialization instructions init<machine name>.rc provides specific initialization instructions init<machine name>.rc is imported by the init.rc program. What is the syntax of these .rc files? The android init language consists of 4 classes of statements: Actions, Commands, Services and Options. Actions and Services declare new sections. All the commands or options belong to the section most recently declared. Actions and Services have to have unique names. If a second Action or Service has the same name of a previous one, it is ignored. Actions Actions are sequences of commands. They have a trigger which is used to determine when the action should occur. Actions take following form. On <trigger> <command> <command> <command>… Services Services are programs which init launches and (optionally) restart when it exists Services take the following form. Service <name> <patchname>  [argument] <option> <option>… Options Options are modifiers to services. These affect how and when init runs a service. Critical This is a device-critical service. If it exits more than four times in four minutes, the device will reboor into recovery mode. Disabled This service will not automatically start with its class. It must be explicitly started by name. Setenv <name> <value> Set the environment variable <name> to <value> in the launched process. User <username> Change to username before executing this service. Currently defaults to root. Group <groupname> [<groupname>] Change to groupname before executing this service. Oneshot Do not restart the service when it exists Class <name> Specify a class name for the service. All services in a named class may be started or stopped together. Onrestart Execute a command when service restarts Triggers Triggers are strings which can be used to match certain kinds of events and used to cause an action to occur. Boot This is the first trigger that will occur when init starts (after /init.conf is loaded) Commands: Exec <path> [<arguments>] Fork and execute a program (<path>). This will block until the program completes execution. Export <name> <value> Set the environment variable <name> equal to <value> in the global environment. Ifup <interface> Bring the network interface <interface> online. Import <filename> Parse and init config file, extending the current configuration. Hostname <name> Set the host name Chdir <directory> Change working directory Chmod <octal-dmoe> <path> Change file access permissions Chwon <owner> <group> <path> Change file owner and group Chroot <directory> Change process root directory Class_start <serviceclass> Start all services of the specified class if they are not already running. Class_stop <serviceclass> Stop all services of the specified class if they are currently running. Domainname <name> Set the domain name Enable <servicename> Turns a disabled service into an enabled one. Insmod <path> Install the module at <path> Mkdir <path> Create a directory at <path> Mount <type><device><dir> Attempt to mount the named device at the directory. Restorecon <path> Restore the file named by <path> to the security context specified in the file_contexts configuration. Setcon <securitycontext> set the current process security context to the specified string. Setenforce 0|1 Set the SELinux system wide enforcing status. 0 = permissive. 1 = enforcing. Setprop <name><value> Set system property <name> to <value> Setrlimit <resource><cur><max> Set the rlimit for a resource Setsebool <name><value> Set SELinux Boolean <name> to <value> Start <service> Start a service Stop <service> Stop a service Symlink <target><path> Create a symbolic link at <path> with the value <target> Trigger <event> Trigger an event. Used to queue an action from another action Wait <path> Poll for the existence of the given file and return when found. Write <path> <string> Open the file at <path> and write a string to it. Examples How to run a script: service my_service /data/test   class main   oneshot Here we are declaring the service named 'my service' with location in /data/test. It belongs to the main class and will start along with any other service that belongs with that class and we declare that the service wont restart when it exits (oneshot). Change file access permissions: chmod 0660   /sys/fs/cgroup/memory/tasks Here we are changing access permissions in path /sys/fs/cgroup/memory/tasks Write a string to a file in a path: write  /sys/fs/cgroup/memory/memory/memory.move_charge_at_immigrate   1 Create a symbolic link: symlink  /system/etc /etc Here we are creating a symbolic link to /system/etc -> /etc Set a specific density of the display: setprop ro.sf.lcd_density 240 Here we are setting a system property of 240 to ro.sf.lcd_density Set your watchdog timer to 30 seconds: service watchdog /sbin/watchdogd 10 20 class core We are petting the watchdog every 10 seconds to get a 20 second margin Change file owner: chown root system /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq The new owner being 'root' from the group 'system'
查看全文
Hi all, Most of IoT customers request to enable/demo i.MX EVK with FSL Zigbee solution. In default i.MX Linux/Android BSP, Zigbee function is not enabled. Here we make a lighting demo setup through i.MX6Q SabreSD, KW20 USB dongle and Philips Hue light. KW20 is configured as Zigbee coordinator, connected with USB OTG in i.MX6Q, then i.MX6Q can issue On/Off, brightness and color control commands through KW20 to toggle Philips Hue light directly. Please find the attachment for details. Best regards, Carl
查看全文
ADB is very well known as the tool to manually install APK’s, but there are some other useful commands. ADB is a command line tool that acts as the bridge between you and your android device. I want to show you some of them, but first, let’s make sure we have everything needed to use ADB. Requirements First, you need to have Java and the Android SDK installed on your PC, you can download it from here: Java SDK: Java SE - Downloads | Oracle Technology Network | Oracle Android SDK: http://developer.android.com/sdk/index.html Once it is installed, it is recommended to update the SDK Manager Once you have done this, flash the Freescale Android BSP onto your board… Once you have installed it, you need to enable USB Debugging in the Developer Options of your board.        Here's the steps to enable USB debugging: Go to Settings. Click on "about tablet" Scroll down to the last row (Build Number) and tap that row 7 times. Return to the previous screen and click on "developer options" Confirm that "usb debugging" is checked. Once you enable it, your OS (assuming you are using Windows) will look for the Android ADB Interface driver. Windows systems are the only ones that need this ADB driver. After this procedure, you can now start using ADB. Open a terminal window and go to the platform-tools directory of your SDK installation to find the ADB program. The usual path to find it would be: adt-bundle-windows-x86 >> sdk >>platform-tools adb start-server                              ::  Starts the ADB server in case it is not running already adb kill-server                   :: Terminates de ADB server adb devices                        :: Checks  and prints the status of each device plugged to your PC  (If you don’t see your device, make sure USB debugging is enabled in your tablet.) adb install  'apk file'       :: It will install an apk to the tablet.   This apk must be located in the same folder where the adb is. adb uninstall 'apk file' :: It will uninstall an apk adb pull 'file'                                               :: It copies a file or directory (and sub-directories) from your device to the PC. adb push 'file'                          :: It copies a file of directory (and sub-directories) from your PC to the device. adb logcat                        :: Prints the logdata to the screen adb logcat –c                  :: Clears the buffer to remove any old log data. adb bugreport               :: Prints dumpsys, dumpstate and logcat. adb shell pm list packages –f    ::  List all installed packages adb shell input keyevent 26     :: Send the power button event to turn on/off the device adb shell screencap –p /sdcard/screen.png      :: Takes a screenshot of the android display adb shell screenrecord /sdcard/demo.mp4      :: Records any activity on the android display Using the window manager There is also a very useful tool to manage the display. This can be ran through a terminal connection to your board. You run this command from the following path /system/bin of your android BSP These are some of the commands available: wm density 'density number'              :: Changes the display density wm size 'display size'                                :: Changes your display’s resolution Using the activity manager In the same path is the activity manager which has several other commands for use: am start 'package'   :: Starts an activity am monitor                     :: Monitors activities am bug-report               :: Requests a bug report am restart                        :: Restarts the OS
查看全文
What is HOB? Hob is a graphical user interface for BitBake. Its primary goal is to enable a user to perform common tasks more easily. It basically runs the Bitbake commands on the background while showing a Graphic User Interface. Hob may not work correctly with Daisy metadata as it is getting deprecated in favor of a new web based interface for Yocto under the name Toaster. Here is what you can do with the current version of Hob on the Freescale Community BSP and BSP Release. - Build images - Edit existing image recipes - Create your own image recipes Note: HOB will write the local.conf file and make modifications which may conflict with baking images outside of HOB. In this case you may need to re-run the environment initialization in order to restore the local.conf file. Starting HOB Once the environment has been initialized (using the setup-environment script on the Freescale Community BSP or the fsl-setup-release on the Freescale BSP Release) use the command below. $ hob & The GUI should then appear: You may then select the MACHINE for which you will build and the Layers of your project. HOB  will take and updated the local.conf and bblayers.conf values so the desired BSP layers will already be selected and available MACHINES on these layers will appear on the drop down menu. Once these options are set HOB will parse the recipes and create a dependency tree in order to show available images for that MACHINE. Image File System Types Advance configuration options include image file system types. Please note that HOB does not support the sdcard format so if it is needed it has to be added manually on the local.conf file and then run bitbake outside of HOB. As HOB changed the local.conf file even if the sdcard format was originally available it may be rewrite and no longer available until the following line is added to local.conf. IMAGE_FSTYPES="tar.bz2 ext3 sdcard" Recipes screen On the recipes screen we can see the recipes included on the image and available recipes, then also package groups. Time to bake! After these configurations you may either build the packages using HOB interface or run Bitbake outside of HOB. (In case you wish to have your image on the sdcard format please see the earlier image types clarification) The resulting image will be stored on <BUILD>/tmp/deploy/images/<MACHINE> You may also save your image recipe with the selected customizations.
查看全文
This document explains how to create a DS-5 project to compile and debug the SDK and OBDS for iMX6 and iMX28 respectively. Attached you can find the .ds file for the iMX28 needed to debug in DS-5.
查看全文
This is a tool can generate a DDR3 script easily for i.MX53 and only need input several parameters based on using DDR datasheet and system architecture. Please find i.Mx6DQSDL DDR3 Script Aid through below link. i.Mx6DQSDL DDR3 Script Aid Please find i.Mx6DQSDL LPDDR2 Script Aid through below link. i.Mx6DQSDL LPDDR2 Script Aid Please find i.Mx6SL LPDDR2 Script Aid through below link. i.Mx6SL LPDDR2 Script Aid Any questions are welcome!
查看全文
Most common issues with bringup and memory stability come down to memory/system setup during startup phase of i.MX device.   This Python script allows you to dump IVT/DCD tables and data from a i.MX binary (either generated as result of build process or a simple dump of SD/NOR/NAND... content) and analyze them in an easier way. Should work with i.MX 6 and i.MX53 binaries.   Parser for i.MX 6 will also try to print out register values it recognizes, and also parse specific register fields, helping to analyze the data faster. This can be extended if needed to other registers/values.   imxbin.py works with Python3.x and imxbin_2x.py with Python 2.x, so choose appropriate version.   Vladan
查看全文
When working on the IOMUX settings of an i.MX processor for our design it’s always good to make use of the IOMUX Tool provided by Freescale on the Download Page of most i.MX processors. We’ll focus on the latest release of the IOMUX tool for i.MX6. The IOMUX tool provides a Graphic User Interface to easily assign internal signals to external pins/balls and resolve any potential pin conflict and muxing options for the different modules available on the i.MX processors. IOMUX Tool Download (Will request to log in) Freescale’s Boards IOMUX settings. On the IOMUX tool package you’ll find the User’s Manual and also a folder containing the muxing options for Freescale’s Reference Boards, which may be of help when working with the Reference Designs as a starting point. You may load these settings files using the file/open option. MMDC pins Since the Multi-mode DDR controller MMDC pins are not muxed these cannot be changed on the IOMUX tool. This because the memory interfaces are much more sensitive to interference and thus have dedicated pins that do not share pad with other signals. The registers are also set on the default value so it’s good to keep this in mind when working with the code provided by the IOMUX tool. Considerations when using generated code The tool can generate code to be used as reference of the IOMUX configuration but still requires manual tweaking and the header files available on the i.MX Processor’s BSP in order to be implemented in an actual application code. It’s important to review the register settings on the Register tab in order to export the desired values; otherwise the code will have the default values for the registers according to the IOMUX tool. This is especially true for the Daisy Chain settings, always manually review these. Import function limitations There is an import function available so IOMUX configuration files saved in previous versions of the IOMUX tool can be loaded on the newest version. However, this feature should be used carefully. When importing a design it’s recommended to save the imported design on the new version of the IOMUX tool as imported.xml; then opening a new configuration and saving it as new.xml and comparing register value differences to manually correct the imported.xml values. In small projects it might be recommended to manually load the IOMUX information on the new IOMUX tool version to avoid register conflicts from version to version. For more information please refer to the documentation available within the IOMUX tool package. An advanced example is also included in that document.
查看全文
Whenever possible is always better to avoid Virtual Machines when compiling Android as the building process might take several hours to even a day or two depending on the resources available to the Virtual Machine. Sometimes, however, a VM is the only option available and here are some useful considerations when using a VM as a host for Android builds. This document addresses some of the requirements for the Kit-Kat Freescale Android BSP although some may also apply to the general Android releases. It’s recommended to use Ubuntu 12.04 64-bits as Host OS. As for HDD space, which is often a limited resource when using VM, Google states that at least 30GB of disk space in order to build the Android Tree. In practice, however, it’s recommended to allocate at least 100GB to the VM HDD if possible, as additional packages and larger images can quickly deplete disk space. Installing Java (not VM specific) It’s recommended (albeit not mandatory) to uninstall any version of Java other than the recommended for the specific Android release for which we will build. In the case of Kit-Kat this is Java 6. Another option is to just switch the java alternatives to the ones we want to use for Android. There is a document with the exact instructions on how to install the required JKD on the following link. How to install Sun's JDK in Ubuntu for Android build Starting KitKat, however, it’s also necessary to install javap (Java Class File Dissasembler) so please also add these steps when following this document. $ sudo update-alternatives --install /usr/bin/javac javac /usr/lib/jvm/jdk1.6.0_45/bin/javac 1 $ sudo update-alternatives --config javac Memory considerations when using a Virtual Machine Using a Virtual Machine slows down the image building considerably. Besides that memory system is often also an issue. Having insufficient RAM especially on the linking part of the image build may cause a number of issues that are difficult to troubleshoot. In these cases it’s good to take a look at the resource monitor to see if indeed the RAM was depleted. One way to make up for the limited RAM is using a bigger swap. Google recommends at least 16GB of RAM/swap so it’s not uncommon to create a 10GB swap when working in VM, to do this please use the following commands. $ sudo fallocate -l 10g /mnt/10GB.swap $ sudo chmod 600 /mnt/10GB.swap $ sudo mkswap /mnt/10GB.swap $ sudo swapon /mnt/10GB.swap This will helps with the memory requirements but won’t speed up the build process. Building time with VM, as previously stated, will take several hours or even a couple of days depending on computing power.
查看全文