i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
For default Android JB4.3 GA1.1.0 BSP, iMX6SL EVK board doesn't support BlueTooth, attached is the patch for the BSP to support AR3002 bluetooth.   The hardware information can be found at: https://community.freescale.com/docs/DOC-95016   iMX6SL_EVK_BlueTooth_Patch_for_JB4.3_1.1.0.tar.gz: these are the patch files. iMX6SL_EVK_BlueTooth_Support_for_JB4.3_1.1.0.tar.gz: these are the patched source code files. Please select one of above to use.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344336 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342059 
View full article
Setting the host          1 - Install NFS Service on host typing: your slackware linux probably already have a version of nfs"utils installed, but if it doesn't you can get it downloading the nfs-utils from:  [1] then as root:  #installpkg nfs-utils-1.0.7-i386-1.tgz 2 - Setup exports typing: $sudo kedit /etc/exports          and add the following line: /tftpboot/ltib/ *(rw,no_root_squash,async)          3 - Restart the NFS server: $sudo /etc/rc.d/rc.rpc restart $sudo /etc/rc.d/rc.nfsd restart          Now the host is ready to use NFS.      Setting Target Linux Image to use NFS          1 - Run LTIB configuration typing: $./ltib -c 2 - On first page menu, go to "Target Image Generation -> Options".               3 - Select the option NFS only and exit LTIB configuration to compile with the new configuration.          4 - LTIB should start new compiling and create a new Linux image on /<ltib instalation folder>/rootfs/boot/zImage         5 - Copy the created image on /<ltib instalation folder>/rootfs/boot/zImage to /tftpboot/zImage 6 - The system is ready to run with NFS. The root file system on target will be located on host on /<ltib instalation folder>/rootfs/                           
View full article
What is HTML5 Video? HTML5 video is an element for the purpose of playing videos or movies in HTML5 specification. HTML5 video is intended by its creators to become the new standard way to show video on the web without plugins. Video will be shown inside the web page, like flash. HTML5 Video Web Page <video> element example <video src="movie.mp4" poster="movie.jpg" controls> </video> HTML5 video page source example <html>           <head>           </head>            <body>                      <video src="http://10.192.225.226/movie.mp4" width="640" height="480"  controls="true">                      </video>            </body> </html> HTML5 Video Rendering Path Performance Data in i.MX6Q with Android ICS With LVDS display, H264@1080p@20Mbps Can reach 30 fps With HDMI 1080p display, H264@1080p@10Mbps Can reach 25 fps HTML5 Video Website Some HTML5 Video website when accessing with android platform www.youtube.com www.iqiyi.com HTML5 reference document SPEC         http://dev.w3.org/html5/spec/single-page.html?utm_source=dlvr.it&utm_medium=feed Wikipedia page        http://en.wikipedia.org/wiki/HTML5
View full article
This example uses the touchscreen that comes with i.MX51 EVK's parallel LCD Download xserver-xorg-input-evtouch (xserver-xorg-input-evtouch_0.8.8-3build1_armel.deb) from https://launchpad.net/ubuntu/lucid/armel/xserver-xorg-input-evtouch/0.8.8-3build1 On i.MX51 EVK board, run “sudo dpkg –i xserver-xorg-input-evtouch_0.8.8-3build1_armel.deb” to install debian package. Remove evdev config file: sudo rm /usr/lib/X11/xorg.conf.d/05-evdev.conf Change the content of 10-evtouch.conf to: sudo vi /usr/lib/X11/xorg.conf.d/10-evtouch.conf Section "InputClass"            Identifier "touchscreen catchall"            MatchIsTouchscreen "on"            Driver "evtouch"            Option "SwapY" "1"            Option "MinX" "32"            Option "MinY" "46"            Option "MaxX" "1001"            Option "MaxY" "967" EndSection   The MinX, MinY, MaxX and MaxY values can be changed to match the exact configuration of your touchscreen Save above configuration and reboot the system.
View full article
The article has just been published by EDN website, under “Design Center” and “BBS” channels. Here is the coverage: 如何灵活使用飞思卡尔i.MX应用处理器的GPIO http://bbs.ednchina.com/FORUM_POST_30_529551_0.HTM http://www.ednchina.com/ART_8800518371_15_20034_AN_20f46fd3.HTM Title translation: How to easily use the GPIO of Freescale i.MX processors. If you are interested in the post and would like to have reply in English, please contact the owner of this post.
View full article
Issue description: ZQ calibration issue with LPDDR2 memory with two chip selects    Micron has verified it on my customer's board with i.MX6Q. (ECT-SYT-1163 for FIC.pdf) The patch is made based on lp 5.1, see attachment.
View full article
In order to get USB cameras (web cams) working on i.MX 51 EVK board running Ubuntu, a few steps must be followed, and they are: Enable USB Camera's drivers on Kernel Test it using Gstreamer or another compatible software (as Cheese) Kernel Driver USB cameras (web cameras) on Linux work over GSPCA driver, to enable this driver you need to go to: ./ltib -c   [*] Configure the kernel     Device Drivers -->          Multimedia Devices -->               [*] Video Capture Adapters -->                    [*] V4L USB Devices -->                         <*> USB Video Class (UVC)                                      [*] UVC input events device support                         <*> GSPCA Based WebCams --> From this point, you need to choose your specific driver. If you don't know, you can select all of those options as a built-in module "<*>" that will work. GSPCA Drivers USB Camera Detection Connect your USB camera to the USB Host port on i.MX 51 EVK board and then type "dmesg", and also check if there is a video0 device using: ubuntu@ubuntu-desktop:~$ ls /dev/video0 /dev/video0 USB Camera Detection Gstreamer Command Line In order to test your USB camera using Gstreamer plugin, use the following command line to perform it: ubuntu@ubuntu-desktop:~$ gst-launch-0.10 v4l2src ! ffmpegcolorspace ! ximagesink and the results: Hi there !!! EOF !
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343344 
View full article
Question: What is minimum requirement for VDDSNVS_IN voltage to keep RTC timing info in SNVS block? In the datasheet, there is requirement for VDDSNVS_IN input and it is 2.9V to 3.3V. Is it recommended requirement for RTC operation? Other security function is not used in SNVS and just interested in basic RTC fuction after power off. Answer: The finall answer is tha to folow our datasheet saying for no matter if you are only RTC keeping application. "The SNVS regulator takes the SNVS_IN supply and generates the SNVS_CAP supply which powers the real time clock and SNVS blocks. If  VDDHIGH_IN is present, then the SNVS_IN supply is internally shorted to the VDDHIGH_IN supply to allow coin cell recharging if necessary. The output voltage is roughly one third(1/3) of SNVS_IN. -- in the SNVS_CAP powered on-chip logics, need min 0.9v for normal operation, we can only guarantee the operation in this condition, whih means min SNVS_IN = 3*SNVS_CAP = around 2.7. with some margin, so min 2.8v is the requireent. Again, we can only guarantee the operation in this condition(VDD_SNVS_CAP >0.9v). The datasheet is correct : VDDSNVS_IN must not be less than 2.8 V (Table 6. Operating Ranges, of IMX6DQCEC,  Rev. 2.2, 07/2013 )  I guess you talked about operating condition in ON mode. In case of OFF mode, VSNVS output of PFUZE depends on LICELL input power and usually coincell can supply under 2.5V output. According to PFUZE spec, VSNVS output in OFF mode is under 1.8V. And as I know, LP (low power) part of SNVS is only operation al in OFF mode so I don't think VDDSNVS_IN requires over 3V in that condition. In my assumption, SNVS can maintain itis data and RTC if VDDSNVS_IN is over 1.1 ~ 1.3V in OFF mode but I just want to know what is our spec for it. If we consider low power modes of the i.MX6, then - according to Table 10 (Stop Mode Current and Power Consumption) of IMX6DQCEC, Rev. 2.3, 07/2013 (for example) - in "SNVS Only" mode VDD_SNVS_IN of 2.8V is considered. Here 2.8 V is taken as minimal value. At least, as we can see, there are no other specifications.
View full article
U-boot expects uImage format for the kernel image. In order for LTIB to generate a uImage file: $ export SYSCFG_KTARG=uImage $ ./ltib -p kernel Setup in U-Boot the kernel bootargs: u-boot> setenv bootargs noinitrd console=ttymxc0,115200 init=/linuxrc root=/dev/nfs nfsroot=10.29.244.27:/tftpboot/rootfs ip=dhcp Change 10.29.244.27 to your host IP. The procedure above is needed when default bootloader used by ltib was redboot. In some ltib releases (before 2010) default bootloader is u-boot. In this case, ltib will create uImage by default
View full article
About softISP Code : https://github.com/NXPmicro/gtec-demo-framework/tree/master/DemoApps/OpenCL/SoftISP/source Document : https://www.nxp.com/docs/en/application-note/AN12060.pdf demo is on path  /opt/imx-gpu-sdk/OpenCL/SoftISP of linux L4.19.35   About eIQ Community: https://community.nxp.com/community/eiq eIQ sample APPs : https://community.nxp.com/docs/DOC-343785 eIQ library source code : https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/meta-ml/recipes-libraries?h=warrior-4.19.35-1.1.0
View full article
On customer design, they may need to fine tune LVDS driver strength for different case, for example, PCB impedance does not match, or the value of terminal resistor in panel side is lower or bigger. In IMX8MPRM.pdf, it has reg for this feature:         LVDS is constant current source, when voltage on terminal or panel side is lower than spec, you need to increase output current to get higher voltage to meet spec. otherwise ,you need to reduce it There is no detail description for these bits, pls refer to below: CC_ADJ = 000b => 3.5mA as default CC_ADJ = 001b => 3.5mA + 0.215mA x 1 CC_ADJ = 010b => 3.5mA + 0.215mA x 2 CC_ADJ = 011b => 3.5mA + 0.215mA x 4 CC_ADJ = 100b => 3.5mA - 0.215mA x 4 CC_ADJ = 101b => 3.5mA - 0.215mA x 3 CC_ADJ = 110b => 3.5mA - 0.215mA x 2 CC_ADJ = 111b => 3.5mA - 0.215mA x 1   Thanks, Lambert
View full article
This patch implements (or exposes) routines to poll the imx uarts. The KGDB drivers need these methods to be implemented or the ttymxc driver is not sufficient. The synthetic CONFIG_CONSOLE_POLL value activates these routines (or CONFIG_SERIAL_MXC_CONSOLE for the polled write). There is still no poll routines in -855-ge067785, which is the September 2010 Linux release from Freescale. Also not in Linux 2.6.36 drivers/serial/imx.c either. $ git diff drivers/serial/mxc_uart.c diff --git a/drivers/serial/mxc_uart.c b/drivers/serial/mxc_uart.c index ae6d2e1..728b607 100644 --- a/drivers/serial/mxc_uart.c +++ b/drivers/serial/mxc_uart.c @@ -1551,6 +1551,28 @@ mxcuart_pm(struct uart_port *port, unsigned int state, unsigned int oldstate)                             clk_enable(umxc->clk);    }  +#ifdef CONFIG_CONSOLE_POLL +/* + * Read a character from the UART. + */ +static inline int mxcuart_console_read_char(struct uart_port *port) +{ +       volatile unsigned int status; +    int ch; + +       do { +               status = readl(port->membase + MXC_UARTUSR2); +       } while ((status & MXC_UARTUSR2_RDR) == 0); +       ch = readl(port->membase + MXC_UARTURXD); +/* Ignore parity errors, etc. */ +/*  status = ch | UART_CREAD_BIT; */ +    ch &= 0xff; + +    return ch; +} +static void mxcuart_console_write_char(struct uart_port *port, char ch); +#endif +    /*!     * This structure contains the pointers to the control functions that are     * invoked by the core serial driver to access the UART hardware. The @@ -1575,14 +1597,18 @@ static struct uart_ops mxc_ops = {                 .config_port = mxcuart_config_port,                 .verify_port = mxcuart_verify_port,                 .send_xchar = mxcuart_send_xchar, +#ifdef CONFIG_CONSOLE_POLL +              .poll_put_char = mxcuart_console_write_char, +              .poll_get_char = mxcuart_console_read_char, +#endif };  -#ifdef CONFIG_SERIAL_MXC_CONSOLE +#if defined(CONFIG_SERIAL_MXC_CONSOLE) || defined (CONFIG_CONSOLE_POLL)     /*     * Write out a character once the UART is ready     */ -static inline void mxcuart_console_write_char(struct uart_port *port, char ch) +static void mxcuart_console_write_char(struct uart_port *port, char ch)    {            volatile unsigned int status;  @@ -1592,6 +1618,10 @@ static inline void mxcuart_console_write_char(struct uart_port *port, char ch)                writel(ch, port->membase + MXC_UARTUTXD);     }  +#endif + +#ifdef CONFIG_SERIAL_MXC_CONSOLE +    /*!     * This function is called to write the console messages through the UART port.     *
View full article
Harware: - i.MX7D-SDB board - QCA9880 card with MINI PCIe Interface The Wifi module is connected to the PCIe slot on the board.     Software: - Ubuntu 18.04 LTS Host - L4.19.35_1.1.0 BSP   Tool: - uuu 1.2.68 for linux (run on ubuntu host)   Toolchain: - The toolchain can be obtained from the Yocto BSP. Please read and follow the steps in i.MX_Yocto_Project_User's_Guide to build the BSP and then read the Chapter of "How to build U-Boot and Kernel in standalone environment" in i.MX_Linux_User's_Guide to build the toolchain.   Build the Kernel: # mkdir imx_build # cd imx_build # git clone https://source.codeaurora.org/external/imx/linux-imx -b imx_4.19.35_1.1.0 # cd linux-imx # source /opt/fsl-imx-fb/4.19-warrior/imx6/environment-setup-cortexa9hf-neon-poky-linux-gnueabi # export ARCH=arm # make clean # make imx_v7_defconfig # make menuconfig - Select the PCIe driver and the Wifi support - PCI controller drivers--->                    DesignWare PCI Core Support----> - Networking support----->                             Wireless----->   - Select the ath10 driver (it supports QCA988X) Device Drivers---->             Network device support----->                                      Wirless LAN----> - Save and Exit. - Add the firmware in the .config file: Get the firmware file (e.g. firmware-2.bin) from your wifi vendor or download it from the web. Put the firmware in linux-imx/firmware/ folder. Edit the .config file and add these two lines: CONFIG_EXTRA_FIRMWARE="board.bin firmware-2.bin" CONFIG_EXTRA_FIRMWARE_DIR="/home/jimmy/imx_build/linux-imx/firmware" - Build the kernel # make Then the zImage will be obtained in arch/arm/boot.   Using uuu to program the SD card: - Downloading demo image of L4.19.35_1.10 from the nxp website. - Copy the zImage to the directory - Copy the uuu (V1.2.68) to the directory - Copy the samples/example_kernel_emmc.uuu to imx7d_kernel_emmc.uuu - Modify the image the imx7d_kernel_emmc.uuu - In the demo image, you will see the files like this: - run uuu and the script to program the images.   Wifi driver loaded and wlan0 is up: # dmesg | grep pci   # ifconfig -a   Reference Document: - i.MX_Linux_User's_Guide.pdf - i.MX_Porting_Guide.pdf  
View full article
Q: MX53 u-boot doc to enable the splash screen and went through Re: MX53 u-boot Splash Screen support but I can't seem to get the splash working on the VGA output.  A: FSL do not have solution / recommendations for VGA splash screen under U-boot. Only LVDS is supported. Typically, the Uboot bootloader does not interact with any display interface and does not have a splash screen displaying capability. To add this feature to Uboot on i.MX5 platform, the IPU driver should be included into the Uboot code. Looks like we do not have ready to use solution for the LCD. As an example for LCD configuring it makes sense to use LCD settings from Linux driver. Another approach - to use Linux (Penguin) logo (assuming Linux is booted quickly after U-boot) - at least, Linux supports more display drivers and its logo using is specified. follow up question is since the Tux the penguin logo is only 80x80 is it possible to make a larger image for the Linux start up logo? yes, you should configure kernel for the new image on make menuconfig That doesn’t help this H/W guy, but I think this may - https://community.freescale.com/thread/304300    look for  “#To change the splash screen of linux kernel (small penguine on top left corner)..“
View full article
Freescale introduces the i.MXS Development Kit, a high performance development kit ideal for Microsoft's Windows Vista™ SideShow™ platform and .NET Micro Framework applications. The advanced i.MXS Development Kit leverages Freescale's i.MXS applications processor, based on the ARM920T™ core, a highly integrated IC that has been in production for nearly two years. The integrated development platform, featuring support of Microsoft's .NET Micro Framework for use with SideShow applications, is designed to enable hardware developers to more quickly and easily design applications targeting Microsoft's highly anticipated Windows Vista operating system. Typical SideShow applications include laptop external displays, remote controls and USB dongles, which can run certain applications without powering up the laptop. The i.MXS Development Kit features a small form-factor reference board that has a 2.5 inch color LCD panel with QVGA resolution. The card includes Freescale’s i.MXS applications processor that provides superb performance and extremely low power consumption, enabling hours of use off a single battery charge. The development kit also includes a USB interface and an expansion connector for add-on modules such as Bluetooth™ technology or the ZigBee™ wireless protocol, creating a comprehensive development platform for a variety of applications. Features i.MXS applications processor, based on the powerful ARM920T™ core Clock source crystal: 32 kilohertz Powered by USB bus voltage or external power adaptor Multi-ICE debug support connector I2C and SSI bus connector for connection to external audio CODEC SMbus interface 32-megabyte (MB) SDRAM device One 8-megabyte (MB) Burst Flash memory device One RS232 transceiver (configured for DCE) supporting on-chip UART1 port 1 UART port at CMOS level for expansion On-Chip USB 1.1 interface On-board 2.5 inch LCD with back-light and QVGA resolution 11 separated GPIO for key-button input LED indicator for power
View full article
We are pleased to announce that Config Tools for i.MX v13.1 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes 13.1 DDR tool     - i.MX93 support for A0 pre-production launch; sync with SW BSP release Pins tool     - Fix incomplete routing of deinit functions  
View full article
     The following steps allow you to toggle a pin on i.MX 8M Mini EVK, you can use the EVK as not gate, trigger a wake up signal, etc. With an script and modifying the device tree you can read an input and get as output the invert input.   On the Host.   Cloning the Linux kernel repository.   Clone the i.MX Linux Kernel repo to the home directory. cd ~ git clone -b lf-5.10.72-2.2.0 https://source.codeaurora.org/external/imx/linux-imx cd linux-imx/   Patching the device tree.   Open the imx8mm-evk.dtsi file: vim arch/arm64/boot/dts/freescale/imx8mm-evk.dtsi For the purpose of this example, uart3 has to be "disabled" in order to avoid pins conflict, so change "okay" to "disabled": &uart3 {        pinctrl-names = "default";        pinctrl-0 = <&pinctrl_uart3>;        assigned-clocks = <&clk IMX8MM_CLK_UART3>;        assigned-clock-parents = <&clk IMX8MM_SYS_PLL1_80M>;        fsl,uart-has-rtscts;        status = "disabled"; }; Add the following lines in the iomuxc node: &iomuxc {       pinctrl-names = "default";       pinctrl-0 = <&pinctrl_hog>; ​       pinctrl_hog: hoggrp {               fsl,pins = <                       MX8MM_IOMUXC_ECSPI1_SS0_GPIO5_IO9               0x19                       MX8MM_IOMUXC_ECSPI1_MISO_GPIO5_IO8              0x19               >;       };   Build the device tree.   Setup your toolchain, for example: source /opt/fsl-imx-wayland/5.10-hardknott/environment-setup-cortexa53-crypto-poky-linux Generate config file. make imx_v8_defconfig Compile the device tree. make freescale/imx8mm-evk.dtb Copy the .dtb file to the EVK, for example with scp: scp imx8mm-evk.dtb root@<EVK_IP>:/home/root Alternatively, you may copy the .dtb file directly to the FAT32 partition where the Kernel and Device Tree files are located.   On the EVK Board.   Switching the device tree.   To copy the updated device tree to the corresponding partition, first create a directory. mkdir Partition_1 Mount the partition one. mount /dev/mmcblk1p1 Partition_1/ Copy or move the device tree into partition one. cp imx8mm-evk.dtb Partition_1/ Reboot the board. reboot   Create an script.   Use vi: vi toggle.sh Add the following lines: #!/bin/bash ​ echo 136 > /sys/class/gpio/export echo in > /sys/class/gpio/gpio136/direction ​ echo 137 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio137/direction echo 0 > /sys/class/gpio/gpio137/value ​ while : do ​ if [[($(cat /sys/class/gpio/gpio136/value) == "0")]]; then         echo 1 > /sys/class/gpio/gpio137/value else         echo 0 > /sys/class/gpio/gpio137/value        fi ​ done Save the file: :wq Change file permissions: chmod +x toggle.sh   Toggling a pin.   In this example we are using the pin "UART3_CTS" like an input and "UART3_RTS" like an output. To toggle the pin, run the script: ./toggle.sh
View full article