i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
The attached patches slow-down the DDR's clock (from 528000000Hz to 396000000Hz) on i.MX6Q Sabre SDB-P boards. These were tested on Android JB4.2.2_1.0.0 and Linux L3.0.35_4.1.0. To verify patches were correctly applied, one the serial console one should see the following TWO bold lines Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ] Boot Device: MMC I2C:   ready DRAM:   1 GB MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3 *** Warning - bad CRC or MMC, using default environment mx6q pll1: 792MHz mx6q pll2: 528MHz mx6q pll3: 480MHz mx6q pll8: 50MHz ipg clock     : 49500000Hz ipg per clock : 49500000Hz uart clock    : 80000000Hz cspi clock    : 60000000Hz ahb clock     : 99000000Hz axi clock   : 198000000Hz emi_slow clock: 99000000Hz ddr clock     : 396000000Hz usdhc1 clock  : 198000000Hz usdhc2 clock  : 198000000Hz usdhc3 clock  : 198000000Hz usdhc4 clock  : 198000000Hz nfc clock     : 24000000Hz In:    serial Out:   serial Err:   serial Found PFUZE100! deviceid=10,revid=10 Net:   got MAC address from IIM: 00:04:9f:02:67:46 FEC0 [PRIME] Hit any key to stop autoboot:  0 kernel   @ 10808000 (4709060) ramdisk  @ 11800000 (183100) kernel cmdline:     use boot.img command line:     console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale Starting kernel ... Uncompressing Linux... done, booting the kernel. . . . sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms Set periph_clk's parent to pll2_pfd_400! arm_max_freq=1.2GHz . . .
View full article
This article describe some bring up tips during i.MX95 board debug, including HW and SW aspects.  
View full article
Overview The purpose of this document is to describe how to enable 3G modem in i.MX sabresx board for Android software. Hardware Changes Unlike other boards of I.mx series, in sabresx board  3G modem doesn't share to use PCIE slot any longer. It is not connected with PCIE slot by default. So if you still want to use 3G modem like in sabresd board. You need to do a tiny hardware rework. Like the below, R177 and R178 is DNP. Just add a zero resistor here. Software patches After you have do hardware rework above, then you should git am the attached patch to add software support which will add the dts config of 3G power. In our official release version, we don't include this patch.
View full article
Some of SDIO cards need SD clock active for 4-bit mode, in order to generate interrupt. But i.MX6 SD controller enables SD clock gated by default, the attached patch is an example to disable SD clock gated. It's able to check if clock gated is enable or not by the register, "uSDHCx_PRES_STATE:SDOFF", of SD controller.
View full article
The default FSL android BSP support 1 SD card slot. If customer need to support more sd slot in android.Please reference below steps. There are two steps need to set up. 1 device/fsl.git NOTE: 1  change the fstab. 2194000 is the address of usdhc2.             2  change the mount point in storage_list.xml diff --git a/sabresd_6dq/fstab.freescale b/sabresd_6dq/fstab.freescale index 7f23edb..1529a27 100644 --- a/sabresd_6dq/fstab.freescale +++ b/sabresd_6dq/fstab.freescale @@ -4,6 +4,7 @@ # specify MF_CHECK, and must come before any filesystems that do specify MF_CHECK /devices/soc0/soc.0/2100000.aips-bus/2198000.usdhc/mmc_host /mnt/media_rw/extsd vfat defaults voldmanaged=extsd:auto +/devices/soc0/soc.0/2100000.aips-bus/2194000.usdhc/mmc_host /mnt/media_rw/extsd_expand vfat defaults voldmanaged=extsd_expand:auto /devices/soc0/soc.0/2100000.aips-bus/2184000.usb/ci_hdrc.0  /mnt/media_rw/udisk vfat defaults voldmanaged=udisk:auto /dev/block/mmcblk3p5    /system      ext4    ro,barrier=1                                                                               wait,verify /dev/block/mmcblk3p4    /data        ext4    nosuid,nodev,nodiratime,noatime,nomblk_io_submit,noauto_da_alloc,errors=panic    wait,encryptable=/dev/block/mmcblk3p9 diff --git a/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml b/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml index 3639bdc..c3f5105 100644 --- a/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml +++ b/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml @@ -41,6 +41,10 @@               android:storageDescription="@string/storage_sd_card"               android:primary="false"               android:removable="true" /> +    <storage android:mountPoint="/storage/extsd_expand" +             android:storageDescription="@string/storage_sd_card" +             android:primary="false" +             android:removable="true" />      <storage android:mountPoint="/storage/udisk" 2  system/core.git NOTE: mkdir the mount point. build@scmbld2:~/maddev_lp5.1_consolidate_ga_10_30/system/core/rootdir$ git diff diff --git a/rootdir/init.rc b/rootdir/init.rc index 2211cc2..fac37c2 100644 --- a/rootdir/init.rc +++ b/rootdir/init.rc @@ -72,7 +72,9 @@ on init      mkdir /storage 0751 root sdcard_r      mkdir /mnt/media_rw/extsd 0755 system system +    mkdir /mnt/media_rw/extsd_expand 0755 system system      symlink /mnt/media_rw/extsd /storage/extsd +    symlink /mnt/media_rw/extsd_expand /storage/extsd_expand      mkdir /mnt/media_rw/udisk 0755 system system
View full article
Compiling kernel module qca9377 in new bsp L5.10.9 has lots of errors.This is because lots of kernel apis has been dropped or changed from kernel5.4 to kernel5.10.But kernel module QCA9377 still using old api.So i fixed this compile errors and attach this patch.
View full article
   Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of Tsinghua University. Customers in other areas can refer to the configurations of ubuntu 18.04 in the document. Updating software packages for ubuntu18.04 LTS 1、Using software updater to update software packages Press Install Now button to update software. Restart ubuntu18.04 2、Installing necessary software packages #sudo apt-get install flex # sudo apt-get install bison # sudo apt-get install gperf # sudo apt-get install build-essential # sudo apt-get install zlib1g-dev # sudo apt-get install lib32ncurses5-dev # sudo apt-get install x11proto-core-dev # sudo apt-get install libx11-dev # sudo apt-get install lib32z1-dev # sudo apt-get install libgl1-mesa-dev # sudo apt-get install tofrodos # sudo apt-get install python-markdown # sudo apt-get install libxml2-utils # sudo apt-get install xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 # sudo apt-get install gcc-multilib g++-multilib # sudo apt-get install subversion # sudo apt-get install openssh-server openssh-client # sudo apt-get install uuid uuid-dev # sudo apt-get install zlib1g-dev liblz-dev # sudo apt-get install liblzo2-2 liblzo2-dev # sudo apt-get install lzop # sudo apt-get install git-core curl # sudo apt-get install u-boot-tools # sudo apt-get install mtd-utils # sudo apt-get install android-tools-fsutils # sudo apt-get install openjdk-8-jdk # sudo apt-get install device-tree-compiler # sudo apt-get install aptitude # sudo aptitude install libcurl4-openssl-dev nss-updatedb 3、Downloading and unpacking Android release package https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applications-processors/android-os-for-i.mx-applications-processors:IMXANDROID?tab=Design_Tools_Tab --O8.1.0_1.3.0_ANDROID_SOURCE_8MQ_GA File name is imx-o8.1.0_1.3.0_8m.tar.gz # cd ~ # tar xzvf imx-o8.1.0_1.3.0_8m.tar.gz Downloading android8.1.0-1.3.0 source code Getting repo # cd ~ # mkdir bin # cd bin # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin   Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL = 'https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/' 3、Setting email address # git config --global user.email "[email protected]" # git config --global user.name "xxxx" [ Email & Name should be yours] 4、Modifying android setup script and Running it Open ~/ imx-o8.1.0_1.3.0_8m /imx_android_setup.sh and add a line like below: ...       if [ "$rc" != 0 ]; then          echo "---------------------------------------------------"          echo "-----Repo Init failure"          echo "---------------------------------------------------"          return 1       fi find -name 'aosp-O8.1.0-1.3.0.xml'| xargs perl -pi -e 's|https://android.googlesource.com/|https://aosp.tuna.tsinghua.edu.cn/|g' fi   # Don't Delete .repo directory and hidden files #rm -rf $android_builddir/.??* ... Then save it and exit. # cd ~/ # source ~/ imx-o8.1.0_1.3.0_8m/imx_android_setup.sh Then android_build directory is created at ~/ # export MY_ANDROID=~/android_build          48 hours later: Compiling android8.1.0-1.3.0 BSP # cd ~/android_build # gedit ./prebuilts/sdk/tools/jack-admin               And find “JACK_SERVER_COMMAND” ,change it to be: JACK_SERVER_COMMAND="java -XX:MaxJavaStackTraceDepth=-1 -Djava.io.tmpdir=$TMPDIR $JACK_SERVER_VM_ARGUMENTS -Xmx4096m -cp $LAUNCHER_JAR $LAUNCHER_NAME"          Save and exit. And run: # ./prebuilts/sdk/tools/jack-admin stop-server # ./prebuilts/sdk/tools/jack-admin start-server # export ARCH=arm64 # export CROSS_COMPILE=~/android_build/prebuilts/gcc/linux-x86/aarch64/aarch64-linuxandroid-4.9/bin/aarch64-linux-android- # export LC_ALL=C # source build/envsetup.sh # lunch evk_8mq-userdebug               Begin to build android BSP for i.MX8MQ # make –j4 NXP TIC weidong sun 2018-08-15
View full article
The ARD has the VGA output hw multiplexed with the on board Eth controlling, on jumpers J14 and J16. If using the VGA out one option for network is to use an USB/Eth adapter. To enable this (tested on BSP 11.05 - 2.6.35): 1. Find out the driver for the adapter you are using. You can connect it to your Linux host for that. $ lsusb ... Bus 002 Device 017: ID 0b95:772a ASIX Electronics Corp. ... $ dmesg | tail ... [3799653.662846] eth2: register 'asix' at usb-0000:00:1d.7-2, ASIX AX88772 USB 2.0 Ethernet, 00:60:6e:00:02:7a ... 2. Enable the driver on the target's kernel: - ./ltib -c - On Ltib menu, select "[*] Configure the Kernel" - On the kernel menuconfig select the driver, in this case: CONFIG_USB_NET_AX8817X located at: -> Device Drivers                                                       -> Network device support (NETDEVICES [=y])         -> USB Network Adapters             -> Multi-purpose USB Networking Framework (USB_USBNET [=y]) 3. Program the kernel to SD: sudo dd if=rootfs/boot/uImage of=/dev/sdd bs=512 seek=2k 4. Set U-boot to load the kernel from the SD and NFS: MX53-ARD-DDR3 U-Boot > set bootcmd 'run bootcmd_sd_nfs' MX53-ARD-DDR3 U-Boot > set bootcmd_sd_nfs 'run bootargs_nfs;run load_kernel;bootm' MX53-ARD-DDR3 U-Boot > set load_kernel 'mmc read 0 ${loadaddr} 0x800 0x1f00' Here you may change the ip from "dhcp" to a fixed address if you are connected directly to host. MX53-ARD-DDR3 U-Boot > set bootargs_nfs 'set bootargs console=ttymxc0,115200 root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp' MX53-ARD-DDR3 U-Boot > set serverip 192.168.2.100 MX53-ARD-DDR3 U-Boot > set nfsroot '/tftpboot/rootfs_ard' MX53-ARD-DDR3 U-Boot > save Saving Environment to MMC... Writing to MMC(0)... done 5. Connect the USB/Eth adapter to the USB port (USB1-J30 or USB2-J31). Instructions to setup the host for NFS can be found on the following page: All Boards NFS.
View full article
Video Unit Test The BSP provides a package that allows testing of several i.MX 31 peripherals on the PDK. The name of this package is 'imx-test'.   The name of the package may vary according to SDK release, at the time of the writing SDK 1.4 was used, on SDK 1.2 the name of a similar package was 'mxc-misc'   For more information on the imx-test package refer to the SDK 1.4 manual, imx31_Linux_RM.pdf, chapter 49 - Unit Tests. This file is available on BSP tarball Testing To test the image sensor and the display on the PDK follow the steps below: Enable imx-test and util-linux packages: $ ./ltib -c Once "ltib" finishes boot the system. On the target board: $ modprobe mxc_v4l2_capture Check if /dev/video0 was created $ ll /dev/video* lrwxrwxrwx  1 root root            6 Jan 1 20:47 /dev/video -> video0 crw-rw----     1 root root    81,   0 Jan 1 20:47 /dev/video0 crw-rw----     1 root root    81, 16 Jan 1 20:46 /dev/video16 Now run the unit tests: $./mxc_v4l2_overlay.out -iw 640 -ih 480 -ow 480 -oh 640 -r 4 -fr 30 -t 10 - capture images with the sensor and display on the LCD $./mxc_v4l2_capture.out -w 640 -h 480 -r 0 -c 150 -fr 30 test3.yuv - capture images and save on /unit-tests/test3.yuv $./mxc_v4l2_output.out -iw 640 -ih 480 -ow 480 -oh 640 -d 4 -fr 60 test3.yuv - capture images and save on /unit-tests/test3.yuv   For usage syntax type: command -help. ./mxc_v4l2_output.out -help Source Code If you want to check the source code, on the host machine "ltib" install path type: $./ltib -m prep -p imx-tests Then, go to <ltib install path>/rpm/BUILD/imx-test-2.3.2/test/mxc_v4l2_test
View full article
To enable USB 2.0 port on BB for USB OTG, you need to apply below two changes: device/fsl.git   diff --git a/imx8q/mek_8q/init.usb.rc b/imx8q/mek_8q/init.usb.rc index af4e388..0f3ab0b 100644 --- a/imx8q/mek_8q/init.usb.rc +++ b/imx8q/mek_8q/init.usb.rc @@ -44,7 +44,7 @@ on early-boot      mount functionfs mtp /dev/usb-ffs/mtp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      mount functionfs ptp /dev/usb-ffs/ptp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      setprop sys.usb.mtp.device_type 3 -    setprop vendor.usb.config "5b110000.usb3" +    setprop vendor.usb.config "ci_hdrc.0"      write /sys/module/libcomposite/parameters/disable_l1_for_hs "y"      symlink /config/usb_gadget/g1/configs/b.1 /config/usb_gadget/g1/os_desc/b.1   vendor/nxp-opensource/kernel_imx.git           revert below patch:           commit 2f9586c120971312e61df464264993899cf34536           Author: yang.tian <[email protected]>           Date:   Tue Jan 7 13:30:02 2020 +0800       MA-15242 Set usb2.0 port as usb host only for mek_8q  
View full article
Using the FEC on U-boot 1 - Start by programming U-boot into the SD or NAND, click here for SD or here for NAND. 2 - Boot the image programed on Step 1, for the SD Card: Personality Board settings:                   12345678 SW22 -> 00000000 SW21 -> 11000000  Debug Board settings:   SW5,6,7,8,9,10 -> OFF                    12345678   SW4 -> 10000001 For NAND:                              12345678   SW22 -> 00100000   SW21 -> 10011000  Debug Board settings:   SW5,6,7,8,9,10 -> OFF                      12345678     SW4 -> 10000001 Stop at u-boot prompt: MX25 U-Boot > 3 - Configure u-boot networking variables, replace the values according to your network configuration: MX25 U-Boot > setenv serverip 192.168.1.1 MX25 U-Boot > setenv ipaddr 192.168.1.2 MX25 U-Boot > setenv eth1addr 00:04:9f:00:3b:33 Update "ethact" var to enable the FEC. MX25 U-Boot > setenv ethact FEC0 4 - With the Ethernet cable connected, start a tftp transfer: MX25 U-Boot > tftpboot 0x80800000 uImage_mx25 FEC: enable RMII gasket Using FEC0 device TFTP from server 192.168.1.1; our IP address is 192.168.1.2 Filename 'uImage_mx25'. Load address: 0x80800000 Loading: #################################################################              #################################################################              #################################################################              #################################################################              #################################################################              #################################################################              ##### done Bytes transferred = 2022396 (1edbfc hex) 5 - If you transfered the kernel image, you can boot it (Don't forget to update bootargs): MX25 U-Boot > bootm 0x80800000
View full article
Platform supported Kinara Ara2: imx95frdm imx8mpfrdm In this article, let's take imx8mpfrdm as example.   1. Create a Debian LSDK2512 release system for SD boot using the command below: $ ./flex-installer -i pf -d /dev/sdX $./flex-installer -b boot_IMX_arm64_lts_6.12.20.tar.zst -f firmware_imx8mpfrdm_sdboot.img -d /dev/sdX -m imx8mpfrdm -r rootfs_lsdk2512_debian_imx8mpevk.tar.zst note: if Debian base rootfs is used, please upgrade to full function Debian rootfs first. 2. Insert SD card on imx8mpfrdm and boot the system. Once the system has completed booting and you reach the kernel prompt: $ date -s "20260101 1100" // set date $ set proxy if needed 3. download rt-sdk-ara2.deb at: https://nxp1.sharepoint.com/:u:/r/teams/ext1081/Shared%20Documents/LF_v6.12.34/Debian%20Packages/r1.3/Package%201/rt-sdk-ara2.deb?csf=1&web=1&e=i4x1zD 4. Get the uiodma.ko kernel module for Debian from NXP. 5. Disable sleep when install package: $ systemctl mask sleep.target suspend.target hibernate.target hybrid-sleep.target 6. Prepare the packages ARA2 needed: $ apt update $ apt install --reinstall -y libc6-dev $ ln -sf /usr/include/aarch64-linux-gnu/sys /usr/include/sys $ apt install -y python3-dev build-essential $ e2fsck -f /dev/mmcblk1p2 7. install Ara2 package: $ dpkg -i rt-sdk-ara2.deb The tail of successful log as follows: ... [ 783.892116] Adding 2097148k swap on /swapfile. Priority:-2 extents:17 across:35913728k SS /swapfile none swap sw 0 0 Swap file of 2G configured and enabled successfully. Enable rt-sdk-ara2.service service... Created symlink '/etc/systemd/system/multi-user.target.wants/rt-sdk-ara2.service' → '/etc/systemd/system/rt-sdk-ara2.service'. rt-sdk-ara2.service has been enabled. To stop the service from starting automatically on boot run: systemctl disable rt-sdk-ara2.service Post-install script completed successfully. 8. overwrite the kernel module: $ cp /root/uiodma.ko /root/kinara/rt_sdk_r1.3/art/linux/drivers/uiodma_cache_management/uiodma.ko $ systemctl unmask sleep.target suspend.target hibernate.target hybrid-sleep.target // re-enable sleep 9. reboot the system: $ reboot You will see the log as bellow: ... [ 57.855988] bash[1492]: +----------+-----------------+ [ 57.856188] bash[1492]: | Product | Current Version | [ 57.856297] bash[1492]: +----------+-----------------+ [ 57.856397] bash[1492]: | firmware | 1.1.2.0 | [ 57.856501] bash[1492]: | proxy | 1.3.0.0 | [ 57.856593] bash[1492]: | sysapi | 1.1.61.0 | [ 57.856695] bash[1492]: +----------+-----------------+ [ 57.856788] bash[1492]: [I:20260109:09:02:44:636750] [DeviceManager] [kinara_main_1479][DeviceManager] [ 57.856894] bash[1492]: +------------+--------------------+ [ 57.857019] bash[1492]: | Product | Supported Versions | [ 57.857124] bash[1492]: +------------+--------------------+ [ 57.857227] bash[1492]: | client_lib | 1.0.0.0 | [ 57.857327] bash[1492]: | client_lib | 1.1.1.0 | [ 57.857419] bash[1492]: | client_lib | 1.1.2.0 | [ 57.857525] bash[1492]: | client_lib | 1.3.0.0 | [ 57.857642] bash[1492]: | cnn_model | 2.0.0.0 | [ 57.857741] bash[1492]: | cnn_model | 2.1.0.0 | [ 57.857833] bash[1492]: | firmware | 0.5.2.0 | [ 57.857931] bash[1492]: | firmware | 1.1.2.0 | [ 57.858030] bash[1492]: | llm_model | 3.0.0.0 | [ 57.858129] bash[1492]: | llm_model | 3.1.0.0 | [ 57.858222] bash[1492]: | pci_driver | 1.0.4.0 | [ 57.858322] bash[1492]: | pci_driver | 1.0.6.6 | [ 57.858421] bash[1492]: | proxy | 0.8.0.0 | [ 57.858533] bash[1492]: | proxy | 0.9.0.0 | [ 57.858633] bash[1492]: | proxy | 1.1.1.0 | [ 57.858732] bash[1492]: | proxy | 1.3.0.0 | [ 57.858823] bash[1492]: +------------+--------------------+ [ 57.858930] bash[1492]: 2026-01-09 09:02:44 - Proxy launched succesfully [ 58.752944] bash[1514]: 2026-01-09 09:02:45 - Hardware bringup is done (1 device(s) configured) and proxy is launched successfully in the background. [ 58.755142] bash[392]: Logs saved in: /root/kinara/rt_sdk_r1.3/saved_logs/rt-sdk-ara2_logs.txt Now, enjoy your AI journey.
View full article
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX8MN-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX8MN-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX8MN-EVK SDK   Import "hello world" example Ensure that we are compiling a debug binary Build Project   Flash the Binary using UUU Tool Connect the IMX8MN-EVK Board to your Host PC via USB   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write hello_world.bin mmc X:1 hello_world_debug.bin Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card   Connect MCU-LINK Pro to the Target   IMX8MN-EVK Debug connection:   Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 0x48000000 hello_world_debug.bin; cp.b 0x48000000 0x7e0000 0x20000; => bootaux 0x7e0000 Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card   Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso:      With the MCU-LINK Pro configured, the IMX8MN-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX8MN based projects.   References: AN14120.pdf 
View full article
Sometimes we got CMA allocation error while there're still many free pages in CMA area.  This article analyze several cases/reason for this kind of failure.
View full article
Overview As you know, R13.4.1 doesn't support Bluetooth. These attached patches enable Bluetooth for R13.4.1. Before applying the patches for MX6 SabreSD, please rework SabreSD. Refer to How to enable BT on board imx6q_sabresd RevC. Hardware i.MX6Dual/Quad or i.MX6DualLite SabreSD board Software i.MX6DQ/MX6DL Android ICS R13.4 or R13.4.1 Release
View full article
Freescale's consumer and industrial i.MX 51 applications processors balance the performance, power consumption, connectivity and multimedia capabilities necessary to drive today's latest and greatest products. Freescale's automotive i.MX 51 processors provide what is necessary to steer today's most advanced automotive systems. i.MX51 Family Comparison i.MX Family Comparison Product Information on Freescale.com i.MX512 Applications Processor i.MX513 Applications Processor i.MX514 Applications Processor i.MX515 Applications Processor i.MX516 Applications Processor Evaluation/Development Boards and Systems IMX51EVK Evaluation Kit Bootloader Installing U-Boot on i.MX51EVK Flashing i.MX51EVK Working with mainline U-Boot Add new iMX5x board on LTIB Compiling U-Boot (from Freescale BSP) using LTIB Changing environment variables storage on U-Boot Linux Flashing Linux application only with SD card Reader Multimedia Using USB Camera Installing OpenCV Library (Open Computer Vision - Image Processing) Android Android without RamDisk Installing TTS library manually Running ADB over USB (iMX51 and Ubuntu communication) Ubuntu Using an USB Touchscreen (Karmic) Using Touchscreen (Lucid) Embedded Software and Tools Android OS for i.MX Applications Processors i.MX51 Current Software Updates and Releases Partners / 3rd-Party Development Tools STK5:  Starter-Kit 5 (Karo Electronics) Additional Resources Board bring-up and DDR initialization tools Develop a Simple OpenVG Application Under Linux: Tutorial i.MX 51 Android ADB over USB IMX51EVK i.MX51 EVK Board USB Camera i.MX51 EVK Compiling U-boot i.MX 51 EVK U-boot i.MX51 EVK Board Video i.MX51 EVK Board OpenCV i.MX51 EVK Board Flashing i.MX51 Flashing Linux Application Only with SD Card Reader I.MX51EVK Install U-Boot i.MX51 EVK Compiling U-boot i.MX51 EVK U-boot i.MX51 EVK Changing Env IMX51 Ubuntu USB TS i.MX 51 Ubuntu TS Lucid
View full article
Play MPEG4 Video only gst-launch filesrc location=test.mpeg ! mfw_vpudecoder codec-type=std_mpeg4 ! mfw_v4lsink H.264 Video only gst-launch filesrc location=test.avi ! mfw_avidemuxer ! mfw_vpudecoder codec-type=std_avc ! mfw_v4lsink AVI(H264+MP3) gst-launch filesrc location=test.avi ! mfw_avidemuxer name=demux demux. !  mfw_vpudecoder \     codec-type=std_avc ! mfw_v4lsink demux. ! queue max-size-buffers=0 ! <mp3_decoder_plugin> ! alsasink MP4(H264+MP3) gst-launch filesrc location=test.mp4 ! mfw_mp4demuxer name=demux demux. ! \    mfw_vpudecoder codec-type=std_mpeg4 ! mfw_v4lsink demux. ! \    queue max-size-buffers=0 ! <mp3_decoder_plugin> ! alsasink <mp3_decoder_plugin> can be replaced by mad RAW Video Test gst-launch videotestsrc ! video/x-raw-yuv,format=\(fourcc\)I420 !  mfw_v4lsink
View full article
To use Android GDB for native code, take mediaserver as an example. Setup on board. adb push prebuilt/android-arm/gdbserver/gdbserver system/bin/ adb shell ps adb shell /system/bin/gdbserver :5039 --attach <PID> & Setup on host. source build/env.sh adb forward tcp:5039 tcp:5039 gdbclient mediaserver b createPlayer c
View full article
Question: In a single uImage to contain the compressed kernel and rootfs, if the uImage is greater than 16MB, the system will not boot and reports errors. Is there a size limitation on uImage?  If so, is there a work around? Answer: uImage should only contains kernel compressed. rootfs should be read through a linux partition after the kernel boots up. Regarding the uImage's size, there is no limitation. In the other hand, a single uImage with kernel and filesystem is needed; in other words, kernel (alias uImage) needs a filesystem to work, and these are two independent systems in that sense. If u-boot, kernel and filesystem are in a single device (SD Card), the filesystem must be mounted in the first partition (SD, eMMC, etc) starting somewhere > 16M/512 sectors. But in cases where: * A fast boot is needed with  very small rootfs * As a intermediate (temporal) rootfs  before switching  to the real rootfs. The usage (actually used when flashing with the MFG tool) of this intermediate system is to load heavy modules, keeping the uImage small. This mechanism is called initramfs and the uImage will contain the kernel and the this mini rootfs compressed as cpio archive. But there appears to be a 16MB limitation. See here:  http://www.isysop.com/unpacking-and-repacking-u-boot-uimage-files/ It seems to be related to alignment suggesting that 24-bit addressing is used instead of 32-bit.  I did notice Thumb mode is used, which seems odd to me.
View full article
Hi All, The i.MX6 Android R13.4-GA.03 patch release is now available on www.freescale.com ·         Files available # Name Description 1 IMX6_R13.4.03_ANDROID_PATCH This patch release is based on the i.MX 6 Android R13.4   release. The purpose of this patch release is correct the PFD workflow in   U-Boot, fix the miscalibration issue for the thermal sensor and corrects   ramp-up time of the internal LDOs
View full article