i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
NETC presents itself as a multi-function PCIe Root Complex Integrated Endpoint (RCiEP) for easy software discovery of peripheral functions. As such, it contains multiple PCIe functions. PCIe RCiEP allows for easy software integration into OSes, which support PCIe but can be easily integrated as a simple platform device for RTOSes or bare metal implementations which do not support it. Configuration and control of ENETC(s) is implemented using a combination of registers and a command message interface implemented using descriptor rings in memory. Key goal of the DPDK is to provide a simple, complete framework for fast packet processing in data plane applications. Using the APIs provided as part of the framework, applications can leverage the capabilities of underlying network infrastructure. DPDK been prominent software in user space for networking applications pushes for eNetc driver to be written in user space. This document introduces overview of the NXP ENETC and how its driver is implemented and integrated into the DPDK. DPDK eNetc Driver support features Multi-queue supported, Packet type parsing, promisc, MAC exact filter table filtering, VLAN exact filter table filtering, Link status interrupt, Rx checksum offload, basic stats.
記事全体を表示
i.MX28 LCD driver 8080 bus interface mechanism please read readme.txt and it will teach you how to use it
記事全体を表示
i.MX27 PDK Board Flashing This tutorial teaches how to flash bootloader using ATK. To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot. Using ATK ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. This section will describe the procedure to erase the flash memory and program the bootloader. 1 - Connect a serial cable between PC and i.MX board. 2 - Some hardware configurations (switches) must be done to flash the board. Set red and cream switches as below: Switch SW5 -> 00000 Switch SW4 -> 10000001 Installing ATK on Linux Download ATK: Download. Extract ATK: # unzip ATK_1_41_STD_installer.zip Execute the default install process: # wine SETUP.EXE Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32) Run ATK: # wine ADSToolkit_std.exe Next Step To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot. PS: On SW5 and SW4, "1" means the keys selected towards the edge of the board. 3 - Run ATK by clicking Start -> Programs -> AdvancedToolKit -> AdvancedToolKit       Set the options:    Device memory -> DDR; Custom Initial File -> (keep it unmarked)    Communication Channel -> Serial Port (Usually COM1) 4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO. Flash Erasing 1 - To erase Flash memory, select the parameters as shown in the figure below: 2 - Turn on the board and press Erase. 3 - ATK shows this message when flash is erased Flash Programming The next step is to program the bootloader image into the board's Flash following the steps below. 1 - Select the parameters as shown in the figure below and press Program. The bootloader binary image file can be found into your Board Support Package Set Program, NAND, Address: 0x00000000 2 - Add it on Image File field and press Program. 3 - Close ATK, turn off the board and set switch back as shown in the picture below. Installing ATK on Linux Download ATK: Download. Extract ATK: # unzip ATK_1_41_STD_installer.zip Execute the default install process: # wine SETUP.EXE Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32) Run ATK: # wine ADSToolkit_std.exe Next Step To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot.
記事全体を表示
In new iMX8QM and iMX8QXP BSP, it had implemented hardware partition to split the resource and memory regions. The default Android Auto BSP had given example for shared memory between M4 and A core, it is used for RPMSG. Here is an example to add a new shared memory for iMX8QXP MEK board with Android Auto P9.0.0_GA2.1.0 BSP, which can be accessed in both M4, Uboot and Linux Kernel. The new shared memory region is from 0xF6000000 to 0xFDFFFFFF, total 128MB, it covers the RPMSG region too. RPMSG shared memory is moved to 0xF6000000 ~ 0xF6BFFFFF, total 12MB. vendor_nxp_fsl-proprietary_uboot-firmware.patch SCFW patch for board file to change the old shared memory region (0x90000000~0x90BFFFFF) to new shared memory region (0xF6000000~0xFDFFFFFF). This patch is applied to android_build/vendor/nxp/fsl-proprietary/uboot-firmware/imx8q_car/board-imx8qxp.c, after patched, copy this file to SCFW porting kit and build out a new SCFW image, put it to "android_build/vendor/nxp/fsl-proprietary/uboot-firmware/imx8q_car/mx8qx-scfw-tcm.bin". vendor_nxp-opensource_uboot-imx.patch This is the Uboot patch to map the shared memory region, if Uboot doesn't need access these memory, this patch is not needed. vendor_nxp-opensource_kernel_imx.patch This is the kernel patch to map the shared memory region. Note: VPU reserved memory address shouldn't be changed, otherwise it will impact the VPU function. So the new reserved memory region had been moved to 0xF600000~0xFDFFFFFF. vendor_nxp_mcu-sdk-auto_SDK_MEK-MIMX8QX.patch M4 patch for RPMSG address changed from 0x90000000 to 0xF6000000. Note: 1. In this example, we put the two shared memory regions together, then it will not split the memory region used in Linux. Another reason for such modification is the limitation of memory region counts in SCFW. 2. Since the RPMSG shared memory had been moved from 0x90000000 to 0xF6000000, the M4 code who used shared memory should also be changed. 2019-07-29 Update: When "#define PHYS_SDRAM_2_SIZE  0x0" in Uboot, it will create a 0 size memory region, this will impact the Uboot shared memory patch. Added the "uboot_imx8_cpu.patch" to avoid such issue.
記事全体を表示
U-boot expects uImage format for the kernel image. In order to LTIB generate a uImage file: $ export SYSCFG_KTARG=uImage $ ./ltib -p kernel Setup in U-Boot the kernel bootargs: u-boot> setenv bootargs noinitrd console=ttymxc0,115200 init=/linuxrc root=/dev/nfs nfsroot=10.29.244.27:/tftpboot/rootfs ip=dhcp Change 10.29.244.27 to your host IP. The procedure above is needed when default bootloader used by ltib was redboot. In some ltib releases (before 2010) default bootloader is u-boot. In this case, ltib will create uImage by default
記事全体を表示
When flashing a Linux System on a SD card using the script mk_mx28_sd on a Ubuntu 12.04 host, one needs to modify it so partitions are created correctly.  Just follow these steps on the console: $ cd $SDK/L2.6.35_10.12.01_SDK_scripts $ cat > first_partition_sector.patch << EOF diff -Naur a/mk_mx28_sd b/mk_mx28_sd --- a/mk_mx28_sd        2010-10-06 09:47:42.000000000 -0500 +++ b/mk_mx28_sd        2012-11-30 13:38:34.508199154 -0600 @@ -178,7 +178,7 @@ n p 1 -1 +2048 +32M t b EOF $ patch -p1 < first_partition_sector.patch then, you can run the mk_mx28_sd command again with the device as parameter                $ cd $LIB $ export PATH=$PATH:$SDK/L2.6.35_10.12.01_SDK_scripts $ mk_mx28_sd /dev/$SDX
記事全体を表示
Even though the Advanced Tool Kit is not a supported tool anymore, it can be used to provision the code and blow fuses of an i.MX device during manufacturing. This is true when the secure boot has been enabled, which means that the code downloaded by the ATK to the target must be signed, as it will be authenticated prior to its execution. Once in secure mode, the Serial Download boot mode (SDP) can only access a restricted range of addresses, which is documented in the DCD section of the reference manual. An attempt to write outside this allowed area will result in an error, and will make the ROM restart the SDP by considering this as an attack. To automatically detect the mode (engineering or secure/production) of the chip, the ATK writes data to a memory location, and by retrieving the response it knows the configuration. The response can be one of two values: 0x56787856 means that the chip is in engineering mode. 0x12343412 means that the chip is in production/secure mode. It should be known that there is a bug that prevents a secure chip from being handled correctly. For instance, to perform the automatic detection mentioned above, the tool writes to 0xFFFF_FFFF for the i.MX25 or even i.MX35. This address is invalid by being outside the allowed address range, so the ROM code aborts the current session, and restarts a new one. The attached DLL library fixes this issue by writing to an appropriate area like the free iRAM space. This will allow use of the ATK for a chip whose secure boot is enabled.
記事全体を表示
Download ATK from Freescale Extract ATK: # unzip ATK_1_41_STD_installer.zip Get the wine-tricks script and install MFC-4.2 and VisualC++-6.0. ./winetricks  vcrun6sp6 Execute the default install process: # wine SETUP.EXE Edit the file /etc/udev/rules.d/50-udev-default.rules to set permission for everyone: KERNEL=="tty[A-Z]*|pppox*|ircomm*|noz*", GROUP="uucp", MODE="0666" Run ATK: # wine ADSToolkit_std.exe
記事全体を表示
i.MX25 for Industrial and General Embedded The i.MX25 family of multimedia applications processors extends the Freescale ARM9™ portfolio and makes the industrial and general embedded market a key focus of i.MX with the integration of many new features. Speed up to 400 MHz, low power consumption and multiple connectivity options support the growing needs of industrial and general embedded products, while allowing customers to reduce their overall system bill of materials cost. The i.MX258 processor provides additional security features making it the ideal solution for payment terminal (POS), or any other type of product needing secure system boot and tamper detection. i.MX25 for Automotive Today's drivers expect more connectivity in more places from more things—phones, media players and, increasingly, cars. Bluetooth™ connectivity is becoming the norm as more people keep their hands on the wheel instead of on the phone. Connectivity and compatibility with media players is becoming a requirement as consumers' media investment goes digital. The challenge: how can designers support high-end features such as connectivity and media playback without charging high-end prices? The i.MX25 family of processors offers integration that tailors itself to the connectivity requirements of today's automobile but eliminates expensive parts not needed for a cost-conscious infotainment system. The i.MX25 applications processor is a Freescale Energy-Efficient Solutions product. Product Information on Freescale.com i.MX257: Multimedia Applications Processor i.MX251: Multimedia Applications Processor i.MX253: Multimedia Applications Processor i.MX255: Multimedia Applications Processor i.MX258: Multimedia Applications Processor Additional Resources i.MX25 PDK Board I.MX25 PDK Board Get Started i.MX25 PDK Board Flashing NAND i.MX25 PDK Board Flashing SPI NOR i.MX25 PDK Board Flashing SD Card i.MX25 PDK Board Running Linux I.MX25 PDK U-boot SplashScreen I.MX25 PDK U-boot SDCard I.MX25 PDK Using FEC i.MX25: When using 120MHz UPLL as clock source, GPT counter returns unexpected results Limitations of the i.MX SIM Controller to Pass the EMV Certification
記事全体を表示
Qtopia Qt Extended, formerly known as Qtopia until September 30, 2008, is an application platform for Embedded Linux-based mobile computing devices such as personal digital assistants, mobile phones, and web pads. It is being developed by Qt Software, a subsidiary of Nokia. [Source: http://en.wikipedia.org] Qt Software discontinues Qt Extended March 3, 2009 — Oslo, Norway — Qt Software today announced that the product, Qt Extended, will be discontinued as a stand-alone product. Instead, selected features will be migrated into the Qt framework which will result in Qt becoming an even richer, cross-platform application framework. The final release of Qt Extended will be version 4.4.3, which will is planned for release on March 5, 2009. Qt Extended will be maintained for one year from that date. Qt Software will honor all existing support agreements, and for customers who need continued access to support beyond the term of their current agreement, Qt Software is offering the possibility of purchasing supplemental support. [Source: http://www.qtsoftware.com/about/news/qt-software-discontinues-qt-extended] Compiling Qtopia Crosscompiling Qtopia for i.MX processors requires some packages to be installed on host (PC). For more details click on your host PC Linux distribution below: All Boards Qtopia All Boards Qtopia on Ubuntu It's possible to compile Qtopia (version 2 or 4) by selecting Qtopia on package list or simply selecting Qtopia profile on Ltib configuration. Starting Qtopia Touchscreen setup When the system starts up, TSLIB_TSDEVICE environment variable must be set and ts_calibration application must be called to calibrate the touchscreen. $export TSLIB_TSDEVICE=/dev/input/event1 /dev/input/event1 is the usual touchscreen device. Some systems can address the touchscreen device to other names. It's possible to check what's the touchscreen device by typing: $cat /dev/input/<supposed device> After the command above, when touchscreen is pressed, some characters will be showed indicating that the <supposed device> device is the touchscreen device and it's working properly. $ts_calibrate Calibrate screen will appear. After touchscreen calibration, Qtopia can be executed by calling the following script: $/etc/rc.d/init.d/qtopia start Qtopia will be started.
記事全体を表示
Attached you can find a document that explains how to add Wi-Fi support in the iMX28evk using Yocto.
記事全体を表示
This is a HW design checklist for customer's reference. Please read and fill it in carefully before requesting a schematic/design review.
記事全体を表示
This tutorial teaches how to program bootloader on a SD Card using ATK. To program kernel and root file system to the SD card, please follow this i.MX35 PDK Linux Booting SD    ATK (Advanced Toolkit)       ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. It can be downloaded here.     Using ATK       This section will describe the procedure to erase and program the bootloader in the SD Card.       1. Connect a serial cable between PC and i.MX board.       2. Set the switches:       Debug Board: SW9 -> 0         SW10 -> 0         Personality Board: SW1 and SW2 (All bits) -> 0     3. Run ATK going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit           Set the options:       i.MX CPU -> i.MX35_TO2       Device memory -> DDR2;       Communication Channel -> Serial Port (Usually COM1)     4. Click Flash Tools to erase, program, or dump the the memory and click GO     Erasing     1. To erase SD Card, select the parameters as below: Select MMC/SD as "Flash Model".     Select Erase on "Operation Type". 2. Turn on the board and press Erase.     3. ATK shows a message: "Flash erase successful!" when card is erased   Programming     Next, program the bootloader image into the memory card following the steps below:     1. Select the parameters: The bootloader binary image file can be found into your Board Support Package (click here to download) Select Program on "Operation Type".     Address: 0x00000000     File: "mx35_3stack_redboot_mmc.bin" (or similar name that indicates a MMC/SD image)     2. Press Program.     3. Close ATK, turn off the board and set switches to:     Debug Board: SW9 -> 0       SW10 -> 0 Personality Board: SW2 (Bits 1 and 2) -> 1       SW2 (All other bits) -> 0       SW1 (All bits) -> 0     4. Open Hyper Terminal, set it 115200,N,8 and see RedBoot Prompt.      
記事全体を表示
SW: Linux 4.14.98_2.2.0 bsp release , gpu sdk 5.3.0 and patch in this doc HW: i.MX8QXP MEK board Inspired by the GIMP adjust color curve tool,  I write similar gui test code for i.MX8QXP gamma curve tuning. That is on display will show one linear curve first, use mouse to change any part of this curve, after that calculate value of point on changed curve , then pass related value to i.MX8QXP DPU gammcor unit , at last the display effect will be changed by DPU. When test code start up , will draw Y=X curve on display, that will from (0,0) to (500, 500) to (1023,1023). After you use mouse drag some part of the curve, will generated a new point (x_new, y_new) which is not on original Y=X curve. Then need draw a new curve that pass  through the (0,0) , (500, 500) , (x_new, y_new), (1023,1023).  That new curve , i choose to use Catmull-Rom Splines to get it. Use Catmull-Rom Splines for approximate a curve that pass through n point, then need n+2 control point. Extra 2 point could be selected as you want ,and they will affect the shape of the curve. Catmull-Rom Splines could pass through all control point, it is C1 continuity, no convex hull property. For example, there is four control point p0, p1 , p2 , p3,  to draw the curve pass through all of them, it could divide to segment p0 to p1 , segment p1 to p2 , segment p2 to p3. For segment p1 to p2 , select four control point as p0,p1, p2, p3, use Catmull-Rom Splines as below: For segment p0 to p1 , need use four control point as p0, p0, p1, p2: For segment p2 to p3, need use four control point as p1, p2, p3, p3: In this test code,  i will use gpu vertex shader to calculate each segment of curve, then use transform feedback to read back point value of each segment to cpu side, cpu side will pass related value to DPU gammcor unit for gamma tuning.   Test steps: Apply 8qxp_dpu_gammacor_4.14.98_2.2.0.diff on linux-imx for i.MX8QXP DPU device driver. Apply dpu_gamma_curve_gpusdk5.3.0.diff on imx-gpu-sdk for build this gui test code. Update the new kernel image, and copy test code to rootfs. Run any other application first to draw some thing on screen, for example  /usr/share/cinematicexperience-1.0/Qt5_CinematicExperience. Then run gui test code in this code, S01_SimpleTriangle_Wayland. Then there will show one linear curve on display , use mouse to change the curve as you like by put mouse cursor close to the curve, press the mouse button , drag it and release the mouse button, you will see the new curve on display , and also the display effect also be changed. Reference: 1>https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-8-processors/i-mx-8x-family-arm-cortex-a35-3d-graphics-4k-video-dsp-error-correcting-code-on-ddr:i.MX8X  2>https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab  3>https://github.com/NXPmicro/gtec-demo-framework  4>https://en.wikipedia.org/wiki/Cubic_Hermite_spline  5>http://www.mvps.org/directx/articles/catmull
記事全体を表示
TFTP     TFTP service will be used to transfer the kernel image from host to target every time the system reboots. Select the Linux distribution: All Boards TFTP Fedora All Boards TFTP on OpenSuse All Boards TFTP on Ubuntu
記事全体を表示
Some processor’s GPIO settings on the i.MX Pins Tool version 7 may not show allow to select direction and just show an option “Input/Output” as shown. This will be fixed, but the settings can be changed on the local processor data as a workaround. For more information and documentation for the Pins Tool for i.MX please visit its home page on the link below: https://www.nxp.com/design/designs/pins-tool-for-i-mx-application-processors:PINS-TOOL-IMX   First, find where the Pins Tool data package is stored. To do this open the Pins Tool and click Help > About. On the About screen click the Details button. Take also note of the name of the package that needs to be fixed.   Go to the location where the data package is stored and find the processor data. The file that would need to be updated is signal_configuration.xml    Find the GPIO pin data and change the directions from the string ““inOut”to the string “in out”. Then save this file.    Close and reopen the Pins Tool. The direction on the updated package should now show the options Input and Output.  
記事全体を表示
These instructions used ltib-imx27ads-20071219. First, get u-boot v2.0: git clone http://git.denx.de/u-boot-v2.git u-boot-v2 Enter the U-Boot directory: cd u-boot-v2 Export the proper compilation paths and environment variables: export ARCH=arm export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" export CROSS_COMPILE=arm-none-linux-gnueabi- Configure it for the i.MX27ADS board: make mx27ads_defconfig You may want to enable the FEC driver: make menuconfig And go to Drivers -> Network drivers and select Yes on i.MX FEC Ethernet driver Exit the config menu (don't forget to save the configuration) and just make it: make Or if you prefer the verbose mode make V=1 After a quick build, you should get a uboot.bin on your current directory. I used the ADS Toolkit to program the NOR flash.
記事全体を表示
The Config Tools for i.MX is a set of configuration tools that provide an efficient method for evaluation and configuration of pins routing and DDR memory settings when designing with NXP's application processors based on Arm® Cortex®-A cores, including i.MX MPUs. The following tools are currently available: DDR Tool DDR Configuration and Validation tool allows you to create a configuration for the DDR component and to validate the DDR configuration using various validation scenarios Features: Support for iMX8M, iMX8MM, iMX8MN, iMX8MP and LX2160A DDR configuration UI using the tokenized RPA tool PHY initialization using dynamic library Import the output of the RPA tool will bypass UI configuration Support for multiple PHY firmware version including fw2020.06 Diagnostic fw2020.06 DDR PHY support for DDR3, DDR4, and LPDDR4 Cell color code Basic/Advanced user mode DDR controller Registers View support Auto-detect of available COM ports USB target connection Basic validation tests support (Write-Read-Compare, Walking Ones, Walking Zeros) DQ ODT and driver strength test vTSA (Virtual Timing Signal Analysis) support - RX data eye, TX data eye Stress tests support Export vTSA results in JPEG format Static Code generation in Uboot style Command line posibility PBL Tool PBL tool helps you create and modify pre-boot initialization data used for configuring LX2 devices. Features: Support for LX2160A Configure reset configuration word (RCW), which is 1024 bits of information Optional configure pre-boot initialization (PBI) command sequence Allow user to have full access to configuration by using Skip error checking and Display all fields Option to directly modify the configuration from RCW registers Import different formats of input Generate different types of output, including a binary file SerDes Tool The SerDes tool allows you to configure the SerDes block and provides you with a GUI application to validate the configuration Features: Support for LX2160A UI for SerDes blocks configuration Per lane tests Bist, Power Transmitter/Receiver, Reset Transmitter/Receiver tests Jitter scope, Pattern Independent Jitter scope, Start/Stop Tx Patter generation tests Read a configuration from the target   Trusted Execution Environment Configuration tool The Trusted Execution Environment (TEE) tool facilitates the protection and isolation of the sensitive parts of the code. Features: Graphical display of memory layout and resulting access to memory regions Configuration of access policies for memory areas, bus masters, and peripherals Configuration of pin and interrupt masking and security, as well as general features related to the ARMv8 core security Configuration of MPU Validation of settings Generation of configuration files (C code or ROM preset data) Pins Tool The Pins Tool is used for pin routing configuration, validation and code generation, including pin functional/electrical properties, power rails, run-time configurations. Features: Desktop application Muxing and pin configuration with consistency checking Multicore support Localized for English and Simplified Chinese Mostly Connected: On-Demand device data download Integrates with any compiler and IDE Supports English and Chinese (simplified) languages, based on locale settings. Please refer to user manual for details. ANSI-C initialization code Graphical processor package view Multiple configuration blocks/functions Easy-to-use device configuration Selection of Pins and Peripherals Package with IP blocks Routed pins with electrical characteristics Registers with configured and reset values Power Groups with assigned voltage levels Source code for C/C++ applications Documented and easy to understand source code CSV Report and Device Tree File Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this blog post. Whats new in v12.1 Pins tool Deinit function now sets also the routing and direction to it's default state. It also tries to route the original peripheral signal to it's default pin.  
記事全体を表示
This is the procedure and patch to set up Ubuntu 13.10 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0. It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-13.10-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0 $ sudo apt-get install libc6-dev-i386 $ sudo apt-get install u-boot-tools $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd $ sudo ln -s /usr/lib/x86_64-linux-gnu/librt.so   /usr/lib/librt.so C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source. tar.gz $ ./L3.0.35_4.1.0_130816_source/install      After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 13.10 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_13.10_64bit_OS.patch What the patch is doing: a) The patch modifies the following files:    dist/lfs-5.1/base_libs/base_libs.spec    dist/lfs-5.1/m4/m4.spec    dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory:    pkgs/m4-1.4.16-1383761043.patch    pkgs/m4-1.4.16-1383761043.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 m4 compilation issue: 1. https://github.com/hashdist/hashstack/commit/f6be2a58de62327d05e052d89c9aa931d4c926b3 2. https://github.com/hashdist/hashstack/issues/81 rpm-fs package failed to build issue: https://community.freescale.com/message/355771#355771 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
記事全体を表示