i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
NFS Network File System (NFS) is a network file system protocol originally developed by Sun Microsystems in 1984, allowing a user on a client computer to access files over a network as easily as if the network devices were attached to its local disks. The use of NFS makes the development work of user space applications easy and fast since all target root file system is located into host (PC) where the applications can be developed and crosscompiled to target system. The target system will use this file system located on host as if it is located on target. NFS service will be used to transfer the root file system from host to target. NFS resources are listed below: All Boards Deploy NFS All Boards NFS on Fedora NFS on Fedora All Boards NFS on Slackware NFS on Slackware All Boards NFS on Ubuntu NFS on Ubuntu
查看全文
The document descript how to use the win32diskimager to create bootable sdcard.  How to resize sdcard mirror rootfs partition. Ex: fsl-image-validation-imx-imx6qpdlsolox.sdcard
查看全文
Overview Measuring the power consumed an i.MX application processor can be a challenging undertaking. This document describes several boards designed to instrument i.MX application boards for current measurements. While this system does not offer many digits of accuracy, it can be used to quantify power consumed by application use cases as well as while in low power modes. The system can be used to instrument up to four power supply rails and measure current in two ranges. Range switching on the sensor boards is controlled via software running on the Kinetis K20 at the heard of the profiler board. Measured data is sent to a host computer over a virtual serial link over USB. Power for the profiler system is obtained from the USB connection although a external 5V supply may be used. Dual-Range Current Sensors INA250 + INA21x Sensor Circuit Description: The INA250 + INA21x Sensor board can measure two ranges using the INA250 and INA21x current sense amplifiers. The high range is measured with an INA250, which has an integrated 0.002 Ohm shunt, and is available in four output gains. The low range is measured with shunt R1 and the INA21x sense amp. The low range shunt is taken out of the circuit (by shorting it) with two paralleled, very low-Rds(on) FETs, Q1 and Q1. VCC_SENSE powers the two sense amplifiers. VCC_FET supplies the gate voltage on Q1 and Q2. The DMN1019 device has a Vgs max of 8V. The sources of both FETs are tied to the i.MX side of the current sense loop, so the gate voltage Q1 and Q2 see is VCC_FET-(rail voltage). The signal /LOW_EN controls the state of both Q1 and Q2. The sense amplifier outputs (HIGH_OUT1 and LOW_OUT1) and rail voltage (V_RAIL_MEASURE) are sent down the ribbon cable (X2) to the profiler board for measurement. When not used for a wire loop for a Hall-effect current probe, resistor R3 should be shorted with a solder bridge, a piece of wire, or a 0.001 Ohm resistor. Schematic: Board Layout: The two large vias by the current sense connection points are provided for use with a 0.1" header and jumper to short the low range shunt, allowing normal operation of the target board when the profiler is not powered. It should be noted a jumper will not be as effective for relatively large currents. BOM: Part   Device C1,C2  0.1uF 0805 Q1,Q2  DMN1019USN-13 SOT23 R1     2 1% 0805 (resize to change low range) R2     10k 0805 R3     Solder bridge/wire loop (see schematic) U1     INA250 TSSOP16 (choose gain, A3 [0.8V/A] or A4 [2.0V/A]) U2     INA21X SC70 (choose desired gain) X2     WM6769CT/0527460871 (bottom contacts) Dual INA21x Sensor Circuit Description: The Dual INA21x Sensor board can measure two ranges using two INA21x current sense amplifiers and two different shunts. The high range shunt (R1) is always in place. The low range shunt is taken out of the circuit (by shorting it) with two paralleled, very low-Rds(on) FETs, Q1 and Q1. VCC_SENSE powers the two sense amplifiers. VCC_FET supplies the gate voltage on Q1 and Q2. The DMN1019 device has a Vgs max of 8V. The sources of both FETs are tied to the i.MX side of the current sense loop, so the gate voltage Q1 and Q2 see is VCC_FET-(rail voltage). The signal /LOW_EN controls the state of both Q1 and Q2. The sense amplifier outputs (HIGH_OUT1 and LOW_OUT1) and rail voltage (V_RAIL_MEASURE) are sent down the ribbon cable (X2) to the profiler board for measurement. Schematic: Board Layout: The two large vias by the current sense connection points are provided for use with a 0.1" header and jumper to short the low range shunt, allowing normal operation of the target board when the profiler is not powered. It should be noted a jumper will not be as effective for relatively large currents. BOM: Part   Device C1,C2  0.1uF 0805 Q1,Q2  DMN1019USN-13 SOT23 R1     0.002 1% 0805 (resize to change high range) R2     0.05 1% 0805 (resize to change low range) R3     10k 0805 U1,U2  INA21X SC70 (choose desired gain) X2     WM6769CT/0527460871  (bottom contacts) Four-Channel Power Profiler Circuit Description: The Four-Channel Power Profiler board has at its heart a Kinetis K20 on a Teensy3.2 board. The ADCs of the K20 measure all the current sense amplifier's outputs, the voltage of each instrumented rail. There is provision for measuring temperature using up to three thermistors. GPIO provide control each sensor board's current range, and optionally, a hardware wake-up signal for the instrumented target board. Up to four dual-range sensor boards can be connected (either sensor board mentioned above). A micro-SD card socket is included for storing measured data (the SD card functionality has been tested but not implemented for use with measurements). Measured data is sent to the host computer over a virtual serial port using the Teensy's USB. Charge pump U1 boosts the 5V supply to 12V. The output is regulated down to 8V on VCC_FET via regulator U2. R2 and C5 provide filtering for the 3.3V supply from the Teensy that feeds the sensor boards through VCC_SENSE. FETs Q1 through Q4 provide voltage level translation which protect the Teensy's GPIO pins from the 8V that's placed on the gates of the shorting FETs on the sensor boards. Regulator IC2 provides power for the micro-SD socket, since the 3.3V regulator on the Teensy does not provide enough capacity. Since there are not "smarts" on the sensor boards, the Teensy has no way of knowing what kind of sensor board is connected or what shunt values and sense amplifier gains are in use. As currently implemented, current and voltage calculations are hard coded in the Teensy application code. Schematic: Board Layout: BOM: Part    Device C1,C2   0.22uF 0805 C3-C7   1uF 0805 C10,C12 1uF 0805 C11     0.1uF 0805 IC2     MCP1825ST-3302 SOT223 Q1-Q4   DMN1019USN SOT23 R2-R4   20k 1% 0805 R5-R8   10k 0805 R9      Ferrite bead 0805 S1-S4   WM6769CT/0527460871 (bottom contacts) U$1     101-00660-68-6-1-ND MICROSD U1      MAX662CPASO8 SO08 U2      78L08SMD SO08 Use mating Molex cables: 8in: 0150200087 or 10in: 0151660091 Using the Power Profiler Obtaining Sensor and Profiler Boards: Bare boards may be ordered directly from OSH Park using these links: INA250 + INA21x Sensor board (order with 2oz copper option selected) Dual INA21x Sensor board (order with 2oz copper option selected) Power Profiler board The sensor boards should be ordered with the 2oz copper option selected to reduce the trace resistance of the target board's current path. No special option is needed for the profiler board. Teensy3.2 boards may be ordered from OSH Park as well, and at a slightly lower price than the manufacturer (PJRC) sells them. Choosing Current Ranges: To choose the value of a shunt resistor, use the following equation: Rsh = Vfs / (Ifs * gain) where: Rsh is the shunt resistance Vfs is the full scale sense amplifier output voltage (3.3V here) Ifs is the full scale current to be measured gain is the gain of the sense amp to be used For example, to measure a 66mA full scale current with a sense amp of gain 1000, Rsh = 3.3V / (0.066A * 1000) = 0.050 Ohms. For sleep/leakage current, say 1mA full scale: Rsh = 3.3V / (0.001 * 1000) = 3.3 Ohms. The pads on both sensor boards for the shunt resistors have been laid out for 0805 SMT resistors. Precision resistors should be used, 1% or better. The highest power dissipation resistor available should be used to minimize resistance change from the shunt resistor heating up; 0805 resistors are typically available with 1/8, 1/4, 1/2 and 1 Watt dissipation. Building and Testing: These boards were designed to be assembled by hand in small quantities. The most difficult components to solder are the ribbon connectors and the SC70 packaged sense amplifiers. A fine tip soldering iron and a microscope are required. Solder wick is helpful for removing solder bridges from between pins (typically the ribbon connector and the sense amplifiers).  Early versions of the profiler board were assembled with header pins soldered to the Teensy and mating female recepticles soldered to the profiler board. Later versions (like in the example below) were assembled with male header pins between the Teensy and the profiler board.  To test the boards after assembly, check for the presence of 8V on the pull-up resistors R5-R8 when a USB cable is plugged into the Teensy. Program the Teensy with suitable application code. Connect the sensor boards to the profiler. Connect all the sensor boards together in series, positive of one to negative of the next and connect to a calibrated current source. (The image below shows an early prototype of the profiler with the sensor boards connected in series. Current is forced through them via the Kelvin contact clips.) Open a terminal window on the host computer. Force known currents and toggle the ranges of each sensor to verify that each sensor operates correctly in both ranges. To check that the profiler measures rail voltage correctly, disconnect the current source and apply the positive side of a voltage source to either side of the sensors still connected in series and connect the ground of the voltage source to a ground point on the profiler. The rail voltage measured by each sensor should match the supplied voltage (0 to 3.3V max). Accuracy/Calibration: After building in excess of 20 sensor boards and 6 profiler boards and checking their measurements against a Keysight B2902 SMU forcing known currents, the profiler system is fairly accurate. Measurements are good down to about 2% of any range's full scale; lower than that gets into the input offset range of the sense amplifier. Individual readings within 1% of that range's full scale when compared against forced current values. No calibration or tuning has been necessary. Measured values should only be considered good to at most 3 significant figures. Limitations: The maximum current through any sensor should be limited to a maximum of 4A. The current limit when using the low range needs to avoid exceeding the power dissipation of the low range shunt resistor. Particularly, the dissipation in the low range shunt resistor can cause resistance changes that would affect measurement accuracy. The voltage of any instrumented rail cannot be greater than 3.3V, the maximum input voltage of the K20's ADC inputs. Minimum resistance the sensor introduces is in high range is about 0.012 to 0.015 Ohms with a 0.002 Ohm shunt. At least 0.005 Ohms comes from the two shorting FETs on the sensor board. The rest comes from the traces on the board as well as the interconnect wires. The bottom line is: the sensor board has to be mounted as closely as possible to the current sense point on the target board. The maximum resistance the sensor introduces depends on the low range shunt. With a 0.020 Ohm low range shunt, the resistance is about 0.025 to 0.030 Ohms. With a 0.050 Ohm low range shunt, the resistance is about 0.065 to 0.075 Ohms. The sensor board needs to be rigidly mounted to prevent ripping up the current sense points on the target board. This can be a challenge when many rails are instrumented. Instrumenting Target Board: When instrumenting a target board, the on-board current sense resistor should be removed. The sensor board should be attached to the target board placed as close as possible to the sense resistor pads. Connection wires to the sensor board should be as short as possible to minimize series resistance. Great care should be taken to prevent movement of the sensor boards that could in turn lift the sense resistor pads off the target board. Foam double sticky tape should be used over clear areas of the target board to avoid dislodging components when the tape is removed. In the photos below, seven power supplies are instrumented on an interposer card. In this example, the sensor boards were affixed to perf board held in place by the headers. Because of the physical constraints of the target board and its power supply card, mounting the sensor boards directly to the interposer was not possible. Four sensors were mounted on one side and three on the other. Notches were cut in the perf board for the sensor's connection wires on the opposite side. Two profiler boards are required for simultaneous use. (Two were also required because the 0.1" headers and jumpers were not installed on the sensor boards to passively short the low-range shunts; all the sensor boards need to be powered to actively short the low-range shunts.)  The positive input of the sensor board (the center of the three connection points) goes to the regulator side of the current sense resistor. The negative input (either of the two outside connections) goes to the i.MX side of the sense resistor. [NOTE: In this example, the power profiler boards have not been fully populated: the thermistor-related components and the micro-SD card socket. The sensor boards were fully populated with the exception of the passive shorting jumper.] Here is another example of a board with six instrumented rails. The sensors in this case are mounted directly on the target board. In this example, the 12V rail is instrumented, which required modding to add a voltage divider to V_RAIL_LOWSIDE on that sensor board.  And here's yet another example of an instrumented i.MX6Q SDB (which still has wires on it from measuring it the old way...). Although it's difficult to see in this photo, all of the sensor boards have a jumper across the low range shunt which permits normal operation of the board without the profiler board attached to provide power to the shorting FETs. Profiler Application Code for Kinetis/Teensy: Below is sample application code for the Teensy for use with four INA250 + INA21x sensor boards populated with the INA250A3 (0.8V/A gain) for the high range and 0.05 Ohm shunts and INA212 (gain 1000). The current range of each channel can be independently changed. This code is also attached below as a file. Data is sent to the host computer over a USB virtual serial port. To reflash/update Teensy code, follow the instructions from PJRC. Download Windows virtual com port driver. /* MIT License (https://spdx.org/licenses/MIT.html) Copyright 2017 NXP Teensy Power Profiler v.2 (revised main board with individual Hi/Lo GPIO, fixed voltage levels, and on-board uSD card socket. Very basic code for the Teensy Power Profiler that sets up the ADCs and controls the GPIO with very basic, single-character serial commands... This version for all INA250A3 on high range, and 0.05Ohms+INA212 (1000 gain) on low range. */ // These constants won't change.  They're used to give names to the pins used: const int LoHiEn1 = 0; const int LoHiEn2 = 1; const int LoHiEn3 = 2; const int LoHiEn4 = 3; const int WakeUp = 5; const int Lo_1 = A0; const int Vrail_1 = A1; const int Hi_1 = A2; const int Lo_2 = A3; const int Vrail_2 = A4;  const int Hi_2 = A5; const int Lo_3 = A6; const int Vrail_3 = A7; const int Hi_3 = A8; const int Lo_4 = A9; const int Vrail_4 = A11; const int Hi_4 = A10; const int Therm1 = A14; #include <math.h> // thermistor temperature calculation stuff... int sensorValue = 0;        // value read from the pot float sensorValuef = 0.0; int B = 4334; // B25/100 value for thermistor NXRT15WF104FA1B040 // other stuff... int delayintvl = 20; int incomingByte; float vrefL = 3.3; float vrefH = 3.3; float vrefV = 3.3; bool one=true;   bool dispone=true; bool two=true;   bool disptwo=true; bool three=true; bool dispthree=true; bool four=true;  bool dispfour=true; int i,j; int num=100; float v1, v2, v3, v4, i1, i2, i3, i4; float il1, il2, il3, il4; void setup() {   // initialize serial communications at 115200 bps:   Serial.begin(115200);   // set analog resolution to 12 bits... (we want more than the 8 default bits...)   analogReadResolution(12);   // set up low/high range wakeup GPIO signals...   pinMode(LoHiEn1, OUTPUT); digitalWrite(LoHiEn1, HIGH);   pinMode(LoHiEn2, OUTPUT); digitalWrite(LoHiEn2, HIGH);   pinMode(LoHiEn3, OUTPUT); digitalWrite(LoHiEn3, HIGH);   pinMode(LoHiEn4, OUTPUT); digitalWrite(LoHiEn4, HIGH);   pinMode(WakeUp, OUTPUT); digitalWrite(WakeUp, HIGH); } void loop() {   // average voltages and currents...   v1=0; v2=0; v3=0; v4=0;   i1=0; i2=0; i3=0; i4=0;   il1=0; il2=0; il3=0; il4=0;   for (i=0; i<num; i++){     v1 = v1+ analogRead(Vrail_1)/4095.*vrefV;     i1 = i1+ analogRead(Hi_1)/4095.*vrefH/0.8*1000;     il1 = il1+ analogRead(Lo_1)/4095.*vrefH/0.05;     v2 = v2+ analogRead(Vrail_2)/4095.*vrefV;     i2 = i2+ analogRead(Hi_2)/4095.*vrefH/0.8*1000;     il2 = il2+ analogRead(Lo_2)/4095.*vrefH/0.05;     v3 = v3+ analogRead(Vrail_3)/4095.*vrefV;     i3 = i3+ analogRead(Hi_3)/4095.*vrefH/0.8*1000;     il3 = il3+ analogRead(Lo_3)/4095.*vrefH/0.05;     v4 = v4+ analogRead(Vrail_4)/4095.*vrefV;     i4 = i4+ analogRead(Hi_4)/4095.*vrefH/0.8*1000;     il4 = il4+ analogRead(Lo_4)/4095.*vrefH/0.05;   }   v1 = v1/num; v2 = v2/num; v3 = v3/num; v4 = v4/num;   i1 = i1/num; i2 = i2/num; i3 = i3/num; i4 = i4/num;   il1 = il1/num; il2 = il2/num; il3 = il3/num; il4 = il4/num;   // print the results to the serial monitor:   if (dispone) {   Serial.print(" RAIL1 (V)= ");  Serial.print(v1);  //Serial.print("\r\n");   if (!one) {Serial.print("    L1 (mA)= ");  Serial.print(il1, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H1 (mA)= ");  Serial.print(i1, 1); }   Serial.print("\r\n");   }   if (disptwo) {   Serial.print(" RAIL2 (V)= ");  Serial.print(v2);  //Serial.print("\r\n");   if (!two) {Serial.print("    L2 (mA)= ");  Serial.print(il2, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H2 (mA)= ");  Serial.print(i2, 1);}    Serial.print("\r\n");   }   if (dispthree) {   Serial.print(" RAIL3 (V)= ");  Serial.print(v3);  //Serial.print("\r\n");   if (!three) {Serial.print("    L3 (mA)= ");  Serial.print(il3, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H3 (mA)= ");  Serial.print(i3, 1);}    Serial.print("\r\n");   }   if (dispfour) {   Serial.print(" RAIL4 (V)= ");  Serial.print(v4);  //Serial.print("\r\n");   if (!four) {Serial.print("    L4 (mA)= ");  Serial.print(il4, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H4 (mA)= ");  Serial.print(i4, 1);}    Serial.print("\r\n");   }   Serial.print("\r\n");   Serial.print("\r\n");   while (Serial.available()) {  // while there are characters in the buffer, grab them all...     incomingByte = Serial.read();  // will not be -1     Serial.print("Incoming byte: "); Serial.print(incomingByte);     // Serial.print("    Delay interval:"); Serial.print(delayintvl);  Serial.print("\r\n");     if (incomingByte == 'h' || incomingByte == 'H'){       Serial.print("\r\n\r\nHelp:\r\n\r\n");       Serial.print("  +/= delay interval +/- 10mS\r\n");       Serial.print("  /- delay interval 20msec/1sec\r\n");       Serial.print("  l/L all rails low/high range in unison\r\n");       Serial.print("  q/w/e/r toggle display of rail 1/2/3/4\r\n");       Serial.print("  1/2/3/4 high range of rail 1/2/3/4\r\n");       Serial.print("  !/@/#/$ low range of rail 1/2/3/4\r\n");       Serial.print("  h print this help...\r\n");       Serial.print("\r\n");       delay(2000);       }     // change delay interval...     if (incomingByte == '+') delayintvl = delayintvl + 10;     if (incomingByte == '=') delayintvl = delayintvl - 10;     if (incomingByte == '_') delayintvl = 20;     if (incomingByte == '-') delayintvl = 1000;     if (delayintvl<1) delayintvl = 20;     // toggle low/high range of all rails in unison...     if (incomingByte == 'L') {       digitalWrite(LoHiEn1, LOW);       digitalWrite(LoHiEn2, LOW);       digitalWrite(LoHiEn3, LOW);       digitalWrite(LoHiEn4, LOW);       one = true; two = true; three = true; four = true;     }     if (incomingByte == 'l') {       digitalWrite(LoHiEn1, HIGH);       digitalWrite(LoHiEn2, HIGH);       digitalWrite(LoHiEn3, HIGH);       digitalWrite(LoHiEn4, HIGH);       one = false; two = false; three = false; four = false;     }     // still unimplemented, but for wakeup of target board...     if (incomingByte == 'w') digitalWrite(WakeUp, LOW);     if (incomingByte == 'W') digitalWrite(WakeUp, HIGH);     // toggle display of rail...     if (incomingByte == 'q') dispone = !dispone;     if (incomingByte == 'w') disptwo = !disptwo;     if (incomingByte == 'e') dispthree = !dispthree;     if (incomingByte == 'r') dispfour = !dispfour;     // change between high/low range..     if (incomingByte == '1') { digitalWrite(LoHiEn1, LOW);  one = true; }     if (incomingByte == '!') { digitalWrite(LoHiEn1, HIGH); one = false;}     if (incomingByte == '2') { digitalWrite(LoHiEn2, LOW);  two = true;}     if (incomingByte == '@') { digitalWrite(LoHiEn2, HIGH); two = false;}     if (incomingByte == '3') { digitalWrite(LoHiEn3, LOW);  three = true;}     if (incomingByte == '#') { digitalWrite(LoHiEn3, HIGH); three = false;}     if (incomingByte == '4') { digitalWrite(LoHiEn4, LOW);  four = true;}     if (incomingByte == '$') { digitalWrite(LoHiEn4, HIGH); four = false;}     }   // wait delayintvl mS after the last reading:   delay(delayintvl); }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Future Work and Improvements Work on a "smart" sensor with a local Kinetis device (KL02Z or KL05Z) on the sensor board itself that has three separate sense amplifiers (one run/high current and two low) has begun. There are several advantages to having a microcontroller on each sensor board: All instrumented rails can be measured simultaneously The sampling rate can be increase over current generation's round robin Measured data is sent over I2C or UART, allowing arbitrary number of rails to be instrumented Each sensor board can provide all its shunt and gain info Sensor board can be used in isolation, i.e., without a master profiler board A GUI interface for the serial data output by the profiler would be really nice... Addditional Information For more information on current measurements in general, see this tutorial series: A Current Sensing Tutorial--Part 1: Fundamentals | EE Times  A Current Sensing Tutorial-Part II: Devices | EE Times  A Current Sensing Tutorial--Part III: Accuracy | EE Times  A Current Sensing Tutorial-Part IV: Layout and Troubleshooting Guidelines | EE Times 
查看全文
The vbs file is a script file in mfgtool. In fsl android lollipop consolidate and later MFGTOOL version, You just need add a new vbs item for new board and have not need to change the ucl2.xml. The below is the example struct. Set wshShell = CreateObject("WScript.shell") wshShell.run "mfgtool2.exe -c ""linux"" -l ""SDCard-Android"" -s ""board=sabresd"" -s ""folder=sabresd"" -s ""soc=6dl"" -s ""mmc=2"" -s ""data_type=-f2fs""" Set wshShell = Nothing Explain for each option: -l: storage type      There three type for android: Nand-Android\eMMC-Android\SDCard-Android -s: extend variable      board: It is used to download uboot and dts in init system.      folder: there are three type: sabresd sabreauto evk                the android image is located in: files/android/%folder%/      soc: Used to define android image name. types: 6q, 6dl, 6sx, 6sl.      mmc: define the storage idex.      data_type: if the type of data partition is f2fs, need define data_type=-f2fs      ldo: if the board is 1.2G, need to define it to -ldo      plus: if the board is 6qp, need too define it to p
查看全文
Purpose:  Introduce how to debug M4 using trace32 and the difference with general debug case.If you are using other jtag debug tools, maybe you need to do the similar configuration. Debug tools: Trace32 – you can refer to http://www.lauterbach.cn/ for more information about this tool. Firmware: Here we using Freertos as the example, but not limited to this. There is one small difference with general debug case to M4 in 6sx, which when you attach M4 and break M4, it may impact the peripheral that A9 is using. You may have found when you break M4, A9 uart console also was frozen at the same time. This is caused by that when M4 enter debug mode, the debug_req will also assert in the peripherals which you are using on the A9 system. So,need configure the peripherals to keep running when the debug_req is assert when do the M4/A9 debug separately. Need configure the DBGEN (*) register in the related peripherals to allow the eripherals not going into debug mode and keep running even if debug_req is HIGH. The peripherals we need take care are: CAN, UART, EPIT,GPT, ENET, PWM. Note: For the CAN, the register bit is called FRZ Here is the details of uart dbgen in the RM: So if we want debug M4 separately,we should disable this bit, as A9 was using this peripheral. Here we take Freertos as the example to illuminate how to debug M4 step by step: Enable DBGEN case: Load M4 image into memory and kick off M4. (You can refer to  for the details)           =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000               ##Starting auxiliary core at 0x9FF00000                ... Attach M4 using the m4.cmm file(attached): Note:  You can find the elf file at the same folder of binary: So now you can debug your code step by step.If you go back to A9 side uart console, you would find the console have been frozen. Disable DBGEN case at A9 side: Load M4 image into memory and kick off M4. (You can refer to  for imx6sx user guide  the details)           =>mm 0x20200b4                              020200b4:00000020 ? 0x820           =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000                ##Starting auxiliary core at 0x9FF00000                ... Attach M4 using the m4.cmm file(attached) In this case you will the A9 uart console still can work, after you break M4. Disable DBGEN case at M4 side: Load M4 image into memory and kick off M4.   =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                     reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000          ##Starting auxiliary core at 0x9FF00000 Attach M4 using the m4_disable_dbgen.cmm  file(attached) In this case you will the A9 uart console still can work, after you break M4.   Notes: For more trace32 usage, please refer to http://www.lauterbach.cn/           For more imx6sx information, please refer to i.MX 6SoloX Family of Applications Processors|NXP.
查看全文
RedBoot is a bootloader, which contains support for some i.MX SoCs. Compiling RedBoot All Boards Compiling RedBoot Configuring RedBoot Configuring RedBoot All Boards Configuring RedBoot Loading Redboot Binary Directly to RAM Minicom Updating RedBoot Updating RedBoot Through RedBoot All Boards Updating RedBoot Through RedBoot IMX27 PDK NAND Flashing RedBoot i.MX31 PDK NAND Flashing RedBoot i.MX35 PDK NAND Flashing Kernel and Root File System Using RedBoot RedBoot Utilities All Boards Transfer Serial RedBoot Fixing Redboot RAM Bug Fixing Redboot RAM bug (CSD1 not activated)
查看全文
The i.MX27 multimedia applications processors balance high performance with low power consumption through an intelligent combination of dedicated hardware video accelerators and a fast ARM926EJ-S™ core. Both the i.MX27 and the i.MX27L processors provide an array of connectivity options and robust security. The rich feature set of the i.MX 27 processors make them an excellent choice for video- and voiceover- IP (V2IP) cordless and mobile phones, intelligent remote controls, point-of-sale terminals, control devices, low to mid end PNDs and many other wireless applications. i.MX Family Comparison Product Information on Freescale.com i.MX27 Multimedia Applications Processor i.MX27L Multimedia Applications Processor Evaluation/Development Boards and Systems IMX27PDK:  i.MX27 Development Kit Bootloader Compiling U-Boot for iMX27ADS Installing U-Boot on iMX27ADS Embedded Software and Tools Android OS for i.MX Applications Processors Partners / 3rd-Party Development Tools STK5:  Starter-Kit V for TX Modules with Freescale i.MX Processors (Karo Electronics) Additional Resources i.MX27 ADS Adding USB Host2 i.MX27 D1 Capture Kernel 2.6.22 Compiling U-Boot for i.MX27ADS IMX27-ADS i.MX27 ADS Board Flashing I.MX27 ADS Board Video i.MX27 ADS Board TV Out i.MX 27 ADS Adding USB Host2 i.MX 27 ADS Board Video GST Encode i.MX 27 ADS Board Video GST Play i.MX 27 ADS Compiling Linux Kernel Mainline i.MX 27 mDDR Issue i.MX 27 PDK I.MX27 PDK Board Flashing IMX27-Lite-Kit i.MX 27 Video GST Caps Installing U-Boot on i.MX27ADS
查看全文
Measuring only 20mm x 50mm, the DART-MX6 from Variscite is the smallest System-on-Module (SoM) supporting Freescale’s i.MX6 quad and dual core ARM Cortex-A9™ processor. The DART-MX6 offers impressive performance and scalability. Together with optimized power consumption this miniature sized SoM is ideal for portable and battery operated embedded systems. The DART-MX6 highly integrated connectivity includes dual band Wi-Fi/BT with optional MIMO, dual USB, Gigabit Ethernet, PCIe and A/V interfaces. Furthermore, the system supports industrial operating temperatures. Performing as the DART-MX6 carrier board, the VAR-DT6CustomBoard completes an attractive full reference kit, which can be used for customers’ evaluation, development and end-product mass production. Key features of the DART-MX6 include: - Miniature size: 20mm x 50mm x 4mm - Freescale i.MX6 800MHz Quad/Dual ARM Cortex-A9 - Up to 1GB LP-DDR2 and 32GB eMMC - Certified Wi-Fi 802.11 a/b/g/n 2.4/5GHz with optional 2x2 MIMO - Bluetooth 4.0/BLE - Full 1080p video encode/decode capability - Vivante GPU 2D/3D graphics accelerator - Display: 2x LVDS, HDMI1.4, MIPI DSI - 10/100/1000 Mbps Ethernet - USB 2.0: Host, OTG - PCIe - Audio In/Out - Camera inputs: MIPI CSI, parallel - Dual CAN, UART, I2C, SPI - Industrial temperature - OS: Linux Yocto, Android Availability and Pricing: The DART-MX6 SoM and development kits are available now. Email [email protected] or call +972 9 9562910 for more information About Variscite: Variscite is a leading System on Modules (SoM) and Single-Board-Computer (SBC) design and manufacture company. A trusted provider of development and production services for a variety of embedded platforms, Variscite transforms clients’ visions into successful products. Learn more about Variscite, visit www.variscite.com
查看全文
In every i.MX BSP you will find a pre-compiled binary to flash on your board, but if you need to recompile, this tutorial will be useful. Redboot source code and pre-built images for many platforms are available on Linux Board Support Package (BSP). As an example, let's compile redboot version 2009_10 that comes with Freescale Linux BSP.   For detailed information about Redboot, check <redboot_folder>/doc Locate the file ecostools.tar.gz and decompress it on /opt directory. (Create this folder if it is not there) $ cd /opt $ sudo tar zxvf <redboot_folder>/tools/ecos_config_tools.tar.gz $ sudo tar zxvf <redboot_folder>/tools/arm-2008q1.tar.gz This creates /opt/ecostools directory with two subdirectories: arm-2008q1 -- GNU tools for compiling, linking, etc. tools -- mainly to have ecosconfig utility program Add /opt/arm-2008q1/bin and /opt/tools/bin to your environment PATH variable. $ export PATH=$PATH:/opt/arm-2008q1/bin:/opt/tools/bin Generating RedBoot Image Decompress the ecos-trunk-080727.tar.bz2 base line source code into <redboot_folder>/src. There should be a 'packages' directory under <redboot_folder>/src/ecos if it is done correctly. $ tar xjvf ecos-trunk-080727.tar.bz2 Go to ecos subdirectory and apply the patches; $ cd ecos $ bunzip2 -c patch-redboot-200910-base.bz2 | patch -p1 The above command assumes the patch file is under the same directory as the <redboot_folder>/src/ecos. Specify the path name for the patch file if necessary. Apply the patch for specific platform. In this case, the used patch is: patch-redboot-200834-mx3.bz2 $ patch-redboot-200910-mx3.bz2 | patch -p1 Define the ECOS_REPOSITORY. On <redboot_folder>, put the entire (absolute) path to redboot folder. I.e. ~/<redboot_folder>/src/ecos/packages $ export ECOS_REPOSITORY=<redboot_folder>/src/ecos/packages To build redboot (for i.MX31 in this example), create a new folder in order to have a clean build: $ mkdir new_redboot $ cd new_redboot $ ecosconfig new mx31_3stack redboot $ ecosconfig import $ECOS_REPOSITORY/hal/arm/mx31/3stack/current/misc/redboot_ROMRAM.ecm $ ecosconfig tree $ make This creates the Redboot image (redboot.bin) under install/bin directory. This image can run from either SDRAM or flash. Note: You can change the board MACH-TYPE at this file: src/ecos/packages/hal/arm/mx27/ads/current/cdl/hal_arm_board.cdl
查看全文
Hello i.MX Community. Attached there is a guide on How to Use an Older Uboot version with 3.1x.xx Kernel Version I hope you find the document and Sample provided useful! Regards!
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343116 
查看全文
Using a USB Touchscreen on Ubuntu   This example uses a XENARC 706TSA monitor http://www.xenarc.com/product/706tsa.html To use a USB touchscreen on i.MX51 EVK, disable all touchscreen drivers on menuconfig and build the kernel: Device Drivers  --->        Input device support  --->        [ ]   Touchscreens  ---> Download xserver-xorg-input-evtouch (0.8.8-ubuntu3 version) from http://launchpadlibrarian.net/24760784/xserver-xorg-input-evtouch_0.8.8-0ubuntu3_armel.deb. X crash is found if using latest 0.8.8-ubuntu6.1 version. For the details. See https://bugs.launchpad.net/ubuntu/+source/xf86-inputevtouch/+bug/511491 On MX51 EVK board, run “sudo dpkg –i xserver-xorg-input-evtouch_0.8.8-0ubuntu3_armel.deb” to install debian package. Add fdi file by "sudo vi ./usr/share/hal/fdi/policy/20thirdparty/50-eGalax.fdi": <?xml version="1.0" encoding="UTF-8"?> <deviceinfo version="0.2">    <device>       <match key="info.product" contains="eGalax">          <match key="info.capabilities" contains="input">             <merge key="input.x11_driver" type="string">evtouch</merge>             <merge key="input.x11_options.minx" type="string">130</merge>             <merge key="input.x11_options.miny" type="string">197</merge>             <merge key="input.x11_options.maxx" type="string">3945</merge>             <merge key="input.x11_options.maxy" type="string">3894</merge>             <merge key="input.x11_options.Rotate" type="string">CCW</merge>             <merge key="input.x11_options.Swapy" type="string">true</merge>             <merge key="input.x11_options.taptimer" type="string">30</merge>             <merge key="input.x11_options.longtouchtimer" type="string">750</merge>             <merge key="input.x11_options.longtouched_action" type="string">click</merge>             <merge key="input.x11_options.longtouched_button" type="string">3</merge>             <merge key="input.x11_options.oneandhalftap_button" type="string">2</merge>             <merge key="input.x11_options.movelimit" type="string">10</merge>             <merge key="input.x11_options.touched_drag" type="string">1</merge>             <merge key="input.x11_options.maybetapped_action" type="string">click</merge>             <merge key="input.x11_options.maybetapped_button" type="string">1</merge>          </match>       </match>    </device> </deviceinfo> Save above configuration. Calibrating Calibration in made by clicking on System -> Administration -> Calibrate Touchscreen Follow the on screen instructions and reboot the system. Calibrating using Xinput Calibrator Xinput_calibrator is another option to calibrate touchscreen. It can be downloaded at: http://www.freedesktop.org/wiki/Software/xinput_calibrator On i.MX5x Ubuntu, unpack the source code: tar -xzvf xinput_calibrator-0.7.5.tar.gz Install xorg-dev, it's required to build xinput_calibrator sudo apt-get install xorg-dev Configure, build and install xinput_calibrator ./configure ./make ./make install Execute xinput_calibrator. A four-point calibration screen will be shown. Follow the instructions on screen and after complete xinput_calibrator will return the calibration parameters. Replace the given calibration parameters on file /usr/share/hal/fdi/policy/20thirdparty/50-eGalax.fdi and reboot the system.
查看全文
A discussion of random hangs and other issues using Windows Embedded Compact on Freescale i.MX6 application processor and how they were solved. This white paper is about the investigation and shares some of our discoveries. All information in this document applies to Windows Embedded Compact 7 and 2013 as well as all variants of the i.MX6.    
查看全文
Some processor’s GPIO settings on the i.MX Pins Tool version 7 may not show allow to select direction and just show an option “Input/Output” as shown. This will be fixed, but the settings can be changed on the local processor data as a workaround. For more information and documentation for the Pins Tool for i.MX please visit its home page on the link below: https://www.nxp.com/design/designs/pins-tool-for-i-mx-application-processors:PINS-TOOL-IMX   First, find where the Pins Tool data package is stored. To do this open the Pins Tool and click Help > About. On the About screen click the Details button. Take also note of the name of the package that needs to be fixed.   Go to the location where the data package is stored and find the processor data. The file that would need to be updated is signal_configuration.xml    Find the GPIO pin data and change the directions from the string ““inOut”to the string “in out”. Then save this file.    Close and reopen the Pins Tool. The direction on the updated package should now show the options Input and Output.  
查看全文
Quick notes on testing audio on the i.MX 8QuadMax MEK board with 4.19.35-1.1.0 BSP. Hardware:   - Connect the MCIMX8QM-CPU to the MCIMX8-8X-BB.  - Connect the IMX-AUD-IO to the Audio Slot 1 on the MCIMX8-8X-BB.  - Short 2 and 3 on J47 on the MCIMX8-8X-BB  - Connect an external powered speaker to RCA connectors Audio OUT FR and/or Audio OUT FL on the IMX-AUD-IO  - Optionally, connect a headphone on J15 on the MCIMX8QM-CPU   Test: Power on the board. aplay -l shows the audio interface available. root@imx8qmmek:~# aplay -l **** List of PLAYBACK Hardware Devices **** card 0: cs42888audio [cs42888-audio], device 0: HiFi cs42888-0 [] Subdevices: 1/1 Subdevice #0: subdevice #0 card 0: cs42888audio [cs42888-audio], device 1: HiFi-ASRC-FE (*) [] Subdevices: 1/1 Subdevice #0: subdevice #0 card 1: wm8960audio [wm8960-audio], device 0: HiFi wm8960-hifi-0 [] Subdevices: 1/1 Subdevice #0: subdevice #0 card 2: imxaudmix [imx-audmix], device 0: HiFi-AUDMIX-FE (*) [] Subdevices: 1/1 Subdevice #0: subdevice #0 card 2: imxaudmix [imx-audmix], device 1: HiFi-AUDMIX-FE (*) [] Subdevices: 1/1 Subdevice #0: subdevice #0 Play file on powered speaker via cs42888: root@imx8qmmek:~# aplay -Dhw:0,0 test.wav Playing WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 48000 Hz, Stereo Play file on headphone via wm8960: root@imx8qmmek:~# aplay -Dhw:1,0 test.wav
查看全文
Q: What is latency figures for the VPU to decode Device: i.MX6Q OS: Linux Resolution:                         1920x1080(HD) Frame rate:                        30 FPS Function:                             Overlay messages. Input/Output:                   8 bit / YUV 4:2:0 / NAL stream Profile level:                      4.1. Constrained Baseline. I and P frames support. A: It depend on the syntax in H.264, includes num_reorder_frames,max_dec_frame_buffering,num_ref_frames,MaxDpbSize,etc. for start latency: it cover vpu driver loading, allocate buffers, init, decoding the first frame less than 100ms on iMX6/Linux. This document was generated from the following discussion: VPU Latency i.MX6
查看全文
[Brief description] (1)Contents The ducoment introduced how to expand Gigabit Ethernet based on i.MX6 PCI Express, and attached schematics in DSN & pdf format. (2)Binary file for EEROM I have the binary file used to debug intel82574 circuit in this schematic, If customer wants to use it to debug board based on i.MX6+Intel82574, she can submit a case for me to get the file by our Salesforece system. Best Regards, TIC Weidong Sun Email: [email protected]
查看全文
    The document is about how to use WSL2 to compile yocto(android is the same process)  
查看全文
We use flash header which will be access by ROM code to do the NAND boot or secure boot. This is a document introduce the flash header.
查看全文