i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Question: The code signing tool(CST) of i.MX6 with "CST -h" command just for viewing help message took about 22 minutes. On other system, it was shorter but still took about 2 minutes. CST version is BLN_CST_MAIN_02.00.00. More test results: 1. Print help message => 4 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --help && date Fri Oct 18 14:10:52 KST 2013 Fri Oct 18 14:15:01 KST 2013 2. Signing 512MB file => 11 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_system.csf" < "example_system.csf" && date Fri Oct 18 14:15:01 KST 2013 CSF Processed successfully and signed data available in out_system.csf Fri Oct 18 14:25:47 KST 2013 3. Signing 3MB file => 17 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_kernel.csf" < "example_kernel.csf" && date Fri Oct 18 14:25:47 KST 2013 CSF Processed successfully and signed data available in out_kernel.csf Fri Oct 18 14:42:39 KST 2013 4. Signing 160KB file => 2 min. dnlk@bauer-mm2014:~/secureboot/bBLN_CST_MAIN_02.00.00/linux$ date && ./cst --output "out_uboot.csf" < "example_uboot.csf" && date Fri Oct 18 14:42:39 KST 2013 CSF Processed successfully and signed data available in out_uboot.csf Fri Oct 18 14:45:05 KST 2013 Answer: The slow performance is caused by lack of entropy source and it takes long time to initialize random number generator. Check amount of entropy  "cat /proc/sys/kernel/random/entropy_avail" Tried to install package rng-tools. 1. $sudo apt-get install rng-tools 2. add the following settings in /etc/default/rng-tools HRNGDEVICE=/dev/urandom RNGDOPTIONS=”-W 90% -t 1? 3. sudo /etc/init.d/rng-tools restart 4. cat /proc/sys/kernel/random/entropy_avail After rng-tools starts, entropy increases from less than 100 to more than 1000, then command ./cst -h can run very smoothly.
View full article
With Qt5  you will find the addition of new technologies that will make your development much easier. Qtquick2 SceneGraph Qml Qt5 is backwards compatible,  that means you can run your Qt 4.8 applications, But that doesn't mean they will have the best performance, sometimes it is better to do a porting to use the newest features. Qt5, has two options to paint components into the screen. Painting in Qt 5 is primarily done either with: The imperative QPainter API Qt’s declarative UI language, QML, and its scene graph back-end. QPainter As this document mentions  Qt5GraphicsOverview | Qt Wiki | Qt Project  The Qpainter engine uses software to paint, and is used when drawing Qimages or Qwidgets. Its  advantage over OpenGL is the high quality when antialiasing is enabled, and a complete feature set. The Qpainter can use an OpenGL engine, but as the document mentions it is more suceptible to state changes. And has to be used carefully. QML & Scene Graph. All visual QML items are rendered using the scene graph, a low-level, high-performance rendering stack, closely tied to OpenGL. Qt Quick 2 makes use of a dedicated scene graph based on OpenGL ES 2.0 or OpenGL 2.0 for its rendering. Using a scene graph for graphics rather than the traditional imperative painting systems (QPainter and similar), means the scene to be rendered can be retained between frames and the complete set of primitives to render is known before rendering starts. This opens up for a number of optimizations, such as batch rendering to minimize state changes and discarding obscured primitives. The QML scene graph is a new back-end for QML in Qt 5, and is based on OpenGL. It generally improves the performance of QML significantly over the QPainter-based back-end used in Qt 4. It achieves better performance in a number of ways: The scene graph uses OpenGL directly instead of going though a QPainter which could be using either the raster or OpenGL paint engine. This means that all the resources, like geometry, textures and shaders can be stored in a format suitable for OpenGL rather than using classes such as QPainterPath, QPixmap, QBrush, or QPen, which the QPainter would need to translate into OpenGL primitives and possibly cache. QML, being a declarative language, defines how the end result should look like, but it doesn’t define how and in which order each individual element is drawn. The drawing can therefore be reordered to reduce the number of state changes, or merged to reduce the number of draw calls. The scene graph uses a separate render thread, and synchronizes the animations with the vertical retrace on platforms where this can be supported. The render thread allows the preparation of the next frame to be done at the same time the current frame is being rendered. This has a positive effect also on single-core systems, since the render thread might block on OpenGL commands. The synchronization with the vertical retrace improves the perceived smoothness of the animations. We have tested on i.MX6 Both options, having the best results using QML Qtquick2 elements. When we tried using QtPainter via Widgets we face the problem that if not using a windowing system like X11 or Wayland the painter wont work well and will only show the QtGLWidget. With QML scene graph we are able to have an OpenGL element and a Qt element on the same environment, and there is an easy way to communicate one with the other and share variables.  Please look at the example results here: I.MX6 scene graph Qt5 - YouTube And the great advantage, the sceneGraph is all accelerated via OpenGL.
View full article
Tested on imx28 EVK Rev. D. When plug-in or plug-out cable on eth0 port, eth1 port (and vice versa) will also be reset and the communication will be interrupted. Reason: Both Ethernet PHYs on EVK board share the same GPIO as their reset pin, in software the function name is mx28evk_enet_gpio_init. So any call to pdata->init() in fec.c will reset both PHY at the same time. In order to avoid such problem, you have to use 2 individual GPIO for the PHY reset.
View full article
Question: How to enable HAB on the MX28, following the recommendations of AN4555 to get the "get_hab_status()" function working, but has run into an issue. Question #1 They believe they have all the HAB components worked out that are inputs to the efltosb tool as they are able to successfully run U-boot to the interactive prompt.  However, at the point where they:     - call the rvt_report_status() function, their board says "### ERROR ### Please RESET the board ###".      - call the rvt_entry(), their board prints some garbage characters on the screen and then hangs. This suggests that there is something wrong with the clock that in turn affects the baudrate on the serial console causing the above behavior. Question #2 Is there a concept of a "Bound Signature" in HABv4 as there is in HABv3? Any chance the addresses for the rvt_ calls are incorrect? Can you provide the u-boot source? Either Bound signature verification or UID is never mentioned in the HABv4 Application Note. So I suppose it is not supported. We have made assumptions about the RVT function pointer offsets.  The HAB 4 API does not explicitly say the offsets but uses a rvt_base::function_name notation.  We have assumed that function pointers are placed in order, at every word offset beyond the RVT header.  We have confirmed the RVT header exists at the latest address in the reference manual based on a memory dump but we cannot be certain the function offsets we have setup are correct. As far as source code, we modeled our changes for our mx28 board off of the hab.c and hab.h files available from the mainline u-boot for the mx6 architecture. This is basically the same code get_hab_status code that is written in the AN4555 document.  We did HAB API function pointer addresses to match the updated RVT base address and assumed offsets. Answer: Here are the first 3 instructions from report_status(), could your customer check the instructions from the address which they called is correct? <report_status>: :   b087b570        addlt   fp, r7, r0, ror r5 :   1c0e1c05        stcne   12, cr1, [lr], {5} :   22182433        andscs  r2, r8, #855638016      ; 0x33000000
View full article
Video decoding gst-launch filesrc location=sample.mp4 ! qtdemux ! ffdec_h264 ! mfw_v4lsink Notes: On LTIB BSP 3.0.35_4.0.0, prep the package and apply the attached patch on top, then build. On Yocto, the easy way to add the gst-ffmpeg package is by adding these two lines on the conf/local.conf file: IMAGE_INSTALL_append = " gst-ffmpeg" LICENSE_FLAGS_WHITELIST = 'commercial'
View full article
File related to the following question: MX53 u-boot Splash Screen support
View full article
In Chinese Twitter: Sino Weibo, one famous distributor mentioned “i.MX28 is the best choice in ARM9 core-based processor, no ‘one of’”. With high integration of analog module and digital module, i.MX28 is attracting more and more engineers in various applications. Despite its advantage, there are some mistakes one may commit or issues they may meet. The note records a number of issues/mistakes. Each case in the note comes from a real story. I hope the note will help you in your development work. And It is definitely welcomed for everyone to add your own content to the note.The more you share, the more you get.
View full article
NOTE: Always de-power the target board and the aggregator when plugging or unplugging smart sensors from the aggregator. NOTE: See this link to instrument a board with a Smart Sensor. This page documents the triple-range "smart" current sensor that's part of a larger system for profiling power on application boards. The smart sensor features a Kinetis KL05Z with three current sense amplifiers. It allows measurement currents in three ranges. Four assembly options allow measurement of rail voltages 0-3.3V (two overall current ranges), 0-6.6V, and 12V. It connects to an aggregator, which powers, controls and aggregates data from a number of smart sensor boards. One of the biggest improvements over the older dual-range measurement system is that the on-sensor microcontroller allows near-simultaneous measurement of all instrumented rails on a board. The dual range profiler can only make one measurement at a time.  These are intended to be used with a microncontroller board to act as a trigger and data aggregator. This aggregator could also be used to reprogram the sensors.  The series resistance added by the smart sensor when in run mode (highest current range) is under 11 milliOhms as measured with 4-point probes and a Keysight B2902B SMU.  A "power oscilloscope" can be made by triggering measurements at regular intervals and presenting the results graphically.... Schematic: Board Layout, Top: Board Layout, Bottom: Here's a photo of two with a nickel is included to show scale. The board measures about 0.5 by 1.3 inches. Connections: The smart sensor header connections are: 5V: powers the 3.3V regulator, which in turn powers everything else on the sensor board 12V: all the gates of all the switching FETs are pulled pulled up to 12V GND: ground connection SCL/TX: I2C clock line  SDA/RX: I2C data line  SWD_CLK:  line for triggering smart sensors to make measurements RESET_B:  line for resetting the smart sensor board SWD_IO: select line for the smart sensor Theory of operation: Three shunts and current sense amplifiers are used to measure current in three ranges. One shunt/sense amp pair has a 0.002Ω shunt integrated into the IC package (U1, INA250). The other two sense amps (U2 and U3, INA212) require an external shunt.  FETs Q1, Q2,  and Q3 are used to switch the two lower range shunt/sense amp pairs in and out of circuit. In normal run operation (highest current range), Q1 (FDMC012N03, with Rds(on) under 1.5mΩ) is turned on, which shorts leaves only U1 in circuit. FETs Q4, Q5 and Q6 translate the voltages to 3.3V so that GPIO on U4 (MCU KL05Z) can control them.  Rail voltage measurement is facilitated via resistors R3, R4, and R12 and Q7. Not all of these are populated in every assembly option. For measuring rail voltages 0-3.3V, R12 is populated. To measure 0-6.6V, R3, R4,and Q7 are populated. When turned on Q7 enables the voltage divider. All of the assembly option population info can be found in the schematic (attached). Regulator U5 (AP2210N) provides the 3.3V supply for all of the components on the board. This 1% tolerance regulator is used to provide a good reference for the ADC in U4.  Microcontroller U4 detects the assembly population option of the board via resistors R9, R10, and R11 so that the same application code can be used across all variations of the sensor boards. GPIO control the FETs and four ADC channels are used to measure the sense amplifier outputs and the rail voltage. Having a microcontroller on the sensor board allows the user to do extra credit things like count coulombs as well as allowing all similarly instrumented rails to measure at the same time via trigger line SWD_CLK. Data communication can be via I2C or UART, since these two pins can do both.  But if multiple sensor boards are to be used with an aggregator, communication needs to be over I2C. Application Code: The latest application code for the KL05Z on the smart sensor resides here: https://os.mbed.com/users/r14793/code/30847-SMRTSNSR-KL05Z/. The latest binary is attached below. In order to re-flash a smart sensor, the modification detailed in the aggregator page needs to be made. Once the modification is completed, leave the aggregator unpowered while pluging the SWD debugger into J5 and the smart sensor to be programmed into JP15. Very old UART-based application code for the KL05Z, built in the on-line MBED compiler (note that it requires the modified mbed library for internal oscillator). This code was used while testing the first smart sensor prototypes. It has since been abandoned. It's published here in the event that a user wants to use a single sensor plugged into JP15 with UART breakout connector J6. /****************************************************************************** * * MIT License (https://spdx.org/licenses/MIT.html) * Copyright 2017-2018 NXP * * MBED code for KL05Z-based "smart" current sensor board, basic testing * of functions via UART (connected via FRDM board and OpenSDA USB virtual * COM port). * * Eventual goal is to have each smart sensor communicate over I2C to an * aggregator board (FRDM board with a custom shield), allowing 1-10 power * supply rails to be instrumented. Extra credit effort is to support * sensors and aggregator with sigrok... * * Because there is no crystal on the board, need to edit source mbed-dev library * to use internal oscillator with pound-define: * change to "#define CLOCK_SETUP 0" in file: * mbed-dev/targets/TARGET_Freescale/TARGET_KLXX/TARGET_KL05Z/device/system_MKL05Z4.c * ******************************************************************************/ #include "mbed.h" // These will be GPIO for programming I2C address... // not yet implemented, using as test pins... DigitalOut addr0(PTA3); DigitalOut addr1(PTA4); DigitalOut addr2(PTA5); DigitalOut addr3(PTA6); // configure pins for measurements... // analog inputs from sense amps and rail voltage divider... AnalogIn HIGH_ADC(PTB10); AnalogIn VRAIL_ADC(PTB11); AnalogIn LOW1_ADC(PTA9); AnalogIn LOW2_ADC(PTA8); // outputs which control switching FETs... DigitalOut VRAIL_MEAS(PTA7); // turns on Q7, connecting voltage divider DigitalOut LOW_ENABLE(PTB0); // turns on Q4, turning off Q1, enabling low measurement DigitalOut LOW1(PTB2); // turns on Q5, turning off Q2, disconnecting shunt R1 DigitalOut LOW2(PTB1); // turns on Q6, turning off Q3, disconnecting shunt R2 // input used for triggering measurement... // will eventually need to be set up as an interrupt so it minimizes delay before measurement InterruptIn trigger(PTA0); // use as a trigger to make measurement... // PTB3/4 can be used as UART or I2C... // For easier development with one smart sensor, we are using UART here... Serial uart(PTB3, PTB4); // tx, rx long int count=0; int n=25; // global number of averages for each measurement int i, temp; bool repeat=true; // flag indicating whether measurements should repeat or not const float vref = 3.3; // set vref for use in calculations... float delay=0.25; // default delay between measurement bool gui = false; // flag for controlling human vs machine readable output bool statistics = false;// flag for outputting min and max along with average (GUI mode only) void enableHighRange(){ LOW_ENABLE = 0; // short both low current shunts, close Q1 wait_us(5); // delay for FET to settle... (make before break) LOW1 = 0; LOW2 = 0; // connect both shunts to make lower series resistance VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(250); // wait for B2902A settling... } void enableLow1Range(){ LOW1 = 0; LOW2 = 1; // disconnect LOW2 shunt so LOW1 can measure wait_us(5); // delay for FET to settle... (make before break) LOW_ENABLE = 1; // unshort low current shunts, open Q1 VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(250); // wait for B2902A settling... } void enableLow2Range(){ LOW1 = 1; LOW2 = 0; // disconnect LOW1 shunt so LOW2 can measure wait_us(5); // delay for FET to settle... (make before break) LOW_ENABLE = 1; // unshort low current shunts, open Q1 VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(500); // wait for B2902A settling... } void enableRailV(){ VRAIL_MEAS = 1; // turn on Q7, to enable R3-R4 voltage divider wait_us(125); // wait for divider to settle... // Compensation cap can be used to make // voltage at ADC a "square wave" but it is // rail voltage and FET dependent. Cap will // need tuning if this wait time is to be // removed/reduced. // // So, as it turns out, this settling time and // compensation capacitance are voltage dependent // because of the depletion region changes in the // FET. Reminiscent of grad school and DLTS. // Gotta love device physics... } void disableRailV(){ VRAIL_MEAS = 0; // turn off Q7, disabling R3-R4 voltage divider } // this function measures current, autoranging as necessary // to get the best measurement... void measureAuto(){ Timer t; float itemp; float tempI=0; float imin = 1.0; // used to keep track of the minimum... float imax = 0; // used to keep track of the maximum... t.start(); // use timer to see how long things take... enableHighRange(); // this should already be the case, but do it anyway... for (i = 0; i < n; i++){ itemp = HIGH_ADC; // read HIGH range sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/0.8; // compute average we just took... if (gui) uart.printf("=> %5.3f ", tempI); if (statistics && gui) uart.printf("[%5.3f/%5.3f] ", imin*vref/0.8, imax*vref/0.8); // if current is below this threshold, use LOW1 to measure... if (tempI < 0.060) { if (!gui) uart.printf("... too Low: %f A, switching to low1 ==>\r\n", tempI); tempI=0; enableLow1Range(); // change FETs to enable LOW1 measurement... imin = 1.0; imax = 0; for (i = 0; i < n; i++){ itemp = LOW1_ADC; // read LOW1 sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/0.05/1000; // compute average we just took... if (gui) uart.printf("%6.4f ", tempI); if (statistics && gui) uart.printf("[%6.4f/%6.4f] ", imin*vref/0.05/1000, imax*vref/0.05/1000); // if current is below this threshold, use LOW2 to measure... if (tempI < 0.0009){ if (!gui) uart.printf("... too Low: %f A, switching to low2 ==>\r\n", tempI); tempI=0; enableLow2Range(); // change FETs to enable LOW1 measurement... imin = 1.0; imax = 0; for (i = 0; i < n; i++){ itemp = LOW2_ADC; // read LOW2 sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/2/1000; // compute average we just took... if (gui) uart.printf("%8.6f ", tempI); if (statistics && gui) uart.printf("[%8.6f/%8.6f] ", imin*vref/2/1000, imax*vref/2/1000); } } t.stop(); // stop the timer to see how long it took do do this... enableHighRange(); if (!gui) uart.printf("\r\nCurrent = %f A Current Measure Time = %f sec\r\n", tempI, t.read()); } // the autoranging should really be done with functions that return values, as should the // functions below... This would make for shorter and more elegant code, but the author // is a bit of a pasta programmer... void measureHigh(){ float highI=0; enableHighRange(); for (i = 0; i < n; i++){ highI += HIGH_ADC; } highI = highI/n; uart.printf("HIghI = %f A\r\n", vref*highI/0.8); } void measureLow1(){ float low1I=0; enableLow1Range(); for (i = 0; i < n; i++){ low1I += LOW1_ADC; } enableHighRange(); low1I = low1I/n; uart.printf("low1I = %f A\r\n", vref*low1I/0.05/1000); } void measureLow2(){ float low2I=0; enableLow2Range(); for (i = 0; i < n; i++){ low2I += LOW2_ADC; } enableHighRange(); low2I = low2I/n; uart.printf("low2I = %f A\r\n", vref*low2I/2/1000); } // measure the rail voltage, default being with // a divide by 2 resistor divider // It has to be switched out when not in use or it will // add to the measured current, at least in the low ranges... void measureRailV(){ float railv=0; float mult = vref*2; // since divide by 2, we can measure up to 6.6V... float vmin = 5; float vmax = 0; float vtemp; enableRailV(); // switch FETs so divider is connected... for (i = 0; i < n; i++){ vtemp = VRAIL_ADC; // read voltage at divider output... if (statistics && vtemp>vmax) vmax = vtemp; // update max if necessary if (statistics && vtemp<vmin) vmin = vtemp; // update min if necessary railv += vtemp; // add current sample to running sum } disableRailV(); // now disconnect the voltage divider railv = railv/n; // compute average (note this is in normalized ADC [0..1]) // Convert to voltage by multiplying by "mult" if (!gui) uart.printf("RailV = %5.3f V ", mult*railv); if (gui) uart.printf("%5.3f ", mult*railv); if (statistics && gui) uart.printf("[%5.3f/%5.3f] ", mult*vmin, mult*vmax); uart.printf("\r\n"); } // not sure how useful this function is... void measureAll(){ measureHigh(); measureLow1(); measureLow2(); measureRailV(); } // test function to see if trigger pin is being hit... // intended for use later to do timed triggering of measurements... void triggerIn(){ uart.printf("You're triggering me! \r\n"); measureAll(); } // main... int main() { // set up basic conditions... Timer m; uart.baud(115200); enableHighRange(); // default state - only HIGH sense amp in circuit, no divider // signal that we're alive... uart.printf("Hello World!\r\n"); // configure the trigger interrupt... trigger.rise(&triggerIn); while (true) { count++; wait(delay); if (repeat){ // if repeat flag is set, keep making measurements... m.reset(); // reset and start timer... m.start(); measureAuto(); // measuring current using auto-ranging... measureRailV(); // measure rail voltage... m.stop(); // stop the timer. if (!gui) uart.printf(" Total Measure Time = %f sec", m.read()); if (!gui) uart.printf("\r\n\r\n"); } // see if there are any characters in the receive buffer... // this is how we change things on the fly... // Commands (single keystroke... it's easier) // t = one shot automeasure // v = measure volt // h = one shot high measure // k = one shot LOW1 measure // l = one shot LOW2 measure (letter l) // r = toggle repeat // R = turn off repeat // + = faster repeat rate // - = slower repeat rate // = = set repeat rate to 0.25 sec // g = use human readable text output // G = use compressed text format for GUI // s = turn statistics output off // S = turn statistics output on (only in GUI mode) // n = decrease number of averages for each measurement // N = increase number of averages for each measurement // // these were for testing FET switching... // 1 = LOW_ENABLE = 0 (the number 1) // 2 = LOW1 = 0 // 3 = LOW2 = 0 // 4 = VRAIL_MEAS = 0 // ! = LOW_ENABLE = 1 // @ = LOW1 = 1 // # = LOW2 = 1 // $ = VRAIL_MEAS = 1 if (uart.readable()){ temp = uart.getc(); if (temp==(int) 't') { if (!gui) uart.printf("Keyboard trigger: "); measureAuto(); measureRailV(); //measureAll(); } if (temp==(int) 'v') { uart.printf("Keyboard trigger: "); measureRailV(); } if (temp==(int) 'h') { uart.printf("Keyboard trigger: "); measureHigh(); } if (temp==(int) 'k') { uart.printf("Keyboard trigger: "); measureLow1(); } if (temp==(int) 'l') { uart.printf("Keyboard trigger: "); measureLow2(); } if (temp==(int) '1') { LOW_ENABLE = 0; uart.printf("Keyboard trigger: LowEnable = %d\r\n", 0); } if (temp==(int) '2') { LOW1 = 0; uart.printf("Keyboard trigger: LOW1 = %d\r\n", 0); } if (temp==(int) '3') { LOW2 = 0; uart.printf("Keyboard trigger: LOW2 = %d\r\n", 0); } if (temp==(int) '4') { VRAIL_MEAS = 0; uart.printf("Keyboard trigger: VRAILMEAS = %d\r\n", 0); } if (temp==(int) '!') { LOW_ENABLE = 1; uart.printf("Keyboard trigger: LowEnable = %d\r\n", 1); } if (temp==(int) '@') { LOW1 = 1; uart.printf("Keyboard trigger: LOW1 = %d\r\n", 1); } if (temp==(int) '#') { LOW2 = 1; uart.printf("Keyboard trigger: LOW2 = %d\r\n", 1); } if (temp==(int) '$') { VRAIL_MEAS = 1; uart.printf("Keyboard trigger: VRAILMEAS = %d\r\n", 1); } if (temp==(int) 'r') { repeat = !repeat; uart.printf("Keyboard trigger: repeat toggle: %s \r\n", repeat ? "true" : "false"); } if (temp==(int) 'R') repeat = false; if (temp==(int) '+') { delay -= 0.05; if (delay<0.05) delay = 0.05; } if (temp==(int) '-') { delay += 0.05; if (delay>1) delay = 1; } if (temp==(int) '=') delay = 0.25; if (temp==(int) 'g') gui = false; if (temp==(int) 'G') gui = true; if (temp==(int) 's') statistics = false; if (temp==(int) 'S') statistics = true; if (temp==(int) 'n') { n -= 25; if (n<25) n = 25; } if (temp==(int) 'N') { n += 25; if (n>1000) n = 1000; } if (temp==(int) 'N' || temp==(int) 'n') uart.printf("/r/n/r/n Averages = %d \r\n\r\b", n); } } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
View full article
Pre-Sales: i.MX8/8X applications in automotive(Chinese Version) https://community.nxp.com/docs/DOC-345825 i.MX8X website design resource guide: (Chinese Version) https://community.nxp.com/docs/DOC-345676 After-Sales: i.MX8X memory configuration&test application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345803 i.MX8X hardware design guide: (Chinese Version) https://community.nxp.com/docs/DOC-346582 i.MX8X_4.19.35_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345713 i.MX8X_4.19.35_kernal customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345714 i.MX8X_4.14.98_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-342448 i.MX8X_4.14.98_kernal customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-344217 i.MX8X_5.4.24_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-347131
View full article
Here is a BDI3000 config file I used with a SABRE SD board sometimes ago that includes DDR initialization. I had several request on this in the past so I am placing it here in case anyone needs it. Please feel free to comment or update the document according to your own experience and results. Regards Sinan Akman
View full article
This is a generic script which flashes a Linux System (U-boot, uImage and root filesystem) into a SD card. Steps:     1. Download the script into a Linux system     2. Make the script executable (chmod +x mk_mx_sd)     3. Run it with '-H' to know its usage.     4. Run the script with real parameters, specifying the paths for U-boot, uImage and the root filesystem as seen above     5. Plug the SD into your target, boot the board and change the corresponding U-boot variables $ IMAGE=/data/BSP/L2.6.35_11.09.01_ER/L2.6.35_11.09.01_ER_images_MX5X $ ./mk_mx_sd  -d /dev/sdc \                       -u $IMAGE/u-boot-mx53-loco.bin \                       -k $IMAGE/uImage \                       -r $IMAGE/rootfs     6. In case you only want to flash a single binary (like U-boot), just specify the U-boot parameter (-u)
View full article
Q: i.Mx53 and a kernel based on our latest Linux BSP (Kernel Version 2.6.35) – They do see problems when mounting SATA Disk which is used for their rootfs. Has anyone seen this before? I am just wondering if the upcoming release might address and fix this? From the MCU i MX Product Update Call_May 2013.ppt presentation i.MX53  external release June 30 th 2013, freescale.com •       There will be patches/features for i.MX53 including Yocto for this kernel  L2.6.35 BSP release •       Validation testing Where can I check which patches / features are in this release? Is there already a Release Note? this is the kernel for the legacy release: http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_maintain The main proposal for the next legacy release is not upgrade kernel, is only make a yocto release. And if you take meta-fsl-arm on master you will find everything from legacy release. I upstreamed every change I made internaly A: Rootwait is in the command line. Please note they can boot with Kernel version 3.2 - but customer requires 2.6.35 Kernel for other reasons. Please find attached the log files I received. A text bootlog (note sometimes booting works) but it is not stable and reliable on 2.6.35 - same HW seems stable on 3.2 Kernel Regarding to the failed messages contained in customer's log, it's a random issue. SATA driver reports that there is an " SError: { DevExch }" on the PHY connection. It seems that the SATA PHY connection is not stable enough. Can you make a double check on the cable connection and the power supply? You can disable the following configuration when build the 2.6.35 kernel image config SATA_AHCI_FSL_NO_HOTPLUG_MODE         bool "Freescale i.MX SATA AHCI NO HOTPLUG mode"         depends on SATA_AHCI_PLATFORM != n         default n         help           In order to decrease the pwr consumption, release the CLK resources such as usb_phy1_clk, when there is no SATA device adaptored into the AHCI SATA port. The HOTPLUG feature can't be enabled in this situation. Please disable this option if the HOTPLUG is mandatory required.           If unsure, say N. ============================ BTW, I just verified the RFS on SATA on i.MX53 LOCO. It's ok. Here is the log: Starting kernel ... Initializing cgroup subsys cpuset Initializing cgroup subsys cpu Linux version 2.6.35.3-01275-ge6b3f3b (r65037@shlinux1) (gcc version 4.7.3 20121001 (prerelease) (crosstool-NG hg+-946d6d133a90) ) #52 PREEMPT Tue Jul 30 11:27:17 CST 2013 CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7d CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache Machine: Freescale MX53 LOCO Board Memory policy: ECC disabled, Data cache writeback Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 250880 Kernel command line: noinitrd console=ttymxc0,115200 root=/dev/sda1 rootwait rw ... mxc_rtc mxc_rtc.0: setting system clock to 1970-01-01 00:00:01 UTC (1) Waiting for root device /dev/sda1... ata1: SATA link up 1.5 Gbps (SStatus 113 SControl 300) ata1.00: ATA-8: SanDisk SSD P4 32GB, SSD 8.00, max UDMA/133 ata1.00: 62533296 sectors, multi 1: LBA48 ata1.00: configured for UDMA/133 ata1: EH complete scsi 0:0:0:0: Direct-Access     ATA      SanDisk SSD P4 3 SSD  PQ: 0 ANSI: 5 sd 0:0:0:0: [sda] 62533296 512-byte logical blocks: (32.0 GB/29.8 GiB) sd 0:0:0:0: [sda] Write Protect is off sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA sda: sda1 sda2 sd 0:0:0:0: [sda] Attached SCSI disk VFS: Mounted root (ext2 filesystem) on device 8:1. Is there a possibility to tweak timing parameters? Maybe that could help to get it more robust? Are there other parameters we can try to play with and could explain failing Sata RFS on some i.Mx53 boards? I got more info from customers and also "hints" to other forum entries realted to that problem. http://lists.debian.org/debian-arm/2012/03/msg00059.html http://debian.2.n7.nabble.com/Linux-2-6-35-3-Kernel-for-ARM-and-SATA-problems-td1664800.html """ Linux version 2.6.35.3-mx53qsb (mike@ubuntu) (gcc version 4.6.1 (Ubuntu/Linaro 4.6.1-9ubuntu3) ) #3 PREEMPT Sat Mar 17 15:34:48 PDT 2012 CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache Machine: Freescale MX53 LOCO Board ... ata1: SATA max UDMA/133 irq_stat 0x00000040, connection status changed irq 28 ... ata1: SATA link down (SStatus 1 SControl 300) ata1: exception Emask 0x10 SAct 0x0 SErr 0x4000000 action 0xe frozen t4 ata1: irq_stat 0x00000040, connection status changed ata1: SError: { DevExch } ata1: hard resetting link ata1: SATA link down (SStatus 1 SControl 300) ata1: EH complete """ http://www.raspberrypi.org/phpBB3/viewtopic.php?f=9&t=4256&start=175 As mentioned custoemr sees simlar problems with our test image. Maybe one way to check, can you provide me our u-boot and uImae you did the test with? Customer confirmed their HW is compatible with MX53 LOCO Board so I would like to make sure they use correct SW and use what you tested. A bit strange is also that this Problem shows never up on a 3.2 based kernel. However the end customer requires to stay on 2.6.35 for other reasons. - kernel 3.2 which is able to initialize always. - protocol logs for good and bad case trans -p uImage.mx5.35 File keyword is ngbl7927a Data transfer to Austin Transcend repository started.   File size is 2.94 MB. Transfer Method:  Serial with no encryption. File 'uImage.mx5.35' (size 2.94 MB) transcended. Retrieve the file with the keyword:  ngbl7927a TransWeb URL:  http://transweb.freescale.net/index.cgi?go=KEYWORD&KEYWORD=ngbl7927a This file will be deleted in three working days. Local Deletion Time:  Thu Aug 15 23:51:16 2013 CST Greenwich Mean Time:  Fri Aug 16 04:51:16 2013 GMT I know that i.MX53 SATA doesn't have the adjust-window like the adjust window contained by i.MX6Q SATA. As I know that we didn‘t release 3.2 kernel version BSP, right? Regarding to the experience of ”http://debian.2.n7.nabble.com/Linux-2-6-35-3-Kernel-for-ARM-and-SATA-problems-td1664800.html”, it seems that the updates of the SATA stack of Linux level up the timing-compatibility of SATA. Derived from the URL listed above. ”I did trace the problems I having to the ahci code in the kernel not properly handling an ahci CONINIT event generated by my WD5000BEVT drive.  Seems this drive has extra SATA features implemented so that it can be used in hot-plug arrays and these features aren't recognized by the kernel driver so it just seems to shut down the drive and ignore it.  The other SATA drive that I do have working with the kernel doesn't implement the extra features so the kernel is happy.  Presumably these problems were fixed in later kernels and the patches didn't make it into Freescales 2.6.35.3 branch. On the other hand, the kernel might be fine and the firmware in the drive isn't conforming to the ahci specs, but I think that wold cause problems with the drive on other systems. ” This document was generated from the following discussion: i.MX53 Sata rootfs problem
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342059 
View full article
Platform: Ubuntu 12.04 Board: Freescale MCIMX6Q-SDP  and  MCIMX-LVDS1 Screen BSP: L3.0.35_4.1.0_ER_SOURCE_BSP Other device: PC , One Router, 3 Network Cable and 2 usb-otg lines The  platform is as follow: Boot form NFS is very convenient in porting and debugging, and will value us much time. If the customers have modified the kernel and rebuild the kernel to generate the uImage running on board, he can directly download the uImage to the board by TFTP network. It is fast and can avoid the normal operation ,  first customers need to copy the images to the mfgtool specified directory and download the u-boot, uImage and file sytem again to the flash device in board, and then change to boot up mode to boot up the board. If customers are doing debug this operation will waste lot of time. So use the NFS is vey convenient. Beyond this, in the target board customers can also read the files and content in host machine. In a word, use NFS it will help save much time and also convenient. So the follows is introduce and show how to set NFS and then boot up the board. 1 Preparation (1)Build the BSP Build up the L3.0.35_4.1.0_ER_SOURCE_BSP use LTIB on the Ubuntu12.04, you can refer to our user guide document here no details. The u-boot, uImage and file system are all under the directory of litb. Boot up from NFS, so when build uImage some items are needed, here you can see the build details in the section of  Setting Target Linux Image to use NFS in this articel. (2)Download the u-boot to the target board Use the mfgtool Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER to download the u-boot to the SD card of MCIMX6Q-SDP board or use dd command to write the u-boot to SD card.( By the way, writing to the EMMC is also OK) 2 Setting the NFS Environment Set host machine 1 - Install NFS Service on host typing:     $sudo apt-get install nfs-kernel-server       2 - Create symbolic link to ltib/rootfs     $sudo ln -s <ltib instalation folder>/rootfs /tftpboot/rootfs       3 - Setup exports typing:     $sudo gedit /etc/exports       and add the following line:     /tftpboot/rootfs/ *(rw,no_root_squash,no_subtree_check,async) 4 - Restart the NFS server:     $sudo /etc/init.d/nfs-kernel-server restart       Now the host is ready to use NFS Setting Target Linux Image to use NFS       1. Run LTIB configuration by typing: $cd <ltib instalation folder>       $./ltib -c       2. On first page menu, go to "Target Image Generation -> Options"       3. Select the option NFS only and exit LTIB configuration to compile with the new configuration. 4. LTIB should start new compiling and create a new Linux image on /<ltib instalation folder>/rootfs/boot/uImage      5. Copy the created image on /<ltib instalation folder>/rootfs/boot/uImage to /tftpboot/uImage 6. The system is ready to run with NFS. The root file system on target will be located on host on /<ltib instalation folder>/rootfs/ 3 Setting the u-boot command line (1)Download the u-boot to the target board fist according to the section 1 (2) Download the u-boot to the target board. Then give the power to the board, boot up board, u-boot boot up. (2)Configuration the Network Configure the Network and IP , to make the target board and the host machine IP are in the local area network of Router. (3)Set the u-boot command line As follow is my setting for you to refer to : 4 Boot up the board Running the “run bootcmd” after setting the u-boot parameters then boot up the kernel and file system. We can see that the board download the uImage by the TFTP from host machine, then boot up the kernel and finally mount the NFS in the kernel. As follows is the details: Downloading the uImage success and boot up kernel: Input root and access the system. Test: Create a new file in the host machine directory, you can see in the next picture: Then open the target board, in the terminal go to the same directory  in the unit_test we can see the same name. So as we can see in the above operation we can see it is very convenient and fast use the NFS. It will help save time and speed the development time.
View full article
This document explains how to create a DS-5 project to compile and debug the SDK and OBDS for iMX6 and iMX28 respectively. Attached you can find the .ds file for the iMX28 needed to debug in DS-5.
View full article
In the old Android release R10.3.x for i.MX5x, I had followed the user guide instructions to install the USB driver and am able to setup the ADB connection successfully. Unfortunately, for the same PC, the ADB fails to detect my i.MX6SL EVK which is using R13.5. Updating the Android SDK tools cannot help. The reason is the new Android device is using a different USB VID from the old release. So, to solve this problem, we need to update the ADB configuration to scan for the new vendor ID. Below are the steps to update the ADB configuration for Windows PC. These steps (and the steps for Linux PC as well) can also be found in the R10,3.x user guide. 1. Run the SDK's tools to generate an ADB configure file: C:\Program Files\Android\android-sdk\tools> android.bat update adb 2. Modify the adb usb configure file to add the new vendor id 0x18d1. File: X:\Profile\<your account>\.android\adb_usb.ini # ANDROID 3RD PARTY USB VENDOR ID LIST -- DO NOT EDIT. # USE 'android update adb' TO GENERATE. # 1 USB VENDOR ID PER LINE. 0x15a2 0x18d1 3. Unpack the Freescale Android USB win driver "android_usb_fsl.zip" in your Android BSP release package. If you can't find this file in your current package, please get the R10.3.x release for i.MX5x and unpack it. 4. File "tetherxp.inf" in the unpacked "android_usb_fsl" may not be the updated one if the "android_usb_fsl.zip" is extracted from an old release. So, please overwrite the file "tetherxp.inf" in unpacked "android_usb_fsl.zip" by the new "tetherxp.inf" in your current Android BSP release. 5. Enable the "USB debugging" option on the i.MX6 device System settings -> Developer options -> USB debugging 6. Connect the Android Device into PC, uninstall your old driver named "Android Phone" in the device manager, then re-install driver by scanning and locating .inf file under the directory you unpack the android_usb_fsl.zip manually. 7. Restart the ADB server C:\Program Files\Android\android-sdk\platform-tools> adb kill-server C:\Program Files\Android\android-sdk\platform-tools> adb start-server 8. Finally, test your ADB connection C:\Program Files\Android\android-sdk\platform-tools> adb devices List of devices attached 0123456789ABCDEF     device Congratulations! Your ADB is now working. If you have additional information about this topic, please feel free to comment. This document was generated from the following discussion: i.MX6: Android connect to ADB
View full article
Hi All, The new Android kk4.4.2_1.0.0 GA release is now available on www.freescale.com ·         Files available                Description IMX6_KK442_100_ANDROID_DOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   KK4.4.2_1.0.0 BSP Documentation. Includes Release Notes, User's Guide, QSG   and FAQ Sheet. IMX6_KK442_100_ANDROID_SOURCE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   KK4.4.2_1.0.0 BSP, Source Code for BSP and Codecs. IMX6_SABRE_AI_KK442_100_ANDROID_DEMO_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite,  and   i.MX 6Solo  Android KK4.4.2_1.0.0 BSP   Binary Demo Files for the SABRE for Automotive Infotainment IMX6SL_EVK_KK442_100_ANDROID_DEMO_BSP i.MX 6Sololite Android KK4.4.2_1.0.0  BSP Binary Demo Files for the i.MX   6SoloLite Evaluation Kit IMX6_SABRE_SD_KK442_100_ANDROID_DEMO_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite,  and   i.MX 6Solo  Android KK4.4.2_1.0.0 BSP   Binary Demo Files for the SABRE Platform and SABRE Board for Smart Devices IMX6_KK442_100_AACP_CODEC_CODA AAC Plus Codec for i.MX 6Quad, i.MX 6Dual, i.MX   6DualLite, i.MX 6Solo and i.MX 6Sololite Android KK4.4.2_1.0.0 BSP IMX6_MFG_kk4.4.2_1.0.0_TOOL i.MX 6Family Manufacturing Toolkit for kk4.4.2_1.0.0. ·         Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board ·         Release Description i.MX Android kk4.4.2_1.0.0 is GA release for Android 4.4.2 Kitkat(KK) on Freescale's i.MX 6Quad, i.MX 6Dual,i.MX 6DualLite, i.MX 6Solo and i.MX 6SoloLite applications processors. i.MX Android kk4.4.2_1.0.0 release includes all necessary codes, documents and tools to assist users in building and running Android 4.4.2 on the i.MX 6Quad, i.MX 6DualLite and i.MX6SoloLite hardware board from the scratch. The prebuilt images are also included for a quick trial on Freescale i.MX 6Quad and i.MX 6DualLite SABRE-SD Board and Platform, i.MX 6Quad and i.MX 6DualLite SABRE-AI Board and Platforms and i.MX6SoloLite EVK Board and Platforms. This release includes all Freescale porting and enhancements based on Android open source code. ·         What's in this release        Android Source Code Patch android_kk4.4.2_1.0.0-ga_core_source.tar.gz:   Freescale i.MX specific patches (apply to Google Android repo) to enable   Android on i.MX based boards. For   example, Hardware Abstraction Layer implementation, hardware codec   acceleration, etc. Documents The   following documents are included in android_kk4.4.x_1.0.0-ga_docs.tar.gz •   Android Quick Start Guide: A manual that explains how to run Android on an i.MX   board by using prebuilt images. •   Android User's Guide: A detailed manual for this release package. •   Android Frequently Asked Questions: A document that contains Frequently Asked   Questions (FAQs). •   Android Release Notes: A document that introduces key updates and known   issues in this release. •   i.MX 6 G2D API User Guide: A document that introduces the G2D API usages. Tools Tools   in android_kk4.4.2_1.0.0-ga_tools.tar.gz •   MFGTool: Manufacturing tools for i.MX platform. •   tool/tetherxp.inf: USB tethering windows .inf driver configuration file. Prebuilt Images You   can test Android with a prebuilt image on i.MX reference board before   building any code: •   android_kk4.4.2_1.0.0-ga_core_image_6qsabresd.tar.gz: Prebuilt images with   default android features for the SABRE-SD board. •   android_kk4.4.2_1.0.0-ga_core_image_6qsabreauto.tar.gz: Prebuilt images with   default android features for the SABRE-AI board. •   android_kk4.4.2_1.0.0-ga_core_image_6slevk.tar.gz: Prebuilt images with   default android features for the 6SoloLite EVK platform. •   android_kk4.4.2_1.0.0-ga_full_image_6qsabresd.tar.gz: Prebuilt images with   Freescale Extended Multimedia features for the SABRE-SD board •   android_kk4.4.2_1.0.0-ga_full_image_6qsabreauto.tar.gz: Prebuilt images with   Freescale Extended Multimedia features for the SABRE-AI board. ·         Known issues For known issues and limitations please consult the release notes
View full article
Hi everybody, The attached document walks you through to build a Linux image for UDOO Quad board with QT5 support by using a Yocto Project build environment. The Kernel used in this process is 3.14.52. I hope you find it useful. Best regards, Carlos
View full article
MX6X_DDR3_调校_应用手册_V4_20150730.doc
View full article