Video decoding | gst-launch filesrc location=sample.mp4 ! qtdemux ! ffdec_h264 ! mfw_v4lsink |
Notes:
IMAGE_INSTALL_append = " gst-ffmpeg"
LICENSE_FLAGS_WHITELIST = 'commercial'
The ffmpeg plugin fails to load in the latest BSP, please share the patch to fix it here as well.
Yes. Two symbols are not defined and when the ffmpeg library is loaded dynamically, it fails so at the end any of the elements are loaded. Steps: Prepare the package, move to source folder and patch (patch -p1 < patchname). By the way, the BSP failing is 3.0.35_4.0.0, which at this moment is the latest.