i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
This tutorial describes the complete procedure for calibrating a touchscreen display using Weston, specifically validated with the DY1212W LVDS panel on the following NXP development platforms: i.MX93‑EVK FRDM‑i.MX95 FRDM‑i.MX8MP While the initial calibration performed by Weston works only temporarily, this guide will walk you through configuring the system so that the calibration becomes persistent across reboots. The steps below include performing the initial calibration, editing Weston’s configuration, creating a calibration helper script, and applying udev rules to store the calibration matrix automatically.   Temporary Touchscreen Calibration To begin, run the following command to perform an initial calibration of your touchscreen: weston-touch-calibrator LVDS-1   After running this command, your display should be correctly calibrated. However, this calibration is not persistent, and you will need to recalibrate after every reboot unless you complete the persistence steps below.   Making the Calibration Persistent Follow the steps below to ensure that calibration settings are preserved across system restarts. Step 1: Edit the Weston Configuration File Open the following file: /etc/xdg/weston/weston.ini Under the [libinput] section, add these lines: [libinput] touchscreen_calibrator=true + calibration_helper=/usr/bin/save-calibration.sh This enables the calibration helper script that will automatically save your settings. Step 2: Create the Calibration Helper Script Create a new script at: /usr/bin/save-calibration.sh   Insert the following content: #!/bin/bash # Store the transformation arguments for the resistive touchscreen as udev rule echo 'SUBSYSTEM=="input", KERNEL=="event[0-9]*", ENV{ID_INPUT_TOUCHSCREEN}=="1", ENV{LIBINPUT_CALIBRATION_MATRIX}="'$2' '$3' '$4' '$5' '$6' '$7'"' >> /etc/udev/rules.d/touchscreen.rules   Make the script executable: chmod 755 /usr/bin/save-calibration.sh   Step 3: Restart Weston and Recalibrate Restart the Weston service: systemctl restart weston   Run the calibration tool again to generate the persistent settings: weston-touch-calibrator LVDS-1 reboot   Conclusion After completing all of the steps above, your touchscreen calibration will now persist across reboots, ensuring a consistent user experience even after powering off the board. This configuration allows the system to automatically store and apply calibration data through a udev rule generated by your helper script. If you encounter any issues or require further assistance, feel free to reach out. Best regards, Chavira
View full article
this poring is based on the imx415 driver, the capture format is based on raw10, the bsp version is 6.6.52, the patches are attached Disclaimer: − “Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.”
View full article
i.MX 93 EVK LF-6.12.49 patches
View full article
GUI Guider version:  1.9.x, 1.10.x LVGL version: v8.x.x , v9.x.x Host software requirements: Ubuntu 20.04, Ubuntu 22.04 or Debian 12 Target  software requirements:  BSP 6.6 or higher  Hardware requirements: FRDM i.MX 93 Development Board i.MX 93 Evaluation Kit FRDM i.MX 91 Development Board i.MX 91 Evaluation Kit i.MX95  Steps: 1. Export your project from the folder GUI-Guider-Projects to your Linux PC. 2. Build an image for iMX9 using The Yocto Project. Based on iMX Yocto Porject Users Guide set directories and download the repo a. Based on iMX Yocto Porject Users Guide set directories and download the repo $ mkdir imx-bsp-6.6 $ cd imx-bsp-6.6 $: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.52-2.2.0.xml $ repo sync Use distro fsl-imx-xwayland and select machine imx93evk and use this commnad with a build folder name: $ MACHINE=imx93evk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh - b bld-imx93evk b. Use bitbake command to start the build process. Also, add the -c populate_sdk to get the toolchain. $ bitbake imx-image-full -c populate_sdk  c. Install the Yocto toolchain located on <build-folder>/tmp/deploy/sdk/.  $ sudo sh ./fsl-imx-xwayland-glibc-x86_64-imx-image-full-armv8a-imx93evk-toolchain-6.6-scarthgap.sh d. Install ninja utility on the build host $ sudo apt update $ sudo apt upgrade -y $ sudo apt install ninja-build   3. Once your Yocto SDK has been generated and installed, you can build the required binaries using the script attached to this post.      a) Place the script           Copy the script into the same directory where your meta-gui-guider folder is located.      b) Run the script to build the Gui Guider binary           The script includes several options to rebuild, clean, or use a different toolchain in                case you are working with a Yocto SDK version other than the default one (6.6-scarthgap). Build Options Build the Gui Guider binary using the default Yocto SDK ./guider_1.9_project_builder.sh Build the Gui Guider binary using another Yocto SDK version ./guider_1.9_project_builder.sh -t <yocto_sdk_path>/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake Prepare the source code before building ./guider_1.9_project_builder.sh -p Clean the previous build and recompile (Use -t if needed to specify a different toolchain) ./guider_1.9_project_builder.sh -c   4. The generated Gui Guider binary can be found at the following path: /meta-gui-guider/recipes-graphics/gui-guider/gui-guider/build/gui_guider Copy this binary to your board using either USB or SCP, and then execute it directly on the target device.   Using this method provides the flexibility to modify the source code before compilation. This is important because, by default, some configuration options are not available when using Gui Guider directly or when compiling inside Yocto. If you encounter any issues during this process, please open a new thread so we can assist you. Best regards, Chavira
View full article
This patch series enables the external 3.3 V and 5 V power rails used by the Raspberry Pi expansion connector on the i.MX93-QSB, i.MX93-FRDM, and i.MX91-FRDM boards. These regulators were already defined in the device tree but left disabled by default. By activating them, the RPI-compatible expansion header can properly power external modules, HATs, and add‑on boards. Changes by board: i.MX93-QSB Enables the 3.3 V and 5 V external supply lines used by the RPI connector.   i.MX93-FRDM Enables the 3.3 V and 5 V external supply lines used by the RPI connector.   i.MX91-FRDM Enables the 3.3 V and 5 V external supply lines used by the RPI connector.   Purpose: Provide proper power to the Raspberry Pi compatible expansion port. Improve hardware compatibility for users attaching external HATs or modules. Align all i.MX9 reference boards to use a consistent power‑tree configuration for the RPI connector.
View full article
SW : uboot-imx lf_v2025.04 HW : i.MX 8MP EVK board, Oscilloscope   1. Introduction This guide explains the concept of DDR clock spread spectrum on the i.MX 8MP EVK platform. Note that the official NXP BSP does not enable this feature by default. Additionally, this guide provides an example code patch and verification steps to enable the LPDDR4 clock spread spectrum feature on the NXP i.MX 8MP EVK board.   2. What is Spread Spectrum? Spread Spectrum (SS) is a technique used to reduce electromagnetic interference (EMI) by slightly modulating the clock frequency around its nominal value. Instead of operating at a fixed frequency (e.g., 800 MHz), the clock signal is varied within a small range (e.g., ±0.5%). This modulation spreads the energy of the clock signal over a wider frequency band, reducing the peak energy at any single frequency. In other words, SS does not change the average clock speed significantly, but it helps to distribute the spectral energy, making the system less likely to violate EMI regulations.   3. Why Enable Spread Spectrum on DRAM Clock? Enabling Spread Spectrum on the DRAM clock helps reduce electromagnetic interference (EMI) by slightly modulating the clock frequency, lowering peak emissions and making it easier to meet regulatory standards such as FCC and CE. This approach improves system reliability by minimizing interference with other components, offers a cost-effective alternative to hardware changes like shielding or PCB redesign, and is widely adopted in high-speed interfaces such as DDR, PCIe, and SATA to ensure compliance without additional hardware complexity.   4. Related registers CCM_ANALOG_DRAM_PLL_SSCG_CTRL                             Note :  PLL_MFREQ_CTL[19 : 12] : Value of modulation frequency control The larger the mfr value, the lower the MF value (the slower the modulation); the smaller the mfr value, the higher the MF value. MF : The frequency of spread spectrum modulation is the speed at which the triangular/sawtooth modulated wave travels back and forth once per second, measured in Hz (commonly in the tens of kHz range). The speed of the spread spectrum "jitter" is determined. Usually, around 20–50 kHz is chosen to make the energy "swipe evenly" within the bandwidth of the EMI test receiver, thereby reducing the peak radiation at a certain frequency point. PLL_MRAT_CTL[9 : 4] : Value of modulation rate control The larger mrr is, the larger MR is (the wider the range); similarly, MR is also directly proportional to mfr and inversely proportional to m. MR : Peak-to-peak percentage of spread spectrum (the percentage of the total range of the clock frequency swinging around the center value). For example, MR = 0.5% means that the frequency swings around the center value by a total of 0.5% (if it is center-spread spectrum, it is usually ±0.25%).The MR determines the depth (width) of the spread spectrum. The larger the MR, the wider the spectral energy distribution and the lower the peak value, but it comes at the cost of jitter/timing margin (timing should be carefully selected for DDR, SerDes, etc.). 5. About Uboot code patch. Please refer the attachment patch file. At high DRAM frequency, Enable SS may cause not stable problem. So, in this case, I will choose 2400Mbps data clock run the test. Firstly, we should make sure that our code include the 2400Mbps PLL setting. DRAM data speed is 2400Mbps, the DRAM clock is 1200MHz. So the DDRC PLL clock should set up with 600MHz. For example, refer the below code. static struct imx_int_pll_rate_table imx8mm_fracpll_tbl[] = {     PLL_1443X_RATE(1000000000U, 250, 3, 1, 0),     PLL_1443X_RATE(933000000U, 311, 4, 1, 0),     PLL_1443X_RATE(900000000U, 300, 2, 2, 0),     PLL_1443X_RATE(800000000U, 200, 3, 1, 0),     PLL_1443X_RATE(750000000U, 250, 2, 2, 0),     PLL_1443X_RATE(650000000U, 325, 3, 2, 0),     PLL_1443X_RATE(600000000U, 300, 3, 2, 0), // 2400Mbps     PLL_1443X_RATE(594000000U, 99, 1, 2, 0),     PLL_1443X_RATE(400000000U, 400, 3, 3, 0),     PLL_1443X_RATE(266000000U, 266, 3, 3, 0),     PLL_1443X_RATE(167000000U, 334, 3, 4, 0),     PLL_1443X_RATE(100000000U, 200, 3, 4, 0), }; PLL output calculator formula is : PLL_out = 24MHz*mdiv/pdiv/(2^sdiv) So, 2400MHz * 300 / 3 / 2^2 = 600MHz   6. Test result Non Enable SS Enable SS with 1% MR and Down spread Enable SS with 2% MR and Down spread Enable SS with 2% MR and Center spread  
View full article
Some customer need to run Zephyr on i.MX8QM CM4, but there is no support on Zephyr mainline(v4.3.0). This article will share the i.MX8QM CM4_0 porting based on Zephyr v4.3.0.  For i.MX8QXP CM4, please refer this link: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-CM4-support-on-Zephyr-v4-3-0/ta-p/2296957   samples/hello_world/ samples/synchronization   Add pd_ignore_unused in bootargs before entering Linux. For the OpenAMP communication, need to refer this Zephyr application. https://github.com/nxp-real-time-edge-sw/heterogeneous-multicore/blob/main/apps/rpmsg_str_echo/zephyr/main.c
View full article
Some customer need to run Zephyr on i.MX8QXP CM4, but there is no support on Zephyr mainline(v4.3.0) This article will share the porting based on Zephyr v4.3.0. For i.MX8QM CM4, please refer this link: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QM-CM4-0-support-on-Zephyr-v4-3-0/ta-p/2296962   samples/hello_world/ samples/synchronization Add pd_ignore_unused in bootargs before entering Linux. For the OpenAMP communication, need to refer this Zephyr application. https://github.com/nxp-real-time-edge-sw/heterogeneous-multicore/blob/main/apps/rpmsg_str_echo/zephyr/main.c
View full article
The purpose of this document is to provide extended guidance for selection of compatible LPDDR4 memory devices that are supported by the Ara240 (aka Ara-2) processors. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the specific SoC requirement documents. LPDDR4 - maximum supported densities SoC Max Data bus width Maximum density Number of Interfaces Assumed memory organization Notes Ara240 64-bit 128Gb/16GB 2 Dual rank, Dual channel device with 17-row addresses 1   LPDDR4 - list of validated memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part# Notes Ara240 64Gb/(8GB) Total 128Gb/(16GB) (2 x 64Gb/8GB) Micron   MT53E2G32D4DE-046 AUT:C  MT53E2G32D4DE-046 WT:C - 64Gb/(8GB) Total 128Gb/(16GB) (2 x 64Gb/8GB)   FORESEE FLXC4008G-30  2 16Gb/(2GB) Total: 32Gb/(4GB) (2 x 16Gb/2GB) Micron MT53E512M32D1ZW-046BAUT:B     - 32Gb/(4GB) Total 64Gb/8GB (2 x 32Gb/4GB)   Micron MT53E1G32D2NP-046 WT:B - 16Gb/(2GB) Total: 32Gb/(4GB) (2 x 16Gb/2GB) SK Hynix H54G46CYRQX053N - 32Gb/(4GB) Total 64Gb/8GB (2 x 32Gb/4GB) SK Hynix H54G56CYRB-X247 421Y H54G56CYRB-X247 316A - 4Gb/(512MB) Total 8Gb/1GB (2 x 4Gb/1GB) SK Hynix H54G26AYRBX256 - 16Gb/(2GB) Total: 32Gb/(4GB) (2 x 16Gb/2GB) Samsung K4F6E3S4HB-KHCL      - 32Gb/(4GB) Total 64Gb/8GB (2 x 32Gb/4GB) ISSI IS43LQ32K01B 2 32Gb/(4GB) Total 64Gb/8GB (2 x 32Gb/4GB) Samsung K4UBE3D4AB-MGCL - 8Gb/(1GB) Total 16Gb/2GB (2 x 8Gb/1GB)   Winbond W66DP2RQQAHJ 2   Note: This device supports operation with LPDDR4 memories only. LPDDR4x operation is not supported. Dual‑mode memories that support both LPDDR4 and LPDDR4x are allowed as long as the device can operate in LPDDR4 mode, including using LPDDR4 I/O voltage levels and initialization sequences.   Note 1: The numbers are based purely on the IP documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, SoC reference manual and on the JEDEC standards JESD209-4C (LPDDR4). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 3: Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. Note 4: All memory parts are in production unless stated otherwise. Checked June 2026 Note 5: The processor does not support BYTE Mode (x8) memories.       
View full article
Platform supported Kinara Ara2: imx95frdm imx8mpfrdm In this article, let's take imx8mpfrdm as example.   1. Create a Debian LSDK2512 release system for SD boot using the command below: $ ./flex-installer -i pf -d /dev/sdX $./flex-installer -b boot_IMX_arm64_lts_6.12.20.tar.zst -f firmware_imx8mpfrdm_sdboot.img -d /dev/sdX -m imx8mpfrdm -r rootfs_lsdk2512_debian_imx8mpevk.tar.zst note: if Debian base rootfs is used, please upgrade to full function Debian rootfs first. 2. Insert SD card on imx8mpfrdm and boot the system. Once the system has completed booting and you reach the kernel prompt: $ date -s "20260101 1100" // set date $ set proxy if needed 3. download rt-sdk-ara2.deb at: https://nxp1.sharepoint.com/:u:/r/teams/ext1081/Shared%20Documents/LF_v6.12.34/Debian%20Packages/r1.3/Package%201/rt-sdk-ara2.deb?csf=1&web=1&e=i4x1zD 4. Get the uiodma.ko kernel module for Debian from NXP. 5. Disable sleep when install package: $ systemctl mask sleep.target suspend.target hibernate.target hybrid-sleep.target 6. Prepare the packages ARA2 needed: $ apt update $ apt install --reinstall -y libc6-dev $ ln -sf /usr/include/aarch64-linux-gnu/sys /usr/include/sys $ apt install -y python3-dev build-essential $ e2fsck -f /dev/mmcblk1p2 7. install Ara2 package: $ dpkg -i rt-sdk-ara2.deb The tail of successful log as follows: ... [ 783.892116] Adding 2097148k swap on /swapfile. Priority:-2 extents:17 across:35913728k SS /swapfile none swap sw 0 0 Swap file of 2G configured and enabled successfully. Enable rt-sdk-ara2.service service... Created symlink '/etc/systemd/system/multi-user.target.wants/rt-sdk-ara2.service' → '/etc/systemd/system/rt-sdk-ara2.service'. rt-sdk-ara2.service has been enabled. To stop the service from starting automatically on boot run: systemctl disable rt-sdk-ara2.service Post-install script completed successfully. 8. overwrite the kernel module: $ cp /root/uiodma.ko /root/kinara/rt_sdk_r1.3/art/linux/drivers/uiodma_cache_management/uiodma.ko $ systemctl unmask sleep.target suspend.target hibernate.target hybrid-sleep.target // re-enable sleep 9. reboot the system: $ reboot You will see the log as bellow: ... [ 57.855988] bash[1492]: +----------+-----------------+ [ 57.856188] bash[1492]: | Product | Current Version | [ 57.856297] bash[1492]: +----------+-----------------+ [ 57.856397] bash[1492]: | firmware | 1.1.2.0 | [ 57.856501] bash[1492]: | proxy | 1.3.0.0 | [ 57.856593] bash[1492]: | sysapi | 1.1.61.0 | [ 57.856695] bash[1492]: +----------+-----------------+ [ 57.856788] bash[1492]: [I:20260109:09:02:44:636750] [DeviceManager] [kinara_main_1479][DeviceManager] [ 57.856894] bash[1492]: +------------+--------------------+ [ 57.857019] bash[1492]: | Product | Supported Versions | [ 57.857124] bash[1492]: +------------+--------------------+ [ 57.857227] bash[1492]: | client_lib | 1.0.0.0 | [ 57.857327] bash[1492]: | client_lib | 1.1.1.0 | [ 57.857419] bash[1492]: | client_lib | 1.1.2.0 | [ 57.857525] bash[1492]: | client_lib | 1.3.0.0 | [ 57.857642] bash[1492]: | cnn_model | 2.0.0.0 | [ 57.857741] bash[1492]: | cnn_model | 2.1.0.0 | [ 57.857833] bash[1492]: | firmware | 0.5.2.0 | [ 57.857931] bash[1492]: | firmware | 1.1.2.0 | [ 57.858030] bash[1492]: | llm_model | 3.0.0.0 | [ 57.858129] bash[1492]: | llm_model | 3.1.0.0 | [ 57.858222] bash[1492]: | pci_driver | 1.0.4.0 | [ 57.858322] bash[1492]: | pci_driver | 1.0.6.6 | [ 57.858421] bash[1492]: | proxy | 0.8.0.0 | [ 57.858533] bash[1492]: | proxy | 0.9.0.0 | [ 57.858633] bash[1492]: | proxy | 1.1.1.0 | [ 57.858732] bash[1492]: | proxy | 1.3.0.0 | [ 57.858823] bash[1492]: +------------+--------------------+ [ 57.858930] bash[1492]: 2026-01-09 09:02:44 - Proxy launched succesfully [ 58.752944] bash[1514]: 2026-01-09 09:02:45 - Hardware bringup is done (1 device(s) configured) and proxy is launched successfully in the background. [ 58.755142] bash[392]: Logs saved in: /root/kinara/rt_sdk_r1.3/saved_logs/rt-sdk-ara2_logs.txt Now, enjoy your AI journey.
View full article
We are pleased to announce that Config Tools for i.MX v25.12 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) DDR tool – Support for detecting multiple boards connected to the host system is added. – Automatic detection and selection of newly connected COM ports is implemented. – A Connection Test option to validate connectivity before running tests on the target is introduced. – i.MX 93 EVK LP4 configuration is added. – Training execution time information for i.MX 95 and i.MX 943 is included in logs. – Bus signal naming in the UI to align with i.MX pin naming conventions is consolidated. – CA bus values for i.MX943 with LPDDR4 are updated. – DRAM density calculation for i.MX 95 and i.MX 943 with LP4/4x is corrected. – Incorrect calculation of number of banks for i.MX 8M with DDR3L is fixed. – CS1_BNDs calculation for i.MX 91 is corrected. SerDes tool – i.MX 943 RFP support is added. System Manager – The ability to export user configuration in the CFG format is added. – Information about atomic resources to the Details view is added. – Generation and configuration of the config_fusa.h file is supported. – Resource and template assignment is improved. – Grayed-out resource assignments for unavailable configuration parameters in the Resources view are implemented. – Validation of configuration and user input is improved. – Problem decorators to the System and Boot view are added. – Design of the Boot and Details view is improved. – 5600 MT/s for i.MX 95 and i.MX 943 with LPDDR5 is enabled. – LP4/4x settings for DDR_SDRAM_ZQ_CNTL for i.MX 95 and i.MX 943 are updated. – Dual-rank configurations for i.MX 91 and i.MX 93 are updated. – LP4/4x configuration to support non-binary densities for i.MX 95 and i.MX 943 is updated. – Support for non-binary aligned LP4 density for i.MX 91 is added. – FRDM board support (LPDDR4X 15x15 at 4000 MT/s) for i.MX 95 is added. – Timing file discrepancies for i.MX 8MN with DDR3L are fixed. – Issue where changing PHY log level did not update generated code is fixed.
View full article
There are two ways to enable support for the imx95-19x19-evk board:   1.  Directly replace the flash.bin from the Yocto release. 1). depoly LSDK2512 on imx95-15x15-evk board which is supported in Debian LSDK2512     A:    $ flex-installer -i pf -d /dev/sdX -F     B: $ flex-installer -i auto -m imx95evk -d /dev/sdX   2). Download prebuild flash.bin for imx95-19x19-evk board from Yocto release:     A: download: https://www.nxp.com/webapp/sps/download/license.jsp? colCode=L6.12.20-2.0.0_MX95&appType=file1&DOWNLOAD_ID=null     B: Extract the downloaded file to obtain the flash.bin file: imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all   3). Overwrite flash.bin     $ sudo umount /dev/sdX; sudo dd if=imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all of=/dev/sdX bs=1024 seek=32   4). Insert the prepared SD card into the board and power it on. After entering the U-Boot prompt, set the boot command:     => setenv bootcmd "setenv bootargs 'root=/dev/mmcblk1p3 rw rootwait console=ttyLP0,115200 earlycon';ext2load mmc 1:1 0x90400000 Image;ext2load mmc 1:1 0x93000000 imx95-19x19-evk.dtb;booti 0x90400000 - 0x93000000"; saveenv     => reset   The Debian system will start automatically.   2. Build the BSP image using FlexBuild: 1).  clone the Flexbuild source code and apply the patch as attached. 2). build the bsp and boot images:       $ bld bsp -m imx95evk       $ bld boot -m imx95evk or download the pre-built image at: http://sun.ap.freescale.net/images/debian/lsdk2512/firmware_imx95evk_19x19_sdboot.img 3). install the image:       $ ./flex-installer -f firmware_imx95evk_sdboot.img -d /dev/sdX -m imx95evk -b boot_IMX_arm64_lts_6.12.20.tar.zst -r rootfs_lsdk2512_debian_imx95evk.tar.zst 4).  Insert the prepared SD card into the board and power it on. After entering the U-Boot prompt, run the following command to boot board:       u-boot=> bootflow scan -lb
View full article
The following is a guide on training a simple model in Pytorch and Tensorflow and deploying it on an application using the i.MX93 Ethos-65 Neural Processing Unit (NPU) and the i.MX95 eIQ Neutron NPU.
View full article
In some applications, we need to shift frequencies to avoid interference from certain frequencies, such as shifting to avoid Wi-Fi interference. The document is a guide for shifting DDR3 frequency.   The document uses the iMX8M Nano DDR3 as an example, but the process is the same for the iMX8M mini, iMX8M Plus, LPDDR4, etc. The main issue is resolving the DDR pll configuration. Before reading this article, we assume you are already familiar with using the DDR stress tool and DDR config rpa, or the DDR tool of the config tools.   pll_to_table_entry_rates.py can help you to find the settings. 
View full article
System Manager configuration via Config tools for i.MX. Create a new project, modify, view or edit available resources for your specific core. What will you learn How to create a new System Manager project Viewing and managing resources Creating and assigning templates Configuration of System Manager Tip: you can skip to a specific chapter   Introduction   New System Manager project     System Manager views   System Manager templates   Assigning a resource   Creating custom template   Exporting code     Download the tools here: https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-development-boards/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX   https://www.nxp.com/products/i.MX95
View full article
The purpose of this page is to provide supportive information for the selection of suitable camera modules that are supported by the i.MX 8M Plus (i.MX8MP). The guide is attached in this page. This helps customers evaluate project feasibility and integration aspects when considering i.MX 8MP SoCs for their products. It is strongly recommended to consult with NXP and the camera module vendor before finalizing the choice of the camera part number to ensure compatibility, availability, longevity, and pricing requirements. NXP Supported Sensors: Sensor Vendor Image Sensor Max Resolution Camera Module OmniVision OS08A20 8MP IMX-OS08A20 EXPI-OS08A20 OmniVision OV2775 2MP   Sony IMX219 8MP   Sony IMX477 12.3MP   Onsemi AR0144 1MP AR0144 Onsemi AR1335 13MP     Partner Enabled Sensors:   Partner Sensor Vendor Image Sensor Max Resolution ISP Tuning Camera Module Location FRAMOS Sony IMX415 8MP ✔   Munich, Germany/ Canada/USA Sony IMX662 2MP FSM:GO Sony IMX678 8MP Sony IMX900 3.2MP Sony IMX676 12MP Innowave Onsemi AR1335 13MP ✔   Austin, Texas, USA/Israel Sony IMX258 13MP Camera Modules Sony IMX219 8MP OmniVision OV5645 5MP   OmniVision OV2710 2MP   Basler Onsemi AR0821 8MP   Basler   Onsemi AR0521 5MP   Onsemi Onsemi AR0830 8MP   Image Sensors, Module available through Future Electronics   Onsemi AR0544 5MP Onsemi AR0821 8MP Onsemi AR0822 8MP Onsemi AR0145 1MP Onsemi AR0235 2MP Onsemi AR1335 13MP PHYTEC Onsemi AR0144 1MP     Germany/ China/India/ USA Onsemi AR0234 2.3MP   Onsemi AR0521 5MP   E-consystems Sony IMX662 2.4MP     Riverside, CA, USA/India Sony IMX900 3.2MP   Onsemi AR0234 2.3MP   CIS Corporation Sony IMX715 12MP ✔   Japan Sony IMX570 0.32MP   Onsemi AR0234CS 2MP   Sony Sony IMX500 12MP     Japan HINO Engg Sony IMX415 8MP ✔   Japan Sony IMX662 2MP   Leopard Imaging Sony IMX500 12MP ✔   Fremont, CA, USA/China   Note: CIS Corporation and HINO Engg currently only support customers in Japan market.
View full article
This article describes how to create a tiny rootfs based on BusyBox.   Test platform: i.MX 95 19x19 LPDDR5 EVK. The attached layer can be used with other platforms as well. Software: Linux BSP 6.12.34-2.1.0 Boot device: SD card   This article provides a custom meta-tiny-rootfs layer, to simplify the enablement. The layer: creates a custom distribution based on Poky, with no extra features creates a custom image based on BusyBox that only starts a terminal removes most of the machine features uses musl, instead of glibc   Using the default DISTRO=fsl-imx-wayland and core-image-minimal, the rootfs size is 800MB. Using the custom DISTRO=tiny-rootfs and core-image-tiny, the rootfs size reduces to 2.6MB.   How to? 1. Prepare the Yocto environment according to Section 3, 4, 5 in i.MX Yocto Project User's Guide. In the next commands, we'll assume the Yocto directory is imx-yocto-bsp, and the build directory is build. 2. Configure the build directory: cd ~/imx-yocto-bsp/ DISTRO=fsl-imx-wayland MACHINE=imx95-19x19-lpddr5-evk source ./imx-setup-release.sh -b build Note: The imx-setup-release.sh script accepts only Wayland distributions. We'll set the custom distro at the next step. 3. Set the custom distro. In the build directory, run: echo 'DISTRO = "tiny-rootfs"' >> conf/local.conf 4. Download the meta-tiny-rootfs archive, and extract it into the ~/imx-yocto-bsp/sources directory. cd ~/imx-yocto-bsp/sources tar -xvf meta-tiny-rootfs.tar.gz 5. Add the meta-tiny-rootfs layer to BBLAYERS: cd ~/imx-yocto-bsp/build bitbake-layers add-layer ../sources/meta-tiny-rootfs 6. Build the core-image-tiny image. bitbake core-image-tiny 7. Write the image on an SD card, and boot. You should be able to see a similar log: [ 6.183401] Run /sbin/init as init process init started: BusyBox v1.37.0 () starting pid 163, tty '': '/bin/mount -t proc proc /proc' starting pid 164, tty '': '/bin/mount -t sysfs sysfs /sys' starting pid 165, tty '': '/bin/mount -t devtmpfs devtmpfs /dev' mount: mounting devtmpfs on /dev failed: Resource busy starting pid 166, tty '': '/bin/mount -o remount,rw /' [ 6.246037] EXT4-fs (mmcblk1p2): re-mounted a5abac39-6c11-419f-97ef-86532e2616ad. starting pid 167, tty '': '/bin/mkdir -p /dev/pts' starting pid 168, tty '': '/bin/mount -t devpts devpts /dev/pts' starting pid 169, tty '': '/bin/mount -a' starting pid 170, tty '': '/sbin/swapon -a' starting pid 176, tty '': '/etc/init.d/rcS' starting pid 177, tty '/dev/ttyLP0': '/usr/sbin/ttyrun ttyLP0 /sbin/getty 115200 ttyLP0' Tiny Rootfs Operating System 1.0.0 imx95-19x19-lpddr5-evk /dev/ttyLP0 imx95-19x19-lpddr5-evk login:   How to add additional features?  If you want to add additional features to DISTRO_FEATURES, MACHINE_FEATURES, or IMAGE_FEATURES, please use the DISTRO_TINY_FEATURES, MACHINE_TINY_FEATURES and IMAGE_TINY_FEATURES variables. For example, to add bluetooth to MACHINE_FEATURES, add the following line in conf/local.conf. MACHINE_TINY_FEATURES = "bluetooth"   Note: If you need to add a package that requires the full libc (instead of musl), add the following in conf/local.conf: TCLIBC = "glibc"   These optimizations were inspired by this presentation: Honey, I shrunk the rootfs!
View full article
NETC presents itself as a multi-function PCIe Root Complex Integrated Endpoint (RCiEP) for easy software discovery of peripheral functions. As such, it contains multiple PCIe functions. PCIe RCiEP allows for easy software integration into OSes, which support PCIe but can be easily integrated as a simple platform device for RTOSes or bare metal implementations which do not support it. Configuration and control of ENETC(s) is implemented using a combination of registers and a command message interface implemented using descriptor rings in memory. Key goal of the DPDK is to provide a simple, complete framework for fast packet processing in data plane applications. Using the APIs provided as part of the framework, applications can leverage the capabilities of underlying network infrastructure. DPDK been prominent software in user space for networking applications pushes for eNetc driver to be written in user space. This document introduces overview of the NXP ENETC and how its driver is implemented and integrated into the DPDK. DPDK eNetc Driver support features Multi-queue supported, Packet type parsing, promisc, MAC exact filter table filtering, VLAN exact filter table filtering, Link status interrupt, Rx checksum offload, basic stats.
View full article
lspci output on iMX95EVK as PCIe RC Please take a good look at the snippet above. It is taken from the console of iMX95 after executing 'lspci' on a specific PCIe device[iMX8MM as PCIe EP] that gets enumerated as BDF[Bus Device Function] 01:00.0. This blog attempts to debunk the mystery revolving around the "Memory at " info of the lspci output. We will discuss what this address is, why it is used and its relevance in the PCIe world. This blog will focus on the following agendas: - 1. PCIe parent and child relationship in Linux Device Tree 2. What is CPU and PCIe address space and the need for address space translation?  3. Assigning resources to a PCIe device in Linux 4. How is address space translation carried out in Linux PCI Subsystem?   PCIe parent and child relationship in Linux Device Tree In the Linux device tree, PCIe parent and child relationship defines how PCIe Root Complex and Endpoints are positioned in the system. A PCIe parent node in the device tree represents a PCIe controller (Root Complex / Host-Bridge). Taking reference from a PCIe node present in the device tree source of imx95: -   pcie@4c300000 {                         compatible = "fsl,imx95-pcie";                         reg = <0x00 0x4c300000 0x00 0x10000 0x00 0x4c360000 0x00 0x20000 0x00 0x60100000 0x00 0xfe00000>;                         reg-names = "dbi\0atu\0config";                         #address-cells = <0x03>   …  }   pcie@4c300000 represents a Designware PCIe controller Root Complex which is a parent to the devices/bridge that will be connected to it. -- 'compatible' property identifies the specific PCIe controller. Its corresponding driver resides in drivers/pci/controller/dwc/pci-imx6.c -- 'reg' property specifies the memory mapped registers of the PCIe controller. Child nodes under PCIe RC represent devices on the PCIe bus. They can be fixed function devices like Wi-fi, Ethernet, NVMe or they can be PCIe bridges which further can have devices connected to it. Taking reference from 'arch/arm64/boot/dts/freescale/imx95.dtsi'   pcie_4ca00000: pcie@4ca00000 {                         compatible = "pci-host-ecam-generic";                         reg = <0x0 0x4ca00000 0x0 0x100000>;                         /* Must be 3. */              …              …              enetc_port0: ethernet@0,0 {                                 compatible = "fsl,imx95-enetc";                                 reg = <0x000000 0 0 0 0>;                                 clocks = <&scmi_clk IMX95_CLK_ENET>,                                          <&scmi_clk IMX95_CLK_ENETREF>;                                 clock-names = "ipg_clk", "enet_ref_clk";                                 nvmem-cells = <&eth_mac0>;                                 nvmem-cell-names = "mac-address";                                 status = "disabled";                         }; }   ethernet@0,0 is a PCIe device at bus 0, device 0, function 0. It is a child of PCIe RC which is memory mapped at 0x4ca00000   These child devices/bridges can either be dynamically discovered using PCI enumeration or they can be statically described in a device tree as seen in the device-tree snippet above in which "ethernet@0,0" entry statically tells the RC that the ethernet child device is connected to it. These child nodes are nested within a PCI parent node of the device tree as seen in the above example.   What is CPU and PCIe address space and the need for address space translation ? CPU address space is the system's physical memory map as seen by the processor. Example of CPU Physical Address Space viewed by Cortex-A55 on iMX95:-   Start address      End address    Module 0x48000000       0x4812FFFF    GIC Programming registers 0x4AA00000      0x4AAFFFFF    Neutron SRAM 0x4AC10000      0x4AC1FFFF    Camera domain block control 0x4E080000       0x4E08FFFF    DDR Controller This address space is kind of a global system view which is managed by system firmware/OS. These addresses are fixed by hardware-design. On the other hand, PCIe address space is local to PCI bus, managed by PCIe subsystem. The  addresses in this space are dynamically assigned. An example of PCIe address space that could look like the following:- 0x00000000   -    0x0FFFFFFF 0x10000000   -    0x1FFFFFFF 0x20000000   -    0x2FFFFFFF It is evident from the above explanation that CPU and PCIe address space operate in a separate and independent address domains. So the CPU cannot access the space of PCIe device unless a translation mechanism is in place. In one of the upcoming sections we will get to that as well but please spare a few minutes and ponder the question below:- Question : Why do you need separate address spaces for CPU and PCIe? Answer : One of the major reasons is modularity. We have separate spaces so that PCIe devices can be designed independently of the CPU architecture. Same card will work in different system. It will always have the flexibility of CPU remapping the PCIe space as and when needed. Also, different address spaces prevent devices to access arbitrary system memory. Based on the discussion in this section, it is evident that the PCIe address space is inherently different from the CPU address space and truth be told- it has its advantages. Therefore we need an entity to translate to/fro these address spaces. Here comes 'iATU' - Internal Address Translation Unit. On iMX SOCs, these hardware units are responsible for carrying out the address translation. These units are a part of Synopsys DesignWare PCIe Controller, providing programmable address translation windows for inbound and outbound transactions. For the readers who are uninitiated on the inbound and outbound transactions in pcie, please spare some time go through this technical blog - Understanding PCIe Outbound/Inbound windows with a use-case - NXP Community Note: - Address translation simply ensures that the CPU can access a PCIe device's memory and vice-versa.   Up until here, the readers must have got a basic picture of PCIe Address Translation. Before jumping into the nitty-gritty of this translation in the Linux PCI subsystem, let's discuss how the resources are assigned to a PCIe device.   Assigning resources to a PCIe device in Linux PCIe devices do not have a direct CPU instruction interface so they communicate through memory-mapped regions. Devices need memory for DMA operations or for MSI/MSIX interrupts. Different devices have different needs, so resources in PCIe could be MMIO where device registers are mapped or memory regions needed for DMA transfer. In linux, pci_assign_resource function of PCI subsystem is responsible for assigning IO and memory resources to the PCIe devices during system initialisation after PCIe devices are enumerated. It is called for all the devices on a PCI bus and based on the PCI devices' resource requirement, it assigns them. But how does the PCI subsystem in linux figure out what resources does the PCIe devices need ? - Every PCIe device has a configuration space defined by the PCIe specification. This includes   BAR[Base Address Registers] - To indicate what type of resource[IO/Mem] does  the device needs and the size of resource. Capabilities - To broadcast the device capabilities such as MSI Interrupts, ASPM low power states etc. Reading the BARs from the PCIe device will tell us what kind and size of the resources are needed by the device. // To determine the size of resource from the BAR of PCIe device:- Step-1: Write all 1's to the target BAR register. Step-2: Read back the value and clear the lower 4 bits (for a memory BAR) or 2 bits (for an I/O BAR), as these are status bits, not part of the size calculation Step-3 Perform Bitwise NOT on the value and add 1 to it. Step-4: The returned value indicates the size. Taking an example to understand this:- Let's assume that after reading back the value in Step-2 above, the BAR returns 0xFFFFF000. The lower 4 bits are already cleared. Step-3  we perform bitwise NOT on the value -> ~(0xFFFFF000) = 0x00000FFF Adding 1 to it : 0x00000FFF + 1 = 0x00001000 The obtained value 0x1000 = 4096 bytes indicates the size, meaning the BAR requires a 4KB memory region. // To determine the type of resource from the BAR of PCIe device:-   A Base Address Register (BAR) in PCI configuration space: Bit 0 → Resource type: 1 = I/O space 0 = Memory space For memory BARs: 00 = 32-bit 10 = 64-bit Bits 1–2 → Addressing type: Bit 3 → Prefetchable flag   Interpreting the value 0xFFFFF000, we get:-   Bit 0 = 0 → Memory space Bits 1–2 = 00 → 32-bit address Bit 3 = 0 → Prefetchable Upper bits → Base address (after masking)   pci_read_bases [drivers/pci/probe.c] in linux PCI subsystem is responsible to figure out the BAR memory size and type requirement during device enumeration. Needless to say, the above sequence of writing to the Endpoint's BAR and identifying the size and type of resource is executed on the PCIe RC. We have the following setup :- iMX95 <------> iMX8MM [RC]                     [EP] After PCIe RC has the size of the BAR that is required, the pci_assign_resource function allocates a memory range and then sets up translation from this memory range to the PCIe address space. we started this blog with a snippet, that shows the following lspci log:-   Referring to the above, please note that the RC driver has allocated: - 0x910100000 - 0x910110000 as the non-prefetchable memory address range, size=64KB The above memory address range is in the PCIe 1 Outbound space memory mapped on iMX95 SoC: -   The range 0x910100000 - 0x910110000 will be mapped to the PCIe address space of the End-point. This essentially means that if the cpu generates any address in between this range [inclusive of start and end-address], a PCIe TLP will be sent by the PCIe controller on the RC to the End-point on the bus. It could be a read or write to the memory of Endpoint. The address to write/read would be decided based on the address space translation. We shall discuss in-detail how this translation is exercised in the linux kernel in the next section.   How is address space translation carried out in Linux PCI Subsystem?   We start with some important questions: - Where is the range 0x910100000 - 0x910110000 specified ? How does the kernel know that it has to map the PCIe 1 Outbound space and not PCIe2 Outbound space or any other address space for that matter? -- Like all good things in Linux, this also starts with a 'device tree binary'. A dtb is passed by Uboot to the kernel so that it could get the hardware description of our board. Since we are using Torradex 's Verdin iMX95 EVK Board as Root Complex, this is the dtb that we are using - imx95-19x19-verdin-adv7535.dtb I will be attaching a working dtb with this blog so that the readers can use it if needed. This dtb includes - arch/arm64/boot/dts/freescale/imx95.dtsi Let's have a look at a particular pcie node of interest: -   'ranges' property is the answer to the questions that were asked in this section earlier.  - This property defines the address translation rules between the parent's address space and the child PCI address space.   Note:- This blog focuses only on 'ranges' property since it is relevant to our discussion. So the readers are advised to look elsewhere if they want to understand other device-tree properties of the PCIe node.  Let's decode the ranges property : It has the following format:- <PCI address><CPU address> <PCI size>      3 cells               2 cells             2 cells             So one entry will have 7 cells. In our dtsi we have 2 entries. 1st is for IO space translation and the 2nd is for Mem space translation. Referring to the second entry  :-   0x82000000 0x0 0x10000000 0x9 0x10000000 0 0x10000000 |------PCI address---------------| |-CPU address-| |---PCI size---|   The above gives us the following info: - MEM Space prefetchable <   0x82000000 0x00 0x10000000   // PCIe address: 0x10000000   0x09 0x10000000              // CPU/system address: 0x910000000   0x00 0x10000000              // Size: 256MB >;   0x82000000 = 1000 0010 0000 0000 0000 0000 0000 0000   Bits 31–30 (10) → Configuration space type: This indicates memory space. Bit 29 (0) → Non-relocatable Bit 28 (0) → Non-prefetchable  (0 means non-prefetchable) Bits 27–24 (0010) → Address space type = Memory So, 0x82000000 means: PCI memory space Non-prefetchable 32-bit address space   Note:- For those of you wondering why lspci output mentions [size=64K] and dts says 256 MB. This is because 256MB is the maximum address space available for the PCIe devices. It is upto the Endpoint device, how large address space does it require and accordingly it gets allocated.     Similary IO space translation is also created from the 1st entry in 'ranges':- < 0x81000000 0x00 0x00 → PCI I/O address: 0x00000000 0x00 0x6ff00000 → CPU/system address: 0x6ff00000 0x00 0x100000 → Size: 1MB >;   we observe the same in the dmesg output of iMX95 Verdin EVK Linux console:-   So the MEM Space mapping is from CPU Address 0x910000000 - 0x091fffffff translated to PCIe Address 0x10000000 - 0x1fffffff It is only fair that we mention the driver that uses the 'ranges' property. The 'ranges' property get parsed in "pci_parse_request_of_pci_ranges -> devm_of_pci_get_host_bridge_resources" of "drivers/pci/of.c"     devm_of_pci_get_host_bridge_resources, for each range automatically  manages the memory allocated for these resources. It ensures that the resources are freed when the device is detached or the driver is removed. We have got the answer what & why is the cpu and pci address range the way it is. But in the lspci, you see 0x910100000 and not 0x910000000 which is what the intended start range is supposed to be as per the dtb. Why is that ? To answer this - we need to go back to the PCIe device enumeration. During PCIe enumeration, in the linux PCI driver the bar resources were determined like we had discussed earlier and then the PCI core driver may assign addresses keeping alignment requirements in mind that is why EP's BAR0 was assigned a PCI bus address as 0x10100000 with a 1MB[0x100000] offset from 0x10000000. And keeping the device tree pci translation window in mind:- 0x10100000 translates to 0x910100000 This translation doesn't happen on its own. Device tree binary just mentions the translation window specifics such as the CPU address space to translate to and the PCI address space to translate from. The actual translation is done via iATU. This is done in the dw_pcie_iatu_setup function of drivers/pci/controller/dwc/pcie-designware-host.c by creating the outbound window using dw_pcie_prog_outbound_atu function. Translation is configured on the RC successfully but there is still something missing. .. .. Inbound window !! Without an inbound window on the Endpoint i.e iMX8MM, the writes/reads to 0x910100000 would be meaningless. On iMX8MM we are using PCI Endpoint test driver which is quite popular in linux community and I would urge the readers to visit this page if they want more info - 9. PCI Endpoint Framework — The Linux Kernel documentation pci_epc_map_addr function in drivers/pci/endpoint/pci-epc-core.c creates inbound window by mapping PCI address [0x10100000] to physical address in EP's memory. That's how the reads and writes go through. If there's no Inbound window configured, something like this unfolds in case of read:-   So now everything is set up. Translation windows are configured in the PCI drivers and you are at linux console. The following sequence unfolds when the CPU issues a memory read:-   In case of memory writes:- The following happens on the Endpoint: - The beauty is that this entire translation happens transparently in hardware - your driver just reads/writes to the CPU address, and the PCI host controller handles all the translation automatically! -- How do we test the Address Translation ?   To test reads and writes, either we can make some changes in the driver itself or use devmem5 user-space binary. We are going to make minor driver side changes on iMX8MM and use devmem5 on the RC. iMX8MM is the PCIe Endpoint and we are using end-point test driver to configure it as such. If  you want to do the same, please follow this blog - Enabling PCIe End-point framework on iMX95 torradex board and iMX8MM EVK - NXP Community On the contrary if you want to make iMX95 as RC and iMX8MM Endpoint, feel free to follow this blog - How to configure iMX95EVK as PCIe Endpoint and test it using PCIe Endpoint Test Framework - NXP Community Two things we are going to do next: - 1. On iMX8MM EP, we are going to write some random values  in the drivers/pci/endpoint/pci-epf-core.c, make the following changes in pci_epf_alloc_space function: -     'space' is the virtual address and 'phys_addr' is the physical address that is contiguous. Please note that it is a crude way to test this translation. There are better ways to do it. Build the kernel after the changes and boot the board with it. Make iMX8MM an Endpoint using PCI Endpoint Test Framework. 2. On iMX95 Verdin EVK [PCIe RC], we are going to read the address 0x910100000 using devmem5 to verify that we can observe the same data on the RC.   That's it for today. This was a long blog and if you feel overwhelmed by the details, please feel free to drop in the DMs or comments so that I can try to make it easier. Until next time! Gaurav Sharma  
View full article
In this blog, we are going to discuss how we can configure iMX95EVK as PCIe Endpoint and test it using a RC which will be iMX8MM. Hardware Components iMX95EVK iMX8MM PCIe M.2 Key E Bridge Ethernet connectivity     Software Components Linux Factory 6.12.20 BSP linux-imx source code - https://github.com/nxp-imx/linux-imx/tree/lf-6.12.20-2.0.0 System setup Step -1 Flash the 6.12.20 BSP on the iMX95 EVK eMMC/SD card and boot with it. Step-2 Fetch linux-imx 6.12.20 source code from the github repo GitHub - nxp-imx/linux-imx at lf-6.12.20-2.0.0 Step-3 Make the following changes to arch/arm64/boot/dts/freescale/imx95-19x19-evk-pcie1-ep.dtso as per the following diff:-   diff --git a/arch/arm64/boot/dts/freescale/imx95-19x19-evk-pcie1-ep.dtso b/arch/arm64/boot/dts/freescale/imx95-19x19-evk-pcie1-ep.dtso index a8e3bbc53894..d082688fc1c2 100644 --- a/arch/arm64/boot/dts/freescale/imx95-19x19-evk-pcie1-ep.dtso +++ b/arch/arm64/boot/dts/freescale/imx95-19x19-evk-pcie1-ep.dtso @@ -11,12 +11,12 @@ &smmu {  };     -&pcie1 { +&pcie0 {         status = "disabled";  };   -&pcie1_ep { +&pcie0_ep {         pinctrl-names = "default"; -       pinctrl-0 = <&pinctrl_pcie1>; +       pinctrl-0 = <&pinctrl_pcie0>;         status = "okay";  };     As you can see, we are trying to enable 'End-point' mode on iMX95EVK's M.2 PCIe 0. The default dtb enables it for PCIe 1. Building the kernel will build this dtb from the dtso changes. Step-4 SCP the dtb to the board and rename it to "imx95-19x19-evk-pcie0-ep.dtb" to avoid confusion. Copy it to the location - /run/media/boot-mmcblk0p1/ Step-5 Boot the board with this DTB by changing the 'fdtfile' variable at Uboot. when the kernel boots up with this dtb, you will see the following pcie dmesg logs on the console through which you can verify if the changes have worked:-   root@imx95evk:~# dmesg | grep pcie-ep [    3.142123] imx6q-pcie 4c300000.pcie-ep: iATU: unroll T, 8 ob, 8 ib, align 4K, limit 1024G [    3.151767] imx6q-pcie 4c300000.pcie-ep: eDMA: unroll T, 4 wr, 4 rd root@imx95evk:~#   0x4c300000 is the address of pcie0 controller Step-6 Execute this script on iMX95EVK - 'conf_pcie0_ep' Step-7 Boot iMX8MM board with this dtb - imx8mm-evk.dtb Step-8 Executing 'lspci' on the iMX8MM, you will see the following output:- That's the iMX95EVK Endpoint that you see on the lspci output of iMX8MM RC.   The address space translation window is configured with the help of the info mentioned in  arch/arm64/boot/dts/freescale/imx8mm.dtsi If the readers want to make sense out of the translation window info mentioned in form of 'ranges' property of PCIe node, they can go through this article in which there is a detailed explanation of what is going behind the scenes - Demystifying the PCIe and CPU address space translation in Linux - NXP Community      
View full article