Using Yocto to build a minimal (3MB) Linux File System for i.MX MPUs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using Yocto to build a minimal (3MB) Linux File System for i.MX MPUs

Using Yocto to build a minimal (3MB) Linux File System for i.MX MPUs

This article describes how to create a tiny rootfs based on BusyBox.

 

Test platform: i.MX 95 19x19 LPDDR5 EVK. The attached layer can be used with other platforms as well.

Software: Linux BSP 6.12.34-2.1.0

Boot device: SD card

 

This article provides a custom meta-tiny-rootfs layer, to simplify the enablement. The layer:

  • creates a custom distribution based on Poky, with no extra features
  • creates a custom image based on BusyBox that only starts a terminal
  • removes most of the machine features
  • uses musl, instead of glibc

 

Using the default DISTRO=fsl-imx-wayland and core-image-minimal, the rootfs size is 800MB.

Using the custom DISTRO=tiny-rootfs and core-image-tiny, the rootfs size reduces to 2.6MB.

 

How to?

1. Prepare the Yocto environment according to Section 3, 4, 5 in i.MX Yocto Project User's Guide.

In the next commands, we'll assume the Yocto directory is imx-yocto-bsp, and the build directory is build.

2. Configure the build directory:

cd ~/imx-yocto-bsp/
DISTRO=fsl-imx-wayland MACHINE=imx95-19x19-lpddr5-evk source ./imx-setup-release.sh -b build

Note: The imx-setup-release.sh script accepts only Wayland distributions. We'll set the custom distro at the next step.

3. Set the custom distro. In the build directory, run:

echo 'DISTRO = "tiny-rootfs"' >> conf/local.conf

4. Download the meta-tiny-rootfs archive, and extract it into the ~/imx-yocto-bsp/sources directory.

cd ~/imx-yocto-bsp/sources
tar -xvf meta-tiny-rootfs.tar.gz

5. Add the meta-tiny-rootfs layer to BBLAYERS:

cd ~/imx-yocto-bsp/build
bitbake-layers add-layer ../sources/meta-tiny-rootfs

6. Build the core-image-tiny image.

bitbake core-image-tiny

7. Write the image on an SD card, and boot. You should be able to see a similar log:

[    6.183401] Run /sbin/init as init process
init started: BusyBox v1.37.0 ()
starting pid 163, tty '': '/bin/mount -t proc proc /proc'
starting pid 164, tty '': '/bin/mount -t sysfs sysfs /sys'
starting pid 165, tty '': '/bin/mount -t devtmpfs devtmpfs /dev'
mount: mounting devtmpfs on /dev failed: Resource busy
starting pid 166, tty '': '/bin/mount -o remount,rw /'
[    6.246037] EXT4-fs (mmcblk1p2): re-mounted a5abac39-6c11-419f-97ef-86532e2616ad.
starting pid 167, tty '': '/bin/mkdir -p /dev/pts'
starting pid 168, tty '': '/bin/mount -t devpts devpts /dev/pts'
starting pid 169, tty '': '/bin/mount -a'
starting pid 170, tty '': '/sbin/swapon -a'
starting pid 176, tty '': '/etc/init.d/rcS'
starting pid 177, tty '/dev/ttyLP0': '/usr/sbin/ttyrun ttyLP0 /sbin/getty 115200 ttyLP0'

Tiny Rootfs Operating System 1.0.0 imx95-19x19-lpddr5-evk /dev/ttyLP0
imx95-19x19-lpddr5-evk login: 

 

How to add additional features?

 If you want to add additional features to DISTRO_FEATURES, MACHINE_FEATURES, or IMAGE_FEATURES, please use the DISTRO_TINY_FEATURES, MACHINE_TINY_FEATURES and IMAGE_TINY_FEATURES variables.

For example, to add bluetooth to MACHINE_FEATURES, add the following line in conf/local.conf.

MACHINE_TINY_FEATURES = "bluetooth"

 

Note: If you need to add a package that requires the full libc (instead of musl), add the following in conf/local.conf:

TCLIBC = "glibc"

 

These optimizations were inspired by this presentation: Honey, I shrunk the rootfs!

附件
无评分
版本历史
最后更新:
‎11-19-2025 01:33 PM
更新人: