i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
LSIO_GPIO0_IO0x toggling on i.MX8QM Issue customer met: Customer met LSIO_GPIO0_IO0x not toggling on i.MX8QM, they are working through the software on their board, part of that involves getting a few GPIO pins working. They have been using several GPIO pins for a while now, we have some simple toggles and some others where we bit bang i2c, all of those have worked fine. However, They have not been able to get 3 pins to either read or set successfully at all: LSIO_GPIO0_IO00 (SIM0_CLK) LSIO_GPIO0_IO01 (SIM0_RST) LSIO_GPIO0_IO02 (SIM0_IO) 1\ Reproduce on our i.MX8QM EVK board  a. Check the hardware connection Check the LSIO_GPIO0_IO00 (SIM0_CLK), LSIO_GPIO0_IO01 (SIM0_RST) and LSIO_GPIO0_IO02 (SIM0_IO) connection in our i.MX8QM EVK board. In the default design in NXP i.MX8QM EVK board, the pins SIM0_CLK, SIM0_RST and SIM0_IO connect to the SIM CARD on the base board.         b. To make these pins work as GPIO pins In the default pins mux, default pins mux on the SIM0, to make these pins work as GPIO, need to mux them to the GPIO functions. SIM0_CLK (SIM0_CLK)     SIM0_RST (SIM0_RST)   SIM0_IO (SIM0_IO)     c. In the source code change these pins mux to GPIO configuration: Defalt setting for these pins : linux-imx/arch/arm64/boot/dts/freescale/imx8qm-mek.dts at lf-6.12.y · nxp-imx/linux-imx · GitHub   pinctrl_sim0: sim0grp {                              fsl,pins = <                                            IMX8QM_SIM0_CLK_DMA_SIM0_CLK           0xc0000021                                            IMX8QM_SIM0_IO_DMA_SIM0_IO                 0xc2000021                                            IMX8QM_SIM0_PD_DMA_SIM0_PD               0xc0000021                                           IMX8QM_SIM0_POWER_EN_DMA_SIM0_POWER_EN                         0xc0000021                                            IMX8QM_SIM0_RST_DMA_SIM0_RST            0xc0000021                              >;               }; Linux dts should set them to GPIO0 functions:               IMX8QM_SIM0_CLK_LSIO_GPIO0_IO00 0xc0000021               IMX8QM_SIM0_RST_LSIO_GPIO0_IO01 0xc2000021               IMX8QM_SIM0_IO_LSIO_GPIO0_IO02 0xc0000021 Build the source code, download the images to board, test on the SIM pins to see if these pins can work or not. Test on the J45 pins 3,5,6.   Test the SIM_CLK as an example: Test commands in Linux echo 480 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio480/direction #output high echo 1 > /sys/class/gpio/gpio480/value #measure the PINs #output low echo 0 > /sys/class/gpio/gpio480/value #measure the PINs Found these pins can not toggling well. 2\ Go next further test and consideration Foud the SCU_GPIO0_00, SCU_GPIO0_01, SCU_GPIO0_02 are also configurate as GPIO function in the SCFW,  in the default setting for the SC_P_SCU_GPIO0_00is the function GPIO0_00 , and when setting the SIM0_CLK to GPIO0_00 function then the GPIO0_00 can not work normally. So if setting the SIM0_CLK as GPIO0_00 function, then we need to set the SC_P_SCU_GPIO0_00 this PIN to others function, so that no conflict of them. Even no use the pin SC_P_SCU_GPIO0_00 in hardware, we also need to set them to others function to avoid the conflict. SCU_GPIO Pins mux: SCU_GPIO0_00 (SCU_GPIO0_00)   SCU_GPIO0_01 (SCU_GPIO0_01)   SCU_GPIO0_02 (SCU_GPIO0_02)         Tested the PINs "SIM0_CLK, SIM0_IO, SIM0_RST" on iMX8QM MEK with base board. All of them works fine.  The key points are already listed. VDD_SIM0 power should be supplied (It is 3.3V on MEK from PF8100 LDO)   Linux dts should set them to GPIO0 functions:     IMX8QM_SIM0_CLK_LSIO_GPIO0_IO00 0xc0000021     IMX8QM_SIM0_RST_LSIO_GPIO0_IO01 0xc2000021     IMX8QM_SIM0_IO_LSIO_GPIO0_IO02 0xc0000021 The default IOMUX for PINs SC_P_SCU_GPIO0_00, SC_P_SCU_GPIO0_01, SC_P_SCU_GPIO0_02 should be changed from 0 to others.  Test on MEK, we used followed codes in SCFW board_init():     else if (phase == BOOT_PHASE_FINAL_INIT)     {         /* Configure SNVS button for rising edge */         SNVS_ConfigButton(SNVS_DRV_BTN_CONFIG_RISINGEDGE, SC_TRUE);           /* Init PMIC if not already done */         pmic_init();         pad_force_mux(SC_P_SCU_GPIO0_00, 2,             SC_PAD_CONFIG_NORMAL, SC_PAD_ISO_OFF);         pad_force_mux(SC_P_SCU_GPIO0_01, 2,             SC_PAD_CONFIG_NORMAL, SC_PAD_ISO_OFF);         pad_force_mux(SC_P_SCU_GPIO0_02, 2,             SC_PAD_CONFIG_NORMAL, SC_PAD_ISO_OFF);     }  Note: In SCFW, should also set SC_P_SCU_GPIO0_00, SC_P_SCU_GPIO0_01, SC_P_SCU_GPIO0_02 to other functions, because they are set to GPIO0_0x function default, if two PINs set to the same functions, such as SIM0_CLK_DMA pin and SCU_GPIO0_00 pin are set to GPIO0_00 together, the function will not work correctly.   Test commands in LInux: echo 480 > /sys/class/gpio/export echo 481 > /sys/class/gpio/export echo 482 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio480/direction echo out > /sys/class/gpio/gpio481/direction echo out > /sys/class/gpio/gpio482/direction #output high echo 1 > /sys/class/gpio/gpio480/value echo 1 > /sys/class/gpio/gpio481/value echo 1 > /sys/class/gpio/gpio482/value #measure the PINs, they are correct high  ( 3V ) #output low echo 0 > /sys/class/gpio/gpio480/value echo 0 > /sys/class/gpio/gpio481/value echo 0 > /sys/class/gpio/gpio482/value #measure the PINs, they are correct low ( 0V ) The test result is based on real measurement on iMX8QM MEK.    Note: 1\In customer's side If still not work, To confirm the issue, please suggest customer build SCFW with parameter "-m", then use followed commands to dump the IOMUX registers: md 0x41F80000 1 md 0x41F80040 1 md 0x41F80080 1 md 0x41F82140 1 md 0x41F82180 1 md 0x41F83000 1   The "md" command should run from SCFW debug UART, not linux/uboot UART. 2\Make sure the hardware in customer's side VDD_SIM0 power should be supplied .    
記事全体を表示
Some customer want to measure DSM power and do some customize in their own board. We supply the the AN13917 to customer already. But some customer also have some questions about it , so here give more details and test for it for customer will more clearly understand and use it. 1 i.MX 93 power mode overview The i.MX 93 supports the following power modes: Run mode: In this mode, the Cortex-A55 CPU is active and running. Some portions can be shut off for power saving. Low-power run mode: This mode is defined as a Low-power run mode with all external power rails on. In this mode, all unnecessary power domains (MIX) can be off. The AONMIX and internal modules, such as OSC24M/PLL, are an exception in this mode. The Cortex CPU in AONMIX handles all the computing and data processing. Cortex-A55 is powered down and DRAM can be in self-refresh/retention mode. Idle mode: This mode is defined as one that a CPU can enter automatically when no threads are engaged, and no high-speed devices are in use. CPU can be put into a power-gated state, but with L3 data retained, DRAM, and bus clocks are reduced. Most of the internal logic is clock-gated; yet is still powered. In this mode, all the external power from PMIC remains the same, and most IPs remain in their state. Therefore, the interrupt response in this mode is quick compared to the Run mode. Suspend mode: This mode is defined as the most power-saving mode since it shuts off all the clocks and all the unnecessary power supplies. In this mode, the Cortex-A55 CPU is fully power gated, all internal digital logic, and the analog circuits that can be powered down are off, and all PHYs are power gated. VDD_SOC(and related digital supply) voltage is reduced to the "Suspend mode" voltage. Compared to Idle, this mode takes a longer time to exit, but it also uses far less energy. BBSM mode: This mode is also called RTC mode. In this mode, to keep RTC and BBSM logic alive, only the power for the BBSM domain remains on. Off mode: In this mode, all power rails are off. 2 Measure the power consumption of the system in the DSM( Deep Sleep Mode) The use case is based on the Suspend mode, which implies the following: CA55 cluster is OFF • MEDIAMIX is OFF • NICMIX is OFF • WAKEUPMIX is OFF • PLL is OFF • 24 M OSC is OFF PMIC is in STBY mode Download the demo images from website: Download the AN13917SW.zip file, upzip it. Copy the uuu and imx93-11x11-evk-dsm.dtb to demo images path. Download the images to board: .\uuu.exe -b emmc_all .\ imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot  .\imx-image-full-imx93evk.wic To measure the power consumption of the system in the DSM, the steps are as follows: Boot the Linux image with imx93-11x11-evk-DSM.dtb. System boot up with the default dtb, when system boot up change it to the imx93-11x11-evk-DSM.dtb, using the following commends: setenv fdtfile imx93-11x11-evk-dsm.dtb saveenv boot To put the system into the Suspend (Deep sleep) mode, run the following command: echo mem > /sys/power/state Measure the power and record the results. About the BCU Tool: BCU (Board Remote Control Utilities):BCU is a software specially designed to control boards/platforms that support remote control. It provides functions such as on/off key operation, board reset, setting boot mode, controlling GPIO, and power measurement through the debug cable. ------->Remote Control function: $ sudo ./bcu reset sd [-board=xxx] version bcu_1.0.158-0-gdb0a8e5 Auto recognized the board: imx8dxlevk set reset high successfully set onoff high successfully set ft_reset high successfully ENABLE remote control set sd_pwr high successfully set sd_wp high successfully set sd_cd high successfully set boot mode successfully set bootmode_sel low successfully Set ALL sense resistances to smaller ones rebooting... reset successfully done -------->Power measurement function: $ sudo ./bcu monitor -hz=1 [-board=xxx] Here for the power measurement function support the boards have power measurement function. This is the example for the power measurement for the i.MX93 EVK board: 1\Download the BCU tool Releases · nxp-imx/bcu Download the bcu_1.1.100 to Windows 2\Connect the i.MX93 EVK board to Windows PC 3\Open the teminal in the Windows PC C:\Users \Desktop>bcu.exe monitor -board=imx93evk11b1 -hz=1 Use the bcu.exe monitor -board=imx93evk11b1 -hz=1 Make sure the board version is proper, current board is B1 version, so the board name is imx93evk11b1. 4\Run the command in the PC : For others mode test can refer to the BCU.pdf file: https://github.com/nxp-imx/bcu/releases/download/bcu_1.1.100/BCU.pdf Note: To make sure the board version are proper with the related command: bcu.exe monitor -board=imx93evk11b1 -hz=1 For the i.MX93 SOM B2 version Board can use the above command. If the board version is old, such as use the i.MX93 SOM B, here you need to use the command: bcu.exe monitor -board=imx93evk11 If using the bcu.exe monitor -board=imx93evk11b1 the test result are not for this board, here can use the ./bcu eeprom -w -board=imx93evk11 to write the eeprom for the imx93evk11. Using the bcu eeprom -r -board=imx93evk11 see the present status. If we met the problem as bellow we need to check and write to the eeprom again. Measure the power in the DSM mode on the i.MX93 board with SOMB2(board name with the i.mx93evk11b1): old EVK imx93evk11 use a 20m Ohms sensing resistor new EVK imx93evk11b1 use a 5m Ohms sensing resistor For the the i.MX93 board with SOM B Measure the power in the DSM mode on the i.MX93 board with SOMB2 result, use the small and larger range test: Measure the power in the DSM mode on the i.MX93 board with SOMB result: Using the command bcu.exe monitor -board=imx93evk11 -hz=1 3 Questions from customer a.The diff/patch between imx93-11x11-evk.dts and imx93-11x11-evk-dsm.dts If customer use the Linux kernel version: L6.1.55 version BSP, they need to use the imx93-11x11-evk-dsm.dtb we supply. And if using the newer than it and newest BSP in our website, they do not need to change the dtb to the and imx93-11x11-evk-dsm.dtb, just using the imx93-11x11-evk.dts will be OK, as for the Atf  also add the has_wakeup_irq = true;   And in the default imx93-11x11-evk.dts already support the  linux-imx/arch/arm64/boot/dts/freescale/imx93-11x11-evk.dts at lf-6.12.y · nxp-imx/linux-imx · GitHub   So customer and directly use on their products. b. NXP i.MX93 EVK DSM power measurement, the GROUP_SOC_FULL  are some difference from our AN. As different chips may show slight differences in static power consumption(SS TT FF) due to process corner variations.  
記事全体を表示
This article describes how to speed-up the Linux boot time on i.MX 6ULZ to under 2s. Software: Linux BSP 6.12.20-2.0.0 Boot device: SD card The attached imx6ulz-fast-boot.tar.gz archive contains a series of patches which reduces the boot time of the i.MX 6ULZ to ~1.9s. What you'll find in the archive: U-Boot patches: Set the BOOTDELAY to 0 in U-Boot Increase the CPU frequency from 396MHz to 792MHz Add quiet to the kernel bootargs, to suppress the kernel's output during boot Kernel patches: Trim down the kernel to create a minimal version Use LZ4 compression type for the kernel image Minimal rootfs based on BusyBox How to? 1. Prepare the Yocto environment according to Section 3, 4, 5 in i.MX Yocto Project User's Guide. Version 6.12.20-2.0.0, for other versions, you may need to make adjustments. 2. Unzip the imx6ulz-fast-boot.tar.gz archive in the sources directory of your Yocto environment just created. cd ~/imx-yocto-bsp/sources tar -xvpzf imx6ulz-fast-boot.tar.gz -C . 3. Remove additional machine features. Add the configuration below in your conf/local.conf: MACHINE_FEATURES:remove = "\ optee \ alsa \ touchscreen screen \ wifi bluetooth \ bcm4339 bcm43455 \ nxp8987-sdio nxpwifi-all-sdio \ rtc qemu-usermode"  4. Build the image. bitbake core-image-busybox The resulted core-image-busybox-imx6ulz-14x14-evk.rootfs.wic should have ~38M. 5. Write the image on an SD card, and boot. It should boot under 2s from reset to prompt. If you are connected to the serial port of the board, press any key continuously to stop in U-Boot.
記事全体を表示
As we haven't provided a guide with steps that implement the Linux OS encryption and signature for i.MX9x products so far. So, the document provides the steps for that. For details related to how to encrypt and sign a bootloader image, please have a reference to This Guide 
記事全体を表示
Background : Some customer wants to know the DRAM's MR register value. But, For now, we do not have any documentation or binary to complete this. So, this article aim to show how to read this register.   Hardware environment : i.MX8ULP EVK board Software environment : uboot-imx : lf_v2024.04   1. The related registers information are as following:   DENALI CTL 165 [READ MODEREG[24:8]] Read the specified memory mode register from specified chip when start bit set. Bits (7:0) define the memory mode register and bits (15:8) define the chip select. Set bit (16) to 1 to trigger.   DENALI CTL 166 [PERIPHERAL MRR - DATA[31:0]] Data and chip returned from memory mode register read requested by the READ MODEREG parameter. Bits (7:0) indicate the read data and bits (15:8) indicate the chip. READ-ONLY   2. Test result :         Type the below command: mrr <chip_select MR_register>  Like the below picture, when type the mrr 0 c, it means the chip select is 1 and the MR register is MR12, then the value of MR12 register can be output , is 0x1c.     Note : When read the MR register, must make sure the register has read right. Because most of MR register only have write right. you can check about it on JDEC spec document.   If you want to get the test binary file, please contact to me, i will send it to you.
記事全体を表示
i.MX8MP and i.MX95 both support USB3.0. In EVK board, USB download pin is USB3.0 with Type-C.  While in other boards, they may delete CC logic design PTN5110, or use USB2.0 signals instead. This document describes how to modify U-Boot to support a design without PTN5110 when using the uuu tool to download.
記事全体を表示
This document explains how to enable and test Bluetooth 6LoWPAN (IPv6 over Low-power Wireless Personal Area Networks) in the i.MX Linux BSP.   Environment   i.MX Linux BSP 6.6.52-2.2.0 (based on Yocto scrathgap) i.MX 93 EVK (2 units) An Embedded Artists 2EL M.2 module with the Murata LBES5PL2EL module (containing NXP IW612) is inserted into the i.MX 93 EVK's M.2 slot and connected to the onboard Wi-Fi/BT antenna. One i.MX 93 EVK will serve as the Peripheral device, while the other will act as the Central device. It should also work with i.MX 8 and 9 series evaluation kit equipped with Bluetooth LE modules.   Configurations   Although the Linux kernel includes a Bluetooth 6LoWPAN driver, it is disabled in the i.MX Linux BSP. Therefore, we will modify the kernel configuration to enable it. Add 2 settings below in kernel configuration file (imx_v8_defconfig) to build the required drivers as modules: CONFIG_6LOWPAN=m CONFIG_BT_6LOWPAN=m These settings can be found in the following section of the Linux kernel menuconfig. CONFIG_6LOWPAN: Depends on: NET [=y] && IPV6 [=y] Location: -> Networking support (NET [=y]) -> Networking options -> 6LoWPAN Support (6LOWPAN [=m]) CONFIG_6LOWPAN  CONFIG_BT_6LOWPAN: Depends on: NET [=y] && BT_LE [=y] && 6LOWPAN [=y] Location: -> Networking support (NET [=y]) -> Bluetooth subsystem support (BT [=y]) -> Bluetooth Low Energy (LE) features (BT_LE [=y]) -> Bluetooth 6LoWPAN support (BT_6LOWPAN [=m]) Rebuild the image containing the Linux kernel and make sure that the required drivers are present in the following paths. /lib/modules/6.6.52-ge0f9e2afd4cf-dirty/kernel/net/6lowpan/6lowpan.ko /lib/modules/6.6.52-ge0f9e2afd4cf-dirty/kernel/net/bluetooth/bluetooth_6lowpan.ko   Operations for Peripheral device   Boot the Peripheral device EVK and log in as the root user. NXP i.MX Release Distro 6.6-scarthgap imx93-11x11-lpddr4x-evk ttyLP0 imx93-11x11-lpddr4x-evk login: root Load the NXP Bluetooth UART driver to enable Bluetooth. # modprobe btnxpuart Start the Bluetooth hci0 interface with the hciconfig command. # hciconfig hci0 up Type hciconfig command to check the BD Address of the Bluetooth hci0 interface and confirm that its status is "UP RUNNING". # hciconfig -a hci0: Type: Primary Bus: UART BD Address: D0:17:69:12:34:56 ACL MTU: 1021:7 SCO MTU: 120:6 UP RUNNING RX bytes:862 acl:0 sco:0 events:59 errors:0 TX bytes:1085 acl:0 sco:0 commands:58 errors:0 Features: 0xbf 0xfe 0x8f 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: PERIPHERAL ACCEPT Name: 'imx93-11x11-lpddr4x-evk' Class: 0x200000 Service Classes: Audio Device Class: Miscellaneous, HCI Version: 5.4 (0xd) Revision: 0x8300 LMP Version: 5.4 (0xd) Subversion: 0x1015 Manufacturer: NXP Semiconductors (formerly Philips Semiconductors) (37) Load the Bluetooth 6LoWPAN driver. # modprobe bluetooth_6lowpan Enable Bluetooth 6LoWPAN. # echo 1 > /sys/kernel/debug/bluetooth/6lowpan_enable Start Bluetooth advertising and waits for a connection request from the Central device. # bluetoothctl advertise on   Operations for Central device   Boot the Central device EVK and log in as the root user. NXP i.MX Release Distro 6.6-scarthgap imx93-11x11-lpddr4x-evk ttyLP0 imx93-11x11-lpddr4x-evk login: root Load the NXP Bluetooth UART driver to enable Bluetooth. # modprobe btnxpuart Start the Bluetooth hci0 interface with the hciconfig command. # hciconfig hci0 up Type hciconfig command to check the BD Address of the Bluetooth hci0 interface and confirm that its status is "UP RUNNING". # hciconfig -a hci0: Type: Primary Bus: UART BD Address: D0:17:69:AB:CD:EF ACL MTU: 1021:7 SCO MTU: 120:6 UP RUNNING RX bytes:862 acl:0 sco:0 events:59 errors:0 TX bytes:1085 acl:0 sco:0 commands:58 errors:0 Features: 0xbf 0xfe 0x8f 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: PERIPHERAL ACCEPT Name: 'imx93-11x11-lpddr4x-evk' Class: 0x200000 Service Classes: Audio Device Class: Miscellaneous, HCI Version: 5.4 (0xd) Revision: 0x8300 LMP Version: 5.4 (0xd) Subversion: 0x1015 Manufacturer: NXP Semiconductors (formerly Philips Semiconductors) (37) Load the Bluetooth 6LoWPAN driver. # modprobe bluetooth_6lowpan Enable Bluetooth 6LoWPAN. # echo 1 > /sys/kernel/debug/bluetooth/6lowpan_enable Send a connection request to the Peripheral device. (In this example, the BD address of the Peripheral device is D0:17:69:12:34:56.) # echo "connect D0:17:69:12:34:56 1" > /sys/kernel/debug/bluetooth/6lowpan_control After waiting for a few tens of seconds, the bt0 network interface will appear. (At the same time, the bt0 network interface will appear on the Peripheral device that accepted the connection.) # ifconfig bt0 bt0: flags=4161<UP,RUNNING,MULTICAST> mtu 1280 inet6 fe80::d017:69ff:feab:cdef prefixlen 64 scopeid 0x20<link> unspec D0-17-69-AB-CD-EF-00-00-00-00-00-00-00-00-00-00 txqueuelen 1000 (UNSPEC) RX packets 9 bytes 884 (884.0 B) RX errors 0 dropped 4 overruns 0 frame 0 TX packets 13 bytes 1069 (1.0 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 The Central device and Peripheral device are now connected via Bluetooth 6LoWPAN.   Testing Send a ping from the Central device to the Peripheral device. (In this example, the IPV6 address of the Peripheral device is fe80::d017:69ff:fe12:3456.) # ping6 fe80::d017:69ff:fe12:3456%bt0 PING fe80::d017:69ff:fe12:3456%bt0 (fe80::d017:69ff:fe12:3456%bt0) 56 data bytes 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=1 ttl=64 time=181 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=2 ttl=64 time=125 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=3 ttl=64 time=67.7 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=4 ttl=64 time=56.1 ms ...   Benchmarking   Run the iperf3 server on the Peripheral device. # iperf3 -s Run the iperf3 benchmark on the Central device. For example, check the TCP connections. # iperf3 -V -c fe80::d017:69ff:fe12:3456%bt0 You can also check UDP connections. For example, the following example sends UDP 200Kbps bandwidth. # iperf3 -V -c fe80::d017:69ff:fe12:3456%bt0 -u -b 200K   Disclaimer   This document is provided as a reference for utilizing NXP products. Please refer to the official product manuals and application notes for formal specifications. Due to differences in software versions and other conditions, actual behavior may differ from the descriptions provided. This document does not verify all functions, so please be sure to conduct appropriate validation and testing to ensure suitability for your intended use.  
記事全体を表示
Streaming different use case pipelines between i.MX 95 and i.MX 8M Plus LF-6.12.20
記事全体を表示
We are pleased to announce that Config Tools for i.MX v25.09 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) • The Release Notes format is updated from plain text to markdown. • The newly generated configuration includes the default NXP copyright notice and is licensed under the BSD-3-Clause license. • DDR tool – ODT and Driver Strength Updates for LP4/LP5 on i.MX 943 and i.MX 95 – Improved DRAM Configuration for i. MX 9x devices – Multicore support is enabled for DDR tests on i.MX 943 and i.MX 95 – Linux support for the DDR tool – Vref DQ Setting now available in the GUI – Board-agnostic SM Support for i.MX 943 and i.MX 95 – DDR part number entry is supported in the GUI – Enhanced logging from the target application – Stress test repetition option is enabled – Updated ODT shmoo scenario values on i.MX 943 and i.MX 95 – Support for SNPS FW and PHY Init 2024.09 SP2 on i.MX 943 and i.MX 95 – AHAB image update to align with BSP for CES parts on i.MX 943 and i.MX 95 – New configuration support for 15x15 on i.MX 943 – Improved bus configuration for single-channel setups – LP4/LP5 CS signal configuration now exposed in the GUI for i.MX 943 and i.MX 95 • Clocks – Supported input frequency setting • System Manager – Initial version of the tool
記事全体を表示
This article describe some bring up tips during i.MX95 board debug, including HW and SW aspects.  
記事全体を表示
based on customer's issue when use PTF pins of imx8ulp as GPIO or gpio hog
記事全体を表示
  This document shows how to use the open source gstreamer1.0-rtsp-server package on i.MX6QDS and i.MX8x to stream video files and camera using RTP protocol.  The i.MX 6ULL and i.MX 7 doesn't have Video Processing Unit (VPU). Real time protocol (RTP) is a very common network protocol for delivering media over IP networks. On the board, you will need a GStreamer pipeline that encodes the raw video, adds the RTP payload, and sends over a network sink. A generic pipeline would look as follows: video source ! video encoder ! RTP payload ! network sink Video source: often it is a camera, but it can be a video from a file or a test pattern, for example. Video encoder: a video encoder as H.264, H.265, VP8, JPEG and others. RTP payload: an RTP payload that matches the video encoder. Network sink: a video sync that streams over the network, often via UDP. Pre-Requisites: MX6x o MX8x board with the L6.6.52 BSP installed. A host PC with either Gstreamer or VLC player installed.   Receiving h264 / h.265 Encoded RTP Video Stream on a Host Using GStreamer: GStreamer is a low-latency method for receiving RTP video. On your host machine, install Gstreamer and send the following command: $ gst-launch-1.0 -v udpsrc port=5000 caps = "application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" ! rtph264depay ! decodebin ! videoconvert ! autovideosink sync=false   Using HOST PC: VLC Player Optionally, you can use VLC player to receive RTP video on a PC. First, in your PC, create a sdp file with the following content:  stream.sdpv=0m=video 5000 RTP/AVP 96c=IN IP4 127.0.0.1a=rtpmap:96 H264/90000 After this, with the GStreamer pipepline on the device running, open this .sdp file with VLC Player on the host PC.   Sending h.264 and h.265 Encoded RTP video stream GStreamer provides an h.264 encoding element by software named x264enc. Use this plugin if your board does not support h.264 encoding by hardware or if you want to use the same pipeline on different modules. Note that the video performance will be lower compared with the plugins with encoding accelerated by hardware. # gst-launch-1.0 videotestsrc ! videoconvert ! x264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Note: Replace <host-machine-ip> by the IP of the host machine. In all examples you can replace videotestsrc by v4l2src element to collect a stream from a camera   i.MX8X # gst-launch-1.0 videotestsrc ! videoconvert ! v4l2h264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000   i.MX8M Mini Quad / 8M Plus # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 i.MX6X The i.MX6QDS does not support h.265 so the h.264 can work: # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Using other video Encoders While examples of streaming video with other encoders are not provided, you may try it yourself. Use the gst-inspect tool to find available encoders and RTP payloaders on the board: # gst-inspect-1.0 | grep -e "encoder"# gst-inspect-1.0 | grep -e "rtp" -e " payloader" Then browse the results and replace the elements in the original pipelines. On the receiving end, you will have to use a corresponding payload. Inspect the payloader element to find the corresponding values. For example: # gst-inspect-1.0 rtph264pay   Install rtp in your yocto different form L6.6.52 BSP, to install gstreamer1.0-rtsp-server in any Yocto Project image, please follow the steps below: Enable meta-multimedia layer: Add the following on your build/conf/bblayers.conf: BBLAYERS += "$"${BSPDIR}/sources/meta-openembedded/meta-multimedia" Include gstreamer1.0-rtsp-server into the image: Add the following on your build/conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server" Run bitbake and mount your sdcard. Copy the binaries: Access the gstreamer1.0-rtsp-server examples folder: $ cd /build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0-rtsp-server/$version/build/examples/.libs Copy the test-uri and test-launch to the rootfs /usr/bin folder. $ sudo cp test-uri test-launch /media/USER/ROOTFS_PATH/usr/bin Be sure that the IPs are correctly set: SERVER: => ifconfig eth0 $SERVERIP CLIENT: => ifconfig eth0 $CLIENTIP Video file example SERVER: => test-uri file:///home/root/video_file.mp4 CLIENT: => gst-launch-1.0 playbin uri=rtsp://$SERVERIP:8554/test You can try to improve the framerate performance using manual pipelines in the CLIENT with the rtspsrc plugin instead of playbin. Follow an example: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test caps = 'application/x-rtp'  ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! queue max-size-buffers=0 ! imxv4l2sink sync=false   Camera example SERVER: => test-launch "( imxv4l2src device=/dev/video0 ! capsfilter caps='video/x-raw, width=1280, height=720, framerate=30/1, mapping=/test' ! vpuenc_h264 ! rtph264pay name=pay0 pt=96 )" CLIENT: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test ! decodebin ! autovideosink sync=false The rtspsrc has two properties very useful for RTSP streaming: Latency: Useful for low-latency RTSP stream playback (default 200 ms); Buffer-mode: Used to control buffer mode. The slave mode is recommended for low-latency communications. Using these properties, the example below gets 29 FPS without a sync=false property in the sink plugin. The key achievement here is the fact that there is no dropped frame: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test latency=100 buffer-mode=slave ! queue max-size-buffers=0 ! rtph264depay ! vpudec ! imxv4l2sink    
記事全体を表示
  This article shows how to use the i.MX6DL/Q to transcode and stream videos on 1080i/p @ 24fps and 720p @ 30fps. For this test, we used one i.MX6DL as server and an i.MX6DL and i.MX6Q as clients. The video is streamed by the server, playing the sound at the same time, while the clients show the video in the HDMI output, as the image below:     This test depends on some GStreamer plugins. To check that the right GStreamer plugins are installed type the following commands: $ gst-inspect-1.0 | grep h264 To return all the H.264 related plugins, or: $ gst-inspect-1.0 decodebin To check directly the command. To connect more than one board to the minicom, open it with the command: $ sudo minicom –s This way, you open the configuration menu. Enter in the “Serial port setup” option and press “A” to set or change the PORTNUMBER, in “ttyUSB$PORTNUMBER”. To set the HDMI output, run the commands below from the U-Boot prompt: => setenv mmcargs 'setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 consoleblank=0' => saveenv Be sure that the IPs are correctly setted: SERVER: => ifconfig eth0 $SERVERIP CLIENTS: => ifconfig eth0 $CLIENTSIP Streaming transcoded video only SERVER: => gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 CLIENTS: => gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, payload=(int)96' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false Streaming transcoded video + audio SERVER: => gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin name=demux demux. ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 demux. ! alsasink CLIENTS: => gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, encoding-name=(string)H264' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false   You can check the results with the 1080p@24fps.
記事全体を表示
Overview The purpose of this document is to provide guidance for FlexIO 8080 display capability. Generally, the 8080 bus interface consists of one chip-select line (CS), one writing-latch line (WR), one reading-latch line (RD), one data/command-select line (RS, also called D/C), and 8 or 16 bidirectional data lines (Data Bus). Since The FlexIO instance of i.MX 943 support only 16 pins, the demo can only support 8 bit 8080 mode(two pin should be used as WR and RD signal.   Below are pins used in the 8 bit 8080 display. Panel Setup The panel in the example is X-LCD-PAR-S035. To use 8 bit 8080 mode, need ser IM[2:0] to be 011. Connection and Software i.MX 943 Need pull down SPI8_SEL1 and SPI8_SEL3 of PCA6416 in SW to select Arduino for 8080 pins D[7:4]. Here is the patch for system manager. For quick verification, use flash_m70 when building bootloader. diff --git a/configs/mx94evk.cfg b/configs/mx94evk.cfg index 9d46976..90bf089 100755 --- a/configs/mx94evk.cfg +++ b/configs/mx94evk.cfg @@ -499,6 +499,9 @@ ENC_PLL OWNER ENDAT2_1 OWNER ENDAT2_2 OWNER ENDAT3_1 OWNER +GPIO2 OWNER +GPIO3 OWNER +FLEXIO1 OWNER FLEXIO3 OWNER FLEXIO4 OWNER FLEXPWM1 OWNER @@ -515,6 +518,7 @@ HIPERFACE_SAFE1_2 OWNER HIPERFACE_SAFE2_1 OWNER HIPERFACE_SAFE2_2 OWNER IRQSTEER_M7_0 OWNER +LPI2C6 OWNER LPIT1 OWNER LPTMR1 OWNER LPTMR2 OWNER @@ -557,6 +561,25 @@ XBAR_DSC3 OWNER PIN_GPIO_IO24 OWNER PIN_GPIO_IO25 OWNER +# 8080 +PIN_GPIO_IO00 OWNER +PIN_GPIO_IO01 OWNER +PIN_GPIO_IO02 OWNER +PIN_GPIO_IO03 OWNER +PIN_GPIO_IO08 OWNER +PIN_GPIO_IO09 OWNER +PIN_GPIO_IO10 OWNER +PIN_GPIO_IO11 OWNER +PIN_GPIO_IO12 OWNER +PIN_GPIO_IO13 OWNER +PIN_GPIO_IO14 OWNER +PIN_GPIO_IO15 OWNER +PIN_GPIO_IO38 OWNER + +# I2C6 +PIN_GPIO_IO28 OWNER   Attached imx943_flexio_8080_8bit.zip is patch for m70 demo based on SDK_25_06_00_MCIMX943-EVK.   i.MX 93 Need pull up EXP_SEL(pin4 R4) of ADP5585 in SW to route some pins. Attached imx93_flexio_8080_8bit.zip is patch for m33 demo based on SDK_25_06_00_MCIMX93-EVK. The running status is similar as i.MX943.
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX8MP-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX8MP-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX8MP-EVK SDK   Import "hello world" example Ensure that we are compiling a debug binary Build Project Flash the Binary using UUU Tool Connect the IMX8MP-EVK Board to your Host PC via USB   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write hello_world.bin mmc X:1 hello_world_debug.bin Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card   Connect MCU-LINK Pro to the Target   IMX8MP-EVK Debug connection:     Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 0x48000000 hello_world_debug.bin; cp.b 0x48000000 0x7e0000 0x20000; => bootaux 0x7e0000 Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card   Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso:          With the MCU-LINK Pro configured, the IMX8MP-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX8MP based projects.   References: AN14120.pdf 
記事全体を表示
The documentation is to provide steps for single secure boot for BSP Android 14.0.0_2.0.0. More details related to secure boot for Android BSP can be found from IMX ANDROID SECURE BOOT. However, the steps in this document facilitate some helps signing an Android boot image in the aspects of - First, the Android build process for signing the image, and second, the FDT signing process must be performed after the SPL/FIT of the signing process. The second one of which is crucial.   Best regards Harvey
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX8MN-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX8MN-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX8MN-EVK SDK   Import "hello world" example Ensure that we are compiling a debug binary Build Project   Flash the Binary using UUU Tool Connect the IMX8MN-EVK Board to your Host PC via USB   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write hello_world.bin mmc X:1 hello_world_debug.bin Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card   Connect MCU-LINK Pro to the Target   IMX8MN-EVK Debug connection:   Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 0x48000000 hello_world_debug.bin; cp.b 0x48000000 0x7e0000 0x20000; => bootaux 0x7e0000 Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card   Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso:      With the MCU-LINK Pro configured, the IMX8MN-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX8MN based projects.   References: AN14120.pdf 
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX8MM-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX8MM-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX8MM-EVK SDK   Import "hello world" example Ensure that we are compiling a debug binary Build Project   Flash the Binary using UUU Tool Connect the IMX8MM-EVK Board to your Host PC via USB   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write hello_world.bin mmc X:1 hello_world_debug.bin Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card Connect MCU-LINK Pro to the Target     IMX8MM-EVK Debug connection:   Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 0x48000000 hello_world_debug.bin; cp.b 0x48000000 0x7e0000 0x20000; => bootaux 0x7e0000 Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card     Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso:      With the MCU-LINK Pro configured, the IMX8MM-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX8MM based projects.   References: AN14120.pdf 
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX93-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX93-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX93-EVK SDK     Import "hello world" example   Ensure that we are compiling a debug binary Build Project   Flash the Binary using UUU Tool Connect the IMX93-EVK Board to your Host PC via USB       Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write sdk20-app.bin mmc X:1 hello_world.bin Note: replace the X with 0 if you are booting from eMMC or 1 if you are booting from SD Card     Connect MCU-LINK Pro to the Target     IMX93-EVK Debug connection:       Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 80000000 hello_world.bin; cp.b 0x80000000 0x201e0000 0x10000; => bootaux 0x1ffe0000 0 Note: replace the X with 0 if you are booting from eMMC or 1 if you are booting from SD Card     Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso:        With the MCU-LINK Pro configured, the IMX93-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX93-based projects.   References: AN14120.pdf 
記事全体を表示
Hello! In this post, we’ll cross-compile a kernel module for Linux 6.12.    This can be done either using a standalone kernel or a Yocto-built kernel.    Requirements:  A compiled Linux kernel 6.12.  A board running the same kernel version (Linux 6.12 in this case).  A cross-compiler toolchain.    This process applies to any i.MX processor, including i.MX8, i.MX8M, i.MX8MM, i.MX8MN, i.MX8MP, i.MX93, i.MX91, i.MX95, as well as the i.MX6 and i.MX7 families.    Step 1: Compile the Linux Kernel and get the Toolchain    First, you need to compile the Linux kernel (6.12 in this case).    You can do this in a standalone environment or using Yocto.     If you are using a Standalone environment, please refer to the Chapter 4.5.12 How to build U-Boot and Kernel in standalone environment of i.MX Linux User's Guide.  Also, in that document section, you will see how to obtain the cross-compiler toolchain.    NOTE: To get the toolchain you need use Yocto at least once (for more information please refer to i.MX Yocto Project User's Guide😞  $ DISTRO=fsl-imx-xwayland MACHINE=Target-Machine bitbake core-image-minimal -c populate_sdk   At the end of the building, you can install your toolchain populated under:    yocto-bsp/build/tmp/deploy/sdk     There you will find a file called:    fsl-imx-wayland-glibc-x86_64-imx-image-core-armv8a-your-machine-name-toolchain-6.12-walnascar.sh    Execute with:  $ sudo ./fsl-imx-wayland-glibc-x86_64-imx-image-core-armv8a-your-machine-name-toolchain-6.12-walnascar.sh   If you use the default installation, you will have your toolchain under /opt in your host machine.      (If you will use the compiled kernel from Yocto, you can avoid below step)  Download Standalone Kernel source by cloning with:  $ git clone https://github.com/nxp-imx/linux-imx -b lf-6.12.y $ cd linux-imx   To build the kernel in the standalone environment for i.MX 6 and i.MX 7, execute the following commands:    $ make imx_v7_defconfig $ Make   To build the kernel in the standalone environment for i.MX 8 and i.MX 9, execute the following commands:  $ make imx_v8_defconfig $ make   The full kernel compilation is required to generate headers and symbol files required for external module compilation, even if you don't plan to boot this kernel directly.      Step 2: Write a simple Kernel Module to test    Now that your kernel is compiled, you can write a basic kernel module for testing.    Create a new directory. It will have our hello.c and Makefile.    We will create the file hello.c:  #include <linux/init.h> #include <linux/module.h> #include <linux/kernel.h> MODULE_LICENSE("GPL"); MODULE_AUTHOR("Salas"); MODULE_DESCRIPTION("A simple kernel module example for cross-compilation."); MODULE_VERSION("0.1"); static int __init hello_init(void) { printk(KERN_INFO "Hello from the kernel module!\n"); return 0; } static void __exit hello_exit(void) { printk(KERN_INFO "Goodbye from the kernel module!\n"); } module_init(hello_init); module_exit(hello_exit);   Then, create a basic Makefile to compile the modules:    # Module name obj-m += hello.o # Build flags ldflags-y += --strip-debug # Kernel source directory (provided by Yocto) KERNEL_SRC ?= /path/to/your/compiled/kernel # Build target all: $(MAKE) -C $(KERNEL_SRC) M=$(PWD) modules # Clean target clean: $(MAKE) -C $(KERNEL_SRC) M=$(PWD) clean # Install target modules_install: $(MAKE) -C $(KERNEL_SRC) M=$(PWD) modules_install   KERNEL_SRC should be your compiled kernel from your Yocto build:   yocto-bsp/build/tmp/work/your-machine-poky-linux/linux-imx/6.12.20+git/build   Or the Standalone : path/to/linux-imx/     Step 3: Set the toolchain and compile the kernel module    Finally, we can compile the kernel module.    First, set the toolchain (in my case):  $ source /opt/fsl-imx-wayland/6.12-walnascar/environment-setup-armv8a-poky-linux   Then, compile using the makefile:  $ make   f everything goes well, at final you will have the generated files:    hello.ko hello.mod hello.mod.c hello.mod.o hello.o Makefile modules.order Module.symvers   The one we need is the hello.ko (Kernel Object).    We can check if the file was created correctly using:    $ readelf -h hello.ko ELF Header: Magic: 7f 45 4c 46 02 01 01 00 00 00 00 00 00 00 00 00 Class: ELF64 Data: 2's complement, little endian Version: 1 (current) OS/ABI: UNIX - System V ABI Version: 0 Type: REL (Relocatable file) Machine: AArch64 Version: 0x1 Entry point address: 0x0 Start of program headers: 0 (bytes into file) Start of section headers: 33992 (bytes into file) Flags: 0x0 Size of this header: 64 (bytes) Size of program headers: 0 (bytes) Number of program headers: 0 Size of section headers: 64 (bytes) Number of section headers: 41 Section header string table index: 40   We can see the Machine is AArch64 and the Type is a Relocatable file.      Step 4: Running the Kernel Object/Module in the board    Transfer the generated hello.ko file from your host machine to your board.    Then, In your board you can run with:    root@imx93evk:~# ls hello.ko root@imx93evk:~# insmod hello.ko root@imx93evk:~# dmesg | tail [ 5140.547447] Hello world from kernel! root@imx93evk:~# rmmod hello.ko root@imx93evk:~# dmesg | tail [ 5140.547447] Hello world from kernel! [ 5153.415215] Goodbye world from kernel!   I hope this can helps to you.    Best regards,  Salas. 
記事全体を表示