Network File System (NFS)
Setting the host
1 - Install NFS Service on host typing:
$sudo apt-get install nfs-kernel-server
2 - Create symbolic link to ltib/rootfs
$sudo ln -s <ltib instalation folder>/rootfs /tftpboot/rootfs
3 - Setup exports typing:
$sudo gedit /etc/exports
and add the following line:
/tftpboot/rootfs/ *(rw,no_root_squash,no_subtree_check,async)
4 - Restart the NFS server:
$sudo /etc/init.d/nfs-kernel-server restart
Now the host is ready to use NFS
Setting Target Linux Image to use NFS
1. Run LTIB configuration by typing:
$cd <ltib instalation folder>
$./ltib -c
2 . On first page menu, go to "Target Image Generation -> Options"
3. Select the option NFS only and exit LTIB configuration to compile with the new configuration.
4. LTIB should start new compiling and create a new Linux image on /<ltib instalation folder>/rootfs/boot/zImage
5. Copy the created image on /<ltib instalation folder>/rootfs/boot/zImage to /tftpboot/zImage
6. The system is ready to run with NFS. The root file system on target will be located on host on /<ltib instalation folder>/rootfs/