i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Some case need configure the GPIO as power off button. One solution is to use “gpio-keys” to send the “KEY_POWER” event to the system. Co-work with systemd, system gets power off.  
查看全文
     
查看全文
Steps to replace the Wi-Fi/Bluetooth firmware on the i.MX 8M series on Linux    Applicable to versions L5.4.47, L5.4.70, L5.10.9   1. Download the newest firmware. you can download the attachment in this thread and unzip it. 2. Copy it to the EVK board. 3. Copy the firmware to /lib/firmware/nxp   root@imx8mmevk: cp pcieuart8997_combo_v4.bin sdiouart8987_combo_v0.bin  /lib/firmware/nxp If the Linux version is L5.4.3,Then the step3 is to copy firmware to lib/firmware/mrvl/ root@imx8mmevk: cp pcieuart8997_combo_v4.bin sdiouart8987_combo_v0.bin  /lib/firmware/mrvl    
查看全文
Purpose This is early communication to notify i.MX 8M Dual/8M QuadLite/8M Quad customers of a potential incorrect PCIe power supply configuration on certain NXP BSP Linux and Android versions. Description The PCIE_VPH power supply is selectable in software  between 1.8V and 3.3V. When the PCIE_VPH supply is configured to operate at 3.3V, the 1.8V internal regulator (disabled by default) must be enabled to prevent overstress conditions on the PCIe PHY. If the 1.8V internal regulator is left disabled when the PCIE_VPH supply is configured to operate at 3.3V, it could potentially impact the product lifetime of the device.   Impact •i.MX 8M Dual/8M QuadLite/8M Quad (other i.MX processors are not impacted) •Only Impacts Linux/Android kernel versions earlier than L5.4.70_2.3.2 or Linux 5.10.9_1.0.0 releases MITIGATION •When the PCIE_VPH supply is configured to operate at 3.3V users need to enable the internal regulator by setting the IOMUXC_GPR_GPR14 and IOMUXC_GPR_GPR16 registers - PCIE1_VREG_BYPASS and PCIE2_VREG_BYPASS bit to 0. •There are 3 software patches for each release. Software patch details in the Code Aurora Forum (CAF): •For L5.4.70_2.3.2 patch release, the git log references are: •MLK-25349-3 PCI: imx: clear vreg bypass when pcie vph voltage is 3v3 •MLK-25349-2 arm64: dts: imx8mq-evk: add one regulator used to power up pcie phy •MLK-25349-1 dt-bindings: imx6q-pcie: add one regulator used to power up pcie phy • •The L5.4.70_2.3.2, LF_5.10 Q2 and later BSP releases correctly configure and enable the internal regulator by setting the IOMUXC_GPR_GPR14 and IOMUXC_GPR_GPR16 registers The Patch MLK-25349 which correctly enables the internal regulator is already included in the L5.4.70_2.3.2 patch release and release versions after it. MITIGATION •The following branches of Linux/Android BSP releases contain the MLK-25349 patch. The patch is attached below for each respective release.   •Other branches which are not listed should try to apply the nearest Patch version patch. If a user encounters any conflicts in applying, they should back porting from below nearest patch release version below. imx_4.9.51_ga, imx_4.9.y_android_imx8m_ga_v2                           - Patch attached  imx_4.9.88_ga, imx_4.9.y_android_2.0.0_ga                                   - Patch attached  imx_4.14.y and imx_4.14.98_2.3.0, imx_4.14.98_2.3.0_android     - Patch attached  imx_4.19.y and imx_4.19.35_1.1.0, imx_4.19.35_1.1.0_android     - Patch attached  imx_5.4.y, imx_5.4.3_2.0.0, imx_5.4.3_2.0.0_android                     - Patch attached Documentation Change Description – 1 of 3 for Datasheet Updated Datasheets and Reference Manual will be published to nxp.com. Updated Hardware Design guide and Schematics have already been published on nxp.com.  Updated the descriptions of PCIE_VPH in the Datasheet Table 8, "Operating ranges"     Documentation Change Description – 2 of 3 for Reference Manual (RM) Updated the description of field 12 "PCIE1_VREG_BYPASS" in 8.2.4.15 GPR14 General Purpose Register (IOMUXC_GPR_GPR14)           Documentation Change Description – 3 of 3 for RM Updated the description of field 12 "PCIE2_VREG_BYPASS" in 8.2.4.17 GPR16 General Purpose Register (IOMUXC_GPR_GPR16)   REFERENCES •i.MX 8M Dual / 8M QuadLite / 8M Quad Product Lifetime Usage  •i.MX 8M Dual / 8M QuadLite / 8M Quad Applications Processors Data Sheet for Industrial Products •i.MX 8M Dual / 8M QuadLite / 8M Quad Applications Processors Data Sheet for Consumer Products •i.MX 8MDQLQ Hardware Developer’s Guide  •i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual  
查看全文
Software environment: L5.4.47_2.2.0 Hardware i.MX8QXPC0 EVK board In the uuu script we can see the bootloader imx-boot-imx8qxpc0mek-sd.bin-flash is necessary. The default BSP build generate in the yocto project is with the spl, some customers are confused about the how to build the imx-boot-imx8qxpc0mek-sd.bin-flash. Here I give the manually compile way and generate it in yocto. In the yocto generate it is more convenient than the manually compile way. Hope this can do help for you.
查看全文
i.MX8DXL DDR3L EVK board, nor flash using is MT25QU512ABB8ESF-0SIT. This doc will show reference of FlexSPI configuration parameters to make booting from MT25Q flash, with QUAD pad and DDR mode. HW: i.MX8DXL DDR3L EVK board SW: Linux 5.4.70 BSP From RM 5.9.3.2 FlexSPI serial flash BOOT operation, the FlexSPI boot flow as :   FlexSPI configuration parameters,  could be think as two kind group: parameter for FlexSPI controller,  parameter related to the operation on nor flash.   Full parameter table check check i.MX8DXL RM Table 5-20. FlexSPI Configuration block. Let us check MT25Q data sheet for its feature, note our target is DDR mode(80MHZ) and QUAD pad:     Now let us change the FlexSPI configuration parameters: 1>readSampleClkSrc , set as 2 , that is loop back from SCK pad; this filed default set as 0, as found default value booting will met failure in this use case, so change to 2. 2>deviceModeCfgEnable set 1, deviceModeSeq.seqNum set 1 , deviceModeSeq. seqId set to 4; deviceModeArg set 0x5f. i.MX8DXL will send some cmd to flash to make MT25Q enter DDR mode and QUAD mode, so deviceModeCfgEnable =1. For seqNum=1, seqId =4; means index 4 of LUT table will store this sequence, and cost one LUT entry. We will explain how to change LUT entry later. For deviceModeArg=0x5f, check MT25Q data sheet, its enhanced volatile register could be write to configure the flash working mode:  3>controllerMiscOption as 0x40, this parameter only for FlexSPI controller itself, means as” External device works using DDR commands”. 4>deviceType=1(Serial Nor),  sflashPadType=4 (QUAD pad),  serialClkFreq=4(80MHZ CLK), these parameter also only for FlexSPI controller. 5>sflashA1Size fill actual size, in terms of bytes 6>LUT entry changes, check 8DXL RM Table 5-21: So LUT entry 0 is sequence for Read command, entry 1 is for Read Status sequence, entry 3 is for Write Enable sequence,  entry 15 is for Dummy command sequence. Other index LUT entry(for example 2,4,6,7,8,10,12,13,14) is could be used for store your sequence for some cmd your flash device neede. We store sequence of writing MT25Q enhance volatile register as LUT entry 4. Check 8DXL RM,  Figure 15-6. LUT and sequence structure:   Each LUT entry (sequence) will using 16 byte,  one sequence consists of up to 8 instructions, each instruction will using 16bit. Each instruction  format as opcode—num_pads—operand. Check RM 15.2.4.8 Programmable Sequence Engine, for supported instructions:   Actually the Write enable sequence is run first before the other sequence, as we will write Mt25Q volatile register, before that need issue Write enable sequence. Check MT25Q data sheet: For this sequence only need one instruction, that is 0x0406, at this time still using is SDR and one pad mode:  Opcode (CMD_SDR),  one pad (0), operand (6).   LUT entry 1, Read status sequence, it is READ STATUS REGISTER (05h) of MT25Q , check data sheet: It use two instructions: 0x0405: opcode(CMD_SDR), pad (one pad), operand (0x5, READ STATUS REGISTER) 0x2404: opcode(READ_SDR), pad (one pad), operand (0x4 , byte number)   LUT entry 4, that is for make MT25Q enter DDR mode and quad pad: From MT25Q data sheet: It will use two instructions, that is 0x0461: opcode (CMD_SDR),  one pad (0), operand (0x61 WRITE ENHANCED VOLATILE CONFIGURATION REGISTER) 0x2001: opcode (WRITE_SDR 08), one pad(0), operand (1 byte data size) The 0x5f will be send out as data.   Next check LUT entry read , at this time MT25Q had enter QUAD pad and DDR mode: LUT entry 0, Read sequence, it is fast read data from MT25Q, from data sheet: will use four instructions , that is : 86ED, opcode (CMD_DDR ), pad ( four pad), operand (0xEDh fast read) 8a18, opcode (RADDR_DDR), pad (four pad), operand (0x18 , three byte address) B210, opcode(DUMMY_ADDR), pad (four pad), operand(0x10, dummy cycle) A604, opcode (READ_DDR), pad (four pad) , operand (0x4, data byte)   Reference: 1.i.MX8DXL Reference Manual 2.MT25Q data sheet              
查看全文
1.  Introduction 1.1.        Purpose This application note introduces a procedure of how to port AVB/TSN stack and run referring feature demos on i.MX8DXL board. This can help users who want to run AVB/TSN demos to quickly understand and customized their own codes. Since many of the standards are only for TSN switch/bridges and i.MX8DXL is design to be a TSN/AVB endpoint, the demos did not implement a full stack or full standards. They only demonstrated the basic end-to-end point (talker to listener) A/V streaming without bridge or switch. The software used for example in this documentation are based on the opensource such as gstreamer and alsa utils.   1.2.        Overview 1.2.1.     AVB/TSN AVB (Audio Video Bridging) is a common name for the set of technical standards which provide improved synchronization, low-latency, and reliability for switched ethernet network. AVB was initially developed by the IEEE Audio Video Bridging task group of the IEEE 802.1 standards committee. In November 2012, AVB group was renamed to TSN (Time-Sensitive Networking) task group to reflect the expanded scope of its work, which is to provide the specifications that will allow time-synchronized low latency streaming services through IEEE 802 networks. The referring standards shows as follows:     TSN protocol additions QoS components supported in HW TSN MAC + SW driver Managed Object components expose i/f to allow support of standardized network config protocols (local & remote) Transport API to allow other transport layer to use TSN QoS Stack extensions to map traffic priority to application task scheduling Real Time, gPTP based, Best Effort 1.2.2.     Demo introduction   The two streams are defined as below to grantee time sensitive (sub-microsecond synchronization), low latency and bandwidth on the ethernet: Stream A: SR class A, AVTP Audio Format, PCM 16-bit sample, 48 kHz, stereo, 12 frames per AVTPDU. Stream B: SR class B, AVTP Compressed Video Format, H.264 profile High, 1920x1080, 30 fps. The two TSN streams would be allocated into different TC (traffic control) class for egress. Different TC class would be mapped to different hardware queues with specific DMA channel which supported by ENET_OoS IP. The demos were built by follow blocks:   Linux Traffic Control: streams egress control Linux ptp: clock sync in network Libavtp: Time Sensitive Applications AV Transport protocol Gstreamer: avtp plugin uses the libavtp to transmit and receive AVTP audio/video (audio pcm, video h264).   1.2.3.     Traffic control Multiply queue qdiscs + CBS: The CBS class is actually handled by hardware IP to select which queue for transmitting.   CBS parameters come straight from the IEEE 802.1Q-2018 specification. They are the following: idleSlope: rate credits are accumulated when queue isn’t transmitting; sendSlope: rate credits are spent when queue is transmitting; hiCredit: maximum amount of credits the queue is allowed to have; loCredit: minimum amount of credits the queue is allowed to have;     2.  Build demo 2.1.        Build yocto $ DISTRO=fsl-imx-xwayland MACHINE=imx8dxlevk source imx-setup-release.sh -b ./xwayland $ bitbake imx-image-full Prepare a SD card and burn it with the built out images. 2.2.        Rebuild kernel Rebuild the kernel after applying the 0001-qenet-add-queue-avoid-panic.patch, and overwrite the Image and imx8dxl-evk.dtb on the boot partition of the SD card. 2.3.        Install the toolchain $ bitbake -f fsl-image-validation-imx -c populate_sdk $ sh tmp/deploy/sdk/fsl-imx-xwayland-glibc-x86_64-fsl-image-validation-imx-aarch64-imx8dxlevk-toolchain-5.4-zeus.sh The toolchain would be installed into /opt/fsl-imx-xwayland/5.4-zeus   2.4.        Create a install folder $ mkdir <your install folder> Create a folder to install all of the shared libraries, binaries and configure files which built out manually in this doc. After built done, you should copy all of the contents in this folder to target board root.   2.5.        Build libavtp $ source /opt/fsl-imx-xwayland/5.4-zeus/environment-setup-aarch64-poky-linux $ git clone https://github.com/Avnu/libavtp.git $ cd libavtp $ meson build --prefix=<your install folder>/usr $ ninja -C build Copy the built out .so and .pc into the toolchain rootfs: $ sudo cp build/libavtp.so* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/lib $ sudo cp build/meson-private/*.pc /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/lib/pkgconfig/ Copy the .so into the install folder: $ cp build/libavtp.so* <install folder>/usr/lib/ To make sure you have avtp package installed correctly:     $ pkg-config --list-all | grep avtp   2.6.        Build ALSA aaf plugin $ cd <yocto build>/tmp/work/aarch64-poky-linux/alsa-plugins/1.1.9-r0/alsa-plugins-1.1.9 $ ./configure --build=x86_64-linux --host=aarch64-poky-linux --target=aarch64-poky-linux --prefix=<install folder>/usr --disable-silent-rules --disable-dependency-tracking --with-libtool-sysroot=<yocto build>/xwayland/tmp/work/aarch64-poky-linux/alsa-plugins/1.1.9-r0/recipe-sysroot --disable-static --enable-aaf --disable-jack --disable-libav --disable-maemo-plugin --disable-maemo-resource-manager --enable-pulseaudio --enable-samplerate --with-speex=lib $ make $ make install   2.7.        Build Gstreamer AVTP plugins (1.17.x) 2.7.1.     Build Gstreamer core $ git clone https://gitlab.freedesktop.org/gstreamer/gstreamer.git $ patch -p1 < gstreamer-1.0-pass-build.patch $ meson build --prefix=<install folder>/usr $ ninja -C build $ sudo ninja -C build install After Gstreamer is installed into <your install folder>, please fix the “prefix” path in the .pc files by, and copy to the toolchain folders: $ cd <your install folder> $ grep -lR <your install folder> ./lib/pkgconfig/ | xargs sed -i 's/<your install folder>/\/usr/g' $ cp -rf ./usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/ 2.7.2.     Build gst-plugins-base $ git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-base.git $ cd gst-plugins-base $ patch -p1 < gst-plugins-base-pass-build.patch $ meson build --prefix=<your install folder>/usr $ ninja -C build $ sudo ninja -C build install   2.7.3.     Build gst-plugins-bad $ git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-bad.git $ cd gst-plugins-bad $ meson build --prefix=<your install folder>/usr $ ninja -C build $ sudo ninja -C build install   After gst-plugins-base and gst-plugins-bad installed into <your install folder>, please fix the “prefix” path in the .pc files and copy them into the toolchain folders: $ cd <your install folder> $ grep -lR <your install folder> ./lib/pkgconfig/ | xargs sed -i 's/<your install folder>/\/usr/g' $ cp -rf ./usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/   2.8.        Build H.264 SW plugins 2.8.1.     Build x264 As the yocto actually has the x264 recipes, but not included in our bblayers, we need to copy the x264 source into our bblayers path under <yocto>/source to build: $ cp -rf ./poky/meta/recipes-multimedia/x264 ./meta-openembedded/meta-multimedia/recipes-multimedia/ $ vi ./meta-openembedded/meta-multimedia/recipes-multimedia/x264_git.bb Remove the LICENSE_FLAGS line $ bitbake -f x264 -c do_install $ sudo cp -rf tmp/work/aarch64-poky-linux/x264/r2917+gitAUTOINC+72db437770-r0/image/usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/ 2.8.2.     Build gst-plugins-ugly $ git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-ugly.git $ cd gst-plugins-ugly $ meson build --prefix=<your install folder>/usr $ ninja -C build $ sudo ninja -C build install   2.8.3.     Build libav $ cp -rf poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-libav meta-openembedded/meta-multimedia/recipes-multimedia/gstreamer-1.0/ Remove the LICENSE_FLAGS line $ vim ./poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-libav_1.16.2.bb $ bitbake -f gstreamer1.0-libav -c do_install $ cp /opt/samba/nxf39444/imx-yocto-bsp-i.mx8dxl/xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0-libav/1.16.2-r0/image/usr/lib/gstreamer-1.0/libgstlibav.so <your install folder>/usr/lib/gstreamer-1.0   2.8.4.     Install binaries Final step is to copy all of your built out files from <your install folder> into your board / root, and boot up the board. $ export GST_PLUGIN_PATH=/usr/lib/gstreamer-1.0/ $ gst-inspect-1.0 To check if the above Gstreamer plugins we built out can be found by gst-instpect.   3.  System Setup 3.1.        VLAN The ENTE_QoS is assigned to eth0 instance. So create eth0.5 for vlan id 5: $ ip link add link eth0 name eth0.5 type vlan id 5 egress-qos-map 2:2 3:3 $ ip link set eth0.5 up   3.2.        Qdiscs The TSN control plane is implemented through the TC (Traffic Control) system. The transmission algorithms specified in the FQTSS (Forwarding and Queuing for Time-Sensitive Streams) chapter of IEEE 802.1Q-2018 are supported via TC Qdiscs (Queuing Discipline). 3.2.1.     MQPRIO qdisc $ tc qdisc add dev eth0 parent root handle 100 mqprio num_tc 3 map 0 0 2 1 0 0 0 0 0 0 0 0 0 0 0 0 queues 1@0 1@1 1@2 hw 1 3.2.2.     CBS qdisc Q1 CBS for audio, Q2 CBS for video: $ tc qdisc replace dev eth0 parent 100:3 handle 888 cbs idleslope 3648 sendslope -996352 hicredit 12 locredit -113 offload 1 $ tc qdisc replace dev eth0 parent 100:2 handle 777 cbs idleslope 98688 sendslope -901312 hicredit 153 locredit -1389 offload 1 3.2.3.     TimeSync Run the ptp4l and phc2sys in background, and use check_clocks to check the ptp sync works. $ ptp4l -i eth0 -f ./gPTP.cfg --step_threshold=1 & $ pmc -u -b 0 -t 1 "SET GRANDMASTER_SETTINGS_NP clockClass 248 clockAccuracy 0xfe offsetScaledLogVariance 0xffff currentUtcOffset 37 leap61 0 leap59 0 currentUtcOffsetValid 1 ptpTimescale 1 timeTraceable 1 frequencyTraceable 0 timeSource 0xa0" $ ./check_clocks -d eth0 4.  Run demo 4.1.        ALSA AAF audio To run the alsa AAF demo, please add aaf0 and converter0 plugin device into /etc/asound.conf: pcm.aaf0 {    type aaf    ifname eth0.5    addr 01:AA:AA:AA:AA:AA    prio 2    streamid AA:BB:CC:DD:EE:FF:000B    mtt 50000    time_uncertainty 1000    frames_per_pdu 12    ptime_tolerance 100 } pcm.converter0 {    type linear    slave {                  pcm "hw:0,0"                  format S16_LE    } } The “aaf0” plugin device defines the ethernet interface which AAF runs on, the socket priority which mapping to Traffic Class in kernel TC, the stream-id for the aaf streaming. The “converter0” plugin device is used for convert the S16_BE format to S16_LE for the wm8960 PCM audio.   Select one device as AVB talker, and run: $ speaker-test -p 25000 -F S16_BE -c 2 -r 48000 -D aaf0   Select one device as AVB listener, and run: $ arecord -F 25000 -t raw -f S16_BE -c 2 -r 48000 -D aaf0 | aplay -F 25000 -t raw -f S16_BE -c 2 -r 48000 -D converter0   You can hear the sound on the listener device.   You can also check which qdisc queue is used for AAF by: $ tc -s qdisc   4.2.        Gstreamer AAF audio Select one device as AVB talker, and run: $ gst-launch-1.0 clockselect. \( clock-id=realtime audiotestsrc samplesperbuffer=12 is-live=true ! audio/x-raw,format=S16BE,channels=2,rate=48000 ! avtpaafpay mtt=50000000 tu=1000000 streamid=0xAABBCCDDEEFF000B processing-deadline=0 ! avtpsink ifname=eth0.5 address=06:98:c0:22:df:35 priority=3 processing-deadline=0 \)   Select one device as AVB listener, and run: $ gst-launch-1.0 clockselect. \( clock-id=realtime avtpsrc ifname=eth0.5 ! avtpaafdepay streamid=0xAABBCCDDEEFF000B ! queue max-size-bytes=0 max-size-buffers=0 max-size-time=0 ! audioconvert ! audioresample !  alsasink device="hw:0,0" \)   5.  Packet sniffer Use tcpdump on board to dump the L2 ethernet packet: $ tcpdump -i eth0 ether proto 0x22f0 -w dump.pcap The AVTP ether protocol code is 0x22f0 embedded inside the ether frame, or you can use "vlan 5" VLAN id for tcpdump parameters to dump. Then open this dump.pcap in the windows/Linux PC by the wireshark tool, it will automatically show the protocol inside the package, it can also parser the IEEE1722 (AVTP) CVF/AFF package header as below:   To measure the package latency from transmit port (talker) to receive port (listener), you can use the tcpdump on both end-points. And compare the Epoch Time the packet dumped: "Epoch Time: 1596252905.688243000 seconds". The delta of the epoch time of the same packet is around 100us~500us. This latency actually includes the AF_PACKET clone cost in kernel netfilter, also the tcpdump application schedule latency.   6.  Revision history summarizes the changes done to this document since the initial release. Table2. Revision history Revision number Date Substantive changes 1 5/2021 Initial release    
查看全文
This doc share one OpenGL ES sample code, it is running on i.MX8 MEK board with QNX SDP7.1. HW: i.MX8 MEK board, HDMI display SW: QNX SDP7.1, i.MX8 MEK board BSP, and this sample code   This sample code will draw 3D object model, and with some animation. Reference: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-8-processors/i-mx-8-family-arm-cortex-a53-cortex-a72-virtualization-vision-3d-graphics-4k-video:i.MX8 https://github.com/NXPmicro/gtec-demo-framework https://github.com/syoyo/tinyobjloader-c https://github.com/nothings/stb https://3dhaupt.com/futuristic-car-game-ready-download/ https://wallpapersafari.com/w/Y5JZNh https://www.pngwing.com/en/free-png-ysaus https://www.shadertoy.com/view/Ms2SWW#
查看全文
   
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. i.MX 6/7 Series Family DDR Tools Overview This page contains the latest releases for the i.MX 6/7 series DDR Tools. The tools described on this page cover the following i.MX 6/7 series SoCs: i.MX 6DQP (Dual/Quad Plus) i.MX 6DQ (Dual/Quad) i.MX 6DL/S (Dual Lite/Solo) i.MX 6SoloX i.MX 6SL i.MX 6SLL i.MX 6UL i.MX 6ULL/ULZ i.MX 7D/S i.MX 7ULP The purpose of the i.MX 6/7 series DDR Tools is to enable users to generate and test a custom DRAM initialization based on their device configuration (density, number of chip selects, etc.) and board layout (data bus bit swizzling, etc.). This process equips the user to then proceed with the bring-up of a boot loader and an OS. Once the OS is brought up, it is recommended to run an OS-based memory test (like Linux memtester) to further verify and test the DDR memory interface. The i.MX 6/7 series DDR Tools consist of: DDR Register Programming Aid (RPA) DDR Stress test _________________________________________________________ i.MX 6/7 Series DDR Stress Test The i.MX 6/7 Series DDR stress test tool is a Windows-based software tool that is used as a mechanism to verify that the DDR initialization is operational prior for use in u-boot and OS bring-up. The DDR Stress Test tool can be found here: i.MX 6/7 DDR Stress Test Tool Note that the DDR Stress test tool supports all of the above i.MX SoCs, however, some of the supported i.MX SoCs named in the tool support multiple i.MX SoCs as follows: MX6DQ – when selected, this supports both i.MX 6DQ and i.MX 6DQP (Plus) MX6DL – when selected, this supports both i.MX 6DL and i.MX 6S (i.MX 6DLS family) MX6ULL – when selected, this supports both i.MX 6ULL and i.MX6 ULZ MX7D – when selected, this supports both i.MX 7D and i.MX 7S _____________________________________________________________________________ i.MX 6/7 Series DDR Register Programming Aid (RPA) The i.MX 6/7 series DDR RPA (or simply RPA) is an Excel spreadsheet tool used to develop DDR initialization for a user’s specific DDR configuration (DDR device type, density, etc.). The RPA generates the DDR initialization script for use with the DDR Stress Test tool. For a history of the previous versions of an RPA, refer to the Revision History tab of the respective RPA. To obtain the latest RPAs, please refer to the following links: i.MX 6DQP i.MX6DQP Register Programming Aids i.MX 6DQ i.MX6DQ Register Programming Aids i.MX 6DL/S i.MX6DL Register Programming Aids i.MX 6SoloX i.MX6SX Register Programming Aids i.MX 6SL i.MX6SL Register Programming Aids  i.MX6SLL i.MX6SLL Register Programming Aids i.MX 6UL/ULL/ULZ i.MX6UL/ULL/ULZ DRAM Register Programming Aids i.MX7D i.MX7D DRAM Register Programming Aids i.MX 7ULP i.MX7ULP DRAM Register Programming Aids _____________________________________________________________________________ DRAM Register Programming Aids FAQ    
查看全文
  Question: How can we generate an ARM DS5 DStream format DDR initialization script using the DRAM Register Programming Aid?  Answer: Some RPAs include a  "DStream .ds file" tab for the ARM DS5 debugger specific commands. The i.MX6UL/ULL/ULZ DRAM Register Programming Aids for example already has this supported. However, the user can easily create  the .ds format from the existing .inc format. The basic steps to convert .inc files to .ds format are as follows: 1)  Replace the one instance of setmem /16 with mem set 2)  In that same line, replace 0x020bc000 = with 0x020bc000 16 3)  Use a Replace All command to change setmem /32 with mem set 4)  Use a Replace All command to change = with 32 5)  Use a Replace All command to change // with # 6)  Save as a .ds file.   Question: When using a 528MHz DRAM Controller interface with a DDR memory of a faster speed bin, which speed bin timing options should one use? Answer: For example, let’s assume our MX6DQ design is using a DDR3 memory from a DDR3-1600 speed bin.  However, the maximum speed of the MMDC interface for the MX6DQ using DDR3 is 528MHz.  Should we use the 1600 speed bin (800MHz clock speed) or the 1066 speed bin (533MHz clock speed)?  In short, the user should use the timings rated for the maximum speed (frequency) with which you are running, in this case DDR3-1066 (533MHz).  In some cases, like when using the MX6DL, the maximum DDR frequency is 400MHz.  In this case, you would want to try and use 800 timings found in the AC timing parameters table.  However, most DDR3 devices have speed bin tables that may go only as low as 1066, in which case you would use the closest speed bin to your operational frequency (i.e. the 1066 speed bin table).     Question: Some timing parameters may specify a min and max number, which should I use? Answer: In most cases, you will want to choose the minimum timings.  Some DRAM controllers may have a tRAS_MAX timing parameter, in which case you would obviously use the maximum tRAS parameter given in the DRAM data sheet. Also, for timing parameters tAONPD and tAOFPD, we also want to use the maximum values given in the DDR3 data sheet. These represent the maximum amount of time the DDR3 device takes to turn on or off the RTT (termination), therefore, we should wait at least this amount of time before issuing any commands or accesses.   Question: Some timing parameters state things like “Greater of 3CK or 7.5ns”; which should I use? Answer: This depends on your clock speed.  Say you are running at 533MHz.  At 533MHz, 7.5ns equates to 4CKs.  In this case, 7.5ns at 533MHz is GREATER than 3CK, so we would use the 7.5ns number, or 4CKs. At 400MHz, 7.5ns equates to 3CKs.  In this case, we’d simply use 3CKs.   Question: I have a design that will throttle the DDR frequency (dynamic frequency scaling).  At full speed, I plan to run at 533MHz, and then I plan to throttle down to say 400MHz whenever possible.  Do I need to re-calculate my 400 MHz timing parameters that were initially set for 533MHz? Answer: It is not necessary to re-calculate timing parameters for 400MHz, and you can re-use the ones for 533MHz.  The timings at 533 MHz are much tighter than 400 MHz, and the key here is to NOT violate timings.  Also, it may be a bit of a hassle maintaining two sets of timing parameters, especially if later in the design, you swap DDR vendors that might require you to re-calculate some timing parameters.  It’s easier to do it once and to come up with a combined worse-case timing parameters for 533MHz, which you know will work at 400MHz.  But, if you don’t mind maintaining two sets of timing parameters, and really want to optimize timings down to the last pico-second for 400MHz, then knock yourself out.   Question: Can I use these Register programming aids for both Fly by and T- Topology ? Answer Yes The DDR register programming aid is agnostic to the DDR layout. The same spreadsheet works for both topologies. We recommend running write leveling calibration for both topologies and the values returned by the Write Leveling routine from the Freescale DDR stress test should be incorporated back to the customer specific initialization script. The DDR stress test also has a feature whereby it evaluates the write leveling values returned from calibration and increments WALAT to 1 if the values exceed a defined limit. The DDR stress test informs the user when the Write Additional latency (WALAT) exceeds the limit and should be increased by 1, and reminds the user to add it back in the customer specific initialization script if required.   WALAT - 0 00000000 WALAT: Write Additional latency. Recommend to clear these bits. Proper board design should ensure that the DDR3 devices are placed close enough to the MMDC to ensure the skew between CLK and DQS is less than 1 cycle.     Question: Can I use the DEFAULT Register programming aid values for MDOR when using an Internal OSC instead of the recommended 32.768 KHZ XTAL ? Answer No, NXP recommends reprogramming these values based on the worse case frequency (Max clock) of the internal OSC of the device to guarantee JEDEC timings are met. Please refer to Internal Oscillator Accuracy considerations for the i.MX 6 Series for more details  
查看全文
Overview AVB/TSN Wikipedia: Audio Video Bridging (AVB) is a common name for the set of technical standards which provide improved synchronization, low-latency, and reliability for switched Ethernet networks. AVB was initially developed by the Institute of Electrical and Electronics Engineers (IEEE) Audio Video Bridging task group of the IEEE 802.1 standards committee. In November 2012, Audio Video Bridging task group was renamed to Time-Sensitive Networking (TSN) task group to reflect the expanded scope of its work, which is to "provide the specifications that will allow time-synchronized low latency streaming services through IEEE 802 networks". Further standardization efforts are ongoing in IEEE 802.1 TSN task group.   AVB and TSN technologies and standards: Standard Area of Definition Title of Standard AVB/TSN IEEE 802.1AS Timing and synchronization Timing and Synchronization for Time-Sensitive Applications (gPTP) AVB TSN IEEE 802.1Qav Forwarding and queuing Forwarding and Queuing for Time-Sensitive Streams (FQTSS) AVB IEEE 802.1Qat Path control and reservation Stream Reservation Protocol (SRP) AVB IEEE 802.1BA Bridging Audio Video Bridging (AVB) Systems AVB IEEE 1722 AVTP AV transport Layer 2 Transport Protocol for Time Sensitive Applications AVB IEEE 1722 AVDECC Device manage and control Device Discovery, Enumeration, Connection Management and Control Protocol AVB IEEE 802.1Qbu and IEEE 802.3br Forwarding and queuing Frame preemption TSN IEEE 802.1Qbv Forwarding and queuing Enhancements for scheduled traffic TSN IEEE 802.1Qca Path control and reservation Path control and reservation TSN IEEE 802.1Qcc Central configuration method Enhancements and performance improvements TSN IEEE 802.1Qci Time-based ingress policing Per-stream filtering and policing TSN IEEE 802.1CB Seamless redundancy Frame replication and elimination for reliability TSN   Since many of the standards are only for TSN switch/bridges and i.MX8MP is design to be a TSN/AVB endpoint, this demo does not implement a full stack or full standards. It only demonstrates the basic end-to-end point (talker to listener) A/V streaming without bridge or switch.   Below table shows what this demo supports: Standard Software Hardware IEEE 802.1AS Linuxptp ENET_QoS IP IEEE 802.1Qav/Qbu/Qbv TC qdisc (taprio, mqprio, etf, cbs) ENET_QoS IP (multi queue + EST, FPE, CBS) IEEE 1722 AVTP Libavtp N/A   Demo introduction Two i.MX8MP EVK boards are used for this demo, one act as a AVB talker to send A/V streams, the other one act as a AVB listener to receive A/V streams who can be playback to audio codec and sink video to screen. The two boards are connected by a RJ45 ethernet cable on each ENET2 port (only ENET2 port has TSN features). Three streams’ type and SR (Stream Reservation) class are defined as below to grantee time sensitive (sub-microsecond synchronization), low latency and bandwidth on the ethernet: Stream A: SR class A, AVTP Compressed Video Format, H.264 profile High, 1920x1080, 30 fps. Stream B: SR class B, AVTP Audio Format, PCM 16-bit sample, 48 kHz, stereo, 12 frames per AVTPDU. Other stream: Best-effort streams These three TSN streams would be allocated into different traffic control (TC) class for egress in Linux. Different TC class would be mapped to different hardware queues with dedicated DMA channel, thanks to the multi-queue support by ENET_QoS IP. Then the traffic control apply different scheduling policy on each queues for different types of streams egress, to make sure highest priority or critical packet can be sent in the correct time slot. The TSN streams are transmitted over Virtual LANs (VLANs). Bridges use the VLAN priority information (PCP) to identify Stream Reservation (SR) traffic classes which are handled according to the Forward and Queuing Enhancements for Time-Sensitive Streams (FQTSS) mechanisms described in Chapter 34 of the IEEE 802.1Q standard.   The demo is built up by following blocks: Linux TC (traffic control): streams egress control to meet AVB/TSN requirements, which take advantage of the i.MX8MP TSN ENET IP. Linux PTP: clock sync in network, which take advantage of the i.MX8MP TSN ENET IP. Libavtp: Time Sensitive Applications AV Transport protocol. ALSA: AVTP audio format plugin uses the libavtp to transmit and receive AVTP audio PCM streams. Gstreamer: avtp plugin uses the libavtp to transmit and receive AVTP audio/video streams (video should be encoded as H264, audio PCM). x264enc and libav is a software H.264 video encoder/decoder, which alternative to the on chip VPU acceleration plugin, due to the VPU plugin is not supported in the latest Gstreamer version (1.17.x).     Traffic control This demo can use two different traffic control qdisc settings: mqprio + cbs: use CBS features taprio + pfifo: use EST and FPE features (802.1Qbu/bv). The pfifo is the default traffic control class, which use FIFO schedule policy for egress packets. The CBS class is actually handled by hardware IP to select which queue for transmit in a certain time slot.   Credit Base Shaper (CBS) CBS parameters come straight from the IEEE 802.1Q-2018 specification. They are the following: idleSlope: rate credits are accumulated when queue isn’t transmitting; sendSlope: rate credits are spent when queue is transmitting; hiCredit: maximum amount of credits the queue is allowed to have; loCredit: minimum amount of credits the queue is allowed to have;     Enhancements to Scheduled Traffic (EST) The IEEE 802.1Qbv defines the schedule for each of the queues on every egress port which makes the implementation aware of traffic arrival schedule. This information can be used to block the lower priority traffic from transmission in this time window/slot. This ensures that scheduled traffic is forwarded from sender to receiver through all the network nodes with a deterministic delay. The i.MX8MP uses the gate control list with configurable time slot and frame preempt (IEEE 802.1Qbu) features to support EST. Other than the CBS, the gate control list control the egress transmission by a fixed open interval for that queue.   Build demo Build L5.4.24_2.1.0 $MACHINE=imx8mpevk DISTRO=fsl-imx-xwayland source imx-setup-release.sh -b build-8mp $bitbake  fsl-image-validation-imx Prepare a SD card and burn it with the built out images. To add tc/tcpdump command in iproute2 package, please add package into IMAGE_INSTALL_append variable into conf/local.conf: IMAGE_INSTALL_append = " iproute2 iproute2-tc tcpdump Rebuild kernel Rebuild the kernel after applying the 0001-qenet-add-queue-avoid-panic.patch (attached), and overwrite the Image and imx8mp-evk.dtb on the boot partition of the SD card.   Install the toolchain $bitbake -f fsl-image-validation-imx -c populate_sdk $sh tmp/deploy/sdk/fsl-imx-xwayland-glibc-x86_64-fsl-image-validation-imx-aarch64-imx8mpevk-toolchain-5.4-zeus.sh The toolchain would be installed into /opt/fsl-imx-xwayland/5.4-zeus/   Create a install folder $mkdir <your install folder> Create a folder to install all of the shared libraries, binaries and configure files which built out manually in this doc. After built done, you should copy all of the contents in this folder to target board root.   Build libavtp $source /opt/fsl-imx-xwayland/5.4-zeus/environment-setup-aarch64-poky-linux $git clone https://github.com/Avnu/libavtp.git $cd libavtp $meson build $ninja -C build Copy the built out .so and .pc into the toolchain rootfs: $sudo cp build/libavtp.so* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/lib/ $sudo cp build/meson-private/*.pc /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/lib/pkgconfig/ To make sure you have avtp package installed correctly: $pkg-config --list-all | grep avtp Copy the .so into the install folder: $cp build/libavtp.so* <install folder>/usr/lib/ Copy header files: $cp libavtp/include/* files <toolchain_path>/sysroots/aarch64-poky-linux/usr/lib Build ALSA aaf plugin The AAF (ALSA AVTP Audio Format) plugin is a PCM plugin that uses Audio Video Transport Protocol (AVTP) to transmit/receive audio samples through a Time-Sensitive Network (TSN) capable network. The plugin enables media applications to easily implement AVTP Talker and Listener functionalities.   $cd <yocto build>/tmp/work/aarch64-mx8mp-poky-linux/alsa-plugins/1.1.9-r0/alsa-plugins-1.1.9 $./configure --build=x86_64-linux --host=aarch64-poky-linux --target=aarch64-poky-linux --prefix=<your install folder>/usr --disable-silent-rules --disable-dependency-tracking --with-libtool-sysroot=/opt/samba/nxa23059/jailhouse/yocto-5.x/build-8mp/tmp/work/aarch64-mx8mp-poky-linux/alsa-plugins/1.1.9-r0/recipe-sysroot  --disable-static  --enable-aaf --disable-jack --disable-libav --disable-maemo-plugin --disable-maemo-resource-manager --enable-pulseaudio --enable-samplerate --with-speex=lib $make $make install   Build Gstreamer AVTP plugins Build Gstreamer 1.17.x (commit e4f7cdb0df7b) $git clone https://gitlab.freedesktop.org/gstreamer/gstreamer.git $cd gstreamer $patch -p1 < gstreamer-1.0-pass-build.patch $meson build --prefix=<your install folder>/usr $ninja -C build $ninja -C build install After Gstreamer is installed into <your install folder>, please fix the “prefix” path in the .pc files by, and copy to the toolchain folders: $cd <your install folder> $grep -lR <your install folder> ./lib/pkgconfig/ | xargs sed -i 's/<your install folder>/\/usr/g' NOTE: Make sure you use the ‘\’ for ‘/’ convert in your path. $cp -rf ./usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/   Build gst-plugins-base (commit 22827e8f) $git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-base.git $cd gst-plugins-base $patch -p1 < gst-plugins-base-pass-build.patch $meson build --prefix=<your install folder>/usr $ninja -C build $ninja -C build install   Build gst-plugins-bad (commit ed14e0d5a) $git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-bad.git $cd gst-plugins-bad $meson build --prefix=<your install folder>/usr $ninja -C build $ninja -C build install If you met gdbus-codegen issue, please remove the “--c-generate-autocleanup” and “--output-directory” parameters in the build/build.ninja If you met issue of include file like: “…/gst/gl/gstglapi.h:24:10: fatal error: gst/gl/gstglconfig.h: No such file or directory.” Please modify the build/build.ninja to correct the -I header file parameter of the build. After gst-plugins-base and gst-plugins-bad installed into <your install folder>, please fix the “prefix” path in the .pc files and copy them into the toolchain folders: $cd <your install folder> $grep -lR <your install folder> ./lib/pkgconfig/ | xargs sed -i 's/<your install folder>/\/usr/g' NOTE: Make sure you use the ‘\’ for ‘/’ convert in your path. $cp -rf ./usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/   Build H.264 SW plugins AVTPDU uses H.264 as payload for streaming, this requires H.264 encoder/decoder plugins, either software or hardware accelerations. Since we upgrade the Gstreamer and its plugins to a new version, the VPU plugins cannot be used anymore. So software H.264 plugins are required: x264 for encoder, libav for decoder.   Build x264 As the yocto actually has the x264 recipes, but not included in our bblayers, we need to copy the x264 source into our bblayers path under <yocto>/source to build: $cp -rf ./poky/meta/recipes-multimedia/x264 ./meta-openembedded/meta-multimedia/recipes-multimedia/ $vi ./meta-openembedded/meta-multimedia/recipes-multimedia/x264_git.bb Remove the LICENSE_FLAGS line $bitbake -f x264 -c do_install $sudo cp -rf tmp/work/aarch64-poky-linux/x264/r2917+gitAUTOINC+72db437770-r0/image/usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/ Build gst-plugins-ugly (commit 995a135d) $git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-ugly.git $cd gst-plugins-ugly$meson build --prefix=<your install folder>/usr $ninja -C build $ninja -C build install If you met build issue, please remove "if have_cxx" from meson.build Build libav As the yocto actually has the libav recipes, but not included in our bblayers, we need to copy the its source into our bblayers path under <yocto>/source: $cp -rf ./poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-libav ./meta-openembedded/meta-multimedia/recipes-multimedia/gstreamer $vi ./meta-openembedded/meta-multimedia/recipes-multimedia/gstreamer/gstreamer1.0-libav_1.16.1.bb Remove the LICENSE_FLAGS line $bitbake -f gstreamer1.0-libav -c do_install $cp tmp/work/aarch64-mx8mp-poky-linux/gstreamer1.0-libav/1.14.0-r0/image/usr/lib/gstreamer-1.0/libgstlibav.so <your install folder>/usr/lib/gstreamer-1.0 Now you have all of the Gstreamer plugins which required for AVB/TSN audio/video demo: avtpsrc, avtpsink, avtpaafpay, avtpaafdepay, avtpcvfpay, avtpcvfdepay x264_enc (encoder), avdec_h264 (decoder)   Install binaries Final step is to copy all of your built out files from <your install folder> into your board / root, and boot up the board. Verify the Gstreamer plugins install correctly or not: $export GST_PLUGIN_PATH= /usr/lib/gstreamer-1.0/ $gst-inspect-1.0 Check if the above Gstreamer plugins we built out can be found by gst-instpect.   System Setup VLAN The ENTE_QoS is assigned to eth1 instance. So create eth1.5 for vlan id 5: $ip link add link eth1 name eth1.5 type vlan id 5 \         egress-qos-map 2:2 3:3 $ip link set eth1.5 up Qdiscs The TSN control plane is implemented through the Linux Traffic Control (TC) System. The transmission algorithms specified in the Forwarding and Queuing for Time-Sensitive Streams (FQTSS) chapter of IEEE 802.1Q-2018 are supported via TC Queuing Disciplines (qdiscs). Linux currently provides the following qdiscs relating to TSN: Multiply queue qdiscs (These two qdiscs are mutually exclusive, select one for your demo): MQPRIO: Mapping the TC class into different hardware queue in IP. TAPRIO: Implements the Enhancements for Scheduled Traffic introduced by IEEE 1Qbv/Qbu. This is supported by i.MX8MP ENET_QoS IP through EST features: Qbv – Time aware shaper Qbu - frame preemption. CBS qdisc: Implements the Credit-Based Shaper introduced by the IEEE 802.1Qav This is supported by i.MX8MP ENET_QoS IP through EST (Enhancements to Scheduled Traffic) features. It works with mqprio qdisc together. ETF qdisc: While not an FQTSS feature, Linux also provides the Earliest TxTime First (ETF) qdisc which enables the LaunchTime Since the i.MX8MP ENET_QoS IP does not support LaunchTime feature, this qdisc configurations would be ignored.   MQPRIO qdisc $tc qdisc add dev eth1 parent root handle 100 mqprio \         num_tc 3 \         map 0 0 2 1 0 0 0 0 0 0 0 0 0 0 0 0 \         queues 1@0 1@1 1@2 \         hw 1 NOTE, since ENET_QoS Q0 does not support hardware CBS, we have to avoid using Q0 for AVB streaming. Here’s the mapping: socket SO_PRIORITY 2 -> TC CLASS 2 -> Q2 socket SO_PRIORITY 3 -> TC CLASS 1 -> Q1 Other socket priority -> TC CLASS 0 -> Q0   TAPRIO qdisc Create a root qdisc handle to map the different CLASS streams to hardware queues w/ GCL (gate control list). This root handle maps the CLASS A stream to queue Q1, CLASS B stream to Q2, and others to Q0 by the “map” and “queues” parameters, same as mqprio above. The Q1/Q2(CLASS1/2) gates are open in the first 300us interval, then only Q1(CLASS1) gate is open in the next 300us with all other CLASS gated. The last sched-entry defines in after Q1 is open after 300us, all of the CLASS gates are open for next 200us. Then loopback to the first sched-entry for gate control. Please note in this demo, we only enable features to support the 802.1Qbv, the Qbu (Frame preempt) requires patches for iproute2. $tc qdisc add dev eth1 parent root handle 100 taprio \         num_tc 3 \         map 0 0 2 1 0 0 0 0 0 0 0 0 0 0 0 0 \         queues 1@0 1@1 1@2 \         base-time 1000000000 \         sched-entry S 0x6 300000 \         sched-entry S 0x2 300000 \         sched-entry S 0x7 200000 \         flags 0x2   CBS qdisc Q1 CBS for video, Q2 CBS for audio: $tc qdisc replace dev eth1 parent 100:2 handle 777 cbs \         idleslope 98688 sendslope -901312 hicredit 153 locredit -1389 \         offload 1 $tc qdisc replace dev eth1 parent 100:3 handle 888 cbs \         idleslope 3648 sendslope -996352 hicredit 12 locredit -113 \        offload 1 NOTE: By default, the Q0 will be allocated for pfifo qdisc class if we do not define them.   ETF qdisc As ENET_QOS does not support hardware launch time in IP, the ETF qdisc would not be used here.   TimeSync Run the ptp4l and phc2sys in background, and use check_clocks to check the ptp sync works. $ptp4l -i eth1 -f ./gPTP.cfg --step_threshold=1 & $pmc -u -b 0 -t 1 "SET GRANDMASTER_SETTINGS_NP clockClass 248 \         clockAccuracy 0xfe offsetScaledLogVariance 0xffff \         currentUtcOffset 37 leap61 0 leap59 0 currentUtcOffsetValid 1 \         ptpTimescale 1 timeTraceable 1 frequencyTraceable 0 \         timeSource 0xa0" $phc2sys -s eth1 -c CLOCK_REALTIME --step_threshold=1 \         --transportSpecific=1 -w &  $./check_clocks -d eth1 The PTP Hardware Clock (PHC)  synced between PTP master/slave means the RMS offset between PHC and GM (master clock) is < 100ns. PHC and system clock (CLOCK_REALTIME) synced means the clock offset < 100ns   NOTE: The check_clocks source code can be downloaded from here. cfg is described below, if you want to identify which is master and which is slave, use “masterOnly 1” or “slaveOnly 1” in this configuration file. #                                                                 # 802.1AS example configuration containing those attributes which # differ from the defaults.  See the file, default.cfg, for the   # complete list of available options.                              #                                                                 [global]                                                          gmCapable               1                                         priority1               248                                        priority2               248                                       logAnnounceInterval     0                                         logSyncInterval         -3                                        syncReceiptTimeout      3                                          neighborPropDelayThresh 800                                       min_neighbor_prop_delay -20000000                                 assume_two_step         1                                         path_trace_enabled      1                                         follow_up_info          1                                         transportSpecific       0x1                                        ptp_dst_mac             01:80:C2:00:00:0E                         network_transport       L2                                        delay_mechanism         P2P                                        Run demo ALSA AAF audio To run the alsa AAF demo, please add aaf0 and converter0 plugin device into /etc/asound.conf: pcm.aaf0 {         type aaf         ifname eth1.5         addr 01:AA:AA:AA:AA:AA         prio 2         streamid AA:BB:CC:DD:EE:FF:000B         mtt 50000         time_uncertainty 1000         frames_per_pdu 12         ptime_tolerance 100 }    pcm.converter0 {         type linear         slave {                 pcm "hw:2,0"                 format S16_LE         } }   The “aaf0” plugin device defines the ethernet interface which AAF runs on, the socket priority which mapping to Traffic Class in kernel TC, the stream-id for the aaf streaming. The “converter0” plugin device is used for convert the S16_BE format to S16_LE for the wm8960 PCM audio.   Select one device as AVB talker, and run: $speaker-test -p 25000 -F S16_BE -c 2 -r 48000 -D aaf0 Select one device as AVB talker, and run: $arecord -F 25000 -t raw -f S16_BE -c 2 -r 48000 -D aaf0 | aplay -F 25000 -t raw -f S16_BE -c 2 -r 48000 -D converter0 You can hear the sound on the listener device. You can also check which qdisc queue is used for AAF by: $tc -s qdisc   Gstreamer AAF audio Select one device as AVB talker, and run: $gst-launch-1.0 clockselect. \( clock-id=realtime \     audiotestsrc samplesperbuffer=12 is-live=true ! \     audio/x-raw,format=S16BE,channels=2,rate=48000 ! \     avtpaafpay mtt=50000000 tu=1000000 streamid=0xAABBCCDDEEFF000B processing-deadline=0 ! \     avtpsink ifname=eth1.5 address=01:AA:AA:AA:AA:AA priority=2 processing-deadline=0 \)   Select one device as AVB listener, and run: $gst-launch-1.0 clockselect. \( clock-id=realtime \     avtpsrc ifname=eth1.5 ! avtpaafdepay streamid=0xAABBCCDDEEFF000B ! \     queue max-size-bytes=0 max-size-buffers=0 max-size-time=0 ! \     audioconvert ! audioresample !  alsasink device="hw:2,0" \)   Gstreamer CVF video Select one device as AVB talker, and run: $gst-launch-1.0 clockselect. \( clock-id=realtime \     videotestsrc is-live=true ! video/x-raw,width=480,height=320,framerate=15/1 ! \     clockoverlay ! x264enc bframes=0  key-int-max=1 speed-preset=1 tune=4 ! h264parse config-interval=-1 ! \     avtpcvfpay processing-deadline=20000000 mtu=1400 mtt=2000000 tu=125000 streamid=0xAABBCCDDEEFF000A ! \     avtpsink ifname=eth1.5 priority=3 processing-deadline=20000000 \) NOTE: To eliminate the h.264 software encoding/decoding overhead with acceptable latency for this demo, we use several parameters for x264enc element: bframes: x264enc and avdec_h264 together was found to have issues, remove bframes in the stream would help. key-int-max: decoder can only decode the frame when a keyframe is present on stream to make sure decoder can work as faster as it can, the distance between two keyframes must be set to closest. speed-preset: to low down the CPU loading for encoding, we use the option to make encoding as faster as we can. (=1 means ultrafast) tune: 4 means zero latency ‘mtu=1400’ parameters for avtpcvfpay element is very important, if using the default mtu=1500, the listener cannot get the AVTPDUs package correctly from VLAN. The reason is unknown yet.   Select one device as AVB listener, and run: $gst-launch-1.0 clockselect. \( clock-id=realtime \     avtpsrc ifname=eth1.5 ! avtpcvfdepay streamid=0xAABBCCDDEEFF000A ! \     queue max-size-bytes=0 max-size-buffers=0 max-size-time=0 ! \     avdec_h264 ! videoconvert ! clockoverlay halignment=right ! waylandsink \)   The demo screenshot below: there are two clocks show on the videotestsrc stream: left one is the timestamp recorded before x264enc encoding on the AVB talker side, right one is the timestamp recorded after avdec_h265 decoding and do video convert to YUV frames on AVB listener side. You can see the timestamp is sync in seconds.     Deep dive Packet sniffer Use tcpdump on board to dump the L2 ethernet packet: ./tcpdump -i eth1 ether proto 0x22f0 -w dump.pcap The AVTP ether protocol code is 0x22f0 embedded inside the ether frame, or you can use "vlan 5" VLAN id for tcpdump parameters to dump. Then open this dump.pcap in the windows/Linux PC by the wireshark tool, it will automatically show the protocol inside the package, it can also parser the IEEE1722 (AVTP) CVF/AFF package header as below:   Precise latency measurement The clockoverlay plugin used in the above talker/listener is actually seconds level precision, which can not reflect the latency from talker videotestsrc -> listener avdec_h264 decoding finish. Here need a little hack to the clockoverlay element in the gst-plugins-base to get the millisecond precision. The patch is attached (gst-plugins-base-clockoverlay-us.patch), please apply and rebuild the gst-plugins-base, then replace the libgstpango.so on the board /usr/lib/gstreamer-1.0/. When doing CVF demo, you can take a picture of the screen, and check the two clock's diff. During my test, the latency is about 50ms, which include all the cost of encoding, AVTP packaging, streaming, ethernet transmit, ethernet receive, AVTP unpack and frame decoding. To measure the package latency from transmit port (talker) to receive port (listener), you can use the tcpdump on both end-points. And compare the Epoch Time the packet dumped: "Epoch Time: 1596252905.688243000 seconds". The delta of the epoch time of the same packet is around 100us~500us. This latency actually includes the AF_PACKET clone cost in kernel netfilter, also the tcpdump application schedule latency.   References Getting started with AVB on Linux: https://tsn.readthedocs.io/avb.html TSN vs AVB: https://dornerworks.com/blog/avb-vs-tsn-choose-the-best-deterministic-ethernet-solution-for-your-networked-devices/ ALSA aaf: https://fossies.org/linux/alsa-plugins/doc/aaf.txt Gstreamer avtp: https://gstreamer.freedesktop.org/documentation/avtp/index.html AVTP: https://avnu.org/wp-content/uploads/2014/05/AVnu-AAA2C_Audio-Video-Transport-Protocol-AVTP_Dave-Olsen.pdf MX8MP RM
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. This is a detailed programming aid for the registers associated with MMDC initialization. The last sheet formats the register settings for use with ARM RealView ICE. It can also be used with the windows executable for the DDR Stress Test. This programming aid was used for internal NXP validation boards.
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with MMDC initialization. The last sheet formats the register settings for use with ARM RealView ICE. It can also be used with the windows executable for the DDR Stress Test. This programming aid was used for internal NXP validation boards.
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with MMDC initialization. The last sheet formats the register settings for use with ARM RealView ICE. It can also be used with the windows executable for the DDR Stress Test. This programming aid was used for internal NXP validation boards.
查看全文
On imx8qm there are two DPUs(display process unit) and one ISI(image subsystem interface), ISI has 5 inputs and two of them are from DPU0 and DPU1.   This document demonstrates on how to loopback DPU1 outputs to ISI. Note that only mipi dsi0 of dpu0 and lvds1 of dpu1 can be loopbacked to isi.   Platform:                            imx8qm b0 mek OS:                                    yocto 4.14.78 ga hardware connection:        imx8qm lvds1 ====> it6263 cable =====> hdmi display.   1st: isi has 8 pipelines which can be assigned to any of the 5 inputs, this doc takes the 5th pipeline to sink the dpu1 input. So you will need to configure the isi_4( start from 0) source in the dts and write a simple v4l2 subdev for capture testing, the default isi_4 device will be /dev/video4.   2st: configure both framegen0 of dpu1 and lvds1's link to pixellink 3.   3st: write a v4l2 userspace program to capture from /dev/video4 device, take this vulkan-capture as an example. Note that Vulkan-capture is rendered by vulkan api, you can also take opengl es for rendering.   See the atttachments for details.   ======================================== 2019/11/12 update patches. ======================================== 2019/12/19 add patch. Support connect real display to DC1-LVDS1   Note: for ISI loopback,  it needs output of 2x GPIO (4x for HDMI-TX or combo PHY) to pixel_link_receiver_address: For iMX8QM: o LVDS: pixel_link_receiver_address[1:0] = do_gpio_dr[7:6]  o MIPI-DSI: pixel_link_receiver_address[1:0] = do_gpio_dr[7:6] o HDMI-TX: odd_pixel_link_receiver_address[1:0] = do_gpio_dr[7:6],even_pixel_link_receiver_address[1:0] = do_gpio_dr[5:4]   For iMX8QXP: o Combo MIPI-DSI / LVDS: pixel_link0_receiver_address[1:0] = do_gpio_dr[7:6], pixel_link1_receiver_address[1:0] = do_gpio_dr[5:4] 
查看全文
platform: imx8qxp c0 mek OS: yocto 4.19.35_1.1.0 hardware connection: imx8qxp lvds0 => dummy panel ,  lvds1 => it6263 => display   On imx8qxp there are one DPU(display process unit) and one ISI(image subsystem interface), ISI supports input from dpu.   dpu block diagram: note that only dsi0 and lvds0 can be used for loopback. and this patch only test the lvds0, since lvds support dummy panel.   Please see the readme in the attchment for how to enale this feature.   Note: for ISI loopback,  it needs output of 2x GPIO (4x for HDMI-TX or combo PHY) to pixel_link_receiver_address: For iMX8QM: o LVDS: pixel_link_receiver_address[1:0] = do_gpio_dr[7:6]  o MIPI-DSI: pixel_link_receiver_address[1:0] = do_gpio_dr[7:6] o HDMI-TX: odd_pixel_link_receiver_address[1:0] = do_gpio_dr[7:6],even_pixel_link_receiver_address[1:0] = do_gpio_dr[5:4]   For iMX8QXP: o Combo MIPI-DSI / LVDS: pixel_link0_receiver_address[1:0] = do_gpio_dr[7:6], pixel_link1_receiver_address[1:0] = do_gpio_dr[5:4]   
查看全文
  This patch will add bootaux command to imx7ulp uboot.   This would make it easier in start M4 binary image in single boot mode.   Feature: 1. Support using m4 image in .bin format. 2. Support bootaux command in u-boot. 3. Support boot from TCM and DDR (DDR not tested, if any issue, pls let me know.).   Note: 1. SDK TCM entry address is 0x1FFD2000. But TCML base address is 0x1FFD0000. Pls take care to set a correct entry address to m4_loadaddr. 2. If user want to use M4 image generated from imx_mkimage, pls refer to bootaux patch in https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/OTA-upgrade-for-smartlocker-in-i-MX7ULP-kernel/ta-p/1112687.   Test procedure: 1. Set u-boot parameters: setenv m4_loadaddr 0x1FFD2000 setenv m4_copyaddr 0x62000000 setenv m4_image hello_world.bin setenv m4_flash_imglen 0x30000 setenv m4_loadimage "fatload mmc '${mmcdev}':'${mmcpart}' '${m4_copyaddr}' '${m4_image}'; cp.b '${m4_copyaddr}' '${m4_loadaddr}' 0x30000" setenv run_m4_image "run m4_loadimage; dcache flush; bootaux '${m4_loadaddr}'" 2. Copy hello_world.bin to SD card and boot board. Make sure board is in single boot mode. 3. Run "run run_m4_image"   4. On M core console.    
查看全文
Default system can’t start Weston GUI in monitor after booting with NFS, so I find a solution to fix that issue. 1.Error messages imx8mpevk login: [31.274389] systemd[1]:weston@root.service: Main process exited, code=exited, status=1/FAILURE [ 31.274928] systemd[1]: weston@root.service: Failed with result 'exit-code'. [04:52:59.571] logind: not running in a systemd session [04:52:59.571] logind: cannot setup systemd-logind helper (-61), using legacy fallback 2.Steps Step 1:Add output in the /etc/xdg/weston/Weston.ini [output] name=HDMI-A-1 mode=1920x1080@60 Step 2:ls /sys/class/drm There will be some device nodes like card0,card1-HDMI-A-1. card1-HDMI-A-1 is we need. Step 3:Change drm_device in /etc/xdg/weston/Weston.ini drm-device=card1 Step 4:Set envs export WESTON_DRM_PRIMARY=HDMI-A-1 export WESTON_DRM_MIRROR=1 export WESTON_DRM_KEEP_RATIO=1 export WESTON_DRM_PREFER_EXTERNAL=1 export WESTON_DRM_PREFER_EXTERNAL_DUAL=1 Step 5:Start Weston weston --tty=7 -B=drm-backend.so --idle-time=0&
查看全文