i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
  Just sharing some experiences during the development and studying.   Although, it appears some hardwares, it focuses on software to speed up your developing on your  hardware.     杂记共享一下在开发和学习过程中的经验。    虽然涉及一些硬件,但其本身关注软件,希望这些能加速您在自己硬件上的开发。   12/16/2025 iMX8MN DDR3 Frequency Shifting iMX8MN DDR3 Frequency Shifting - NXP Community   3/4/2025 GPIO USB ID GPIO USB ID - NXP Community   1/20/2025 MDIO on GPIOs MDIO on GPIOs - NXP Community   12/09/2024 GPIO LEDs https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/GPIO-LEDs/ta-p/2009743     10/22/2024 iMX93-EVK PWM LED https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX93-EVK-PWM-LED/ta-p/1978047   07/25/2024 iMX secondary boot collection https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-secondary-boot-collection/ta-p/1916915   07/25/2024 HSM Code-Signing Journey https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244 25JUL2024 - add pkcs11 proxy                         HSM Code-Signing Journey_25JUL2024.pdf                          HSM Code-Signing Journey_25JUL2024.txt   06/06/2024 HSM Code-Signing Journey https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244     02/07/2024 Device Tree Standalone Compile under Windows https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Device-Tree-Standalone-Compile-under-Windows/ta-p/1855271   02/07/2024 i.MX8X security overview and AHAB deep dive i.MX8X security overview and AHAB deep dive - NXP Community   11/23/2023 “Standalone” Compile Device Tree https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Standalone-Compile-Device-Tree/ta-p/1762373     10/26/2023 Linux Dynamic Debug https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Dynamic-Debug/ta-p/1746611   08/10/2023 u-boot environment preset for sdcard mirror u-boot environment preset for sdcard mirror - NXP Community   06/06/2023 all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek all(bootloader, device tree, Linux kernel, rootfs)... - NXP Community     09/26/2022 parseIVT - a script to help i.MX6 Code Signing parseIVT - a script to help i.MX6 Code Signing - NXP Community   Provide  run under windows   09/16/2022   create sdcard mirror under windows create sdcard mirror under windows - NXP Community     08/03/2022   i.MX8MM SDCARD Secondary Boot Demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011     02/16/2022 mx8_ddr_stress_test without UI   https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/mx8-ddr-stress-test-without-UI/ta-p/1414090   12/23/2021 i.MX8 i.MX8X Board Reset https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-i-MX8X-Board-Reset/ta-p/1391130       12/21/2021 regulator userspace-consumer https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/regulator-userspace-consumer/ta-p/1389948     11/24/2021 crypto af_alg blackkey demo crypto af_alg blackkey demo - NXP Community   09/28/2021 u-boot runtime modify Linux device tree(dtb) u-boot runtime modify Linux device tree(dtb) - NXP Community     08/17/2021 gpio-poweroff demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/gpio-poweroff-demo/ta-p/1324306         08/04/2021 How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709       07/14/2021 SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416     04/07/2021 i.MX8QXP eMMC Secondary Boot https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45       03/25/2021 sc_misc_board_ioctl to access the M4 partition from A core side sc_misc_board_ioctl to access the M4 partition fr... - NXP Community     03/17/2021 How to Changei.MX8X MEK+Base Board  Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8X-MEK-Base-Board-Linux-Debug-UART/ba-p/1246779#M43     03/16/2021 How to Change i.MX8MM evk Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938#M40       05/06/2020 Linux fw_printenv fw_setenv to access U-Boot's environment variables Linux fw_printenv fw_setenv to access U-Boot's env... - NXP Community     03/30/2020 i.MX6 DDR calibration/stress for Mass Production https://community.nxp.com/docs/DOC-346065     03/25/2020 parseIVT - a script to help i.MX6 Code Signing https://community.nxp.com/docs/DOC-345998     02/17/2020 Start your machine learning journey from tensorflow playground Start your machine learning journey from tensorflow playground      01/15/2020 How to add  iMX8QXP PAD(GPIO) Wakeup How to add iMX8QXP PAD(GPIO) Wakeup    01/09/2020 Understand iMX8QX Hardware Partitioning By Making M4 Hello world Running Correctly https://community.nxp.com/docs/DOC-345359   09/29/2019 Docker On i.MX6UL With Ubuntu16.04 https://community.nxp.com/docs/DOC-344462   09/25/2019 Docker On i.MX8MM With Ubuntu https://community.nxp.com/docs/DOC-344473 Docker On i.MX8QXP With Ubuntu https://community.nxp.com/docs/DOC-344474     08/28/2019 eMMC5.0 vs eMMC5.1 https://community.nxp.com/docs/DOC-344265     05/24/2019 How to upgrade  Linux Kernel and dtb on eMMC without UUU How to upgrade Linux Kernel and dtb on eMMC without UUU     04/12/2019 eMMC RPMB Enhance and GP https://community.nxp.com/docs/DOC-343116   04/04/2019 How to Dump a GPT SDCard Mirror(Android O SDCard Mirror) https://community.nxp.com/docs/DOC-343079   04/04/2019 i.MX Create Android SDCard Mirror https://community.nxp.com/docs/DOC-343078   04/02/2019: i.MX Linux Binary_Demo Files Tips  https://community.nxp.com/docs/DOC-343075   04/02/2019:       Update Set fast boot        eMMC_RPMB_Enhance_and_GP.pdf   02/28/2019: imx_builder --- standalone build without Yocto https://community.nxp.com/docs/DOC-342702   08/10/2018: i.MX6SX M4 MPU Settings For RPMSG update    Update slide CMA Arrangement Consideration i.MX6SX_M4_MPU_Settings_For_RPMSG_08102018.pdf   07/26/2018 Understand ML With Simplest Code https://community.nxp.com/docs/DOC-341099     04/23/2018:     i.MX8M Standalone Build     i.MX8M Standalone Build.pdf     04/13/2018:      i.MX6SX M4 MPU Settings For RPMSG  update            Add slide CMA Arrangement  Consideration     i.MX6SX_M4_MPU_Settings_For_RPMSG_04132018.pdf   09/05/2017:       Update eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 09/01/2017:       eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 08/30/2017:     Dual LVDS for High Resolution Display(For i.MX6DQ/DLS)     Dual LVDS for High Resolution Display.pdf 08/27/2017:  L3.14.28 Ottbox Porting Notes:         L3.14.28_Ottbox_Porting_Notes-20150805-2.pdf MFGTool Uboot Share With the Normal Run One:        MFGTool_Uboot_share_with_NormalRun_sourceCode.pdf Mass Production with programmer        Mass_Production_with_NAND_programmer.pdf        Mass_Production_with_emmc_programmer.pdf AndroidSDCARDMirrorCreator https://community.nxp.com/docs/DOC-329596 L3.10.53 PianoPI Porting Note        L3.10.53_PianoPI_PortingNote_151102.pdf Audio Codec WM8960 Porting L3.10.53 PianoPI        AudioCodec_WM8960_Porting_L3.10.53_PianoPI_151012.pdf TouchScreen PianoPI Porting Note         TouchScreen_PianoPI_PortingNote_151103.pdf Accessing GPIO From UserSpace        Accessing_GPIO_From_UserSpace.pdf        https://community.nxp.com/docs/DOC-343344 FreeRTOS for i.MX6SX        FreeRTOS for i.MX6SX.pdf i.MX6SX M4 fastup        i.MX6SX M4 fastup.pdf i.MX6 SDCARD Secondary Boot Demo        i.MX6_SDCARD_Secondary_Boot_Demo.pdf i.MX6SX M4 MPU Settings For RPMSG        i.MX6SX_M4_MPU_Settings_For_RPMSG_10082016.pdf Security        Security03172017.pdf    NOT related to i.MX, only a short memo
View full article
Application Note AN13872  Enabling SWUpdate on i.MX 6ULL, i.MX 8M Mini, and i.MX 93 is available on www.nxp.com    SWUpdate: Embedded Systems become more and more complex. Software for Embedded Systems have new features and fixes can be updated in a reliable way. Most of time, we need OTA(Over-The-Air) to upgrade the system. Like Android has its own update system. Linux also need an update system. SWUpdate project is thought to help to update an embedded system from a storage media or from network. However, it should be mainly considered as a framework, where further protocols or installers (in SWUpdate they are called handlers) can be easily added to the application. Mongoose daemon mode: Mongoose is a daemon mode of SWUpdate that provides a web server, web interface and web application. Mongoose is running on the target board(i.MX8MM EVK/i.MX8QXP MEK).Using Web browser to access it.   Suricatta daemon mode: Suricatta regularly polls a remote server for updates, downloads, and installs them. Thereafter, it reboots the system and reports the update status to the server. The screenshot is SWUpdate scuricatta working with hawkbit server.          
View full article
Symptoms   Trying to initialize a repo, for example:  $repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml we have the below log: File "/home/username/bin/repo", line 51 def print(self, *args, **kwargs): ^ SyntaxError: invalid syntax   Workaround (1)   The first workaround consist in change the python alternatives (caused when you have installed two or more python versions). NOTE: in my case, the python version that i want to change as first priority is python3.8 $sudo update-alternatives --install /usr/bin/python python /usr/bin/python3.8 1   Then we run: $sudo update-alternatives --config python    To verify if your python priority was changed successfully try: $python --version   You should see the version configured as priority number 1.     Workaround (2)   The workaround is very simple, only we need modify the repo file $ nano ~/bin/repo   and we will change the python interpreter in the first line (from python to python3): ORIGINAL FILE   EDITED FILE   After to do this change, repo will works fine again.     I hope this can helps to you!   Best regards.
View full article
Description       This doc explain how to enable the plugin boot on i.MX6Q/6DL and which used for change the pll2 clock and add the spread spectrum support to pass the EMI test. we still list the source codes of 3.0.35 and 4.1.15. to explain the dts/non-dts kernel support.       本文旨在说明如何在i.MX6Q/6DL上实现plugin启动,以支持展频和改变pll2的频率,其目的是为了通过 EMI测试。也附上了基于3.0.35和4.1.15的源代码,以供参考   Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 SabreSDP https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false          Version: MX6Q_PLUGIN_FC_SSC_V7-20200915_chn..pdf(chinese version)add baidou support MX6Q_PLUGIN_FC_SSC_V7-20170504_eng-chapter-imx6dl.doc+MX6Q_PLUGIN_FC_SSC_V3-20170309_eng.doc(english version)      
View full article
This article will describe one suggestion for one issue that UART continuously generate RX interrupts and receive 0xFF even when Rx line is continuously high in some cases on imx6 series. Below I will explain with imx6DL. Some settings are just to make it easier to reproduce. BSP version: L5.4.70-2.3.0 Board HW: MCIMX6DL-SDB When issue happen Config imx6DL UART3 as the serial port to 1200 baud, 8-N-1 format. Keep the RX Line high. Make the RX line low and keep it for a short time (360 usec-370 usec).   At this condition, you will find that the UART will continuously generate RX interrupts and show receiving 0xFF even you make the RX line return to be high. Why issue happen The low time is not in the correct range and out of our spec. In the imx6DL AEC document, there is one chapter named UART Receiver like blow   If using 1200 band, that means one valid bit time is 833 usec. And there is a definition that “tolerate 1/(16 x Fbaud_rate) tolerance in each bit”. That’s means in the case of 1200 baud. A range of valid bit is 781 to 885 usec. But is reproducing, the Low level time is 360 usec. This time out of range will make UART state machine to be confused. How to fix Actually, the best way is following our spec. If there is such an unknown situation in the customer’s environment, then the following method could be regarded as a suggestion to fix the issue meet by the customer. The interrupt handler will check USR1[AWAKE]. 2    If AWAKE is asserted, clear it and proceed as usual (assume we have valid data), else, check if USR1[AGTIM] is asserted. 3    if AGTIM is asserted, clear it and proceed as usual, else perform software reset (assume we have invalid data). Checking AGTIM is for one race condition when the RX fifo has some characters (less than RXTL) but no more data is coming in. When following this procedure, the UART will perform a software reset when a block interrupt occurs. Notes: From customer report, error could be cleared if a valid start-bit is detected on the RX line. This needs to be verified by the customer themselves. Test code has been included in attachment.   Besst Regards
View full article
Hello there. Here is a good way to use U-boot in an efficient way with custom scripts. The bootscript is an script that is automatically executed when the boot loader starts, and before the OS auto boot process. The bootscript allows the user to execute a set of predefined U-Boot commands automatically before proceeding with normal OS boot. This is especially useful for production environments and targets which don’t have an available serial port for showing the U-Boot monitor. This information can be find in U-Boot Reference Manual.   I will take the example load a binary file in CORTEX M4 of IMX8MM-EVK. In my case, I have the binary file in MMC 2:1 called gpio.bin and I will skip those steps because that is not the goal.   First, you need the u-boot-tools installed in your Linux machine: sudo apt install u-boot-tools   That package provide to us the tool mkimage to convert a text file (.src, .txt) file to a bootscript file for U-Boot.   Now, create your custom script, in this case a simple script for load binary file in Cortex M4: nano mycustomscript.scr  and write your U-Boot commands: fatload mmc 2:1 0x80000000 gpio.bin cp.b 0x80000000 0x7e0000 0x10000 bootaux 0x7e0000   Now we can convert the text file to bootscript with mkimage. Syntax: mkimage -T script -n "Bootscript" -C none -d <input_file> <output_file> mkimage -T script -n "Bootscript" -C none -d mycustomscript.scr LCM4-bootscript   This will create a file called LCM4-bootscript (Or as your called it).   A way to load this bootscript file to U-Boot is using the UUU tool, in U-Boot set the device in fastboot with command: u-boot=> fastboot 0 Then in linux with the board connected through USB to PC run the command: sudo uuu -b fat_write LCM4-bootscript mmc 2:1 LCM4-bootscript   Now we have our bootscript in U-Boot in MMC 2:1.   Finally, we can run the bootscript in U-Boot: u-boot=> load mmc 2:1 ${loadaddr} LCM4-bootscript 158 bytes read in 2 ms (77.1 KiB/s) u-boot=> source ${loadaddr} ## Executing script at 40400000 6656 bytes read in 5 ms (1.3 MiB/s) ## No elf image at address 0x007e0000 ## Starting auxiliary core stack = 0x20020000, pc = 0x1FFE02CD...   And the Cortex M4 booted successfully:    I hope this can helps to you.   Best regards.   Salas.  
View full article
Dynamic debug is designed to allow you to dynamically at runtime  enable/disable  kernel code to obtain additional kernel information. Currently, if ``CONFIG_DYNAMIC_DEBUG`` is set, then all ``pr_debug()``/``dev_dbg()`` and ``print_hex_dump_debug()``/``print_hex_dump_bytes()`` calls can be dynamically enabled per-callsite.    
View full article
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is the detailed programming aid for the registers associated with DRAM initialization (DDR3 and LPDDR2) of the MX6UL/ULL/ULZ (consolidated RPA). The last work sheet tab in the tool formats the register settings for use with the ARM DS5/RealView debugger. It can be manually converted by the user to a DCD file format used by uboot or other bootloaders (note the removal of debugger specific commands in this tab). The programming aids were developed for internal NXP validation and development boards.   This tool serves as an aid to assist with programming the DDR interface of the MX6UL/ULL/ULZ and is based on the DDR initialization scripts developed by the R&D team and no guarantees are made by this tool.   The following are some general notes regarding this tool: Refer to the "How To Use" tab in the tool as a starting point to use this tool. Note that in the "DStream .ds file" tab there are DS5 debugger specific commands that should be commented out or removed when using the DRAM initialization for non-debugger specific applications (like when porting to bootloaders). This tool may be updated on an as-needed basis for bug fixes or future improvements.  There is no schedule for aforementioned maintenance.  
View full article
The HSM Coding-Signing is new. When we follow the instructions in Code-Signing Tool User’s Guide , still has something to overcome, most of them are related to the OS. Actually, Code-Signing Tool User’s Guide  can not give detail every “obvious” step. The purpose of this document is to share the experiences on my system. Hope those experience can give you some clues on your system.     25JUL2024 - add pkcs11 proxy                         HSM Code-Signing Journey_25JUL2024.pdf                          HSM Code-Signing Journey_25JUL2024.txt  
View full article
This article is rather short that only mentions the script that is needed to make an iMX93EVK act as a USB mass storage device so that whenever you connect your iMX device to a windows/linux system via USB, it should get enumerated something like a usb drive.  The storage that is used in this example is mmc so the expectation is that you have inserted a mmc card in the slot. Below is the script:- #!/bin/sh   # This composite gadget include function: # - MASS STORAGE     # # Exit status is 0 for PASS, nonzero for FAIL # STATUS=0   # Check if there is udc available, if not, return fail UDC_DIR=/sys/class/udc if test "$(ls -A "$UDC_DIR")"; then echo "The available udc:" for entry in "$UDC_DIR"/* do echo "$entry" done else STATUS=1 echo "No udc available!" exit $STATUS; fi   id=1; udc_name=ci_hdrc.0 #back_file=/dev/mmcblk1 back_file=/tmp/lun0.img   mkdir /sys/kernel/config/usb_gadget/g$id cd /sys/kernel/config/usb_gadget/g$id   # Use NXP VID, i.MX8QXP PID echo 0x1fc9 > idVendor echo 0x12cf > idProduct   mkdir strings/0x409 echo 123456ABCDEF > strings/0x409/serialnumber echo NXP > strings/0x409/manufacturer echo "NXP iMX USB Composite Gadget" > strings/0x409/product   mkdir configs/c.1 mkdir configs/c.1/strings/0x409   echo 5 > configs/c.1/MaxPower echo 0xc0 > configs/c.1/bmAttributes   mkdir functions/mass_storage.1 echo $back_file > functions/mass_storage.1/lun.0/file ln -s functions/mass_storage.1 configs/c.1/   echo $udc_name > UDC First execute the script. After that insert the g_mass_storage module in the kernel by executing :- modprobe g_mass_storage file=/dev/mmcblk1 removable=1 In the dmesg output, you will see something like below:-   After that you can connect a C type USB cable to the USB1 port of imx93evk and the other end to any USB ports of a laptop. The moment it is connected, you would be able to see a USB drive similar to what you get when we connect a pen-drive. 
View full article
Usually, device tree source files are not a signal pure dts file. It could include dtsi, dts or C code heads .h files. Need C compiler finish the pre-compile to a pure dts file first. It is integrated inside the like Linux build system(Makefile, etc.). This document shows the original way to compile device tree. This document will show compile device tree under windows.    
View full article
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
View full article
We will build a remote debug environmet of Qt Creator in this user guide.   Contents 1 Change local.conf file in Yocto 2 2 Build and deploy Yocto SDK 2 2.1 Build full image SDK . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2 2.2 Deploy SDK . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2 3 Configure QT Kit 2 3.1 Setup device . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2 3.2 Configure QT version . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3 3.3 Configure gcc and g++ manually . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4 3.4 Configure gdb manually . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5 3.5 Configure Kit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5 3.6 Very important thing!! . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5 4 Test result
View full article
Hello everyone, this document will explain on how to create and run a custom script for UUU (Universal Update Utility) tool Requirements: I.MX 8M Mini EVK Linux Binary Demo Files - i.MX 8MMini EVK (L5.10.35) UUU Serial console emulator (tera term or putty) Text editor (Notepad++, nano, etc) UUU is a pretty flexible tool since it uses the Fastboot protocol through uboot to flash the desired images, this will make possible to create a custom script to add many uboot commands to customize further the boot settings. In this example I will create a custom script which will flash uboot and Linux rootfs and write a Cortex-M binary to the FAT partition of the eMMC. At the same time I’ll create and modify a set of environmental variables, this variables will have a set of uboot commands that will load to the TCM this same binary before the device starts booting into Linux.   Creating the script For this document I'll be using Notepad++ but any text editor may be used instead, since the scripts used by UUU are written in plain text. The very first line of the script must be the version number which will represent the minimum UUU version that UUU can parse this script. For this case that version is 1.2.39 After it, we will add all standard commands to flash uboot and filesystem into the eMMC. Note: This may be also copied from the uuu.auto script inside the Demo files. Please note that the UUU commands format is PROTOCOL: CMD, for this example we will be using mainly SDP and FB protocols which corresponds to the serial download protocol and Fastboot respectively. For a list of all supported UUU protocols and commands please refer to the UUU documentation here: https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.4.165/UUU.pdf Now add the following commands to the script, this will download and write into eMMC FAT partition, which was created when flashing the .wic image, the Cortex-M binary.   FB: ucmd setenv fastboot_buffer ${loadaddr} FB: download -f hello_world_test.bin FB[-t 20000]: ucmd fatwrite mmc ${emmc_dev}:1 ${fastboot_buffer} hello_world_test.bin ${fastboot_bytes}   #fatwrite write file into a dos filesystem "<interface> <dev[:part]> <addr> <filename> [<bytes> [<offset>]] - write file 'filename' from the address 'addr' in RAM  to 'dev' on 'interface' Note: The Cortex-M binary was named as hello_world_test.bin, but any example name may be used. At this point, in the script we will be using only uboot commands as seen above, in this case was fatwrite. The script will look as following: If the script is run now uboot (imx-boot-imx8mmevk-sd.bin-flash_evk), rootfs (imx-image-multimedia-imx8mmevk.wic) will be flashed and the Cortex-M binary (hello_world_test.bin) written to the FAT partition of the eMMC. To add environmental variables to modify uboot boot settings, i.e. overwrite the dtb variable so the EVK will select the RPMSG dtb, this in case the Cortex-M example needs to be run at the same time as Cortex-A. FB: ucmd setenv fdtfile imx8mm-evk-rpmsg.dtb Next add to the UUU script the set of uboot commands in form of environmental variables that will load to the TCM the Cortex-M binary   FB: ucmd setenv loadm4image "fatload mmc ${emmc_dev}:1 0x48000000 hello_world_test.bin; cp.b 0x48000000 0x7e0000 0x20000" FB: ucmd setenv m4boot "run loadm4image; bootaux 0x48000000" Note: This can be changed to load it to different targets not only TCM, for example DRAM. Now for the set of environmental variable to run when uboot starts booting into Linux we may add it to the variable mmcboot. Also adding the command to save the environmental variables set so the settings persist after reboot, this by adding the following commands to the script:   FB: ucmd setenv mmcboot "run m4boot; $mmcboot" FB: ucmd saveenv The resulting script will be the following: Now just save the script and name it as you see fit, for this example the name will be custom_script.auto.   Running the script To run a UUU script is pretty simple, just make sure that the files used in the script are in the same folder as the script. Windows > .\uuu.exe  custom_script.auto Linux $ sudo ./uuu custom_script.auto   Wait till it finish, turn the board off, set it to boot from eMMC and turn it on, the EVK will boot into Linux automatically and will launch the Cortex-M core automatically. We may also, double check that the environmental variables were written correctly by stopping at uboot and using the printenv command For this test I have used the Prebuilt image which includes sample Cortex-M4 examples for the EVK   further flexibility UUU scripts can be customized even more, for example using macros, so the script can take input arguments so it may be possible to select the uboot, rootfs, Cortex-M binary and dtb to be used when booting, and to be used for other i.MX chips as well. The resulting script will be as following: Note: Here is assumed that the dtb file is already at the FAT partition, if not same procedure may be added as the Cortex-M binary. To run a script which expect to have input arguments is as follow: Windows > .\uuu.exe -b uuu_cortexM_loader.auto imx-boot-imx8mmevk-sd.bin-flash_evk imx-image-multimedia-imx8mmevk.wic hello_world_test.bin imx8mm-evk-rpmsg.dtb Linux $ sudo ./uuu -b uuu_cortexM_loader.auto imx-boot-imx8mmevk-sd.bin-flash_evk imx-image-multimedia-imx8mmevk.wic hello_world_test.bin imx8mm-evk-rpmsg.dtb Please find both UUU scripts attached and feel free to use them. Hope this helps everyone to better understand how this tool works and the capabilities it have.
View full article
In some cases, i.MX board connect to different module. It has very tiny changes, such as just one gpio different driver strength. We can build an entire new software to handle this requirement. Here we introduce another way, using u-boot to modify the device tree(dtb) at runtime.   Here is u-boot fdt command for  How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709   run loadfdt fdt addr ${fdt_addr_r} fdt print /soc/bus/pinctrl/uart3grp fdt rm /soc/bus/pinctrl/uart3grp fdt print serial2 fdt set serial2 status disabled fdt print serial2 fdt print gpio4 fdt resize fdt mknode gpio4 gpio_hog_demo fdt set gpio4/gpio_hog_demo gpio-hog fdt set gpio4/gpio_hog_demo gpios <7 0> fdt set gpio4/gpio_hog_demo output-high fdt print gpio4 run mmcargs run loadimage booti ${loadaddr} - ${fdt_addr_r} root@imx8mmevk:~# cat /sys/kernel/debug/gpio gpiochip0: GPIOs 0-31, parent: platform/30200000.gpio, 30200000.gpio: gpio-5 ( |PCIe DIS ) out hi gpio-13 ( |ir-receiver ) in hi IRQ ACTIVE LOW gpio-15 ( |cd ) in hi IRQ ACTIVE LOW gpiochip1: GPIOs 32-63, parent: platform/30210000.gpio, 30210000.gpio: gpio-38 ( |? ) out hi gpio-42 ( |reset ) out lo ACTIVE LOW gpio-51 ( |regulator-usdhc2 ) out lo gpiochip2: GPIOs 64-95, parent: platform/30220000.gpio, 30220000.gpio: gpio-80 ( |status ) out hi gpiochip3: GPIOs 96-127, parent: platform/30230000.gpio, 30230000.gpio: gpio-117 ( |PCIe reset ) out hi gpiochip4: GPIOs 128-159, parent: platform/30240000.gpio, 30240000.gpio: gpio-135 ( |gpio_hog_demo ) out hi gpio-141 ( |spi1 CS0 ) out hi ACTIVE LOW gpio-149 ( |wlf,mute ) out hi ACTIVE LOW root@imx8mmevk:~# [ 33.758914] VSD_3V3: disabling dtc_utils-v1.6.1-win-x86_64.zip by msys2   
View full article
Hello everyone, In this document I'll explain on how to build the UUU (Universal Update Utility) using windows 10 PC. This may be useful in case of adding custom commands to run during the flash using built-in scripts, be it for debugging, fuse blowing, etc. First we need to download and install Visual Studio community, for this guide I'll use community 2019, version it is available here: https://visualstudio.microsoft.com/thank-you-downloading-visual-studio/?sku=Community&rel=16 For workloads select Universal Windows Platform development.   When installing, make sure to select and install the Git for windows complement, at the top select Individual components, this will display a new list, scroll down to code tools and you will find Git for windows, check this box In case Visual Studio is already installed, you may open the installer again and chose modify, this will let you install the complement as well. After the installation is complete we may run the git commands on the power shell. Now open the windows power shell and type the following commands: git clone https://github.com/NXPmicro/mfgtools.git // clones the MFGTool (UUU) source code from the github cd mfgtools // enters the mfgtools folder we just cloned git submodule init // creates the local configuration file for the submodules git submodule update // set the submodules to the commit specified by the main repository. At this point we can edit the built in scripts to add our custom commands, for this guide I'll add the printenv uboot command at the end of the flashing process. For this I'll enter the folder mfgtools/uuu, and edit emmc_burn_all.lst with any text editor, i.e. Notepad ++, add the command FB: ucmd printenv.   Save and close the editor, it is possible to add most uboot commands like for example the fuse commands to burn eFuses. Then we can now build the tool, opening msvc/uuu-static-link.sln with Visual studio, select solution uuu-static-link.sln   And finally build the solution: The executable (uuu.exe) would be at the following path: mfgtools\msvc\x64\Debug   Finally we run the built in script we modified and check the results. Find attached both the powershell and uboot logs, I tested this using an i.MX8MN with L5.4.47_2.2.0, running the following command: ./uuu.exe -v -b emmc_all imx-boot-imx8mnevk-sd.bin-flash_evk imx-image-full-imx8mnevk.wic Hope this may found useful for anyone trying to achieve something similar.
View full article
  Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 family developement board https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false  
View full article
i.MX93 eMMC Secondary Boot          i.MX93 eMMC Secondary Boot.zip   i.MX8MP eMMC Secondary Boot           i.MX8MP eMMC Secondary Boot.zip i.MX8MM SDCARD Secondary Boot Demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011   i.MX8QXP eMMC Secondary Boot https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45    i.MX6 SDCARD Secondary Boot Demo           i.MX6_SDCARD_Secondary_Boot_Demo.pdf      
View full article
Hello everyone! In this quick example its focused on how to customize uboot code to generate an uboot image with a silent console so its speed up the flash and boot time, this may provide helpful for customers who have a bigger images or just want to have a silent console. Note: this should not be enabled if the image is still being under test, since this will disable all communication with the debug terminal and there won't be boot messages. Requirements: I.MX 8M Nano DDR4 EVK i.MX 8M Nano EVK Prebuilt image (6.1.1-1.0.0) UUU tool First clone the code from the uboot repository: $ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.1.1-1.0.0 $ cd uboot-imx After we get the code, then proceed to enable the silent console in the uboot defconfig: $ nano configs/imx8mn_ddr4_evk_defconfig CONFIG_SILENT_CONSOLE=y CONFIG_SILENT_U_BOOT_ONLY=y For this to actually work we need to create the silent environmental variable and give it a value different from "0": $ nano include/configs/imx8mn_evk.h "silent=1\0"      \ As specified in our Linux porting guide: Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command, set Target-Machine to the machine you are building for. See Section "Build configurations" in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG) Set up the host terminal window toolchain environment: $ source/opt/fsl-imx-xwayland/6.1.1/environment-setup-aarch64-poky-linux $ export ARCH=arm64 Build uboot binary: $ make distclean $ make imx8mn_ddr4_evk_defconfig $ make Build ARM Trusted Firmware (ATF) $ cd .. $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.1.1-1.0.0 $ cd imx-atf/ $ make PLAT=imx8mn bl31 In case you get the error aarch64-poky-linux-ld.bfd: unrecognized option '-Wl,-O1' $ unset LDFLAGS Download the DDR training & HDMI binaries $ cd .. $ mkdir firmware-imx $ cd firmware-imx $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.19.bin $ chmod a+x firmware-imx-8.19.bin $ ./firmware-imx-8.19.bin Accept EULA and the firmware will be deployed. Download imx-mkimage and build the boot image $ cd .. $ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.1.1-1.0.0 $ cd imx-mkimage $ cp ../uboot-imx/spl/u-boot-spl.bin iMX8M/ $ cp ../uboot-imx/u-boot-nodtb.bin iMX8M/ $ cp ../uboot-imx/arch/arm/dts/imx8mn-ddr4-evk.dtb iMX8M/ $ cp ../imx-atf/build/imx8mn/release/bl31.bin iMX8M/ $ cp ../firmware-imx/firmware-imx-8.19/firmware/ddr/synopsys/ddr4_* iMX8M/ $ cp ../uboot-imx/tools/mkimage iMX8M/mkimage_uboot $ make SOC=iMX8MN flash_ddr4_evk After this we can download our uboot image to our board, we can either use the uboot image for boot or for flashing purpose only. We can compare the time it takes using UUU with a standard pre-built image uuu -V -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-full-imx8mnevk.wic It takes 485.5 seconds using normal uboot with debug console enabled. uuu -V -b emmc_all flash.bin imx-image-full-imx8mnevk.wic It takes 477.5 seconds using silent uboot console. Even if the speed is not greatly improved (~8 seconds), in larger files it could help to speed up flashing, even if wants to have the console silent is a good option. Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
View full article