コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers, fridges and washing machines, they all have one thing in common: Near-field-communication (NFC) which allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be identified and authenticated without any user interaction. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC.
記事全体を表示
This session will go over all the available tools and documents provided by NXP to accelerate your design with i.MX applications processors, from hardware design check-lists, to DDR bring-up tools, from IOMUX aid tool to Yocto BSP customization. Get an insight of what NXP can provide to ease the development process.
記事全体を表示
Signal integrity, EMI, RFI...They are all the result of how well you manage the Electromagnetic fields in your designs. EM fields live in spaces, not conductors. The material presented focuses on the basic physics of electromagnetic energy, presented in an entertaining and easy-to-understand format with plenty of diagrams. Attendees will discover how understanding the behavior of EM fields can help them to design PCBs that will be more robust and have better EMC performance. This is not rocket science, but an easy-to-understand application of PCB geometry.
記事全体を表示
Deep dive into the vision processing architecture of the i.MX 8 family. Learn how to access the advanced processing features, the vision SDK, and the vision-based applications enabled by the i.MX 8 processor. This class provides an introduction to understanding the unique way in which machine vision is handled by i.MX 8. It forms a basic introduction class that is a precursor to the more advanced "Call Your Shot!" pool table demo class.
記事全体を表示
In recent years, automotive cybersecurity has become a top priority for OEMs as several well publicized attacks on production vehicles stirred up public and government concern over both security and safety of connected vehicle systems. In this talk we will: Review major milestones and headlines related to automotive cybersecurity for 2016; Compare and contrast security techniques used in traditional IT infrastructure versus automotive computing systems; Examine where these traditional techniques fall short for automotive applications.
記事全体を表示
This hands-on session introduces the MCUXpresso suite of tools (IDE, SDK, Config Tools) and shows users how to rapidly start development with thousands of Kinetis and LPC MCUs based on the ARM® Cortex®-M core. Using either Kinetis or LPC development hardware, attendees will build a custom SDK, configure pins and clocks settings, generate a project, import and debug an application.
記事全体を表示
The material presented will be focused on the physics of electromagnetic energy basic principles, presented in easy to understand language with plenty of diagrams. Attendees will discover how understanding the behavior of EM fields can help to design PCBs that will be more robust and have better EMC performance. This is not rocket science, but an easy to understand application of PCB geometry.
記事全体を表示
Future networks will still use CAN to a huge extend - but the variety of trends is also significantly increasing. This session shows key values, technical background and differentiators of the different CAN trends and the NXP implementation.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
A guide to using HAB on i.MX family of processors. Learn features and tools available to help deploy signed and encrypted images.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
Near Field Magnetic Induction (NFMI) technology, demonstrating a family of ultra-low-power, single-chip solutions enabling wireless audio streaming that are highest quality ear-to-ear communications for hearables and data communication.
記事全体を表示
Extend your logistics track and trace with condition insights. NTAG SmartSensor enables sensing and logging with NFC readout. NTAG SmartSensor enables your IoT application for smart logistics, smart healthcare, drug delivery and smart packaging.
記事全体を表示
Learn how to develop a wireless connected product using BLE and/or Thread protocols.
記事全体を表示
Learn how to develop a wireless connected product using BLE and/or Thread protocols.
記事全体を表示
This presentation will present a simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC.
記事全体を表示
Design, Software & Services Hands-On Workshop: Design with Embedded Solutions for the Always-On Market Using the New LPC54114 Power-Efficient MCU  DES-N2084 & DES-N1956 Hands-On Workshop: FreeRTOS Solutions for Kinetis MCUs  DES-N1960 Hands-On Workshop Kinetis Enablement  Hands-On Workshop: Securing the IoT One Edge Node at a Time with Kinetis DES-N1931 i.MX 6QuadPlus and i.MX 6DualPlus Applications Processors-Performance-Tier Multicores for Visually Stunning Graphics-Centric Applications  DES-N1940 i.MX 8 Graphics Architecture   Kinetis® MCU Security Technology  Linear Technology: Proven & Scalable Power Solutions for the Latest QorIQ Series Processors  Logic Devices: Case Studies of Practical Examples of Power, Space and Cost Savings with NXP Innovative Logic Solutions Micron Technology: Memory Choices for NXP Microprocessors  Security 101: Introduction to Security Acceleration in QorIQ® Processors  TQ-Systems: How to Speed Up and Optimize Your Design with Modular Approach  USB Type-C Overview  Smart Home & Buildings Bluetooth® Smart Mesh: Simple and Easy-to-Use Low-Power Wireless Networking Protocol Hands-On Workshop: Advanced Thread® Stack Class on Routing, Border Router, Security, Low Power and Commissioning  Hands-On Workshop: Use NFC Pairing to Connect Multiple Bluetooth® and Wi-Fi® Devices with a Simple Tap  How to Choose the Right NFC Solution for Your Use Case Insight & Innovation LPC Microcontrollers Portfolio, Enablement Overview and Roadmap  INS-N1819 Sensor Deep-Dive Demos and Data Collection Techniques  Secure Mobile, Healthcare & Wearables MHW-N1990 Enabling Ultimate Miniaturization and Customization with the Latest Single Chip System Module Technology  MHW-N2009 Hands-On Workshop Develop your IoT and Wearable Applications Instantly with Hexiwear.pdf  MHW-N1917 Wireless Charging Lets You Cut that Cord!  Smart Machinery & Industrial Automation SMI-N1948 Hands-On Workshop - Kinetis Motor Suite.pdf  Smart Networks NET-N1865 Introduction to QorIQ LS1012A - the Worlds Smallest and Lowest Power 64-bit Processor.pdf 
記事全体を表示
In this class, you will learn to use NXP’s FreeMASTER debug tool to aid in system development and debug. Although it is has many uses in various applications, we will demonstrate the features and use of FreeMASTER to simplify the development process with a motor control example based on our MagniV MC9S12ZVMRM microcontroller. Participants will see how useful and easy it is to use and configure so that system variables can be adjusted on the fly or watch system parameters real time.
記事全体を表示
Expect your platform to boot in less than one second...do your customer's demand it? Even if that is not fast enough for some cases...we will discuss what can be done to improve the booting performance. Learn from the experts on how to architect and optimize the boot process from boot ROM, boot loader through to OS and applications.
記事全体を表示