Connects - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

Discussions

Sort by:
Learn how NXP provides support for ODP and DPDK without sacrificing performance. Learn how we're leveraging specific acceleration advantages of the NXP data plane architectures, such as packet IO, classification, scheduling, crypto, etc. This session will provide a comparative analysis and evolution of both of these open-source, platform independent and vendor-neutral standard APIs for optimized packet processing and traditional networking services in user space. It will help you choose the right API for your project, based on design requirements.   We will also cover how the ODP and DPDK can provide the necessary infrastructure for virtualized environments.
View full article
Learn about NXP's secured IoT Gateway platform with sensor fusion, local and cloud analytic. IoT data aggregation, sensor fusion and analytic processes are run in VMs providing VM isolation advantage. IoT processes can also run in Virtualized Network Functions (VnF) that can run as service chains across end-to-end virtualized network equipment
View full article
NXP’s latest and most powerful Microprocessor requires the latest and fastest memories to keep it running efficiently. During this session, we will discuss the new memories supported on the new i.MX 8 processor family. For DRAM, this will include DDR4 and Low Power DDR4. For non-volatile memory this will include Octal SPI NOR (XccelaTM Flash) which offers up to 400MB/s as well as the latest eMMC 5.X devices that also support high speeds. These devices are offered with Commercial, Industrial or Automotive temperature and quality ratings. I will include a section on packaging technologies that can provide designers with innovative ways to reduce size. These include Package on Package and Multi-Chip Packages. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8 systems. Micron will be giving away 2-1/2” 120GB SSDs to the first 50 attendees of this session.
View full article
ARM® mbed™ OS is an open source embedded operating system designed specifically for simplifying the development of scalable Internet of Things (IoT) devices. It includes all of the features you need to develop a connected-product based on ARM Cortex®-M microcontrollers such as Kinetis and LPC MCUs.  In this hands on workshop you will get familiar with the features of mbed OS and learn how to develop and debug mbed OS applications with a traditional IDE.
View full article
As geometries continue to shrink and switching speeds increase, designing electromagnetic systems and printed circuit boards to meet the required signal integrity and EMC specifications has become even more challenging. A new design methodology is required, specifically, the utilization of an electromagnetic physics-based design methodology to control the field energy in your design. This session will review basic EM theory and introduce some new guidelines for designing compliant printed circuited boards.
View full article
Security has never been more critical than it is today. Learn how the QorIQ Trust Architecture can be leveraged to increase the security of your design. Different phases in a product's life cycle can expose different vulnerabilities for attackers to exploit. This session covers secure device life cycle management as a concept, while also providing specific examples of secure implementations using QorIQ Trust Architecture.
View full article
Systems are complex, and increasing complexity does not translate to product differentiation. Extracting the maximum networking performance, battery life or graphics capability requires knowledge of the underlying silicon and software. Developer resources are tight, and shifting the focus to product development above platform development maximizes return on investment. Freescale has deep enablement technology, comprehensive support and a vibrant ecosystem available to assist getting your product to market quickly. For automotive, consumer, industrial and networking applications, learn how NXP extends the broad technology and support available today with custom access to experts. A brief overview of the products and services available across NXP will be augmented with case studies and expert Q&A.
View full article
In designing cooking appliances, there is ample consideration given to power required from a home's wired electrical system as well as the performance needed to maintain safety and operating temperatures. NXP's solid state RF cooking team has developed a portable food heating appliance using solid state RF energy which is capable of operating on battery power. This session will cover the key challenges and approaches to delivering energy to heat food in a portable, on-the-go appliance.
View full article
Learn how smart amplifier technology from NXP helps your small speakers reach their full potential to maximize user experience.
View full article
Sensors are key to differentiate your products in the market and add context awareness, tamper detection, a robust user interface and intelligent wake-up. This class will step through all the leading applications in the IoT and IMM markets and provide a demonstration of the Sensor Toolbox tools for your product.
View full article
Learn about the key benefits and target applications of the new K27/K28 MCUs with extra-large embedded memory and power-efficient dual-USB MCUs based on ARM® Cortex-M4® core.
View full article
In the last 10 years, Green Hills has observed carmaker and Tier 1 customers expand from the traditional segments of powertrain, airbags and braking ECUs into graphics-rich dashboards, open source operating sytems and the secure Connected Car. A leading requirement is ECU consolidation while keeping ASIL safety intact. This requires the run-time architecture to safety and securely run guest operating systems Linux or Android on the same single core (or across multiple cores as SMP) alongside safety or security-critical applications like instrument clusters, gateways, V2X and ADAS. Here, we'll take a closer look at the customer’s pain points and goals, and we’ll summarize various industry solutions, including the INTEGRITY Multivisor secure hypervisor.
View full article
In recent years, automotive cybersecurity has become a top priority for OEMs as several well publicized attacks on production vehicles stirred up public and government concern over both security and safety of connected vehicle systems. In this talk we will: Review major milestones and headlines related to automotive cybersecurity for 2016; Compare and contrast security techniques used in traditional IT infrastructure versus automotive computing systems; Examine where these traditional techniques fall short for automotive applications.
View full article
Introduction to NXP’s state-of-the-art 1-chip next generation software defined radio(SDR) system solution covering global radio reception standards (Mercury family).
View full article
Writing automotive software to process signal coming from radar frontends is not an easy job. NXP’s radarSDK helps removing complexity by providing a complete API to access hardware engines inside the SoC together with a library consisting of optimized signal processing kernels that execute on the SPT accelerator. This session introduces the audience into the programming mode of radarSDK.
View full article
As the US Government prepares to mandate Car-to-Car communication in the US, the car industry is gearing up to provide cars which support this Dedicated Short Range Communications technology. We look at what benefits this will bring to road users, how the ITS-G5 standard is being deployed around the globe, and the challenges faced by the car industry in bringing this to market, and NXP’s leadership role in this deployment.
View full article
In Automotive, the need for communication between various ECUs has grown as the number of ECU’s have grown as well. Implementing a software solution which is scalable, portable, open and easy to program is key to offering a complete software enablement to our customers. This session will present our software solution for communication between multiple SOCs with different operating systems across  multiple physical areas.
View full article
This presentation dedicated to IVI provides an overview of the software and hardware enablement available to accelerate customer time-to-market and reduce development risks. Namely i.MX 8, Ethernet Switch and PHY, audio tuner and amplifier, power management, supported by a Linux Genivi compliant BSP.
View full article
This session will provide an overview of NXP’s automotive MCUs and MPUs portfolio. It will describe the roadmaps of the most recent solutions addressing ADAS, gateway, body electronics, safety and security applications.
View full article
Automotive Ethernet PHYs enable future driving scenarios by providing the necessary physical throughput power. While software brings added value for security, diagnosis, energy efficiency and safety. As the functional requirements for automotive PHY drivers differ from general purpose applications, additional functionality is needed to closely monitor and diagnose the device and to create advanced use cases like Layer-1 wake-up and sleep. In this session, these specific requirements for automotive Ethernet PHY SW are discussed. Existing PHY SW frameworks such as Linux or AUTOSAR are introduced and compared. Finally, the session will touch upon typical application scenarios which require interaction with PHY SW. This includes use cases like gPTP time synchronization and 802.1X Port-based Network Access Control (PNAC).
View full article