i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
The purpose of this document is to provide extended guidance for the selection of compatible LPDDR4/4X memory devices that are supported by the i.MX 93 series of processors. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs. The i.MX 93 series of processors supports different packages, and each have their own maximum supported LPDDR4/4x data rates. Please refer to the respective datasheets. Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. NOTE: Some of the LPDDR4/4X devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low-speed operation is planned in the use case, please consult with the memory vendor about the configuration aspects and possible customization of the memory device so correct functionality is ensured. LPDDR4/4X - Maximum Supported Densities SoC Max Data bus width Maximum density Assumed memory organization Notes i.MX 93 (i.MX 93xx) 16-bit 16 Gb / (2 GB) single rank, single channel device with 17-row addresses (R0 - R16) 1, 2, 3   LPDDR4/4X - List of Validated Memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part# Notes i.MX 93 16 Gb/ (2 GB) Micron LPDDR4/4x: MT53E1G16D1FW-046 AAT:A  (Z32N) MT53E1G16D1ZW-046 AAT:C (Z42N) 7   4, 8 8 Gb/ (1 GB) Micron LPDDR4/4x: MT53D512M16D1DS-046 AAT (Z11M) 4, 10 16 Gb/ (2 GB) Micron LPDDR4/4x: MT53E1G32D2FW-046 AUT:B (Z42M) 4, 5, 10 8 Gb/ (1 GB) Nanya LPDDR4: NT6AN512M16AV-J1I LPDDR4x: NT6AP512M16BV-J1I 4, 8 4 Gb/ (512 MB) Nanya LPDDR4x: NT6AP256M16AV  4, 8 16 Gb/ (2 GB) Kingston LPDDR4: D1611PM3BDGUI-U 4, 8 16 Gb/ (2 GB) Kingston LPDDR4: C1612PC2WDGTKR-U  7, 9 4 Gb/ (512 MB) ISSI LPDDR4: IS43LQ16256B-062BLI 4, 8 2Gb / (256 MB) ISSI LPDDR4: IS43LQ16128A-062BSLI 4, 6, 8   8 Gb/ (1 GB) CXMT LPDDR4/4x: CXDB4CBAM-EA-M 4, 9 16 Gb/ (2 GB) JSC LPDDR4x: JSL4BAG167ZAMF  4, 8 8 Gb/ (1 GB) JSC LPDDR4x: JSL4B8G168ZAMF-05x  4, 8 4 Gb/ (512 MB) JSC LPDDR4x: JSL4A4G168ZAMF-05 4, 8 2Gb / (256 MB) Winbond  LPDDR4x: W66BQ6NBHAGJ 4, 6, 8 8Gb / (1 GB) IM (Intelligent Memory) LPDDR4x: IM8G16L4JCB-046I 4, 11 16Gb / (2 GB) IM (Intelligent Memory) LPDDR4/4x: IMAG16L4KBBG 4, 8 4Gb / (512 MB) Samsung LPDDR4: K4F4E164HD-THCL 4, 8 8 Gb / (1 GB) AM (Alliance Memory) LPDDR4X: AS4C512M16MD4V-053BIN 4, 8 4 Gb / (512 MB) ISSI LPDDR4/4X: IS43LQ16256B-053BLI 4, 8 8 Gb / (1 GB) ISSI LPDDR4/4X: IS46LQ16512B-046BLA2 4, 8 32 Gb / (4GB) 16 Gb / (2Gb) usable by i.MX93 ISSI LPDDR4/4X: IS46LQ32K01B-046BLI 4, 8   Note 1: The numbers are based purely on the IP documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, SoC reference manual and on the JEDEC standards JESD209-4B/JESD209-4-1 (LPDDR4/4X). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4/4X devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The SoC also supports dual rank single channel devices therefore, 16Gb/2GB density can be also achieved by using a dual rank single channel device with 16-row addresses (R0 - R15). Note 4: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 5: This is a dual channel x32 device. Since i.MX93 only supports 16-bit LPDDR4/X data bus, it can only interface with one of the channels and therefore, utilize only half of the device's density. As indicated in the table - the device has 32Gb/4GB density however, only 16Gb/2GB can be used. There is no functional problem with using only one channel of a dual channel device as the channels are independent in LPDDR4/4X.  Note 6: This is a new JEDEC 100 ball package, half the size of the standard 200 ball package. This 100 ball package has the same performance and functionality as the 200 ball package, and has the added advantage of being smaller and cheaper than the standard package. Note 7: This device has been EoLed by the manufacturer and has been updated by a new memory part number  Note 8: Part is active. Reviewed Nov 2025 Note 9: Part is obsolete. Note 10: This device will be EoLed in Q2 24 by the manufacturer and will not be updated by a new memory part number Note 11: DQ eye marginalities were identified during TSA analysis. vTSA and stability testing did not identify any issues.
View full article
The purpose of this document is to provide extended guidance for selection of compatible LPDDR5 and LPDDR4x memory devices that are supported by the i.MX 95 and i.MX 952 processors. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs. Please note that some of the LPDDR4x devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low speed operation is planned in the use case, please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured. LPDDR5 - maximum supported densities SoC Max Data bus width Maximum density Assumed memory organization Notes i.MX 95 32-bit 128Gb/16GB dual rank, dual channel device with 17-row addresses and x8 (byte mode) organization 1, 3, 7 i.MX 952 32-bit 128Gb/16GB dual rank, dual channel device with 17-row addresses and x8 (byte mode) organization 1, 3, 7, 9   LPDDR5 - list of validated memories Note: The memory vendors often list their devices as LPDDR5x in their high-level product information while in fact, they are in most cases backward compatible with the LPDDR5 mode. This may lead to the false impression that there are not so many LPDDR5 devices on the market. In such cases, it is strongly recommended to check the full datasheet to confirm if the device is in fact LPDDR5/LPDDR5x or LPDDR5x only. The SoC cannot be used with devices that only support the LPDDR5X mode. The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor  Validated Memory Part#  Notes i.MX 95 128Gb/16GB Micron MT62F4G32D8DV-023 FAAT:C - 64Gb/8GB  Samsung K3KL9L90QM-MHCT - 32Gb/4GB  Samsung K3KL8L80QM-MHCT 2 32Gb/4GB  Samsung K3KL8L80EM-MUCV 2        64Gb/8GB  SK HYNIX H58G66DK9VX067N 2 64Gb/8GB Micron MT62F2G32D4DS-023 FAAT:C 2, 6 32Gb/4GB Micron MT62F1G32D2DS-020 WT:D 2 16Gb/2GB Micron MT62F1G16D1DS-023 IT:B 2 64Gb / 8GB Rayson RS2G32LO5D24DB-31BT 2 64Gb / 8GB CXMT CXDB6CCBM-MA-A 2 i.MX 952 128Gb/16GB Micron MT62F4G32D8DV-023 FAAT:C 9 32Gb/4GB Micron MT62F1G32D2DS-020 WT:D 2   LPDDR5 - list of incompatible devices The SoC cannot be used with memory devices that only support the LPDDR5x mode. LPDDR4x - maximum supported densities SoC Max Data bus width Maximum density Assumed memory organization Notes i.MX 95 32-bit 128Gb/16GB dual rank, dual channel device with 17-row addresses 1 i.MX 952 32-bit 128Gb/16GB dual rank, dual channel device with 17-row addresses 1, 9   LPDDR4x - list of validated memories   The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part# Notes i.MX 95 64Gb/8GB Micron   MT53E2G32D4DE-046 AUT:C  5 8Gb/1GB Micron MT53E256M32D1KS-046 IT:L 2 128Gb/16GB Micron MT53E4G32D8GS-046 2 64Gb/8GB SK Hynix H54G66BYYVPX104 2 32Gb/4GB Intelligent Memory IMBG32L4KBB_V10 2 48Gb/6GB Micron MT53E1536M32D4DT-046 WT:A 3, 8 24Gb/3GB Micron MT53E768M32D4DT-053 AIT:E 3, 8 8Gb/1GB Samsung K4U8E3S4ADGHCL  2 32Gb/4GB Intelligent Memory IMBG32LK4BBG-046I 2 32Gb/4GB Alliance Memory AS4C1G32MD4V-046BIN 2 64Gb/8GB Rayson ATL4X8G32M2D-46IT 2 64Gb/8GB Rayson ATL4X8G32M2D-46AIT 2 64Gb/8GB DW DWCTB36HLC0 2 i.MX 952 64Gb/8GB Micron   MT53E2G32D4DE-046 AUT:C  9   LPDDR4/4X - list of incompatible devices Note: This SoC supports LPDDR4x memory devices. This SoC is not compatible with memories that only support LPDDR4. Combo Devices that support both LPDDR4x and LPDDR4 are compatible with the SoC. Note 1: The numbers are based purely on the IP documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, SoC reference manual and on the JEDEC standards JESD209-5 (LPDDR5) and JESD209-4C/JESD209-4-1 (LPDDR4/4X). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 3: Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. Note 4: All memory parts are available at vendors unless stated otherwise. Checked Q2 2026 Note 5: Memory device supports both LPDDR4x and LPDDR4, however can only be used in LPDDR4x mode Note 6: Not validated by NXP but confirmed working on a non NXP Board Note 7: The maximum density supported may change in the future when DRAM vendors make higher density options available Note 8: This DRAM part number is not recommended for new designs Note 9: This SoC is in Pre-Production
View full article
This article describe some bring up tips during i.MX95 board debug, including HW and SW aspects.  
View full article
The purpose of this page is to provide supportive information for the selection of suitable camera modules that are supported by the i.MX95. The guide is attached in this page. This helps customers evaluate project feasibility and integration aspects when considering i.MX95 SoCs for their products. It is strongly recommended to consult with NXP and the camera module vendor before finalizing the choice of the camera part number to ensure compatibility, availability, longevity, and pricing requirements.   NXP Supported Sensors: Sensor Vendor Image Sensor Max Resolution Camera Module OmniVision OS08A20 8MP IMX95-OS08A20 | NXP Semiconductors EXPI-OS08A20 OmniVision OX05B1S 5MP   OmniVision OX03C10 3MP   Onsemi AR0144 1MP AR0144   Partner Enabled Sensors: Partner Sensor Vendor Image Sensor Max Resolution ISP Tuning Camera Module Location FRAMOS Sony IMX662 2MP ✔ FSM:GO Munich, Germany/ Canada/USA Sony IMX678 8MP Sony IMX900 3.2MP Sony IMX676 12MP Onsemi Onsemi AR2020 19MP   Module available through Future Electronics   Entron OmniVision OS08A20 8MP ✔ EXPI-OS08A20 China Onsemi AR0820 8MP Order with Entron Onsemi AR0823 8MP Technexion Onsemi AR0144 1MP       Onsemi AR0145 1MP     Onsemi AR0234 2MP     Onsemi AR0235 2MP     Onsemi AR0236 2MP     Onsemi AR0521 5MP     Onsemi AR0522 5MP     Onsemi AR0544 5MP     Onsemi AR0821 8MP       Onsemi AR0822 8MP     Onsemi AR0830 8MP     Onsemi AR1335 13MP     PHYTEC Onsemi AR0144 1MP     Germany/ China/India/ USA Onsemi AR0234 2.3MP   Onsemi AR0521 5MP   E-consystems Sony IMX662 2.4MP     Riverside, CA, USA/India Sony IMX900 3.2MP    
View full article
The purpose of this document is to specify the maximum LPDDR3, LPDDR4, & LPDDR4X densities that are supported by i.MX 8ULP processor along with a running list of tested memories to aid project feasibility assessment capabilities of customers that are evaluating the SoCs for usage in their products.  It is strongly recommended to consult with NXP and the memory vendor the final choice of the memory part number to ensure that the device meets all the compatibility, availability, longevity and pricing requirements. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs. For any questions related to specific DRAM part numbers please contact the respective DRAM vendor. For any questions regarding the i.MX SoC please contact your support representative or enter a support ticket.  LPDDR4/LPDDR4X Maximum Support Density Please note that the SoC limits the addressable DDR memory map range to 2GB. SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8ULP 32-bit 16Gb/2GB single-rank, dual-channel  device with 16-row addresses (R0-R15) 1, 2, 6,11   LPDDR4 - list of validated memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part#  Notes i.MX 8ULP 16Gb/2GB Micron MT53D512M32D2DS-053 WT:D  10 16Gb/2GB Micron MT53E512M32D1ZW-046 WT:B  8 64Gb/8GB Micron MT53E2G32D4DE-046 WT:A  3, 4, 8 32Gb/4GB Micron MT53E1G32D2FW-046 AUT:B  3, 4, 10 16Gb/2GB Nanya NT6AN512T32AV-J2 3, 7, 8 8Gb/1GB Forsee FL4C2001G-D9  3, 10   LPDDR4x - list of validated memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Mamory Vendor Validated Memory Part# Notes i.MX 8ULP 16Gb/ 2GB Nanya NT6AP512T32AV-J2  3, 7, 8 2Gb/ 256MB Fidelix FMF2D32VAC-4CDIR 3 4Gb/ 512MB Winbond W66CQ2NQUAFJ  3, 8 8Gb/1GB Alliance Memory AS4C256M32MD4V-062BAN  3, 8 32Gb/4GB Micron MT53E1G32D2FW-046 AUT:B (Z42M) 3, 4, 10 16Gb/ 2GB Micron MT53D512M32D2DS-053 WT:D  10 16Gb/ 2GB Micron MT53E512M32D1ZW-046 WT:B  9   LPDDR3 Maximum Support Density Please note that the SoC limits the addressable DDR memory map range to 2GB. SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8ULP 32-bit 16Gb/2GB Single Channel, Dual Chip Select 5,11   LPDDR3 - list of validated memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part#  Notes i.MX 8ULP 16Gb/2GB Micron  MT52L512M32D2PF-107 WT:B  8   Note 1: The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC and on the memory device used on NXP evaluation boards, and on the JEDEC standards JESD209-4/JESD209-4B (LPDDR4/4X). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 4: As the i.MX 8ULP DDR memory map is limited to 2GB, only up to 2GB of the device can be utilized even though the device density exceeds the 2GB range. Note 5: The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC and on the memory device used on NXP evaluation boards, and on the JEDEC standards JESD209-3C (LPDDR3). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk.  Note 6: The SoC supports also LPDDR4/4X devices with 17-row address bits however, given the SoC's memory map constraints (see Note 4), full density of those devices cannot be utilized since the dual channel (x32) 17-row address memory devices have the density of 4GB and higher. Note 7: By default, LPDDR4/4X devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity. Please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured. Note 8: Part is active. Reviewed Jan 2026 Note 9: Part is active as MT53E512M32D1ZW-046BWT:B.  Note 10: Part is obsolete. Note 11: i.MX 8ULP does not support Non-Power of 2 Memory densities (e.g. 3,6,12 Gb).
View full article
The purpose of this document is to provide supportive information for selection of suitable LPDDR4, DDR4 and DDR3L devices that are supported by i.MX 8M family of processors to aid project feasibility assessment capabilities of customers that are evaluating the SoCs for usage in their products.  It is strongly recommended to consult with NXP and the memory vendor the final choice of the memory part number to ensure that the device meets all the compatibility, availability, longevity and pricing requirements. Please note that some of the LPDDR4 devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low speed operation is planned in the use case, please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs available on NXP.com Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. For any questions related to specific DRAM part numbers please contact the respective DRAM vendor. For any questions regarding the i.MX SoC please contact your support representative or enter a support ticket.  LPDDR4 - maximum supported densities Please note that the SoCs only support memory devices that support either the LPDDR4 mode or support both LPDDR4 and LPDDR4X modes. Memory devices that support only the LPDDR4X mode are not supported. SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8M Quad 32-bit 32Gb/4GB dual rank, dual-channel  device with 16-row addresses (R0-R15) 1, 2, 4 i.MX 8M Mini  32-bit 64Gb/8GB dual rank, dual-channel  device with 17-row addresses (R0-R16) 1, 2 i.MX 8M Nano  16-bit 32Gb/4GB dual rank, single-channel  device with 17-row addresses (R0-R16) 1, 2, 3, 12 i.MX 8M Plus  32-bit 64Gb/8GB dual rank, dual-channel  device with 17-row addresses (R0-R16)  1, 2   LPDDR4 - list of validated memories Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required. SoC Density Memory Vendor Validated Memory Part#  Notes i.MX 8M Quad  24Gb/3GB    Micron MT53B768M32D4NQ-062 WT:B  15 32Gb/4GB Micron MT53D1024M32D4DT-046 AAT:D  14 4Gb/512MB ISSI IS43LQ16256B-062BLI  5, 14 8Gb/1GB ISSI IS43LQ32256B-062BLI  5, 14 i.MX 8M Mini 16Gb/2GB Micron MT53D512M32D2DS-053 WT:D  15 16Gb/2GB    ESMT M56Z16G32512A-SMBIG 5, 14 32Gb/4GB Micron MT53E1G32D2FW-046 WT:A  5, 14 64Gb/8GB Micron MT53E2G32D4DT-046 AIT:A  5, 14 64Gb/8GB Micron MT53E2G32D4DE-046 AUT:C 5, 14 32Gb/4GB Intelligent Memory IMBG32L4KBB 5,14 32Gb/4GB Kingston B3221PM3BDGUI -U 5 i.MX 8M Nano  16Gb / 2GB  Kingston C1612PC2WDGTKR-U  15 16Gb / 2GB  Kingston  D1611PM3BDGUI-U 5,14 32Gb / 4GB Micron MT53E2G32D4DT-046 AIT:A  5, 13, 15 16Gb / 2GB Intelligent Memory  IMAG16L4KBB 5,14 4Gb / 512MB Nanya NT6AN256M16AV-J2 5,14 4Gb / 512MB  Winbond W66CP6RBQAHJ 5,14 8Gb / 1GB ISSI IS43LQ16512A-053BLI 5,14 8Gb / 1GB  Micron MT53D512M32D2DS-053 WT:D 13, 15   i.MX 8M Plus   48Gb/6GB  Micron MT53E1536M32D4DT-046 WT:A  15 64Gb/8GB  Micron MT53E2G32D4DE-046 AUT:C  5, 14 32Gb/4GB Samsung K4FBE3D4HB-KHCL  5, 14 32Gb/4GB Kingston B3221PM3BDGVIW-U 5, 14 64Gb/8GB Kingston Q6422PM3BDGVK-U  5, 14 8Gb/1GB Winbond W66DP2RQQAHJ  5, 14 32Gb/4GB ISSI IS46LQ32K01S2A-046BLA2 5, 14 16Gb/2GB ISSI IS46LQ32512A-046BLA3 5 32Gb/4GB ISSI IS43LQ32K01S2A-046BLI 5, 14 32Gb/4GB IM IMBG32LK4BBG-046I 5, 14   LPDDR4 - list of incompatible devices Given the limitations mentioned in this document, the following memory devices were identified as incompatible with the particular SoCs as detailed in the following table:   Memory Vendor Memory Part# Density Incompatible SoCs Incompatibility reason Samsung K4FHE3S4HA-KU(H/F)CL 24Gb/3Gb i.MX 8M Quad  The memory device requires 17th row address bit to function. Samsung K4UHE3S4AA-KU(H/F)CL K4UJE3D4AA-KU(H/F)CL 24Gb/3Gb 48Gb/6GB i.MX 8M Quad i.MX 8M Mini i.MX 8M Nano i.MX 8M Plus The memory device only supports the LPDDR4X mode. Samsung K4FCE3Q4HB-KU(H/F)CL K4UCE3Q4AB-KU(H/F)CL 64Gb/8GB i.MX 8M Quad i.MX 8M Mini i.MX 8M Nano i.MX 8M Plus A byte mode memory device. The memory device only supports the LPDDR4X mode.    DDR4 - maximum supported densities SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8M Quad  32-bit 32Gb/4GB x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses 1, 6 i.MX 8M Mini  32-bit 64Gb/8GB x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses 1, 7 i.MX 8M Nano  16-bit 64Gb/8GB x8, 16Gb device with 2 bank group addresses, 17-row addresses and 10 column addresses 1, 8 i.MX 8M Plus  32-bit 64Gb/8GB x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses 1, 7   DDR4 - list of validated memories Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required.   SoC Density Memory Vendor Validated Memory Part#  Notes i.MX 8M Quad 32Gb/4GB Micron 4x MT40A512M16JY-083EAAT  15 i.MX 8M Mini  16Gb/2GB Micron 2x MT40A512M16LY-075:E  15 i.MX 8M Nano 16Gb/2GB Micron 1x MT40A1G16RC-062E:B  15 8Gb/1GB Rayson 1x RS512M16Z2DD-62DT 14 8Gb/1GB UniIC SCB12Q8G160BF-06SI 14 i.MX 8M Plus 64Gb/8GB Micron 4x MT40A1G16RC-062E:B  15 16Gb/2GB Nanya NT5AD512M16C4-JRI  14   DDR3L - maximum supported densities SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8M Quad  32-bit 32Gb/4GB x16, 8Gb device with 16-row addresses and 10 column addresses 1, 9 i.MX 8M Mini  32-bit 64Gb/8GB x8, 8Gb device with 16-row addresses and 11 column addresses 1, 10 i.MX 8M Nano  16-bit 32Gb/4GB x8, 8Gb device with 16-row addresses and 11 column addresses 1, 11 i.MX 8M Plus  i.MX 8M Plus does not support DDR3L   DDR3L - list of validated memories Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required. SoC Density Vendor Validated Memory Part#  Notes i.MX 8M Quad  16Gb/2GB Micron 4x MT41K256M16TW-107 AAT  14 i.MX 8M Mini  16Gb/2GB Micron 4x MT41K256M16TW-107 AAT  14              i.MX 8M Nano 8Gb/1GB Micron MT41K512M16VRN-107  15   Note 1: The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, and on the JEDEC standards JESD209-4/JESD209-4A (LPDDR4), JESD279-4/JESD279-4A (DDR4), and JESD79-3E/JESD79-3F/JESD79-3-1A (DDR3/DDR3L). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The memory vendors often do not offer so many variants of single-channel memory devices. As an alternative, a dual-channel device with only one channel connected may be used. For example: A dual-rank, single-channel device with 16-row address bits has a density of 16Gb. If such a device is not available at the chosen supplier, a dual-rank, dual-channel device with 16-row address bits can be used instead. This device has a density of 32 Gb however since only one channel can be connected to the SoC, only half of the density is available (16 Gb). Usage of more than one discrete memory chips to overcome market constraints is not supported since only point-to-point connections are assumed for LPDDR4. Note 4: Devices with 17-row addresses (R0-R16) are not supported by the DDR Controller Note 5: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 6: The density can be achieved by connecting 2 single-rank discrete devices with one 16Gb die each. Since the SoC supports x8 devices and also has connectivity for a second rank, usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 32Gb/4GB of address space dedicated for the DDR. Two x16 16Gb devices giving 32Gb/4GB in total is, therefore, the optimal choice that balances the maximum density aspects, the signal integrity aspects (only two discrete devices used), and bandwidth aspects (full data bus width used). Note 7: The density can be achieved by connecting 4 single rank discrete devices with one 16Gb die each, 2 devices connected to each chip select. Since the SoC supports x8 devices, the usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 64Gb/8GB of address space dedicated for the DDR. Four x16 16Gb devices giving 64Gb/8GB in total is the optimal choice that balances the maximum density aspects, the signal integrity aspects (only four discrete devices used), and the bandwidth aspects (full data bus width used). Note 8: The density can be achieved by connecting 4 single rank discrete devices with one 16Gb die each, 2 devices connected to each chip select.  Note 9: The density can be achieved by connecting 4 single rank discrete devices with one 8Gb die each, 2 devices connected to each chip select, or by connecting 2 dual rank discrete devices with two 8Gb dies each. Since the SoC supports x8 devices, the usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 32Gb/4GB of address space dedicated for the DDR. Four x16 8Gb devices giving 32Gb/4GB in total is, therefore, the optimal choice that balances the maximum density aspects, the signal integrity aspects (four discrete devices used), and bandwidth aspects (full data bus width used). Note 10: The density can be achieved by connecting 8 single rank discrete devices with one 8Gb die each, 4 devices connected to each chip select or by connecting 4 dual rank discrete devices with two 8Gb dies each. Note that the first option significantly exceeds the number of devices used on the validation board (4 discrete devices) therefore, it is not guaranteed that the i.MX would be able to drive the signals with margin to the required voltage levels due to increased loading on the traces. A significant effort would be required in terms of PCB layout and signal integrity analysis. Practically, it is not recommended to use more than 4 discrete DDR3L devices. This corresponds to the maximum density of 32Gb/4GB in the case of the single rank devices containing one 8Gb die or 64Gb/8GB in case of the dual-rank devices, each containing two 8Gb dies. Note 11: The density can be achieved by connecting 4 single rank discrete devices with one 8Gb die each, 2 devices connected to each chip select or by connecting 2 dual rank discrete devices with two 8Gb dies each. Note 12: For single-channel (x16) memory devices, the current maximum available density in the market is 16Gb/2GB (Q1 2022). Note 13: Only one channel of the device (and hence, half of its density) was utilized due to the reduced data bus width (x16) of the SoC. Note 14: Part is active. Reviewed Jan 2026 Note 15: Part will either EoL or is not recommended for new designs by the respective vendor.   Additional Links https://community.nxp.com/t5/iMX-and-Vybrid-Support/i-MX-8-8X-8XL-maximum-supported-LPDDR4-and-DDR3L-densities/ta-p/1152715           
View full article
The purpose of this document is to provide supportive information for selection of suitable LPDDR4 and DDR3L devices that are supported by i.MX 8/8X/8XLite family of processors to aid project feasibility assessment capabilities of customers that are evaluating the SoCs for usage in their products.  It is strongly recommended to consult with NXP and the respective memory vendor, the final choice of the memory part number to ensure that the device meets all the compatibility, availability, longevity and pricing requirements. Please note that some of the LPDDR4 devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low speed operation is planned in the use case, please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the respective NXP i.MX 8 Hardware Developer's Guide available on NXP.com The i.MX8/8X/8XL Reference manuals declare that there are 16GB allocated for the DDR. Please note that this is only the address space, which is reserved for the DDR memory in the memory map. This specification does not guarantee that the entire region can be utilized as the maximum achievable densities listed below in the tables are restricted mainly by the addressing capabilities of the DDR controller, width of the data bus and other implementation-specific parameters as well as availability of supported devices on the market. Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. For any questions related to specific DRAM part numbers please contact the respective DRAM vendor. For any questions regarding the i.MX SoC please contact your support representative or enter a support ticket.  LPDDR4 - maximum supported densities Please note that the SoCs only support memory devices that support either the LPDDR4 mode or support both LPDDR4 and LPDDR4X modes. Memory devices that support only the LPDDR4X mode are not supported. SoC Package Max data bus width Maximum density Assumed memory organization Notes i.MX 8QM/8QP 29x29 mm 32-bit (per controller) 32Gb/4GB (per controller) dual rank, dual-channel  device with 16-row addresses (R0-R15) 1, 2, 4 i.MX 8QXP/8DXP 21x21 mm 32-bit 32Gb/4GB dual rank, dual-channel  device with 16-row addresses (R0-R15) 1, 2, 4 i.MX 8QXP/8DXP 17x17 mm 16-bit 16Gb/2GB dual rank, single-channel  device with 16-row addresses (R0-R15) 1, 2, 3, 4, 9 i.MX 8XLite 15x15 mm 16-bit 32Gb/4GB dual rank, single channel  device with 17-row addresses (R0-R16) 1, 2, 3, 9   LPDDR4 - list of validated memories The validation process is an ongoing effort - updates of the table are expected. SoC Density Memory Vendor Validated Memory Part# Notes i.MX 8QM/8QP 24Gb/3GB (per controller) Micron MT53B768M32D4NQ-062 AIT:B   12, 13 32Gb/4GB (per controller)  Samsung K4FBE3D4HB-KHCL  10, 11 32Gb/4GB (per controller) Micron MT53E1G32D2FW-046 AUT:B (Z42M) 10, 11 32Gb/4GB (per controller) Micron MT53D1024M32D4DT-046 AAT:D   12 16Gb/2GB (per controller) Micron MT53D512M32D2DS-046 WT:D  10, 12 16Gb/2GB (per controller) Nanya NT6AN512T32AC-J1J  10, 11 16Gb/2GB (per controller) Nanya NT6AN512T32AC-J1H  10, 11 32Gb/4GB (per controller) Nanya NT6AN1024F32AC-J2J  10, 11 32Gb/4GB (per controller) Nanya NT6AN1024F32AC-J2H  10, 11 i.MX 8QXP/8DXP 24Gb/3GB Micron MT53B768M32D4NQ-062 AIT:B   12, 13 32Gb/4GB Nanya NT6AN1024F32AC-J2J  10, 11 32Gb/4GB Nanya NT6AN1024F32AC-J2H  10, 11 16Gb/2GB Nanya NT6AN512T32AC-J2J  10, 11 16Gb/2GB Nanya NT6AN512T32AC-J2H  10, 11 32Gb/4GB Micron MT53D1024M32D4DT-046 AAT:D   11 i.MX 8XLite 8Gb/1GB Micron MT53D512M16D1DS 046 AAT ES:D & Z9XGG   12 12Gb/1.5GB Micron MT53E768M16D1ZW-046 AAT:C 10, 11, 13 4Gb/0.5GB Samsung K4F4E164HD-THCL  10, 11 8Gb/1GB ISSI IS43LQ16512A-053BLI 10, 11 8Gb/1GB Nanya NT6AN512M16AV-J1I  10, 11   LPDDR4 - list of incompatible devices Given the limitations mentioned in this document, the following memory devices were identified as incompatible with the particular SoCs as detailed in the following table:   Memory vendor Part Number Density Incompatible SoCs Incompatibility reason Samsung K4FHE3S4HA-KU(H/F)CL 24Gb/3Gb i.MX8QM/8QP, i.MX8QXP/8DXP The memory device requires 17th row address bit to function. Samsung K4UHE3S4AA-KU(H/F)CL 24Gb/3Gb i.MX8QM/QP, i.MX8QXP/8DXP, i.MX8DXL, i.MX8SXL The memory device only supports the LPDDR4X mode. Samsung K4UJE3D4AA-KU(H/F)CL 48Gb/6GB i.MX8QM/QP, i.MX8QXP/8DXP, i.MX8DXL, i.MX8SXL The memory device only supports the LPDDR4X mode. Samsung K4FCE3Q4HB-KU(H/F)CL 64Gb/8GB i.MX8QM/QP, i.MX8QXP/8DXP, i.MX8DXL, i.MX8SXL A byte mode memory device. Samsung K4UCE3Q4AB-KU(H/F)CL 64Gb/8GB i.MX8QM/QP, i.MX8QXP/8DXP, i.MX8DXL, i.MX8SXL A byte mode memory device. The device only supports the LPDDR4X mode.    DDR3L - maximum supported densities SoC Package Max data bus width Maximum density Assumed memory organization Notes i.MX 8QXP/8DXP 21x21 mm 32-bit 64Gb/8GB x8, 8Gb device with 16-row addresses and 11 column addresses 5, 6 i.MX 8QXP/8DXP 17x17 mm 16-bit 32Gb/4GB x8, 8Gb device with 16-row addresses and 11 column addresses 5, 7 i.MX 8XLite 15x15 mm 16-bit 16Gb/2GB x8, 8Gb device with 16-row addresses and 11 column addresses 5, 8   DDR3L - list of validated memories The validation process is an ongoing effort -  updates of the table are expected. SoC Density Memory Vendor Validated Mamory Part#  Notes i.MX 8QXP/8DXP 8Gb/1GB Micron 2x MT41K256M16TW-093 IT:P 12 i.MX 8XLite 4Gb/512MB Micron MT41K256M16TW-093 IT:P 12   Note 1: The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, and on the JEDEC standard JESD209-4A. Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that a DRAM with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The memory vendors often do not offer so many variants of single-channel memory devices. As an alternative, a dual-channel device with only one channel connected may be used. For example: A dual-rank, single-channel device with 16-row address bits has a density of 16Gb. If such a device is not available at the chosen supplier, a dual-rank, dual-channel device with 16-row address bits can be used instead. This device has a density of 32 Gb however since only one channel can be connected to the SoC, only half of the density is available (16 Gb). Usage of more than one discrete memory chip to overcome market constraints is not supported since only point-to-point connections are assumed for LPDDR4. Note 4: Devices with 17-row addresses (R0-R16) are not supported by the SoCs.  Note 5: The numbers are based purely on the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, and on the JEDEC standard JESD79-3E/JESD79-3F. Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that a DRAM with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 6: The density can be achieved by connecting 8 single rank discrete devices with one 8Gb die each, 4 devices connected to each chip select, or by connecting 4 dual rank discrete devices with two 8Gb dies each. Note that this number of discrete devices significantly exceeds the number of devices used on the validation board (2 discrete devices, not taking into account the device used for ECC) therefore, it is not guaranteed that the i.MX would be able to drive the signals with margin to the required voltage levels due to increased loading on the traces. A significant effort would be required in terms of PCB layout and signal integrity analysis hence practically, it is not recommended to use more than 2 discrete DDR3L devices. This corresponds to the maximum density of 16Gb/2GB in the case of the single rank devices containing one 8Gb die or 32Gb/4GB in the case of the dual-rank devices containing two 8Gb dies (x16 8Gb devices with 16-row addresses and 10 column addresses assumed instead of x8 devices in such case). Note 7: The density can be achieved by connecting 4 single rank discrete devices with one 8Gb die each, 2 devices connected to each chip select, or by connecting 2 dual rank discrete devices with two 8Gb dies each. Note that the first option exceeds the number of devices used on the validation board (2 discrete devices) therefore, it is not guaranteed that the i.MX would be able to drive the signals with margin to the required voltage levels due to increased loading on the traces. A significant effort would be required in terms of PCB layout and signal integrity analysis, hence practically, it is not recommended to use more than 2 discrete DDR3L devices. This corresponds to the maximum density of 16Gb/2GB in the case of the single rank devices containing one 8Gb die or 32Gb/4GB in the case of the dual-rank devices containing two 8Gb dies. Note 8: The density can be achieved by connecting 2 single rank discrete devices with one 8Gb die each to the i.MX. 8XLite supports only one chip select for DDR3L therefore, dual-rank systems are not supported. Note 9: For single-channel (x16) memory devices, the current maximum available density in the market is 16Gb/2GB (2025). Note 10: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 11: Part is active. Reviewed Aug 2025 Note 12: Part is being End Of Life'd (EoL) by Vendor or obsolete. Note 13: Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. Additional Links i.MX 8M Quad/8M Mini/8M Nano/8M Plus - LPDDR4, DDR4 and DDR3L memory compatibility guide 
View full article
   Memory Compatibility Guides   Processor/Family Link to Guide i.MX 8/8X/8XLite DDR3L and LPDDR4 i.MX 8M Quad/8M Mini/8M Nano/8M Plus DDR3L, DDR4, LPDDR4 i.MX 8ULP  LPDDR3, LPDDR4 & LPDDR4x i.MX 93 LPDDR4/LPDDR4x i.MX 95 LPDDR5/LPDDR4x - New Other Processor Families Please contact NXP Support or Sales   Additional Resources i.MX Memory Fact Sheet DDR memory selection & enablement for i.MX platforms Smarter World Blog Building Resilient Embedded Systems: NXP’s Approach to DDR Memory Selection and Support DDR Configuration Tools DDR Configuration tool for i.MX  Developer Resources i.MX Developer Resources SW & Tools
View full article
This blog enables support of Qemu emulation for iMX8MM EVK.  Imagine not having the hardware but still you want to test the software. Qemu gives you exactly that. 1. Booting uboot, linux and user-space application even when you do not possess a real hardware. 2. Early firmware development when the silicon doesn’t yet exist. 3. Linux driver development, debugging and testing.
View full article
We are pleased to announce that Config Tools for i.MX 26.03 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) Version 26.03 System Manager Memory sector information for resources with memory configuration is added to the Resources overview. Support for memory sectors splitting. Memory configuration input for resources using MBC/MRC is improved. Support for macOS (aarch64 and x86_64) is added. Clocks Hierarchy for local configuration element settings is supported. TEE Multicore Interrupt Handling for Single Security Domain is supported. Option to filter only user-defined memory regions is added. Interrupts are now separated into groups based on the core.
View full article
This page serves as a hub to gather the links to all the currently available ISP supported camera lists for the i.MX Applications processors.  Camera Compatibility Guides Processor/Family Link to Guide i.MX8M PLUS i.MX8M Plus ISP Camera Compatibility Guide i.MX95 i.MX95 ISP Camera Compatibility Guide   Additional Resources i.MX Camera Software Pack AN AN14376: i.MX Camera Software Pack | NXP Semiconductors
View full article
The purpose of this page is to provide supportive information for the selection of suitable camera modules that are supported by the i.MX 8M Plus (i.MX8MP). The guide is attached in this page. This helps customers evaluate project feasibility and integration aspects when considering i.MX 8MP SoCs for their products. It is strongly recommended to consult with NXP and the camera module vendor before finalizing the choice of the camera part number to ensure compatibility, availability, longevity, and pricing requirements. NXP Supported Sensors: Sensor Vendor Image Sensor Max Resolution Camera Module OmniVision OS08A20 8MP IMX-OS08A20 EXPI-OS08A20 OmniVision OV2775 2MP   Sony IMX219 8MP   Sony IMX477 12.3MP   Onsemi AR0144 1MP AR0144 Onsemi AR1335 13MP     Partner Enabled Sensors:   Partner Sensor Vendor Image Sensor Max Resolution ISP Tuning Camera Module Location FRAMOS Sony IMX415 8MP ✔   Munich, Germany/ Canada/USA Sony IMX662 2MP FSM:GO Sony IMX678 8MP Sony IMX900 3.2MP Sony IMX676 12MP Innowave Onsemi AR1335 13MP ✔   Austin, Texas, USA/Israel Sony IMX258 13MP Camera Modules Sony IMX219 8MP OmniVision OV5645 5MP   OmniVision OV2710 2MP   Basler Onsemi AR0821 8MP   Basler   Onsemi AR0521 5MP   Onsemi Onsemi AR0830 8MP   Image Sensors, Module available through Future Electronics   Onsemi AR0544 5MP Onsemi AR0821 8MP Onsemi AR0822 8MP Onsemi AR0145 1MP Onsemi AR0235 2MP Onsemi AR1335 13MP PHYTEC Onsemi AR0144 1MP     Germany/ China/India/ USA Onsemi AR0234 2.3MP   Onsemi AR0521 5MP   E-consystems Sony IMX662 2.4MP     Riverside, CA, USA/India Sony IMX900 3.2MP   Onsemi AR0234 2.3MP   CIS Corporation Sony IMX715 12MP ✔   Japan Sony IMX570 0.32MP   Onsemi AR0234CS 2MP   Sony Sony IMX500 12MP     Japan HINO Engg Sony IMX415 8MP ✔   Japan Sony IMX662 2MP   Leopard Imaging Sony IMX500 12MP ✔   Fremont, CA, USA/China   Note: CIS Corporation and HINO Engg currently only support customers in Japan market.
View full article
Use Raspberry Pi Debug Probe with OpenOCD and i.MX93 FRDM   This document explains the integration process of the Raspberry Pi Debug Probe (Very low cost debugger) with the OpenOCD (On Chip Debugger) tool with the i.MX93 FRDM board.   Also, we will use GDB (GNU DeBugger) to interact with the OpenOCD.   1. Install and Configure OpenOCD   Update and install dependencies sudo apt update sudo apt install build-essential libtool automake pkg-config libusb-1.0-0-dev libhidapi-dev libftdi1-dev libjim-dev jimsh   Clone the OpenOCD repo git clone https://github.com/openocd-org/openocd.git cd openocd   Run ./bootstrap to create the configuration file git submodule update --init --recursive ./bootstrap ./configure --enable-cmsis-dap --enable-hidapi   Make OpenOCD make -j$(nproc) sudo make install   Download the configuration file for i.MX93 You can dowload the  imx93.cfg  in the Table 2. Software requirements on Ubuntu PC of the AN14367 Then, copy the downloaded file to the openocd/tcl/target/ as below: cp ../imx93_new-b42b7c4cac18508442d3df035cec1c6d.cfg tcl/target/imx93.cfg   2. Create UDEV rules   sudo nano /etc/udev/rules.d/99-openocd.rules Add the below in that file: ATTRS{idVendor}=="2e8a", ATTRS{idProduct}=="000c", MODE="660", GROUP="plugdev", TAG+="uaccess"   Reload rules sudo udevadm control --reload-rules && sudo udevadm trigger   3. Connecting the Hardware   To make the DAP works in the i.MX93 FRDM, we must rework the board removing the resistors R3017 and R3018:     Now, we need to connect the Raspberry Pi Debug Probe with the SWD (P14) of our i.MX93 FRDM board:       4. Running the Debug Session   In this moment, with the RP Debug Probe connected, we can Boot the i.MX93 FRDM board and run the below command to start the OpenOCD: $ openocd -s tcl -f interface/cmsis-dap.cfg -c "adapter speed 1000" -f target/imx93.cfg   tic-mpu@tic-mpu:~/Debug_test/openocd$ openocd -s tcl -f interface/cmsis-dap.cfg -c "adapter speed 1000" -f target/imx93.cfg Open On-Chip Debugger 0.12.0+dev-02429-ge4c49d860 (2026-03-21-23:05) Licensed under GNU GPL v2 For bug reports, read http://openocd.org/doc/doxygen/bugs.html adapter speed: 1000 kHz Warn : DEPRECATED: auto-selecting transport "swd". Use 'transport select swd' to suppress this message. Info : Listening on port 6666 for tcl connections Info : Listening on port 4444 for telnet connections Info : Using CMSIS-DAPv2 interface with VID:PID=0x2e8a:0x000c, serial=E6633861A33A1B2C Info : CMSIS-DAP: SWD supported Info : CMSIS-DAP: Atomic commands supported Info : CMSIS-DAP: Test domain timer supported Info : CMSIS-DAP: FW Version = 2.0.0 Info : CMSIS-DAP: Interface Initialised (SWD) Info : SWCLK/TCK = 0 SWDIO/TMS = 0 TDI = 0 TDO = 0 nTRST = 0 nRESET = 0 Info : CMSIS-DAP: Interface ready Info : clock speed 1000 kHz Info : SWD DPIDR 0x5ba02477 Info : imx93.a55.0: hardware has 6 breakpoints, 4 watchpoints Info : [imx93.a55.0] external reset detected Info : [imx93.a55.0] Examination succeed Info : [imx93.m33] Cortex-M33 r1p0 processor detected Info : [imx93.m33] target has 8 breakpoints, 4 watchpoints Info : [imx93.m33] Examination succeed Info : [imx93.ahb] Examination succeed Info : [imx93.a55.0] starting gdb server on 3333 Info : Listening on port 3333 for gdb connections Info : [imx93.m33] starting gdb server on 3334 Info : Listening on port 3334 for gdb connections Info : [imx93.ahb] gdb port disabled   From the Logs, we can see we have two ports: 3333 for Cortex A55 [imx93.a55.0] 3334 for Cortex M33 [imx93.m33]   Install gdb-multiarch   Now, we can install GDB: sudo apt install gdb-multiarch And start a Debug session: $ gdb-multiarch ~/linux-imx/vmlinux   $ gdb-multiarch ~/linux-development/linux-imx/vmlinux GNU gdb (Ubuntu 15.1-1ubuntu1~24.04.1) 15.1 Copyright (C) 2024 Free Software Foundation, Inc. License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html> This is free software: you are free to change and redistribute it. There is NO WARRANTY, to the extent permitted by law. Type "show copying" and "show warranty" for details. This GDB was configured as "x86_64-linux-gnu". Type "show configuration" for configuration details. For bug reporting instructions, please see: <https://www.gnu.org/software/gdb/bugs/>. Find the GDB manual and other documentation resources online at: <http://www.gnu.org/software/gdb/documentation/>. For help, type "help". Type "apropos word" to search for commands related to "word"... Reading symbols from /home/tic-mpu/linux-development/linux-imx/vmlinux... (gdb) target extended-remote localhost:3333 Remote debugging using localhost:3333 0x00000000fff118fc in ?? ()   A simple example of how to read a register with GDB: (gdb) x/xw 0x43810000 0x43810000: 0x02010001     Happy debugging!     Best regards, Salas. 
View full article
Tested in FRDM-i.MX91 Written in C LF-6.12.49
View full article
Updated for "phase 3" after a 3rd software lockup symptom found and fixed. Updated doc/patch: Software-lockup-issue-phase3_20260318-public.pdf 0001-clk-fix-sleeping-function-called-from-invalid-contex.patch 0001-ddr-perf-fix-sleeping-function-called-from-invalid-c.patch 0001-gpu-imx-dpu-Access-ExtDst-FetchUnit-Hscaler-Vscaler-new_L4.14.98.patch (this patch will depends on https://github.com/nxp-imx/linux-imx/commit/70744429841f08efc42a63380198cdae7f9a602f) --- 20260318   This is a summary for the software lockup issue found in the following platform: −i.MX8/8X −Linux 4.14.98_2.3.3   Issue description: •Issue happens during the boot procedure, at the systemd stage. •The symptom of the issue: −From user perspective, the symptom varies, but mainly fall into several types: §At the console, there may be login prompt, but no response (only echo) when input user/password. Unable to login. §Some user service in systemd failed to start. E.g. weston. −When checking the task status using sysrq (w/t), many tasks, including some kernel core tasks stays in “D” (uninterruptable sleep) state. E.g. agetty, login, chvt, etc. •Kernel itself is still alive. This can be verified by triggering some drivers, such as plugin a USB device. Issue can be reproduced on MEK through long time stress.   Please refer to the doc/patch attached for details.
View full article
There are currently no additional test programs in I.MX Jailhouse program. This demo shares how to test RM67199 MIPI panel in Jailhouse inmate.   Please refer run.sh in attachments. modprobe jailhouse insmod jailhouse_clk.ko # adjust pixel clock for MIPI PANEL RMP67199 echo 129937500 > /sys/bus/platform/devices/jailhouse_clk/rate_pix export PATH=$PATH:/usr/share/jailhouse/tools/ jailhouse enable /root/imx8mm.cell jailhouse cell linux /root/imx8mm-inmate-demo.cell /root/Image.bin -d /root/imx8mm-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc3,115200 earlycon=ec_imx6q,0x30890000,115200 root=/dev/mmcblk2p2 rootwait rw"  
View full article
There are currently no additional test programs in I.MX Jailhouse program. This demo shares how to test USB function in Jailhouse inmate. Inmate boot log: root@imx8mmevk:~# dmesg | grep usb [ 0.312280] usbcore: registered new interface driver usbfs [ 0.317206] usbcore: registered new interface driver hub [ 0.322279] usbcore: registered new device driver usb [ 0.911649] usbcore: registered new device driver r8152-cfgselector [ 0.917711] usbcore: registered new interface driver r8152 [ 0.994200] usbcore: registered new interface driver uas [ 0.999359] usbcore: registered new interface driver usb-storage [ 1.005192] usbcore: registered new interface driver usbserial_generic [ 1.011486] usbserial: USB Serial support registered for generic [ 1.017274] usbcore: registered new interface driver ftdi_sio [ 1.022813] usbserial: USB Serial support registered for FTDI USB Serial Device [ 1.029852] usbcore: registered new interface driver usb_serial_simple [ 1.036148] usbserial: USB Serial support registered for carelink [ 1.042016] usbserial: USB Serial support registered for flashloader [ 1.048144] usbserial: USB Serial support registered for funsoft [ 1.053931] usbserial: USB Serial support registered for google [ 1.059643] usbserial: USB Serial support registered for hp4x [ 1.065185] usbserial: USB Serial support registered for kaufmann [ 1.071051] usbserial: USB Serial support registered for libtransistor [ 1.077334] usbserial: USB Serial support registered for moto_modem [ 1.083371] usbserial: USB Serial support registered for motorola_tetra [ 1.089745] usbserial: USB Serial support registered for nokia [ 1.095368] usbserial: USB Serial support registered for novatel_gps [ 1.101486] usbserial: USB Serial support registered for siemens_mpi [ 1.107612] usbserial: USB Serial support registered for suunto [ 1.113316] usbserial: USB Serial support registered for vivopay [ 1.119111] usbserial: USB Serial support registered for zio [ 1.124578] usbcore: registered new interface driver usb_ehset_test [ 1.215499] usbcore: registered new interface driver usbhid [ 1.220879] usbhid: USB HID core driver [ 1.396384] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests [ 42.414253] usb 1-1: new high-speed USB device number 2 using ci_hdrc [ 42.577822] usb-storage 1-1:1.0: USB Mass Storage device detected [ 42.579492] scsi host0: usb-storage 1-1:1.0  
View full article
Some customer need to run Zephyr on i.MX8QXP CM4, but there is no support on Zephyr mainline(v4.3.0) This article will share the porting based on Zephyr v4.3.0. For i.MX8QM CM4, please refer this link: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QM-CM4-0-support-on-Zephyr-v4-3-0/ta-p/2296962   samples/hello_world/ samples/synchronization Add pd_ignore_unused in bootargs before entering Linux. For the OpenAMP communication, need to refer this Zephyr application. https://github.com/nxp-real-time-edge-sw/heterogeneous-multicore/blob/main/apps/rpmsg_str_echo/zephyr/main.c
View full article
Some customer need to run Zephyr on i.MX8QM CM4, but there is no support on Zephyr mainline(v4.3.0). This article will share the i.MX8QM CM4_0 porting based on Zephyr v4.3.0.  For i.MX8QXP CM4, please refer this link: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-CM4-support-on-Zephyr-v4-3-0/ta-p/2296957   samples/hello_world/ samples/synchronization   Add pd_ignore_unused in bootargs before entering Linux. For the OpenAMP communication, need to refer this Zephyr application. https://github.com/nxp-real-time-edge-sw/heterogeneous-multicore/blob/main/apps/rpmsg_str_echo/zephyr/main.c
View full article
This tutorial describes the complete procedure for calibrating a touchscreen display using Weston, specifically validated with the DY1212W LVDS panel on the following NXP development platforms: i.MX93‑EVK FRDM‑i.MX95 FRDM‑i.MX8MP While the initial calibration performed by Weston works only temporarily, this guide will walk you through configuring the system so that the calibration becomes persistent across reboots. The steps below include performing the initial calibration, editing Weston’s configuration, creating a calibration helper script, and applying udev rules to store the calibration matrix automatically.   Temporary Touchscreen Calibration To begin, run the following command to perform an initial calibration of your touchscreen: weston-touch-calibrator LVDS-1   After running this command, your display should be correctly calibrated. However, this calibration is not persistent, and you will need to recalibrate after every reboot unless you complete the persistence steps below.   Making the Calibration Persistent Follow the steps below to ensure that calibration settings are preserved across system restarts. Step 1: Edit the Weston Configuration File Open the following file: /etc/xdg/weston/weston.ini Under the [libinput] section, add these lines: [libinput] touchscreen_calibrator=true + calibration_helper=/usr/bin/save-calibration.sh This enables the calibration helper script that will automatically save your settings. Step 2: Create the Calibration Helper Script Create a new script at: /usr/bin/save-calibration.sh   Insert the following content: #!/bin/bash # Store the transformation arguments for the resistive touchscreen as udev rule echo 'SUBSYSTEM=="input", KERNEL=="event[0-9]*", ENV{ID_INPUT_TOUCHSCREEN}=="1", ENV{LIBINPUT_CALIBRATION_MATRIX}="'$2' '$3' '$4' '$5' '$6' '$7'"' >> /etc/udev/rules.d/touchscreen.rules   Make the script executable: chmod 755 /usr/bin/save-calibration.sh   Step 3: Restart Weston and Recalibrate Restart the Weston service: systemctl restart weston   Run the calibration tool again to generate the persistent settings: weston-touch-calibrator LVDS-1 reboot   Conclusion After completing all of the steps above, your touchscreen calibration will now persist across reboots, ensuring a consistent user experience even after powering off the board. This configuration allows the system to automatically store and apply calibration data through a udev rule generated by your helper script. If you encounter any issues or require further assistance, feel free to reach out. Best regards, Chavira
View full article