i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
The i.MX31 multimedia applications processors are designed for a broad range of industrial, consumer and automotive applications. Based on an ARM1136JF-S™ core, both the i.MX31 and the i.MX31L processors are engineered to deliver powerful performance while minimizing power consumption. The rich feature set of the i.MX31 processors make them an excellent choice for portable media players, portable navigation devices, medical/industrial monitoring systems, automotive infotainment systems and many general embedded applications. i.MX Family Comparison Product Information on Freescale.com i.MX31 Multimedia Applications Processor Evaluation/Development Boards and Systems IMX31PDK:  i.MX31 Product Development Kit Getting Started Getting Started with the i.MX31PDK Board Flashing i.MX31 PDK Board I.MX31 PDK Board using RedBoot Miscellaneous Tutorials Blinking iMX31PDK LEDs using U-Boot How to Test i.MX31 RNGA Hardware? How to Test i.MX31 TvOut on i.MX31PDK How to Use Clock Out on i.MX31 Issues when interfacing Micron's 78nm mDDRs IMX31ADS Getting Started Getting Started with the i.MX31ADS Board Flashing I.MX31 ADS Board Miscellaneous Tutorials Booting Linux from NAND Flash on the i.MX31ADS Compiling Linux kernel from mainline to i.MX31ADS Issues when interfacing Micron's 78nm mDDRs Embedded Software and Tools Android OS for i.MX Applications Processors Partners / 3rd-Party Development Tools Starterkit STKa31 (Technology in Quality) Additional Resources i.MX31 ADS i.MX31 PDK i.MX31 PDK Board Alpha Blending i.MX31 PDK Board DirectFB i.MX31 PDK Board V4L tests i.MX31 PDK Contents i.MX31 PDK Setting Buttons and Jumpers i.MX31 Lite Kit
查看全文
Freescale's ARM11™-based i.MX 35 processor family provides the perfect balance of performance, power consumption, connectivity, and media capabilities necessary to drive today's multimedia applications. i.MX35 Family Comparison i.MX Family Comparison Product Information on Freescale.com i.MX351 Multimedia Applications Processor i.MX353 Multimedia Applications Processor i.MX355 Multimedia Applications Processor i.MX356 Multimedia Applications Processor i.MX357 Multimedia Applications Processor Evaluation/Development Boards and Systems IMX35PDK: i.MX35 Product Development Kit (PDK) Embedded Software and Tools Android OS for i.MX Applications Processors i.MX35 Current Software Updates and Releases Additional Resources Develop a Simple OpenVG Application Under Linux: Tutorial i.MX35 PDK i.MX35 PDK Linux Booting SD I.MX35 PDK Board Flashing SD Card i.MX35 PDK Board Flashing NAND i.MX35 PDK NAND Flashing Kernel and Root File System Using RedBoot i.MX35 PDK NAND Creating and Flashing UBIFS image
查看全文
Freescale's consumer and industrial i.MX 51 applications processors balance the performance, power consumption, connectivity and multimedia capabilities necessary to drive today's latest and greatest products. Freescale's automotive i.MX 51 processors provide what is necessary to steer today's most advanced automotive systems. i.MX51 Family Comparison i.MX Family Comparison Product Information on Freescale.com i.MX512 Applications Processor i.MX513 Applications Processor i.MX514 Applications Processor i.MX515 Applications Processor i.MX516 Applications Processor Evaluation/Development Boards and Systems IMX51EVK Evaluation Kit Bootloader Installing U-Boot on i.MX51EVK Flashing i.MX51EVK Working with mainline U-Boot Add new iMX5x board on LTIB Compiling U-Boot (from Freescale BSP) using LTIB Changing environment variables storage on U-Boot Linux Flashing Linux application only with SD card Reader Multimedia Using USB Camera Installing OpenCV Library (Open Computer Vision - Image Processing) Android Android without RamDisk Installing TTS library manually Running ADB over USB (iMX51 and Ubuntu communication) Ubuntu Using an USB Touchscreen (Karmic) Using Touchscreen (Lucid) Embedded Software and Tools Android OS for i.MX Applications Processors i.MX51 Current Software Updates and Releases Partners / 3rd-Party Development Tools STK5:  Starter-Kit 5 (Karo Electronics) Additional Resources Board bring-up and DDR initialization tools Develop a Simple OpenVG Application Under Linux: Tutorial i.MX 51 Android ADB over USB IMX51EVK i.MX51 EVK Board USB Camera i.MX51 EVK Compiling U-boot i.MX 51 EVK U-boot i.MX51 EVK Board Video i.MX51 EVK Board OpenCV i.MX51 EVK Board Flashing i.MX51 Flashing Linux Application Only with SD Card Reader I.MX51EVK Install U-Boot i.MX51 EVK Compiling U-boot i.MX51 EVK U-boot i.MX51 EVK Changing Env IMX51 Ubuntu USB TS i.MX 51 Ubuntu TS Lucid
查看全文
Use the EPDC Unit Test to exercise your EPD panel 1.  Introduction The i.MX 6Solo/6DualLite and i.MX 6SoloLite processors contain an Electrophoretic Display Controller (EPDC) designed to drive E-INK(TM) EPD panels supporting a wide variety of TFT backplanes. Detailed information about the EPDC is available in the i.MX 6Solo/6DualLite and i.MX 6SoloLite Reference Manuals. Information about programming the EPDC and integrating support for a particular panel into the Linux BSP is provided in the Linux BSP Reference Manual. Now that you have your panel hardware and software integrated, how can you tell if it is all working? Or perhaps you're using a standard panel that doesn't seem to be working - how can you test it at the lowest level? The answer is the EDPC Unit Test. 2. Running the EPDC Unit Test Most i.MX processor hardware modules have an associated unit test in the unit_tests directory of the root file system image. The basics of running the EPDC unit test are simple. After logging in as root on the debug console, change to the unit tests directory and execute the test as follows: $ cd /unit_tests $ ./mxc_epdc_fb_test.out Without any arguments, the unit test runs thirteen individual tests and takes about 8 minutes to complete. You will get a lot of output on the panel and it may not be obvious that the images are displaying correctly. Running the unit test with no arguments is a nice automated way to make sure your panel is at least displaying something, and is not causing a crash or hang. But to really verify correctness each test should be run individually and the output carefully reviewed. This can be accomplished by passing a test number option as follows: $ ./mxc_epdc_fb_test.out -n 1 To show a list of all the available options, as well as a list of the individual test numbers, use the "-h" argument. The helpful output is shown below. $ ./mxc_epdc_fb_test.out -h EPDC framebuffer driver test program. Usage: mxc_epdc_fb_test [-h] [-a] [-p delay] [-u s/q/m] [-n ]         -h        Print this message         -a        Enabled animation waveforms for fast updates (tests 8-9)         -p        Provide a power down delay (in ms) for the EPDC driver                   0 - Immediate (default)                   -1 - Never                    ms - After ms milliseconds         -u        Select an update scheme                   s - Snapshot update scheme                   q - Queue update scheme                   m - Queue and merge update scheme (default)         -n        Execute the tests specified in expression                   Expression is a set of comma-separated numeric ranges                   If not specified, tests 1-13 are run Example: ./mxc_epdc_fb_test.out -n 1-3,5,7 EPDC tests: 1 - Basic Updates 2 - Rotation Updates 3 - Grayscale Framebuffer Updates 4 - Auto-waveform Selection Updates 5 - Panning Updates 6 - Overlay Updates 7 - Auto-Updates 8 - Animation Mode Updates 9 - Fast Updates 10 - Partial to Full Update Transitions 11 - Test Pixel Shifting Effect 12 - Colormap Updates 13 - Collision Test Mode 14 - Stress Test In addition to "-n" to run individual tests, the "-a" and "-u" options are provided to set animation mode and waveform used, respectively. These options make sense only for some of the individual tests, as noted in the next section. The "-u s" (snapshot) mode purposely does not allow pending updates, so some of the tests will cause the driver to issue the following warning in snapshot mode: imx_epdc_fb: No free intermediate buffers available. The "-p" (power down delay) option allows you to specify how soon the device driver automatically powers down the controller after all pending updates have completed. The default is 0 (zero), meaning power down immediately. Use "-1" to disable power down (i.e. never power down). Sidebar: You can use another unit test, "dump-clocks.sh", to view the state of the EPDC clocks (i.e. the power state of the module). In the example below, a "1" in the third column indicates that the clock is running; a "0" indicates the clock is gated: $ ./dump-clocks.sh | grep epdc epdc_pix_clk             pll5_video_main_clk       1   26666667 epdc_axi_clk             pll2_pfd2_400M             1  198000000 3.  Individual Test Details Important! The notes below assume you are running the version of the unit test binary in the tar file attached to this How-to. Please extract the file mxc_epdc_fb_tests.out from the tar file into your rootfs unit_tests directory before running the test. Most tests begin with a screen blank operation (all white pixels). Each test works with all three update schemes (snapshot, queue, queue and merge) unless otherwise noted. 3.1 Test 1: Basic Updates Draws the following patterns: Crosshatch Squares Text Ginger image Colorbar 3.2 Test 2: Rotation Updates Draws text, squares, crosshatch, and square outlines in all rotation modes: No rotation Clockwise (90 degrees) Upside down (180 degrees) Counterclockwise (270 degrees) The square outlines are drawn first in RGB format and then in Y8 format. 3.3 Test 3: Grayscale Framebuffer Updates Draws a top half black screen and then a colorbar, rotated clockwise. First draws in normal Y8 format and then in inverted Y8 format. 3.4 Test 4: Auto-waveform Selection Updates Draws several small squares using auto-waveform selection. Note: unlike the i.MX508 EPDC driver, the i.MX 6 driver does not report the final waveform selection to user-level applications. This test also verifies that squares at non-8-bit aligned pixels can be drawn. 3.5 Test 5: Panning Updates Draws a colorbar to an off-screen region. Draws the Ginger image to the frame buffer. Sets the focus (pan) to the colorbar, then updates portions of the screen. You should see the colorbar poke through. Slowly pans from Ginger to the entire colorbar. Use pan to flip between black and white buttons. Flashes buttons using pixel inversion. Flashes buttons using panning. 3.6 Test 6: Overlay Updates Switches between the frame buffer (FB) and the alternate (overlay) frame buffer as follows: Draws Ginger to the FB. Draws the colorbar to the alternate frame buffer. Shows the FB (Ginger). Shows the alternate FB (colorbar). Shows FB again (Ginger). Shows half FB, half alternate FB. Shows cutout region of alternate FB. Shows cutout in upper corner. Shows black screen. Shows clockwise-rotated text overlay in center. 3.7 Test 7: Auto-Updates Important! The auto-update mechanism must be enabled in the kernel configuration for this test to work. Enable it using the LTIB Kernel configuration menu item "Device Drivers->Graphics support->E-Ink Auto-update Mode Support." Also, please check the Linux BSP Release Notes for any issues with this feature. 3.8 Test 8: Animation Mode Updates Shows how normal (gray level) and monochrome (black and white) updates compare in appearance and performance. Quickly flashes back and forth between black and white screens. Draws normal squares. Draws black and white squares. Draws Ginger in gray scale and monochrome. Draws colorbar in gray scale and monochrome. Draws normal Y8 colorbar and monochrome colorbar. Draws inverted normal Y8 colorbar and inverted monochrome colorbar. You can run this test in animation mode using the "-a" command line option. Animation mode only updates monochrome pixels, so you will notice a drawing speed improvement. Also, you will see the implementation of one of the "rules" of using this mode: The screen must be blanked (all white or all black) when switching in and out of animation mode. 3.9 Test 9: Fast Updates Animates a square across the screen and down one side. This test can also be run in animation mode using "-a". See the animation mode notes in the Test 8 description above. 3.10 Test 10: Partial to Full Update Transitions Draws small gray squares using separate updates in partial update mode (only pixels that change are updated). Then re-draws the entire screen in one update using full update mode. In full update mode, you will notice the entire screen transition from black to the final grey value. 3.11 Test 11: Test Pixel Shifting Effect Draws a short, two pixel line and then sends two updates one pixel apart in distance and 5 seconds apart in time. Nothing much to see here; just verifies that a one pixel update shift works. 3.12 Test 12: Colormap Updates Creates a colormap and uses it to draw full screen blanks and to draw a color bar. In this test, you should follow along with the text printed in the debug console and verify each state: Screen should be black. Screen should be white now. Screen should still be white. Should be inverted color bar (white to black, left to right). Colorbar again, with no CMAP (black to white, left to right). Posterized colorbar. In the above output, "CMAP" means colormap and "Posterized colorbar" is a colorbar drawn from only black and white components. 3.13 Test 13: Collision Test Mode Draws two overlapping rectangles. Tests for collision on the first rectangle, which should result in the message: Collision test result = 0 Then draws the same overlapping rectangles, this time testing for collision on the second rectangle. The result should be: Collision test result = 1 Note: This test cannot be run using the snapshot scheme. If you try to use "-u s" it will print a message and return. 3.14 Test 14: Stress Test Draws thousands of random rectangles on the screen in different rotations. Runs for about 8 minutes. This test must be explicitly specified on the command line; it does not run by default. For example: $ ./mxc_epdc_fb_test.out -n 14 Note: This test cannot be run using the snapshot scheme. If you try to use "-u s" it will print a message and return. 4. Customizing A great way to know what's really going on in each test is to look at the source code. You may want to customize the source as well - say to add a new test that exercises some cool feature of your panel. Fortunately, the source is included in the BSP distribution so you can extract, customize, and rebuild it as needed. The magic of LTIB is beyond the scope of this article, but here are some hints: # Extract the unit test source from the imx-test package: $ ./ltib -m prep -p imx-test # Source is now in rpm/BUILD/imx-test-12.08.00/test/mxc_fb_test/mxc_epdc_fb_test.c (your package version number my be different). # Build from source: $ ./ltib -m scbuild -p imx-test # Deploy all unit test binaries to ltib rootfs directory: $ ./ltib -m scdeploy -p imx-test # Alternatively you can copy just the epdc unit test binary as follows: $ sudo cp rpm/BUILD/imx-test-12.08.00/platform/IMX6S/mxc_epdc_fb_test.out rootfs/unit_tests/ As noted in the Individual Test Details section, you should replace the file mxc_epdc_fb_test.c referenced above with the one found in the tar file attached to this How-to. 5. Something is wrong! Of course there are many things that can go wrong that are beyond the scope of this article, but assuming your hardware is working and the panel options are correctly configured in the BSP (again, beyond our scope), here are some things to check: Is the kernel configured correctly for EPDC support? Check that the following item is enabled in the LTIB Kernel configuration menu: "Device Drivers->Graphics support->E-Ink Panel Framebuffer." Are the U-boot kernel command line arguments set correctly for EPDC? For example, "video=mxcepdcfb:E060SCM consoleblank=0". The "consoleblank=0" command is useful to prevent entering low power suspend mode while you are testing. Does the "Tux" image display correctly on your panel after system boot? If so, the EPDC driver was a least able to perform the initial framebuffer update to your panel. Note: for Tux to display at boot, you need to disable LCDIF support at "Device Drivers->Graphics support->Support MXC ELCDIF framebuffer." Are there any EPDC-related error messages in the kernel log after boot? You can check with "dmesg | grep epdc".
查看全文
The i.MX53 family of processors represents Freescale's next generation of advanced multimedia and power-efficient implementation of the ARM Cortex™-A8 core with core processing speeds up to 1.2 GHz. It is optimized for both performance and power to meet the demands of high-end, advanced applications. Ideal for a broad range of applications in the consumer, automotive, medical and industrial markets, the i.MX53 includes an integrated display controller, full HD capability, enhanced graphics and connectivity features. i.MX Family Comparison Product Information on Freescale.com i.MX534 Multimedia Applications Processor i.MX535 Multimedia Applications Processor i.MX536 Multimedia Applications Processor i.MX537 Multimedia Applications Processor Evaluation/Development Boards and Systems i.MX53 Quick Start Board Android How to enable WIFI support for iMX53 QSB Android IMX53 QSB android recovery mode Linux I.MX53 QSB Board Get Started How to flash a 4GB SD Card with the image used in training Enabling Dual Display in UBUNTU with the iMX53 QSB @running_dual_display SABRE Platform for Tablets based on i.MX53 Linux i.MX53 ARD Dual LVDS Enabling Dual LVDS panels i.MX53 USB Eth NFS Using an USB/Eth adapter to boot NFS User Applications i.MX53 Qt LVDS display Touch on Qt with LVDS display Embedded Software and Tools Android OS for i.MX Applications Processors i.MX53 Current Software Updates and Releases Partners / 3rd-Party Development Tools Rainbow-G11D:  i.MX53 Development Kit (iWave Embedding Intelligence) STKa53:  Starterkit STKa53 (Technology in Quality) DS-5:  ARM Development Studio 5 (ARM) Additional Resources Board Bring-up and DDR Initialization Tools Building QT5 for i.MX53 Change AUDMUX src_port causes "imx_ssi_irq mxc_ssi SISR 8003a3 SIER 180100 fifo_errs=XXXX" ConnectCore® i.MX53 / Wi-i.MX53 by Digi International Develop a Simple OpenVG Application Under Linux: Tutorial Embedded i.MX5x Application Development Kit for Android -$199 HDMI Audio Setting How to Enable the souphttpsrc Plugin on i.MX53 i.MX53 ARD Dual LVDS Imx53-fastboot-example i.MX53 Memory Calibration Script (AN4466) i.MX53 QSB Android Recovery Mode I.MX53 QSB Board Get Started i.MX53 QSB Board Video IMX53 QSB enable WIFI android i.MX53 QSB Ubuntu Dual Display i.MX53 Quick Start Board IMX53 SABRE AI i.MX53 Start-R Lab Exercise - Prof. Massimo Violante Politecnico of Torino i.MX53 Start-R Lab Exercise - Developing a loadable kernel module to manage GPIOs in i.MX53QSB i.MX53 USB Eth NFS i.MX53 Qt LVDS Display NOVPEK i.MX53 by NovTech Running Dual Display on i.MX53QSB bin2txt.pyw (U-boot splash screen support)
查看全文
In some cases it is desired to directly have progressive content available from a TV-IN interface through the V4L2 capture device. In the BSP, HW accelerated de-interlacing is only supported in the V4L2 output stream. Below is a patch created against a rather old BSP version that adds support for de-interlaced V4L2 capture. The patch might need to be adapted to newer BSPs, However, the logic and functionality is there and should shorten the development time. This patch adds another input device to the V4L2 framework that can be selected to perform the deinterlacing on the way to memory. The selection is done by passing the index “2” as an argument to the VIDIOC_S_INPUT  V4L2 ioctl. Attached is also a modified the tvin unit test to give an example of how to use the new driver. An example sequence for running the test is as follows: modprobe mxc_v4l2_capture ./mxc_v4l2_tvin_vdi.out -ow 720 -oh 480 -ol 10 -ot 20 -f YU12 Some key things to note: This driver does not support resize or color space conversion on the way to memory. The requested format and size should match what can be provided directly by the sensor. The driver was tested on a Sabre AI Rev A board running Linux 12.02. This code is not an official delivery and as such no guarantee of support for this code is provided by Freescale.
查看全文
Here is an example for i.MX28 EVK board to support SPI NOR boot in uboot, kernel and MFGTool.   Attached files are the patches to support SPI NOR flash on i.MX28 EVK bord based on L2.6.35 ER11.09.01 BSP. It was verified on Spansion s25fl256s SPI NOR. "ER11.09.01_uboot_imx28_spi_nor.patch" is the Uboot patch. "ER11.09.01_kernel_imx28_spi_nor.patch" is the kernel patch. "ucl.xml" is the updated MFGTool config file, please update it to "Mfgtools-Rel\Profiles\MX28 Linux Update\OS Firmware\ucl.xml".   The uboot boot paramters for SPI: setenv bootargs_base 'setenv bootargs console=ttyAM0,115200' setenv loadaddr 0x42000000 setenv bootargs_spi 'setenv bootargs ${bootargs} root=/dev/mtdblock2 rootfstype=jffs2 rootwait rw ip=none' setenv bootcmd_spi 'run bootargs_base bootargs_spi;sf probe 2:0; sf read ${loadaddr} 0x100000 0x300000;bootm' setenv bootcmd 'run bootcmd_spi' saveenv   To boot the board from SPI NOR s25fl256s, the 4KB page region of the NOR should be put to top, the last 128KB of the NOR address space. The uboot.sb is about 220KB, it can't be put to 4KB and 64KB combined region. The IMX28 boot ROM can only handle simple page size for boot. All 4KB page region or all 64KB page region are both OK for boot, but combined region can't boot.   For default, the s25fl256s NOR's 128KB 4KB page size region is at the bottom of the NOR, we should update the OTP to set this region to TOP, in Uboot, we run the followed command to burn the OTP: MX28 U-Boot -> sf probe 2:0 MX28 U-Boot -> sf set_config_reg 0x04   To boot the i.MX28 EVK board from SPI2 NOR flash, the BM3~0 should be 0010.   In this example, we only used the JFFS2 file system. To support the UBIFS, there is a known issue, that the UBIFS will use vmalloc to alloc memory, and if SPI driver used the DMA, kernel will halt with error "kernel BUG at arch/arm/mm/dma-mapping.c:409!".   For 11.09.01 BSP, the default MFGTool rootfs "initramfs.cpio.gz" will be bigger than 4MB, but in i.MX28 bootlets code, the BSP only set ramdisk to 4MB, so we need modify this limitation for MFGTool.   Use command "./ltib -p imx-bootlets -m prep" to get the bootlets code, modify "ltib/rpm/BUILD/imx-bootlets-src-11.09.01/linux_prep/core/setup.c", function setup_initrd_tag(), change from "params->u.initrd.size =  0x00400000;" to "params->u.initrd.size =  0x00500000;". Modify "ltib/rpm/BUILD/imx-bootlets-src-11.09.01/updater.bd" and "updater_ivt.bd", change from "load 0.b    > 0x40800000..0x40c00000;" to "load 0.b    > 0x40800000..0x40d00000;".   Now the MFGTool rootfs size can be 5MB.   2013-05-09: Updated hardware rework: On iMX28 EVK board, rework J89 as followed and mount R320,R321,R322 and C178. MX28 U49 Pin1 /CS <-> NOR Pin7 CS# MX28 U49 Pin2  D0 <-> NOR Pin8 SI/IO1 MX28 U49 Pin5 DIO <-> NOR Pin15 SI/IO0 MX28 U49 Pin6 CLK<-> NOR pin 16 SCK. MX28 U49 Pin8 VCC <-> NOR Pin2 VCC                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                 MX28 U49 Pin4 GND <-> NOR Pin10 VSS MX28 U49 Pin3 /WP <-> NOR Pin9 WP MX28 U49 Pin7 /Hold <-> NOR Pin pin1 hold   Software reset issue for 32MB SPI NOR: For 32MB SPI NOR, after booted into kernel, the kernel driver will set SPI NOR to 4 bytes address mode, but for iMX28 SPI boot, it can only boot with 3 bytes address mode, if reset the iMX28 board but SPI NOR was not reset, it will fail to reboot. Hardware solution: when iMX28 was reboot, reset the SPI NOR too, the SPI NOR will work in 3 bytes address mode as default. Software solution: In kernel SPI NOR driver, always switch SPI NOR to 3 bytes address mode after each SPI NOR access, and switch to 4 bytes address mode before each access. There is no such issue if the SPI NOR size is less than 32MB.    
查看全文
The original implementation is from Frias Renato for Sabreauto board. How to define the booting time? The booting time we defined here is from the board be powered up to the main application working and main application be showed directly to the end user, for example: for the media play purpose board, the booting time count to the first video frame be shown on the screen. For minimizing the booting time, some methods be tried. Optimizing for performance. Remove unnecessary modules at boot time. Start main application at the first time after the kernel be boot up. Optimizing for performance: U-Boot:   1:Enable MMU and L2-Cache.   2:Optimizing memset and memcpy.   3:Implementation of SDMA, accelerate copying data from NOR flash to memory.   4:Implementation of uSDHC’s ADMA, improve performance for SD card read. Kernel:   1:Optimizing _memcpy_fromio function at  arch/arm/kernel/io.c Remove unnecessary modules: U-Boot:   1: Disable uart output at u-boot procedure and add quiet parameter to Kernel boot.   2: Remove boot up delay at u-boot.   3: Disable I2C, SPI, SPLASH_SCREEN at u-boot. Kernel: Below removing unnecessary modules just for Sabresd board boot up through SD card and MIPI camera overlay on LVDS screen application, for other special board and special board usage application please don’t use below directly.   1: Modify arch/arm/mach-mx6/board-mx6q_sabresd.c just keep necessary module initialization at  mx6_sabresd_board_init : iomux configuration, uart0, voda, ipu, ldb, v4l2, mipi-csi, i2c1, uSDHC1, pwm0, dvfs, mipi camera clock.   2: Update Linux kernel configuration file. Try to just keep necessary module and configuration to keep minim size. Build necessary modules from external to Kernel itself. Create uImage from Image instead of zImage to reduce Kernel self extraction time. Use ext4 file system on SD card to accelerate rootfs mounting.    Notice: Kernel configuration remove NETWORK support, it includes Unix Domain Socket, the udev mechanism need it, so this kernel configuration can't support rootfs udev dynamic /dev/ nodes and all /dev/ nodes must be created before boot up at rootfs. Start main application at the first time after the kernel boots up. As normal boot up procedure, the init process will handle sysinit script firstly, this script will do some initialization and preparation for most of the user process, But this script normally will be executed for about 1~5 seconds, so now try do main application before the sysinit, while the necessary preparation of main application will be handle by this application internally. See below example for MIPI camera overly on LVDS screen: /etc/inittab ::once:/unit_tests/mxc_v4l2_overlay.out -iw 640 -ih 480 -it 0 -il 0 -ow 1024 -oh 768 -ot 0 -ol 0 -r 0 -t -1 -d 0 -fg -fr 30 ::once:/etc/rc.d/rcS ::once:/sbin/getty -L ttymxc0 115200 vt100 # GENERIC_SERIAL Test result of fast boot on Sabresd board for MIPI camera overly on LVDS screen: The main application be executed from the board be powered up is about 958ms.    Running Bootloader [0.356417 0.356417] [ 0.046637] _regulator_get: get() with no identifier [ 0.958425  0.602008] starting pid 21, tty '': '/unit_tests/mxc_v4l2_overlay.out -iw 640 -ih 480 -it 0 -il 0 -ow 1024 -oh 768 -ot 0 -ol 0 -r 0 -t -^@ [0.969609 0.011184] starting pid 22, tty '': '/etc/rc.d/rcS' [0.973368 0.003759] g_display_width = 1024, g_display_height = 768 [0.977540 0.004172] g_display_top = 0, g_display_left = 0 [0.980927 0.003387] starting pid 23, tty '': '/sbin/getty -L ttymxc0 115200 vt100 ' [1.048454 0.067527] Mounting /proc and /sys [1.089526 0.041072] Setting the hostname to freescale [1.116635 0.027109] Mounting filesystems [1.527320 0.410685] sensor chip is ov5640_mipi_camera [1.530627 0.003307] sensor frame size is 640x480 [1.533482 0.002855] sensor frame format is UYVY [1.640221 0.106739] frame_rate is 30 [1.642249 0.002028] [1.642270 0.000021] frame buffer width 0, height 0, bytesperline 0 [1.989728 0.347458] [1.990761 0.001033] arm-none-linux-gnueabi-gcc (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) 4.6.2 20110630 (prerelease) [2.001161 0.010400] root filesystem built on Tue, 11 Sep 2012 11:43:24 +0800 [2.006249 0.005088] Freescale Semiconductor, Inc. [2.009394 0.003145] [2.009531 0.000137] freescale login: Please see below fast boot video. I also attached sample code for U-boot and kernel for your reference. Patch code based on L3.0.35_12.09.01_GA.
查看全文
Pre-requisites: An TFTP server U-boot with TFTP capabilities If you need to run a script (for example, running multiple setenv's commands) in U-boot for many boards, you can instead create a U-boot script (called script image), place it into your tftp folder, then ask U-boot to fetch it and run it. For example, you want to run the following setenv instructions setenv loadaddr 0x10800000 setenv bootargs_base 'setenv bootargs console=ttymxc0,115200' setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666' setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev 3;mmc read ${loadaddr} 0x800 0x2000;bootm' run bootcmd_mmc save it into a file, I choose the name 'myscript'; under your <U-boot folder>/tools, execute $ mkimage -T script -C none -n 'My Script' -d myscript myscript.img and copy myscript.img file into your TFTP folder. On the target, set the following two variables (serverip and bootcmd) # Set the Server IP, where the TFTP server is running setenv serverip <the server IP> # In case the server IP is static, you can place this line into the U-boot script setenv scriptaddr 0x10700000 setenv scriptname myscript.img # You can use either TFTP or DHCP setenv tftpcmd tftp # or 'dhcp'  in case you want to use dhcp U-boot command # Not needed for dhcp setenv ipaddr <the target IP> # needed in case the command tftp is used setenv gatewayip <the Gateway IP> # needed in case the command tftp is used setenv bootcmd '${tftpcmd} ${scriptaddr} ${scriptname}; source ${scriptaddr}' saveenv reset That is all you need to do. Enjoy U-booting!
查看全文
Introduction LVDS display panel driving data flow: Display quality: To get the best display quality for 24bit LVDS display panel in Android, we should use 32bit framebuffer, make IPUv3 display Engine and LDB output 24bit pixels, since RGB component information is aligned from source to destination.  2 stages to enable display: Uboot splash screen and Kernel framebuffer Guidelines Uboot splash screen:    Change should be done in board file, like board/freescale/mx6q_sabresd/mx6q_sabresd.c:    1. Set video mode in struct fb_videomode according to the new 24bit LVDS display panel’s spec(please, refer to the example at the end of this doc).    2. Set up pwm, iomux/display related clock trees in lcd_enable(). Note that these should be aligned with Kernel settings to support smooth UI transition        from Uboot splash screen to Kernel framebuffer.    3. Set the output pixel format of IPUv3 display engine and LDB to IPU_PIX_FMT_RGB24 when calling ipuv3_fb_init().    4. Set pixel clock according to the new 24bit LVDS display panel’s spec when calling ipuv3_fb_init().    5. If dual LDB channels are needed to support tough display video mode(high resolution or high pixel clock frequency), we need to enable both of the two LDB        channels and set LDB to work at split mode. LDB_CTRL register should be set accordingly in lcd_enable(). Kernel framebuffer:    As we may add ‘video=‘  and ‘ldb=’ options in kernel bootup command line, Kernel code is more flexible to handle different LVDS display panels with various display color depth than Uboot code. For detail description of ‘video=’ and ‘ldb=’ option, please refer to MXC Linux BSP release notes and Android User Guide. Some known points are:    1. Add a video mode in struct fb_videomode in drivers/video/mxc/ldb.c according to the new 24bit LVDS display panel’s spec(please, refer to the example at        the end of this doc).    2. Set up pwm backlight/display related iomux in platform code.   3. Set appropriate ‘video=‘ option in kernel bootup command line, for example:        video=mxcfb0:dev=ldb,LDB-NEW,if=RGB24,fbpix=RGB32     4. Set appropriate ‘ldb=‘ option in kernel bootup command line if dual LDB channels are needed to support tough display video mode, for example:        ldb=spl0 (IPUv3 DI0 is used)  or  ldb=spl1 (IPUv3 DI1 is used)    5. Set appropriate ‘fbmem=‘ option in kernel bootup command line to reserve enough memory for framebuffer. For example, if we use 1280x800 LVDS panel        for fb0 and fb0 is in RGB32 pixel format, then ‘fbmem=12M’ should be used, since the formula is:        fbmem= width*height*3(triple buf)*Bytes_per_pixel= 1280*800*3*4B=12MB An Example to Set struct fb_videomode:    Let’s take a look at the timing description quoted from a real 1280x800@60 24bit LVDS panel spec: And, standard linux struct fb_videomode definition in include/linux/fb.h: struct fb_videomode {         const char *name;       /* optional */         u32 refresh;            /* optional */         u32 xres;         u32 yres;         u32 pixclock;         u32 left_margin;         u32 right_margin;         u32 upper_margin;         u32 lower_margin;         u32 hsync_len;         u32 vsync_len;         u32 sync;         u32 vmode;                u32 flag; };    What we need to do is to set every field of struct fb_videomode correctly according to the timing description of LVDS display panel’s spec:     1. name: we can set it to ‘LDB-WXGA’.    2. refresh: though it’s optional, we can set it to typical value, that is, 60(60Hz refresh rate).    3. xres: the active width, that is, 1280.    4. yres: the active height, that is, 800.    5. pixclock: calculate with this formula – pixclock=(10^12)/clk_freq. Here, typically, for this example, pixclock=(10^12)/71100000=14065.    6. left_margin/right_margin/hsync_len:        They are the same to HS Back Porch(HBP)/HS Front Porch(HFP)/HS Width(HW) in the spec. Since the spec only tells us that typically        HBP+HFP+HW=160. We may set left_margin=40, right_margin=40, hsync_len=80.    7. upper_margin/lower_margin/vsync_len:        Similar to horizontal timing, the vertical ones can be set to upper_margin=10, lower_margin=3, vsync_len=10.    8. sync: Since the timing chart tells us that hsync/vsync are active low, so we don’t need to set FB_SYNC_HOR_HIGH_ACT or        FB_SYNC_VERT_HIGH_ACT. Moreover, clock polarity and data polarity are invalid, so we set sync to be zero here.    9. vmode: this is a progressive video mode, so set vmode to FB_VMODE_NONINTERLACED.    10. flag: the video mode is provided by driver, so set flag to FB_MODE_IS_DETAILED.
查看全文
How to add Ethernet UI support in ICS     How to add Ethernet UI support in ICS 1.  Introduction 2.  New feature detail   1.  Introduction   If you want to add Ethernet UI support , you need manually apply the attached patches in this file which is based on Android ICS and i.MX6.        About what the patches do, here is some comments: framework/base-----0001-ENGR00220371-Ethernet-add-support-for-ethernet.patch        By default, Android has no support for Ethernet UI. So if you want to add Ethernet UI , add Ethernet state tracker & Ethernet service & Ethernet manager & Ethernet monitor like WiFi. Meanwhile we need add Ethernet display support in status bar. Here this patch can solve it. Build---0001-ENGR00220371-Ethernet-add-ethernet-support.patch        add package directory compile. packages\apps\Settings---0001-ENGR00220371-Ethernet-add-app-UI-in-setting.patch        add UI logic in setting app. packages\providers\DownloadProvider---0001-ENGR00220371-Ethernet-add-downloadinfo.patch        add ConnectivityManager.TYPE_ETHERNET type support in download provider’s DownloadInfo.   2.  New feature detail   After applying the above patches, you will get the following features: Icon for Ethernet connection status. If on, a green icon will appear in status bar; If off,no icon will appear.     Add “Ethernet configuration” UI.  Choose box is designed for turn on or off Ethernet.      Only Ethernet is turned on, Ethernet configuration can be configured static IP.   First boot, Ethernet device default may not be eth0. So change it from the device list. Use imx6-ics-ethernet-v3.zip. It has updated and fixed the following issues compared with the previous two versions:   1. fix static IP not work issue. 2. fix dns using default 8.8.8.8 issue. 3. eth0 is the default interface, no longer need to choose it from the list. 4. dhcp is default mode. and if you are using static IP. After reboot, it will restore to dhcp again. 5. no need to edit dns again.   List the bug list for update. If using ethernet as upstream type, you need to apply the attached fix-use-ethernet-as-upstream.patch.   For JB4.2.2 and JB4.3, we have written one apk for this. Anyone who is interested in this can get it.
查看全文
Android Power Debug and Optimization Introduction Android Power Management on i.MX Overview How to do power optimization for Android on i.MX How to check high power consumption on i.MX How to debug suspend/resume problems on i.MX Introduction This document describes i.MX Android power issues debug and power consumption optimization. Android Power Management on i.MX Overview What Power Manager introduced by Android • Early Suspend    It is allow drivers like LCD, keypad backlight, touch-screen, gsensor, to be notified when user-space writes to /sys/power/request_state to indicate that the user visible sleep state should change. These drivers will act as like Linux stand suspend() to let these devices entry in suspend for better battery life. •Late Resume    Late resume is matching with early suspend. It will resume the devices suspended during early suspend after the Stand Linux resume finished •Wake Locks     Wake locks are used by applications, services, kernel drivers to request CPU resources. A locked wakelock, depending on its type, prevents the system from entering suspend or other low-power states. It as a core member in android power management architecture from framework to kernel What introduced by i.MX to enhance the power framework BusFreq Support High bus, Low power audio bus and Low bus totally 3 system bus working points. Switching between these 3 bus mode according clock flags automatically. DDR running frequency will change according bus mode changing (highest 528/400MHz and lowest at 24MHz for MX6DQ/DL). CPUFreq The CPU frequency scaling device driver allows the clock speed of the CPUs to be changed on the fly. Once the CPU frequency is changed, the GP voltage will be changed to the voltage value. Enhance the default interactive governor for better performance on SDHC/GPU etc. System Power Profile Service and App (just for MX6DQ/DL) Support 3 profiles currently: Normal mode, Power Saving Mode and Performance Mode to get much better balance between performance and power consumption. Profiles can be customized according customers’ HW /MD design, including: CPU running max freq, trigger temperature, CPU running minimal freq, running cpu LDO bypass mode           i.MX6X has built-in LDO module, but also allows you to use external LDO suppliers. SW will provide the configuration using external LDO or internal LDO. How to do power optimization for Android on i.MX Suspend Mode All devices enter in suspend or low power Config GPIO PADs as High Z or input mode (depending on HW design,FSL provide Ref code) Cut off LDOs which no modules need (depending on HW design, FSL provide Ref code) DDR enter in self-refresh mode (FSL done) Config DDR IO Float pin to reduce the DDR IO consumption (FSL done) ARM core entry stop mode (WFI) (FSL done) All PLLs will cut off, just 32KHZ sleep clock living (FSL done) Notify the PMIC entry in standby to save some power (FSL done) User Idle Mode Optimization on device driver for WiFi, 3G, BT, screen brightness modules, etc., to save some power Let some device/GPIOs entry in suspend mode/low power mode Active power saving profile to reduce some system power loading. GPU 2D/3D auto entry in Stop/Standby mode if no activity needs update. (FSL done) Enable CPUFreq reduce ARM CORE power consumption (FSL done) Busfreq scanning to let system work at lower Freq to save power (FSL done) Audio/Video Playback Mode Optimization on device driver for WiFi, 3G, BT, screen brightness modules, etc., to save some power Let some device/GPIOs entry in suspend mode/low power mode Disable HW 3D acceleration for some Apps such as System UI, Music Player, etc., to save some power when System in IDLE or music playing mode. Enable CPUFreq and SOC WAIT mode, decrease CPU Freq/Voltage to save power for ARM CORE when no there is no task need cpu to handle(FSL done) Busfreq scanning will set bus work at low power audio bus mode to save some power (FSL done for audio case) DDR enter in self-refresh mode (FSL done for audio case) Reduce the screen brightness will save some power (for video case) VPU clock auto-gating to save power on SOC domain (for video case, FSL done) GPU 2D/3D auto-gating to save some power on SOC domain (FSL done) Try VDOA+IPU to bypass GPU in video playback(not comment for Android platform, pure Linux environment using this method, for it has some limitation such as the input/output size limit), this can save some power on DDR domain. How to check high power consumption on i.MX Idle Audio/Video Playback high power consumption Check the CPUFreq and  Bus_freq is enabled           cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor           cat /sys/devices/platform/imx_busfreq.0/enable Check whether the system bus working poing   For MX6Q:           cat /sys/kernel/debug/clock/osc_clk/pll2_528_bus_main_clk/periph_clk/mmdc_ch0_axi_clk/rate   For MX6DL/SL:           cat /sys/kernel/debug/clock/osc_clk/pll2_528_bus_main_clk/pll2_pfd_400M/periph_clk/mmdc_ch0_axi_clk/rate Check CPU Loading and Interrupt(cat /proc/interrupts) Check clock tree carefully to see which clocks arenot gated off  but no any modules need them.            powerdebug –d  -c SUSPEND MODE high power consumption Make sure all device entries are in suspend mode Make sure the system entry in DSM(measure the voltage &current of VDDARM_CAP, VDDSOC_CAP,DDR_1V5, VDD_HIGH…)      Some tips help to locate the problems Add debug message in device drivers which may lead high power consumption Enable PM debug in kernel Catch the waveform from these modules which may impact the high power consumption Remove devices from the board or do H/W rework to exclude some H/W problems How to debug suspend/resume problems on i.MX System could not entry in suspend mode Check below settings has been disabled: GPS has been disabled Don't connect USB cable to the board (adb will hold a wake lock) RIL will hold a wake lock if RIL failed to initialize (logcat -b radio) Setting->Application->Developer options->stay awake (stay awake not set) Check all wake locks which holed by kernel have been released          echo 15 > /sys/module/wakelock/parameters/debug_mask Check all user wake locks have been releaed          echo 15 > /sys/module/userwakelock/parameters/debug_mask System hang when resume or suspend Enable PM debug system to get more info about PM in kernel     make menuconfig  enable the PM debug sys [*] Power Management support                                                           [*]   Power Management Debug Support                                                           [*]     Verbose Power Management debugging Add no_console_suspend to the boot option for kernel         This makes the system print more useful info before entry in suspend Check the PMIC_STBY_REQ signal. Measure the VDDARM_IN Using Trace32 or ICE to locate the problem. Using RAMCONSOLE to dump the kernel log after reboot. Kernel resume back from suspend  but Android not    This is usually because of the wrong key layout file Use tool to get power key scan code        getevent  Correct the Keylayout         system/usr/keylayout/****.kl Correct the scandcode with your power key report value to Match the POWE key
查看全文
Print caller stack may help you to analyze the program and find out the caller stack more easily. You can write your code like this: Java:      Exception e = new Exception();      Log.e(TAG,"xxx",e); C++ file:       #include <utils/Callstack.h>      android::CallStack stack;      stack.update(1,30);      stacn.dump("xxx"); Then you can see the function's caller stack in Android main log file. C file: #include <corkscrew/backtrace.h> #define MAX_DEPTH 31 #define MAX_BACKTRACE_LINE_LENGTH 800 static backtrace_frame_t mStack[MAX_DEPTH]; static size_t mCount; void csupdate(int32_t ignoreDepth, int32_t maxDepth) {     if (maxDepth > MAX_DEPTH) {         maxDepth = MAX_DEPTH;     }     ssize_t count = unwind_backtrace(mStack, ignoreDepth + 1, maxDepth);     mCount = count > 0 ? count : 0; } void csdump(const char* prefix)\ { size_t i = 0;     backtrace_symbol_t symbols[MAX_DEPTH];     get_backtrace_symbols(mStack, mCount, symbols);     for (i = 0; i < mCount; i++) {         char line[MAX_BACKTRACE_LINE_LENGTH];         format_backtrace_line(i, &mStack[i], &symbols[i],                 line, MAX_BACKTRACE_LINE_LENGTH);         ALOGE("%s%s", prefix, line);     }     free_backtrace_symbols(symbols, mCount); } void myFunc() {      csupdate(1, 30);      csdump("myprefix"); } In Android.mk, add libcorkscrew, as below LOCAL_SHARED_LIBRARIES := libxxx libyyy libcorkscrew
查看全文
Graphics are a big topic in the Android platform, containing java/jni graphic framework and 2d/3d graphic engines (skia, OpenGL-ES, renderscript). This document describes the general Android graphic stack and UI features on Freescale devices. 1. Android Graphic Stacks All Android 3D apps and games have the following graphic stack: Android system UI and all Apps UI follow 2D graphic stack as below, the hardware render will accelerate Android 2D UI with GPU HW OpenGL-ES 2.0 to improve the whole UI performance. Hardware acceleration can be disabled on i.mx6 in device/fsl/imx6/soc/imx6dq.mk USE_OPENGL_RENDERER := false Then rebuild frameworks/base/core/jni, and replace libandroid_runtime.so Surfaceflinger is responsible of all surface layers composition, and  then generate the framebuffer pixmap for display devices. these graphic surface layers are from 2D/3D apps. Hwcomposer is the alternative module of Surfaceflinger with OpenGL-ES. Hwcomposer is used to combine the specific surface layers supported by specific vendor devices. Freescale i.MX6 devices use GPU 2D to combine most surface layers, and the system power can be reduced with GPU 2D instead of GPU 3D. The typical power saving case is video playback. Hwcomposer with GPU 2D can offload GPU 3D task when running game and benchmarks, it is proved to improve the overall system performance about 20%. 2. Performance measurment Show FPS for Android system performance For NFS boot you can set “debug.sf.showfps” to 1 in init.freescale.rc (“setprop debug.sf.showfps 1”) and then reboot the system. For SD or EMMC boot, you can issue command “setprop debug.sf.showfps 1” in console, then find system_server thread by top and kill it to reset the system. Graphic benchmarks for 3D capability measurement Quadrant Full test benchmark cover CPU, Memory, IO, 2D and 3D GLBenchmark http://www.glbenchmark.com/ NenaMark2 https://market.android.com/details?id=se.nena.nenamark2 An3DBench http://www.androidzoom.com/android_applications/tools/an3dbench_hnog.html AnTutu http://www.antutu.com/software.html 3DMark http://www.futuremark.com/benchmarks/3dmark06/introduction/ Browser benchmarks http://www.webkit.org/perf/sunspider/sunspider.html http://v8.googlecode.com/svn/data/benchmarks/current/run.html http://www.craftymind.com/guimark2/ http://www.craftymind.com/factory/guimark/GUIMark_HTML4.html http://themaninblue.com/writing/perspective/2010/03/22/ 3.  Android UI features Dual display with same content This feature is supported in the default image in Android i.MX 6 release package. In this feature, LVDS panel and HDMI output can be supported simultaneously. It is only enabled when the HDMI TV has been connected with the board. Overscan for TV devices Some TVs may miss display the contents in overscan area. To avoid the contents in overscan area being lost, the common implement is by underscanning with an adjustable black border and letitng the viewer adjust the width of the black border. The downscan operation is done by surfaceflinger when it does surface composition through HW OpenGL ES. There is no performance impact since all the work is done by GPU HW. Overscan can be configured in display setting in visual mode: 32 bits color depth 32bpp UI can be supported by adding “bpp=32” in uboot as below: setenv bootargs ‘… video=mxcdi1fb:RGB666,XGA,bpp=32 …’, also can configure it in display setting. Enable 32bpp frame buffer and application surface buffer will be allocate to RGBA8888 format instead of default RGB565 format, that means more system memory is allocated. After enabling 32bpp, if some applications still don't have better UI quality, check to see if  there is hard code to request RGB565 format surface (should request RGBA8888 format to get better quality). Sample code is attached to test for 32bpp (left is on 16bpp, right is on 32bpp) Display Visual Setting The display setting is the add-on feature in FSL Android release, it is very convenient for end-users to change display property, mostly for the following features: Dual display enablement Display color depth setting(16bpp, 32bpp) Overscan adjustment in horizontal and vertical orientation 4. Issue Diagnosis Application Compatibility Some Android applications may not run correctly on some Android releases. It may cause application compatibility, so check the application in other platforms. For example Neocore and Asphalt 5 can run on Eclair, Froyo, and Gingerbread, but will not correctly run on Honeycomb. GPU Compatibility Some game UIs may not correctly display on our Android release. When encountering this kind of issue, the customer can check whether it is caused by the game using an OpenGL extension which our GPU does not support. They can download another data package (for example not extension data package) to have a check. Others Enlarge GPU memory if you encounter UI abnormally displaying after running an application for a while. Some applications need Wifi connections, so monitor the console log to see whether there are any error reports.
查看全文
Description about VPU & IPU usage in Android R13.4 GA release for i.MX6DQ
查看全文
Trace the malloc and expose violate access to freed memory Introduction Libc has a malloc debug framework for difference debugger. Each debugger takes as a libraries, and override the default malloc/free/calloc/realloc/, hooked before calling the real functions. NOTE: This tip assume that you are working with an eng or userdebug build of the platform, not on a production device. Trace the low level malloc/free in bionic Bionic has a malloc debugger called leak debugger, which can record all the malloc/free in low level. And developers can use ddms on host to check each block of memory on heap by malloc. And ddms support convert caller function address to name conver. That makes easy for us to check which component, which function allocated for how many memories. You can turn on memory tracking with debug level 1: $ adb shell setprop libc.debug.malloc 1 $ adb shell stop $ adb shell start You need to restart the runtime so that zygote and all processes launched from it are restarted with the property set. Now all Dalvik processes have memory tracking turned on. You can look at these with DDMS, but first you need to turn on its native memory UI: Open ~/.android/ddms.cfg Add a line "native=true" Upon relaunching DDMS and selecting a process, you can switch to the new native allocation tab and populate it with a list of allocations. This is especially useful for debugging memory leaks. NOTE: to solve the module symbols, please export two env on HOST: $ export PATH=$PATH:<android src>/prebuilt/linux-x86/toolchain/arm-linux-androideabi-4.4.x/bin $ export ANDROID_PRODUCT_OUT=<android src>/out/target/product/<platform> Expose the memory access to freed area In this release he Electric Fence 2.2.0 has been ported to Android. it's also a memory debugger tool as above leak debugger. It helps you detect two common programming bugs: software that overruns the boundaries of a malloc() memory allocation, and software that touches a memory allocation that has been released by free(). It will dump the call stack and mmap of the process, if the malloc/free is not called with correct parameters. It will also make a segment fault, when applications want to access the address which is freed. The usage of efence is almost same as above, which we define it's debug level to 15: $ adb shell setprop libc.debug.malloc 15 After setting this property, you can run your applications, and if there's any memory leakage, logcat will show information. Example: Access the memory, which has been freed already: root@android:/data # setprop libc.debug.malloc 15 I/libc    ( 4136): setprop using MALLOC_DEBUG = 1 (leak checker) root@android:/data # ./memtest I/libc    ( 4138): ./memtest using MALLOC_DEBUG = 15 (efence) F/libc    ( 4138): Fatal signal 11 (SIGSEGV) at 0x4015bff4 (code=2) I/DEBUG  ( 3856): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** I/DEBUG  ( 3856): Build fingerprint: 'freescale/sabresd_6dq/sabresd_6dq:4.0.4/R13.5-rc1/eng.b03824.20120711.11133 8:eng/test-keys' I/DEBUG  ( 3856): pid: 4138, tid: 4138  >>> ./memtest <<< I/DEBUG  ( 3856): signal 11 (SIGSEGV), code 2 (SEGV_ACCERR), fault addr 4015bff4 I/DEBUG  ( 3856):  r0 00000000  r1 00000002  r2 40151c6c  r3 00000000 I/DEBUG  ( 3856):  r4 4015bff4  r5 bec75a54  r6 00000001  r7 bec75a5c I/DEBUG  ( 3856):  r8 00000000  r9 00000000  10 00000000  fp 00000000 I/DEBUG  ( 3856):  ip 00000000  sp bec75a20  lr 40133f8f  pc 0000a554  cpsr 60000010 I/DEBUG  ( 3856):  d0  203f810033915fe5  d1  0000000000000000 I/DEBUG  ( 3856):  d2  0000000000000000  d3  0000000000000000 I/DEBUG  ( 3856):  d4  0000000000000000  d5  0000000000000000 I/DEBUG  ( 3856):  d6  0000000000000000  d7  204cb48d00000000 I/DEBUG  ( 3856):  d8  0000000000000000  d9  0000000000000000 I/DEBUG  ( 3856):  d10 0000000000000000  d11 0000000000000000 I/DEBUG  ( 3856):  d12 0000000000000000  d13 0000000000000000 I/DEBUG  ( 3856):  d14 0000000000000000  d15 0000000000000000 I/DEBUG  ( 3856):  d16 41c0265a46a47ae1  d17 3f50624dd2f1a9fc I/DEBUG  ( 3856):  d18 41c9c8aff2800000  d19 0000000000000000 I/DEBUG  ( 3856):  d20 0000000000000000  d21 0000000000000000 I/DEBUG  ( 3856):  d22 0000000000000000  d23 0000000000000000 I/DEBUG  ( 3856):  d24 0000000000000000  d25 0000000000000000 I/DEBUG  ( 3856):  d26 0000000000000000  d27 0000000000000000 I/DEBUG  ( 3856):  d28 0000000000000000  d29 0000000000000000 I/DEBUG  ( 3856):  d30 0000000000000000  d31 0000000000000000 I/DEBUG  ( 3856):  scr 00000010 I/DEBUG  ( 3856): I/DEBUG  ( 3856):          #00  pc 0000a554  /data/memtest I/DEBUG  ( 3856):          #01  pc 00016834  /system/lib/libc.so (__libc_init) I/DEBUG  ( 3856): I/DEBUG  ( 3856): code around pc: I/DEBUG  ( 3856): 0000a534 e3a0000a ebfff8d1 e3a01001 e1a00004  ................ I/DEBUG  ( 3856): 0000a544 e5c4100a ebfff8d9 e3560001 e3a03000  ..........V..0.. I/DEBUG  ( 3856): 0000a554 e5c43000 0a000064 e59f21f0 e2857004  .0..d....!...p.. I/DEBUG  ( 3856): 0000a564 e5954004 e08f1002 e1a00004 ebfff8c0  .@.............. I/DEBUG  ( 3856): 0000a574 e3500000 0a00003f e59fc1d4 e1a00004  ..P.?........... I/DEBUG  ( 3856): I/DEBUG  ( 3856): code around lr: I/DEBUG  ( 3856): 40133f6c 68200701 0001f020 454e1046 2e00d018  .. h ...F.NE.... I/DEBUG  ( 3856): 40133f7c 2102da01 1c81e000 43394338 f7eb4622  ...!....8C9C"F.. I/DEBUG  ( 3856): 40133f8c 4605ed56 d1ec2800 da062e00 0101f008  V..F.(.......... I/DEBUG  ( 3856): 40133f9c f06f4620 f7ea4200 4628e8d4 87f0e8bd  Fo..B....(F.... I/DEBUG  ( 3856): 40133fac eff0f7e9 6003234b 30fff04f bf00e7f6  ....K#.`O..0.... I/DEBUG  ( 3856): I/DEBUG  ( 3856): memory map around addr 4015bff4: I/DEBUG  ( 3856): 40150000-4015a000 I/DEBUG  ( 3856): 4015a000-4015d000 I/DEBUG  ( 3856): 4015d000-4015e000 I/DEBUG  ( 3856): I/DEBUG  ( 3856): stack: I/DEBUG  ( 3856):    bec759e0  00000000 I/DEBUG  ( 3856):    bec759e4  00000000 I/DEBUG  ( 3856):    bec759e8  00000000 I/DEBUG  ( 3856):    bec759ec  4012090f  /system/lib/libefence.so I/DEBUG  ( 3856):    bec759f0  4015a014 I/DEBUG  ( 3856):    bec759f4  00002000 I/DEBUG  ( 3856):    bec759f8  00000004 I/DEBUG  ( 3856):    bec759fc  40120df1  /system/lib/libefence.so I/DEBUG  ( 3856):    bec75a00  4015bff4 I/DEBUG  ( 3856):    bec75a04  bec75a54  [stack] I/DEBUG  ( 3856):    bec75a08  00000001 I/DEBUG  ( 3856):    bec75a0c  bec75a5c  [stack] I/DEBUG  ( 3856):    bec75a10  00000000 I/DEBUG  ( 3856):    bec75a14  400d9167  /system/lib/libc.so I/DEBUG  ( 3856):    bec75a18  df0027ad I/DEBUG  ( 3856):    bec75a1c  00000000 I/DEBUG  ( 3856): #00 bec75a20  00008924  /data/memtest I/DEBUG  ( 3856):    bec75a24  bec75a54  [stack] I/DEBUG  ( 3856):    bec75a28  00000001 I/DEBUG  ( 3856):    bec75a2c  bec75a5c  [stack] I/DEBUG  ( 3856):    bec75a30  00000000 I/DEBUG  ( 3856):    bec75a34  400d9837  /system/lib/libc.so I/DEBUG  ( 3856): #01 bec75a38  00000000 I/DEBUG  ( 3856):    bec75a3c  00000000 I/DEBUG  ( 3856):    bec75a40  00000000 I/DEBUG  ( 3856):    bec75a44  00000000 I/DEBUG  ( 3856):    bec75a48  00000000 I/DEBUG  ( 3856):    bec75a4c  b00046ef  /system/bin/linker I/DEBUG  ( 3856):    bec75a50  00000001 I/DEBUG  ( 3856):    bec75a54  bec75b79  [stack] I/DEBUG  ( 3856):    bec75a58  00000000 I/DEBUG  ( 3856):    bec75a5c  bec75b83  [stack] I/DEBUG  ( 3856):    bec75a60  bec75b8f  [stack] I/DEBUG  ( 3856):    bec75a64  bec75ba2  [stack] I/DEBUG  ( 3856):    bec75a68  bec75bc5  [stack] I/DEBUG  ( 3856):    bec75a6c  bec75bde  [stack] I/DEBUG  ( 3856):    bec75a70  bec75c08  [stack] I/DEBUG  ( 3856):    bec75a74  bec75c20  [stack] I/DEBUG  ( 3856):    bec75a78  bec75c57  [stack] I/DEBUG  ( 3856):    bec75a7c  bec75c61  [stack] I/BootReceiver( 3551): Copying /data/tombstones/tombstone_00 to DropBox (SYSTEM_TOMBSTONE) D/dalvikvm( 3551): GC_CONCURRENT freed 398K, 10% free 8805K/9735K, paused 3ms+5ms [2] + Segmentation fault  ./memtest
查看全文
document about how to use usb camera on imx6 android-4.0 platform.
查看全文
1. Making information easier for our members to find, and make the community more effective: If you submit a discussion and it is a question, check the “Mark this discussion as a question” box when you are creating the discussion. This will highlight the discussion as a request for help. Acknowledge a reply as “Answer” when it answers your question, or identify it as “Helpful” if a reply was helpful. This will recognize the members who are taking the time to help other members. Select applicable categories when entering your discussions. This makes it easy to filter on and view related content in the “Content” tab. Tag everything. This helps surface the most relevant search results and it helps to bring appropriate content to your “What Matters” Activity stream. 2. Getting FSL help: Even though you can have and use multiple accounts in the community, It is generally good practice to use a single account.  Furthermore, it behooves community members to use your primary Freescale.com account when submitting community questions.  This allows Freescale support to see more information about you that you may not expose in your community profile, such as your company name and location.  This information helps us to assign the proper support resources to your issue.
查看全文
Introduction This guide provides a step by step explanation of what is involved in adding a new WiFi driver and making a new WiFi card work well in a custom Android build. (This guide was written for Android 4.1 but should be applicable to previous Android releases and hopefully future releases.) Contents Understand how Android WiFi works Port WiFi driver. Compile a proper wpa_supplicant in your BoardConfig.mk Modify your wifi.c in HAL. Launch wpa_supplicant and dhcpcd services in init.rc. Several debug tips. Understand How Android WiFi Works As the following figure, Android wireless architecture can be divided into three parts: Java Framework(WifiManager, WifiMonitor etc..), HAL(wifi.c,wpa_supplicant,netd) kernel space modules(wireless stack, wifi drivers) Java Framework communicate with wpa_supplicant using native interface (wifi.c). Wpa_supplicant and netd uses wireless extension or nl80211 to control WiFi drivers. Port WiFi driver Usually WiFi driver is provided as a kernel module. There are mainly two types of Android WiFi architecture:nl80211 and wext. With the implementation of nl80211/cfg80211 many wireless drivers in main line kernel  support nl80211 interface instead of wireless extension. For different vendors’ WiFi drivers, writing one Android.mk to add its compile into Android is what you should do. Here take atheros’s AR6kl as an example: ath6kl_module_file :=drivers/net/wireless/ath/ath6kl/ath6kl_sdio.ko $(ATH_ANDROID_SRC_BASE)/$(ath6kl_module_file):$(mod_cleanup) $(TARGET_PREBUILT_KERNEL) $(ACP)         $(MAKE) -C $(ATH_ANDROID_SRC_BASE) O=$(ATH_LINUXPATH) ARCH=arm CROSS_COMPILE=$(ARM_EABI_TOOLCHAIN)/arm-eabi- KLIB=$(ATH_\ LINUXPATH) KLIB_BUILD=$(ATH_LINUXPATH)         $(ACP) -fpt $(ATH_ANDROID_SRC_BASE)/compat/compat.ko $(TARGET_OUT)/lib/modules/         $(ACP) -fpt $(ATH_ANDROID_SRC_BASE)/net/wireless/cfg80211.ko $(TARGET_OUT)/lib/modules/ include $(CLEAR_VARS) LOCAL_MODULE := ath6kl_sdio.ko LOCAL_MODULE_TAGS := optional LOCAL_MODULE_CLASS := ETC LOCAL_MODULE_PATH := $(TARGET_OUT)/lib/modules LOCAL_SRC_FILES := $(ath6kl_module_file) include $(BUILD_PREBUILT) Compile a proper wpa_supplicant in your BoardConfig.mk In Android’s external directory, there are two wpa_supplicant_* projects. For wext-based wifi driver, wpa_supplicant_6 can be used. For nl80211-based WiFi driver, wpa_supplicnat_8 can only be used. But if WiFi vendors supply their own customized wpa_supplicant, it will be much easier to debug the communication between wpa_supplicant and WiFi drivers. No matter which supplicant  you choose, just control their compile in your BoardConfig.mk. Take atheros’s ath6kl as an example: ifeq ($(BOARD_WLAN_VENDOR),ATHEROS) BOARD_WLAN_DEVICE                        := ar6003 BOARD_HAS_ATH_WLAN                      := true WPA_SUPPLICANT_VERSION                  := VER_0_8_ATHEROS WIFI_DRIVER_MODULE_PATH                  := "/system/lib/modules/ath6kl_sdio.ko" WIFI_DRIVER_MODULE_NAME                  := "ath6kl_sdio" WIFI_DRIVER_MODULE_ARG                  := "suspend_mode=3 wow_mode=2 ar6k_clock=26000000 ath6kl_p2p=1" WIFI_DRIVER_P2P_MODULE_ARG              := "suspend_mode=3 wow_mode=2 ar6k_clock=26000000 ath6kl_p2p=1 debug_mask=0x2413" WIFI_SDIO_IF_DRIVER_MODULE_PATH          := "/system/lib/modules/cfg80211.ko" WIFI_SDIO_IF_DRIVER_MODULE_NAME          := "cfg80211" WIFI_SDIO_IF_DRIVER_MODULE_ARG          := "" WIFI_COMPAT_MODULE_PATH                  := "/system/lib/modules/compat.ko" WIFI_COMPAT_MODULE_NAME                  := "compat" WIFI_COMPAT_MODULE_ARG                  := "" endif then you need to provide a proper wpa_supplicant.conf  for your device. wpa_supplicant.conf  is very important because the control socket for android is specified in this file(ctrl_interface=). This file should be copied to /system/etc/wifi. Minimum required config options in wpa_supplicant.conf : There are two different ways in which wpa_supplicant can be configured, one is to use a "private" socket in android namespace, created by socket_local_client_connect() function in wpa_ctrl.c and another is by using a standard UNIX socket. Android private socket ctrl_interface=wlan0 update_config=1 - Unix standard socket ctrl_interface=DIR=/data/system/wpa_supplicant GROUP=wifi update_config=1 Modify your wifi.c in HAL Here what you should do is modifying some codes like wifi_load_driver and wifi_unload_driver. For Broadcom or CSR’s wifi driver, you can directly use the original wifi.c. But for atheros’s ath6kl driver, there are total three  .ko modules to install. So some micro variables and codes need to be changed to adapt it. Launch wpa_supplicant and dhcpcd services in init.rc If you have configured to use android private socket, you should do like this: service wpa_supplicant /system/bin/wpa_supplicant -Dwext -iwlan0 -c / data/misc/wifi /wpa_supplicant.conf socket wpa_wlan0 dgram 660 wifi wifi disabled oneshot or if you have configured to use unix standard socket, you should do like this: service wpa_supplicant /system/bin/wpa_supplicant -Dwext -iwlan0  -c/data/misc/wifi/wpa_supplicant.conf disabled oneshot If WiFi driver is not “wext” but “nl80211”, you should change it to –Dnl80211. For dhcpcd, you should lunch it like the following: service dhcpcd_wlan0 /system/bin/dhcpcd -ABKL     class late_start     disabled oneshot The parameters “-ABKL” can largely enhance wifi connection speed.  About what “ABKL” stand for, you can refer to dhcpcd’s GNU manual. Several debug tips Incorrect permissions will result in wpa_supplicant not being able to create/open the control socket andlibhardware_legacy/wifi/wifi.c won't connect. Since Google modified wpa_supplicant to run as wifi user/group the directory structure and file ownership should belong to wifi user/group (see os_program_init() function in wpa_supplicant/os_unix.c ). Otherwise errors like: E/WifiHW  (  😞 Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": No such file or directory will appear. Also wpa_supplicant.conf should belong to wifi user/group because wpa_supplicant will want to modify this file. How to Enable debug for wpa_supplicant.               By default wpa_supplicant is set to MSG_INFO that doesn't tell much.                    To enable more messages:                 modify common.c and set wpa_debug_level = MSG_DEBUG                 modify common.h and change #define wpa_printf from if ((level) >= MSG_INFO) to if ((level) >= MSG_DEBUG)         3. WiFi driver’s softmac.               For most vendors’ WiFi driver, the mac address is fixed. We should add one softmac rule to let WiFi driver’s mac is unique for each board.
查看全文