i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Quick guide on how to get started with Linux on i.MX 6UL EVK board using MfgTool from L3.14.52 release: Download MfgTool from here (Version is IMX6_L3.14.52_MFG_TOOL (REV L3.14.52_1.1.0) under “Programmers (Flash, etc.)”): http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6ultralite-processor-low-power-secure-arm-cortex-a7-core:i.MX6UL?fpsp=1&tab=Design_Tools_Tab Unpack the archive and unpack mfgtools-with-rootfs.tar.gz edit cfg.ini and change following entries: mmc needs to be set to 1 6uluboot needs to be set to evk 6uldtb needs to be set to 14x14-evk Connect USB cable, USB debug cable to your PC.Open terminal to serial port (115200, 8N1). Insert uSD card to the slot on i.MX 6UL CPU module Set boot switches on SW602 [2:1] to on:off Power on the board Start MfgTool2.exe. HID device should be detected. Press "Start" button. Downloading should start. Executed steps are visible in the debug terminal. When you see "Done" printed, downloading has succeeded. Set boot switches on SW602 [2:1] to off:on, SW601[4:1] TO off:on:off:on Reset i.MX 6UL EVK (or power off then on), and boot to Linux. In case of any error, inspect serial output on debug terminal to see what has gone wrong. This document was generated from the following discussion: Getting started with i.MX6UL EVK and MfgTool L3.14.52
查看全文
In some customers’ design they use the different DRAM from the one used on our reference board. So customers need to customize the DRAM to make it work well on their design. About the i.MX6x hardware design customers can refer to IMX6DQ6SDLHDG.pdf and the section 5 DRAM interface requirements for migration on AN4397. After finishing the hardware design there are two tools important for the DRAM boot up and debug: DRAM Register Programming aid And DRAM Stress Test 1\DRAM Register Programming aid Our expert team create the script to make it easier to work on DDR initialization. You can see all the scripts on different chips and the link is: i.MX Design&Tool Lists The script include 3 sections, when you open it you can see the details. Run basic DDR initialization and test memory and open a debugger memory window pointing to the DDR memory map starting address. Try writing a few words and verify if they can be read correctly. If not, re-check the DDR initialization sequence and if the DDR has been correctly soldered onto the board. It is also recommended to re-check the schematic to ensure the DDR memory has been connected to the SoC correctly. In some cases, a DRAM calibration routine may need to be executed. About the details use and introduction on this script you can refer to Freescale i.MX6 DRAM Port Application Guide-DDR3 After configure the DRAM, you need to use the DRAM Stress Test to perform calibrations the performance and then regulate some parameters. 2\DRAM Stress Test DDR_Stress_Tester is a software application for fine tuning DDR parameters and verifying DDR performance on i.MX6 boards. It performs write leveling, DQS gating, read/write delay calibration on the target board to match the layout of the board and archive the best DDR performance. In addition, the stress test can help the user to verify the DDR performance on their boards. The DDR stress test tool serves two purposes. First, it can perform calibrations for DDR3 to match the MMDC PHY delay settings with PCB for optimal DRAM performance. The process is fully automatic, and therefore the customers can get there DDR3 working in much shorter time. In addition, the tool can run a memory stress test to verify the DDR3 functionality as well as the reliability. The stress test can help verifying the hardware connections, MMDC registers parameters, and DDR3 mode registers setting. The most important purpose of the test is that it allows the customers to verify that the DDR3 operations are stable on their board. The newest version  of DRAM Stress Test tool you can see in our community: i.MX6/7 DDR Stress Test Tool V2.51 And the old version you can see in the follow link: i.MX6 DDR Stress Test Tool V1.0.3 About how to use this tool you can read the use guide. Besides , you also can refer to the Freescale i.MX6 DRAM Port Application Guide-DDR3 By the way, if customers use the different DRAM from our reference design when the use the mfgtool to download the images, they need to build manufacturing images for mfgtool. Take the Linux 3.14.52 BSP as an example: $ bitbake fsl-image-mfgtool-initramfs Hope this can help you.
查看全文
Not all of imx6 boards can support SDR104, refer to imx6sx Reference Manual, BOOT_CFG1[2:3] = 11 is SDR104 normally hardware support 3.3v, but SDR104 only supports 1.8v. refer to the AI board schematic, you can find as below: For current yocto driver, which already supports sd3.0 standard, but kernel should change something to support this, for customer, one can refer to the source code in the yocto, the path:root/arch/arm/boot/dts/imx6sx-sdb.dts or path:root/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi For supporting SDR104, should change the dts file, because of 1.8v only, should remove no-1-8-v in the source code, then add vmmc-supply according to the dts file above. for example, based on the schematic, you can find: &usdhc1 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_usdhc1>; cd-gpios = <&gpio1 1 0>; no-1-8-v; keep-power-in-suspend; enable-sdio-wakeup; status = "okay"; }; &usdhc3 { pinctrl-names = "default", "state_100mhz", "state_200mhz"; pinctrl-0 = <&pinctrl_usdhc3>; pinctrl-1 = <&pinctrl_usdhc3_100mhz>; pinctrl-2 = <&pinctrl_usdhc3_200mhz>; cd-gpios = <&gpio6 15 0>; wp-gpios = <&gpio1 13 0>; /* * Due to board issue, we can not use external regulator for card slot * by default since the card power is shared with card detect pullup. * Disabling the vmmc regulator will cause unexpected card detect * interrupts. * HW rework is needed to fix this isssue. Remove R695 first, then you * can open below line to enable the using of external regulator. * Then you will be able to power off the card during suspend. This is * especially needed for a SD3.0 card re-enumeration working on UHS mode * Note: reg_sd3_vmmc is also need to be enabled */ /* vmmc-supply = <&reg_sd3_vmmc>; */ keep-power-in-suspend; enable-sdio-wakeup; status = "okay"; }; reg_sd3_vmmc: sd3_vmmc{ compatible = "regulator-fixed"; regulator-name = "P3V3_SDa_SWITCHED"; regulator-min-microvolt = <3300000>; regulator-max-microvolt = <3300000>; gpio = <&gpio7 8 GPIO_ACTIVE_HIGH>; enable-active-high; /* remove below line to enable this regulator */ status="disabled"; };
查看全文
i.MX6UL CSI (CMOS Sensor Interface) host port support BT.656(CCIR656) Interlace mode by hardware.  It can received  PAL(720pix X 576pix) and NTSC(720pix X 480 pix) format data from camera. This document introduce how to add this feature to Linux L3.14.38-ga and receive ADV7180 output. Software: yocto L3.14.38-ga. Hareware:  i.mx6ul-evk + ADV7180. ADV7180: PAL 720pix X576pix  ,  YUV4:2:2(UYVY) interlace output. LCD Display screen resolution:  800 X 480,  RGB565. 1) Note : For BT.656 mode,   parallel data port is  CSI_DATA[9:2], not CSI_DATA[13:6].    So,  "pinctrl_csi1" is the same as "ov5640" in "imx6ul-14x14-evk.dts": pinctrl_csi1: csi1grp {    fsl,pins = <     MX6UL_PAD_CSI_MCLK__CSI_MCLK  0x1b088     MX6UL_PAD_CSI_PIXCLK__CSI_PIXCLK 0x1b088     MX6UL_PAD_CSI_VSYNC__CSI_VSYNC  0x1b088     MX6UL_PAD_CSI_HSYNC__CSI_HSYNC  0x1b088     MX6UL_PAD_CSI_DATA00__CSI_DATA02 0x1b088     MX6UL_PAD_CSI_DATA01__CSI_DATA03 0x1b088     MX6UL_PAD_CSI_DATA02__CSI_DATA04 0x1b088     MX6UL_PAD_CSI_DATA03__CSI_DATA05 0x1b088     MX6UL_PAD_CSI_DATA04__CSI_DATA06 0x1b088     MX6UL_PAD_CSI_DATA05__CSI_DATA07 0x1b088     MX6UL_PAD_CSI_DATA06__CSI_DATA08 0x1b088     MX6UL_PAD_CSI_DATA07__CSI_DATA09 0x1b088     MX6UL_PAD_SNVS_TAMPER5__GPIO5_IO05 0x17059            /* configue csi_reset in this case */     MX6UL_PAD_SNVS_TAMPER6__GPIO5_IO06 0x17059            /* configure csi_en in this case*/    > 2) Applay the video driver patches as attatched.   $git am 0001-Enable-CSI-support-BT656-interlace-and-add-adv7180.patch 3) Build the kernel.    make imx_v7_defconfig    make -j4 4) Use  unit_tests "mx6s_v4l2_capture_uyvy.out" to test it,  source code is attached "mx6s_v4l2_capture.c": Copy "mx6s_v4l2_capture_uyvy.out" to target device FS  "/unit_tests" folder, and run it like this: ./mx6s_v4l2_capture_uyvy.out -m 0 -t 50 -d /dev/video0 5) In this "mx6s_v4l2_capture.c" demo test code,   it can utilize software algorithm to implement CSC(Color Space Conversion) from YUV4:2:2 to RGB. PXP module can realize hardware CSC and image resize. 6) How to use CSI + PXP to preview camera, refer to  unit_tests "imx-test" package "pxp_v4l2_test" - "pxp_v4l2_test.c"  . Run following command in Target device FS:   /unit_tests /*Record raw camera UYVY data(720x576) to save in test1.yuv */ ./mx6s_v4l2_capture_uyvy.out -m 0 -t 10 -of test1.yuv -d /dev/video0 /*Play this test1.yuv file(UYVY) by PXP engine and resize to full screan(800x480) */ ./pxp_v4l2_test.out -sx 800 -sy 480 -res 720:576 -dst 0:0:800:480 -a 100 -f 5 test1.yuv BLANK 7) The "pxp_v4l2_preview_test.c" demo attached  is  a TV-in demo for i.MX6ul which support ADV7180 camera preview by PXP in time. This demo implements scaling image frame to full screen, Alpha blending and Composite two image together function by PXP hardware.
查看全文
1. Enable QtMultimedia 1) In “source/meta-qt5/recipes-qt/qt5/qtmultimedia_git.bb”, add “gstreamer” at the end of “PACKAGECONFIG ??=” .      For example on  L3.14.52  bsp, build  x11  backend: PACKAGECONFIG ??= "${@bb.utils.contains('DISTRO_FEATURES', 'alsa', 'alsa', '', d)} \                    ${@bb.utils.contains('DISTRO_FEATURES', 'pulseaudio', 'pulseaudio', '', d)} \                    gstreamer" 2) Build qtmultimedia:  bitbake qtmultimedia 3) Copy the built package to target file system.      For example : cp  -a ./build-x11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtmultimedia/5.5.0+gitAUTOINC+46a83d5b86-r0/image/usr/   /usr   export  DISPLAY=:0 Video example application located at : /usr/share/qt5/examples/multimedia/video/qmlvideo 2. Enable Qt Logging Info export  QT_LOGGING_RULES=<category>[.type]=ture|false      For example: Turn on all debug logging:      export QT_LOGGING_RULES=*.debug=true Turn on all logging level of all multimedia module:      export QT_LOGGING_RULES=qt.multimedia.*=true 3. Performance Checking Gstreamer: overlaysink fps=51.585      gst-launch-1.0 playbin uri=file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi  video-sink=”overlaysink sync=false” Gstreamer: glimagesink fps=43.850      gst-launch-1.0 playbin uri=file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi video-sink="glimagesink sync=false" Qtmultimedia: fps=45.201      ./qmlvideo  -url file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi -hide-perf Current qt5 multimedia has a special video node for imx6 at     "/src/plugins/videonode/imx6" which uses GPU DirectVIV to accelerate the video rendering. So  the rendering performance is almost same as the glimagesink. For check the free run frame rate, the qt multimedia source need change a little bit to set sink sync as false and calculate the real video rendering rate. Set sync as false: In "/src/plugins/gstreamer/mediaplayer/qgstreamerplayersession.cpp" QGstreamerPlayerSession::playbinNotifySource(): -       g_object_set(G_OBJECT(self->m_videoSink), "sync", !self->m_isLiveSource, NULL); +       g_object_set(G_OBJECT(self->m_videoSink), "sync", false/!self->m_isLiveSource/, NULL); Get fps: In "/src/gsttools/qgstvideorenderersink.cpp" +#include <QTime> +gint g_frame_showed; +QTime g_time; + bool QVideoSurfaceGstDelegate::start(GstCaps *caps) … +   g_frame_showed = 0; +   g_time.restart(); … void QVideoSurfaceGstDelegate::stop() … +   printf(">>>>> fps=%f:\n", (gdouble)g_frame_showed*1000/g_time.elapsed()); … bool  QVideoSurfaceGstDelegate::handleEvent(QMutexLocker *locker) …             const bool rendered = m_activeRenderer->present(m_surface, buffer); +   g_frame_showed++; … Or use the attached patch: qtmultimedia_fps_check.diff 4. Streaming Playing:  HTTP RTP RTSP HTTP: ./qmlvideo -url http://10.192.225.205/streaming/http/H264_HP13_1280x720_29_2850_AAC_LC_44_64_NobodyMTV.mp4 RTSP: ./qmlvideo -url rtsp://10.192.225.205/MPEG4_SP1_720x576_30fps_282_AMRNB_TVC.mp4 RTP: QT mediaplayer use gstreamer playbin as the backend, playbin don’t support rtp address as uri. So QT mediaplayer can’t support RTP playing directly. 5. Audio Recording /usr/share/qt5/examples/multimedia/audiorecorder/audiorecorder This is a widget application, not a QML application. It use QAudioRecorder as its background worker. By default it will use pulsesrc and lamemp3enc to recorder audio as mkv file at user home folder with name of clip_0001.mkv, clip_0002.mkv, and so on. If need special pipeline for recording, example use imxmp3enc to record mp3 files, we need change the function GstElement *QGstreamerCaptureSession::buildEncodeBin in  “src/plugins/gstreamer/mediacapture/qgstreamercapturesession.cpp” as well as QGstreamerMediaContainerControl(QObject *parent) in “src/plugins/gstreamer/mediacapture/qgstreamermediacontainercontrol.cpp” 6. Camera Widgets Application: “/usr/share/qt5/examples/multimediawidgets/camera/camera” QML Application: “/usr/share/qt5/examples/multimedia/declarative-camera/declarative-camera” Qt Multimedia has some bugs on L3.14.52 with QCamera for recording. Use the attached patches: 0001-gstreamer-fix-camerabin-not-negotiated-error.patch 0001-QCamera-can-t-set-recording-container-format-video-a.patch 0002-QtCamera-change-default-encoding-parameters-to-use-N.patch If you want use overlaysink as the preview sink, then use following patch: 0003-use-overlaysink-as-the-preview-sink.patch Both applications need to set environment variable QT_GSTREAMER_CAMERABIN_VIDEOSRC to use imxv4l2src If camera device is other than /dev/video0, set environment variable QT_GSTREAMER_CAMERABIN_VIDEOSRC_DEVICE to the right camera device, such as "/dev/video1" ,  for example: export QT_GSTREAMER_CAMERABIN_VIDEOSRC=imxv4l2src export DISPLAY=:0 export QT_GSTREAMER_CAMERABIN_VIDEOSRC_DEVICE="/dev/video1" By default, the “post-preview” feature of camerabin was disabled by the patches provided, since the imxv4l2src can’t work with “post-preview” internal “videoconvert” element. To enable “post-preview”  feature, one need uncomment following line //g_object_set(G_OBJECT(m_camerabin), POST_PREVIEWS_PROPERTY, TRUE, NULL); in “/qtmultimedia/src/plugins/gstreamer/camerabin/camerabinsession.cpp”, Function: CameraBinSession::CameraBinSession(GstElementFactory *sourceFactory, QObject *parent) And Change “videoconvert” to “imxvideoconvert_g2d” or “imxvideoconvert_ipu” or “imxvideoconvert_pxp” in line : csp = gst_element_factory_make ("videoconvert", "preview-vconv"); of  file “/gstreamer1.0-plugins-bad/gst-libs/gst/basecamerabinsrc/gstcamerabinpreview.c”  function: GstCameraBinPreviewPipelineData *gst_camerabin_create_preview_pipeline (GstElement * element,   GstElement * filter)
查看全文
Introduction Even though we have provided MQX OS support for imx6SX M4 core, we don’t need such complex operation system running on M4 core in some cases. For users who want to simplify and accelerate their M4 application development, bare metal codes without OS support is also a good choice. This demo will show how to develop bare metal codes for i.MX SoloX. Verified Platform imx6sx sabresd Application Notes How to develop bare metal codes running on M4 core .pdf Demo files a9_launch_m4: Run at A9 core and launch M4 core m4_apps: Run at M4 core
查看全文
Following docs(English or Chinese version) are also can be referred as a hand on guide. Freescale i.MX6 DRAM Port Application Guide-DDR3 飞思卡尔i.MX6平台DRAM接口高阶应用指导-DDR3篇 Please find i.Mx6DQSDL LPDDR2 Script Aid through below link. i.Mx6DQSDL LPDDR2 Script Aid Please find i.Mx6DQSDL DDR3 Script Aid through below link. i.Mx6DQSDL DDR3 Script Aid Please find i.MX6SX DDR3 Script Aid through below link.. i.MX6SX DDR3 Script Aid Any questions are welcome! Change History: 0.02 - Add total 1Gbit density supporting.
查看全文
Hello,   recently I'm running CTS test on MX6Q SabreSD to fix some of the issues my customer found, and found that "factory reset" is an important step during the test-environment setup but not mentioned in i.MX CTS test report.   "Factory reset" is need on official CTS page: Setting up CTS | Android Open Source Project     Without factory reset, the CTS test result in "android.core.tests.libcore.package.libcore" package looks like: There are total 8 failed items.     If we run "factory reset" before conduct the CTS test in in "android.core.tests.libcore.package.libcore" package, only 2 failed items found as below:   PS: and those 2 failed items can be waived, according to the test-house of CTS tests. PS1: the test reports of are also attached.       Please do run "factory reset" before CTS test, verified working on 4.2.2 and should also work on the version above according to the pages I found on Google when trying to fix this issue. Unfortunately "factory reset" is not documented in the environment setup process in i.MX CTS test report, you will need this if you are following the steps in i.MX CTS test report.   Best regards, Jim.
查看全文
The default BSP release supports sii902x hdmi card via LCDIF in i.MX6 Solo, but doesn't support it via IPU display interface in i.MX6 Dual/Quad/Plus. The patch provides support for the Sii902x HDMI video driver for i.MX6 Dual/Quad/Plus. Useful documents: MCIMXHDMICARD: Schematic for sii902x hdmi card MCIMX6Q-SMART DEVICE PLATFORM: Schematic for i.MX6 Quad Sabre SDP Software version: Linux 3.14.52_1.1.0-ga Verified platform: imx6q-sabresd imx6qp-sabresd Patch: 0001-video-mxc-sii902x-add-sii902x-hdmi-card-driver.patch 0002-arch-arm-boot-dts-add-sii902x-hdmi-card-devicetree-n.patch Features: Support video mode setup via uboot command; Support video mode setup via device tree; Supprt HDMI hot-plug; Support many video modes and a dynamic switching between them; Notes: The default settings( don't add "video=" to bootcmd) are as follows: ---------------------------------------------------------------------------------------- ------------ /sys/class/graphics/fb0 DISP4 BG - DI1 U:1024x768p-60 ldb 2-layer-fb-bg ------------ /sys/class/graphics/fb1 DISP4 FG overlay 2-layer-fb-fg ------------ /sys/class/graphics/fb2 DISP3 BG - DI1 U:1920x1080p-60 hdmi 2-layer-fb-bg ------------ /sys/class/graphics/fb3 DISP3 FG overlay 2-layer-fb-fg ------------ /sys/class/graphics/fb4 DISP3 BG sii902x_hdmi 1-layer-fb ------------ /sys/class/graphics/fb5 DISP4 BG --------------------------------------------------------------------------------------- If you want sii902x_hdmi to be fb0, you can add following arguments to bootcmd: video=mxcfb0:dev=sii902x_hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:off video=mxcfb2:off video=mxcfb2:off consoleblank=0 Risks: Sometimes the sii902x will fail to read hdmi edid information, and the modelist of this framebuffer will be NULL. At this time, the driver will setup a default video mode which has been tuned  on imx6q-sabresd and imx6qp-sabresd. The default video mode is as follows: /* 1080p @ 56 Hz */ 60, 1920, 1080, 7692, 100, 40, 30, 3, 10, 2, 0, FB_VMODE_NONINTERLACED, 0 The user can modify this default setting for their case. Specially, there are some risks to use 1080p@60 video mode for imx6qp-sabresd. The hdmi device will has no valid hdmi signal output in this case. For example, /* 1080p @ 60 Hz */ 60, 1920, 1080, 6734, 148, 88, 36, 4, 44, 4, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_NONINTERLACED, 0 The user sholud set these values according to hareware parameters.
查看全文
The Linux L3.14.52_1.1.0 GA and i.MX 6SoloX FreeRTOS release is now available on www.nxp.com Files available: # Name Description 1 fsl-yocto-L3.14.52_1.1.0-ga.tar.gz Linux 3.14.52_1.1.0 BSP documentation. 2 L3.14.52_1.1.0-ga_images_MX6QDLSOLO.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo Files 3 L3.14.52_1.1.0-ga_images_MX6SLEVK.tar.gz i.MX 6SololiteEVK Linux Binary Demo Files 4 L3.14.52_1.1.0-ga_images_MX6SXALL.tar.gz i.MX 6SoloX Linux Binary Demo Files 5 L3.14.52_1.1.0-ga_images_MX6UL.tar.gz i.MX 6UltraLite Linux Binary Demo Files 6 L3.14.52_1.1.0_ga-mfg-tools.tar.gz i.MX Manufacturing Toolkit for Linux L3.14.52 BSP 7 L3.14.52_1.1.0-ga_gpu-tools.tar.gz L3.14.52_1.1.0 i.MX VivanteVTK file 8 FreeRTOS_BSP_1.0.0_iMX6SX.exe FreeRTOS™ BSP for the i.MX 6SoloX ARM® Cortex®-M4 core. --- Windows installer 9 FreeRTOS_BSP_1.0.0_iMX6SX.tar.gz FreeRTOS™ BSP for the i.MX 6SoloX ARM® Cortex®-M4 core. --- Linux installer Target boards: i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board i.MX 6SoloLite EVK Board i.MX 6SoloX SABRE-SD Board i.MX 6SoloX SABRE-AI Board i.MX 6UltraLite EVK Board What’s New: LinuxBSP New features added for all supported boards: Yocto Project upgraded to version 1.8 Fido. Supports the GCC 4.9.2 toolchain. The Linux kernel is upgraded to v3.14.52. The U-Boot is upgraded to 2015.04. New graphics features: GPU driver upgraded to Vivante v5.0.11p7.4. DirectFB support removed. XWayland support added. Last release to provide graphics software floating point binaries. New multimedia features and changes: Qt 5.5 support integrated, which supports hardware accelerated QML video. Qt 5 is not supported for SoC without hardware graphics. Qt 5 video is not supported on SoC without VPU. Video compositing plugins based on PXP are supported. GStreamer playback engine API is supported, providing high level APIs for media playback and operations. Video overlay composition meta (meta:GstVideoOverlayComposition) is supported in i.MX video sinks, convert and compositor. This feature accelerates the text image (such as subtitle, timestamp) blending with video in these plugins with hardwares. Supports the Broadcom/Murata BCM4339 Bluetooth/Wi-Fi module. FreeRTOS: Add Peripheral support: i.MX 6SoloX ADC, i.MX 6SoloX CCM, i.MX GPIO, i.MX I2C, i.MX MU, i.MX UART, i.MX WDOG, ECSPI, EPIT, FlexCAN, LEME, RDC, SEMA4 Add Multi-core communication support: RPMsg More details, please refer to formal Release Notes.
查看全文
This is a HW design checklist for customer's reference. Please read and fill it in carefully before requesting a schematic review.
查看全文
This tool is also for emmc user partition mirror. Just give this tool the emmc files. The typical use case is for emmc mass production by emmc offline programming. Ver 0.4.0 2/14/2017 Support Android 7 Nougat. AndroidSDCARDMirrorCreator_Version_0.4.0_02142017.tgz Ver 0.3.2: 6/13/2016 Using static link simg2img AndroidSDCARDMirrorCreator_Version_0.3.2_06132016.tgz Ver 0.3.1: 5/31/2016 Remove some redundent code   AndroidSDCARDMirrorCreator_Version_0.3.1_05312016.tgz Ver 0.3: 5/25/2016 Add Marshmallow partition layout AndroidSDCARDMirrorCreator_Version_0.3_05252016.tgz Ver 0.2: Add Lollipop partition layout 1. Directory AndroidSDCARDMirrorCreator |-- AndroidSDCARDMirrorCreator.sh        --- main script |-- CFG.INC                              --- configuration file |-- KitKat_LAYOUT.INC                    --- KitKat partition layout |-- LAYOUT.INC -> Lollipop_LAYOUT.INC    --- symbol link to partition layout |-- Lollipop_LAYOUT.INC                  --- Lollipop partition layout `-- readme.txt                           --- this file 2. Need "root" run or "sudo" to run 3. parted and kpartx must be installed    sudo apt-get instal parted kpartx 4. test pass under the debian 8.2 and ubuntu 12.04 5. The AndroidSDCARDMirrorCreator.sh will look for LAYOUT.INC.    please make symbol link to the correct partition layout.    The default symbol link has created for Lollipop_LAYOUT.INC (LAYOUT.INC -> Lollipop_LAYOUT.INC) 6. Command    AndroidSDCARDMirrorCreator.sh -c    AndroidSDCARDMirrorCreator.sh -p 7. Example:    Suppose    The AndroidSDCARDMirrorCreator directory is in    ~/AndroidSDCARDMirrorCreator       The Android Images are in    ~/SD and ~/eMMC       Sdcdard Mirror:    cd ~/SD    ~/AndroidSDCARDMirrorCreator/AndroidSDCARDMirrorCreator.sh -c    eMMC Mirror:    cd ~/eMMC    ~/AndroidSDCARDMirrorCreator/AndroidSDCARDMirrorCreator.sh -c    8. Once the Mirror has been created. Can be reused. Just use kpartx.
查看全文
       There are 8 UART ports on i.mx6ul and one uniform Linux driver for these UARTs. Form UART1~UART6, there is no special operation or attention to use them. But for UART7/UART8, there is a special rule to enable them.       According to i.mx6ul RM, we can see UART7/8 RTS pins are muxed with ENET TX_CLK pins. When SION bit of ENET_TX_CLK is set, we need switch to other MUX mode as input signal for UARTx_RTS. Otherwise, UARTx_RTS will be interrupted by loopback ENET clock signal. So we should set IOMUXC_UART7_RTS_B_SELECT_INPUT and IOMUXC_UART8_RTS_B_SELECT_INPUT registers to 0x2/03 to avoid ENET clock's conflict no matter whether we enable UART7/8 RTS/CTS function or not. Let's summarize the different scenarios to enable UART7/8 as follows: 1. ENET driver is disabled and UART7/8 is enabled. There is no special operation to do, just use UART7/8 like other UARTs 2. ENET and UART7/8 are both enabled. There are two use models, RTS/CTS enabled or disabled.     2a. If we enable RTS/CTS feature and configure RTS/CTS pins in the device tree, of course, we should avoid the conflict between UART CTS/RTS pins and ENET TX_CLK pins. There is no special operation to do becuase your RTS/CTS device tree would automatically set  IOMUXC_UART7_RTS_B_SELECT_INPUT/ IOMUXC_UART8_RTS_B_SELECT_INPUT register to correct value.     2b. If we don't enable RTS/CTS feature and no RTS/CTS pin configuration in devcie tree, we should manually add code to set  IOMUXC_UART7_RTS_B_SELECT_INPUT/  IOMUXC_UART8_RTS_B_SELECT_INPUT register because the default value is 0x0(ENETx_TX_CLK_ALT1) Here is an example to show how to use UART7 on EVK board in scenario 2b. 1. modify imx6ul-14x14-evk.dts to enable UART7     a. remove all  LCD settings to disable lcdif because we configure UART7 TX/RX pin pad to LCD data line     b. add UART7 related settings                &uart7 {                     pinctrl-names = "default";                     pinctrl-0 = <&pinctrl_uart7>;                    status = "okay";                 };               &iomuxc {                   pinctrl-names = "default";                   pinctrl-0 = <&pinctrl_hog_1>;                   ....                           pinctrl_uart7: uart7grp {                           fsl,pins = <                                       MX6UL_PAD_LCD_DATA16__UART7_DCE_TX 0x1b0b1                                       MX6UL_PAD_LCD_DATA17__UART7_DCE_RX 0x1b0b1                           >;                  }; 2. add code to set IOMUXC_UART7_RTS_B_SELECT_INPUT register in arch/arm/mach-imx/mach-imx6ul.c          static void __init imx6ul_init_machine(void)          {               struct device *parent;               void __iomem *iomux;               struct device_node *np;               ...........               imx6ul_pm_init();               np = of_find_compatible_node(NULL,NULL,"fsl,imx6ul-iomuxc");               iomux = of_iomap(np, 0);               writel_relaxed(0x2,iomux+0x650);            } 3. build zImage and imx6ul-14x14-evk.dtb 4. Test in linux console      root@imx6ulevk: ls /dev/ttymxc*                      //you can see ttymxc6 is in the list     root@imx6ulevk: echo hello > /dev/ttymxc6         root@imx6ulevk:
查看全文
The i.MX Android L5.1.1_2.1.0 GA release is now available on the Web Site.  (i.MX6 BSP Updates and Releases à Android) ·        Files available android_L5.1.1_2.1.0-ga_doc.tar.gz​​​ i.MX6 Android L5.1.1_2.1.0 BSP Documentation android_L5.1.1_2.1.0-ga_core_source.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite and i.MX6SX Android L5.1.1_2.1.0 BSP, Source Code for BSP and Codecs. android_L5.1.1_2.1.0-ga_images_6qsabreauto.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.1.1_2.1.0 BSP Binary Demo Files for the SABRE for Automotive Infotainment. android_L5.1.1_2.1.0-ga_images_6dqsabresd.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.1.1_2.1.0 BSP Binary Demo Files for the SABRE Platform and SABRE Board for Smart Devices. android_L5.1.1_2.1.0-ga_images_6slevk.tar.gz i.MX 6Sololite Android L5.1.1_2.1.0 BSP Binary Demo Files for the SoloLite evaluation kit. android_L5.1.1_2.1.0-ga_images_6sx.tar.gz i.MX 6SoloX Android L5.1.1_2.1.0 BSP Binary Demo Files. android_L5.1.1_2.1.0-ga_tools.tar.gz i.MX 6 Family Manufacturing Toolkit for L5.1.1_2.1.0 ·        Supported Hardware SoC/Boards: o  i.MX 6Quad SABRE-SD board and platform o  i.MX 6DualLite SABRE-SD platform o  i.MX 6Quad SABRE-AI board and platform o  i.MX 6QuadPlus SABRE-AI board and platform o  i.MX 6DualLite SABRE-AI board and platform o  i.MX 6SoloLite EVK platform o  i.MX 6SoloX SABRE-SD board o  i.MX 6SoloX SABRE-AI board and platform o  i.MX 7Dual SABRE-SD board and platform ·        Change List Compared to the L5.1.1_2.0.0_6qp-ga release, this release has the following major changes: o  Upgraded the Linux kernel version from the L3.14.38_6qp-ga release to the L3.14.52-ga release. o  Added i.MX 6QuadPlus SABRE-SD board support. o  Enabled Broadcom BCM4339 Wi-Fi and Bluetooth module. o  Fixed screen tearing in recovery mode during factory resetting and OTA upgrading. o  Fixed system hang-up issue when playing some short videos for a long time. o  Moved all Freescale extended API to freescale-extended.jar. o  Enabled the ZRAM function for Android platform to enlarge the memory size. o  Integrated 2015-11 AOSP Security patches. ·        Features For features please consult the release notes. ·        Known issues For known issues and more details please consult the release notes.
查看全文
Some Chinese customers using i.MX series SoC maybe encounter some issues when they download android , u-boot & kernel source code by 'git' command, the following steps will show customer how to get them: 1. Getting repo --No.1 methord # cd ~ # mkdir myandroid # mkdir bin # cd bin # git clone git://aosp.tuna.tsinghua.edu.cn/android/git-repo.git/ <if git failed, use : git clone https://aosp.tuna.tsinghua.edu.cn/android/git-repo.git/> # cd git-repo # cp ./repo ../ --No.2 methord # cd ~ # mkdir bin # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo [Note]Customers can select one of above to get "repo" 2. Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From        REPO_URL = 'https://gerrit.googlesource.com/git-repo' To        REPO_URL = 'git://aosp.tuna.tsinghua.edu.cn/android/git-repo'        like following: ## repo default configuration ## REPO_URL = 'git://aosp.tuna.tsinghua.edu.cn/android/git-repo' REPO_REV = 'stable' 3、Setting email address # cd ~/myandroid # git config --global user.email "[email protected]" # git config --global user.name "weidong.sun" [ Email & Name should be yours] 4、Getting manifest # ~/bin/repo init -u https://aosp.tuna.tsinghua.edu.cn/android/platform/manifest -b android-5.1.1_r1 # cd ~/myandroid/.repo # gedit manifest.xml        Then change the value of fetch to " git://aosp.tuna.tsinghua.edu.cn/android/ ", like following: <manifest>   <remote name="aosp"            fetch="git://aosp.tuna.tsinghua.edu.cn/android/" />   <default revision="refs/tags/android-5.1.1_r1" ...... [Note] android-5.1.1_r1 is version of branch,customer can change it to another. 5、# ~/bin/repo sync          [Note] During runing repo sync, maybe errors will occur like the following: ...... * [new tag]         studio-1.4 -> studio-1.4 error: Exited sync due to fetch errors          Then 'repo sync' exits. But don't worry about it, continue to run the command please ! " ~/bin/repo sync", downloading source code will be continous. 6、Getting Cross Compiler # cd ~/myandroid/prebuilts/gcc/linux-x86/arm # git clone https://aosp.tuna.tsinghua.edu.cn/android/platform/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6 # cd arm-eabi-4.6 # git checkout android-4.4.3_r1 7、Getting linux kernel source code        Probably, customer can't normally get linux kernel by using "git clone" command, she can download it directly from the following weblink:        http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/        At first, create a temperary directory, then download kernel into the directory. see following steps: # cd ~ /Downloads # mkdir linux-kernel   Atfer downloading l5.1.1_2.1.0-ga.tar.gz, use 'tar zxvf l5.1.1_2.1.0-ga.tar.gz' command to decompress it.        Then you can find a subdirectory name " l5.1.1_2.1.0-ga" is created, linux source code is in the directory, we should copy all files in the directory to ~/myandroid/kernel_imx/ # cd ~/myandroid # mkdir kernel_imx # cd kernel_imx # cp -a ~ /Downloads/linux-kernel/l5.1.1_2.1.0-ga ./ 8、Getting uboot source code               Probably, customer can't normally get linux kernel by using "git clone" command, she can download it directly from the following weblink:       http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/        We can use similar way to that of linux kernel to get u-boot source code: # cd ~ /Downloads # mkdir u-boot        Download l5.1.1_2.1.0-ga.tar.gz file, and save it in ~ /Downloads/ u-boot, then decompress it, then u-boot source code will be in ~ /Downloads/ u-boot / l5.1.1_2.1.0-ga/, we should copy all file in the path to ~/myandroid/bootable/bootloader/uboot-imx/ # cd ~/myandroid/bootable/bootloader # mkdir uboot-imx # cd uboot-imx # cp -a ~ /Downloads/u-boot/l5.1.1_2.1.0-ga/* ./ 9、Patch android BSP source code        android_L5.1.1_2.1.0_consolidated-ga_core_source.gz is the name of patch. Run following command to patch android. # copy android_L5.1.1_2.1.0_consolidated-ga_core_source.gz /opt/ # tar zxvf android_L5.1.1_2.1.0_consolidated-ga_core_source.gz # cd /opt/ android_L5.1.1_2.1.0_consolidated-ga_core_source/code/ # tar zxvf L5.1.1_2.1.0_consolidated-ga.tar.gz # cd ~/myandroid # source /opt/ android_L5.1.1_2.1.0_consolidated-ga_core_source/code/ L5.1.1_2.1.0_consolidated-ga/ and_patch.sh # help # c_patch /opt/ android_L5.1.1_2.1.0_consolidated-ga_core_source/code/ L5.1.1_2.1.0_consolidated-ga/ imx_L5.1.1_2.1.0-ga        If everything is OK, the following logs will display on console:               **************************************************************        Success: Now you can build the Android code for FSL i.MX platform               ************************************************************** 10、Patch Freescale extended feathures code        Please refer to chapter 3.3 of Android_User's_Guide.pdf to patch another 2 files:        (1) android_L5.1.1_2.1.0_consolidated-ga_omxplayer_source.gz        (2) android_L5.1.1_2.1.0_consolidated-ga_wfdsink_source.gz [Note]       As for other steps, such as compiling etc, please refer to Android_User's_Guide.pdf that released by NXP. TICS team Weidong Sun 04/01/2016
查看全文
Multicore programming guide with Linux 3.14.52_1.1.0 and FreeRTOS BSP for i.MX 6SoloX
查看全文
The default FSL android BSP support 1 SD card slot. If customer need to support more sd slot in android.Please reference below steps. There are two steps need to set up. 1 device/fsl.git NOTE: 1  change the fstab. 2194000 is the address of usdhc2.             2  change the mount point in storage_list.xml diff --git a/sabresd_6dq/fstab.freescale b/sabresd_6dq/fstab.freescale index 7f23edb..1529a27 100644 --- a/sabresd_6dq/fstab.freescale +++ b/sabresd_6dq/fstab.freescale @@ -4,6 +4,7 @@ # specify MF_CHECK, and must come before any filesystems that do specify MF_CHECK /devices/soc0/soc.0/2100000.aips-bus/2198000.usdhc/mmc_host /mnt/media_rw/extsd vfat defaults voldmanaged=extsd:auto +/devices/soc0/soc.0/2100000.aips-bus/2194000.usdhc/mmc_host /mnt/media_rw/extsd_expand vfat defaults voldmanaged=extsd_expand:auto /devices/soc0/soc.0/2100000.aips-bus/2184000.usb/ci_hdrc.0  /mnt/media_rw/udisk vfat defaults voldmanaged=udisk:auto /dev/block/mmcblk3p5    /system      ext4    ro,barrier=1                                                                               wait,verify /dev/block/mmcblk3p4    /data        ext4    nosuid,nodev,nodiratime,noatime,nomblk_io_submit,noauto_da_alloc,errors=panic    wait,encryptable=/dev/block/mmcblk3p9 diff --git a/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml b/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml index 3639bdc..c3f5105 100644 --- a/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml +++ b/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml @@ -41,6 +41,10 @@               android:storageDescription="@string/storage_sd_card"               android:primary="false"               android:removable="true" /> +    <storage android:mountPoint="/storage/extsd_expand" +             android:storageDescription="@string/storage_sd_card" +             android:primary="false" +             android:removable="true" />      <storage android:mountPoint="/storage/udisk" 2  system/core.git NOTE: mkdir the mount point. build@scmbld2:~/maddev_lp5.1_consolidate_ga_10_30/system/core/rootdir$ git diff diff --git a/rootdir/init.rc b/rootdir/init.rc index 2211cc2..fac37c2 100644 --- a/rootdir/init.rc +++ b/rootdir/init.rc @@ -72,7 +72,9 @@ on init      mkdir /storage 0751 root sdcard_r      mkdir /mnt/media_rw/extsd 0755 system system +    mkdir /mnt/media_rw/extsd_expand 0755 system system      symlink /mnt/media_rw/extsd /storage/extsd +    symlink /mnt/media_rw/extsd_expand /storage/extsd_expand      mkdir /mnt/media_rw/udisk 0755 system system
查看全文
Sorry I can't find a place to share this input file. It is to reproduce the VPU JPEG decoder issue I reported in Corrupted MJPG decoding result with FSL 3.10.17 BSP on i.MX6Q VPU​
查看全文
Hardware connection: there are two board-to-board connectors on E-INK daughter card IMXEBOOKDC4, while there is only one on i.MX7D Sabre board, as the picture below. This might be a bit confusing to connect the two: Checked with internal, the original design was trying to wire both eLCDIF and EPDC bus out to one daughter card, add the flexibility to have different configurations on one display daughter card(LCD/EPD). On i.MX7D Sabre board, only one connector is available for EPDC bus. Here is how we connect i.MX7D Sabre and IMXEBOOKDC4: Software setup: here we use pre-build L3.14.38_6UL7D_Beta Linux as our boot-image, steps to setup/boot/test EPDC: 1. download and decompress BSP pre-build image package "L3.14.38_beta_images_MX6UL7D.tar.gz", you should be able to find the SD image in it -- "fsl-image-gui-x11-imx7dsabresd.sdcard" 2. program the SD image on your SD card(>800 MBytes) with command(I'm running this in Ubuntu): "dd if=fsl-image-gui-x11-imx7dsabresd.sdcard of=/dev/sdb;sync" 3. insert SD card to the slot(J6) on i.MX7D Sabre board, connect debug-UART and power-on the board 4. modify the u-boot environment variables as below:      a.) setenv fdt_file imx7d-sdb-epdc.dtb           (originally this is "fdt_file=imx7d-sdb.dtb")      b.) setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=${mmcroot} epdc video=mxcepdcfb:E060SCM,bpp=16'           (originally this is "mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}") 5. boot into Linux kernel, run unit-test: "/unit_tests/mxc_epdc_fb_test.out", should be able to have test patterns running on EPD.
查看全文
The i.MX 6 Linux L3.10.17_1.0.3 Patch release is now available. Patch Release Notes can be found on  www.freescale.com . This release supports the following i.MX 6 reference boards: ·        i.MX 6 Quad/DualLite/Solo SABRE SD ·        i.MX 6 Quad/DualLite/Solo SABRE Auto ·        i.MX 6 SoloLite This patch release is based on the i.MX 6 Linux L3.10.17_1.0.0 GA release. Release changes the following components: ·        Kernel branch: imx_v2013.04_3.10.17_1.0.0_ga ·        U-Boot branch: imx_3.10.17_1.0.0_ga ·        Graphics: gpu-viv-bin-mx6q, 3.10.17_1.0.3 ·        Graphics: gpu-viv-g2d, 3.10.17_1.0.3 ·        Graphics: Xorg-driver, 3.10.17_1.0.3 More detailed patch description: Please consult the release notes document.
查看全文