i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Detailed Features List of i.MX35 PDK board I.MX35 CPU Card Additional Resources I.MX35 PDK Board Flashing SD Card i.MX35 PDK Board Flashing NAND i.MX35 PDK Linux Booting SD Loading Redboot Binary Directly to RAM Fixing Redboot RAM Bug Fixing Redboot RAM bug (CSD1 not activated)
查看全文
Patch to enable SSI_ASRC_P2P capture function for SebreSD board Modified based on https://community.freescale.com/docs/DOC-95342#comment-9739 You can use 'arecord -Dhw:0,1 -c 2 -f S16_LE -r 44100 | aplay' to test this patch. Currently only supports 16bit output width, for 24bit, the voice of the captured data will be much bigger in one channel than the other for this patch.
查看全文
Build the Demonstration Platform To make a demonstration platform, the CPU board is directly connected to the Personality board using the 500-pin connector that is keyed to avoid misconnections, so there is only one way to connect the CPU board to the Personality board. The Debug board is not used. Connect platform to PC
查看全文
The attached document describes how to calculate ESAI Mclk Bitclk LRclk for imx6 sabreauto board based on 3.10.17 linux kernel.
查看全文
Hi all, Cortex-M4 for i.MX6SoloX that is new to i.MX6SX customers. They concerns GPIO ISRs response time are not real time and hugh latency while Android/Linux is running on Cortex-A9 in i.MX6SoloX. I shared my test steps, report and image for your reference. Best regards, Carl
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343007 
查看全文
How To Convert RealView CP15 Config To OpenOCD? # arm11 mcr <jtag_target> <coprocessor> <opcode 1> <CRn> <CRm> <opcode 2> <32bit value to write> Setting CP15 Control RealView: setreg @CP15_CONTROL=0x00050078 OpenOCD: arm11 mcr 1 15 0 1 0 0 0x00050078 Setting CP15 Peripheral Memory Remap RealView: setreg @CP15_PERIP_MEM_REMAP=0x40000015 OpenOCD: arm11 mcr 1 15 0 15 2 4 0x40000015
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341566 
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344462 
查看全文
This is done with the 11.09 BSP for imx53 specifically. Attached is an amrnb.spec file, I put it in ltib/dist/lfs-5.1/amrnb. Then I extracted opencore-amr-0.1.3.tar.gz and put it in ltib/rpm/BUILD. I built with ltib ( ALl this could be added to the ltib menus as well 😞 ./ltib –m scbuild –p amrnb ./ltib –m scdeploy –p amrnb Then I applied the patch to .ltib for gst-plugins-ugly and built that with ltib. It will play a .3gp file with this pipeline: gst-launch filesrc location=/media/sd/test.3gp ! qtdemux name=demux demux.audio_00 ! queue ! amrnbdec ! alsasink demux.video_00 ! multiqueue ! mfw_vpudecoder ! mfw_isink Regards, Randy Krakora
查看全文
Question: The i.MX6 documentation gives several different values for the maximum frequency of the IPU’s HSP_CLK clock. What are the correct HSP_CLK maximum frequency values for the i.MX6 Dual/Quad and Solo/DualLite? Can HSP_CLK run at 270 MHz on both the DQ and SDL CPUs, but it’s not clear from the documentation if this is permitted. Maximum HSP_CLK frequencies listed in the reference manual (DQ😞 264 MHz (Table 9-2 (IPU IP Parametric Table), Table 9-5 (IPU Clock Sources)) 266 MHz (Table 18-3 (System Clock Frequency Values)) Maximum HSP_CLK frequencies listed in the reference manual (SDL😞 270 MHz (Table 9-2 (IPU IP Parametric Table), Table 9-5 (IPU Clock Sources), Table 18-3 (System Clock Frequency Values)) Answer: Referring to Figure 18-2, IPU1_HSP_CLK_ROOT may be selected to have 1 of 4 sources. These sources are highlighted in yellow on the northwest corner of the page and the previous paragraph states these are max values. Possible sources are 540, 528, 396, and 480 MHz. The 480 MHz is divided by 4 before the selector, so winds up being 120 MHz. Per the diagram, these are all divided by 2 for IPU1_HSP_CLK_ROOT. The result is 270, 264, 198, and 60 MHz choices. Therefore, the max for IPU1_HSP_CLK_ROOT is 270 MHz for DQ. MX6D/Q and MX6S/DL are different with respect to max HSP_CLK frequency. MX6D/Q = 264 MHz max MX6S/DL = 270 MHz max
查看全文
i.MX6 4.0.0 BSP release doesn't support ASRC_P2P function. This patch provides the reference codes to enable ASRC_P2P function for SSI. It can convert input sample rate to 44.1K_16bit/44.1K_24bit and 48K_16bit/48K_24bit. You can modify the configurations in the Board file. By the way, the SSI controler works at slave mode. Known limitations for the patch: -- The SDMA doesn't support SSI Dual FIFO when using ASRC_P2P function. -- From the waveform, the converted 24bit data have some abnormal data(values between 0 and 1) , but can't hear any abnormal sound from headphone. One suggestion is given under https://community.freescale.com/docs/DOC-95340
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343054 
查看全文
We have a ATK tool which can program image, also it can burn fuse for i.MX51. Since fuse is one time program, so please take care the fuse can't be turn back after programmed.
查看全文
Debugging with Eclipse and GDB on Linux user space This is a good open-source choice to debug i.MX processors. The integration of popular tools like Eclipse and GDB offers a good and stable connection between host and target. The first step is to install the tools on host. Click here to get instructions of how to install the tools. Let's debug a ready hello world program into the ltib. To extract the hello world package, type on ltib directory: $./ltib -m prep -p helloworld Change the code of hello.c to: #include <stdio.h> int main(int argc, char** argv) {     int i;     for (i = 0; i < 100; ++ i)     {         printf(“Welcome to GDB ! %d /n”, i);     }     return 0; } Change the Makefile to add debug symbols Change the two following lines from: CFLAGS = -Wall CXXFLAGS = -Wall To: CFLAGS = -Wall -g CXXFLAGS = -Wall -g Build and deploy the new source-code: $./ltib –p helloworld –m scbuild $./ltib –p helloworld –m scdeploy Configuring the Target On target, gdbserver needs to be run to perform debug. The gdbserver command has the following structure: gdbserver ip_host:port /full/path/app/app_name If gdbserver is not installed on target, select gdb package on ltib configuration. In this example our host has the 192.168.16.35 IP address and our HelloWorld application is located at /usr/bin/hello on the target board. Execute the gdbserver: gdbserver 192.168.16.35:10000 /usr/bin/hello You can use other port number as long as you use the same number when configuring the Eclipse. Setting a GDB Debug Session on Eclipse Now we will configure Eclipse C/C++ to start a GDB session with our remote i.MX board. We will need to know which is the target board’s IP address. To get your target’s IP address: /sbin/ifconfig In our example the target board has the 192.168.16.36 IP address. Open-up Eclipse and choose the C/C++ perspective. We will import the HelloWorld executable built by LTIB. Go to the menu File -> Import You will see the “Import” screen. Select “C/C++ Executable” option. Hit the “Next” button. Eclipse automaticaly creates a new project when whe use the “Import” option. In the next screen, select the “Search Directory” option and hit the “Browse” button. This session is incomplete and is being edited...
查看全文
Q: How to setup camera under Android? helping a customer (RTX) debug some issues with camera. They're using i.MX 6Solo and Android 13.4-GA on custom hardware. They added a new camera driver which seems to work when using small console capture program (no gui, no preview), so the route from camera to /dev/video0 seems to work. However, when they try to use camera from Android, entire system freezes. They located the crash to following line in ipu_common.c which basically enables camera CSI0: ipu_cm_write(ipu, reg | IPU_CONF_CSI0_EN, IPU_CONF); While investigating IPU setup, we noticed that CPMEM setup for IDMAC channel 0 is "off": ch 0 word 0 - 00000000 25800000 00000000 E0000000 00077C4F ch 0 word 1 - 01B086B0 00394EC0 0087C000 00009FC0 0000027F As seen from above, EBA0 points to 0x0D843580 and EBA1 to 0x0E53B000, which is in EIM memory space, not DDR memory space, which probably causes issues. We're not sure what could be causing this as camera driver doesn't provide any such address and mostly just handles communication to camera chip. But something gets off in Android framework and we could use any hints about what to look for. A: You can reference to the "i.MXAndroidR13.4GAAdvancedUserGuide.html" "3 Camera&Video Recorder customization" for how to change the camera in Android. Another thing needs be checked is the camera sensor driver, you can reference to "kernel_imx\drivers\media\video\mxc\capture\ov5642.c", "static struct v4l2_int_ioctl_desc ov5642_ioctl_desc", did you implemented the same v4l2_int_ioctl_desc functions? Customer HW is set up so that DDR memory space starts at 0x80000000. This causes problems in myandroid/hardware/imx/mx6/libcamera/CamerHAL.cpp when obtaining buffer addresses where camera should store data. GPU will only return OFFSET into 2GB memory space it can address, so it will return an address below 0x80000000. This needs to be adjusted before passing onto V4L2 when starting capturing.
查看全文
There developed the controller uses i.MX53 + Linux. Has developed a solution for building distributed information and control systems. Prototmpy been in operation for over a year. Examples: - Control Electromagnetic stirring (mixer) http://ontecom.com/en/catalog/ems / Rusal, Krasnoyarsk. - Moniroring and management of pumping stations. - Monitoring and control of climate control systems. You can create a smart home systems and iot. There is experience with PLC (Power Line Communication) Qualcomm/Atheros. In my spare time I develop a budget solution for PLC (Power Line Communication) control / monitoring components smart home. Based on the standard IEC 61131-3 developed software - distributed information management system. The solution is cross-platform. In a single system may be computers of different architectures and various operating systems. Such signals are synchronized controller ARM / Linux, and x86 server (Win, Linux, VMS, ...) Uses wxWidgets. Articles on this subject is, but in Russian.
查看全文
The i.MX27 Application Development System (MCIMX27ADSE) is a development tool which is designed to run software applications designed for the i.MX27 processor. Features i.MX27 Multimedia Application Processor Two clock-source crystals, 32 KHz and 26 MHz Power management & Audio IC (MC13783) included battery charging, 10bit ADC, buck switchers, boost switcher, regulators, amplifiers, CODEC, SSI audio bus, real time clock, SPI control bus, USB OTG transceiver & touchscreen interface Multi-ICE debug support Two 512Mbit DDR-SDRAM devices, configured as one 128MB, 32-bit device One 256Mbit Burst Flash with 128Mbit Pseudo Static RAM (PSRAM) memory device, configured as one 16MB flash with 8MB PSRAM, 16-bit device An single board system with connections for LCD display panel, Keypad and Image sensor. Complex Programmable Logic Device (CPLD) for reducing glue logic interface Software readable board revisions Configuration and user definable DIP switches Two SD/MMC, MS memory card connectors PCMCIA & ATA Hard Disk Drive (HDD) Two RS-232 transceivers and DB9 connectors (one configured for DCE and one for DTE operation) supporting on-chip UART ports External UART with RS-232 transceiver and DB9 connector Infrared transceiver that conforms to Specification 1.4 of the Infrared Data Association USB Host (HS & FS), USB OTG (HS & HS) interface Separate LCD panel assembly that connects to the main board Separate keypad unit with 36 push button keys Separate CMOS Image Sensor Card A 3.5 mm headset jack, a 3.5 mm line out jack, a 3.5 mm line in jack, a 3.5 mm microphone jack and a 2.5 mm microphone and headset jack Cirrus Logic CS8900A-CQ3Z Ethernet controller (10BASE-T), with RJ-45 connector AMD AM79C874 NetPHY (10BASE-T & 100BASE-X), with RJ-45 connector Two 32 × 3-pin DIN expansion connectors with most i.MX27 I/O signals Variable resistor for emulation of a battery voltage level NAND Flash card (Plugs into Main Board) which is included in the ADS kit LED indicators for power, Ethernet activity, and two LEDs for user defined status indication Universal power supply with 5 volt output @ 5 Amperes USB, RS-232 and RJ45 cables available in kit Kit Contains a main board an LCD display panel a keypad a NAND flash card an image sensor a TV encoder card, etc It supports application software, target-board debugging or optional extra memory.
查看全文
1) rtsp gst-launch-1.0 rtspsrc location=rtsp://192.168.0.105:10000 name=source ! queue ! rtph264depay ! vpudec ! overlaysink source. ! queue ! rtpmp4gdepay ! aacparse ! beepdec ! alsasink pc side: open vlc, choose media , then choose stream and rtsp, then choose the port to 10000 2)udp imx side: gstream 0.1 version: gst-launch udpsrc do-timestamp=false uri=udp://192.168.0.255:10000 caps="video/mpegts" ! aiurdemux streaming_latency=400 name=d d. ! queue ! vpudec low-latency=true ! queue ! mfw_v4lsink sync=true d. ! queue ! beepdec ! alsasink sync=true gstream 1.0 version: gst-launch-1.0 udpsrc do-timestamp=false uri=udp://192.168.0.255:10000 caps="video/mpegts" ! aiurdemux streaming-latency=400 name=d d. ! queue ! vpudec ! queue ! overlaysink sync=true d. ! queue ! beepdec ! pulsesink sync=true pc side: open vlc , then choose media, then choose stream and add the ts file, then choose dup(legacy) in the destinationsetup, then set the same broadcasting address as the gstreamer command set, then streaming.
查看全文
For early i.MX 8QuadXPlus MEK boards with C0 chips, power on the board when the board is connected to the PC with USB Type-C cable may cause the PC to shut down directly. This is a hardware known issue. another type of TCPC PHY chip will be used in later boards to fix this issue. If you have this kind of i.MX 8QuadXPlus MEK boards with c0 chips already, you can take below way to avoid this issue: 1. change the boot switch to "serial download mode", firstly power on the board, then connect the board to PC with Type-C cable. 2. download the attached files, uncompress this two files and put them in the same folder. 3. open the command window, change the working directory to the one contains the files just downloaded, and execute "uuu uuu_change_DRP_to_DFP.auto-imx8qxpc0mek" on command window. After the command being successfuley executed, the board can be powerwed up when the board is connected to PC with type-C cable.
查看全文