i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345359 
View full article
Q: To do a triple display demo based on imx6 SDP. The 3 channel are 1 lvds & 1hdmi & 1 lcd  and the OS is Android JB4.3. The dual display works and those 2 screens can all display the Android desktop. The setting as below. setenv bootargs console=ttymxc0,115200 init=/init rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=lcd,CLAAWVGA,if=RGB565 video=mxcfb2:off video=mxcfb3:dev=hdmi,1920x1080M60,if=RGB24 fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale static struct ipuv3_fb_platform_data sabresd_fb_data[] = {         { /*fb0*/         .disp_dev = "lcd",         .interface_pix_fmt = IPU_PIX_FMT_RGB565,         .mode_str = "CLAA-WVGA",         .default_bpp = 16,         .int_clk = true,         .late_init = false,         }, {         .disp_dev = "ldb",         .interface_pix_fmt = IPU_PIX_FMT_RGB666,         .mode_str = "LDB-XGA",         .default_bpp = 16,         .int_clk = false,         .late_init = false,             }, {         .disp_dev = "ldb",         .interface_pix_fmt = IPU_PIX_FMT_RGB666,         .mode_str = "LDB-XGA",         .default_bpp = 16,         .int_clk = false,         .late_init = false,         }, {         .disp_dev = "hdmi",         .interface_pix_fmt = IPU_PIX_FMT_RGB24,         .mode_str = "1920x1080M60",         .default_bpp = 16,         .int_clk = true,         .late_init = false,             }, }; static struct fsl_mxc_hdmi_core_platform_data hdmi_core_data = {         .ipu_id = 1,          .disp_id = 1, }; static struct fsl_mxc_lcd_platform_data lcdif_data = {         .ipu_id = 0,         .disp_id = 0,         .default_ifmt = IPU_PIX_FMT_RGB565, }; static struct fsl_mxc_ldb_platform_data ldb_data = {         .ipu_id = 0,         .disp_id = 1,         .ext_ref = 1,         .mode = LDB_SEP1,         .sec_ipu_id = 1,         .sec_disp_id = 0, }; A: Android BSP doesn't support triple display, and so the change in kernel would not make the 3rd display work.
View full article
Q: The i.MX 6Dual/6Quad Applications Processor Reference Manual Rev. D says that i.MX6 supports eMMC 4.5.  But does the current BSP(L3.0.35_12.08.00) support eMMC 4.5?  If not, does Freescale have it in their release plan? A: i.MX 6Dual/6Quad RM and Datasheet declare that the uSDHC module is "fully compliant with the MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.2/4.3/4.4/4.41, including high-capacity (> 2 GB) HC MMC cards."  Therefore, if your eMMC4.5 card is backward-compatible with eMMC4.4, you can use it in eMMC4.4 mode to enable eMMC4.4 functionality and performance on the i.MX6 platform. For example, the current i.MX6 Linux BSP (L3.0.35_4.1.0) has added code to interface with an eMMC4.5 card to operate as an eMMC4.4 card. See the following code in drivers/mmc/core/mmc.c:         card->ext_csd.rev = ext_csd[EXT_CSD_REV];         /* workaround: support emmc 4.5 cards to work at emmc 4.4 mode */         if (card->ext_csd.rev > 6) {                 printk(KERN_ERR "%s: unrecognised EXT_CSD revision %d\n",                         mmc_hostname(card->host), card->ext_csd.rev);                 err = -EINVAL;                 goto out;         }
View full article
When configuring i.MX6 IPU IDMAC CPMEM parameters or debugging it, it's hard to find the value of a parameter inside the 160 bits word. This web tool separates the 160 bits words into parameters making it easier to check their values. Link: i.MX Tools 
View full article
When the customer want to use the PCIE module on the i.MX6SX SDB board, they can use the oscillator to do the pretset, there are the test report.
View full article
Video in Host Side Converting images (png, jpg, etc) to YUV format ffmpeg -f image2 -i test.png -pix_fmt yuv420p test.yuv Converting AVI files to YUV format To convert AVI to YUV you can use the lav2yuv program. In Ubuntu Linux this program is in mjpegtools package. This is the way to convert: lav2yuv myfile.avi > myfile.yuv Converting YUV video files to AVI (DivX) Use the ffmpeg tool: ffmpeg -s 176x144 -i kuuba_maisema_25fps_qcif.yuv -vcodec mpeg4 -sameq -aspect 4:3 ~/kuuba.avi You need to specify the video dimensions (176 × 144), the video codec (mpeg4), and the aspect ratio (4:3). Converting MP4 to AVI Use the mencoder tool: mencoder Bike1.mp4 -ovc lavc -oac lavc -o NewBike1.avi
View full article
In order to create this Ogg Theora encoder example you need to add libogg, libvorbis and libtheora to your system. Download these libs from http://www.theora.org/downloads/ : libogg-1.1.3, libvorbis-1.2.0 and libtheora-1.0.tar.bz2 Copy them to /opt/ltib/pkgs Create the directories ltib/dist/lfs-5.1/libogg, ltib/dist/lfs-5.1/libvorbis, ltib/dist-5.1/lfs/libtheora. Copy these spec files to its respective directories: File:Libogg.gz File:Libvorbis.gz File:Libtheora.gz Execute this sequence to compile and install these libs: $ ./ltib -p libogg.spec -m prep $ ./ltib -p libogg.spec -m scbuild $ ./ltib -p libogg.spec -m scdeploy $ ./ltib -p libvorbis.spec -m prep $ ./ltib -p libvorbis.spec -m scbuild $ ./ltib -p libvorbis.spec -m scdeploy $ ./ltib -p libtheora.spec -m prep $ ./ltib -p libtheora.spec -m scbuild $ ./ltib -p libtheora.spec -m scdeploy Now download and compile yuv2theora.c encoder example: File:Yuv2theora.gz $ ./ltib -m shell LTIB> gcc yuv2theora.c -o yuv2theora `pkg-config --libs --cflags theora` In this example we used a video sample (YUV420) on CIF format: http://140.116.72.80/~jhlin5/ns2/yuv_to_avi/paris_cif.yuv Update: All these libraries were added on LTIB Savannah CVS, then you just need to use them and compile the above code.
View full article
For OpenSuse Users: Open a terminal as root Edit tftp file # vi /etc/xinetd.d/tftp Change the disable to no: service tftp {   socket_type = dgram   protocol = udp   wait = yes   user = root   server = /usr/sbin/in.tftpd   server_args = -s /tftpboot   disable = no }
View full article
Question: After a JTAG Reset with his GHS MULTI Probe on i.MX6 Hardware, read the SRC_SRSR register the corresponding reset source bits (JTAG reset) are not set. The contents: SRSR = 0x1      WARM Boot = 0x0      jtag_sw_rst = 0x0      jtag_rst_b = 0x0      wdog_sw_rst = 0x0      ipp_user_reset_b = 0x0      cpu_reset_b = 0x0      ipp_reset_b = 0x1 Tried to reproduce this with my DSTRAM probe, and issued a "reset reset.system" command in DS-5 Debugger but Program Counter stays at current vaule. Obviously my SRSR bits don't change either. Answer: Seems " jtag_rst_b" is a HW reset, please check the connection between JTAG port and i.Mx6 JTAG_TRST pin. And confirm the waveform on rest pin when JTAG reset run.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344474 
View full article
Hi, My board is imx6dl_sabreauto and I use android4.4.2 source!The system stop at "Freeing init memory", when the system boot. I found the boot message no have follow message: mmc0: new high speed DDR MMC card at address 0001 mmcblk0: mmc0:0001 SEM08G 7.39 GiB mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB input: WM8962 Beep Generator as /devices/platform/imx-i2c.0/i2c-0/0-001a/input/input7 mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4 mmcblk0: p4 size 13336576 extends beyond EOD, truncated asoc: wm8962 <-> imx-ssi.1 mapping ok input: wm8962-audio DMIC as /devices/platform/soc-audio.5/sound/card0/input8 input: wm8962-audio Headphone Jack as /devices/platform/soc-audio.5/sound/card0/input9 mmcblk0boot1: unknown partition table Please help me! Thank  you!
View full article
On power-up of a system, the bootloader performs initial hardware configuration, and is responsible for loading the Linux kernel in memory. Several bootloaders are available which support i.MX SoCs: Barebox (http://www.barebox.org/) RedBoot (http://ecos.sourceware.org/redboot/) U-Boot (http://www.denx.de/wiki/U-Boot/) Qi (http://wiki.openmoko.org/wiki/Qi)
View full article
Note that this document only applies for REV2 of the SCM QWKS board Refer to the attached presentation to check how the OV5640 camera can be connected to the QWKS rev2 with a retrofit of the OV5640 camera set as in the image below Enjoy!!!
View full article
In this post, we will review the YOLO model export process for three popular NXP families: i.MX8MP, i.MX93, and i.MX95. These processors are increasingly used in edge AI applications such as smart vision, industrial automation, robotics, and intelligent HMI systems. Although they all support machine learning deployment, the export path, supported runtimes, and hardware acceleration options may differ depending on the device. The purpose of this guide is to provide a clearer starting point for developers who want to take a trained YOLO model and prepare it for execution on these i.MX platforms. Whether your workflow targets CPU, NPU. YOLO Model Export Workflow for i.MX Processors 1) Install Ultralytics Install or upgrade the Ultralytics package from PyPI: pip install -U ultralytics   2) Export the YOLO Model (TFLite INT8) Export your trained YOLO model to TensorFlow Lite (TFLite) format with INT8 quantization: yolo export model=<your_model>.pt format=saved_model quantize=8 Example: yolo export model=yolov8n.pt format=saved_model quantize=8   Notes: The model must be exported in TFLite format and fully INT8 quantized. After the export process, a directory named "<your_model>_saved_model" Inside this directory, you should use the following file as the input for the converter called "<your_model>_full_integer_quant.tflite"  This is the fully quantized INT8 model required for NPU deployment. Using any other file from the export directory may result in compatibility issues or prevent proper NPU acceleration. After obtaining the *_full_integer_quant.tflite file, you can proceed with the needed conversion workflow to generate the final model optimized for execution on the NPU. For additional valid export options, please refer to the official Ultralytics documentation: https://docs.ultralytics.com/modes/export/ At this stage: The model can run on CPU for: i.MX8MP i.MX93 i.MX95 On i.MX8MP, this TFLite model can also be deployed to the NPU using the appropriate delegate. 3) i.MX93  Compile for Ethos-U NPU (Vela) For i.MX93, an additional compilation step is required to use the Ethos-U NPU. Run the Vela compiler to convert the TFLite model into an optimized format: vela <model>.tflite --output-dir <output_folder> Notes: This step generates a model optimized for the Ethos-U NPU. The resulting output files are required for deployment using the NPU delegate on the i.MX93 platform. Please ensure that the model complies with the Ethos-U operator constraints, as only supported operations can be accelerated by the NPU. This command can be executed directly on the i.MX93 target, or alternatively by using the eIQ Toolkit (please refer to the eIQ Converter documentation for more details). 4)  i.MX95 Convert Model Using Neutron SDK For i.MX95, the model must be converted using the Neutron Converter, depending on the BSP version installed on your board. .\neutron-converter.exe ` --input "<model>.tflite" ` --target imx95 ` --output "<model_neutron>.tflite" ` --optimization-level OOpt Notes: The Neutron toolchain prepares the model for i.MX95 NPU acceleration. Supported formats and flags may vary depending on the Neutron SDK version. Always verify compatibility with your BSP release. You can check the compatibility details of the Neutron SDK in the "docs" folder of your downloaded Neutron SDK package.   5) Benchmark the Model After exporting and converting the model, you can validate performance using benchmarking tools. Typical options include: TFLite benchmark tool (CPU / delegate): benchmark_model --graph=<model>.tflite --num_threads=X 6) Results iMX8MP CPU root@imx8mpevk:~# /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model --graph=yolov8n_full_integer_quant.tflite --mum_threads=4 INFO: STARTING! WARN: Unconsumed cmdline flags: --mum_threads=4 INFO: Log parameter values verbosely: [0] INFO: Graph: [yolov8n_full_integer_quant.tflite] INFO: Signature to run: [] INFO: Loaded model yolov8n_full_integer_quant.tflite INFO: Created TensorFlow Lite XNNPACK delegate for CPU. INFO: The input model file size (MB): 3.42652 INFO: Initialized session in 86.368ms. INFO: Running benchmark for at least 1 iterations and at least 0.5 seconds but terminate if exceeding 150 seconds. INFO: count=1 curr=1029584 p5=1029584 median=1029584 p95=1029584 INFO: Running benchmark for at least 50 iterations and at least 1 seconds but terminate if exceeding 150 seconds. INFO: count=50 first=986237 curr=985536 min=983921 max=993982 avg=985863 std=1497 p5=984152 median=985947 p95=986715 INFO: Inference timings in us: Init: 86368, First inference: 1029584, Warmup (avg): 1.02958e+06, Inference (avg): 985863 INFO: Note: as the benchmark tool itself affects memory footprint, the following is only APPROXIMATE to the actual memory footprint of the model at runtime. Take the information at your discretion. INFO: Memory footprint delta from the start of the tool (MB): init=11.207 overall=40.918 root@imx8mpevk:~#   NPU root@imx8mpevk:~# /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model --graph=yolov8n_full_integer_quant.tflite --num_threads=4 --external_delegate_path=/usr/lib/libvx_delegate.so INFO: STARTING! INFO: Log parameter values verbosely: [0] INFO: Num threads: [4] INFO: Graph: [yolov8n_full_integer_quant.tflite] INFO: Signature to run: [] INFO: #threads used for CPU inference: [4] INFO: #threads used for CPU inference: [4] INFO: External delegate path: [/usr/lib/libvx_delegate.so] INFO: Loaded model yolov8n_full_integer_quant.tflite INFO: Vx delegate: allowed_cache_mode set to 0. INFO: Vx delegate: device num set to 0. INFO: Vx delegate: allowed_builtin_code set to 0. INFO: Vx delegate: error_during_init set to 0. INFO: Vx delegate: error_during_prepare set to 0. INFO: Vx delegate: error_during_invoke set to 0. INFO: EXTERNAL delegate created. INFO: Explicitly applied EXTERNAL delegate, and the model graph will be completely executed by the delegate. INFO: The input model file size (MB): 3.42652 INFO: Initialized session in 39.515ms. INFO: Running benchmark for at least 1 iterations and at least 0.5 seconds but terminate if exceeding 150 seconds. INFO: count=1 curr=16831746 p5=16831746 median=16831746 p95=16831746 INFO: Running benchmark for at least 50 iterations and at least 1 seconds but terminate if exceeding 150 seconds. INFO: count=50 first=67167 curr=67190 min=67048 max=67366 avg=67187 std=64 p5=67094 median=67184 p95=67295 INFO: Inference timings in us: Init: 39515, First inference: 16831746, Warmup (avg): 1.68317e+07, Inference (avg): 67187 INFO: Note: as the benchmark tool itself affects memory footprint, the following is only APPROXIMATE to the actual memory footprint of the model at runtime. Take the information at your discretion. INFO: Memory footprint delta from the start of the tool (MB): init=9.47266 overall=224.398 root@imx8mpevk:~# iMX93 CPU root@imx93evk:~# /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model --graph=yolov8n_full_integer_quant.tflite --num_threads=2 INFO: STARTING! INFO: Log parameter values verbosely: [0] INFO: Num threads: [2] INFO: Graph: [yolov8n_full_integer_quant.tflite] INFO: Signature to run: [] INFO: #threads used for CPU inference: [2] INFO: #threads used for CPU inference: [2] INFO: Loaded model yolov8n_full_integer_quant.tflite INFO: Created TensorFlow Lite XNNPACK delegate for CPU. INFO: The input model file size (MB): 3.42652 INFO: Initialized session in 57.963ms. INFO: Running benchmark for at least 1 iterations and at least 0.5 seconds but terminate if exceeding 150 seconds. INFO: count=3 first=247896 curr=198973 min=198973 max=247896 avg=215381 std=22991 p5=198973 median=199275 p95=247896 INFO: Running benchmark for at least 50 iterations and at least 1 seconds but terminate if exceeding 150 seconds. INFO: count=50 first=199533 curr=198880 min=197719 max=205262 avg=199032 std=1005 p5=198344 median=198886 p95=199961 INFO: Inference timings in us: Init: 57963, First inference: 247896, Warmup (avg): 215381, Inference (avg): 199032 INFO: Note: as the benchmark tool itself affects memory footprint, the following is only APPROXIMATE to the actual memory footprint of the model at runtime. Take the information at your discretion. INFO: Memory footprint delta from the start of the tool (MB): init=11.2539 overall=40.9961 root@imx93evk:~#   NPU root@imx93evk:~# /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model --graph=yolov8n_full_integer_quant_vela.tflite --num_threads=2 --external_delegate_path=/usr/lib/libethosu_delegate.so INFO: STARTING! INFO: Log parameter values verbosely: [0] INFO: Num threads: [2] INFO: Graph: [yolov8n_full_integer_quant_vela.tflite] INFO: Signature to run: [] INFO: #threads used for CPU inference: [2] INFO: #threads used for CPU inference: [2] INFO: External delegate path: [/usr/lib/libethosu_delegate.so] INFO: Loaded model yolov8n_full_integer_quant_vela.tflite INFO: Ethosu delegate: device_name set to /dev/ethosu0. INFO: Ethosu delegate: cache_file_path set to . INFO: Ethosu delegate: timeout set to 60000000000. INFO: Ethosu delegate: enable_cycle_counter set to 0. INFO: Ethosu delegate: enable_profiling set to 0. INFO: Ethosu delegate: profiling_buffer_size set to 2048. INFO: Ethosu delegate: pmu_event0 set to 0. INFO: Ethosu delegate: pmu_event1 set to 0. INFO: Ethosu delegate: pmu_event2 set to 0. INFO: Ethosu delegate: pmu_event3 set to 0. INFO: EXTERNAL delegate created. INFO: EthosuDelegate: 8 nodes delegated out of 15 nodes with 8 partitions. INFO: Explicitly applied EXTERNAL delegate, and the model graph will be partially executed by the delegate w/ 8 delegate kernels. INFO: Created TensorFlow Lite XNNPACK delegate for CPU. INFO: The input model file size (MB): 2.9511 INFO: Initialized session in 638.148ms. INFO: Running benchmark for at least 1 iterations and at least 0.5 seconds but terminate if exceeding 150 seconds. INFO: count=7 first=87215 curr=81264 min=81079 max=87215 avg=82056.4 std=2107 p5=81079 median=81187 p95=87215 INFO: Running benchmark for at least 50 iterations and at least 1 seconds but terminate if exceeding 150 seconds. INFO: count=50 first=81497 curr=81232 min=80887 max=81783 avg=81153.1 std=178 p5=80921 median=81148 p95=81497 INFO: Inference timings in us: Init: 638148, First inference: 87215, Warmup (avg): 82056.4, Inference (avg): 81153.1 INFO: Note: as the benchmark tool itself affects memory footprint, the following is only APPROXIMATE to the actual memory footprint of the model at runtime. Take the information at your discretion. INFO: Memory footprint delta from the start of the tool (MB): init=7.36328 overall=8.73828 root@imx93evk:~# iMX95 CPU root@imx95evk:~# /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model --graph=yolov8n_full_integer_quant.tflite --num_threads=6 INFO: STARTING! INFO: Log parameter values verbosely: [0] INFO: Num threads: [6] INFO: Graph: [yolov8n_full_integer_quant.tflite] INFO: Signature to run: [] INFO: #threads used for CPU inference: [6] INFO: #threads used for CPU inference: [6] INFO: Loaded model yolov8n_full_integer_quant.tflite INFO: Created TensorFlow Lite XNNPACK delegate for CPU. INFO: The input model file size (MB): 3.42652 INFO: Initialized session in 35.268ms. INFO: Running benchmark for at least 1 iterations and at least 0.5 seconds but terminate if exceeding 150 seconds. INFO: count=7 first=115073 curr=74468 min=74170 max=115073 avg=80310.4 std=14192 p5=74170 median=74581 p95=115073 INFO: Running benchmark for at least 50 iterations and at least 1 seconds but terminate if exceeding 150 seconds. INFO: count=50 first=74143 curr=74135 min=73657 max=76392 avg=74346.9 std=447 p5=73829 median=74307 p95=75020 INFO: Inference timings in us: Init: 35268, First inference: 115073, Warmup (avg): 80310.4, Inference (avg): 74346.9 INFO: Note: as the benchmark tool itself affects memory footprint, the following is only APPROXIMATE to the actual memory footprint of the model at runtime. Take the information at your discretion. INFO: Memory footprint delta from the start of the tool (MB): init=11.5195 overall=40.8867 root@imx95evk:~# NPU: root@imx95evk:~# /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model --graph=yolov8n_full_integer_quant_neutron.tflite --num_threads=6 --external_delegate_path=/usr/lib/libneutron_delegate.so INFO: STARTING! INFO: Log parameter values verbosely: [0] INFO: Num threads: [6] INFO: Graph: [yolov8n_full_integer_quant_neutron.tflite] INFO: Signature to run: [] INFO: #threads used for CPU inference: [6] INFO: #threads used for CPU inference: [6] INFO: External delegate path: [/usr/lib/libneutron_delegate.so] INFO: Loaded model yolov8n_full_integer_quant_neutron.tflite INFO: EXTERNAL delegate created. INFO: NeutronDelegate delegate: 1 nodes delegated out of 33 nodes with 1 partitions. INFO: Neutron delegate version: v1.0.0-7399a58e, zerocp enabled. INFO: Explicitly applied EXTERNAL delegate, and the model graph will be partially executed by the delegate w/ 1 delegate kernels. INFO: Created TensorFlow Lite XNNPACK delegate for CPU. INFO: The input model file size (MB): 3.20989 INFO: Initialized session in 12.756ms. INFO: Running benchmark for at least 1 iterations and at least 0.5 seconds but terminate if exceeding 150 seconds. INFO: count=17 first=31509 curr=27588 min=27555 max=31509 avg=29101.2 std=1166 p5=27555 median=29071 p95=31509 INFO: Running benchmark for at least 50 iterations and at least 1 seconds but terminate if exceeding 150 seconds. INFO: count=50 first=28068 curr=29081 min=26573 max=31340 avg=29104.1 std=1204 p5=27306 median=29141 p95=31171 INFO: Inference timings in us: Init: 12756, First inference: 31509, Warmup (avg): 29101.2, Inference (avg): 29104.1 INFO: Note: as the benchmark tool itself affects memory footprint, the following is only APPROXIMATE to the actual memory footprint of the model at runtime. Take the information at your discretion. INFO: Memory footprint delta from the start of the tool (MB): init=6.98438 overall=12.2344 root@imx95evk:~ Disclaimer: Ultralytics YOLO models have not been officially validated/supported by NXP. Therefore, compatibility with i.MX processors and their corresponding NPUs cannot be guaranteed. Some models or configurations may not work as expected depending on operator support and hardware limitations.
View full article
This is a simple known-how for how to enable KASAN on L4.14.98 with i.MX8/8X and also a collection of related patches for fixing issues reported by KASAN.   Enable KASAN: It's very simple, just enable "CONFIG_KASAN" in kernel configuration. Besides this, adjusting the kernel's loading address is also required, due to KASAN (which will alloc more memory as a "tracker" for each allocation). For e.g., on imx8qxp MEK, we need to change the kernel loadaddr in uboot:     0x80280000 --> 0xE0280000 through uboot env: setenv loadaddr 0xE0280000 After this, it supposed to be working.   KASAN related patches on L4.14.98: KASAN will do detection/sanitizing for any memory allocation/access. In case of L4.14.98 on i.MX8/8X, there're several "BUG" reported by KASAN in default BSP. The attached patches are a collection for these issues.    Note: not all "BUG" reported by KASAN are really bug. Most of them are just some programming rule related problems and may not really cause memory access violation.
View full article
Kindly note that application note “AN12812: Using Code-Signing Tool with Hardware Security Module" has been removed from nxp.com. The AN is obsolete, the CST User’s guide describes how to use CST with an HSM using PKCS#11 interface. You can download CST package with its documentation from https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX_CST_TOOL_NEW  
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343113 
View full article
Add MIPI DSI support in uboot, the mipi panel is hx8369.
View full article
The Android O8.0.0_1.4.0 for i.MX 7ULP RFP(GA) release is now available on IMX_SW web page. Overview -> BSP Updates and Releases -> Android O8.1.0 for i.MX 7ULP GA.   Files available:   # Name Description 1 android_o8.1.0_1.4.0_7ulp-ga_docs.tar.gz Android O8.1.0_1.4.0 for 7ULP GA Documentation 2 imx-o8.1.0_1.4.0_7ulp-ga.tar.gz i.MX Android proprietary source code for Android O8.1.0_1.4.0_7ULP_GA 3 android_o8.1.0_1.4.0_7ulp-ga_image_7ulpevk.tar.gz Prebuilt images with NXP extended features for the i.MX7ULP EVK board 4 android_o8.1.0_1.4.0_7ulp-ga_tools.tar.gz Manufacturing Toolkit and VivanteVTK for Android O8.1.0_1.4.0_7ULP_GA 5 fsl_aacp_dec_O8.1.0-7ULP_GA.tar.gz AAC Plus Codec for  O8.1.0_1.4.0_7ULP_GA   Target boards: i.MX 7ULP EVK   Features and Known issues For features and known issues, please consult the Release Notes in detail.#
View full article
I.MX6 CoreBoard Computer On Module • Processor Freescale i.MX 6Quad, 1GHz • RAM 1GB DDR3 SDRAM 64-bit • ROM 4GB NAND Flash    UP to 16GB • ROM 2M SPI Nor Flash • Power supply Single 5V • Size 40mm SO-DIMM • Temp.-Range     0 to + 95C (Consumer)               -20 to + 105C (Extended Consumer)               -40 to +105C (Industrial)               -40 to + 125C (Automotive) Key Features • 10/100Mbps Ethernet • One High Speed USB 2.0 ports • Full HD LCD controller, 24bpp • OpenGL ES 2.0 and OpenVG 1.1        hardware accelerators • Multi-format HD 1080p60 video decoder and 1080p30 encoder hardware engine • Two Camera Interfaces • NEON MPE coprocessor — SIMD Media Processing Architecture — dual, single-precision floating point execute pipeline • Unified 1MB L2 cache • Several interfaces: 5x UART, 2x SDIO, 1x SSI/AC97/I2S, 3x I2C, 2xCSPI • 3.3V I/O • 2x Controller Area Network (FlexCAN) • PCIe 2.0 (1-lane) LVDS Option only: • Dual LVDS display port • SATA OS Support • Linux • Android
View full article