i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
There are several vulnerabilities been found recently as below: ZIMPERIUM’s report: http://jiveon.jivesoftware.com/mpss/c/7gA/PDcDAA/t.1p4/5z0zjG0pTd2TX1EnZDdFDQ/h3/hAMy2Th8Lsdoz-2BI-2B-2B4FlQpxshE-2Fm9XH3UWXhoYdrt6y4Crt0q1GUsW8pizm7YGWnxGc52SR4U4vCgooHeqoe1S9fu9dc4l1m2ew0Kz-2BSCbA-3D     They are reported as CVE-2015-1538, CVE-2015-1539, CVE-2015-3824, CVE-2015-3826, CVE-2015-3827, CVE-2015-3828 and CVE-2015-3829.   Trendmicro’s  report:http://blog.trendmicro.com/trendlabs-security-intelligence/trend-micro-discovers-vulnerability-that-renders-android-devices-silent/   All above vulnerabilities are related with stagefright’s stackoverflow, which exist all android version since JellyBean 4.2. The stagefright is the default Multimedia framework in Android’s AOSP source code.   To avoid attacking toward stagefright, it is recommended to have patches in this attach, which should be applied to myandroid/frameworks/av.   Reference: https://github.com/WhisperSystems/TextSecure/issues/381   This document was generated from the following discussion: Android vulnerability related with stagefright   Created by Hui Fang
View full article
GStreamer has a simple feature to enable tracing, allowing the developer to do basic debugging. These can be done in two ways: Adding the parameter --gst-debug=LIST to the pipeline (a pipeline is a executed gst-launch command) Prepending the environment variable GST_DEBUG=LIST' LIST is a a comma-separated argument, indicating the GStreamer elements to trace. For example, if one needs to trace the sink element      $ GST_DEBUG=*sink*:5 gst-launch playbin2 uri=file:///sample.avi or      $ gst-launch playbin2 uri=file:///sample.avi --gst-debug=*sink*:5 Both commands produces the same log. In case want to trace for than one element, so can simple add the <element>:5, for example      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi The number 5 indicates the log category, where 5 is the highest (the most verbose log you can get) and 0 produces no output (5=LOG, 4=DEBUG, 3=INFO, 2=WARN, 1=ERROR). Log can be huge in each pipeline run. One way to filter it is using the grep command. Before grepping, one needs to redirect the standard error to the standard output (GStreamer log goes always to stderr), so      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi 2>&1 | grep <filter string> In case the log needs to be shared, it is important to remove the 'color' of the log, again, one just needs to add the parameter --gst-debug-no-color or prepend the env variable GST_DEBUG_NO_COLOR=1 ----- More shell variables that GStreamer react, can be found here https://developer.gnome.org/gstreamer/0.10/gst-running.html
View full article
1) rtp linux side: gst-launch mfw_v4lsrc fps-n=30 ! vpuenc codec=6 ! queue ! rtph264pay ! udpsink host=192.168.0.105 port=5000 –v pc side: open the attached H264.sdp file using VLC. Then you can find the picture from camera on mx6 board, pls don’t forget to load camera module 2) Receive Pipeline from Board to PC: gst-launch -v gstrtpbin name=rtpbin udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=96' port=5000 ! rtpbin.recv_rtp_sink_0 rtpbin. ! rtph264depay ! queue ! ffdec_h264 ! queue ! autovideosink sync=false  udpsrc port=5001 ! rtpbin.recv_rtcp_sink_0 sync=false rtpbin.send_rtcp_src_0 ! udpsink port=5005 sync=false async=false Output: Setting pipeline to PAUSED ... Pipeline is live and does not need PREROLL ... Setting pipeline to PLAYING ... New clock: GstSystemClock /GstPipeline:pipeline0/GstRtpBin:rtpbin.GstGhostPad:send_rtcp_src_0: caps = application/x-rtcp /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSession:rtpsession0.GstPad:send_rtcp_src: caps = application/x-rtcp /GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = application/x-rtcp /GstPipeline:pipeline0/GstRtpBin:rtpbin.GstGhostPad:send_rtcp_src_0.GstProxyPad:proxypad2: caps = application/x-rtcp /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSession:rtpsession0.GstPad:recv_rtp_sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpBin:rtpbin.GstGhostPad:recv_rtp_sink_0: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpBin:rtpbin.GstGhostPad:recv_rtp_sink_0.GstProxyPad:proxypad1: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSession:rtpsession0.GstPad:recv_rtp_src: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:src: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpPtDemux:rtpptdemux0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpH264Depay:rtph264depay0.GstPad:src: caps = video/x-h264, stream-format=(string)byte-stream, alignment=(string)nal /GstPipeline:pipeline0/GstRtpH264Depay:rtph264depay0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstRtpBin:rtpbin.GstGhostPad:recv_rtp_src_0_2621786612_96.GstProxyPad:proxypad4: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96 /GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/x-h264, stream-format=(string)byte-stream, alignment=(string)nal /GstPipeline:pipeline0/GstQueue:queue0.GstPad:src: caps = video/x-h264, stream-format=(string)byte-stream, alignment=(string)nal /GstPipeline:pipeline0/ffdec_h264:ffdec_h2640.GstPad:sink: caps = video/x-h264, stream-format=(string)byte-stream, alignment=(string)nal /GstPipeline:pipeline0/ffdec_h264:ffdec_h2640.GstPad:src: caps = video/x-raw-yuv, width=(int)352, height=(int)288, framerate=(fraction)25/1, format=(fourcc)I420, interlaced=(boolean)false /GstPipeline:pipeline0/GstQueue:queue1.GstPad:sink: caps = video/x-raw-yuv, width=(int)352, height=(int)288, framerate=(fraction)25/1, format=(fourcc)I420, interlaced=(boolean)false /GstPipeline:pipeline0/GstQueue:queue1.GstPad:src: caps = video/x-raw-yuv, width=(int)352, height=(int)288, framerate=(fraction)25/1, format=(fourcc)I420, interlaced=(boolean)false /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstXvImageSink:autovideosink0-actual-sink-xvimage.GstPad:sink: caps = video/x-raw-yuv, width=(int)352, height=(int)288, framerate=(fraction)25/1, format=(fourcc)I420, interlaced=(boolean)false /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0.GstGhostPad:sink: caps = video/x-raw-yuv, width=(int)352, height=(int)288, framerate=(fraction)25/1, format=(fourcc)I420, interlaced=(boolean)false /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0.GstGhostPad:sink.GstProxyPad:proxypad0: caps = video/x-raw-yuv, width=(int)352, height=(int)288, framerate=(fraction)25/1, format=(fourcc)I420, interlaced=(boolean)false /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSession:rtpsession0.GstPad:sync_src: caps = application/x-rtcp /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:rtcp_sink: caps = application/x-rtcp /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:rtcp_src_-1673180684: caps = application/x-rtcp /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink_rtcp: caps = application/x-rtcp ^CCaught interrupt -- handling interrupt. Interrupt: Stopping pipeline ... Execution ended after 26282965149 ns. Setting pipeline to PAUSED ... Setting pipeline to READY ... /GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = NULL /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstXvImageSink:autovideosink0-actual-sink-xvimage.GstPad:sink: caps = NULL /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0.GstGhostPad:sink: caps = NULL /GstPipeline:pipeline0/GstQueue:queue1.GstPad:src: caps = NULL /GstPipeline:pipeline0/GstQueue:queue1.GstPad:sink: caps = NULL /GstPipeline:pipeline0/ffdec_h264:ffdec_h2640.GstPad:src: caps = NULL /GstPipeline:pipeline0/ffdec_h264:ffdec_h2640.GstPad:sink: caps = NULL /GstPipeline:pipeline0/GstQueue:queue0.GstPad:src: caps = NULL /GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = NULL /GstPipeline:pipeline0/GstRtpH264Depay:rtph264depay0.GstPad:src: caps = NULL /GstPipeline:pipeline0/GstRtpH264Depay:rtph264depay0.GstPad:sink: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin.GstGhostPad:recv_rtp_src_0_2621786612_96: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin.GstGhostPad:send_rtcp_src_0: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpPtDemux:rtpptdemux0.GstPad:src_96: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpPtDemux:rtpptdemux0.GstPad:sink: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink_rtcp: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:src: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:rtcp_src_-1673180684: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:src_-1673180684: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:rtcp_sink: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:sink: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSession:rtpsession0.GstPad:sync_src: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSession:rtpsession0.GstPad:send_rtcp_src: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSession:rtpsession0.GstPad:recv_rtp_src: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin/GstRtpSession:rtpsession0.GstPad:recv_rtp_sink: caps = NULL /GstPipeline:pipeline0/GstRtpBin:rtpbin.GstGhostPad:recv_rtp_sink_0: caps = NULL /GstPipeline:pipeline0/GstUDPSrc:udpsrc0.GstPad:src: caps = NULL Setting pipeline to NULL ... Freeing pipeline ...
View full article
If your target system does not have an Ethernet port it is possible to transfer files, such as the kernel image over serial port, using ymodem. On minicom: RedBoot> load -r -b 0x100000 -m ymodem zImage Where "zImage" is the file to be transferred. On minicom press "CTRL + a" and "s", choose ymodem and select the file to be transferred.
View full article
on Host: libx11-dev libpng-dev libjpeg-dev libxext-dev x11proto-xext-dev qt3-dev-tools-embedded libxtst-dev On Target (i.MX device) alsa-utils libpng tslib
View full article
U-Boot is a bootloader, which supports some i.MX SoCs. Configuring U-Boot LTIB Creating Uimage Uboot U-boot FW Printenv FW Env File Add New i.MX5x Board on LTIB i.MX25 PDK I.MX25 PDK U-boot SplashScreen I.MX25 PDK U-boot SDCard i.MX27 ADS Board Compiling U-Boot for i.MX27ADS i.MX31 ADS Board I.MX31ADS Installing Uboot Blink i.MX31 PDK LEDs Using U-Boot i.MX51 EVK Board i.MX51 EVK U-boot i.MX51 EVK Compiling U-boot i.MX51 EVK Changing Env I.MX51EVK Install U-Boot i.MX53 Board i.MX53 USB Eth NFS i.MX53 ARD Dual LVDS i.MX53 QSB Board Get Started Additional Resources Script to Flash a Linux System into a SD card All Boards U-boot All Boards LTIB Creating Uimage Uboot Configuring U-Boot Running a Script in U-boot Transferring File Over Serial Transferring file over network U-boot.bin
View full article
D1 Capture - kernel 2.6.22 diff --exclude CVS -uNr linux-2.6.22/include/asm-arm/arch-mxc/memory.h linux-2.6.22.modified/include/asm-arm/arch-mxc/memory.h --- linux-2.6.22/include/asm-arm/arch-mxc/memory.h     2009-07-16 16:29:45.000000000 -0300 +++ linux-2.6.22.modified/include/asm-arm/arch-mxc/memory.h     2009-07-15 15:38:34.000000000 -0300 @@ -28,6 +28,7 @@     /* Size of contiguous memory for DMA and other h/w blocks */     #define CONSISTENT_DMA_SIZE     SZ_16M    +     /*!      * @defgroup Memory_MX27 Memory Map      * @ingroup MSL_MX27 @@ -48,7 +49,7 @@     #ifdef CONFIG_DMA_ZONE_SIZE     #define MXC_DMA_ZONE_SIZE     ((CONFIG_DMA_ZONE_SIZE * SZ_1M) >> PAGE_SHIFT)     #else    -#define MXC_DMA_ZONE_SIZE     ((12 * SZ_1M) >> PAGE_SHIFT)   +#define MXC_DMA_ZONE_SIZE     ((20 * SZ_1M) >> PAGE_SHIFT)     #endif      static inline void __arch_adjust_zones(int node, unsigned long *zone_size, diff --exclude CVS -uNr linux-2.6.22/drivers/media/video/mxc/capture/mxc_v4l2_capture.c linux-2.6.22.modified/drivers/media/video/mxc/capture/mxc_v4l2_capture.c ---    linux-2.6.22/drivers/media/video/mxc/capture/mxc_v4l2_capture.c     2009-07-16 16:29:43.000000000 -0300 +++ linux-2.6.22.modified/drivers/media/video/mxc/capture/mxc_v4l2_capture.c     2009-07-16 16:08:02.000000000 -0300 @@ -1650,9 +1650,9 @@                  /* setup cropping */                 cam->crop_bounds.left = 0; -             cam->crop_bounds.width = 640; +             cam->crop_bounds.width = 800;                 cam->crop_bounds.top = 0; -             cam->crop_bounds.height = 480; +             cam->crop_bounds.height = 600;                 cam->crop_current = cam->crop_defrect = cam->crop_bounds;                 ipu_csi_set_window_size(cam->crop_current.width,                                                       cam->crop_current.height); @@ -1663,7 +1663,7 @@                 cam->standard.id = V4L2_STD_UNKNOWN;                 cam->standard.frameperiod.denominator = 30;                 cam->standard.frameperiod.numerator = 1; -             cam->standard.framelines = 480; +             cam->standard.framelines = 600;                 cam->streamparm.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;                 cam->streamparm.parm.capture.timeperframe =                 cam->standard.frameperiod; cam->streamparm.parm.capture.capability = V4L2_CAP_TIMEPERFRAME; diff --exclude CVS -uNr linux-2.6.22/drivers/media/video/mxc/capture/ov2640.c linux-2.6.22.modified/drivers/media/video/mxc/capture/ov2640.c ---    linux-2.6.22/drivers/media/video/mxc/capture/ov2640.c     2009-07-16 16:29:45.000000000 -0300 +++ linux-2.6.22.modified/drivers/media/video/mxc/capture/ov2640.c     2009-07-16 16:07:03.000000000 -0300 @@ -698,12 +698,12 @@     #endif                            g_cam->streamparm.parm.capture.capturemode = 1;                 } else { -          out_width = 640; -          out_height = 480; +          out_width = 800; +          out_height = 600;                 g_cam->crop_bounds.left = 0; -          g_cam->crop_bounds.width = 640; +          g_cam->crop_bounds.width = 800;                 g_cam->crop_bounds.top = 0; -          g_cam->crop_bounds.height = 480; +          g_cam->crop_bounds.height = 600;                 g_cam->crop_current = g_cam->crop_defrect = g_cam->crop_bounds;     #ifdef CONFIG_ARCH_MX3                              ipu_csi_set_window_size(g_cam->crop_current.width ,
View full article
Question: Did we tested active PCIe components while the Cortex-A9 was in Sleep Mode (suspend to memory)? Answer: It's a known issue that PCIe can't support suspend/resume. And can't be built in kernel image if the system want suspend/resume. I think PCIe will be active while core is in sleep more. Is it different scenario? No, the pcie core is not active, it is in L2 state after suspend, and it can't resume back to L0 state when system resume is called. So, DO NOT let pcie do suspend operation right now. BTW, the tested device: * INTEL x1 1000M CT network card. * INTEL iwl wifi cards. * x1 pcie to usb3.0 card Yes, this patch had been tested on imx_3.0.35_4.0 release, and would be merged into next 3.0.35 release. TO1.2 is used. We tested the Patch against imx_3.0.35_4.0 release
View full article
The default FSL android BSP support 1 SD card slot. If customer need to support more sd slot in android.Please reference below steps. There are two steps need to set up. 1 device/fsl.git NOTE: 1  change the fstab. 2194000 is the address of usdhc2.             2  change the mount point in storage_list.xml diff --git a/sabresd_6dq/fstab.freescale b/sabresd_6dq/fstab.freescale index 7f23edb..1529a27 100644 --- a/sabresd_6dq/fstab.freescale +++ b/sabresd_6dq/fstab.freescale @@ -4,6 +4,7 @@ # specify MF_CHECK, and must come before any filesystems that do specify MF_CHECK /devices/soc0/soc.0/2100000.aips-bus/2198000.usdhc/mmc_host /mnt/media_rw/extsd vfat defaults voldmanaged=extsd:auto +/devices/soc0/soc.0/2100000.aips-bus/2194000.usdhc/mmc_host /mnt/media_rw/extsd_expand vfat defaults voldmanaged=extsd_expand:auto /devices/soc0/soc.0/2100000.aips-bus/2184000.usb/ci_hdrc.0  /mnt/media_rw/udisk vfat defaults voldmanaged=udisk:auto /dev/block/mmcblk3p5    /system      ext4    ro,barrier=1                                                                               wait,verify /dev/block/mmcblk3p4    /data        ext4    nosuid,nodev,nodiratime,noatime,nomblk_io_submit,noauto_da_alloc,errors=panic    wait,encryptable=/dev/block/mmcblk3p9 diff --git a/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml b/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml index 3639bdc..c3f5105 100644 --- a/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml +++ b/sabresd_6dq/overlay/frameworks/base/core/res/res/xml/storage_list.xml @@ -41,6 +41,10 @@               android:storageDescription="@string/storage_sd_card"               android:primary="false"               android:removable="true" /> +    <storage android:mountPoint="/storage/extsd_expand" +             android:storageDescription="@string/storage_sd_card" +             android:primary="false" +             android:removable="true" />      <storage android:mountPoint="/storage/udisk" 2  system/core.git NOTE: mkdir the mount point. build@scmbld2:~/maddev_lp5.1_consolidate_ga_10_30/system/core/rootdir$ git diff diff --git a/rootdir/init.rc b/rootdir/init.rc index 2211cc2..fac37c2 100644 --- a/rootdir/init.rc +++ b/rootdir/init.rc @@ -72,7 +72,9 @@ on init      mkdir /storage 0751 root sdcard_r      mkdir /mnt/media_rw/extsd 0755 system system +    mkdir /mnt/media_rw/extsd_expand 0755 system system      symlink /mnt/media_rw/extsd /storage/extsd +    symlink /mnt/media_rw/extsd_expand /storage/extsd_expand      mkdir /mnt/media_rw/udisk 0755 system system
View full article
Fixing Redboot RAM bug (CSD1 not activated) Introduction i.MX 35 PDK board has 256 MB of RAM, due to a bug in Redboot bootloader compiled for the board effectively there is only 128 MB available.This procedure fixes this bug to be able to use 256 MB of RAM. Redboot supporting 256 MB of RAM 1. Download the attached Redboot256.bin file. 2. Flash the new redboot image instead of the old one: Configuring RedBoot
View full article
You can but building times will take much longer (approximately 2 times longer for the core-image-minimal) compared to a build done on a native machine. In case you can not do the build on a native machine, make sure your virtual has enough hard-disk room (at least 50GB). For example, these are the build folders sizes after baking core-image-minimal: build$ du -h --max-depth=1 1.3G    ./sstate-cache 3.2M    ./cache 12K    ./.hob 32K    ./conf 22G    ./tmp 23G    . The tmp folder is by far the largest (containing building statistics, source code, deployed images, etc.) build/tmp$ tree -L 2 -d . ├── buildstats │   ├── cogl-imx6qsabresd │   ├── fsl-image-gui-imx6qsabresd │   ├── fsl-image-gui-sdk-imx6qsabresd │   ├── mesa-dri-imx6qsabresd │   ├── mesa-imx6qsabresd │   └── pseudo-native-imx6qsabresd ├── cache │   └── default-eglibc ├── deploy │   ├── images │   ├── licenses │   └── rpm ├── log │   ├── cleanlogs │   └── cooker ├── pkgdata │   ├── all-poky-linux │   ├── all-poky-linux-gnueabi │   ├── armv7a-vfp-neon-poky-linux-gnueabi │   ├── imx6qsabresd-poky-linux │   └── imx6qsabresd-poky-linux-gnueabi ├── sstate-control ├── stamps │   ├── all-poky-linux │   ├── all-poky-linux-gnueabi │   ├── armv7a-vfp-neon-poky-linux-gnueabi │   ├── imx6qsabresd-poky-linux │   ├── imx6qsabresd-poky-linux-gnueabi │   ├── work-shared │   └── x86_64-linux ├── sysroots │   ├── imx6qsabresd │   ├── imx6qsabresd-tcbootstrap │   └── x86_64-linux ├── work │   ├── all-poky-linux │   ├── all-poky-linux-gnueabi │   ├── armv7a-vfp-neon-poky-linux-gnueabi │   ├── imx6qsabresd-poky-linux │   ├── imx6qsabresd-poky-linux-gnueabi │   └── x86_64-linux └── work-shared     └── gcc-4.7.2-r13
View full article
Extending to the impact produced by being the First to release WEC7 on i.MX6 Development Platform, iWave Systems adds yet another accomplishment by announcing the availability of Windows Embedded Compact 7 (WEC7) reference BSP for Freescale’s i.MX6x SABRE SDB/SDP. The Freescale’s i.MX6x SABRE SDB/SDP Platform is powered with Freescale’s i.MX6 Quad/Dual Lite 1GHz, MMPF0100 Freescale PMIC. The WEC7 BSP release supports SATA II, Standard SD/SDIO, Gigabit Ethernet, LVDS, Touch Panel, HDMI port and also necessary hardware codecs supported by the CPU. Debugging tools like KITL and CETK are also supported. All the latest features that WEC7 offers such as Silverlight 3.0, MPEG-4 HD, Expression Blend, Active Sync and also Adobe Flash10.1 are made available.                                                                                                                                                                 Benefits: WEC7 Source code can be easily customized with respect to the target hardware platform Simple and low cost integration for any Freescale i.MX6x based platform       Quick time to market Highlights: Ideal for Quick Proof of concept (POC) development Shortens up to 60% of the new product development life cycle                                       Quick customization services in a very short period Features: Standard Features: i.MX6 Quad/Dual Lite 1GHz CPU MMPF0100 Freescale PMIC 1 GB DDR3 RAM Serial console SD boot SATA II SD/SDIO HDMI Gigabit Ethernet USB OTG Audio LVDS display Touch Optional Features: PCIe Camera CAN GPS VPU (HD Coding and Decoding supported) GPU (Open GL, Open VG, Direct3DM and DirectDraw) Target Applications: Automotive IVI Telematics Interactive POS Industrial HMI Medical Click Here for more details on WEC7 BSP Support for Freescale's i.MX6x Sabre SDB/SDP by iWave Click Here for more details on WEC7 BSP Support for various other i.MX processors
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343046 
View full article
Overview: This document is written for Freescale customers who have Freescale AC3 release packages (excluded package). (If you did not have the AC3 release package, you can disregard this document.) Freescale OMX Player in Android release supports audio track selection when playing files with multiple audio tracks. However, most customers don't use this enhanced API to select the audio track even if current audio codec is not supported. To avoid a soundless output when partial audio track can be played, this document provides the method to select the available audio track automatically to play. The patch in this document is not included in our current release because it did not match with our track selection rule - play the first track. If you have any idea with this issue, feel free to add comments into this document. Issue description: Software: R13.4-GA or R13.4.1 Android releases Hardware: MX6Dual/Quad SabreSD board Test source: 1.mkv Test Step: 1. Lunch Gallery from main menu. 2. Play the video And you can see the watch the video without any sound Root Reason: The file has 2 audio track DTS & AC3: audio track 1 is DTS and track 2 is AC3. OMX Player will choose the first audio track to play as default audio track, which is DTS audio. However, the software only supports the AC3 audio codec, so it could not set up audio decoder for DTS track. If we choose to play the AC3 track, sounds could be heard. How to fix: The audio track index is set in GMPlayer::LoadParser(). You can get audio format to check whether it is supported by decoder. Please see the patch audio_track_slection.diff
View full article
i.MX27 PDK Board Flashing This tutorial teaches how to flash bootloader using ATK. To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot. Using ATK ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. This section will describe the procedure to erase the flash memory and program the bootloader. 1 - Connect a serial cable between PC and i.MX board. 2 - Some hardware configurations (switches) must be done to flash the board. Set red and cream switches as below: Switch SW5 -> 00000 Switch SW4 -> 10000001 Installing ATK on Linux Download ATK: Download. Extract ATK: # unzip ATK_1_41_STD_installer.zip Execute the default install process: # wine SETUP.EXE Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32) Run ATK: # wine ADSToolkit_std.exe Next Step To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot. PS: On SW5 and SW4, "1" means the keys selected towards the edge of the board. 3 - Run ATK by clicking Start -> Programs -> AdvancedToolKit -> AdvancedToolKit       Set the options:    Device memory -> DDR; Custom Initial File -> (keep it unmarked)    Communication Channel -> Serial Port (Usually COM1) 4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO. Flash Erasing 1 - To erase Flash memory, select the parameters as shown in the figure below: 2 - Turn on the board and press Erase. 3 - ATK shows this message when flash is erased Flash Programming The next step is to program the bootloader image into the board's Flash following the steps below. 1 - Select the parameters as shown in the figure below and press Program. The bootloader binary image file can be found into your Board Support Package Set Program, NAND, Address: 0x00000000 2 - Add it on Image File field and press Program. 3 - Close ATK, turn off the board and set switch back as shown in the picture below. Installing ATK on Linux Download ATK: Download. Extract ATK: # unzip ATK_1_41_STD_installer.zip Execute the default install process: # wine SETUP.EXE Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32) Run ATK: # wine ADSToolkit_std.exe Next Step To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot.
View full article
After porting u-boot to your i.MX5x board you might want add it on LTIB menu, "Choose your board for u-boot" section. For this, edit ltib/config/platform/imx/main.lkc to add your board: Enter board on menu: comment "Choose your board for u-boot" choice prompt "board" default BOARD_MX51_BBG depends on PLATFORM = "imx51" help This menu will let you choose the board you use. ... + config BOARD_MX53_MYBOARD + bool "mx53_myboard" ... endchoice Add the "mx53_myboard_config" that matches your board configuration on the u-boot Makefile to PKG_U_BOOT_CONFIG_TYPE: config PKG_U_BOOT_CONFIG_TYPE   string   ... + default "mx53_myboard_config" if ( PLATFORM = "imx51" && BOARD_MX53_MYBOARD && !PKG_KERNEL_UPDATER )   ...
View full article
Quick Steps Four quick steps to build and flash a UBIFS image on i.MX35 NAND (K9LBG08U0D-PCB0), for information on how to you another memory, please see next section. Enable MTD_UBI and UBIFS_FS on kernel Create UBI image from rootfs (used for NFS) - ON PC mkfs.ubifs -v -r rootfs -m 2048 -e 258048 -c 966 -o ubifs.img ubinize -o ubi.img -m 2048 -p 256KiB -s 2048 ubinize.cfg Format NAND using UBI image - ON TARGET ubiformat -f ubi.img /dev/mtd8 Load UBI file system load -r -b 0x100000 zImage fis create -f 0x300000 kernel fis load kernel exec -c "noinitrd console=ttymxc0 115200 ubi.mtd=8 root=ubi0:rootfs rw rootfstype=ubifs ip=none" How To First of all, install mtd-utils on both target and host: Target: ./ltib -c Package list [*] mtd-utils Host sudo aptget install mtd-utils 1. Enable MTD_UBI and UBIFS_FS on kernel MTD_UBI -> Device Drivers     -> Memory Technology Device (MTD) support (MTD [=y])           -> UBI - Unsorted block images                   <*> Enable UBI                    (4096) UBI wear-leveling threshold (NEW)                    (1) Percentage of reserved eraseblocks for bad eraseblocks handling (NEW)                 < > MTD devices emulation driver (gluebi) (NEW)                    ** UBI debugging options **                    [ ] UBI debugging (NEW) UBIFS_FS -> File systems         ->Miscellaneous filesystems             <*> UBIFS file system support                 [ ] Extended attributes support (NEW)                 [ ] Advanced compression options (NEW)                 [ ] Enable debugging (NEW) 2. Create UBI image On TARGET Collect some information needed in order to create the UBI image according to your NAND device root@freescale \~$ cat /proc/mtd dev:   size   erasesize name mtd0: 00080000 00020000 "Bootloader" mtd1: 00400000 00020000 "nor.Kernel" mtd2: 01e00000 00020000 "nor.userfs" mtd3: 01c00000 00020000 "nor.rootfs" mtd4: 00003000 00020000 "FIS directory" mtd5: 02001000 00020000 "Redboot config" mtd6: 00300000 00040000 "nand.bootloader" mtd7: 00500000 00040000 "nand.kernel" mtd8: 10000000 00040000 "nand.rootfs" mtd9: 00800000 00040000 "nand.configure" mtd10: 6f000000 00040000 "nand.userfs" I will use mtd8, because I want the NAND rootfs MTD partition. More on [1] root@freescale ~$ ubiattach /dev/ubi_ctrl -m 8 UBI: attaching mtd8 to ubi0 UBI: physical eraseblock size:   262144 bytes (256 KiB) UBI: logical eraseblock size:    258048 bytes UBI: smallest flash I/O unit:    2048 UBI: VID header offset:          2048 (aligned 2048) UBI: data offset:                4096 UBI: empty MTD device detected UBI: create volume table (copy #1) UBI: create volume table (copy #2) UBI: attached mtd8 to ubi0 UBI: MTD device name:            "nand.rootfs" UBI: MTD device size:            256 MiB UBI: number of good PEBs:        979 UBI: number of bad PEBs:         45 UBI: max. allowed volumes:       128 UBI: wear-leveling threshold:    4096 UBI: number of internal volumes: 1 UBI: number of user volumes:     0 UBI: available PEBs:             966 UBI: total number of reserved PEBs: 13 UBI: number of PEBs reserved for bad PEB handling: 9 UBI: max/mean erase counter: 0/0 UBI: image sequence number: 0 UBI: background thread "ubi_bgt0d" started, PID 2098 UBI device number You will need: -p = physical eraseblock size = 256KiB -e = logical eraseblock size = 258048 -m = smallest flash I/O unit = 2048 -s = VID header offset = 2048 -c = available PEB = 966 Values only for iMX35 PDK NAND - K9LBG08U0D-PCB0 3. ON HOST - Now, create the images (two steps) You need to create ubinize.cfg file! ubinize.cfg [ubifs] mode=ubi image=ubifs.img vol_id=0 vol_size=237MiB vol_type=dynamic vol_name=rootfs vol_flags=autoresize $ mkfs.ubifs -v -r rootfs -m 2048 -e 258048 -c 966 -o ubifs.img mkfs.ubifs      root:                rootfs/      min_io_size:    2048      leb_size:         258048      max_leb_cnt:   966      output:            ubifs.img      jrn_size:          8388608      reserved:         0      compr:            lzo      keyhash:         r5      fanout:            8      orph_lebs:       1      super lebs:      1      master lebs:    2      log_lebs:         4      lpt_lebs:          2      orph_lebs:       1      main_lebs:       132      gc lebs:           1      index lebs:       2      leb_cnt:           142      UUID:              CC2057F9-B20F-46D1-A399-1FCA95DCAFF7 Success\! $ ubinize -o ubi.img -m 2048 -p 256KiB -s 2048 ubinize.cfg $ ls -lh u* -rw-r--r-- 1 daiane daiane 35M 2010-11-26 15:21 ubifs.img -rw-r--r-- 1 daiane daiane 36M 2010-11-26 15:22 ubi.img -rw-r--r-- 1 daiane daiane 113 2010-11-26 15:22 ubinize.cfg $ sudo cp ubi.img rootfs/home/ 4. Format NAND using UBI image - ON TARGET Turn on target (or reset it) and format MTD partition $ cd /home $ ubiformat -f ubi.img /dev/mtd8 5. Load UBI file system Reset and change redboot script: .. fis load kernel .. exec -c "noinitrd console=ttymxc0 115200 ubi.mtd=8 root=ubi0:rootfs rw rootfstype=ubifs ip=none"
View full article
Q: How to get the CSI BT656 without HSYNC/VSYNC working. The problem, is that all implemented driver in the BSP are using the external HSYNC/VSYNC synchronization signal. The SW designer is actually struggling to find the right way to generate the end of field active interrupt (end of frame). > mxc_v4l2_still.out I get an: > ERROR: v4l2 capture: mxc_v4l_read timeout counter 0 > > When using mxc_v4l2_capture.out or mxc_v4l2_tvin.out I get an: > ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0 > To help him implementing the driver, I need to get some insight on the IPUx_CSIn_CCIR_CODE_1/2/3 as it seems that the bit description 21 to 19 (CSI_STRT_FLD0_ACTV) is not described (same for all the multiple bit field in this register. Maybe it should match the ITU656, but here as well the driver examples does not match the bit description of the ITU standard. So my questions: IS it really possible to implement the BT656 with SAV / EAV and without external HSYNC/VSYNC? If yes, is it possible to review the IPUx_CSIn_CCIR_CODE_1/2/3 fields and communicate which parameter should be provided here? i.MX6Q A:      For no VSYNC and HSYNC case, in the sensor driver such as "linux-3.0.35\drivers\media\video\mxc\capture\adv7180.c", function ioctl_g_ifparm(), you should set p->u.bt656.bt_sync_correct to 0;      p->u.bt656.bt_sync_correct = 1; // It means external VSYNC and HSYNC will be used for SYNC.      p->u.bt656.bt_sync_correct = 0; // No external VSYNC and HSYNC, embedded EAV and SAV will be used for SYNC.      In iMX6 BSP, the CCIR related code is ready in "linux-3.0.35\drivers\mxc\ipu3\ipu_capture.c", function ipu_csi_init_interface(), no code modification was needed, that code was verified work.      For BT656 mode, your sensor driver such as adv7180, should also report correct parameters in function function ioctl_g_ifparm().      p->u.bt656.clock_curr = 0;  // This will tell linux-3.0.35\drivers\media\video\mxc\capture\mxc_v4l2_capture.c to use "IPU_CSI_CLK_MODE_CCIR656_INTERLACED" in function mxc_v4l2_s_param().      The current iMX6 BSP mxc_v4l2_capture.c driver doesn't support BT656 progressive mode, it only supports BT656 interlace mode. To support BT656 progressive mode, the customer should modify the code in mxc_v4l2_s_param(), let csi_param.clk_mode = IPU_CSI_CLK_MODE_CCIR656_PROGRESSIVE. This is exactly what they are doing, but still it doesn’t work. Actually, they see the code being executed following the right steps in the ipu_csi_init_interface() going through PAL 720x625 configuration. But still, they get the timeout! else if (cfg_param.clk_mode == IPU_CSI_CLK_MODE_CCIR656_INTERLACED) {       if (width == 720 && height == 625) {         /* PAL case */         /*         Field0BlankEnd = 0x6, Field0BlankStart = 0x2,         Field0ActiveEnd = 0x4, Field0ActiveStart = 0           */         ipu_csi_write(ipu, csi, 0x40596, CSI_CCIR_CODE_1);         /*         Field1BlankEnd = 0x7, Field1BlankStart = 0x3,         Field1ActiveEnd = 0x5, Field1ActiveStart = 0x1           */         ipu_csi_write(ipu, csi, 0xD07DF, CSI_CCIR_CODE_2);         ipu_csi_write(ipu, csi, 0xFF0000, CSI_CCIR_CODE_3); So, I believe the parameters are wrong. What could be missing. Can you review the driver? For me it looks like the adv example, except the bt_sync_correct=0, which is what we want. You can suggest the customer to capture the CSI data bus to check if there is correct output from sensor, such as EAV/SAV. For the "timeout" error, it always means there is no correct data on CSI data bus. This document was generated from the following discussion: CSI BT656
View full article
Configuring RedBoot The configuration is made using a Minicom session that need to be established between host and target through serial port. To have an operational system been executed just on the power on, configure the right for Boot script. The chooses are shown in Boot Script section. To avoid the start of operational system, power on the board and press CTRL-C immediately. Wait until RedBoot> prompt appears. Overview The main command for beginners is fconfig -l that can be abbreviated as fc -l    This command shows the actual configuration of Redboot, like: RedBoot> fc -l Run script at boot: true Boot script: .. load -r -b 0x100000 /tftpboot/zImage .. exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/n" Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false RedBoot> Run script at boot: set true for booting with a script or false to always enter on prompt directly Boot script: define what commands to execute as script at the startup Boot script timeout: how many time to wait before execute boot script Use BOOTP for network configuration: set true for getting configuration from BOOTP or false for manually configuring gateway and IP address Gateway IP address: The IP address of the gateway Local IP address: The board IP address Local IP address mask: The board IP mask address Default server IP address: The host IP address when NFS and TFTP server are running Configuring Network Execute the command to configure network parameters: RedBoot> fc This step guarantee the possibilities to load images from some server previously connected and configured. For Use BOOTP for network configuration: answer false. For Gateway IP address: type the gateway IP address of your network; For Local IP address: type an IP address to your board, it needs to be a valid IP in your network; For Local IP address mask: type the IP mask address; For Default server IP address: type the IP of your host server where are running TFTP and NFS. Pay special attencion for Update RedBoot non-volatile configuration - continue (y/n)?. Answer y to have your configuration saved in the flash. To verify if your configuration is working use ping, be patient this command is very slow: RedBoot" ping -h 10.29.244.99 Network PING - from 10.29.241.6 to 10.29.244.99 PING - received 10 of 10 expected Use the "-n" option to change the number of pings and the "-r" option to speed things up, such as: ping -n 3 -h 10.29.244.99 -r 10. The boot script configuration is done in the next section. Boot Script NFS Boot In NFS Boot mode, a kernel image and a root file system image are loaded from a configured server through TFTP and NFS that can be executed doing the development more easy. To configure RedBoot for NFS Boot reset the board and press CTRL-C immediately. In a Minicom session type fc to modify the configuration boot. Enter the script boot below: RedBoot> fc Run script at boot: true Boot script: Enter script, terminate with empty line >> load -r -b 0x100000 /tftpboot/zImage >> exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.244.99:/tftpboot/rootfs init=/linuxrc ip=10.29.241.6:10.29.244.99" >> Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0x00080000: . ... Erase from 0x00080000-0x000a0000: . ... Program from 0x07ee0000-0x07f00000 at 0x00080000: . RedBoot> The script is composed by two lines. The first line load the kernel image (zImage) by TFTP from /tftpboot, the directory configured in TFTP.\ The second line executes the kernel and mount the root file system using NFS. The path /tftpboot/ltib indicates the path that should be exported in the host machine. (It's the path in the /etc/exports) 10.29.244.99 is the host IP address 10.29.241.6 is the target IP address Flash Boot For flash boot the Boot Script differs a little bit: fis init kernel exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock8 rw rootfstype=jffs2 ip=none" The value for root can be different for each board type.
View full article
document about how to use usb camera on imx6 android-4.0 platform.
View full article