i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
    Test envs: BOARD: i.MX 8MN EVK BSP: L6.6.36   The L6.6.y includes the feature about supporting starting Cortex-M33 from non-TCM address for i.MX93, but not for i.MX8M series.    LF-7815 remoteproc: imx_rproc: support starting Cortex-M33 from non-TCM address for i.MX93 https://github.com/nxp-imx/linux-imx/commit/680aa11c7bdaddf6bbffd74bc0a94ef67593b69b#diff-66a34e17e82d281936f559217adc3983b39abeb2e478967f3d5cef2eed5b67fcR693   For older BSP, customer can refer this full patch set https://patchew.org/linux/[email protected]/   If you want to test ELF in DDR on i.MX8M series and i.MX93 platform with L6.6.y, please use below patch set.  
記事全体を表示
some customers have issue with uboot resetting on new bsp because of lack of mac address and different design fom nxp evk board, this doc shows how to set the mac address in different way(fuse, dts file, header file), then check the different HW design between customized board with nxp board, according to the HW design to change the uboot 
記事全体を表示
Please notice the following patches are only tested in the environment that is listed below. For the environment with other software versions or hardware equipment, some other editing  may be required Environment: i.MX 8MP EVK MIPI DSI: MX8-DSI-OLED1 (RM67191) Software: LF5.15.71 U-boot: 1. Apply '0001-Modify-u-boot-to-show-logo-seamlessly.patch' to make sure display related models won't be power off, which will help to achieve seamless display. Kernel: 1. Apply '0001-Keep-NXP-logo-until-Weston-is-booted-8MP-MIPI.patch' to make sure MIPI-DSI related models won't be re-init in the booting progress.
記事全体を表示
Please notice the following patches are only tested in the environment that is listed below. For the environment with other software versions or hardware equipment, some other editing  may be required Environment: i.MX 93 EVK LVDS:LVDS BOE EV121WXM-N10-1850  Software: LF6.1.36 U-boot: 1. Apply '0001-Add-LVDS-driver-and-BOE-12.1-EV121WXM-N10-1850-LVDS-.patch' to enable EV121WXM-N10-1850  in U-boot stage. If other LVDS panel is used here, you will need porting your specific LVDS device in this step. 2. Apply '0002-Modify-u-boot-to-show-logo-seamlessly.patch' to make sure display related models won't be power off, which will help to achieve seamless display. Kernel: 1. Apply '0001-Keep-NXP-logo-until-Weston-is-booted-for-i.MX93-in-L.patch' to make sure LVDS related models won't be init in the booting progress.
記事全体を表示
Please notice the following patches are only tested in the environment that is listed below. For the environment with other software versions or hardware equipment, some other editing  may be required Environment: i.MX 8MP EVK LVDS:LVDS BOE EV121WXM-N10-1850  LVDS to MiniSAS panel:XMX-LVDS-MINISAS Software: LF5.15.71 U-boot: 1. Apply '0001-Enable-DY1212W-4856-in-U-boot-for-i.MX8MP.patch' to enable EV121WXM-N10-1850  in U-boot stage. If other LVDS panel is used here, you will need porting your specific LVDS device in this step. 2. Apply '0002-Modify-u-boot-to-show-logo-seamlessly-for-i.MX8MP.patch' to make sure display related models won't be power off, which will help to achieve seamless display. 3. In the original U-boot driver, PWM isn't enable. Therefore, apply '0003-Enable-PWM-and-BACKLIGHT-in-U-boot-and-modify-to-sho.patch' to enable PWM. Kernel: 1. Apply '0001-Enable-DY1212W-4856-in-Kernl-for-i.MX8MP.patch' to enable EV121WXM-N10-1850  in Kernel. If other LVDS panel is used here, you will need porting your specific LVDS device in this step. 2. Apply '0002-Modify-Kernel-to-show-logo-seamlessly-for-i.MX8MP.patch' to make sure LVDS related models won't be init in the booting progress. 3. Apply '0003-Enable-PWM-and-BACKLIGHT-in-Kernel-and-modify-to-sho.patch' to make sure we could edit backlight of panel in Kernel. 
記事全体を表示
  JEIDA-24 is adopted in most use-cases, and also the default format in Linux BSP(6.x)  Actually, JEIDA-18 is also supported in Linux BSP by not mentioned explicitly.   JEIDA-18 can be supported in two configuration: 1. Keep JEIDA-24 setting to display controllers, skip 4th data-lane in hardware connection: according JEIDA-24 output waveform, it has 4 data-lane enabled on LVDS bus: since the data-bits on TxOUT3 are the LSBs of the pixels, to change from JEIDA-24(RGB888, 4 data-lane) to JEIDA-18(RGB666, 3 data-lane), it can be achieved by skipping the TxOUT3 output(4th data-lane) in hardware connection, to make the JEIDA-18 format as the picture below(JEIDA-18 LCD panels only require 3 data-lanes)   2. Change the display controller settings to JEIDA-18: one reference by Variscite, one of the SoM vendor: https://variwiki.com/index.php?title=DART-MX8M-PLUS_Display&release=mx8mp-yocto-mickledore-6.1.36_2.1.0-v1.3 related setting quoted from the link above: Supported "data-mapping" values are "jeida-18", "jeida-24" and "vesa-24". Supported "fsl,data-mapping" values are "jeida", and "spwg". Supported "fsl,data-width" values are <18>, and <24>.    "data-mapping"= "jeida-18", "jeida-24" and "vesa-24" are handled in DRM driver, as the link below: https://github.com/nxp-imx/linux-imx/blob/d23d64eea5111e1607efcce1d601834fceec92cb/drivers/gpu/drm/drm_of.c#L451 if (!strcmp(mapping, "jeida-18")) return MEDIA_BUS_FMT_RGB666_1X7X3_SPWG; if (!strcmp(mapping, "jeida-24")) return MEDIA_BUS_FMT_RGB888_1X7X4_JEIDA; if (!strcmp(mapping, "vesa-24")) return MEDIA_BUS_FMT_RGB888_1X7X4_SPWG;    Here the variable “MEDIA_BUS_FMT_RGB666_1X7X3_SPWG" is handled in ldb driver(MX8MP) as the link below: https://github.com/nxp-imx/linux-imx/blob/d23d64eea5111e1607efcce1d601834fceec92cb/drivers/gpu/drm/bridge/fsl-ldb.c#L144 switch (bridge_state->output_bus_cfg.format) { case MEDIA_BUS_FMT_RGB666_1X7X3_SPWG: lvds_format_24bpp = false; lvds_format_jeida = true; break; case MEDIA_BUS_FMT_RGB888_1X7X4_JEIDA: lvds_format_24bpp = true;  the bus_format would be "MEDIA_BUS_FMT_RGB666_1X18" in this configuration:  https://github.com/nxp-imx/linux-imx/blob/d23d64eea5111e1607efcce1d601834fceec92cb/drivers/gpu/drm/imx/imx8mp-ldb.c#L178 switch (ldb_ch->bus_format) { case MEDIA_BUS_FMT_RGB666_1X7X3_SPWG: imx_crtc_state->bus_format = MEDIA_BUS_FMT_RGB666_1X18; break;    “MEDIA_BUS_FMT_RGB666_1X18” is not handled in LCDIF driver:  https://github.com/nxp-imx/linux-imx/blob/d23d64eea5111e1607efcce1d601834fceec92cb/drivers/gpu/imx/lcdifv3/lcdifv3-common.c#L310 switch (bus_format) { case MEDIA_BUS_FMT_RGB565_1X16: disp_para |= DISP_PARA_LINE_PATTERN(LP_RGB565); break; case MEDIA_BUS_FMT_RGB888_1X24: disp_para |= DISP_PARA_LINE_PATTERN(LP_RGB888_OR_YUV444); break; default: dev_err(lcdifv3->dev, "unknown bus format: %#x\n", bus_format); return;    hence there would be error message below in this configuration, which can be ignored: imx-lcdifv3 32e80000.lcd-controller: unknown bus format: 0x1009  
記事全体を表示
Hibernation mode (suspend to disk) will be useful for boot time optimization, especially under heavy application usage cases. This article is a quick guide for how to enable hibernation mode in Linux running on i.MX93. Some limitation and pitfalls will also be introduced.   Detail PDF attached.    
記事全体を表示
There are two ethernet ports in i.MX8MP: FEC0 and FEC1(eQOS). Normally we use iperf to test ethernets ports performance. However, when using tftp test, the result is different in two ports. This document describe how to fine tune parameters to increase speed under tftp test or other use case. It is suitable for most i.MX serials and most BSP version.
記事全体を表示
Poring from MCIMX6Y2CVM05AB to MCIMX6Y1DVM05AB Backgroud: Our customers encounter Kernel stuck at starting kernel issue. Here is detail description as below: (1 )Using customer board, and the main chip is MCIMX6Y1DVM05AB. (2) MCIMX6Y2CVM05AB works fine using the same image. (3)The kernel version is L5.10.52. But the old L4.14.98 works fine. (4)Using imx6ull evk's dtb has the same symptom. (imx6ull-14x14-evk.dtb in L5.10.52 prebuild image from NXP. (5)The  L4.14.98 versionBSP both  MCIMX6Y1DVM05AB and MCIMX6Y2CVM05AB can work well For the L5.10.52 only the MCIMX6Y2CVM05AB can work​. Kernel crash at here:   Generally speaking, most customer need to porting from old chip to new, for this customer need to use porting from the new product to old products they have their reasons.     Two reasons: (1) Their previous project use MCIMX6Y1DVM05AB. And also have MCIMX6Y1DVM05AB stock. (2) And the customer needs 15kpcs for urgent demand. But there is no MCIMX6Y2CVM05AB stock in their city.​ Porting steps: For these two products, they are difference, but most pins to pins in design. 1\Found the difference for this two product: See the datasheet: https://www.nxp.com.cn/docs/en/data-sheet/IMX6ULLCEC.pdf https://www.nxp.com.cn/docs/en/data-sheet/IMX6ULLIEC.pdf     For the MCIMX6Y1DVM05AB do not have the LCD/CSI, one CAN, one Ethernet,one ADC.   2\Check the customer’s board dts setting and modify Ask customer for their Board dts file and check: The MCIMX6Y1DVM05AB chip has only followed features, so customer should make sure the related drivers are removed from dts. That means in climaxL5.10.52.7z, customer should disable the followed drivers: pxp, lcdif, can2. (csi and fec2 are already disabled) (1) Disable the fec2   (2)CSI disable   (3)Lcdif disable   (4)CAN 2 Remove     Result: After remove these unused functions. The MCIMX6Y1DVM05AB could boot well on customer’s board. If customer use the MCIMX6Y2CVM05AB, all these functions need to add.  
記事全体を表示
This document is about enable iMX93 PWM and PWM led HW:   iMX93 11x11 EVK SW:   lf-6.6.3-1.0.0 PWM: TPM3 CH0, CH2            TPM4 CH2 Note: The i.MX PWM and           PWM led are already            enabled in lf-6.6.3-1.0.0  
記事全体を表示
share more detailed steps how to bring up stereo capture of basler camera by imx8mp
記事全体を表示
This is an example for user to transfer files between i.MX8MP Linux platform and other devices via Bluetooth. Environment : Hardware : i.MX8MP LPDDR4 EVK Board, Android Phone Software : L6.6.23-2.0.0   Step1 : Build Yocto image and burnt to the SD card or EMMC repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.23-2.0.0.xml repo sync DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build-xwayland Add the following code to "conf/local.conf"          IMAGE_INSTALL:append = " glibc-gconv-utf-16" bitbake imx-image-full uuu -b emmc_all imx-image-full-imx8mp-lpddr4-evk.rootfs-20240919015845.wic Step2 : Test steps Boot board with "imx8mp-evk-usdhc1-m2.dtb" file. load Wi-Fi Firmware           root@imx8mp-lpddr4-evk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf Load BT firmware and enable BT          root@imx8mp-lpddr4-evk:~# modprobe btnxpuart          root@imx8mp-lpddr4-evk:~# hciconfig                    root@imx8mp-lpddr4-evk:~# hciconfig hci0 up connect  the BT of Android Phone          root@imx8mp-lpddr4-evk:~# bluetoothctl          [bluetooth]# default-agent          [bluetooth]# agent on          [bluetooth]# discoverable on          [bluetooth]# scan on          [bluetooth]# scan off                    [bluetooth]# pair 90:F0:52:92:A6:6C          we need to type Yes on board and click 配对 on phone.                           [bluetooth]# connect 90:F0:52:92:A6:6C                 [Meizu16m]# quit          Transfer file          1). Android Phone-> i.MX8MP EVK Board          root@imx8mp-lpddr4-evk:~# /usr/libexec/bluetooth/obexd -a -n -r /root/ & obexctl                   Then select a file on your phone ad choose transfer by Bluetooth.                   2).i.MX8MP EVK Board -> Android Phone          [obex]# connect 90:F0:52:92:A6:6C                   [90:F0:52:92:A6:6C]# send /home/root/test.txt          Note :  1. Do not suggestion use IOS phone. 2. If your i.MX8MP board can not scan your BT device, Suggest change the device BT name and run on "scan on" command again.  
記事全体を表示
We are pleased to announce that Config Tools for i.MX v16.1 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) • Clocks – Disabling enabled clock outputs that have settings with shared bit-fields after reopening the configuration is fixed. – Clock slices with multiple outputs are supported. • TEE – An incorrect number of the MPU region attributes shown for the configuration of RT1180 is fixed. – An incorrect domain visibility and tab names when DAC is disabled on RT1180 is fixed.
記事全体を表示
The purpose of this document is to provide extended guidance for the selection of compatible LPDDR4 memory devices that are supported by the i.MX 91 series of processors. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs. Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity.   LPDDR4 - Maximum Supported Densities SoC Max Data bus width Maximum density Assumed memory organization Notes i.MX 91 (i.MX 91xx) 16-bit 16 Gb / (2 GB) single rank, single channel device with 17-row addresses (R0 - R16) 1, 2, 3   LPDDR4 - List of Validated Memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part# Notes i.MX 91 16 Gb / (2 GB) Micron MT53E1G16D1FW-046 AAT:A MT53E1G16D1ZW-046 AAT:C 5    2 Gb / (256 MB)  Winbond  W66BP6NBHAHJ 4 8 Gb / (1 GB) Nanya NT6AN512M16AV-J1I   4 Gb / (512 MB) Nanya NT6AN256M16AV-J1I 4 8 Gb / (1 GB) ISSI IS43LQ16512B-046BLI 4 12 Gb / (1.5 GB) Micron MT53E768M16D1ZW-046 4 16 Gb / (2 GB) Intelligent Memory IMAG16L4KBBG 4 2 Gb / (256 MB) Nanya NT6AN128M16AV-J1 4 4 Gb / (512 MB) UniIC SCB11N4G160BF-04ZI 4 4 Gb / (512 MB) ISSI IS43LQ16256B-053BLI 4 4 Gb / (512 MB) Winbond W66CP6RBHAHJ 4     Note: This device supports operation with LPDDR4 memories only. LPDDR4x operation is not supported. Dual‑mode memories that support both LPDDR4 and LPDDR4x are allowed as long as the device can operate in LPDDR4 mode, including using LPDDR4 I/O voltage levels and initialization sequences. NOTE: LPDDR4 devices from certain memory vendors may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low-speed operation is planned in the use case, please consult with the memory vendor about the configuration aspects and possible customization of the memory device so correct functionality is ensured. Note 1: The numbers are based purely on the IP documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, SoC reference manual and on the JEDEC standards JESD209-4B (LPDDR4). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The SoC also supports dual rank single channel devices therefore, 16Gb/2GB density can be also achieved by using a dual rank single channel device with 16-row addresses (R0 - R15). Note 4: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 5: The memory part number is not recommended for new designs and superseded by a new part number
記事全体を表示
The layer attached to this article is obsolete. Please use the meta-imx-fastboot GitHub repo instead.   The purpose of this article is to show how to reduce the boot time on i.MX 8QXP using U-Boot Falcon Mode. The general technique is presented in the AN14093. This article was tested on LF-6.6.23-2.0.0 BSP. How to do it 1. Follow the steps in the i.MX Yocto Project User's Guide and prepare your Yocto building environment. We will further assume that the BSP is in the ~/imx-yocto-bsp directory and the build directory is ~/imx-yocto-bsp/build. 2. Unpack the attached archive in ~/imx-yocto-bsp/sources. This should create the ~/imx-yocto-bsp/sources/meta-imx-fastboot directory.  3. Add the meta-imx-fastboot layer to your build using the following command: bitbake-layers add-layer ~/imx-yocto-bsp/sources/meta-imx-fastboot 4. If you've previously built an image in the same tree, clean the u-boot-imx and imx-boot packages using the following command: bitbake -c clean u-boot-imx imx-boot 5. Build the new image. Out of the box, this package is configured for core-image-minimal. We will show you below how to adapt it for other images: bitbake core-image-minimal 6. Write the resulted image on eMMC/SD using your preferred method and boot the board. 7. By default, the board will boot normally. To enable fast boot, stop the board in U-Boot, and run the following command: u-boot => run prepare_fdt 8. Reboot the board. From this point on, the board should boot in fast mode. Far less messages will be printed by the kernel or systemd during boot. You may further optimize the boot time by removing unnecessary features from the kernel and/or removing unnecessary services started by systemd. Please refer to AN14093. 9. If you ever want to re-enter U-Boot, please keep the 'c' key pressed in the serial console during board power-on. It's easiest if you press and keep the 'c' key pressed before powering on/pressing the reset button. How it works The layer we've added contains patches for U-Boot, ATF and imx-mkimage. In addition, it modifies the core-image-minimal recipe. In U-Boot, the necessary options for Falcon Mode are added in a new configuration file, named imx8qxp_mek_falcon_defconfig, as well as an implementation of the spl_start_uboot() function. In ATF, the device tree load address is added in the correct parameter. In mkimage, two new targets are created: kernel-atf-container.img (to be deployed in the boot partition) and uImage (to be deployed in the rootfs). The change in the core-image-minimal recipe ensures that the new files are copied in the resulting image. If you want to build a different image, you need to copy the content of core-image-minimal.bbappend in a new file, named according to the image you want to build. For example, if you want to build imx-image-full, you could use the following command: cp ~/imx-yocto-bsp/sources/meta-imx-fastboot/recipes-fsl/images/core-image-minimal.bbappend ~/imx-yocto-bsp/sources/meta-imx-fastboot/recipes-fsl/images/imx-image-full.bbappend       *** DISCLAIMER *** Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
記事全体を表示
This article describes how to use the Preempt-RT Linux kernel in the i.MX Linux BSP 6.6.23_2.0.0. This is particularly useful for platforms such as i.MX 95, for which there is not yet a Real-Time Edge Software release.    How to do it    1. Follow the steps in the i.MX Yocto Project User's Guide and build your preferred image, for example core-image-minimal. Will further assume that the BSP is in the ~/imx-yocto-bsp directory and the build directory is ~/imx-yocto-bsp/build. 2. Unpack the attached archive in ~/imx-yocto-bsp/sources. This should create the ~/imx-yocto-bsp/sources/meta-otherkernels directory. This archive will work out of the box for i.MX 95 and i.MX 93, and may require some modifications for other platforms, as described below. 3. Add the meta-otherkernels to your build using the following command: bitbake-layers add-layer ~/imx-yocto-bsp/sources/meta-otherkernels 4. Add the OVERRIDES .= ":preempt-rt" to ~/imx-yocto-bsp/build/conf/local.conf file using the following command: echo 'OVERRIDES .= ":preempt-rt"' >> ~/imx-yocto-bsp/build/conf/local.conf This enables the Preempt-RT kernel for your build. You can always go back to your regular kernel by removing this line from ~/imx-yocto-bsp/build/conf/local.conf. 5. Build again your image. After booting this image, you can check the kernel version using: uname -a      How it works    The meta-otherkernels layer contains a .bbappend  for the linux-imx kernel recipe which replaces the sources URL with the Real-Time Edge kernel when the "preempt-rt" override is active. In addition, due to the fact that the current real-time kernel does not support all the board configurations, the layer config file (meta-otherkernels/conf/layer.conf) removes from the build the device tree files that are not supported (when "preempt-rt" override is active).   If you use this layer for other SoCs (other than i.MX 93/i.MX 95), you may need to edit the meta-otherkernels/conf/layer.conf and add the unsupported device trees. If an  unsupported device tree is left, Yocto will give an error during build.        *** DISCLAIMER *** Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
記事全体を表示
This article describe i.MX8MP normal HAB security boot, and server/client mode. For server/client mode, it is based on customer requirement, because private is stored in server can't be accessed.
記事全体を表示
This knowledge base add imx8ulp swupdate support based on AN13872. Uboot patch: add_swupdate_support_for_imx8ulp_in_uboot.patch swupdate-scripts patch: 0001-add-imx8ulp-support-in-swupdate-scripts.patch Note You must generate new key referring  5.4.3.3 Generating a key before build. Commands 1. base image build command   ./assemble_base_image.sh -b imx8ulp -e emmc -d doublecopy -m   2. update image build command   ./swu_update_image_build.sh -e -s ./priv.pem -b imx8ulp -g   3. flash command:   uuu -b emmc_all .\imx-boot-imx8ulp-lpddr4-evk-sd.bin-flash_singleboot_m33 .\swu_doublecopy_rescue_imx8ulp_emmc_20240914.sdcard       Useful links: https://sbabic.github.io/swupdate/building-with-yocto.html#automatic-sha256-in-sw-description https://sbabic.github.io/swupdate/sw-description.html?highlight=hwrevision   
記事全体を表示