i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Compiling kernel module qca9377 in new bsp L5.10.9 has lots of errors.This is because lots of kernel apis has been dropped or changed from kernel5.4 to kernel5.10.But kernel module QCA9377 still using old api.So i fixed this compile errors and attach this patch.
View full article
    Below mentioned are the step to enable secure boot in imx8m nano board. Mentioned each step log and address for imx8m nano board tested with LPDDR4.   secure boot feature uses digital signatures to prevent unauthorized software execution during the device boot sequence. In case a malware takes control of the boot sequence, sensitive data, services and network can be impacted. Download the CST(code signing tool) from the below mentioned link https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true 1. Generating a PKI tree The Code Signing Tools package contains an OpenSSL based key generation script under keys/ directory. The hab4_pki_tree.sh script is able to generate a PKI tree containing up to 4 Super Root Keys (SRK) as well as their subordinated IMG and CSF keys. $ ./hab4_pki_tree.sh ... Do you want to use an existing CA key (y/n)?: n Do you want to use Elliptic Curve Cryptography (y/n)?: n Enter key length in bits for PKI tree: 2048 Enter PKI tree duration (years): 5 How many Super Root Keys should be generated? 4 Do you want the SRK certificates to have the CA flag set? (y/n)?: y 2. Generating a SRK Table and SRK Hash The next step is to generated the SRK Table and its respective SRK Table Hash from the SRK public key certificates created in one of the steps above. The srktool can be used for generating the SRK Table and its respective SRK Table Hash. - Generating SRK Table and SRK Hash in Linux 64-bit machines: $ ../linux64/bin/srktool -h 4 -t SRK_1_2_3_4_table.bin -e \ SRK_1_2_3_4_fuse.bin -d sha256 -c \ SRK1_sha256_2048_65537_v3_ca_crt.pem,\ SRK2_sha256_2048_65537_v3_ca_crt.pem,\ SRK3_sha256_2048_65537_v3_ca_crt.pem,\ SRK4_sha256_2048_65537_v3_ca_crt.pem The SRK_1_2_3_4_table.bin and SRK_1_2_3_4_fuse.bin files can be used in further steps as explained in HAB guides available under doc/imx/habv4/guides/ directory. 3. step-by-step procedure on how to sign and securely boot a bootloader image on i.MX8M Nano devices 3.1 Enabling the secure boot support in U-Boot clone the u-boot from the git link https://source.codeaurora.org/external/imx/uboot-imx Enable the secure boot support in u-boot - Defconfig: CONFIG_SECURE_BOOT=y CONFIG_IMX_HAB=y from 2020.04 u-boot Build images $ make imx8mn_evk_defconfig $ make Output images $(UBOOT_SRC)/u-boot-nodtb.bin $(UBOOT_SRC)/spl/u-boot-spl.bin $(UBOOT_SRC)/arch/arm/dts/fsl-imx8mm-evk.dtb‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 3.2 ARM Trusted Firmware Get the ATF from the below mentioned source link https://source.codeaurora.org/external/imx/imx-atf Build images $ make PLAT=imx8mn bl31 Output images $(ATF_SRC)/build/imx8mn/release/bl31.bin‍‍‍‍‍‍‍‍‍‍‍‍ 3.3 Get DDR FW images $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.0.bin $ chmod 777 firmware-imx-8.0.bin $ ./firmware-imx-8.0.bin Accept the LICENSE AGREEMENT $ cd firmware-imx-8.0.bin‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍/firmware/ddr/synopsys‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Output images $(DDRFW_SRC)/lpddr4_* 3.4 Get IMX-MKIMAGE source https://source.codeaurora.org/external/imx/imx-mkimage Below mentioned are the steps to generate bootloder using mkimage Gather necessary images SPL and U-boot images - u-boot-nodtb.bin - u-boot-spl.bin - fsl-imx8mm-evk.dtb‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ ATF image - bl31.bin DDR firmware images - lpddr4_pmu_train_1d_dmem.bin - lpddr4_pmu_train_1d_imem.bin - lpddr4_pmu_train_2d_dmem.bin - lpddr4_pmu_train_2d_imem.bin Copy these files to imx-mkimage/iMX8M directory 3.5 Build i.MX8MN boot image flash.bin $ make SOC=iMX8MN flash_evk ========= OFFSET dump ========= Loader IMAGE: header_image_off 0x0 dcd_off 0x0 image_off 0x40 csf_off 0x24a00 spl hab block: 0x911fc0 0x0 0x24a00 Second Loader IMAGE: sld_header_off 0x58000 sld_csf_off 0x59020 sld hab block: 0x401fcdc0 0x58000 0x1020 $ make SOC=iMX8MN print_fit_hab ./print_fit_hab.sh 0x60000 evk.dtb 0x40200000 0x5B000 0xC3AB0 0x402C3AB0 0x11EAB0 0x78F0 0x960000 0x1263A0 0xA1B0 0xBE000000 0x130550 0x10 3.6 Creating the CSF description file The build log provided by imx-mkimage can be used to define the "Authenticate Data" parameter in CSF. - SPL "Authenticate Data" addresses in flash.bin build log: spl hab block: 0x911fc0 0x0 0x24a00 - "Authenticate Data" command in csf_spl.txt file: Blocks = 0x911fc0 0x0 0x24a00 "flash.bin" - FIT image "Authenticate Data" addresses in flash.bin build log: sld hab block: 0x401fcdc0 0x57c00 0x1020 - FIT image "Authenticate Data" addresses in print_fit_hab build log: 0x40200000 0x5B000 0xC3AB0 0x402C3AB0 0x11EAB0 0x78F0 0x960000 0x1263A0 0xA1B0 0xBE000000 0x130550 0x10 - "Authenticate Data" command in csf_fit.txt file: Blocks = 0x401fcdc0 0x57c00 0x1020 "flash.bin", \ 0x40200000 0x5B000 0xC3AB0 "flash.bin", \ 0x402C3AB0 0x11EAB0 0x78F0 "flash.bin", \ 0x960000 0x1263A0 0xA1B0 "flash.bin", \ 0xBE000000 0x130550 0x10 "flash.bin"   3.7 Avoiding Kernel crash in closed devices - Add Unlock MID command in csf_spl.txt: [Unlock] Engine = CAAM Features = MID 3.8 Signing the flash.bin binary The CST tool is used for singing the flash.bin image and generating the CSF binary. Users should input the CSF description file created in the step above and receive a CSF binary, which contains the CSF commands, SRK table, signatures and certificates. - Create SPL CSF binary file: $ ./cst -i csf_spl.txt -o csf_spl.bin - Create FIT CSF binary file: $ ./cst -i csf_fit.txt -o csf_fit.bin 3.8 Assembling the CSF in flash.bin binary ------------------------------------------- The CSF binaries generated in the step above have to be inserted into the flash.bin image. The CSF offsets can be obtained from the flash.bin build log: - SPL CSF offset: csf_off 0x24a00 - FIT CSF offset: sld_csf_off 0x59020 The signed flash.bin image can be then assembled: - Create a flash.bin copy: $ cp flash.bin signed_flash.bin - Insert csf_spl.bin in signed_flash.bin at 0x24a00 offset: $ dd if=csf_spl.bin of=signed_flash.bin seek=$((0x24a00)) bs=1 conv=notrunc - Insert csf_fit.bin in signed_flash.bin at 0x59020 offset: $ dd if=csf_fit.bin of=signed_flash.bin seek=$((0x59020)) bs=1 conv=notrunc - Flash signed flash.bin image: $ sudo dd if=signed_flash.bin of=/dev/sd<x> bs=1K seek=33 && sync 3.9 Verifying HAB events ------------------------ The next step is to verify that the signatures included in flash.bin image is successfully processed without errors. HAB generates events when processing the commands if it encounters issues. Prior to closing the device users should ensure no HAB events were found, as the example below: - Verify HAB events: => hab_status Secure boot disabled HAB Configuration: 0xf0, HAB State: 0x66 3.10 Programming SRK Hash ------------------------- The U-Boot fuse tool can be used for programming eFuses on i.MX SoCs. - Dump SRK Hash fuses values in host machine: $ hexdump -e '/4 "0x"' -e '/4 "%X""\n"' SRK_1_2_3_4_fuse.bin 0x20593752 0x6ACE6962 0x26E0D06C 0xFC600661 0x1240E88F 0x1209F144 0x831C8117 0x1190FD4D - Program SRK_HASH[255:0] fuses on i.MX8MN devices: => fuse prog 6 0 0x20593752 => fuse prog 6 1 0x6ACE6962 => fuse prog 6 2 0x26E0D06C => fuse prog 6 3 0xFC600661 => fuse prog 7 0 0x1240E88F => fuse prog 7 1 0x1209F144 => fuse prog 7 2 0x831C8117 => fuse prog 7 3 0x1190FD4D 3.10 Completely secure the device ---------------------------------- Additional fuses can be programmed for completely secure the device, more details about these fuses and their possible impact can be found at AN4581[1]. - Program SRK_LOCK: => fuse prog 0 0 0x200 - Program DIR_BT_DIS: => fuse prog 1 3 0x8000000 - Program SJC_DISABLE: => fuse prog 1 3 0x200000 - JTAG_SMODE: => fuse prog 1 3 0xC00000
View full article
This document shows how to build genivi step by step, but I haven’t tested the images yet, before building the images, pls refer to the host setup and host packages according to the yocto project user’s guide, I don’t mention here again, this is for imx8mq as example, you can choose the different board name to build   Before building the genivi package, customer also can refer to the kernel and image name from: https://github.com/GENIVI/meta-ivi/tree/master   4.9.88 IMAGE   1. Create a bin folder in the home directory $ mkdir ~/bin (this step may not be needed if the bin folder already exists) $ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo    2. Add the following line to the .bashrc file to ensure that the ~/bin folder is in your PATH variable. export PATH=~/bin:$PATH    3. Yocto Project Setup $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_genivi.xml $ repo sync   4.update Weston 3.0.0 to Weston 4.0.0 $ git clone https://git.yoctoproject.org/git/meta-freescale -b warrior   then replace the wayland directory in "imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland" with the "meta-freescale/recipes-graphics/wayland" in cloned directory.   5.image build DISTRO=nxp-imx-genivi-wayland MACHINE=imx8mqevk source ./nxp-setup-genivi.sh -b genivi-wayland   $bitbake  pulsar-image    6.Error fix if you don’t update Weston, you should get the error message like The error shows required Weston >=4.0.0, but current bsp includes Weston version is 3.0.0, so you need to update the Weston to the 4.0.0 step by step $ git clone https://git.yoctoproject.org/git/meta-freescale -b warrior $ rm -rf ../sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland $ cp -r meta-freescale/recipes-graphics/wayland ../sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/   $ bitbake -c cleansstate wayland-ivi-extension $ bitbake  wayland-ivi-extension $ bitbake  pulsar-image   4.14.95 IMAGE   1. Create a bin folder in the home directory $ mkdir ~/bin (this step may not be needed if the bin folder already exists) $ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo   2. Add the following line to the .bashrc file to ensure that the ~/bin folder is in your PATH variable. export PATH=~/bin:$PATH   3.Yocto Project Setup $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-warrior -m imx-4.19.35-1.1.0_genivi.xml $ repo sync   4. change Weston 6.0.1 to Weston 5.0.0 $ git clone https://git.yoctoproject.org/git/meta-freescale -b zeus   then replace the wayland directory in "imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland" with the "meta-freescale/recipes-graphics/wayland" in cloned directory.   5.image build $ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland   $ bitbake  meta-ivi-image    6.Error fix if you don’t change Weston, you should get the error message like so try to change the Weston to the 5.0.0 step by step $ git clone https://git.yoctoproject.org/git/meta-freescale -b zeus $ rm -rf ../sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland $ cp -r meta-freescale/recipes-graphics/wayland ../sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics   $ bitbake -c cleansstate weston $ bitbake  weston $ bitbake  meta-ivi-image     5.4.24 IMAGE   1. Create a bin folder in the home directory $ mkdir ~/bin (this step may not be needed if the bin folder already exists) $ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo   2. Add the following line to the .bashrc file to ensure that the ~/bin folder is in your PATH variable. export PATH=~/bin:$PATH   3.Yocto Project Setup $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.24-2.1.0_genivi.xml $ repo sync   4. image build $ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b build-wayland   $ bitbake  meta-ivi-image    
View full article
In this doc will show how to use i.MX8QXP DPU do image warp.   SW: i.MX Linux BSP L5.4.24_2.1.0 bsp release and patch in this doc HW: i.MX8QXP MEK board, ov5640 camera, HDMI display   Introduction Image Warping is the process of digitally manipulating image data such that the image’s projection precisely matches a specific projection surface or shape.   i.MX8QXP DPU controller could do image warp work by its blit engine and display engine. I choose to enable blit engine’s fetchwarp9 unit to do warp work. Check i.MX8QXP RM, Blit Engine support Image Warp as: “Performs a re-sampling of the source image with any pattern. The sample point positions are read from a compressed coordinate buffer.” So you need prepare two input buffers, one buffer store original image data, the other buffer store resample point coordinate, DPU blit engine will read that two buffer by fetchwarp9 unit, then output result image buffer which contain warped image data. Note i.MX8QXP DPU blit engine fetchwarp9 unit, for the input original image buffer, support RGB and YUV 4:4:4 format. The resample point coordinate buffer contents is depend on what kind warp transformation in your use case; and for each resample point coordinate format check i.MX8QXP RM fecthwarp unit description as below. In this doc, using the 2xs12.4 format, each point x coordinate use (12+4) bit, same as y coordinate.   For DPU fetchwarp9 unit, to enable it work for image warp, check i.MX8QXP RM:   2.Patch notes and test code imx8-dpu-warp-kernel.diff contain the kernel side change for drm ioctl api permission and add vmap function of ion dma_buf_ops. libg2d.so contain the binary for adding warp feature. g2d.h is header file which add define for G2D_WARP and G2D_YUV4. imx8-ov5640-dpu-warp-render.c is a sample code which show how to call g2d lib to image warp, need open the G2D_WARP flag. And this code contain some example calculate the coordinate buffer of rotate, swirl, barrel distortion, affine transformation, perspective transformation, wave transformation. And this code will show read camera input frame then add warp process , then render warp image frame to display.   The test cmd usage as below, read 1080P frame from ov5640 camera, do warp then render warp image to drm plane. Note as dpu fetchwarp9 unit support YUV 4:4:4 input image frame, so below cmd need set parameter YUV4, which will ask ISI driver output YUV 4:4:4 image frame. imx8-ov5640-dpu-warp-render  -i /dev/video0 -f YUV4  -S 1920,1080  -M imx-drm -p 91:38 -F XB24  -b 6  -e g2d  -t 5         -i <video-node> set video node (default: /dev/video0)         -f <fourcc>     set input format using 4cc         -S <width,height>       set input resolution         -s <width,height>@<left,top>    set crop area         -M <drm-module> set DRM module         -o <connector_id>:<crtc_id>:<mode>      set a mode         -p <connector_id>:<crtc_id>     output to a plane         -F <fourcc>     set output format using 4cc         -t <warptype>   set 0 neutual 1 rotate 2 swirl 3 divisionmodel 4 affine 5 perpsptive 6 wave         -b buffer_count set number of buffers        3.Example original image:                     Reference: https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM https://www.nxp.com/webapp/Download?colCode=L5.4.24_2.1.0_MX8QXPC0&appType=license https://en.wikipedia.org/wiki/Image_geometry_correction https://lists.freedesktop.org/archives/dri-devel/2012-March/019778.html https://store.kde.org/p/1246558 https://github.com/ImageMagick/ImageMagick        
View full article
This is a detailed programming aid for the registers associated with i.MX 8MMini (m845S) DDR initialization.  For more details, refer to the main mScale DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467 Please note that this page is only intended to store the RPA spreadsheets. For questions, please create a new community thread.
View full article
This is a detailed programming aid for the registers associated with i.MX 8M (m850D) DDR initialization.  For more details, refer to the main mScale DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467 Please note that this page is only intended to store the RPA spreadsheets. For questions, please create a new community thread.
View full article
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519   To reduce the number of attachments, older RPAs may be found in the attached zip file. Note: Devices with 17-row addresses (R0-R16) are not supported by this SoC.  ***IMPORTANT: For SCFWv1.7.0 and later, you must use the following RPA versions or later: MX8QXP_C0_B0_LPDDR4_RPA_1.2GHz_v16 MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16 MX8QuadXPlus_DualXPlus_C0_B0_DDR3L_RPA_v22 MX8DualX_C0_B0_DDR3L_RPA_v20 Older versions of the RPA are not aligned to SCFWv1.7.0 and later.  If trying to use an older version of an RPA with SCFWv1.7.0, it will cause the SCFW not to boot.  The offending lines in the DCD output are as follows: For MX8QXP/DualX: DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ If the user wishes to use an older RPA with SCFW 1.7.0 and later (not recommended), then the above lines must be removed from older RPA DCD file outputs.  In addition, wrapping these lines are "#ifndef SCFW_DCD", "#else", and "#endif" preprocessor commands.  These should be removed as well.  For example of MX8QXP: [remove] #ifndef SCFW_DCD [remove] -/* For 1200MHz DDR, DRC 600MHz operation */ [remove] DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ [remove] #else <keep code as is> [remove] #endif
View full article
To enable USB 2.0 port on BB for USB OTG, you need to apply below two changes: device/fsl.git   diff --git a/imx8q/mek_8q/init.usb.rc b/imx8q/mek_8q/init.usb.rc index af4e388..0f3ab0b 100644 --- a/imx8q/mek_8q/init.usb.rc +++ b/imx8q/mek_8q/init.usb.rc @@ -44,7 +44,7 @@ on early-boot      mount functionfs mtp /dev/usb-ffs/mtp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      mount functionfs ptp /dev/usb-ffs/ptp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      setprop sys.usb.mtp.device_type 3 -    setprop vendor.usb.config "5b110000.usb3" +    setprop vendor.usb.config "ci_hdrc.0"      write /sys/module/libcomposite/parameters/disable_l1_for_hs "y"      symlink /config/usb_gadget/g1/configs/b.1 /config/usb_gadget/g1/os_desc/b.1   vendor/nxp-opensource/kernel_imx.git           revert below patch:           commit 2f9586c120971312e61df464264993899cf34536           Author: yang.tian <yang.tian@nxp.com>           Date:   Tue Jan 7 13:30:02 2020 +0800       MA-15242 Set usb2.0 port as usb host only for mek_8q  
View full article
The Guide is how to use Ubuntu filesystem with i.MX8 series platform.At present, I had try it on i.MX8QXP with 4.14.98 kernel with ubuntu16.04. The Document will be continuously updated with enable VPU, ubuntu18.04. The desktop we can chose Gnome or weston.  Because driver  support issue, gc7000 series gpu not support render Gnome destop but it can render weston destop.  Update 2019/7/31: Ubuntu-i.MX8-weston.pdf   Feature: weston + ubuntu18.04 + 4.14.98 kernel VPU (enable with gplay or gst-play)  GPU (could render desktop and run GPU demo under root privileges on Weston Desktop) I also try ubuntu with gnome desktop, ubuntu18.04 can not run gnome, need use ubuntu19.04. But Gnome Desktop just render by CPU.  ------------------------------------------------------------------------------------- Update 2020/3/6: Ubuntu-i.MX8M.pdf Just a simple guide for IMX8M series, will be  continuously updated. 
View full article
Multicore programming guide with Linux 3.14.52_1.1.0 and FreeRTOS BSP for i.MX 6SoloX
View full article
  Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 family developement board https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false  
View full article
Following docs(English or Chinese version) are also can be referred as a hand on guide. Freescale i.MX6 DRAM Port Application Guide-DDR3 飞思卡尔i.MX6平台DRAM接口高阶应用指导-DDR3篇   Please find i.Mx6DQSDL LPDDR2 Script Aid through below link. i.Mx6DQSDL LPDDR2 Script Aid  Please find i.Mx6DQSDL DDR3 Script Aid through below link. i.MX6DQSDL DDR3 Script Aid  Please find i.MX6SX DDR3 Script Aid through below link. i.MX6SX DDR3 Script Aid  Please find i.MX6SL LPDDR2 Script Aid through below link.. i.MX6SL LPDDR2 Script Aid  Please find i.MX6UL DDR3 Script Aid through below link. I.MX6UL DDR3 Script Aid  Please find i.MX6UL LPDDR2 Script Aid through below link. i.MX6UL_LPDDR2_Script_Aid  Please find i.MX6ULL LPDDR2 Script Aid through below link. i.MX6ULL_LPDDR2_Script_Aid 
View full article
To disable the Android dm-verity in the new devices you should have the below. A Window/Linux computer The Android SDK platform-packages tools. Download the Android Packages tool. To use the Android kernel or give root access to your Android device, it is needed to have some tools from the Android SDK like ADB or fastboot. To download those tools just go to below web-page: https://developer.android.com/studio#downloads Go to the “command line tools only” part and download the sdk-tools-windows-4333796.zip package. Note: Is recommended to store the content of the zip file in path that you could find without any problem since the Android SDK tools can only be run by the terminal console.   Unlock your Android device. On the Android GUI go to Settings -> systems -> About Phone At the bottom, you should see the build number of your Android device. Tap it multiple times until appears on the screen that you are a developer now. Go to the developer options and search for the OEM unlock option. You need to activate that option. Open the power-shell terminal and go to the path where you stored the zip file.   Example for Windows: cd C:\users\diego\Documents\platform-tools‍ Then you will use the ADB tool (Adroid Debug Bridge). To use it you need to run adb.exe in your power-shell terminal. To run an executable in the Windows terminal is just with ".\". Connect the serial download cable to the host computer (the Type C for the i.MX8M and i.MX8MM. The OTG for the i.M6 SabreSD boards). Open the adb server. .\adb.exe start-server‍ See your connected devices. .\adb.exe devices‍ You should see your device and the serial number that is assigned to the device. Then, enter into Bootloader mode. .\adb.exe reboot bootloader‍       Note to see if your board successfully entered to Bootloader mode. In your serial terminal, you should see that you are in Bootloader mode. Once inside the Bootloader mode, using fastboot you can unlock your phone. First, see if your computer recognizes your board once inside the Bootloader mode. .\fastboot.exe devices‍ If you do not see any device, go to Appendix A of the document. Finally, Unlock and reboot the board. .\fastboot.exe oem-unlock .\fastboot.exe reboot‍‍         Unlock the dm-verity option. After the board rebooted. Start again the adb server .\adb.exe start-server .\adb.exe devices‍‍ Then root the board .\adb.exe root ‍ After rooting the board, disable the dm-verity option .\adb.exe disable-verity‍ After disabling the verity option, it will request you to reboot your board. Just reboot your board. .\adb.exe reboot ‍ With that, you should have successfully disabled the verity option on your board.   Appendix A Update the USB driver (For Windows only) If your computer does not recognize once you are inside the bootloader mode. What you need to do is update the USB driver. To update the driver, follow the below steps. First, open your device manager and locate the Universal Serial Bus devices -> USB download gadget. Then press the right-click and select the Update driver option. Select the “Browse my computer for driver software” option. Select the “Let me pick from a list of available drivers on my computer” option.     Select the ADB Device Model.   And accept to install the driver. After that, your computer should recognize the board being into Bootloader mode.   Appendix B connects your Android device to a Linux computer through ADB.   You could face some adb problems if you want to connect your Android device to a Linux computer. If you want to use adb, the Android image does not allow you due to a permission problem. To make it work, you need to create a new rule for a plug device. To make the new rule, create a document inside the /etc/udev/rules.d named 51-android.rules. Inside the document write the following:   SUBSYSTEM=="usb", ATTR{idVendor}=="18d1", ATTR{idProduct}=="d002", MODE="0660",  GROUP="plugdev", SYMLINK+="android%n"‍‍   Where the ATTR{idVendor} and ATTR{idProduct} is the USB id for the board. To know that information. Write lsusb and your Android device is the one named Google Inc. Then reboot your computer. With this new rule, ADB should work as usual. Hope this document could be useful to someone. Best regards, Diego.
View full article
adv7180 is the 8 bits parallel CSI interface TVin to iMX8QXP validation board. Its weaving mode de-interlace can be supported on both iMX8QXP B0 and C0 chips, but blending mode de-interlace can only work on iMX8QXP C0 chips.   ISL79987 is the 4 virtual channel TVin chip which can input 4 CVBS cameras to iMX8QXP with MIPI CSI2 inteface, it can only work with iMX8QXP C0 chips. The iMX8QXP B0 chips have MIPI CSI2 virtual channel errata.   To test the capture to file: $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -num 300 -fmt YUYV -of   To test the preview on screen: $ killall weston $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -fmt RGBP -num 30000   Note: 1. For weaving mode de-interlace, when the ISI is doing de-interlace, it can't do CSC at the same time, so preview will get color issue, because the real output video is always YUYV format. 2. For blending mode de-interlace, it must use ISI0, so for ISL79987, only one camera can use blending mode, the other three cameras are still using weaving mode. The preview color is OK for such use case. 3. The patch is for L4.19.35 BSP.     2019-11-14 update: Add the test application "mx8_v4l2_cap_drm.tar.gz" to support YUYV render to display. Test command to render 4 weaving mode cameras:    ./mx8_v4l2_cap_drm.out -cam 0xF -fmt YUYV -num 30000     2020-04-29 update: Add "0006-isl7998x-fix-the-mipi_bps-overwrite-issue-from-set_f.patch", it fixed the issue that MIPI bps information in isl7998x_data->format.reserved[0] had been overwritten by isl7998x_set_fmt().   2021-06-11 update: Added the patches based on L5.4.70_2.3.0 GA BSP.
View full article
In order to improve the speed of compilation, VMWare Player 14.0 is installed on local hard disk, and Ubuntu 18.04 LTS is installed on a SSD with at least 500GB size and USB3.1 specification. When installing ubuntu 18.04 LTS to SSD, it should be allocated at least 350GB of disk space, because compiling this version of android requires a larger disk space. The following are detailed compilation steps: Part l Configuring Ubuntu 18.04 LTS 1. Installing Ubuntu 18.04 on VMplayer 14.0 After installation is done, root user should be set at first. # sudo passwd root Then follow these steps to configuration ubuntu 18.04 for environment of compiliation --Changing sources of ubuntu 18.04 mirror If you are Chinese users, you can do the step, which can improve your system performance. # sudo cp /etc/apt/sources.list /etc/apt/sources.list.bak # sudo geit /etc/apt/source.list Comment I.MX customers outside China do not need to modify Ubuntu source list, or can modify it to local mirror site of Ubuntu 18.04, which can improve the speed of software upgrade.    Delet all sources and copy following lines here, Then save it and exit Changing ubuntu source deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse    Then running these 2 commands to update sources and packages    # sudo apt-get update    # sudo apt-get upgrade 2. Installing packages for compiliation Packages for compiliation # sudo apt-get install flex bison gperf build-essential zlib1g-dev lib32ncurses5-dev x11proto-core-dev libx11-dev lib32z1-dev libgl1-mesa-dev tofrodos python-markdown libxml2-utils xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 gcc-multilib g++-multilib subversion openssh-server openssh-client uuid uuid-dev zlib1g-dev liblz-dev lzop liblzo2-2 liblzo2-dev git-core curl # sudo apt-get install u-boot-tools mtd-utils android-tools-fsutils openjdk-8-jdk device-tree-compiler aptitude libcurl4-openssl-dev nss-updatedb # sudo apt-get install chrpath texinfo gawk cpio diffstat gdisk m4 libz-dev libssl-dev Part 2 Compiling Android Q10.0.0_2.1.0 BSP 1. Downloading NXP source code for Android Q10.0.0_2.1.0    File name is imx-android-10.0.0_2.1.0.tar.gz.    Copy the file to ~/, and decompress it.    # cd ~/    # tar zxvf ./imx-android-10.0.0_2.1.0.tar.gz    Then “imx-android-10.0.0_2.1.0” directory is created at ~/, now run the command to download android source code. # source ./imx-android-10.0.0_2.1.0/imx_android_setup.sh Comment imx_android_setup.sh is a script file, which includes all steps needed by the environment of android Q10.0.0_2.1.0 BSP. If network environment is enough good, several hours later, it will be done. 2. Compiling Android Q10.0.0_2.1.0 Referring to steps in Android_User's_Guide.pdf, We summaries steps for compilation here: (1) Preparing cross-compile tool chain    In Android_User's_Guide.pdf, 2 kinds of tool chain are recommended for users. --- gcc-arm-8.3-2019.03-x86_64-aarch64-elf.tar.xz --- gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz    Users can select one of them, and then decompress it to /opt/ directory. On how to download them or more details, see Android_User's_Guide.pdf, page 3. Here we will use gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz as tool chain. (2) Beginning to Compile Android Q10.0.0_2.1.0 BSP    Since this version of Android BSP requires high memory capacity when compiling, if the memory configuration of the virtual machine is incorrect, it is very likely to cause the compilation to fail. The following is a list of variable tests for user reference: # cd android_build # export AARCH64_GCC_CROSS_COMPILE=/opt/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/aarch64-linux-gnu- # source build/envsetup.sh # lunch evk_8mp-userdebug # ./imx-make.sh -j2 2>&1 | tee build-log.txt Part 3 Errors During Compilation 1. Allocating 8GB Memory For VMware Player # ./imx-make.sh -j1 2>&1 | tee build-log.txt 2. Allocating 12GB Memory For VMware Player # ./imx-make.sh -j4 2>&1 | tee build-log.txt # ./imx-make.sh -j4 2>&1 | tee build-log.txt (Run it again) # ./imx-make.sh -j4 2>&1 | tee build-log.txt (Run it again)       So if we use 4 thread to compile BSP, command for compilation will have to be run for 3 times. NXP TIC Team Weidong Sun 2020/4/30
View full article
Platform: i.MX8QXP/8QM OS: Linux Supported Camera Modules: Max9286 + Max9271 + OV10635, Default BSP Max9286 + Max96705 + AR0144, patch Max9286 + Max96705 + OV9284, patch Max9286 + Max96705 + AP0101 + AR0132, patch NVP6324 + NVP2431 + IMX225, patch TP2855 + TP3812 + IMX307, patch ISL7998x + NTSC/PAL Sensor, patch adv7180 + NTSC/PAL Sensor, patch Detailed description in the attachment.
View full article
    Xenomai is real-time framework, which can run seamlessly side-by-side Linux as a co-kernel system, or natively over mainline Linux kernels (with or without PREEMPT-RT patch). The dual kernel nicknamed Cobalt, is a significant rework of the Xenomai 2.x system. Cobalt implements the RTDM specification for interfacing with real-time device drivers. The native linux version, an enhanced implementation of the experimental Xenomai/SOLO work, is called Mercury. In this environment, only a standalone implementation of the RTDM specification in a kernel module is required, for interfacing the RTDM-compliant device drivers with the native kernel. You can get more detailed information from Home · Wiki · xenomai / xenomai · GitLab       I have ported xenomai 3.1 to i.MX Yocto 4.19.35-1.1.0, and currently support ARM64 and test on i.MX8MQ EVK board. I did over night test( 5 real-time threads + GPU SDK test case) and stress test by tool stress-ng on i.MX8MQ EVK board. It looks lile pretty good. Current version (20200730) also support i.MX8MM EVK.     You need git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-4.19.35-1.1.0-20200818 (which inlcudes all patches and bb file) and add the following variable in conf/local.conf before build xenomai by command bitbake xenomai.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. The following is test result by the command (/usr/xenomai/demo/cyclictest -p 99 -t 5 -m -n -i 1000  -l 100000😞 //Over normal Linux kernel without GPU SDK test case T: 0 ( 4220) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 9 Max: 23 T: 1 ( 4221) P:99 I:1500 C: 66672 Min: 7 Act: 10 Avg: 10 Max: 20 T: 2 ( 4222) P:99 I:2000 C: 50001 Min: 7 Act: 12 Avg: 10 Max: 81 T: 3 ( 4223) P:99 I:2500 C: 39998 Min: 7 Act: 11 Avg: 10 Max: 29 T: 4 ( 4224) P:99 I:3000 C: 33330 Min: 7 Act: 13 Avg: 10 Max: 26 //Over normal Linux kernel with GPU SDK test case T: 0 ( 4177) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 11 Max: 51 T: 1 ( 4178) P:99 I:1500 C: 66673 Min: 7 Act: 12 Avg: 10 Max: 35 T: 2 ( 4179) P:99 I:2000 C: 50002 Min: 7 Act: 12 Avg: 11 Max: 38 T: 3 ( 4180) P:99 I:2500 C: 39999 Min: 7 Act: 12 Avg: 11 Max: 42 T: 4 ( 4181) P:99 I:3000 C: 33330 Min: 7 Act: 12 Avg: 11 Max: 36   //Cobalt with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M --timeout 600s --metrics-brief T: 0 ( 4259) P:50 I:1000 C:3508590 Min:      0 Act:    0 Avg:    0 Max:      42 T: 1 ( 4260) P:50 I:1500 C:2338831 Min:      0 Act:    1 Avg:    0 Max:      36 T: 2 ( 4261) P:50 I:2000 C:1754123 Min:      0 Act:    1 Avg:    1 Max:      42 T: 3 ( 4262) P:50 I:2500 C:1403298 Min:      0 Act:    1 Avg:    1 Max:      45 T: 4 ( 4263) P:50 I:3000 C:1169415 Min:      0 Act:    1 Avg:    1 Max:      22   //Cobalt without GPU SDK test case T: 0 ( 4230) P:50 I:1000 C: 100000 Min: 0 Act: 0 Avg: 0 Max: 4 T: 1 ( 4231) P:50 I:1500 C:   66676 Min: 0 Act: 1 Avg: 0 Max: 4 T: 2 ( 4232) P:50 I:2000 C:   50007 Min: 0 Act: 1 Avg: 0 Max: 8 T: 3 ( 4233) P:50 I:2500 C:   40005 Min: 0 Act: 1 Avg: 0 Max: 3 T: 4 ( 4234) P:50 I:3000 C:   33338 Min: 0 Act: 1 Avg: 0 Max: 5 //Cobalt with GPU SDK test case T: 0 ( 4184) P:99 I:1000 C:37722968 Min: 0 Act: 1 Avg: 0 Max: 24 T: 1 ( 4185) P:99 I:1500 C:25148645 Min: 0 Act: 1 Avg: 0 Max: 33 T: 2 ( 4186) P:99 I:2000 C:18861483 Min: 0 Act: 1 Avg: 0 Max: 22 T: 3 ( 4187) P:99 I:2500 C:15089187 Min: 0 Act: 1 Avg: 0 Max: 23 T: 4 ( 4188) P:99 I:3000 C:12574322 Min: 0 Act: 1 Avg: 0 Max: 29 //Mercury without GPU SDK test case T: 0 ( 4287) P:99 I:1000 C:1000000 Min: 6 Act: 7 Avg: 7 Max: 20 T: 1 ( 4288) P:99 I:1500 C:  666667 Min: 6 Act: 9 Avg: 7 Max: 17 T: 2 ( 4289) P:99 I:2000 C:  499994 Min: 6 Act: 8 Avg: 7 Max: 24 T: 3 ( 4290) P:99 I:2500 C:  399991 Min: 6 Act: 9 Avg: 7 Max: 19 T: 4 ( 4291) P:99 I:3000 C:  333322 Min: 6 Act: 8 Avg: 7 Max: 21 //Mercury with GPU SDK test case T: 0 ( 4222) P:99 I:1000 C:1236790 Min: 6 Act: 7 Avg: 7 Max: 55 T: 1 ( 4223) P:99 I:1500 C:  824518 Min: 6 Act: 7 Avg: 7 Max: 44 T: 2 ( 4224) P:99 I:2000 C:  618382 Min: 6 Act: 8 Avg: 8 Max: 88 T: 3 ( 4225) P:99 I:2500 C:  494701 Min: 6 Act: 7 Avg: 8 Max: 49 T: 4 ( 4226) P:99 I:3000 C:  412247 Min: 6 Act: 7 Avg: 8 Max: 53 //////////////////////////////////////// Update for Yocto L5.4.47 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.47 2.2.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP). You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git,  and git checkout xenomai-5.4.47-2.2.0. You need to add the following variable in conf/local.conf before build xenomai by command bitbake imx-image-multimedia.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.4.70 2.3.0  /////////////////////////////////////////////////////////// New release  for Yocto release L5.4.70 2.3.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP) and i.MX8QM/QXP. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.0. Updating: 1, Support i.MX8QM and i.MX8QXP 2, Fix altency's the issue which uses legacy API to get time   //////////////////////////////////////// update for Yocto L5.4.70 2.3.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-5.4.70-2.3.2. Updating: 1, Enable Xenomai RTDM driver in Linux Kernel 2, Currently CAN, UART, GPIO,  SPI and Ethernet (in debug for RTNet)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf to enable relative device in Xenomai domain, for example rt-imx8mp-flexcan.   //////////////////////////////////////// Update for Yocto L5.4.70 2.3.4  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.4. You need to git clone  https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.4. Updating: 1, Enable RTNet FEC driver 2, Currently CAN, UART, GPIO,  SPI and Ethernet ( FEC Controller)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf and KERNEL_DEVICETREE += " freescale/imx8mm-rt-ddr4-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mmddr4evk.conf to enable rt_fec device in Xenomai domain. Verifying the network connection by RTnet Ping Between i.MX8M Mini EVK and i.MX8M Plus EVK a, Setup test environment 1, Connect ENET1 of  i.MX8M Plus EVK (used as a master) and  ENET of i.MX8M Mini EVK (used as a slave) of  to a switch or hub 2, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Plus EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.101" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -65,7 +65,7 @@ TDMA_MODE="master" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 3, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Mini EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.102" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -59,13 +59,13 @@ STAGE_2_CMDS="" # TDMA mode of the station ("master" or "slave") # Start backup masters in slave mode, it will then be switched to master # mode automatically during startup. -TDMA_MODE="master" +TDMA_MODE="slave" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 4, rename imx8mm-rt-ddr4-evk.dtb to imx8mm-ddr4-evk.dtb in /run/media/mmcblk1p1,  rename imx8mp-rt-evk.dtb to imx8mp-evk.dtb in /run/media/mmcblk1p1, and reboot board. 5, Run the below command on i.MX8M Mini EVK board. cd /usr/xenomai/sbin/ ./rtnet start & 5, Run the below command on i.MX8M Plus EVK board. cd /usr/xenomai/sbin/ ./rtnet start & When you see the log (rt_fec_main 30be0000.ethernet (unnamed net_device) (uninitialized): Link is Up - 100Mbps/Full - flow control rx/tx) and you can run command "./rtroute" to check route table if the slave IP (192.168.100.102) is in route.. b, Verify the network connection using the command below: ./rtping -s 1024 192.168.100.102 //////////////////////////////////////// Update for Yocto L5.10.52 2.1.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.52 2.1.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.52-2.1.0. Updating: 1, Upgrade Xenomai to v3.2 2, Enable Dovetail instead of ipipe. Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch.  Latency testing of Xenomai3.2+Dovetail with isolating CPU 2,3 ( Xenomai 3.2 on 8MM DDR4 EVK with GPU test case (GLES2/S08_EnvironmentMappingRefraction_Wayland) + iperf3 + 2 ping 65000 size + stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief )😞 The following is test result by the command (/usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000) root@imx8mmddr4evk:~# /usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000 # /dev/cpu_dma_latency set to 0us policy: fifo: loadavg: 5.96 6.04 6.03 7/155 1349 T: 0 ( 615) P:50 I:1000 C:63448632 Min: 0 Act: 0 Avg: 0 Max: 55 T: 1 ( 616) P:50 I:1500 C:42299087 Min: 0 Act: 0 Avg: 1 Max: 43 T: 2 ( 617) P:50 I:2000 C:31724315 Min: 0 Act: 0 Avg: 1 Max: 51 T: 3 ( 618) P:50 I:2500 C:25379452 Min: 0 Act: 0 Avg: 1 Max: 53 T: 4 ( 619) P:50 I:3000 C:21149543 Min: 0 Act: 0 Avg: 1 Max: 47 //////////////////////////////////////// Update for Yocto L5.10.72 2.2.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.72 2.2.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.72-2.2.2. Updating: 1, Upgrade Xenomai to v3.2.1 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.15.71 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.15.71 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.15.71-2.2.0. Updating: 1, Upgrade Xenomai to v3.2.2 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai"   //////////////////////////////////////// Update for Yocto L6.1.55 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L6.1.55 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git recipes-rtlinux-xenomai -b Linux-6.1.x Updating: 1, Upgrade Xenomai to v3.2.4 and support i.MX93 2, Enable EVL (aka Xenomai 4) for i.MX93 and legacy i.MX(6/7D/8X/8M) Copy recipes-rtlinux-xenomai to <Yocto folder>/sources/meta-imx/meta-bsp/, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "evl" IMAGE_INSTALL:append += " libevl"  
View full article
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with MMDC initialization. The last sheet formats the register settings for use with ARM RealView ICE. It can also be used with the windows executable for the DDR Stress Test. This programming aid was used for internal NXP validation boards.
View full article
The iMX8QM LVDS has followed work mode, (There are two LVDS modules in IMX8QM): Single mode (LVDS panel connects to one channel) panel 1 and panel 2 can be different panels: Dual channel split mode (The panel needs two LVDS channels, CH0 for 1,3,5,7,... pixels and CH1 for 2,4,6,8,... pixels): Mirror dual mode (The two panels on same LDB PHY should be same panels on pixel clock and resolution, panel 1 and panel 2 are same; panel 3 and panel 4 are same): The reference patch is based on L5.4.3_GA1.0.0 BSP. LVDS single mode and dual channel split mode are supported in default Linux BSP. Patch 0002 can be used to test this dual mode on MEK board, some rework is needed on MEK board:     R194, R195, R208, R209, R213, R214 should be mounted. And the I6263 board can't be connected to LVDS0_CH0 and LVDS0_CH1 at the same time. The I6263 board can't be connected to LVDS1_CH0 and LVDS1_CH1 at the same time too. Note: for iMX8QXP, there is no mirror dual mode support, because its two LVDS ports are from two different LDB modules, there are no CH1 for them: Note: for iMX8QXP dual channel split mode (The pixel order can be switched: LDB1_CH0 for 1,3,5,7,... pixels and LDB2_CH0 for 2,4,6,8,... pixels; or LDB2_CH0 for 1,3,5,7,... pixels and LDB1_CH0 for 2,4,6,8,... pixels), iMX8QM LVDS has no such feature.
View full article