i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Questions: 1.  Are there any hardware limitations (such as in the Host Controller IP block itself, how this IP block was implemented or in the DMA engine) to how many device endpoints the i.MX53 can handle on Host2 or Host3?  The Reference Manual notes that the OTG controller supports up to 8 endpoints but does not provide information on the Host Controller. 2.  Do any of the device validation tests for verifying the i.MX53 design (or USB cert tests) test compatibility/performance with multiple devices and multiple endpoints? 3.  What are the maximum number of endpoints Freescale has tested with? Problem Background: During extensive testing the customer observes 100% CPU utilization with only 6 endpoints (can be a combination of multi-endpoint devices or single-endpoint devices - see below for test configuration details) using our latest Linux reference BSP (2.6.35 Kernel).  They have tested with the Adeneo WEC7 BSP and the open source Linux kernel based on 3.11 for the QSB and have observed similar performance limitations. This has been tested with multiple packet sizes and device/endpoint configurations and no impact has been shown in varying these parameters. The customer did note that they are only receiving/processing a single interrupt at the 1ms boundary regardless of the number of devices/endpoints.  Processing this interrupt takes approximately 23us for one device and an additional 17us for each additional device endpoint after the first that is processed. The customer hardware configuration for their testing looks something like this: On the customer's board: [i.MX53 Host2/Host3] -> [SMSC 3315 USB High Speed ULPI PHY] -> [SMSC LAN9514 On-board 4-port USB 2.0 HS Hub] External: [SMSC LAN9514 Port #1] -> [SMSC USB2415 4-Port USB 2.0 HS Hub] -> Medical device w/ endpoints #1-4 [SMSC LAN9514 Port #2] -> [SMSC USB2415 4-Port USB 2.0 HS Hub] -> Medical device w/ endpoints #5-8 [SMSC LAN9514 Port #3] ->  Medical device w/ endpoint #9 [SMSC LAN9514 Port #4] ->  Medical device w/ endpoint #10 Answer: Hosts do not have endpoints. Only devices have endpoints. EHCI compliance hosts, like all i.MX devices, use a linked list of queues (for bulk/control transport). Each queue has a queuehead that represents a corresponding endpoint and has the endpoint's capabilities. On the queue are transfer descriptors that have the information of which data is to be moved to/from the endpoint of the device. All of this is in main memory and read/written under DMA.  There is no limit on how many devices/endpoints a host can service, other than the amount of available main memory (DRAM). The CPU has to build the linked lists, but this is  normally not taking much bandwidth. My guess at this time is that there may be a problem in the USB driver, or the application that is using the driver, or a problem with data alignment. For efficient operation, data must be aligned on 32-bit boundaries. Buffers are best aligned on 64-byte boundaries.
View full article
Notes: First run the playback pipeline then the streaming pipeline. The above example streams H263 video and AMR audio data. Change codec format to your needs. In case where the iMX is the streaming machine, the audio encoder 'amrnbenc' must be installed before. This scenario has not been tested Shell variables and pipelines Playback machine (receiver) # On playback machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where PC does the playback     AUDIO_DEC_SINK="rtpamrdepay ! amrnbdec ! alsasink "     VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\""     VIDEO_DEC_SINK="rtph263pdepay ! ffdec_h263 ! autovideosink" ## End of IMX2PC Settings ## PC2IMX: Case where iMX does the playback     AUDIO_DEC_SINK="rtpamrdepay ! mfw_amrdecoder ! alsasink "     VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\""     VIDEO_DEC_SINK="rtph263pdepay ! vpudec ! mfw_v4lsink " ## End of PC2IMX Settings PLAYBACK_AUDIO="udpsrc caps=\"application/x-rtp,media=(string)audio,clock-rate=(int)8000,encoding-name=(string)AMR,encoding-params=(string)1,octet-align=(string)1\" \             port=5002 ! rtpbin.recv_rtp_sink_1 \         rtpbin. ! $AUDIO_DEC_SINK \      udpsrc port=5003 ! rtpbin.recv_rtcp_sink_1 \      rtpbin.send_rtcp_src_1 ! udpsink port=5007 sync=false async=false" PLAYBACK_VIDEO="udpsrc caps=$VIDEO_CAPS port=5000 ! rtpbin.recv_rtp_sink_0 \         rtpbin. ! $VIDEO_DEC_SINK \         udpsrc port=5001 ! rtpbin.recv_rtcp_sink_0 \         rtpbin.send_rtcp_src_0 ! udpsink port=5005 sync=false async=false" PLAYBACK_AV="$PLAYBACK_VIDEO $PLAYBACK_AUDIO" # Playback pipeline gst-launch -v gstrtpbin name=rtpbin $PLAYBACK_AV Streaming Machine (sender) # On Streaming machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where iMX does the streaming     IP=x.x.x.x # IP address of the playback machine     VIDEO_SRC="mfw_v4lsrc"     VIDEO_ENC="vpuenc codec=h263 ! rtph263ppay "    AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " ## END IMX2PC settings ## PC2IMX: Case where PC does the streaming     IP=y.y.y.y # IP address of the playback machine     VIDEO_SRC="v4l2src"     VIDEO_ENC="ffenc_h263 ! rtph263ppay "     AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " # END PC2PC settings STREAM_AUDIO="$AUDIO_ENC ! rtpbin.send_rtp_sink_1 \         rtpbin.send_rtp_src_1 ! udpsink host=$IP port=5002 \         rtpbin.send_rtcp_src_1 ! udpsink host=$IP port=5003 sync=false async=false \         udpsrc port=5007 ! rtpbin.recv_rtcp_sink_1" STREAM_VIDEO="$VIDEO_SRC ! $VIDEO_ENC ! rtpbin.send_rtp_sink_0 \         rtpbin.send_rtp_src_0 ! queue ! udpsink host=$IP port=5000 \         rtpbin.send_rtcp_src_0 ! udpsink host=$IP port=5001 sync=false async=false \         udpsrc port=5005 ! rtpbin.recv_rtcp_sink_0" STREAM_AV="$STREAM_VIDEO $STREAM_AUDIO" # Stream pipeline gst-launch -v gstrtpbin name=rtpbin $STREAM_AV
View full article
1. Follow all instructions from Freescale's github repo except the last bitbake command 2. Run hob under the build folder build$ hob & 3. On the GUI, select machine and image, then build 4. In case you need to flash an SD Card, hob does not produce an .sdcard image, so as a workaround, close hob and on the same console run build$ bitbake <image>     where image must be the same as the one you choose with hob 5. Flash your SD card build$ sudo dd if=tmp/deploy/images/fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=4M NOTES: In case of building issues, please follow this link In case of booting issues, make sure: 1. board DIP switches are set correctly 2. you have chosen the correct machine before baking If issues persist, report it to the community
View full article
Freescale's consumer and industrial i.MX 51 applications processors balance the performance, power consumption, connectivity and multimedia capabilities necessary to drive today's latest and greatest products. Freescale's automotive i.MX 51 processors provide what is necessary to steer today's most advanced automotive systems. i.MX51 Family Comparison i.MX Family Comparison Product Information on Freescale.com i.MX512 Applications Processor i.MX513 Applications Processor i.MX514 Applications Processor i.MX515 Applications Processor i.MX516 Applications Processor Evaluation/Development Boards and Systems IMX51EVK Evaluation Kit Bootloader Installing U-Boot on i.MX51EVK Flashing i.MX51EVK Working with mainline U-Boot Add new iMX5x board on LTIB Compiling U-Boot (from Freescale BSP) using LTIB Changing environment variables storage on U-Boot Linux Flashing Linux application only with SD card Reader Multimedia Using USB Camera Installing OpenCV Library (Open Computer Vision - Image Processing) Android Android without RamDisk Installing TTS library manually Running ADB over USB (iMX51 and Ubuntu communication) Ubuntu Using an USB Touchscreen (Karmic) Using Touchscreen (Lucid) Embedded Software and Tools Android OS for i.MX Applications Processors i.MX51 Current Software Updates and Releases Partners / 3rd-Party Development Tools STK5:  Starter-Kit 5 (Karo Electronics) Additional Resources Board bring-up and DDR initialization tools Develop a Simple OpenVG Application Under Linux: Tutorial i.MX 51 Android ADB over USB IMX51EVK i.MX51 EVK Board USB Camera i.MX51 EVK Compiling U-boot i.MX 51 EVK U-boot i.MX51 EVK Board Video i.MX51 EVK Board OpenCV i.MX51 EVK Board Flashing i.MX51 Flashing Linux Application Only with SD Card Reader I.MX51EVK Install U-Boot i.MX51 EVK Compiling U-boot i.MX51 EVK U-boot i.MX51 EVK Changing Env IMX51 Ubuntu USB TS i.MX 51 Ubuntu TS Lucid
View full article
Hi all,      I have a problem about usb mass storage driver, that's it can't enumerate my mass storage device.      but it can enumerate my mouse, keyboard...etc hid device.      anyone have idea about it ?      I always get below messages when my mass storage device plugs in.      and below is my dmesg information      My hardware -->      Type A receptacle on otg controller ~
View full article
The attached document describes how to calculate ESAI Mclk Bitclk LRclk for imx6 sabreauto board based on 3.10.17 linux kernel.
View full article
LTIB does not support X11 acceleration, since the packages are too old. Ubuntu 11.10 prebuilt image part of i.MX6 BSP has Xorg version 1.10.4. Yocto 1.4 has Xorg version 1.11.4. This document is based on Yocto 1.4.1 yocto and Freescale BSP 3.5.7 Alpha release. Few simple steps to enable 1.14.0. 1. Let us consider your Yocto directory is  $(rootfs_builder) 2. Edit vi sources/meta-fsl-arm/conf/machine/include/imx-base.inc      PREFERRED_VERSION_xserver-xorg_mx6 = "2:1.14.0" 3.Edit vi sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/xorg-driver/xf86-video-imxfb-vivante_3.5.7-1.0.0.bb      SRC_URI = "${FSL_MIRROR}/xserver-xorg-video-imx-viv-${PV}.tar.gz \            file://Makefile-fix-cross-compile.patch \                    file://0001-add-compat.h.patch" 4. Copy the attached Makefile-fix-cross-compile.patch into sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/xorg-driver/xf86-video-imxfb-vivante/. 5. In the build directory, delete the tmp directory. Otherwise there will be build errors (I did not found easy way) 6. bitbake fsl-image-x11 7. Now the image is ready to flash. 8. Boot the board with the newly built image. 9. Check the Xorg version log in /var/log/Xorg.0.log. It will be 1.14.0. 10. Before executing any of the X11-EGL application, export VIV_DESKTOP=0 to the terminal. You can see the application running. There are some known issues related to performance in 3.5.7 Alpha release.
View full article
i.MX6Q PCIe EP/RC Validation and Throughput Hardware setup     * Two i.MX6Q SD boards, one is used as PCIe RC; the other one is used as PCIe EP. Connected by 2*mini_PCIe to standard_PCIe  adaptors, 2*PEX cable adaptors,  and one PCIe cable. Software configurations     * When building RC image, make sure that         CONFIG_IMX_PCIE=y         # CONFIG_IMX_PCIE_EP_MODE_IN_EP_RC_SYS is not set         CONFIG_IMX_PCIE_RC_MODE_IN_EP_RC_SYS=y     * When build EP image, make sure that         CONFIG_IMX_PCIE=y         CONFIG_IMX_PCIE_EP_MODE_IN_EP_RC_SYS=y         # CONFIG_IMX_PCIE_RC_MODE_IN_EP_RC_SYS is not set Features     * Set-up link between RC and EP by their stand-alone 125MHz running internally. * In EP's system, EP can access the reserved ddr memory    (default address:0x40000000) of PCIe RC's system, by the   interconnection between PCIe EP and PCIe RC. NOTE: The layout of the 1G DDR memory on SD boards is 0x1000_0000 ~ 0x4FFF_FFFF) Use mem=768M in the kernel command line to reserve the 0x4000_0000 ~ 0x4FFF_FFFF DDR memory  space used to do the EP access tests. (The example of the RC’s cmd-line: Kernel command line: noinitrd console=ttymxc0,115200 mem=768M root=/dev/nfs nfsroot=10.192.225.216:/home/r65037/nfs/rootfs_mx5x_10.11,v3,tcp ip=dhcp rw) Throughput results ARM core used as the bus master, and cache is disabled ARM core used as the bus master, and cache is enabled IPU used as the bus master(DMA) Data size in one write tlp 8 bytes 32 bytes 64 bytes Write speed ~109MB/s ~298MB/s ~344MB/s Data size in one read tlp 32 bytes 64 bytes 64 bytes Read speed ~29MB/s ~100MB/s ~211MB/s IPU used as the bus master(DMA) Here is the summary of the PCIe throughput results tested by IPU. Write speed is about 344 MB/s. Read speed is about 211MB/s ARM core used as the bus master (define EP_SELF_IO_TEST in pcie.c driver) write speed ~300MB/s. read speed ~100MB/s. Cache is enabled. PCIe EP: Starting data transfer... PCIe EP: Data transfer is successful, tv_count1 54840us, tv_count2 162814us. PCIe EP: Data write speed is 298MB/s. PCIe EP: Data read speed is 100MB/s. Regarding to the log, the data size of each TLP when cache is enabled, is about 4 times of the data size in write, and 2 times of the data size in read, when the cache is not enabled. Cache is disabled Cache is enabled Data size in one write tlp 8 bytes 32 bytes Write speed ~109MB/s ~298MB/s Data size in one read tlp 32 bytes 64 bytes Read speed ~29MB/s ~100MB/s Cache is not enabled PCIe EP: Starting data transfer... PCIe EP: Data transfer is successful, tv_count1 149616us, tv_count2 552099us. PCIe EP: Data write speed is 109MB/s. PCIe EP: Data read speed is 29MB/s. One simple method used to connect the imx6 pcie ep and rc View of the whole solution: HW materials: 2* iMX6Q SD boards,  2* Mini PCIe to STD PCIe adaptors, one SATA2 data cable. the mini-pcie to standard pcie exchange adaptor. Here is the URL: http://www.bplus.com.tw/Adapter/PM2C.html How to make it. signals connections Two adaptors, one is named as A, the other one is named as B. A                  B TXM <----> RXM TXN <----> RXN RXM <----> TXM RXN <----> TXN A1 connected to B3 A2 connected to B4 A3 connected to B1 A4 connected to B2 Connect the cable to the adaptor. Connect the SATA2 data cable to Mini PCIe to STD PCIe adaptor (A)    Connect the SATA2 data cable to Mini PCIe to STD PCIe adaptor (B) NOTE: * Please keep length of Cable as short as possible.  Our cable is about 12cm. * Please connect shield wire in SATA2 Cable to GND at both board. * Please boot up PCIe EP system before booting PCIe RC system. Base one imx_3.0.35 mainline, the patch, and the IPU test tools had been attached. NOTE: * IPU tests usage howto. Unzip the xxx.zip, and run xxx_r.sh to do read tests, run xxx_w.sh to do the write tests. Tests log: EP: root@freescale ~/pcie_ep_io_test$ ./pcie-r.sh pass cmdline 14, ./pcie_ipudev_test.out new option : c frame count set 1 new option : l loop count set 1 new option : i input w=1024,h=1024,fucc=RGB4,cpx=0,cpy=0,cpw=0,cph=0,de=0,dm=0 new option : O 640,480,RGB4,0,0,0,0,0 new option : s show to fb 0 new option : f output file name ipu1-1st-ovfb new option : ÿ show_to_buf:0, input_paddr:0x1000000, output.paddr0x18800000 ====== ipu task ====== input:         foramt: 0x34424752         width: 1024         height: 1024         crop.w = 1024         crop.h = 1024         crop.pos.x = 0         crop.pos.y = 0 output:         foramt: 0x34424752         width: 640         height: 480         roate: 0         crop.w = 640         crop.h = 480         crop.pos.x = 0         crop.pos.y = 0 total frame count 1 avg frame time 19019 us, fps 52.579000 root@freescale ~/pcie_ep_io_test$ ./pcie-w.sh pass cmdline 14, ./pcie_ipudev_test.out new option : c frame count set 1 new option : l loop count set 1 new option : i input w=640,h=480,fucc=RGB4,cpx=0,cpy=0,cpw=0,cph=0,de=0,dm=0 new option : O 1024,1024,RGB4,0,0,0,0,0 new option : s show to fb 1 new option : f output file name ipu1-1st-ovfb new option : ÿ show_to_buf:1, input_paddr:0x18a00000, output.paddr0x1000000 ====== ipu task ====== input:         foramt: 0x34424752         width: 640         height: 480         crop.w = 640         crop.h = 480         crop.pos.x = 0         crop.pos.y = 0 output:         foramt: 0x34424752         width: 1024         height: 1024         roate: 0         crop.w = 1024         crop.h = 1024         crop.pos.x = 0         crop.pos.y = 0 total frame count 1 avg frame time 11751 us, fps 85.099140 root@freescale ~$ ./memtool -32 01000000=deadbeaf Writing 32-bit value 0xDEADBEAF to address 0x01000000 RC: Before run "./memtool -32 01000000=deadbeaf" at EP. root@freescale ~$ ./memtool -32 40000000 10 Reading 0x10 count starting at address 0x40000000 0x40000000:  00000000 00000000 00000000 00000000 0x40000010:  00000000 00000000 00000000 00000000 0x40000020:  00000000 00000000 00000000 00000000 0x40000030:  00000000 00000000 00000000 00000000 After run "./memtool -32 01000000=deadbeaf" at EP. root@freescale ~$ ./memtool -32 40000000 10 Reading 0x10 count starting at address 0x40000000 0x40000000:  DEADBEAF 00000000 00000000 00000000 0x40000010:  00000000 00000000 00000000 00000000 0x40000020:  00000000 00000000 00000000 00000000 0x40000030:  00000000 00000000 00000000 00000000 Labels parameters
View full article
Q: Some background; this instrument has one display connected to the LVDS output of the i.MX6Solo and the SVGA monitor is using the IPU port with an external Analog Devices ADV7125 DAC to actually drive the monitor (or projector).  From Tektronix: We got our kernel logo to show up on an external SVGA monitor as well as on the internal LVDS display so we now at least know that the hardware is functional. However, when our application starts running and writing to the fb0 (background) and fb1 (foreground/overlay) frame buffers, the external monitor (fb2 frame buffer) doesn't get updated. We need to know how to get the same data going to the external monitor as goes to the internal LVDS display.  the external monitor is 800x600 and the internal is 800x480 so we'd further like those 480 lines to show up centered in the 600 line monitor. We are also hoping that this can be down without having to write/DMA all of the data twice. The answer given is SR #1122663812 was "If the customer is using Linux, fb2 should also be drawed by their application."  This was considered in adequate and Tek replied: I would like to know if they are saying that the IPU absolutely cannot automatically do what we want and if not, why not?  I would like to have some detailed information to at least convince us that they've looked into this and it really isn't possible. A: In our Linux BSP we don't support such feature. And in android BSP it was already supported. The customer must draw the fb2 by their application, ipu doesn't have the feature that combining the fb0 and overlay fb1, then resize it to fb2 automatically. The customer application can drawing their UI into a memory, then use v4l2 output to draw this buffer to both fb0 and fb2, in this case, resizing will be implemented in V4l2 output driver with IPU hardware. And if the customer needs overlay on fb2, they must combine the two layer into memory with IPU task first, then using V4l2 output to render it to display fb2. For how to use IPU task, the customer can reference to BSP unit test code: imx-test-1.1.0\test\mxc_ipudev_test The summary: for dual display case, the fb0 and fb2 are just two framebuffer memory, they must be filled before rendering to display, on iMX6S/DL, only the fb0 has the hardware overlay (fb1); if the customer wants to show same contents on two displays in Linux, their application must draw the two framebuffers, but we had some hardware method to improve the performace, using GPU or IPU task. In Android, the application will not draw frame buffer directly, it will use Android surface flinger middleware to draw, so this feature was implemnted in surface flinger; but in Linux, there is no such middleware, and application draws the framebuffer directly, so the application should handle it. This document was generated from the following discussion: i.MX6Solo LDB/LVDS &amp; LCD Ports Active Simultaneously
View full article
Question: The description of the IOMUXC_GPR2 register is wrong. It contains exactly the same description as the LDB_CTRL register. The bits in the LDB_CTRL register work as advertised opposed to the GPR2 register. Answer: This is intentional. The LDB_CTRL description in the RM says "The register is implemented in the IOMUX Controller block (IOMUXC), as the register IOMUXC_GPR2.". And you will notice the two registers have the same address.
View full article
Hi all, I shared my test results and solutions in attachments. Best regards, Carl
View full article
About this document This document describe the setup detail for Robot Operating systems on  ubuntu 14.04 running on MX6QDL based boards. 1. Software & Hardware requirements Supported NXP HW boards: i.MX 6QuadPlus SABRE-SD Board and Platform i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board i.MX 6SoloX SABRE-SD Board i.MX 6SoloX SABRE-AI Board i.MX 7D Sabre Board Software:  Gcc toolchain, Ubuntu 14.04v installed on your board. 2. Installation For install ROS on iMX boards you need to have Ubuntu 14.04 rootfs installed in your board, for installation steps please follow up: https://community.freescale.com/docs/DOC-330147 Run your rootfs target and Configure your Ubuntu repositories to allow "restricted," "universe," and "multiverse.  $sudo nano /etc/apt/sources.list Your file should then look like this: deb http://ports.ubuntu.com/ubuntu-ports/ trusty main universe multiverse restricted deb-src http://ports.ubuntu.com/ubuntu-ports/ trusty main universe multiverse restricted deb http://ports.ubuntu.com/ubuntu-ports/ trusty-updates main universe multiverse restricted Make your installation up to date: $ sudo apt-get update $ sudo apt-get upgrade Set your locale: $ sudo update-locale LANG=C LANGUAGE=C LC_ALL=C LC_MESSAGES=POSIX Add ROS ARM repos & Key $ sudo sh -c 'echo "deb http://packages.ros.org/ros/ubuntu $(lsb_release -sc) main" > /etc/apt/sources.list.d/ros-latest.list' $ sudo apt-key adv --keyserver hkp://pool.sks-keyservers.net --recv-key 0xB01FA116 $ sudo apt-get update There are many different libraries and tools in ROS - not all compile fully on ARM. In this case we are going to install the ROS Base, however any other packages can be installed individually ROS-Base: (Bare Bones) ROS package, build, and communication libraries. No GUI tools. $ sudo apt-get install python-rosdep python-wstool build-essential cmake xserver-xorg-dev-lts-utopic mesa-common-dev-lts-utopic \ libxatracker-dev-lts-utopic libopenvg1-mesa-dev-lts-utopic libgles2-mesa-dev-lts-utopic libgles1-mesa-dev-lts-utopic\ libgl1-mesa-dev-lts-utopic libgbm-dev-lts-utopic libegl1-mesa-dev-lts-utopic Alternatively, try installing just this to fix dependency issues, and then install ROS base (includes ROS package, build, and communication libraries. No GUI tools.😞 $ sudo apt-get install libgl1-mesa-dev-lts-utopic $ sudo apt-get install ros-indigo-ros-base Before you can use ROS, you will need to initialize rosdep. It enables you to easily install system dependencies for source you want to compile and is required to run some core components in ROS. $ sudo rosdep init $ rosdep update Install rosinstall: $ sudo apt-get install python-rosinstall Verifying OS name. If you installed the Linaro ALIP rootfs, make sure your OS name defined at /etc/lsb-release is as the following. Since ros does not recognize Linaro as an OS, this is necessary. $ lsb_release -a You should get: No LSB modules are available. Distributor ID: Ubuntu Description:    Ubuntu 14.04.4 LTS Release:        14.04 Codename:       trusty In any case you get a different output, the following is for Ubuntu 14.04, trusty. Modify the release number and name as per your target. DISTRIB_ID=Ubuntu DISTRIB_RELEASE=14.04 DISTRIB_CODENAME=trusty DISTRIB_DESCRIPTION="Ubuntu 14.04" 3. Testing The Installation Run ROS $ roscore You should get: ... logging to /root/.ros/log/1c07caa4-1dd3-11b2-b860-00049f0399fe/roslaunch- imx6q-2707.log Checking log directory for disk usage. This may take awhile. Press Ctrl-C to interrupt Done checking log file disk usage. Usage is <1GB. Started roslaunch server http://i.Mx6q:37547/ ros_comm version 1.11.16 SUMMARY ======== PARAMETERS * /rosdistro: indigo * /rosversion: 1.11.16 NODES auto-starting new master process[master]: started with pid [2718] ROS_MASTER_URI=http://imx6q:11311/ setting /run_id to 1c07caa4-1dd3-11b2-b860-00049f0399fe process[rosout-1]: started with pid [2731] started core service [/rosout] Open a new Terminal and Create the user catkin_ws Workspace. The catkin_ws workspace will contain the user packages. $ source /opt/ros/indigo/setup.bash $ mkdir -p ~/catkin_ws/src $ cd ~/catkin_ws/src $ catkin_init_workspace $ cd ~/catkin_ws/ $ catkin_make The  catkin_make command is a convenience tool for working with catkin_workspace. If you look in your current directory you should now have a 'build' and 'devel' folder. Inside the 'devel' folder you can see that there are now several setup.*sh files. Sourcing any of these files will overlay this workspace on top of your environment. To understand more about this see the general catkin documentation: http://wiki.ros.org/catkin Before continuing source your new setup.*sh file: $ source devel/setup.bash To make sure your workspace is properly overlayed by the setup script, make sure ROS_PACKAGE_PATH environment variable includes the directory you're in. $ echo $ROS_PACKAGE_PATH /home/youruser/catkin_ws/src:/opt/ros/indigo/share:/opt/ros/indigo/stacks Next you should go ahead and learn how to use the workspace. If you are following the ROS tutorials series instead of the catkin tutorials, please continue with Creating a ROS Package. For more testing on your installation, you can try the ROS Tutorials (http://wiki.ros.org/ROS/Tutorials)
View full article
Notes: + Run the pipelines in the presented order + The above example streams H263 video. + the gl command is equal to 'gst-launch' (two instead of 'gst-launch'.size() chars ) + Pending work: H264 test cases and other scenarios. Scenario Shell variables and pipelines # Export always these variables on the i.MX export VSALPHA=1 export WIDTH=320 export HEIGHT=240 export SEP=20 # decoded and displayed Uni-directional: from PC to i.MX. PC is streaming 4 H.263 streams and i.MX displays all in the screen. # On i.MX (Target) gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8890 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=0 axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8891 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=0 axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8892 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8893 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT & # On PC (Source) export IP_iMX= # Place the IP address of the i.MX board gst-launch -v videotestsrc ! ffenc_h263 ! rtph263pay ! multiudpsink clients=IP_iMX:8890,IP_iMX:8891,IP_iMX:8892,$IP_iMX:8893 Uni-directional: from PC to i.MX. PC is streaming one H.264 stream and i.MX displays it on the screen # On i.MX (Target) # Make sure you set the caps correctly, specially the sprop-parameter-sets cap. The one show below is just an example and works with the source file sintel_trailer-1080p.mp4 export VSALPHA=1 GST_DEBUG=*:2 gst-launch -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, sprop-parameter-sets=(string)\"Z2QAMqw05gHgCJ+WEAAAAwAQAAADAwDxgxmg\\,aOl4TLIs\", payload=(int)96' port=8890 ! rtph264depay ! vpudec ! mfw_isink sync=false # On PC (Source) gst-launch -v filesrc location=sintel_trailer-1080p.mp4 typefind=true ! qtdemux ! rtph264pay ! multiudpsink clients=10.112.102.168:8890 Bi-directional: PC is streaming 4 H.263 streams to i.MX, iMX displays it and sends the four back to PC # On i.MX export IP_PC= # Place the IP address of the PC host machine gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8890 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=0 axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9990 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8891 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=0 axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9991 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8892 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9992 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8893 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9993 & # On PC ## Stream received from iMX export IP_iMX= # Place the IP address of the i.MX board gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9990 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9991 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9992 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9993 ! rtph263depay ! ffdec_h263 ! xvimagesink & ## Stream sent to iMX gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 !  ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8890 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8891 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8892 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8893 &
View full article
Introduction Hardware Connections Device Tree Configuration Rebuilding Image Requirements Kernel Device Tree Application Driver Main Init Driver Write Read Building and Run the SPI Application Driver Conclusion   Introduction   This document describes how to interface and use Xtrinsic FXLS8471Q digital accelerometer with IMX6Q processor. For this purpose, UDOO Quad board is used with NXP Linux image for IMX6QSABRE-SD board with Kernel 3.14.56 (not with Udoobuntu) to simulate working with a custom board, the process to customize and build such image for UDOO Quad board is described here: Building Linux Image with QT5 for UDOO Quad    On the sensor side FRDM-FXS-MULTI(-B) sensor expansion board which features many of the Xtrinsic sensors introduced in 2013 including the FXSL8471Q is used.   Hardware Connections    The SPI signals from FRDM-FXS-MULTI are routed to SPI1 module of UDOO Quad. FXLS8471Q provides an INT pin which is indicated on image below, however on this implementation polling method is used. Please note that Chip Select is not controlled automatically by SPI module, therefore this pin is configured as GPIO. Besides these signals, reset and power source pins were also connected.   The following figure shows the pins used in FRDM-FXS-MULTI which are connected with UDOO Quad board.           The pins used on the UDOO Quad side are shown in the images below. You can find UDOO Quad pinout diagram here Index of /download/files/pinout.                             Device Tree Configuration   As mentioned at the beginning of this document, a NXP Linux image for IMX6Q-SABRESD is used. In order to customize this image to be used with the UDOO Quad board it is necessary to build a .dtb that matches with it. This task was accomplished obtaining dts and dtsi source files listed below from Kernel Linux Repository for UDOO at UDOOboard (UDOOboard) · GitHub.   imx6qdl-udoo.dtsi imx6qdl-udoo-externalpins.dtsi imx6q-udoo-hdmi.dts   These files were copied into the IMX6Q-SABRESD build source folder and a imx6q-udoo.dtb was generated. This process is described on Building Linux Image with QT5 for UDOO Quad    The following snippets show how the nodes involved on the SPI configuration were set for UDOO Quad board. Please note that each device tree should match your custom board.   In imx6qdl-udoo-externalpins.dtsi verify that ecspi1 node matches with the one shown below.   &ecspi1 {     fsl,spi-num-chipselects = <1>;     cs-gpios = <&gpio5 17 0>;     pinctrl-0 = <&pinctrl_ecspi1>;     pinctrl-names = "default";     status = "disabled";     spidev0: spi@0 {         #address-cells = <1>;         #size-cells = <1>;         compatible = "spidev";         reg = <0>;         spi-max-frequency = <2000000>;     }; };     As you can see on snippet above, ecspi1 node uses pinctrl_ecspi1 as the pin configuration node which is defined in the same file and it looks as follows.          pinctrl_ecspi1: ecspi1grp {             fsl,pins = <             MX6QDL_PAD_DISP0_DAT22__ECSPI1_MISO  0x100b1             MX6QDL_PAD_DISP0_DAT20__ECSPI1_SCLK  0x100b1             MX6QDL_PAD_DISP0_DAT21__ECSPI1_MOSI  0x100b1             MX6QDL_PAD_DISP0_DAT23__GPIO5_IO17   0x80000000             >;         };   However, as you may know each pin on i.MX devices has up to 8 potential functions, and on the other side, one function can be available in different pins.   For example, ECSPI1_MISO can be mapped to 4 different pins     and each pin can have different functions. From all the available functions in a pin one is chosen to be the pad (pin) name. In the image below DISP0_DATA22 was chosen to be the pad name.       Now, back to pinctrl_ecspi1 node, the macros used here are defined in imx6q-pinfuc.h, as you can see DISP0_DAT20 - DISP0_DAT23 are the pads used with the ECSPI signals.   It is necessary to check it that there are no other configurations for DISP0_DAT20 - DISP0_DAT23 and if they are it is necessary to comment out them or delete them. In this case there were other configurations for these pins in imx6qdl-udoo-externalpins.dtsi and they were commented out.     &iomuxc {     imx6q-udoo {         // External Pinout GPIOs         external_hog: hoggrp-2 {         fsl,pins = <             MX6QDL_PAD_CSI0_DAT11__GPIO5_IO29    0x80000000  // {{external-gpio-0}}             MX6QDL_PAD_CSI0_DAT10__GPIO5_IO28    0x80000000  // {{external-gpio-1}}             MX6QDL_PAD_SD1_CLK__GPIO1_IO20       0x80000000  // {{external-gpio-2}}             MX6QDL_PAD_SD1_DAT0__GPIO1_IO16      0x80000000  // {{external-gpio-3}}             MX6QDL_PAD_SD1_DAT1__GPIO1_IO17      0x80000000  // {{external-gpio-4}}             MX6QDL_PAD_SD1_CMD__GPIO1_IO18       0x80000000  // {{external-gpio-5}}             MX6QDL_PAD_SD4_DAT1__GPIO2_IO09      0x80000000  // {{external-gpio-6}}             MX6QDL_PAD_SD4_DAT2__GPIO2_IO10      0x80000000  // {{external-gpio-7}}             MX6QDL_PAD_SD1_DAT3__GPIO1_IO21      0x80000000  // {{external-gpio-8}}             MX6QDL_PAD_SD1_DAT2__GPIO1_IO19      0x80000000  // {{external-gpio-9}}             MX6QDL_PAD_GPIO_1__GPIO1_IO01        0x80000000  // {{external-gpio-10}}             MX6QDL_PAD_GPIO_9__GPIO1_IO09        0x80000000  // {{external-gpio-11}}             MX6QDL_PAD_GPIO_3__GPIO1_IO03        0x80000000  // {{external-gpio-12}}             MX6QDL_PAD_SD4_DAT0__GPIO2_IO08      0x80000000  // {{external-gpio-13}}             MX6QDL_PAD_CSI0_DAT4__GPIO5_IO22     0x80000000  // {{external-gpio-14}}             MX6QDL_PAD_CSI0_DAT16__GPIO6_IO02    0x80000000  // {{external-gpio-15}}             MX6QDL_PAD_CSI0_DAT14__GPIO6_IO00    0x80000000  // {{external-gpio-16}}             MX6QDL_PAD_CSI0_DAT15__GPIO6_IO01    0x80000000  // {{external-gpio-17}}             MX6QDL_PAD_CSI0_DAT12__GPIO5_IO30    0x80000000  // {{external-gpio-18}}             MX6QDL_PAD_CSI0_DAT13__GPIO5_IO31    0x80000000  // {{external-gpio-19}}             MX6QDL_PAD_EIM_D28__GPIO3_IO28       0x80000000  // {{external-gpio-20}}             MX6QDL_PAD_EIM_D21__GPIO3_IO21       0x80000000  // {{external-gpio-21}}             MX6QDL_PAD_DISP0_DAT6__GPIO4_IO27    0x80000000  // {{external-gpio-22}}             MX6QDL_PAD_DISP0_DAT7__GPIO4_IO28    0x80000000  // {{external-gpio-23}}             MX6QDL_PAD_DISP0_DAT8__GPIO4_IO29    0x80000000  // {{external-gpio-24}}             MX6QDL_PAD_DISP0_DAT9__GPIO4_IO30    0x80000000  // {{external-gpio-25}}             MX6QDL_PAD_DISP0_DAT10__GPIO4_IO31   0x80000000  // {{external-gpio-26}}             MX6QDL_PAD_DISP0_DAT11__GPIO5_IO05   0x80000000  // {{external-gpio-27}}             MX6QDL_PAD_DISP0_DAT12__GPIO5_IO06   0x80000000  // {{external-gpio-28}}             MX6QDL_PAD_DISP0_DAT13__GPIO5_IO07   0x80000000  // {{external-gpio-29}}             MX6QDL_PAD_DISP0_DAT14__GPIO5_IO08   0x80000000  // {{external-gpio-30}}             MX6QDL_PAD_DISP0_DAT15__GPIO5_IO09   0x80000000  // {{external-gpio-31}}             MX6QDL_PAD_DISP0_DAT16__GPIO5_IO10   0x80000000  // {{external-gpio-32}}             MX6QDL_PAD_DISP0_DAT17__GPIO5_IO11   0x80000000  // {{external-gpio-33}}             MX6QDL_PAD_DISP0_DAT18__GPIO5_IO12   0x80000000  // {{external-gpio-34}}             MX6QDL_PAD_DISP0_DAT19__GPIO5_IO13   0x80000000  // {{external-gpio-35}}             //MX6QDL_PAD_DISP0_DAT20__GPIO5_IO14   0x80000000  // {{external-gpio-36}}             //MX6QDL_PAD_DISP0_DAT21__GPIO5_IO15   0x80000000  // {{external-gpio-37}}             MX6QDL_PAD_EIM_A16__GPIO2_IO22       0x80000000  // {{external-gpio-38}}             MX6QDL_PAD_GPIO_18__GPIO7_IO13       0x80000000  // {{external-gpio-39}} (KEY_VOL_UP)             MX6QDL_PAD_NANDF_D0__GPIO2_IO00      0x80000000  // {{external-gpio-40}} (HOME)             MX6QDL_PAD_NANDF_D3__GPIO2_IO03      0x80000000  // {{external-gpio-41}} (SEARCH)             MX6QDL_PAD_NANDF_D2__GPIO2_IO02      0x80000000  // {{external-gpio-42}} (BACK)             MX6QDL_PAD_NANDF_D1__GPIO2_IO01      0x80000000  // {{external-gpio-43}} (MENU)             MX6QDL_PAD_GPIO_19__GPIO4_IO05       0x80000000  // {{external-gpio-44}} (KEY_VOL_DOWN)            // MX6QDL_PAD_DISP0_DAT22__GPIO5_IO16   0x80000000  // {{external-gpio-45}}             //MX6QDL_PAD_DISP0_DAT23__GPIO5_IO17   0x80000000  // {{external-gpio-46}}             MX6QDL_PAD_EIM_D25__GPIO3_IO25       0x80000000  // {{external-gpio-47}}             MX6QDL_PAD_KEY_ROW1__GPIO4_IO09      0x80000000  // {{external-gpio-48}}             MX6QDL_PAD_KEY_COL1__GPIO4_IO08      0x80000000  // {{external-gpio-49}}             MX6QDL_PAD_EIM_OE__GPIO2_IO25        0x80000000  // {{external-gpio-50}}             MX6QDL_PAD_EIM_CS1__GPIO2_IO24       0x80000000  // {{external-gpio-51}}             MX6QDL_PAD_EIM_CS0__GPIO2_IO23       0x80000000  // {{external-gpio-52}}             MX6QDL_PAD_EIM_D24__GPIO3_IO24       0x80000000  // {{external-gpio-53}}             MX6QDL_PAD_GPIO_8__GPIO1_IO08        0x80000000  // {{external-gpio-54}}             MX6QDL_PAD_GPIO_7__GPIO1_IO07        0x80000000  // {{external-gpio-55}}             >;         };     Finally, in imx6q-udoo-hdmi.dts enable ECSPI by including an ecspi1 node reference and setting the status property to "okay".   dts-v1/; #include "imx6q.dtsi" #include "imx6qdl-udoo.dtsi" #include "imx6qdl-udoo-externalpins.dtsi" / {     model = "UDOO Quad Board";     compatible = "udoo,imx6q-udoo", "fsl,imx6q";        mxcfb1: fb@0 {         compatible = "fsl,mxc_sdc_fb";         disp_dev = "hdmi";         interface_pix_fmt = "RGB24";         mode_str ="1920x1080M@60";         default_bpp = <32>;         int_clk = <0>;         late_init = <0>;         status = "okay";     }; }; &ecspi1 {     status = "okay"; };   Note: This could be done in .dtsi but the side effect is that any configuration including the dtsi will have ECSPI1 enabled by default.   Finally it is necessary to rebuild the device tree and copy it to the FAT partition of the sdcard. This process is explained in next section.   Rebuilding Image   Requirements In order to build an image as well as an application it is necessary to install a tool to cross-compile code, this way we will be able to generate executable files for ARM architecture in our host machine. This tool is called meta-toolchain, the following commands are used to install it.   In the following instructions it is considered that the build directory is ~/fsl-release_bsp/build_imx6qsabresd_qt5/   $ cd ~/fsl-release_bsp $ source setup-environment build_imx6qsabresd_qt5 $ bitbake meta-toolchain $ sh tmp/deploy/sdk/fsl-imx-x11-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-<kernel>.sh Kernel   In order to enable the kernel SPI driver it is necessary to set it in the menuconfig and rebuild zImage.   Go to kernel directory within the Yocto build directory that we created. $ cd <build_directory>/tmp/work-shared/imx6qsabresd/kernel-source$   Launch menuconfig for imx $ source /opt/fsl-imx-x11/<kernel version>/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi $ make imx_v7_defconfig $ make menuconfig   Enable SPI Driver by going to Device Drivers --> SPI Support and seting '*' to SPI device Driver, save changes and then exit.     And build zImage $ make zImage   The generated file is located in <build_directory>/tmp/work-shared/imx6qsabresd/kernel-source/arch/arm/boot$ and it must be copied to the FAT partition of the SD card.   Device Tree   To build the device tree go to kernel directory within the Yocto build directory that we created. $ cd <build_directory>/tmp/work-shared/imx6qsabresd/kernel-source$   Build dtb file $ source /opt/fsl-imx-x11/<kernel version>/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi $ make imx_v7_defconfig $ make imx6q-udoo-hdmi.dtb   The generated file is located in <build_directory>/tmp/work-shared/imx6qsabresd/kernel-source/arch/arm/boot/dts$ and it must be renamed as imx6q-udoo.dtb and copied to the FAT partition of the SD card.   Application Driver   The SPI kernel driver uses a structure named spi_ioc_transfer which describes a single SPI transfer. It holds pointers to userspace buffers with transmit and receive data, length of buffers, speed, bits per word among other configurations. For further details you can refer to /include/uapi/linux/spi/spidev.h on your kernel source. In the next section the application driver is explained.   The source files of the application driver as well as the device tree sources can be found in the attached.zip file.   Main   The following code shows function main where the SPI driver is initialized driver using "/dev/spidev0.0" which is listed under /dev (in the target root file system) after SPIdev driver is enabled in menuconfig and kernel is rebuilt as indicated in previous section. Then it reads who am i register just for sanity check purpose and initializes and calibrates the sensor and enters in an endless loop where it reads the sensor whenever there is new data ready. Raw data is returned in 6 bytes, so it is managed to get X, Y and Z values and finally these values are converted to G's values and it waits until a key is pressed to continue to read the following value.     /****************************************************************************** * Main ******************************************************************************/ int main(){      //enableGPIO(); //In case of using interrupt instead of polling      file = spi_init("/dev/spidev0.0"); //dev      who();      FXLS8471Q_Init();      FXLS8471Q_Calibration();      while(1)      {          checkData();          if (DataReady) // Is a new set of data ready?          {              buffer = (unsigned char *)spi_read(OUT_X_MSB_REG, 6, file); // Read data output registers 0x01-0x06              printf("AccData[0] = 0x%X \n AccData[1] = 0x%X \n AccData[2] = 0x%X \n AccData[3] = 0x%X \n AccData[4] = 0x%X \n AccData[5] = 0x%X \n", AccData[0], AccData[1], AccData[2], AccData[3], AccData[4], AccData[5]);              Xout_14_bit = ((short) (AccData[0] << 8 | AccData[1])) >> 2; // Compute 14-bit X-axis output value              Yout_14_bit = ((short) (AccData[2] << 8 | AccData[3])) >> 2; // Compute 14-bit Y-axis output value              Zout_14_bit = ((short) (AccData[4] << 8 | AccData[5])) >> 2; // Compute 14-bit Z-axis output value              Xout_g = ((float) Xout_14_bit) / SENSITIVITY_2G; // Compute X-axis output value in g's              Yout_g = ((float) Yout_14_bit) / SENSITIVITY_2G; // Compute Y-axis output value in g's              Zout_g = ((float) Zout_14_bit) / SENSITIVITY_2G; // Compute Z-axis output value in g's              //printf(" X = %d Y = %d Z = %d \n\n", AccData[0], AccData[2], AccData[4]);              //printf("Xval = %d Yval = %d Zval = %d \n", Xout_14_bit, Yout_14_bit, Zout_14_bit);              printf(" XG = %f YG = %f ZG = %f \n\n", Xout_g, Yout_g, Zout_g);              getchar();         }      }      close(file); } Init Driver   The spi_init function opens a file for the driver "/dev/spidev0.0" which is passed as a parameter from main(), then the SPI configuration parameters are read just for informative purpose. Finally struct xfer which is of type spi_ioc_transfer is initialized.   /********************************* SPIdev Init **********************************************/ int spi_init(char filename[40]) { int file; unsigned char mode, lsb, bits; unsigned int baudrate = 524250, speed; printf("SPI Init \n"); if ((file = open(filename,O_RDWR)) < 0) { printf("Failed to open the bus."); /* ERROR HANDLING; you can check errno to see what went wrong */ com_serial=0; exit(1); } if (ioctl(file, SPI_IOC_RD_MODE, &mode) < 0) { perror("SPI rd_mode"); return -1; } if (ioctl(file, SPI_IOC_RD_LSB_FIRST, &lsb) < 0) { perror("SPI rd_lsb_fist"); return -1; } if (ioctl(file, SPI_IOC_RD_BITS_PER_WORD, &bits) < 0) { perror("SPI bits_per_word"); return -1; } if (ioctl(file, SPI_IOC_RD_MAX_SPEED_HZ, &speed) < 0) { perror("SPI max_speed_hz"); return -1; } printf("%s: spi mode %d, %d bits %s per word, %d Hz max\n",filename, mode, bits, lsb ? "LSB first" : "MSB first", baudrate); xfer[0].len = 3; /* Length of command to write*/ xfer[0].cs_change = 0; /* Keep CS activated */ xfer[0].delay_usecs = 0; //delay in us xfer[0].speed_hz = 524250; //speed xfer[0].bits_per_word = 8; // bites per word 8 xfer[1].len = 4; /* Length of Data to read */ xfer[1].cs_change = 0; /* Keep CS activated */ xfer[1].delay_usecs = 0; xfer[1].speed_hz = 524250; xfer[1].bits_per_word = 8; printf("SPI Init Finished \n"); return file; }     Write   The SPI communication is started with the  falling edge on chip select pin. A write operation is initiated by transmitting a 1 for the R/W bit. Then the 8-bit register address, ADDR[7:0] is encoded in the first and second serialized bytes. Data to be written starts in the third serialized byte. The order of the bits is as follows:   Byte 0: R/W, ADDR[6], ADDR[5], ADDR[4], ADDR[3], ADDR[2], ADDR[1], ADDR[0] Byte 1: ADDR[7], X, X, X, X, X, X, X Byte 2: DATA[7], DATA[6], DATA[5], DATA[4], DATA[3], DATA[2], DATA[1], DATA[0]   The SPI communication is finished with the  falling edge on chip select pin.   A you can see below array buf keeps the destination address and the data to be transferred, then xfer structure is configured to point to buf as the transfer buffer and the length of the data es set to 2 + data size (the first 2 bytes are for the destination address which is splitted in 2 bytes). Finally the transfer is started by the ioctl command.   /******************** Write a byte to the FXLS8471Q *************************** * Byte 0: 1,ADDR[6],ADDR[5],ADDR[4],ADDR[3],ADDR[2],ADDR[1],ADDR[0] * Byte 1: ADDR[7],0,0,0,0,0,0,0 * Byte 2: DATA[7],DATA[6],DATA[5],DATA[4],DATA[3],DATA[2],DATA[1],DATA[0] ******************************************************************************/ void spi_write(int registerAddress, int nbytes, char data, int file) { unsigned char buf[32]; int status; memset(buf, 0, sizeof buf); buf[0] = 0x80 | registerAddress; buf[1] = 0x80 & registerAddress; buf[2] = data; xfer[0].tx_buf = (unsigned long)buf; xfer[0].len = nbytes + 2; /* Length of command to write*/ status = ioctl(file, SPI_IOC_MESSAGE(1), xfer); if (status < 0) { perror("SPI_IOC_MESSAGE"); return; } com_serial=1; failcount=0; }     Below is the write operation which writes the value 0x3D to the CTRL_REG1 (0x2A).     Read   Similarly a read operation is initiated by transmitting a 0 for the R/W bit. Then the 8-bit register address, ADDR[7:0] is encoded in the first and second serialized bytes. The data is read from the MISO pin (MSB first).   In this case the array buf keeps the address that is going to be read and the third byte is just a dummy byte to be transferred. Structure xfer keeps transfer buffer pointer which in this case is buf and receive buffer which is AccData, the lenght of the command to write and the length of data to read is also specified and finally the read command is executed with ioctl call.     /********************** Read a byte from the FXLS8471Q *********************** * Byte 0: 0,ADDR[6],ADDR[5],ADDR[4],ADDR[3],ADDR[2],ADDR[1],ADDR[0] * Byte 1: ADDR[7],0,0,0,0,0,0,0 * Byte 2: 0,0,0,0,0,0,0,0 ******************************************************************************/ char * spi_read(int registerAddress, int nbytes, int file) { int status; memset(buf, 0, sizeof buf); memset(AccData, 0, sizeof AccData); buf[0] = 0x7F & registerAddress; buf[1] = 0x80 & registerAddress; buf[2] = 0x00; xfer[0].tx_buf = (unsigned long)buf; xfer[0].len = 2; /* Length of command to write*/ xfer[1].rx_buf = (unsigned long) AccData; xfer[1].len = nbytes; /* Length of Data to read */ xfer[1].speed_hz = 524250; status = ioctl(file, SPI_IOC_MESSAGE(2), xfer); if (status < 0) { perror("SPI_IOC_MESSAGE"); return 0; } com_serial=1; failcount=0; return AccData; }     The screenshot below shows the read operation which reads the correct value 0x6A from the WHO_AM_I register (0x0D).     Building and Run the SPI Application Driver   In order to build the application please save the source files and the Makefile (attached) on any place on your host machine and go to that directory where you saved them. Then build the application with the Meta-toolchain using the Make file with the following commands.   Build application driver $ cd <folder wher spi device driver source is saved> $ source /opt/fsl-imx-x11/<kernel version>/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi $ make   A spi_test file will be created in the same folder, copy this file into the sdcard on the Root File System partition in /home/root. Finally when booting the target execute the application. You must see the following output.       Conclusion   This document summarizes the steps to create a SPI application driver. As you saw it is necessary to rebuild the device tree and the kernel, and to do this it is necessary to install metatoolchain. The application driver uses the SPI kernel driver and its main functions are next: Init SPI Driver Read Write Init sensor Callibrate Sensor Polling data ready function   I would say that the core of the application driver are the read and write functions which configure the SPI kernel driver and pass data to it in the format required by the sensor.   For specific details on the driver please see the attached .zip file which contains the application driver code, the Makefile with the one it is build and the device tree sources.   I hope you find this document useful.     Carlos
View full article
[Brief description] (1)Contents The ducoment introduced how to expand Gigabit Ethernet based on i.MX6 PCI Express, and attached schematics in DSN & pdf format. (2)Binary file for EEROM I have the binary file used to debug intel82574 circuit in this schematic, If customer wants to use it to debug board based on i.MX6+Intel82574, she can submit a case for me to get the file by our Salesforece system. Best Regards, TIC Weidong Sun Email: [email protected]
View full article
Two IPUs are supported in i.MX6Q SoC, each IPU supports 1920x1080 resolution, and 4 kinds of interfaces on i.MX6Q PADs can be used to connect display devices: HDMI, Digital RGB24, LVDS1+LVDS2, MIPI DSI. In the documents, we will discuss how to expand VGA port with digital RGB and realize dual-display via HDMI & VGA, The solution has been validated on Android4.2.2 and Android4.4.2 BSP released by NXP. 1.  Expanding VGA port based on digital RGB24 interface with ADV7125 Schematic is in attachments. 2. Configurations of envionment variables in u-boot The following settings are for booting via NFS, users can adjust them to boot via Flash on board. setenv ipaddr 192.168.1.103 setenv serverip 192.168.1.102 setenv gateway 192.168.1.1 setenv ethaddr 00:04:9f:00:ea:d3 setenv bootargs_base 'setenv bootargs console=ttymxc0,115200' setenv bootargs_android 'setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 androidboot.hardware=freescale' setenv bootargs_nfs 'setenv bootargs ${bootargs} ip=${ipaddr}:${serverip}:${gateway}:${netmask}::eth0 off root=/dev/nfs nfsroot=${serverip}:${nfsroot}' setenv bootargs_disp 'setenv bootargs ${bootargs} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb1:dev=lcd,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off fbmem=32M vmalloc=400M' setenv bootcmd_net 'run bootargs_base bootargs_android bootargs_nfs bootargs_disp;tftpboot ${loadaddr} uImage;bootm' 3. Configurations in BSP file (1)IOMUX of DISP0 port (in header file)     MX6Q_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK,     MX6Q_PAD_DI0_PIN15__IPU1_DI0_PIN15,        /* DE */     MX6Q_PAD_DI0_PIN2__IPU1_DI0_PIN2,        /* HSync */     MX6Q_PAD_DI0_PIN3__IPU1_DI0_PIN3,        /* VSync */     MX6Q_PAD_DISP0_DAT0__IPU1_DISP0_DAT_0,     MX6Q_PAD_DISP0_DAT1__IPU1_DISP0_DAT_1,     MX6Q_PAD_DISP0_DAT2__IPU1_DISP0_DAT_2,     MX6Q_PAD_DISP0_DAT3__IPU1_DISP0_DAT_3,     MX6Q_PAD_DISP0_DAT4__IPU1_DISP0_DAT_4,     MX6Q_PAD_DISP0_DAT5__IPU1_DISP0_DAT_5,     MX6Q_PAD_DISP0_DAT6__IPU1_DISP0_DAT_6,     MX6Q_PAD_DISP0_DAT7__IPU1_DISP0_DAT_7,     MX6Q_PAD_DISP0_DAT8__IPU1_DISP0_DAT_8,     MX6Q_PAD_DISP0_DAT9__IPU1_DISP0_DAT_9,     MX6Q_PAD_DISP0_DAT10__IPU1_DISP0_DAT_10,     MX6Q_PAD_DISP0_DAT11__IPU1_DISP0_DAT_11,     MX6Q_PAD_DISP0_DAT12__IPU1_DISP0_DAT_12,     MX6Q_PAD_DISP0_DAT13__IPU1_DISP0_DAT_13,     MX6Q_PAD_DISP0_DAT14__IPU1_DISP0_DAT_14,     MX6Q_PAD_DISP0_DAT15__IPU1_DISP0_DAT_15,     MX6Q_PAD_DISP0_DAT16__IPU1_DISP0_DAT_16,     MX6Q_PAD_DISP0_DAT17__IPU1_DISP0_DAT_17,     MX6Q_PAD_DISP0_DAT18__IPU1_DISP0_DAT_18,     MX6Q_PAD_DISP0_DAT19__IPU1_DISP0_DAT_19,     MX6Q_PAD_DISP0_DAT20__IPU1_DISP0_DAT_20,     MX6Q_PAD_DISP0_DAT21__IPU1_DISP0_DAT_21,     MX6Q_PAD_DISP0_DAT22__IPU1_DISP0_DAT_22,     MX6Q_PAD_DISP0_DAT23__IPU1_DISP0_DAT_23,     MX6Q_PAD_NANDF_D4__GPIO_2_4,        /* ADV7125 Power on / off (2) Frame buffer static struct ipuv3_fb_platform_data qcorein_fb_data[] = { /*    {     .disp_dev = "ldb",     .interface_pix_fmt = IPU_PIX_FMT_RGB666,     .mode_str = "LDB-WXGA",     .default_bpp = 16,     .int_clk = false,     .late_init = false,     }, */     {     .disp_dev = "hdmi",     .interface_pix_fmt = IPU_PIX_FMT_RGB24,     .mode_str = "1920x1080M@60",     .default_bpp = 32,     .int_clk = false,     .late_init = false,     },     {     .disp_dev = "lcd",     .interface_pix_fmt = IPU_PIX_FMT_RGB24,     .mode_str = "1920x1080",     .default_bpp = 32,     .int_clk = false,     }, }; (3) Settings about IPUs /* HDMI -- IPU1_DI0 */ static struct fsl_mxc_hdmi_core_platform_data hdmi_core_data = {     .ipu_id = 1,     .disp_id = 1, }; /* RGB24 DISP0 LCD(Here is RGB24-->VGA via ADV7125 -- IPU0_DI0 */ static struct fsl_mxc_lcd_platform_data lcdif_data = {     .ipu_id = 0,     .disp_id = 0,     .default_ifmt = IPU_PIX_FMT_RGB24, }; (4) Adding LCD data in board_init() funtion static void __init mx6_qcorein_board_init(void) { .... imx6q_add_lcdif(&lcdif_data); ... } (5) Adding mxc_lcd.c driver to linux kernel When using make menuconfig to configure kernel, don't forget to add LCD driver to kernel.  Note: If users are using other version of android BSP, she can do porting according to above thinking. Weidong Sun NXP TIC team
View full article
First upload the U-Boot firmware using Network (Transferring file over network) or Serial (Transferring file over serial) This is a common serial transfer output: => loady ## Ready for binary (ymodem) download to 0xa0800000 at 115200 bps... CCmode, 1359(SOH)/0(STX)/0(CAN) packets, 9 retries ## Total Size      = 0x0002a388 = 172936 Bytes Unprotect the bootloader flash area: protect off C0000000 C003FFFF Erase the flash blocks: erase C0000000 C003FFFF Copy from RAM to Flash: If firmware has been thansfered over serial: cp.b A0800000 C0000000 2a388 If firmware has been transfered over tftp: cp.b 100000 C0000000 2a388 Installing U-Boot using BDI3000 You can use a BDI2000/3000 to write to the S71WS256 pSRAM: Get this config file. Thanks to the folks at Ultimate Solutions for being such a nice people and writing an almost ready file! Edit the [FLASH] section to this: [FLASH] CHIPTYPE              S29M32X16 CHIPSIZE                0x2000000 BUSWIDTH             16 FILE                        /home/lsantos/work/i.mx27/u-boot/u-boot-v2/uboot.bin ; change to you path FORMAT                 BIN 0xC0000000 ERASE                   0xC0000000 ERASE                   0xC0008000 ERASE                   0xC0018000 ERASE                   0xC0010000 ERASE                   0xC0020000 Don't forget to edit the [HOST] section to your machine's IP address. Telnet to the BDI - CONFIG: loading configuration file passed - CONFIG: loading register definition passed - TARGET: processing reset request - TARGET: BDI asserts TRST and RESET - TARGET: BDI removes TRST - TARGET: Bypass check 0x00000001 => 0x00000002 - TARGET: JTAG exists check passed - Core#0: ID code is 0x07926121 - TARGET: All ICEBreaker access checks passed - TARGET: BDI removes RESET - TARGET: BDI waits for RESET inactive - TARGET: resetting target passed - TARGET: processing target startup .... - TARGET: processing target startup passed Erase the first 128 KiB ADS>erase Erasing flash at 0xc0000000 Erasing flash at 0xc0008000 Erasing flash at 0xc0018000 Erasing flash at 0xc0010000 Erasing flash at 0xc0020000 Erasing flash passed Write the flash ADS>prog Programming /home/lsantos/work/i.mx27/u-boot/u-boot-v2/uboot.bin , please wait .... Programming flash passed Check everything went really well ADS>verify Verifying /home/lsantos/work/i.mx27/u-boot/u-boot-v2/uboot.bin , please wait .... Verifying target memory passed Now you can unplug the BDI and reset the board U-Boot 2.0.0-rc9-00136-gbf725a2-dirty (Jun 17 2009 - 15:45:23)  Board: Freescale i.MX27 ADS cfi_probe: cfi_flash base: 0xc0000000 size: 0x02000000  chip id: [2,882,1,01d] mpll:     265999329 Hz spll:     239999725 Hz arm:      177332886 Hz perclk1:    8866644 Hz perclk2:   17733288 Hz perclk3:   44333221 Hz perclk4:   17733288 Hz clkin26:   26000000 Hz ahb:       44333221 Hz ipg:       22166610 Hz Malloc space: 0xa7b00000 -> 0xa7f00000 (size  4 MB) Stack space : 0xa7af8000 -> 0xa7b00000 (size 32 kB) envfs: wrong magic on /dev/env0 no valid environment found on /dev/env0. Using default environment running /env/bin/init...  Hit any key to stop autoboot:  2  type update_kernel [<imagename>] to update kernel into flash type udate_root [<imagename>] to update rootfs into flash  uboot:/ Of course, this setup works with Redboot, just change the FILE entry at the [FLASH] section or use the prog command: ADS>prog 0xc0000000 /home/lsantos/work/i.mx27/redboot/build/install/bin/redboot.bin BIN Programming /home/lsantos/work/i.mx27/redboot/build/install/bin/redboot.bin , please wait .... Programming flash passed ADS>verify Verifying /home/lsantos/work/i.mx27/redboot/build/install/bin/redboot.bin , please wait .... Verifying target memory passed Rebooting ++... Read from 0x07ee0000-0x07f00000 at 0xc1fe0000: . ... Read from 0x07ed3000-0x07ed4000 at 0xc1fff000: . **Warning** FLASH configuration checksum error or invalid key Use 'fconfig -i' to [re]initialize database PMIC ID: 0x0000009b [Rev: 3.3] Ethernet FEC MAC address: is not set  Board Type: ADS Clock input: 26 MHz Booting from [NOR flash]  PHY ID 22 @ 1 FEC: [ HALF_DUPLEX ] [ disconnected ] [ 10M bps ]: Ethernet eth0: MAC address 00:04:9f:00:af:7a Can't get BOOTP info for device!  RedBoot(tm) bootstrap and debug environment [ROMRAM] Non-certified release, version FSL 200749 - built 19:37:28, Jun 17 2009  Platform: MX27 ADS/EVB (Freescale i.MX27 based) PASS 2.1 [x32 SDR] Copyright (C) 2000, 2001, 2002, 2003, 2004 Red Hat, Inc.  RAM: 0x00000000-0x07f00000, [0x00025260-0x07ed1000] available FLASH: 0xc0000000 - 0xc2000000, 256 blocks of 0x00020000 bytes each. RedBoot>
View full article
There are several vulnerabilities been found recently as below: ZIMPERIUM’s report: http://jiveon.jivesoftware.com/mpss/c/7gA/PDcDAA/t.1p4/5z0zjG0pTd2TX1EnZDdFDQ/h3/hAMy2Th8Lsdoz-2BI-2B-2B4FlQpxshE-2Fm9XH3UWXhoYdrt6y4Crt0q1GUsW8pizm7YGWnxGc52SR4U4vCgooHeqoe1S9fu9dc4l1m2ew0Kz-2BSCbA-3D     They are reported as CVE-2015-1538, CVE-2015-1539, CVE-2015-3824, CVE-2015-3826, CVE-2015-3827, CVE-2015-3828 and CVE-2015-3829.   Trendmicro’s  report:http://blog.trendmicro.com/trendlabs-security-intelligence/trend-micro-discovers-vulnerability-that-renders-android-devices-silent/   All above vulnerabilities are related with stagefright’s stackoverflow, which exist all android version since JellyBean 4.2. The stagefright is the default Multimedia framework in Android’s AOSP source code.   To avoid attacking toward stagefright, it is recommended to have patches in this attach, which should be applied to myandroid/frameworks/av.   Reference: https://github.com/WhisperSystems/TextSecure/issues/381   This document was generated from the following discussion: Android vulnerability related with stagefright   Created by Hui Fang
View full article
GStreamer has a simple feature to enable tracing, allowing the developer to do basic debugging. These can be done in two ways: Adding the parameter --gst-debug=LIST to the pipeline (a pipeline is a executed gst-launch command) Prepending the environment variable GST_DEBUG=LIST' LIST is a a comma-separated argument, indicating the GStreamer elements to trace. For example, if one needs to trace the sink element      $ GST_DEBUG=*sink*:5 gst-launch playbin2 uri=file:///sample.avi or      $ gst-launch playbin2 uri=file:///sample.avi --gst-debug=*sink*:5 Both commands produces the same log. In case want to trace for than one element, so can simple add the <element>:5, for example      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi The number 5 indicates the log category, where 5 is the highest (the most verbose log you can get) and 0 produces no output (5=LOG, 4=DEBUG, 3=INFO, 2=WARN, 1=ERROR). Log can be huge in each pipeline run. One way to filter it is using the grep command. Before grepping, one needs to redirect the standard error to the standard output (GStreamer log goes always to stderr), so      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi 2>&1 | grep <filter string> In case the log needs to be shared, it is important to remove the 'color' of the log, again, one just needs to add the parameter --gst-debug-no-color or prepend the env variable GST_DEBUG_NO_COLOR=1 ----- More shell variables that GStreamer react, can be found here https://developer.gnome.org/gstreamer/0.10/gst-running.html
View full article
About this document This document describe the setup detail for Interfacing, Installing, programming (basis) and testing depth cameras with MX6QDL based boards using the Robotic Operating System (ROS). If you are not using ROS you can also install the proper drivers and compile, in your Ubuntu system as explained on document:  https://community.freescale.com/docs/DOC-330278 1. Software & Hardware requirements Supported NXP HW boards: i.MX 6QuadPlus SABRE-SD Board and Platform i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board Depth sensors tested: Microsoft Kinect, ASUS Xtion. Software:   Gcc, Ubuntu 14.04v, OpenCV, Openni, Python, ROS. 2. Installation on ROS For installation steps of ROS on iMX6 boards in your board, please follow up: https://community.freescale.com/docs/DOC-3301478 Before you can use ROS, you will need to initialize rosdep. It enables you to easily install system dependencies for source you want to compile and is required to run some core components in ROS. $ sudo rosdep init $ rosdep update There are many different libraries and tools in ROS - not all compile fully on ARM. In this case we already have installed the ROS Base, however any other packages need to be installed individually. First install the following dependencies, which will take some time and space (~1.4 GB): $ sudo apt-get install --no-install-recommends freeglut3-dev libfreenect-dev libusb-1.0-0-dev libudev-dev ros-indigo-camera-info-manager ros-indigo-dynamic-reconfigure ros-indigo-image-transport ros-indigo-image-proc ros-indigo-depth-image-proc ros-indigo-tf ros-indigo-openni-launch ros-indigo-freenect-* ros-indigo-depthimage-to-laserscan ros-indigo-image-view ros-indigo-camera-info-manager ros-indigo-dynamic-reconfigure libudev-dev doxygen graphviz openjdk-6-jdk ros-indigo-openni2-camera ros-indigo-openni2-launch ros-indigo-rqt-common-plugins ros-indigo-rqt-graph There is no any additional installation to run kinect with ROS, If you are using kinect you can pass to part 4. However the packages used to run the PrimeSense / Asus Xtion on the i.Mx6 are not available over apt yet, so they need to be compiled from source. To use OpenNI2 with ROS, we only need the shared OpenNI2 libraries and the Drivers. Clone OpenNI2 $ git clone https://github.com/OpenNI/OpenNI2 $ cd OpenNI2 Edit ThirdParty/PSCommon/BuildSystem/Platform.Arm $ nano ThirdParty/PSCommon/BuildSystem/Platform.Arm and replace CFLAGS += -march=armv7-a -mtune=cortex-a9 -mfpu=neon -mfloat-abi=softfp #-mcpu=cortex-a8 with CFLAGS += -march=armv7-a -mtune=cortex-a9 -mfpu=neon -mfloat-abi=hard Add support for pthread library: $ nano ThirdParty/PSCommon/BuildSystem/CommonCppMakefile Search the line 95 and add the code between the two lines: OUTPUT_NAME = $(EXE_NAME)                                                   # We want the executables to look for the .so's locally first:     LDFLAGS += -Wl,-rpath ./ +   ifneq ("$(OSTYPE)","Darwin") +       LDFLAGS += -lpthread +   endif     OUTPUT_COMMAND = $(CXX) -o $(OUTPUT_FILE) $(OBJ_FILES) $(LDFLAGS) endif Save the file and exit Then run make to compile the OpenNI2 drivers and libraries $ PLATFORM=Arm make ALLOW_WARNINGS=1 Once the compilation is done, run the linux install script $ cd Packaging/Linux $ sudo ./install.sh Copy libraries and includes to the system paths $ cd ../../ $ sudo cp -r Include /usr/include/openni2 $ sudo cp -r Bin/Arm-Release/OpenNI2 /usr/lib/ $ sudo cp Bin/Arm-Release/libOpenNI2.* /usr/lib/ Create a package config file $ sudo nano /usr/lib/pkgconfig/libopenni2.pc and fill it with this: prefix=/usr exec_prefix=${prefix} libdir=${exec_prefix}/lib includedir=${prefix}/include/openni2 Name: OpenNI2 Description: A general purpose driver for all OpenNI cameras. Version: 2.2.0.0 Cflags: -I${includedir} Libs: -L${libdir} -lOpenNI2 -L${libdir}/OpenNI2/Drivers -lDummyDevice -lOniFile -lPS1080.so This will enable ubuntu to find the location of the drivers, libraries and include files. To make sure it is correctly found, run $ pkg-config --modversion libopenni2 Which should give the same version as defined in the file above (2.2.0.0). Now the Xtion is ready to be used. Plug it in (if it is already, unplug it first), then run the sample program $ ./Bin/Arm-Release/SimpleRead Then create a catkin workspace as described here, and check out the following packages in the src folder of the catkin workspace: $ cd ~/catkin_ws/src $ git clone https://github.com/ros-drivers/openni2_camera $ git clone https://github.com/ros-drivers/openni2_launch $ git clone https://github.com/ros-drivers/rgbd_launch Now the ros packages checked out above to the catkin workspace can be compiled with catkin_make $ cd ~/catkin_ws $ catkin_make Once the packages are compiled, the Xtion is ready for use with ROS with 3. Testing The Installation Kinect. Open at least 3 bash terminals: Terminal 1: Run ROS $ roscore Terminal 2:  launch the Freenect $ roslaunch freenect_launch freenect.launch Terminal 3: run the image capture $ rosrun image_view image_view image:=camera/rgb/image_color or: $ rosrun image_view image_view image:=camera/rgb/image_rect_mono or: $ rosrun image_view disparity_view image:=camera/depth/disparity It will open a new terminal with the rgb points, mono  and depth images  from the Kinect. Xtion.  Terminal 1: Run ROS $ roscore Terminal 2:  launch Openni2 $ roslaun openi2_launch openni2.launch Terminal 3: you can use rqt or Rviz session to visualize the sensor e.g: $ rqt or $ rosrun rqt_graph rqt_graph In the “rqt” window select “Plugins” -> “Visualization” -> “Image View“                                                             (optional) Install PySide, in any case you get an error with python rqt graph: $ pip install PySide $ cd ~/ Note: rqt and Rviz demand a lot of i.MX GPU work, so general graphic functionality will be affected. For this case is suggested to run rviz in a remote Network ROS session. References: -       www.ros.org -     https://dobots.nl/2014/05/05/asus-xtion-using-openni2-and-ros-on-udoo/
View full article