i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
This is a hack to support programming EEPROM I2C devices for MX28 boot. See post at: Re: mx28 boot issues with SSP (SD card) *** USE AT YOUR OWN RISK ***
View full article
This document provides steps to perform the system upgrade/OTA update for Android on i.MX platforms. Compile the Android images and generate an OTA Package: source build/envsetup.sh lunch sabresd_6dq-userdebug make -j4 make otapackage You can find your OTA package in the below path: ls out/target/product/sabresd_6dq/sabresd_6dq-ota-<xxx>.zip Copy the above OTA zip package to the device in sdcard using adb push adb push out/target/product/sabresd_6dq/sabresd_6dq-ota-<xxx>.zip /sdcard Move the package from sdcard to the location: /cache/update.zip Make the directory and perform the below steps on the device: mkdir -p /cache/recovery touch /cache/recovery/command echo "--update_package=/cache/update.zip" > /cache/recovery/command reboot recovery The recovery automatically applies the command and installs this update package. Note: In this document, the setup is for the i.MX6Q SABRESD Board. So, PathName and OTA package name subject to change based on target device compilation.
View full article
current imx6 bsp, not only ltib but also yocto couldn't support subtitle. now we have two solution to support subtitle on yocto, 1)one is extract the subtitle, then draw the subtitle on the video by UI, which is supported by the imxplayer. this solution is using QT by imxplayer, so if you build yocto, should choose QT as target. basicly, aiurdemux send the text to the QT by appsink, then QT draw the text on the UI layer. when build the yocot, pls using the command as below: " bitbake fsl-image-qt5" copy the font libary to the /usr/lib/fonts, then when you play the imxplayer, choose the font you need. 2)another one is blending the subtitle on the video buffer by gstreamer, then output with video enable gst pango lib in gstreamer1.0-plugins-base change playbin flag to disable native video flag basetextoverlay apply patch http://cgit.freedesktop.org/gstreamer/gst-plugins-base/commit/ext/pango/gstbasetextoverlay.c?id=267a8c24af4f02ba6f3075bd589d3c5d1dc826e9 use following command line gst-launch-1.0 playbin flags=0x17 uri=file://$VIDEO_FILE suburi=file://$SUBTITLE_FILE
View full article
Platform: i.MX8QXP/8QM OS: Linux Supported Camera Modules: Max9286 + Max9271 + OV10635, Default BSP Max9286 + Max96705 + AR0144, patch Max9286 + Max96705 + OV9284, patch Max9286 + Max96705 + AP0101 + AR0132, patch NVP6324 + NVP2431 + IMX225, patch TP2855 + TP3812 + IMX307, patch ISL7998x + NTSC/PAL Sensor, patch adv7180 + NTSC/PAL Sensor, patch Detailed description in the attachment.
View full article
This is an example of QR code encoding using i.MX28. The encoded QR image can show on the LCD display directly using frame buffer and the image saved as a BMP file. Board : i.MX28EVK BSP : L2.6.35_1.1.0_130130_source QR Code Lib:  qrencode-3.4.4.tar.gz Download from https://fukuchi.org/works/qrencode/ Libqrencode is a C library for encoding data in a QR Code symbol. This library is a free software made by Kentaro Fukuchi. Build the QR Code Lib source code into rootfs. 1. Create a new folder in <ltib>/dist/lfs-5.1/.     e.g. <ltib>/dist/lfs-5.1/qrencode 2. Copy the qrencode.spec to this new created folder 3. Build the source code    ./ltib –p qrencode.spec –m prep    ./ltib –p qrencode.spec –m scbuild    ./ltib –p qrencode.spec –m scdeploy Create and build the application in unit_test: - I use the existing unit_test package to build my application code. 1. Extract the source code of unit_test    ./ltib –p imx-test –m prep 2. cd <ltib>/rpm/BUILD/imx-test-2.6.35.3-1.1.0/test 3. mkdir qr_test 4. copy the Makefile and qr_test.c to qr_test folder 5. Build the unit_test     ./ltib –p imx-test  –m scbuild     ./ltib –p imx-test  –m scdeploy After built the code successfully, the qr_test.out will be generated in the unit_test folder. I start the board with NFS, so I can run the qr_test.out on the board directly. The command is : ./qr_test.out   (the default QR encode text is “http://www.freescale.com”) Or input the new text like this : ./qr_test.out –t https://community.freescale.com/community/imx The QR code  show on the display: And the BMP files will be generated in the unit_test folder.
View full article
Installing U-Boot on i.MX51EVK using BDI3000 Unlike older i.MX processor you don't need to select CONFIG_SKIP_LOWLEVEL_INIT because U-Boot lowlevel for i.MX51 doesn't reconfigure RAM memory. It is configured on DCD table. Copy u-boot.bin to /tftpboot because BDI3000 will load it from there. Connect the serial console cable on your i.MX51EVK board and connect to it using minicom. Connect to your BDI3000 through telnet and execute these commands: FSL-iMX51> load 0x97800000 u-boot.bin Loading u-boot.bin , please wait .... Loading program file passed FSL-iMX51> rm pc 0x97800000 FSL-iMX51> go When you execute the last command (“go”) you will see U-Boot starting on serial console.
View full article
The resource management service offers the possibility to divide the system into groups of resources or partitions. Resources within a partition can not access resources outside of it's partition. Partitioning a system is useful to isolate resources from one another, this gives you the ability to have for instance FreeRTOS and Linux each running simultaneously with its own set of resources. In the FreeRTOS/Linux example you could partition/divide the system into two groups/partitions where all resources/peripherals needed by FreeRTOS would be completely isolated from the resources needed by Linux, if any of the resources on the Linux partition tried to access a resource on the FreeRTOS partition the transaction would result in a bus error, as if the resource tried to access a region outside of its memory map. The partitioning mechanism is enforced by hardware and the configuration of the underlying hardware is completely abstracted by the SCFW API. The system partitioning can be performed in two ways: At boot time by modifying the function board_system_config on the board.c portion of the SCFW porting kit that corresponds to your board. This is used for software that is loaded as part of the boot process. At run time by calling the resource management service functions available. This is used to partition software that is launched by an operating system, e.g. an M4 used as sensor fusion and loaded/started by Linux. A partition can have: Resources (peripherals) Pads Memory regions All of the items mentioned above can be grouped within a partition. It is important to note that: At boot time all resources are grouped into a single partition. Resources can only be assigned to another partition by a resource within it's own partition.  Initial partitioning state of the system At boot time the system is initially configured in three partitions: The first partition (SCFW) contains all the resources, pads and memory required by the System Controller Unit (SCU) to execute the System Controller Firmware. The second partition (SECO) contains all the resources required by the Security Controller to execute. The third partition (Boot) contains all of the remaining resources, pads and memory available for the whole system. Once Linux and the M4 boot a typical use case is to partition the system as follows: In this case the boot partition is split into the ATF/Linux partition and the M4 partition. The ARM Trusted Firmware environment add a layer of abstraction to secure the environment and it is assigned cores and memory to execute in this privileged state, all the remaining resources, pads and memory are assigned to the Linux partition. The M4 partition contains all the resources required by the M4 to execute, as well as the resources required by the application running on the M4. Resource partitioning - Boot time configuration The SCFW porting kit provides an example on doing boot time configuration at the board.c file under platform/board/mx8q<x or m>_<your board>/board.c, board_system_config is the function in charge of partitioning the system at boot time. From the sc_fw_port.pdf (porting guide) document included in the porting kit - Boot Flags chapter: Here are a few important points to highlight: The code will only execute if the SC_BD_FLAGS_ALT_CONFIG is set under the boot flags (more details in the Usage chapter of the sc_fw_port.pdf), the flags are set while building the image with mkimage. An example is provided to build an image with partitioning enabled: flash_linux_m4: $(MKIMG) mx8qx-ahab-container.img scfw_tcm.bin u-boot-atf.bin m4_image.bin ./$(MKIMG) -soc QX -rev B0 -append mx8qx-ahab-container.img -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a35 0x80000000 -p3 -m4 m4_image.bin 0 0x34FE0000 -out flash.bin‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The example above can be found under your i.MX8 variant on the soc.mak file, in the example above the SC_BD_FLAGS_ALT_CONFIG flag is being set by -flags 0x00200000 and the partition for the M4 is defined as the third one by the -p3 parameter. Without the -flags 0x00200000 (setting SC_BD_FLAGS_ALT_CONFIG) parameter on mkimage NO partition happens at boot time, if the target used to build the image does not set this flag, then the SCU does not partition the system. On the board.c file the code in charge of checking for this flag is the following: /* Configure initial resource allocation (note additional allocation and assignments can be made by the SCFW clients at run-time */ if (alt_config != SC_FALSE) {‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ if the alt_config flag is not set, then the partitioning is skipped. The function rm_dump(pt_boot); dumps the partitioning state of the whole system, it can be called before and after the partitioning to make sure the device was partitioned as expected. Here is how a partition dump looks like: *** Partitions ********************************** Partition: 0 Parent: 0 DID: 2 Flags: Used Secure Isolated Partition: 1 Parent: 0 DID: 0 Flags: Used Isolated Partition: 2 Parent: 0 DID: 1 Flags: Used Secure Restricted Isolated *** Resources *********************************** Partition: 0 SC_PID0 SC_SEMA42 SC_TPM SC_PIT SC_UART ... Continues .... DBLOGIC DRC_0 DRC_1 Partition: 1 SC_PID1 SC_PID2 SC_PID3 SC_PID4 ... Continues .... BOARD_R5 BOARD_R6 BOARD_R7 Partition: 2 SECO CAAM_JR1 CAAM_JR1_OUT *** Memory Regions ****************************** Partition: 0 000: 0x030FE0000 - 0x03101FFFF Partition: 1 001: 0x000000000 - 0x01BFFFFFF 002: 0x034000000 - 0x037FFFFFF 003: 0x038000000 - 0x03BFFFFFF 004: 0x060000000 - 0x06FFFFFFF 005: 0x070000000 - 0x07FFFFFFF 006: 0x080000000 - 0x0FFFFFFFF 007: 0x400000000 - 0x43FFFFFFF 008: 0x880000000 - 0xFFFFFFFFF Partition: 2 *** Pads **************************************** Partition: 0 M40_I2C0_SCL M40_I2C0_SDA ... Continues .... SCU_BOOT_MODE4 SCU_BOOT_MODE5 Partition: 1 SIM0_CLK SIM0_RST SIM0_IO ... Continues .... ENET1_RGMII_RXD2 ENET1_RGMII_RXD3 COMP_CTL_GPIO_1V8_3V3_ENET_ENETA Partition: 2‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The dump contains the configuration of the partition, for instance: *** Partitions ********************************** Partition: 0 Parent: 0 DID: 2 Flags: Used Secure Isolated‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ On the example above the Partition parent is partition 0 (itself, this is the System Controller partition, all partitions spawn from this one). The Domain ID (DID) is 2, this ID is used to identify the partition by the hardware, it is used to enforce hardware isolation. It is also a secure and isolated partition, the meaning of these flags can be found below and in the sc_fw document: Secure - boolean indicating if this partition should be secure; only valid if caller is secure Isolated - boolean indicating if this partition should be HW isolated; set SC_TRUE if new DID is desired Restricted - boolean indicating if this partition should be restricted; set SC_TRUE if masters in this partition cannot create new partitions Grant - boolean indicating if this partition should always grant access and control to the parent Coherent - boolean indicating if this partition is coherent; set SC_TRUE if only this partition will contain both AP clusters and they will be coherent via the CCI The rest of the sections of the dump highlight all the resources, pads and memory regions enclosed in each partition. For more details on the definition of all the API calls please refer to the respective sc_fw_api document for each SoC variant. Resource partitioning - Run time configuration  The run time partitioning doesn't differ from the example provided on the porting kit, that example can be used as a base to create a partition at run time by calling the SCFW API.  Examples The following examples will show how to modify the default partition configuration on the evaluation boards, i.MX8QM MEK will be used as a reference. With BSP 4.14.98_2.3.0, the porting kit can be obtained from i.MX Software and Development Tools | NXP . Default configuration without partitioning First we will dump the default configuration without partition, e.g. without setting the ALT_CONFIG flag, most mkimage targets with a single image are configured this way, see the soc.mak and related files under scripts: soc.mak\iMX8QM - imx-mkimage - i.MX Mkimage Bootloader Tool  For details on how to create a bootable image see i.MX8 Boot process and creating a bootable image  We can see that the targets flash and flash_spl do not set any flags on the image, therefore no partition of the system will occur at boot time. flash: $(MKIMG) $(AHAB_IMG) scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append $(AHAB_IMG) -c -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍‍‍ We will build the SCFW with the Debug Monitor enabled in order to be able to dump the partitions: make qm R=B0 B=mek M=1‍‍‍‍ Now we copy the SCFW binary we just build (scfw_tcm.bin under build_mx8qm_b0) to the mkimage iMX8QM folder, along with the SECO FW, ATF (bl31.bin) and u-boot. On mkimage the flash target will be used to create a bootable image with the SCFW we just build: make SOC=iMX8QM flash‍‍‍‍‍ Flash the image to your sd card sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 sync‍‍‍‍‍‍‍‍ The MEK has two serial ports, the first one (usually ttyUSB0) is used by the A cores (u-boot/Linux in this case), the second one is used by one of the M4 cores OR the SCFW, in this case it will be used by the SCFW.  Unfortunately there aren't enough serial ports on the MEK board to allow a dedicated port for SCU, M4 cores and A cores, so in order to use the Debug Monitor on the MEK the SCFW has to take over the M4_0 UART terminal. On the SCFW Debug monitor terminal type "dump rm" this will dump all the partition information, the full log is attached to this document (imx8qm_mek_no_partition.txt). On this log it can be seen that 4 partitions are created: Partition 0 --> SCFW Partition 1 --> ATF Partition 2 --> SECO Partition 3 --> U-boot/Linux/M4 cores/Rest of the system The ATF partition is created at run time by the ATF to run in its secure state, no extra partition is created at boot time, if an image without ATF where to be used only three partitions would be seen: Partition 0 --> SCFW Partition 1 --> U-boot/Linux/M4 cores/Rest of the system Partition 2 --> SECO Default configuration with partitioning enabled Now we will create an image with the SC_BD_FLAGS_ALT_CONFIG flag set, so that partitioning occurs at boot time, for demonstration purpose we will use the same target previously used but we will modify it to set the ALT_CONFIG flag, so on mkimage modify the flash target as follows: On iMX8QM/soc.mak flash: $(MKIMG) $(AHAB_IMG) scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append $(AHAB_IMG) -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍ After the modification build the image again make clean make SOC=iMX8QM flash‍‍‍‍ On mkimage's output you should be able to see: FLAG: 0x00200000 Note how the same SCFW is used as in the previous example, same for ATF, SECO, U-boot the only required change in this case is to enable the ALT_CONFIG flag in the image. Flash the sd card with the new image sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 ‍‍‍ Dumping again the partitioning on the Debug monitor shows how the system now created additional partitions for the M4 cores and a shared partition: Partition 0 --> SCFW Partition 1 --> ATF (Created at run time by the ARM Trusted Firmware) Partition 2 --> SECO Partition 3 --> M4_0 Partition 4 --> M4_1 Partition 5 --> Shared partition Partition 6 --> U-boot/Linux/rest of the system The full log is attached as well. Modifying default configuration Now we will modify the default SCFW configuration to move some resources/pads from the M4 partition to the A cores partition (u-boot/Linux). All FlexCAN resources and pads will be moved from the M4 partition to the A core partition. From sc_fw_api_qm_b0.pdf Resource List: From sc_fw_api_qm_b0.pdf Pad List: Not all resources are available on all variants, for details on what resources/pads are available on your device please refer to its respective api document. Go back to the SCFW porting kit and open platform/board/mx8qm_mek/board.c, go to the definition of board_system_config which is the function where partitioning occurs. The code first verifies if the alt_config flag is set, and if not it skips partitioning, so all partitioning happens within the following if statement: /* Configure initial resource allocation (note additional allocation and assignments can be made by the SCFW clients at run-time */ if (alt_config != SC_FALSE) ‍‍‍‍‍‍‍‍‍‍‍ The following partitions and memory regions are declared within this if statement: sc_rm_pt_t pt_m4_0; sc_rm_pt_t pt_m4_1; sc_rm_mr_t mr_m4_0, mr_m4_1; sc_rm_pt_t pt_sh; sc_rm_mr_t mr_sh;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ pt_m4_0 is the partition for the M4_0 core, its memory region is declared as mr_m4_0. Likewise for the M4_1 pt_m4_1 and mr_m4_1 are the partitions and memory regions assigned to the M4. pt_sh and mr_sh are the shared partition and memory region. A shared partition is created but it can only have a shared memory region. Pads and resources CANNOT BE SHARED there is no mechanism to protect the pads and resources from contention, if access to a resource is required by multiple partitions a virtual resource needs to be created, in this way the partition that requires access asks the partition that owns the resource to configure/use the resource on its behalf. See the VIRT_I2C example on the Linux BSP. The partition that hosts all remaining resources is the pt_boot partition, this can be seen as the A cores partition, all resources and memory regions not assigned to the M4 partitions will be left on the pt_boot partition where the A cores are. The code is documented well and self-explanatory, for instance the following line marks all resources within the M4_0 subsystem to be moved to the M4_0 partition: /* Mark all M4_0 subsystem resources as movable */ BRD_ERR(rm_set_subsys_rsrc_movable(pt_boot, SC_R_M4_0_PID0, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_M40_I2C0_SCL, SC_P_M40_GPIO0_01, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The resource list in the sc_fw_api_qm_b0.pdf document shows what resources belong to the M4 subsystem: Next some other resources required by the M4 are assigned to its partition, such as MUs used to communicate with the other cores, timers and the IRQ steer resource. In this case we are interested on having the FlexCAN resources/pads on the A cores side, these resources/pads are being assigned to the M4_1 partition as can be seen on the previous partitions dumps and the following code: /* Move some resources not in the M4_1 subsystem */ BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_IRQSTR_M4_1, SC_R_IRQSTR_M4_1, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_UART_2, SC_R_UART_2, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_UART0_CTS_B, SC_P_UART0_RTS_B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_6B, SC_R_MU_6B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_7B, SC_R_MU_7B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_9B, SC_R_MU_9B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_GPT_3, SC_R_GPT_3, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_FSPI_0, SC_R_FSPI_0, SC_TRUE)); /* Move some pads not in the M4_1 subsystem */ BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_FLEXCAN0_RX, SC_P_FLEXCAN2_TX, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_QSPI0A_DATA0, SC_P_COMP_CTL_GPIO_1V8_3V3_QSPI0, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Previous dump: *** Resources *********************************** Partition: 4 M4_1_PID0 UART_2 CAN_0 CAN_1 CAN_2 IRQSTR_M4_1 *** Pads **************************************** Partition: 4 M41_I2C0_SCL M41_I2C0_SDA M41_GPIO0_00 M41_GPIO0_01 UART0_RTS_B UART0_CTS_B FLEXCAN0_RX FLEXCAN0_TX FLEXCAN1_RX FLEXCAN1_TX FLEXCAN2_RX FLEXCAN2_TX So we just need to remove the following lines from the board.c: BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_FLEXCAN0_RX, SC_P_FLEXCAN2_TX, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ That way the resources/pads won't be marked to be moved to the M4_1 partition and they will be left on the pt_boot partition (A core partition). If a resource needs to be added to the M4 partition just add the calls to rm_set_resource_movable to assign it. Now we just need to rebuild the scfw and our image: make qm R=B0 B=mek M=1‍‍‍‍‍ Then on mkimage (with the flags set modification above): make SOC=iMX8QM flash‍‍‍‍ Flash the sd card with the new image: sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 ‍‍‍ Now when the dump is done we can see that the FlexCAN resources and pads belong to the same partition as the A cores (partition 6). *** Resources *********************************** Partition: 6 FTM_1 CAN_0 CAN_1 CAN_2 DMA_1_CH0 *** Pads **************************************** Partition: 6 COMP_CTL_GPIO_1V8_3V3_GPIOLHT FLEXCAN0_RX FLEXCAN0_TX FLEXCAN1_RX FLEXCAN1_TX FLEXCAN2_RX FLEXCAN2_TX COMP_CTL_GPIO_1V8_3V3_GPIOTHR The device tree would still need to be modified to configure the pads and FlexCAN resources. System Controller Firmware 101 
View full article
First download and install imx31_ads_20071008-rel5b-ltib.iso. Download and extract u-boot-1.3.3.tar.bz2. Place toolchain on PATH: $ export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" Export the CROSS_COMPILE name to U-Boot $ export CROSS_COMPILE=arm-none-linux-gnueabi- Enter in the u-boot-1.3.3 directory. Create configuration to i.MX31ADS board: $ make mx31ads_config Compile U-Boot to selected board: $ make If compilation goes fine you will see the u-boot.bin on current directory.
View full article
Ridgerun SDK for iMX6 based boards now supports the X11 protocol. The server-client based protocol is now supported by our professional SDK using hardware floating point which enables a high performance and provides all the advantages that comes with X.  In the RidgeRun SDK you'll also find complete integration of Qt4.8.5 using an X-based windowing system. We currently support Matchbox and Enlightenment which is a complete desktop environment. Contact RidgeRun for more details at : [email protected] or Please Click -> Contact Us RidgeRun Home Page : www.ridgerun.com RidgeRun iMX6 based solutions : iMX6 Based Solutions
View full article
Hi team, My customer is facing the issue of unexpected behavior of i.MX6Q SSI. The customer uses SSI as slave/Network mode. And they want to transfer 4 time-slot data. As for the register setting, RFEN0, RFEN1 and RDMAE is set to 1. And only first time slot data is transferred. Do you have any ideas about the cause of this? Thanks, Miyamoto This document was generated from the following discussion: 
View full article
i.MX31 - 3 Stack There are two boot modes for IMX31PDK. In Internal Boot mode, the processor will execute an address from internal memory, and in External Boot mode the processor will execute an address from a external memory properly configured. This modes can be configured setting the values of dip switch SW5-SW10 shown in image below. Debug board. Top view. External Boot from Flash In this mode, the processor will execute an address into a external flash (NAND). If there is a bootloader saved in the right place in flash, it will be executed and the system will start. If there are a kernel image and a root file system saved configured, the operational system will start. The values for the IMX31PDK dip switches programming the boot sequence are show in table below. SW5 SW6 SW7 SW8 SW9 SW10 Internal Boot (programming flash) 0 0 0 0 0 0 External Boot from Flash 0 1 0 0 0 0 Internal Boot The Internal Boot mode enables ATK to communicate with processor and perform the writing of images into flash (bootloader image, kernel image and root file system image).
View full article
This document describes the steps for flashing eMMC from SD Card on i.MX6Q SabreSD board. Download the prebuilt images (Linux 4.1.15) of i.MX6Q SabreSD board from this link. Flash the sdcard image on SD Card. sudo dd if=<sdcard_image> of=/dev/sdX bs=1M && sync Select Boot Mode to SD Card and boot the board from SD Card. Stop the console at u-boot and execute below command. ums 0 mmc 1                 // this will mount SD card as USB Mass Storage to your system Copy bootloader image from system to USB Mass Storage cp <u-boot_image> /media/username/<rootfs>/home/root/ Eject the USB Mass Storage and terminate the ums process by pressing ctrl+c in u-boot. Power Off and Power On the board and login to the kernel console. Flash the bootloader image to eMMC dd if=/home/root/<u-boot_image> of=/dev/mmcblk3 bs=512 seek=2 conv=fsync Mount the partition 1 of SD Card to copy the kernel image and DTB file to /home/root folder. mount /dev/mmcblk2p1 /mnt/ cp -r /mnt/zImage /mnt/imx6q-sabresd.dtb /home/root umount /dev/mmcblk2p1 Make partitions on eMMC manually as per section 4.3.3 in this document using fdisk /dev/mmcblk3 command. Format the partition 1 on eMMC as VFAT and partition 2 as ext4 with below commands mkfs.vfat /dev/mmcblk3p1 mkfs.ext4 /dev/mmcblk3p2 Mount the partion 1 of eMMC and copy kernel image & DTB file. mount /dev/mmcblk3p1 /mnt/ cp -r /home/root/zImage /home/root/imx6q-sabresd.dtb /mnt/ umount /dev/mmcblk3p1 Mount the partion 2 of eMMC & SD Card and copy the file system. mount /dev/mmcblk3p2 /mnt/                                                         // mount partition 2 of SD Card mkdir /home/root/rootfs && mount /dev/mmcblk3p2 rootfs     // mount partition 2 of eMMC cp -ar /mnt/* /home/root/rootfs/ sync umount /dev/mmcblk2p2 umount /dev/mmcblk3p2 Change the Boot Mode to eMMC Power Up the Board. (this will boot the images from eMMC) NOTE: Above steps does not require any other images for eMMC. All the images for eMMC and SD Card are same. Regards, Shivani
View full article
Question: Using Linux SDK 4.1.0, with CAAM drivers enabled, there is little noticeable difference in the performance of openssd compared to a kernel without the CAAM drivers. Tests were done using openssd. Test image AES-128 8192 byte block (M Bytes/sec) “openssl speed –evp aes-128-cbc” AES-128 8192 byte block (M Bytes/sec) With /dev/crypto “openssl speed –evp aes-128-cbc -engine cryptodev”  Ubuntu 11.04 Image 19.010 N/A Timesys 20.518 N/A SDK 4.1.0 LTIB 22.013 21.984 (errors reported) One can see that with SDK 4.1.0, performance is worse with crypto enabled.  This is probably due to the overhead of a faulty driver or incorrect implementation. The lowest number is for Ubuntu which could be attributed to the Unity GUI. Conclusion:  CAAM driver is not functional or I am using an improper testing procedure. Test Procedure: Board used is iMX6Q Sabre SDP Openssl was used for testing. Two command line commands were used, with and without the cryptodev engine. openssl speed –evp aes-128-cbc openssl speed –evp aes-128-cbc -engine cryptodev Openssl versions used in each build are slightly different: Ubuntu:              openssl 1.0.0e Timesys:              openssl  1.0.1e SDK 4.1.0:            openssl  1.0.1c Three versions of Linux were tested. Default kernel  4.0.0 with Ubuntu rootfs form image tarballs. Timesys kernel and root file system Kernel built with SDK 4.1.0 using LTIB with hardware crypto enabled Both 1 and 2 above did not have CRYPTODEV set in .config which contains the line “# CONFIG_CRYPTO_CRYPTODEV is not set” Option 3 had the line in .config as, “CONFIG_CRYPTO_CRYPTODEV=y” All three builds generate “/proc/crypto”  whose contents are attached.  A partial listing of /proc/crypto lists “caam” as a driver for all encryption methods supported.  Example printout for aes shown below: ame         : cbc(aes) driver       : cbc-aes-caam module       : kernel priority     : 3000 refcnt       : 1 selftest     : passed type         : ablkcipher async        : yes blocksize    : 16 min keysize  : 16 max keysize  : 32 ivsize       : 16 geniv        : eseqiv All three builds have “caam” and “enable_wait_mode=off” in the kernel command line in u-boot. Only option #3 contains both device file in “/dev/crypto” and an entry in “/proc/crypto” root@freescale ~$ cd / root@freescale /$ ls /proc/cr* /proc/crypto root@freescale /$ ls /dev/cr* /dev/crypto root@freescale /$ Test #1—Kernel build 4.1.0 openssl speed test without caam engine root@freescale ~$ openssl speed -evp aes-128-cbc                    Doing aes-128-cbc for 3s on 16 size blocks: 3471184 aes-128-cbc's in 2.94s Doing aes-128-cbc for 3s on 64 size blocks: 986286 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 256 size blocks: 249743 aes-128-cbc's in 2.93s Doing aes-128-cbc for 3s on 1024 size blocks: 64343 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 8192 size blocks: 7954 aes-128-cbc's in 2.96s OpenSSL 1.0.1c 10 May 2012 built on: Sat Sep 7 18:47:34 PDT 2013 options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) idea(int) blowfish(ptr) compiler: gcc -fPIC -DOPENSSL_PIC -DOPENSSL_THREADS -D_REENTRANT -DDSO_DLFCN -DHAVE_DLFCN_H -DL_ENDIAN -DTERMIO -O3 -fomit-frame-pointer -Wall The 'numbers' are in 1000s of bytes per second processed. type 16 bytes     64 bytes    256 bytes 1024 bytes   8192 bytes aes-128-cbc 18890.80k    21040.77k    21820.55k 21962.41k    22013.23k root@freescale ~$ Test #2—Timesys kernel build of openssd without /dev/crypto # openssl speed -evp aes-128-cbc Doing aes-128-cbc for 3s on 16 size blocks: 3361305 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 64 size blocks: 924423 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 256 size blocks: 236623 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 1024 size blocks: 59967 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 8192 size blocks: 7514 aes-128-cbc's in 3.00s OpenSSL 1.0.1e 11 Feb 2013 built on: Thu Sep 5 21:54:37 EDT 2013 options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) blowfish(ptr) compiler: armv7l-timesys-linux-gnueabi-gcc -fPIC -DOPENSSL_PIC -DOPENSSL_THREADS -D_REENTRANT -DDSO_DLFCN -DHAVE_DLFCN_H -I/here/workdir/factory/build_armv7l-times ys-linux-gnueabi/toolchain/usr/include -DL_ENDIAN -DTERMIO -DOPENSSL_NO_KRB5 -DOPENSSL_NO_IDEA -DOPENSSL_NO_MDC2 -DOPENSSL_NO_RC5 -Os -pipe -Wa,--noexecstack -Wall The 'numbers' are in 1000s of bytes per second processed. type 16 bytes     64 bytes    256 bytes 1024 bytes   8192 bytes aes-128-cbc 17926.96k    19721.02k    20191.83k 20468.74k    20518.23k #  Test #3—Ubuntu rootfs and kernel image root@linaro-ubuntu-desktop:/# openssl speed -evp aes-128-cbc Doing aes-128-cbc for 3s on 16 size blocks: 3030128 aes-128-cbc's in 2.98s Doing aes-128-cbc for 3s on 64 size blocks: 852897 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 256 size blocks: 220572 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 1024 size blocks: 55534 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 8192 size blocks: 6846 aes-128-cbc's in 2.95s OpenSSL 1.0.0e 6 Sep 2011 built on: Wed Oct 5 01:45:02 UTC 2011 options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) blowfish(ptr) compiler: cc -fPIC -DOPENSSL_PIC -DZLIB -DOPENSSL_THREADS -D_REENTRANT -DDSO_DLFCN -DHAVE_DLFCN_H -DL_ENDIAN -DTERMIO -O2 -Wa,--noexecstack -g -Wall The 'numbers' are in 1000s of bytes per second processed. type             16 bytes     64 bytes 256 bytes   1024 bytes   8192 bytes aes-128-cbc 16269.14k    18195.14k    18822.14k 18955.61k    19010.99k root@linaro-ubuntu-desktop:/# Test #4—SDK 4.1.0 openssl speed test with “/dev/crypto” .  Note errors. root@freescale ~$ openssl speed -evp aes-128-cbc -engine cryptodev  invalid engine "cryptodev" 716715216:error:25066067:DSO support routines:DLFCN_LOAD:could not load the shared library:dso_dlfcn.c:187:filename(/usr/lib/engines/libcryptodev.so): /usr/lib/eng ines/libcryptodev.so: cannot open shared object file: No such file or directory 716715216:error:25070067:DSO support routines:DSO_load:could not load the shared library:dso_lib.c:244: 716715216:error:260B6084:engine routines:DYNAMIC_LOAD:dso not found:eng_dyn.c:450: 716715216:error:2606A074:engine routines:ENGINE_by_id:no such engine:eng_list.c:417:id=cryptodev 716715216:error:25066067:DSO support routines:DLFCN_LOAD:could not load the shared library:dso_dlfcn.c:187:filename(libcryptodev.so): libcryptodev.so: cannot open shared object file: No such file or directory 716715216:error:25070067:DSO support routines:DSO_load:could not load the shared library:dso_lib.c:244: 716715216:error:260B6084:engine routines:DYNAMIC_LOAD:dso not found:eng_dyn.c:450: Doing aes-128-cbc for 3s on 16 size blocks: 3572980 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 64 size blocks: 966002 aes-128-cbc's in 2.94s Doing aes-128-cbc for 3s on 256 size blocks: 255307 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 1024 size blocks: 62967 aes-128-cbc's in 2.93s Doing aes-128-cbc for 3s on 8192 size blocks: 7890 aes-128-cbc's in 2.94s OpenSSL 1.0.1c 10 May 2012 built on: Sat Sep 7 18:47:34 PDT 2013 options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) idea(int) blowfish(ptr) compiler: gcc -fPIC -DOPENSSL_PIC -DOPENSSL_THREADS -D_REENTRANT -DDSO_DLFCN -DHAVE_DLFCN_H -DL_ENDIAN -DTERMIO -O3 -fomit-frame-pointer -Wall The 'numbers' are in 1000s of bytes per second processed. type 16 bytes     64 bytes    256 bytes 1024 bytes   8192 bytes aes-128-cbc 19055.89k    21028.61k    21786.20k 22006.21k    21984.65k root@freescale ~$ Answer: I do not know what is recent state of official Freescale BSP regarding CAAM, but to get OpenSSL working under CAAM support with reasonable acceleration  : https://community.freescale.com/message/318188#318188 The patches was used below : http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.0.35_4.0.0 Direct link to the patches: http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_3.0.35_4.0.0&id=6068d7a77b2101c172fc2f003f90b1febbf99505 http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_3.0.35_4.0.0&id=b30237c79003223c6e8035d5be183cd4f0b469f9
View full article
   Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of University of Science and Technology of China. Preparations Installing Ubuntu16.04.2 LTS Customer can download ubuntu-16.04.2-desktop-amd64.iso from https://www.ubuntu.com/download/desktop        Then install it to VMware workstation player v12 or PC, after finishing installation, use “Software Update” to update system. In order to compile android8.0.0-1.0.0 BSP, necessary packages should also be installed on Ubuntu 16.04. $ sudo apt-get install gnupg $ sudo apt-get install flex $ sudo apt-get install bison $ sudo apt-get install gperf $ sudo apt-get install build-essential $ sudo apt-get install zip $ sudo apt-get install zlib1g-dev $ sudo apt-get install libc6-dev $ sudo apt-get install lib32ncurses5-dev   $ sudo apt-get install x11proto-core-dev $ sudo apt-get install libx11-dev $ sudo apt-get install lib32z1-dev   $ sudo apt-get install libgl1-mesa-dev $ sudo apt-get install tofrodos $ sudo apt-get install python-markdown $ sudo apt-get install libxml2-utils $ sudo apt-get install xsltproc $ sudo apt-get install uuid-dev:i386 liblzo2-dev:i386   $ sudo apt-get install gcc-multilib g++-multilib $ sudo apt-get install subversion $ sudo apt-get install openssh-server openssh-client $ sudo apt-get install uuid uuid-dev $ sudo apt-get install zlib1g-dev liblz-dev $ sudo apt-get install liblzo2-2 liblzo2-dev $ sudo apt-get install lzop $ sudo apt-get install git-core curl $ sudo apt-get install u-boot-tools $ sudo apt-get install mtd-utils $ sudo apt-get install android-tools-fsutils $ sudo apt-get install openjdk-8-jdk More detail, see Android_User’s_Guide.pdf ( android 8.0.0-1.0.0 BSP documents) Downloading and unpacking Android release package https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applications-processors/android-os-for-i.mx-applications-processors:IMXANDROID?tab=Design_Tools_Tab --IMX_O8.0.0_1.0.0_ANDROID_SOURCE File name is mx-o8.0.0_1.0.0_ga.tar.gz # cd ~ # tar xzvf mx-o8.0.0_1.0.0_ga.tar Downloading Android 8.0.0-1.0.0 source code Getting repo # cd ~ # mkdir bin # cd bin # curl https://storage-googleapis.proxy.ustclug.org/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From            REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL ='git-repo - Git at Google ' 3、Setting email address # git config --global user.email "[email protected]" # git config --global user.name "xxxx"  [ Email & Name should be yours]   4、Modifying android setup script and Running it          Open ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh and add a line like below: ......       if [ "$rc" != 0 ]; then          echo "---------------------------------------------------"          echo "-----Repo Init failure"          echo "---------------------------------------------------"          return 1       fi find -name 'aosp-O8.0.0-1.0.0.xml'| xargs perl -pi -e 's|https://android.googlesource.com/|git://mirrors.ustc.edu.cn/aosp/|g' fi   # Don't Delete .repo directory and hidden files #rm -rf $android_builddir/.??*    Then save it and exit. # cd ~/ # source ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh Then android_build directory is created at ~/ # export MY_ANDROID=~/android_build [Note] imx_android_setup.sh will be in charge of downloading all android source code. 5.Begin to compile android 8.0.0 BSP $ export ARCH=arm $ export CROSS_COMPILE=${MY_ANDROID}/prebuilts/gcc/linux-x86/arm/arm-linuxandroideabi-4.9/bin/arm-linux-androideabi- $ cd ~/android_build $ source build/envsetup.sh $ lunch sabreauto_6q-userdebug $ make –j4 Errors: ...... “Try increasing heap size with java option '-Xmx<size>'.” ...... Logs for compiling     weidong@ubuntu:~/android_build$ lunch sabreauto_6q-userdebug   ============================================ PLATFORM_VERSION_CODENAME=REL PLATFORM_VERSION=8.0.0 TARGET_PRODUCT=sabreauto_6q TARGET_BUILD_VARIANT=userdebug TARGET_BUILD_TYPE=release TARGET_PLATFORM_VERSION=OPD1 TARGET_BUILD_APPS= TARGET_ARCH=arm TARGET_ARCH_VARIANT=armv7-a-neon TARGET_CPU_VARIANT=cortex-a9 TARGET_2ND_ARCH= TARGET_2ND_ARCH_VARIANT= TARGET_2ND_CPU_VARIANT= HOST_ARCH=x86_64 HOST_2ND_ARCH=x86 HOST_OS=linux HOST_OS_EXTRA=Linux-4.4.0-116-generic-x86_64-with-Ubuntu-16.04-xenial HOST_CROSS_OS=windows HOST_CROSS_ARCH=x86 HOST_CROSS_2ND_ARCH=x86_64 HOST_BUILD_TYPE=release BUILD_ID=1.0.0-rfp-rc4 OUT_DIR=out AUX_OS_VARIANT_LIST= ============================================ weidong@ubuntu:~/android_build$ make -j4 ============================================     ============================================ PLATFORM_VERSION_CODENAME=REL PLATFORM_VERSION=8.0.0 TARGET_PRODUCT=sabreauto_6q TARGET_BUILD_VARIANT=userdebug TARGET_BUILD_TYPE=release TARGET_ARCH=arm TARGET_ARCH_VARIANT=armv7-a-neon TARGET_CPU_VARIANT=cortex-a9 HOST_ARCH=x86_64 HOST_2ND_ARCH=x86 HOST_OS=linux HOST_OS_EXTRA=Linux-4.4.0-116-generic-x86_64-with-Ubuntu-16.04-xenial HOST_CROSS_OS=windows HOST_CROSS_ARCH=x86 HOST_CROSS_2ND_ARCH=x86_64 HOST_BUILD_TYPE=release BUILD_ID=1.0.0-rfp-rc4 OUT_DIR=out ============================================ [38/38] bootstrap out/soong/.minibootstrap/build.ninja.in [1/2] out/soong/.bootstrap/bin/minibp out/soong/.minibootstrap/build.ninja.in [4/4] out/soong/.bootstrap/bin/minibp out/soong/.bootstrap/build.ninja [791/792] glob vendor/*/*/Android.bp [47/47] out/soong/.bootstrap/bin/soong_build out/soong/build.ninja out/build-sabreauto_6q.ninja is missing, regenerating... [9/1005] including ./cts/Android.mk ... cts/hostsidetests/os/test-apps/StaticSharedNativeLibProvider/Android.mk:23: warning: FindEmulator: find: `cts/hostsidetests/os/test-apps/StaticSharedNativeLibProvider/src': No such file or directory cts/hostsidetests/os/test-apps/StaticSharedNativeLibProvider1/Android.mk:23: warning: FindEmulator: find: `cts/hostsidetests/os/test-apps/StaticSharedNativeLibProvider1/src': No such file or directory [690/1005] including ./system/sepolicy/Android.mk ... ./system/sepolicy/Android.mk:107: warning: BOARD_SEPOLICY_VERS not specified, assuming current platform version [1005/1005] including ./vendor/nxp/linux-firmware-imx/firmware/Android.mk ... No private recovery resources for TARGET_DEVICE sabreauto_6q platform_testing/build/tasks/tests/instrumentation_metric_test_list.mk: warning: continuous_instrumentation_metric_tests: Unknown installed file for module perf-setup.sh platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module RecyclerViewTests platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module SettingsFunctionalTests platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module LauncherFunctionalTests platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module EmergencyInfoTests platform_testing/build/tasks/tests/native_metric_test_list.mk: warning: continuous_native_metric_tests: Unknown installed file for module perf-setup.sh test/vts/tools/build/tasks/vts_package.mk:222: warning: FindEmulator: cd: vendor/google_vts/testcases: No such file or directory test/vts/tools/build/tasks/vts_package.mk:222: warning: FindEmulator: cd: vendor/google_vts/testcases: No such file or directory test/vts/tools/build/tasks/vts_package.mk:222: warning: FindEmulator: cd: vendor/google_vts/testcases: No such file or directory ./test/vts/utils/python/archive/Android.mk:28: warning: overriding commands for target `default' ./test/vts/runners/host/tcp_server/Android.mk:19: warning: ignoring old commands for target `default' build/core/Makefile:34: warning: overriding commands for target `out/target/product/sabreauto_6q/root/init.rc' build/core/base_rules.mk:378: warning: ignoring old commands for target `out/target/product/sabreauto_6q/root/init.rc' ...... ......  CC      lib/vsprintf.o   CC      lib/panic.o   CC      lib/strto.o   CC      lib/strmhz.o   LD      lib/built-in.o   CC      examples/standalone/hello_world.o   CC      examples/standalone/stubs.o   LD      examples/standalone/libstubs.o   LD      examples/standalone/hello_world   OBJCOPY examples/standalone/hello_world.bin   OBJCOPY examples/standalone/hello_world.srec   LD      u-boot   OBJCOPY u-boot-nodtb.bin   OBJCOPY u-boot.srec   SHIPPED dts/dt.dtb   SYM     u-boot.sym   COPY    u-boot.dtb   CAT     u-boot-dtb.bin   COPY    u-boot.bin   CFGS    board/freescale/mx6qsabreauto/mx6qp.cfg.cfgtmp   MKIMAGE u-boot-dtb.imx   CFGCHK  u-boot.cfg make[1]: Leaving directory '/home/weidong/android_build/out/target/product/sabreauto_6q/obj/BOOTLOADER_OBJ' make: Leaving directory '/home/weidong/android_build/vendor/nxp-opensource/uboot-imx' /bin/bash: line 0: [: =: unary operator expected [  3% 2129/63758] Check module type: out/target/common/obj/APPS/Browser2_intermediates/link_type packages/apps/Browser2/Android.mk: warning: Browser2 (java:sdk) should not link to legacy-android-test (java:platform) [  3% 2171/63758] Ensuring Jack server is installed and started Jack server already installed in "/home/weidong/.jack-server" Launching Jack server java -XX:MaxJavaStackTraceDepth=-1 -Djava.io.tmpdir=/tmp -Dfile.encoding=UTF-8 -XX:+TieredCompilation -cp /home/weidong/.jack-server/launcher.jar com.android.jack.launcher.ServerLauncher Server updated, waiting for restart ...... ...... D [M]  drivers/rpmsg/imx_rpmsg_tty.ko   LD [M]  drivers/video/backlight/l4f00242t03.ko   CC      arch/arm/boot/compressed/misc.o   LD [M]  drivers/video/backlight/platform_lcd.ko   LD [M]  drivers/video/backlight/lcd.ko   CC      arch/arm/boot/compressed/decompress.o   CC      arch/arm/boot/compressed/string.o   SHIPPED arch/arm/boot/compressed/hyp-stub.S   SHIPPED arch/arm/boot/compressed/lib1funcs.S   SHIPPED arch/arm/boot/compressed/ashldi3.S   SHIPPED arch/arm/boot/compressed/bswapsdi2.S   AS      arch/arm/boot/compressed/hyp-stub.o   AS      arch/arm/boot/compressed/lib1funcs.o   AS      arch/arm/boot/compressed/ashldi3.o   AS      arch/arm/boot/compressed/bswapsdi2.o   AS      arch/arm/boot/compressed/piggy.o   LD      arch/arm/boot/compressed/vmlinux   OBJCOPY arch/arm/boot/zImage   Kernel: arch/arm/boot/zImage is ready make[1]: Leaving directory '/home/weidong/android_build/out/target/product/sabreauto_6q/obj/KERNEL_OBJ' make: Leaving directory '/home/weidong/android_build/vendor/nxp-opensource/kernel_imx' make: Entering directory '/home/weidong/android_build/vendor/nxp-opensource/kernel_imx' make[1]: Entering directory '/home/weidong/android_build/out/target/product/sabreauto_6q/obj/KERNEL_OBJ'   CHK     include/config/kernel.release   GEN     ./Makefile   CHK     include/generated/uapi/linux/version.h   Using /home/weidong/android_build/vendor/nxp-opensource/kernel_imx as source for kernel   CHK     include/generated/utsrelease.h   CHK     include/generated/timeconst.h   CHK     include/generated/bounds.h   CHK     include/generated/asm-offsets.h   CALL    /home/weidong/android_build/vendor/nxp-opensource/kernel_imx/scripts/checksyscalls.sh make[1]: Leaving directory '/home/weidong/android_build/out/target/product/sabreauto_6q/obj/KERNEL_OBJ' make: Leaving directory '/home/weidong/android_build/vendor/nxp-opensource/kernel_imx'   ...... ...... [ 83% 53244/63758] Building with Jack: out/target/co...ARIES/framework_intermediates/with-local/classes.dex FAILED: out/target/common/obj/JAVA_LIBRARIES/framework_intermediates/with-local/classes.dex /bin/bash out/target/common/obj/JAVA_LIBRARIES/framework_intermediates/with-local/classes.dex.rsp Out of memory error (version 1.3-rc7 'Douarn' (445000 d7be3910514558d6715ce455ce0861ae2f56925a by [email protected])). GC overhead limit exceeded. Try increasing heap size with java option '-Xmx<size>'. Warning: This may have produced partial or corrupted output. [ 83% 53247/63758] //external/llvm/lib/CodeGen/SelectionDAG:libLLVMSelectionDAG clang++ DAGCombiner.cpp ninja: build stopped: subcommand failed. 19:17:25 ninja failed with: exit status 1 build/core/main.mk:21: recipe for target 'run_soong_ui' failed make: *** [run_soong_ui] Error 1   ******************************************************* solve the issue: Try increasing heap size with java option '-Xmx<size>'. -- run commands below on command line #export JACK_SERVER_VM_ARGUMENTS="-Dfile.encoding=UTF-8 -XX:+TieredCompilation -Xmx4g" #./prebuilts/sdk/tools/jack-admin kill-server #./prebuilts/sdk/tools/jack-admin start-server ******************************************************* #make -j4   //continue compiling   ...... ...... [ 50% 1/2] glob vendor/*/*/Android.bp [  0% 1/10515] Ensuring Jack server is installed and started Jack server already installed in "/home/weidong/.jack-server" Server is already running ...... ...... Creating filesystem with parameters:     Size: 1585446912     Block size: 4096     Blocks per group: 32768     Inodes per group: 8064     Inode size: 256     Journal blocks: 6048     Label: system     Blocks: 387072     Block groups: 12     Reserved block group size: 95 Created filesystem with 2216/96768 inodes and 171147/387072 blocks Running:  build_verity_tree -A aee087a5be3b982978c923f566a94613496b417f2af592639bc80d141e34dfe7 out/target/product/sabreauto_6q/obj/PACKAGING/systemimage_intermediates/system.img /tmp/tmpPnRk1H_verity_images/verity.img f26a84a2c66d866f5322986e7a093812329d87579e5859aa32a2cf4c21f69661 aee087a5be3b982978c923f566a94613496b417f2af592639bc80d141e34dfe7 Running:  system/extras/verity/build_verity_metadata.py build 1585446912 /tmp/tmpPnRk1H_verity_images/verity_metadata.img f26a84a2c66d866f5322986e7a093812329d87579e5859aa32a2cf4c21f69661 aee087a5be3b982978c923f566a94613496b417f2af592639bc80d141e34dfe7 /dev/block/by-name/system verity_signer build/target/product/security/verity.pk8 ['verity_signer', '/tmp/tmpvXftO2.table', 'build/target/product/security/verity.pk8', '/tmp/tmpbfl4fq.sig'] appending /tmp/tmpPnRk1H_verity_images/verity_metadata.img to /tmp/tmpPnRk1H_verity_images/verity.img Running:  fec -e -p 0 out/target/product/sabreauto_6q/obj/PACKAGING/systemimage_intermediates/system.img /tmp/tmpPnRk1H_verity_images/verity.img /tmp/tmpPnRk1H_verity_images/verity_fec.img encoding RS(255, 253) to '/tmp/tmpPnRk1H_verity_images/verity_fec.img' for input files:        1: 'out/target/product/sabreauto_6q/obj/PACKAGING/systemimage_intermediates/system.img'        2: '/tmp/tmpPnRk1H_verity_images/verity.img' appending /tmp/tmpPnRk1H_verity_images/verity_fec.img to /tmp/tmpPnRk1H_verity_images/verity.img Running:  append2simg out/target/product/sabreauto_6q/obj/PACKAGING/systemimage_intermediates/system.img /tmp/tmpPnRk1H_verity_images/verity.img   [100% 10515/10515] Install system fs image: out/target/product/sabreauto_6q/system.img out/target/product/sabreauto_6q/system.img+out/target/product/sabreauto_6q/obj/PACKAGING/recovery_patch_intermediates/recovery_from_boot.p maxsize=1644331392 blocksize=4224 total=704129669 reserve=16612992   #### make completed successfully (01:21:12 (hh:mm:ss)) ####   NXP TIC team Weidong sun 2018-06-01
View full article
GTK+ GTK is a graphic library developed initially by Gimp (Gimp ToolKit). GTK was selected as default GUI to create the Gnome Desktop and currently it is used on many desktop environment (XFCE, LXDE, etc). When GTK was developed it was depending on X Server (X11) but currently it can run over DirectFB. In order to add GTK+ support on i.MX board you need first to choice DirectFB or X11 to be it's default graphic infrastructure. The following pages contain informations and instruction of how to compile and use them. If you want to compile GTK over DirectFB: All Boards DirectFB If you want to compile GTK over X11: All Boards X11 All Boards GTK Manually All Boards GTK Glade GTK Demo GTK2 package comes with "gtk-demo". It's a demo executable to demonstrate some GTK gadgets. In order to use it with DirectFB, compile the following packages using LTIB: [*] GTK2 [*] DirectFB [*]  configure for use with touchscreen [*]  DirectFB-examples "if you would like to test DirectFB" [*] Liberation fonts [*] Tslib After starting Linux on i.MX, load the following modules: mx# /etc/rc.d/init.d/gtk2 start gtk: creating gdk-pixbuf.loaders mx# /etc/rc.d/init.d/pango start pango: creating module list Execute gtk-demo: mx# /usr/bin/gtk-demo GTK Demo with X If you would like to test the gtk-demo application over X, start X first (tested on i.MX25 PDK): mx# Xfbdev -screen 480×640 -mouse tslib,,device=/dev/input/event1 & mx# export DISPLAY=:0.0 mx# /usr/bin/gtk-demo
View full article
Changing the storage for U-boot environment variables   U-Boot on Freescale BSP has a compiling option that allows you to choose the storage for environment variables.   1 - Extract the u-boot source using LTIB: ./ltib -m prep -p u-boot   2 - The source will be extracted to <ltib path>/rpm/BUILD/u-boot-2009.08   3 - On u-Boot source locate the i.MXEVK config file, <ltib path>/rpm/BUILD/u-boot-2009.08/include/configs/mx51_bbg.h   4 - To change the storage of variables environment to SD card, on this file, comment out CONFIG_FSL_ENV_IN_SF and define CONFIG_FSL_ENV_IN_MMC:   //#define CONFIG_FSL_ENV_IN_SF   #define CONFIG_FSL_ENV_IN_MMC 5 - Adjust CONFIG_ENV_SECT_SIZE and CONFIG_ENV_OFFSET accordingly. Recall that sd card read block size is 512B.   For example:   #define CONFIG_ENV_SECT_SIZE (256 * 512)   #define CONFIG_ENV_SIZE CONFIG_ENV_SECT_SIZE   #if defined(CONFIG_FSL_ENV_IN_MMC)   #define CONFIG_ENV_IS_IN_MMC 1 #define CONFIG_ENV_OFFSET (1023 * 512)   6 - Save the file.   7 - Recompile u-boot: ./ltib -m scbuild -p u-boot   8 - Your new compiled u-boot image will be saved at: <ltib path>/rpm/BUILD/u-boot-2009.08/u-boot.bin
View full article
Question: What does it means by depending on load? Is there a value? This is  related with i.MX6D Answer: The comment about the "load" means the total system load on the 2.5V rail. We understand that people design systems, not just MX6 devices. The documentation confusion stems from the design team changing from allowing customers to use the LDOs to power system devices back to just using the LDOs to power the MX6. Reasons - thermals, and also concern for uncontrolled system noise injection into the MX6 and causing failures.
View full article
One of the features that many users have asked about but still is a work in progress for android, is the extended desktop capabilities. Currently android allows you to mirror your desktop in two displays, but you are still unable to extend your desktop like you would with any other OS like Linux or Windows. This tutorial is intended to show you how to use a special object that allows you to control what should appear on a secondary or external display, replacing the screen mirroring. So how do we do this? A presentation is a container to display a user interface, in the form of a view hierarchy on an external display. This is pretty much like a Dialog since it displays its UI separated from its activity, but the difference is that the presentation shows in an external display while the dialog displays it in the primary screen. Now, because of this, the resources that are to be used by the UI on an external display are different then the resources used in the primary screen, the context of the presentation is NOT the activity. How do we choose where to send this presentation? The easiest way to do this is to use the MediaRouter API. What the mediarouter does is it keeps track of which audio and video routes are available on the system. The MediaRouter sends notifications whenever routes are selected or unselected. An application can simple watch for these notifications and show or dismiss a presentation on the preferred presentation display automatically. The preferred presentation display is the display that the mediarouter recommends that the application should use if it wants to show content on the secondary display. IF there is not a preferred presentation display, the application should show its content locally without using a presentation. Using the Mediarouter The MediaRouter is a system service obtained by calling getSystemService() and asking for the MEDIA_ROUTER_SERVICE. We should use the mediarouter to create and show a presentation on the preferred presentation display: MediaRouter mediaRouter = (MediaRouter) context.getSystemService(Context.MEDIA_ROUTER_SERVICE); MediaRouter.RouteInfo route = mediaRouter.getSelectedRoute(); if (route != null) { Display presentationDisplay = route.getPresentationDisplay(); if (presentationDisplay != null) { Presentation presentation = new MyPresentation(context, presentationDisplay); presentation.show(); } } In order to use this framework in your app, you need to get an instance of the MediaRouter framework object and attach a MediaRouter.Callback object to listen for event in available media routes. The android apps that implement the media router API need to include a Cast button to allow users to select a media route to play media on a secondary output device. The recommended way to implement the Cast button  is to extend your activity from ActionBarActivity() and use the onCreateOptionMenu() method to add an options menu. The Cast button must use the MediaRouteActionProvider class as its action: <?xml version="1.0" encoding="utf-8"?> <menu xmlns:android="http://schemas.android.com/apk/res/android" xmlns:app="http://schemas.android.com/apk/res-auto" > <item android:id="@+id/media_route_menu_item" android:title="@string/media_route_menu_title" app:actionProviderClass="android.support.v7.app.MediaRouteActionProvider" app:showAsAction="always" /> </menu> The media router framework communicates with an app through a callback object that you attach to the mediarouter framework object.  Its necessary to extend the callback object in order to receive messages when a media route is connected. Once your callback is defined for the media router,  you need to attach it to the media router object.  The following sample demonstrates how to use the lifecycle methos to appropriately add and remove your app’s media router callback object. You need to add and remove it because it needs to be free for whenever you close the app or have it in the background so other apps use it if necessary. public class MediaRouterPlaybackActivity extends ActionBarActivity { private MediaRouter mMediaRouter; private MediaRouteSelector mSelector; private Callback mMediaRouterCallback; // your app works with so the framework can discover them. @Override protected void onCreate(Bundle savedInstanceState) { super.onCreate(savedInstanceState); setContentView(R.layout.activity_main); // Get the media router service. mMediaRouter = MediaRouter.getInstance(this); ... } // Add the callback on start to tell the media router what kinds of routes // your app works with so the framework can discover them. @Override public void onStart() { mMediaRouter.addCallback(mSelector, mMediaRouterCallback, MediaRouter.CALLBACK_FLAG_REQUEST_DISCOVERY); super.onStart(); } // Remove the selector on stop to tell the media router that it no longer // needs to discover routes for your app. @Override public void onStop() { mMediaRouter.removeCallback(mMediaRouterCallback); super.onStop(); } ... } Remote playback This approach sends control commands to a secondary device to initiate playback and to control the playback that is in progress (play, stop, fast-forward, rewind, etc). When your app supports this type of media route, you must need to create a RemotePlaybackClient boject using a remote playback MediaRoute.RouteInfo object received through your app’s MediaRouter.Callback object. The following sample code demonstrates a controller method that creates a new remote playback cliente and sends it a video for playback. private void updateRemotePlayer(RouteInfo route) { // Changed route: tear down previous client if (mRoute != null && mRemotePlaybackClient != null) { mRemotePlaybackClient.release(); mRemotePlaybackClient = null; } // Save new route mRoute = route; // Attach new playback client mRemotePlaybackClient = new RemotePlaybackClient(this, mRoute); // Send file for playback mRemotePlaybackClient.play(Uri.parse( "http://archive.org/download/Sintel/sintel-2048-stereo_512kb.mp4"), "video/mp4", null, 0, null, new ItemActionCallback() { @Override public void onResult(Bundle data, String sessionId, MediaSessionStatus sessionStatus, String itemId, MediaItemStatus itemStatus) { logStatus("play: succeeded for item " + itemId); } @Override public void onError(String error, int code, Bundle data) { logStatus("play: failed - error:"+ code +" - "+ error); } }); } } For more information on how to use the media router, you can visit developer.android.com
View full article
Download ATK from Freescale Extract ATK: # unzip ATK_1_41_STD_installer.zip Get the wine-tricks script and install MFC-4.2 and VisualC++-6.0. ./winetricks  vcrun6sp6 Execute the default install process: # wine SETUP.EXE Edit the file /etc/udev/rules.d/50-udev-default.rules to set permission for everyone: KERNEL=="tty[A-Z]*|pppox*|ircomm*|noz*", GROUP="uucp", MODE="0666" Run ATK: # wine ADSToolkit_std.exe
View full article