i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
This doc show how to use i.MX8QXP Display Controller GammaCor unit to tune gamma. HW: i.MX8QXP MEK board, HDMI monitor SW: i.MX Linux 4.14.98_2.2.0 BSP release, patch in this doc 1.Introduce gamma The gamma, gamma correction, gamma encoding, gamma compression , these words all related one kind operation , see wiki page of it: The device used for image capture/print/display follow this power-law. For example the camera captured image , to view this image on display device as good as original captured image : gamma encoding when camera saved sensor data to image file,  and  gamma decoding when that image file display on your PC LCD monitor. That is : 2. i.MX8QXP Display Controller Gamma Correction Unit The Gamma Correction unit position is located between Frame Gen unit and TCon unit.   More detail see below contents from i.MX8QXP RM: So GammaCor unit could be used as adjust display gamma , or brightness or contrast. To used it, need follow the steps at RM 15.9.2.4.4.8.3.   Something need to note: You need program 33 sample point value into the register, these sample point value range is from 0 to 1023. Note, first write is start sample point value , then the other is delta value: current sample point minus previous sample point value. You can use GammaCor unit on any channel of R/G/B. If you use normalized function f(x), the following formula should be used to clut[i = 0..32] = round( f(i * 32 / 1023) * 1023) 3. i.MX8QXP Linux device driver patch and test code Apply attached  patch 8qxp_dpu_gammacor_4.14.98_2.2.0.diff on Linux kernel. In the kernel patch, function dpu_gammacor_update, I choose not calculate delta value between each sample pint , let user space application calculate delta value and passed to kernel. Apply 8qxp-dpu-gammacor-modetst.diff on libdrm-imx, to get test application which is based on modetest.  Test app will read one greyscale image file 720P.rgb, put it under same folder of test application , calculate sample point value by pow function  , and calling drmModeCrtcSetGamma to pass related value to kernel,  next loop will change sample point value, and will see that greyscale image will changed on HDMI monitor. After system boot up, run below cmd to check result of test application systemctl stop weston ./gamma_show_rgba.out -P 29@32:1280x720@AB24 Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.2.0_MX8QXP&appType=license c> https://source.codeaurora.org/external/imx/libdrm-imx/ d> https://en.wikipedia.org/wiki/Gamma_correction
記事全体を表示
Contents 1 创建 i.MX8QXP Linux 4.14.98_ga 板级开发包编译环境 2 1.1 下载板级开发包 ...................................................... 2 1.2 创建yocto编译环境: ................................................ 3 2 Device Tree ............................................................. 15 2.1 恩智浦的device Tree结构 ..................................... 15 2.2 device Tree的由来(no updates) ............................ 18 2.3 device Tree的基础与语法(no updates) ................. 20 2.4 device Tree的代码分析(no updates) .................... 42 3 恩智浦i.MX8XBSP 包文件目录结构 ......................... 75 4 恩智浦i.MX8XBSP的编译(no updates) .................... 77 4.1 需要编译哪些文件 ................................................ 77 4.2 如何编译这些文件 ................................................ 78 4.3 如何链接为目标文件及链接顺序 ........................... 79 4.4 kernel Kconfig ...................................................... 81 5 恩智浦BSP的内核初始化过程(no updates) .............. 81 5.1 初始化的汇编代码 ................................................ 83 5.2 初始化的C代码 ..................................................... 87 5.3 init_machine ....................................................... 100 6 恩智浦BSP的内核定制 ........................................... 103 6.1 DDR修改 ............................................................ 103 6.2 IO管脚配置与Pinctrl驱动 .................................... 105 6.3 新板bringup ........................................................ 120 6.4 更改调试串口 ...................................................... 128 6.5 uSDHC设备定制(eMMC flash,SDcard, SDIOcard) 135 6.6 LVDS LCD 驱动定制 .......................................... 144 6.7 GPIO_Key 驱动定制 .......................................... 147 6.8 GPIO_LED 驱动定制 ......................................... 151 6.9 Fuse nvram驱动 ................................................. 154 6.10 SPI与SPI Slave驱动 ........................................... 155 6.11 USB 3.0 TypeC 改成 USB 3.0 TypeA(未验证) ... 162 6.12 汽车级以太网驱动定制 ....................................... 162 6.13 i.MX8DX MEK支持 ............................................. 180 6.14 NAND Flash支持与烧录 ..................................... 181
記事全体を表示
目录 1 i.MX8X 板级开发包镜像结构 ...................................... 3 2 创建 i.MX8QXP Linux 4.19.35 板级开发包编译环境 ... 3 2.1 下载板级开发包 ....................................................... 3 2.2 创建yocto编译环境: ................................................. 4 2.3 独立编译 ............................................................... 10 3 i.MX8X SC firmware ................................................. 16 3.1 SC firmware 目录结构 ........................................... 16 3.2 SC firmware 启动流程 ........................................... 17 3.3 SC firmware定制 ................................................... 17 4 i.MX8X ATF .............................................................. 28 5 FSL Uboot 定制 ........................................................ 30 5.1 FDT支持 ............................................................... 31 5.2 DM(driver model)支持 ........................................... 36 5.3 Uboot目录 结构 ..................................................... 50 5.4 Uboot编译 ............................................................. 52 5.5 Uboot初始化流程 .................................................. 53 5.6 uboot 定制 ............................................................ 63 5.7 uboot debug信息 ................................................... 78
記事全体を表示
For early i.MX 8QuadXPlus MEK boards with C0 chips, power on the board when the board is connected to the PC with USB Type-C cable may cause the PC to shut down directly. This is a hardware known issue. another type of TCPC PHY chip will be used in later boards to fix this issue. If you have this kind of i.MX 8QuadXPlus MEK boards with c0 chips already, you can take below way to avoid this issue: 1. change the boot switch to "serial download mode", firstly power on the board, then connect the board to PC with Type-C cable. 2. download the attached files, uncompress this two files and put them in the same folder. 3. open the command window, change the working directory to the one contains the files just downloaded, and execute "uuu uuu_change_DRP_to_DFP.auto-imx8qxpc0mek" on command window. After the command being successfuley executed, the board can be powerwed up when the board is connected to PC with type-C cable.
記事全体を表示
Introduction EVIS (Enhanced Vision Instruction Set) is an API level program language, which is applicable on GC7000XSVX (i.MX8QM) and VIP8000NanoSi (i.MX8MP). The instructions take advantage of the enhanced vision capabilities in the vision-capble hardware, with low-latency. It provides additional functionality for vision image processing beyond the functions provided through the Khronos Group OpenVX API. In the i.MX8QM/i.MX8MP BSP, the OpenCL compiler also support the EVIS instructions. So, it is also an OpenCL VX Extension API. The source file can found in /usr/include/CL/cl_viv_vx_ext.h. Hardware Requirements i.MX8QM (GC7000XSVX) supports EVIS1. i.MX8MP (VIP8000NanoSi) supports EVIS2. Packed Data Types To fully utilize the computing power of the instructions, the extension API support packed data types. For example, in standard OpenCL, a vector char4 will occupy 4x 32-bit registers, while a packed char16 only occupies 128 bits. Thus use packed data types as possible.  The char, unsigned char, short, unsigned short, integer, unsigned integer, float packed data types are supported. They are defined with vxc_ prefix i.e. vxc_char, vxc_uchar, vxc_short, vxc_ushort, vxc_int, vxc_uint, vxc_float, followed by a literal value n that defines the number of elements in the packed data. Supported values of n are 2, 4, 8, and 16 for all the packed data types. Table 1 List of packed data type Type Description vxc_charn A vector of n packed signed character value vxc_ucharn A vector of n packed unsigned character value vxc_shortn A vector of n packed signed short value vxc_ushortn A vector of n packed unsigned short value vxc_intn A vector of n packed signed integer value vxc_uintn A vector of n packed unsigned integer value vxc_floatn A vector of n packed float value OP_CODE Instructions OP_CODE instructions operate on packed data. The enumeration can be found in /usr/include/CL/cl_viv_vx_ext.h. Only EVIS1 supports instructions: VXC_IAdd VXC_MagPhase VXC_BiLinear VXC_SelectAdd VXC_BitReplace VXC_Filter VXC_DP2x16/VXC_DP2x16_b Objects load and store Packed type image data read/write: supported types are packed 8-bit/16bit integer, 16bit float. Image read/write for image1d_t/image1d_array/image2d_t. Offset should be composed by using VXC_5BITOFFSET_XY(x, y). VXC_OP4(img_load, Dest, Image, Coord, Offset, Info) VXC_OP4_NoDest(img_store, Image, Coord, Color, Info) Parameters:         img_load/img_store    Read/write image data.          Dest                            The destination loading the data to.         Image                          The packed image data read from for img_load. The packed image data writing to for img_store.         Coord                          Coordinates to read/write the image data.         Color                           The image data being written to Image for img_store.         Info                              See more info in VXC_MODIFIER(StartBin, EndBin, SourceBin, RoundingMode, Clamp). VXC_MODIFIER(StartBin, EndBin, SourceBin, RoundingMode, Clamp) Parameters:         StartBin/EndBin           The first bin/the last bin for consecutive packed data.         SourceBin                    Not used.          RoundingMode            0: Toward Zero (truncated), 1: Toward Infinity (rounded up), 2: To Nearest Even, 3: not used.         Clamp                          0: no, result is truncated to fit result type (just the lower bits are copied), 1: yes, result is clamped to fit the result type. For example, int2 coord = (int2)(get_global_id(0), get_global_id(1)); vxc_uchar16 r1; VXC_OP4(img_load, r1, in_image, coord, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0)); VXC_Filter This interface applies a specified filter on a 3x3 pixel block. VXC_OP4(filter, Dest, Src0, Src1, Src2, Info) Parameters:         filter                           Filter modes.         Dest                          The filtered image.         Src0                          The first row pixels for 3x3 filter.         Src1                          The second row pixels for 3x3 filter.         Src2                          The third row pixles for 3x3 filter.         Info                            See more info in VXC_MODIFIER_FILTER(StartBin, EndBin, SourceBin, Filter, Clamp). VXC_MODIFIER_FILTER(StartBin, EndBin, SourceBin, Filter, Clamp) Parameters:         StartBin/EndBin        The first bin/the last bin for consecutive packed data.         SourceBin                 Not used.         Filter                          Filter modes are listed in table 2.         Clamp                        0: no, result is truncated to fit result type (just the lower bits are copied), 1: yes, result is clamped to fit the result type. Table 2. List of filter modes: Filter Mode Description VXC_FM_BOX Compute a 3x3 box filter: |1/9, 1/9, 1/9, 1/9, 1/9, 1/9, 1/9, 1/9, 1/9|. VXC_FM_Guassian Compute a 3x3 Gaussian filter: |1/16, 2/16, 1/16, 2/16, 4/16, 2/16, 1/16, 2/16, 1/16|. VXC_FM_SobelX Compute a 3x3 Sobel filter in the x-direction: |-1, 0, 1, -2, 0, 2, -1, 0, 1|. VXC_FM_SobelY Compute a 3x3 Sobel filter in the y-direction: |-1, -2, -1, 0, 0, 0, 1, 2, 1|. VXC_FM_ScharrX Compute a 3x3 Scharr filter in the x-direction: |3, 0, -3, 10, 0, -10, 3, 0, -3|. VXC_FM_ScharrY Compute a 3x3 Scharr filter in the y-direction: |3, 10, 3, 0, 0, 0, -3, -10, -3|. VXC_FM_Max Get the maximum from a 3x3 kernel. VXC_FM_Min Get the minimum from a 3x3 kernel. VXC_FM_Median Get the median from a 3x3 kernel. For example (details in Gaussian Filter examples), int2 coord_in1 = coord + (int2)(-1, -1);\n\ VXC_OP4(img_load, lineA, in_image, coord_in1, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int2 coord_in2 = coord + (int2)(-1, 0);\n\ VXC_OP4(img_load, lineB, in_image, coord_in2, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int2 coord_in3 = coord + (int2)(-1, 1);\n\ VXC_OP4(img_load, lineC, in_image, coord_in3, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int info = VXC_MODIFIER_FILTER(0, 13, 0, VXC_FM_Guassian, 0);\n\ VXC_OP4(filter, out, lineA, lineB, lineC, info); ;\n\ VXC_AbsDiff Calculates a result for the absolute difference between a and b. It works on packed data, so it can compute 16x 8-bit values or 8x 16-bit values. VXC_OP3(abs_diff, Dest, Src0, Src1, Info) Parameters:         abs_diff                 Specify the function of absolute difference.         Dest                      Destination to store the result.         Src0                      The first source to calculate the absolute difference.         Src1                      The second source to calculate the absolute differenece.         Info                       See more info in VXC_MODIFIER(StartBin, EndBin, SourceBin, RoundingMode, Clamp). There are also other interfaces will not be specified here, which can be found in the /usr/include/CL/cl_viv_vx_ext.h, i.e. VXC_IAdd, VXC_IAccSq, VXC_Lerp, VXC_MagPhase, VXC_MulShift, VXC_Clamp, VXC_BiLinear, VXC_SelectAdd, VXC_AtomicAdd, VXC_BitExtract and VXC_BitReplace.  Further Reading: OpenVX Vision Image Extension API Introduction - DP Dot Products
記事全体を表示
This guide is about how to use EVIS to create user nodes and kernels in OpenVX to implement image processing on NPU(i.MX8MP)/GPU(i.MX8QM). Take gaussian filter as an example. It is tested on i.MX8QM and i.MX8MP. User Node Creation from User Kernel 1. Define a user node Register a user kernel by its ID or name For example, #define VX_KERNEL_NAME_GAUSSIAN "com.nxp.extension.gaussian" #define VX_KERNEL_ENUM_GAUSSIAN 100 Get the kernel reference by the ID or name For example, vx_kernel kernel = vxGetKernelByName(context, VX_KERNEL_NAME_GAUSSIAN); vx_kernel kernel = vxGetKernelByEnum(context, VX_KERNEL_ENUM_GAUSSIAN ); Create a user node vx_node node = vxCreateGenericNode(graph, kernel); Set input/output node parameters For example, vx_status status = vxSetParameterByIndex(node, index++, (vx_reference)in_image); status |= vxSetParameterByIndex(node, index++, (vx_reference)out_image); 2. Create InputValidator/OutputValidator functions for the node The validators are only used for graph verification. For example, static vx_status VX_CALLBACK vxGaussianInputValidator(vx_node node, vx_uint32 index) static vx_status VX_CALLBACK vxGaussianOutputValidator(vx_node node, vx_uint32 index, vx_meta_format metaObj) ToDo: a. InputValidator: Get the reference to the parameter object   vx_parameter paramObj = NULL; vx_image imgObj = NULL; paramObj=vxGetParameterByIndex(node, index); vxQueryParameter(paramObj, VX_PARAMETER_REF, &imgObj, sizeof(vx_image)); Check meta-data restriction vxQueryImage(imgObj, VX_IMAGE_FORMAT, &imgFmt, sizeof(imgFmt)); Check consistency with other parameters if (VX_DF_IMAGE_U8==imgFmt) status = VX_SUCCESS; else status = VX_ERROR_INVALID_VALUE; b. OutputValidator Set the meta_format object with expected meta-data for the output status |= vxSetMetaFormatAttribute(metaObj, VX_IMAGE_FORMAT, &imgFmt, sizeof(imgFmt)); status |= vxSetMetaFormatAttribute(metaObj, VX_IMAGE_WIDTH, &width, sizeof(width)); status |= vxSetMetaFormatAttribute(metaObj, VX_IMAGE_HEIGHT, &height, sizeof(height)); 3. Create Initializer function for the node. The initializer is used to specify workdim, global work size and local work size for the user kernel. These parameters are similiar to that in OpenCL. For example,                                                                                    /* workdim, globel offset, globel scale, local size, globel size */ vx_kernel_execution_parameters_t shaderParam = {2,               {0, 0, 0},        {0, 0, 0},        {0, 0, 0},   {0, 0, 0}}; vx_status VX_CALLBACK vxGaussianInitializer(vx_node nodObj, const vx_reference *paramObj, vx_uint32 paraNum) Set attribute to the node vxSetNodeAttribute(nodObj, VX_NODE_ATTRIBUTE_KERNEL_EXECUTION_PARAMETERS, &shaderParam, sizeof(vx_kernel_execution_parameters_t)); Note: The links below are guides about OpenCL on GPU, which are helpful to understand OpenVX implemented on GPU/NPU. OpenCL Work Item Ids: Global/Group/Local OpenCL Programming Guide OpenCL Resources Introduction to OpenCL 4. Create Deinitializer function for the node (Optional) It is used to de-allocate memory allocated at initializer. User Kernel on NPU/GPU Creation 1. Create description of a user kernel For example, vx_kernel_description_t vxGaussianKernelVXCInfo = { VX_KERNEL_ENUM_GAUSSIAN, VX_KERNEL_NAME_GAUSSIAN, nullptr, vxGaussianKernelParam, (sizeof(vxGaussianKernelParam)/sizeof(vxGaussianKernelParam[0])), vxGaussianValidator, nullptr, nullptr, vxGaussianInitializer, nullptr }; 2. Register the new kernel For example, static vx_kernel_description_t* kernels[] = { &vxGaussianKernelVXCInfo, }; 3. Write kernel source implemented on NPU/GPU For example, char vxcKernelSource[] = { "#include \ \n\ \n\ \n\ __kernel void gaussian\n\ ( \n\ __read_only image2d_t in_image, \n\ __write_only image2d_t out_image \n\ ) \n\ { \n\ int2 coord = (int2)(get_global_id(0), get_global_id(1)); \n\ int2 coord_out = coord; \n\ vxc_uchar16 lineA, lineB, lineC, out;\n\ int2 coord_in1 = coord + (int2)(-1, -1);\n\ VXC_OP4(img_load, lineA, in_image, coord_in1, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int2 coord_in2 = coord + (int2)(-1, 0);\n\ VXC_OP4(img_load, lineB, in_image, coord_in2, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int2 coord_in3 = coord + (int2)(-1, 1);\n\ VXC_OP4(img_load, lineC, in_image, coord_in3, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int info = VXC_MODIFIER_FILTER(0, 13, 0, VXC_FM_Guassian, 0);\n\ VXC_OP4(filter, out, lineA, lineB, lineC, info); ;\n\ VXC_OP4_NoDest(img_store, out_image, coord_out, out, VXC_MODIFIER(0, 13, 0, VXC_RM_TowardZero, 0)); \n\ }\n\ " }; Note: the source is written by EVIS instructions with less latency. But the EVIS instructions are limited. These fucntions defination can be found in "cl_viv_vx_ext.h" located at "/usr/include/CL/cl_viv_vx_ext.h". Read back the processed data by GPU/NPU to check if the operations are correct. For example, status = vxCopyImagePatch(vx_out_image, &rect, 0, &addressing, data2, VX_READ_ONLY, VX_MEMORY_TYPE_HOST); 4. Build the NPU/GPU source code runtime For example, programObj = vxCreateProgramWithSource(ContextVX, 1, programSrc, &programLen); vxBuildProgram(programObj, "-cl-viv-vx-extension"); 5. Add kernel to the program For example, ... kernelObj = vxAddKernelInProgram(programObj, kernels[i]->name, kernels[i]->enumeration, kernels[i]->numParams, kernels[i]->validate, kernels[i]->initialize, kernels[i]->deinitialize ); ... for(vx_uint32 j=0; j < kernels[i]->numParams; j++) { status = vxAddParameterToKernel(kernelObj, j, kernels[i]->parameters[j].direction, kernels[i]->parameters[j].data_type, kernels[i]->parameters[j].state ); 6. Finalize the kernel creation For example, status = vxFinalizeKernel(kernelObj); Exercise The example is attached. You can build and test it on i.MX8QM or i.MX8MP. Results on i.MX8QM: References: Khronosdotorg/resources.md at master · KhronosGroup/Khronosdotorg · GitHub  Further Reading: OpenVX Vision Image Extension API Introduction - Basic API OpenVX Vision Image Extension API Introduction - DP Dot Products
記事全体を表示
www.nxp.com公网资源 .............................................. 2 1.1 www.nxp.com Documentation ................................ 3 1.2 www.nxp.com Tools&Software ............................... 7 2 nxp share point资源(仅对有访问权限客户开放) ....... 14 2.1 i.MX 8X Family Board, Software POR and How to Purchase ...................................................................... 14 2.2 Development Platforms ........................................ 14 2.3 Device Dcoumentation ......................................... 15 2.4 Security Reference Manual .................................. 16 2.5 Software Documentation ...................................... 16 3 nxp 社区资源 ........................................................... 16
記事全体を表示
Default Ethernet feature is removed for Android Auto (both Android_Pie9.0 and Android10) Below are the patched to bring Ethernet feature back to Android Auto. Please try to apply the according patches if you want to enable Ethernet. For Android_Pie9.0_Auto(example with car2 build): --- a/arch/arm64/configs/android_car2_defconfig +++b/arch/arm64/configs/android_car2_defconfig @@ -245,7 +245,7 @@ CONFIG_DM_VERITY_FEC=y CONFIG_NETDEVICES=y CONFIG_MACVTAP=m CONFIG_TUN=y -# CONFIG_ETHERNET is not set +CONFIG_ETHERNET=y CONFIG_MDIO_BUS_MUX_MMIOREG=m CONFIG_AT803X_PHY=m CONFIG_MARVELL_PHY=m @@ -517,7 +517,7 @@ CONFIG_SQUASHFS=y CONFIG_SQUASHFS_DECOMP_MULTI=y CONFIG_SQUASHFS_XATTR=y CONFIG_SQUASHFS_LZ4=y -# CONFIG_NETWORK_FILESYSTEMS is not set +CONFIG_NETWORK_FILESYSTEMS=y   --- a/imx8q/mek_8q/mek_8q.mk +++ b/imx8q/mek_8q/mek_8q.mk @@ -46,6 +46,7 @@ PRODUCT_COPY_FILES += \      $(IMX_DEVICE_PATH)/fstab.freescale.car:$(TARGET_COPY_OUT_VENDOR)/etc/fstab.freescale \      $(IMX_DEVICE_PATH)/early.init_car.cfg:$(TARGET_COPY_OUT_VENDOR)/etc/early.init.cfg \      $(IMX_DEVICE_PATH)/required_hardware_auto.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/required_hardware.xml \ +    frameworks/native/data/etc/android.hardware.ethernet.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.ethernet.xml \      device/fsl/imx8q/init.recovery.freescale.car.rc:root/init.recovery.freescale.rc   For Android10_Auto,(example with car build): --- a/arch/arm64/configs/android_car_defconfig +++ b/arch/arm64/configs/android_car_defconfig @@ -23,6 +23,8 @@ CONFIG_SCHED_AUTOGROUP=y CONFIG_SCHED_TUNE=y CONFIG_RELAY=y CONFIG_BLK_DEV_INITRD=y +CONFIG_FEC=y +CONFIG_AT803X_PHY=y # CONFIG_RD_BZIP2 is not set # CONFIG_RD_LZMA is not set # CONFIG_RD_XZ is not set @@ -246,7 +248,6 @@ CONFIG_DM_VERITY=y CONFIG_DM_VERITY_FEC=y CONFIG_NETDEVICES=y CONFIG_TUN=y -# CONFIG_ETHERNET is not set   --- a/imx8q/mek_8q/mek_8q.mk +++ b/imx8q/mek_8q/mek_8q.mk @@ -46,6 +46,7 @@ PRODUCT_COPY_FILES += \      $(IMX_DEVICE_PATH)/fstab.freescale.car:$(TARGET_COPY_OUT_VENDOR)/etc/fstab.freescale \      $(IMX_DEVICE_PATH)/early.init_car.cfg:$(TARGET_COPY_OUT_VENDOR)/etc/early.init.cfg \      $(IMX_DEVICE_PATH)/required_hardware_auto.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/required_hardware.xml \ +    frameworks/native/data/etc/android.hardware.ethernet.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.ethernet.xml \      device/fsl/imx8q/init.recovery.freescale.car.rc:root/init.recovery.freescale.rc   Note: Please also check for below file, if fec1 is disabled, please also apply below diff. --- a/arch/arm64/boot/dts/freescale/imx8qm-mek-car2.dts +++ b/arch/arm64/boot/dts/freescale/imx8qm-mek-car2.dts @@ -147,10 +147,6 @@ status = "disabled"; }; -&fec1 { - status = "disabled"; -}; - &fec2 { status = "disabled"; };
記事全体を表示
Tested on Android 10 (android_Q10.0.0_1.0.0) After your the first BSP build the kernel sources are at: ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/ For the i.MX8M Mini, You can check the defconfig files being used on: ${MY_ANDROID}/device/fsl/imx8m/evk_8mm/UbootKernelBoardConfig.mk # imx8mm kernel defconfig TARGET_KERNEL_DEFCONFIG := android_defconfig TARGET_KERNEL_ADDITION_DEFCONF := android_addition_defconfig You could change one of them to add the desired configuration. - android_defconfig - is ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/arch/arm64/configs/android_defconfig - android_addition_defconfig - is on the same folder ${MY_ANDROID}/device/fsl/imx8m/evk_8mm/ "merge_config.sh" is called to generate the final defconfig file prior to building the kernel Check out: https://source.android.com/devices/architecture/kernel/config For example, I want to add DEVMEM support on my build: 1. Change the defconfig I add the line below to android_addition_defconfig CONFIG_DEVMEM=y (Or could have added it android_defconfig) 2. Build the kernel ./imx-make.sh kernel -c -j8 3. Verify your change After compiling, you can confirm your change by reading: ${MY_ANDROID}/out/target/product/evk_8mm/obj/KERNEL_OBJ/.config Then rebuild boot.img and reprogram the target.
記事全体を表示
Click to view the webinar recording View More Information and Order the Vision Starter Kit
記事全体を表示
The i.MX8QuadMax SMARC System On Module integrates Dual Cortex A72 + Quad Cortex A53 Cores, Dual GPU systems, 4K H.265 capable VPU dual failover-ready display controller based i.MX8 QuadMax SoC with on SOM Dual 10/100/1000 Mbps Ethernet PHY, USB 3.0 hub and IEEE 802.11a/b/g/n/ac Wi-Fi & Bluetooth 5.0 module.
記事全体を表示
Sometimes it is helpful/faster to build a i.MX8MM boot binary outside of the Yocto environment. There are instructions on how to accomplish this on different places, this document tries to provide an example for the i.MX8M Mini LPDDR4 EVK, whenever possible pointing how to build for other boards. For the 8MM SoC a boot image is generated by imx-mkimage tool and requires: - u-boot - ARM trusted firmware image - ddr training firmware 1. Download and Build u-boot: mkdir imx-boot-bin cdimx-boot-bin git clone https://source.codeaurora.org/external/imx/uboot-imx.git cd uboot-imx/ git checkout -b imx_v2019.04_4.19.35_1.1.0 origin/imx_v2019.04_4.19.35_1.1.0 (Optional) Here you can "git log -1" to check that the commit matches SRCREV on the recipe. Next, use the BSP SDK script to setup the cross compilation environment, instructions on how to build it are here. source /opt/fsl-imx-wayland/4.19-warrior/environment-setup-aarch64-poky-linux export ARCH=arm Build make clean Supported boards have configuration files on "configs". Using the LPDDR4 EVK here: make imx8mm_evk_defconfig make 2.   Download and build the ARM Trusted Firmware cd .. git clone https://source.codeaurora.org/external/imx/imx-atf.git cd imx-atf/ git checkout -b imx_4.19.35_1.1.0 origin/imx_4.19.35_1.1.0 (Optional) Again, you can "git log -1" to check that the commit matches SRCREV on the recipe. https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/meta-bsp/recipes-bsp/imx-atf/imx-atf_2.0.bb?h=warrior-4.19.35-1.1.0 Build: make PLAT=imx8mm bl31 If you run into this error: aarch64-poky-linux-ld.bfd: unrecognized option '-Wl,-O1' aarch64-poky-linux-ld.bfd: use the --help option for usage information make: *** [Makefile:712: build/imx8mm/release/bl31/bl31.elf] Error 1 try:  unset LDFLAGS make PLAT=imx8mm bl31 3. Download the LPDDR4 training binaries It is on firmware-imx, recipe is here: https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/meta-bsp/recipes-bsp/firmware-imx?h=warrior-4.19.35-1.1.0 cd .. mkdir firmware-imx cd firmware-imx wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.5.bin chmod a+x firmware-imx-8.5.bin ./firmware-imx-8.5.bin 4. Download imx-mkimage and build the boot image cd .. git clone https://source.codeaurora.org/external/imx/imx-mkimage.git cd imx-mkimage/ git checkout -b imx_4.19.35_1.1.0 origin/imx_4.19.35_1.1.0 (Optional) "git log -1" matches SRCREV on: https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/meta-bsp/recipes-bsp/imx-mkimage/imx-mkimage_git.inc?h=warrior-4.19.35-1.1.0 Now, you can check the build targets and required binaries at iMX8M/soc.mak For the flash_evk for the imx8mm we will need binaries: u-boot: u-boot-spl.bin, u-boot-nodtb.bin, fsl-imx8mm-evk.dtb  ARM trusted firmware: bl31.bin LPDDR4 files: lpddr4_pmu_train_1d_imem.bin lpddr4_pmu_train_1d_dmem.bin lpddr4_pmu_train_2d_imem.bin lpddr4_pmu_train_2d_dmem.bin mkimage for mkimage_uboot Copy all these to imx-mkimage/iMX8M/ cp ../uboot-imx/spl/u-boot-spl.bin iMX8M/ cp ../uboot-imx/u-boot-nodtb.bin iMX8M/ cp ../uboot-imx/arch/arm/dts/fsl-imx8mm-evk.dtb iMX8M/ cp ../imx-atf/build/imx8mm/release/bl31.bin iMX8M/ cp ../firmware-imx/firmware-imx-8.5/firmware/ddr/synopsys/lpddr4_pmu_train_* iMX8M/ cp ../uboot-imx/tools/mkimage iMX8M/mkimage_uboot Build: make SOC=iMX8MM flash_evk Output binary is on ./iMX8M/flash.bin 5. Program on the SD Card: sudo dd if=iMX8M/flash.bin of=/dev/<path to your sd> bs=1024 seek=33
記事全体を表示
This package is a OTA upgrade implementation for smartlocker in i.MX7ULP kernel. The bootaux command for i.MX7ULP can also be applied to other projects. File description: smartlocker OTA upgrade user manual. Modified u-boot. Modification involves: Add bootaux command. To use this command, the M4 image will be read out from boot partition to TCM_L. (Or DDR and then it will be copied to TCM_L in the command) It took 19ms to read M4 image. Change u-boot default env. If M4 image and zImage read failed, recovery M4 image and zImage will be loaded. patch of u-boot changes. u-boot defconfig for bootaux change. sh script, updater.sh. Example for upgrade package. Power shutdown in copying upgrade files may cause file broken. So currently, we use below copy strategy: Copy upgrade file to target directory as tmp file. Delete target file. Rename tmp file to target file.
記事全体を表示
         This document will describe how to add open JDK to i.MX yocto BSP. It will take two versions of Linux BSP as an example, one is the lower version of L4.1.15-2.0.0, the other is the latest version of L4.19.35-1.1.0. Adding openjdk-8 to L4.1.15-2.0.0(Ubuntu 16.04 LTS platform) Before adding an open JDK, you must download L4.1.15-2.0.0 BSP according to the i.MX_Yocto_Project_User's_Guide.pdf, and ensure that it can pass the compilation normally, that is to say, there is no error in the compilation. In this example, BSP is compiled using the following command. # DISTRO=fsl-imx-wayland MACHINE=imx6sxsabresd source fsl-setup-release.sh -b build-wayland # bitbake fsl-image-qt5          Then follow the steps below to add openjdk to the yocto layer:   Fetching openjdk-8 from Yocto website # cd ~/imx-release-bsp # cd sources # git clone git://git.yoctoproject.org/meta-java # cd meta-java # git checkout -b krogoth origin/krogoth  [Comment]    Yocto’s version is described in i.MX_Yocto_Project_User's_Guide.pdf 2. Modifying related configurations (1) build-wayland/conf/local.conf Add following lines to the file: # Possible provider: cacao-initial-native and jamvm-initial-native PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native" # Possible provider: cacao-native and jamvm-native PREFERRED_PROVIDER_virtual/java-native = "cacao-native" # Optional since there is only one provider for now PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native" IMAGE_INSTALL_append = " openjdk-8" Save it and exit (2)build-wayland/conf/bblayers.conf Add java layer to the file, like below: BBLAYERS = " \   ${BSPDIR}/sources/poky/meta \   ${BSPDIR}/sources/poky/meta-poky \   \   ${BSPDIR}/sources/meta-openembedded/meta-oe \   ${BSPDIR}/sources/meta-openembedded/meta-multimedia \   \   ${BSPDIR}/sources/meta-fsl-arm \   ${BSPDIR}/sources/meta-fsl-arm-extra \   ${BSPDIR}/sources/meta-fsl-demos \   ${BSPDIR}/sources/meta-java \ "…… Save it and exit. 3. Build openjdk-8 # cd ~/imx-release-bsp # source setup-environment build-wayland #bitbake openjdk-8 -c fetchall          Fetch all packages related to openjdk-8. [error handling]          During downloading packages, you may encounter errors like the following. (1)Fetch fastjar-0.98.tar.gz errors          The error is caused by invalid web address, we can download it from another link, see below: http://savannah.c3sl.ufpr.br/fastjar/fastjar-0.98.tar.gz copy the link to firefox in Ubuntu platform, and it will be downloaded into ~/Downloads # cd ~/imx-release-bsp/downloads # cp ~/Downloads/ fastjar-0.98.tar.gz ./ # touch fastjar-0.98.tar.gz.done   (2)Fetch “classpath-0.93.tar.gz” error          Download it from : http://mirror.nbtelecom.com.br/gnu/classpath/classpath-0.93.tar.gz And copy it to ~/imx-release-bsp/downloads, and create a file named classpath-0.93.tar.gz.done in the directory. # cd ~/imx-release-bsp/downloads # cp ~/Downloads/ classpath-0.93.tar.gz ./ # touch classpath-0.93.tar.gz.done (3) 8 files with tar.bz2 (hotspot-Java jvm)          These similar errors are very likely to be encountered.          These errors are caused by the bad network environment. You can download these packages manually. These are Java virtual machine source packages, i.e. hotspot JVM [Solution] # mkdir ~/temp # cd temp # wget http://www.multitech.net/mlinux/sources/56b133772ec1.tar.bz2 # wget http://www.multitech.net/mlinux/sources/ac29c9c1193a.tar.bz2 # wget http://www.multitech.net/mlinux/sources/1f032000ff4b.tar.bz2 # wget http://www.multitech.net/mlinux/sources/81f2d81a48d7.tar.bz2 # wget http://www.multitech.net/mlinux/sources/0549bf2f507d.tar.bz2 # wget http://www.multitech.net/mlinux/sources/0948e61a3722.tar.bz2 # wget http://www.multitech.net/mlinux/sources/48c99b423839.tar.bz2 # wget http://www.multitech.net/mlinux/sources/bf0932d3e0f8.tar.bz2          Then create .tar.bz2.done files for each package via touch command   # touch 56b133772ec1.tar.bz2.done # touch ac29c9c1193a.tar.bz2.done # touch 1f032000ff4b.tar.bz2.done # touch 81f2d81a48d7.tar.bz2.done # touch 0549bf2f507d.tar.bz2.done # touch 0948e61a3722.tar.bz2.done # touch 48c99b423839.tar.bz2.done # touch bf0932d3e0f8.tar.bz2.done          Like below:          Then copy these files to ~/ fsl-release-bsp/downloads/ # bitbake openjdk-8 -c compile          After openjdk compilation, you will be prompted as follows:          At last , install openjdk-8 to images # bitbake fsl-image-qt5          Done: [Additional description]          The above method of adding openjdk-8 is the steps after BSP compilation. Users can also add openjdk-8 before BSP compilation, and then compile it with BSP          According to steps in i.MX_Yocto_Project_User's_Guide.pdf, After running the following two commands, users can modify bblayers.conf and local.conf directly.          For example, steps below have been validated: … … # repo sync # cd ~/fsl-release-bsp # DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 # gedit ./conf/bblayers.conf          Add the same contents as above. # gedit ./conf/local.conf          Add the same contents as above. # bitbake fsl-image-gui          During compilation, users may encounter some errors, which can be handled by referring to the methods described above Adding openjdk-8 to L4.19.35-1.1.0(Ubuntu 18.04 LTS Platform) In fact, the steps to add openjdk-8 to l4.19.35 are the same as those described above, and the following steps have been verified. Before adding openjdk-8, i.mx8qxp full image has been compiled with 2 commands below, so we only need to add openjdk-8 here. # DISTRO=fsl-imx-xwayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-xwayland # bitbake imx-image-full # cd sources # git clone git://git.yoctoproject.org/meta-java # cd meta-java # git checkout -b warrior origin/warrior          Release L4.19.35_1.1.0 is released for Yocto Project 2.7 (Warrior). # cd ~/imx-release-bsp-l4.19.35 # source setup-environment build-xwayland-imx8qxpmek # gedit ./conf/bblayers.conf          Add meta-java to it.          ……            ${BSPDIR}/sources/meta-java \          ……          Save and exit. # gedit ./conf/local.conf          Add these lines to it.          # Possible provider: cacao-initial-native and jamvm-initial-native PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native" # Possible provider: cacao-native and jamvm-native PREFERRED_PROVIDER_virtual/java-native = "cacao-native" # Optional since there is only one provider for now PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native" IMAGE_INSTALL_append = " openjdk-8" Save and exit.   # cd ~/imx-release-bsp-l4.19.35/build-xwayland-imx8qxpmek # bitbake openjdk-8 -c fetch # bitbake openjdk-8 -c compile [Errors] [Solution] # gedit ./ tmp/work/x86_64-linux/openjdk-8-native/172b11-r0/jdk8u-33d274a7dda0/hotspot/make/linux/Makefile Comment the following lines: ----------------------------------------- check_os_version: #ifeq ($(DISABLE_HOTSPOT_OS_VERSION_CHECK)$(EMPTY_IF_NOT_SUPPORTED),) #       $(QUIETLY) >&2 echo "*** This OS is not supported:" `uname -a`; exit 1; #endif -----------------------------------------          Then continue # cd ~/imx-release-bsp-l4.19.35/build-xwayland-imx8qxpmek # bitbake openjdk-8 -c compile [comment]          Probably similar errors will be encountered during compiling other packages, we can use the same way like above to solve it, see bellow, please! Done:          At last, install openjdk-8 to images. # bitbake imx-image-full          Installation is done. NXP TIC Team  Weidong Sun 12/31/2019
記事全体を表示
The D-PHY PLL (in the red circle in the picture below) is the PLL that drives the MIPI Clock lane. It must be set in accordance with the video to be sent to the display.   Calculating the video bandwidth The video bandwidth is calculated with the following equation: Pixels per second = Horizontal res. x Vertical res. x Frame rate x Bits per pixel Taking as example the 1080p60 OLED display RM67191: Pixels per second = 1920 x 1080 x 60 x 24 Pixels per second = 2985984000 = 2,98Gpixels/sec Pixel clock calculation The Display pixel clock can be obtained on the display driver. In this example for RM67191, the pixel clock is 132Mpixel/sec, see file: panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Line 530: .pixelclock = { 66000000, 132000000, 132000000 }, Or the number can be obtained with the following equation: pixel clock = (hactive + hfront_porch + hsync_len + hback_porch) x (vactive + vfront_porch + vsync_len + vback_porch) x frame rate pixel clock = (1080 + 20 + 2 +34) × (1920 + 10 + 2 + 4) x 60 pixel clock = 132000000 (rounded up) Bit clock calculation (clock lane) The mipi-dphy bit_clk is the output clock and is calculated on file sec-dsim.c (line 1283): sec-dsim.c\bridge\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Bit clock can be calculated with the following equation: bit_clk = Pixel clock * Bits per pixel / Number of lanes In the case of 1980p60 (Raydium display), It is:   bit_clk = pixel clock * bits per pixel / number of lanes bit_clk = 132000000 * 24 / 4 bit_clk = 792000000 Other important timing parameters like 'p', 'm', 's' are obtained on the table in the following header file: sec_mipi_dphy_ln14lpp.h\imx\drm\gpu\drivers - linux-imx - i.MX Linux kernel 
記事全体を表示
In case you missed our recent webinar, you can check out the slides and comment below with any questions.
記事全体を表示