i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Hello everyone, this document will share an step by step guide of the configuration needed in a Linux PC to compile the SDK examples we provide, as well as how to download them in an easy way. Requirements: I.MX 8M Mini EVK SDK package (for i.MX8MM) UUU tool First step would be to get the SDK package, this include documentation and code, which is available at the MCUXpresso builder webpage: https://mcuxpresso.nxp.com/en/welcome Click on the select a development board and select the package for your development kit or the i.MX MPU   This guide is focused on Linux build so will select GCC package and Linux host PC as the environment. Click on build and wait for the SDK package to be ready for download. Note1: Click on select all if the whole middleware package is desired Note2: it is possible to select each middleware that are desired. On new window select download SDK Select on new pop-up window download both SDK and documentation Read and accept EULA so the download start Decompress the package using the following command: $ tar -xvzf ~/SDK_2_13_0_EVK-MIMX8MM.tar.gz -C ~/SDK_2_13_0_EVK-MIMX8MM Next will be to download the GCC from the ARM webpage, gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 https://developer.arm.com/downloads/-/gnu-rm Note that the GCC version used is based on the minimum version required, since this was tested and supported, this could be found within the SDK documentation (~/SDK_2_13_0_EVK-MIMX8MM/docs/MCUXpresso SDK Release Notes for EVK-MIMX8MM) Once downloaded we can decompress and configure the environment: $ tar -xf gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ sudo apt-get install cmake  Check the version >= 3.0.x $ cmake --version Once this is done we enter the path of the example of our choice and compile using the script, as necessary using debug, release or all. $ cd ~/SDK_2_13_0_EVK-MIMX8MM/boards/evkmimx8mm/demo_apps/hello_world/armgcc $./build_release.sh The binary (elf and bin) will be found inside the folder according to whether we use debug or release script. For this example we used release script: $ cd release Once builded we can move/download the binaries from the Linux host PC to the board by using the UUU tool with the command fat_write #### we put the board in fastboot mode by entering the command in the uboot terminal fastboot 0 #### From the Linux terminal introduce the UUU command to  download to the FAT partition of the eMMC of the baord: ## For rproc it is needed the .elf binary ## $ uuu -v -b fat_write hello_world.elf mmc 0:1 hello_world.elf ## For bootaux it is needed the .bin binary ## $  uuu -v -b fat_write hello_world.bin mmc 0:1 hello_world.bin Once with the binaries in the FAT partition of the SD/eMMC of our board we can make the necessary modifications (device tree/bootargs) to test the Cortex-M examples. For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
查看全文
  Platform: i.MX8MP EVK , L6.1.22-2.0.0 LT9211 is a chip that can realize the conversion of MIPI DSI signals to LVDS signals. This patch is based on this mainline driver:https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/gpu/drm/bridge/lontium-lt9211.c Keypoint Move lt9211_host_attach function to lt9211_attach to skip bridge attach error.  
查看全文
Installing the new release (Ubuntu 22.04) was detected some NXP boards as iMX8MNEVK, iMX8MM-EVK, iMX8MP-EVK and iMX8ULP-EVK had an issue with the WIFI module that basically it does not initialize at boot. Remember, the supported WIFI modules in Ubuntu 22.04 in the EVKs are the following:       • NXP 88W8987       • NXP 88W9098       • NXP 88W8997       • NXP IW416       • NXP 88W8801       • NXP IW612 To initialize the WIFI module of NXP EVKs in Ubuntu 22.04 you can set the following command in console:   sudo modprobe moal mod_para=nxp/wifi_mod_para.conf   That command find the correct driver for our WIFI module and then initialize it, but this only works when Ubuntu is working and if you reset the EVK you need to set the command again.   The definitive solution is create a custom startup script as a service:   Step 1: Go to etc/systemd/system   cd etc/systemd/system   Step 2: In this directory create a new file with the name of your preference but the extension must be .service. You can do it with nano or vim: sudo nano or sudo vim   The file must contain: [Unit] Description=”Wifi Start” [Service] ExecStart=sudo modprobe moal mod_para=nxp/wifi_mod_para.conf [Install] WantedBy=multi-user.target   Now save the file, in my case the name was wifi_start.service.   Step 3: Now we need to enable the script in the startup/boot sequence following the command: sudo systemctl enable wifi_start.service   Remember in wifi_start.service is the name as you saved your file.   Finally, each time you boot your board, the WIFI module will initialize automatically.   Boards tested: iMX8MN (With WIFI module NXP 88W8987) iMX8MM (With WIFI module NXP 88W8987) iMX8MP (With WIFI module NXP 88W8997) iMX8ULP (With WIFI module NXP IW416)  
查看全文
This demo for all(bootloader, device tree, Linux kernel, rootfs) in spi. It uses raw read(sf read)/raw write(sf write in uuu script) to achieve that. sf probe 0; sf read ${fdt_addr} 0x500000 0x100000; sf read ${loadaddr} 0x600000 0x1E00000; sf read ${initrd_addr} 0x2400000 0x600000; setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate} rdinit=/linuxrc; booti ${loadaddr} ${initrd_addr} ${fdt_addr} |-- 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch --- patch for this demo |-- demo_binary | |-- flash.b0.bin --- b0 bootloader | |-- flash.bin --- c0 bootloader | |-- Image-imx8qxpc0mek.bin --- Linux kernel | |-- imx8qxp-mek.dtb --- device tree | |-- uramdisk_boot.rootfs.aarch64.img --- ram disk | |-- uuu.qspi.all.b0.uuu --- uuu script for b0 | `-- uuu.qspi.all.uuu --- uuu script for c0 `-- readme.txt --- this file # The spi layout used is: # - --------- -------------------------------------------- # | | flash.bin | env | dtb | Image |rootfs| # - --------------- -------------------------------------- # ^ ^ ^ ^ ^ ^ ^ # | | | | | | | # 0 4kiB 4MiB 5MiB 6MiB 36MiB 42MiB 0x1000 0x400000 0x500000 0x600000 0x2400000 Test: HW: i.MX8QXP MEK SW: lf-5.10.72-2.2.0 + 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch Test log: SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB device 0 offset 0x500000, size 0x100000 SF: 1048576 bytes @ 0x500000 Read: OK device 0 offset 0x600000, size 0x1e00000 SF: 31457280 bytes @ 0x600000 Read: OK device 0 offset 0x2400000, size 0x600000 SF: 6291456 bytes @ 0x2400000 Read: OK [ 4.787552] imx6q-pcie 5f010000.pcie: unable to add pcie port. [ 4.797467] Freeing unused kernel memory: 2944K [ 4.807379] Run /linuxrc as init process Starting syslogd: OK Starting klogd: OK Running sysctl: OK Starting network: OK /bin/sh: can't access tty; job control turned off / #  
查看全文
In this article, I will explain how to set up the iMX8M Plus to use the 4K Dart BCON Basler Camera module. Requirements: Evaluation Kit for the i.MX 8M Plus Applications Processor. (i.MX 8M Plus Evaluation Kit | NXP Semiconductors) Basler Camera for i.MX 8M Plus (4K dart BCON for MIPI camera module for i.MX 8M Plus | NXP Semiconductors). Embedded Linux for i.MX Applications Processors (Embedded Linux for i.MX Applications Processors | NXP Semiconductors) (For this example we will use BSP version Linux 5.15.71_2.2.0) Serial Console Emulator Basler Camera Specifications and Manuals: Basler Camera Specifications at this link: Embedded Vision Kits daA3840-30mc-IMX8MP-EVK - Embedded Vision Kits (baslerweb.com). Basler Manual to identify and setting up the hardware at this link: daA3840-30mc-IMX8MP-EVK | Basler Product Documentation (baslerweb.com) Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor. (Video: Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor | NXP Semiconductors) Steps After setting up the hardware we will need to turn on the iMX8M Plus and follow these steps: 1. Stop the boot process on Uboot by pressing any key. 2. Use the following command to list interfaces. => mmc list Output example => FSL_SDHC: 1 (SD) => FSL_SDHC: 2 The above command will show you the device number in this example for SD, the device number is 1. 3. Then use fatls <interface> <device[:partition]> [<directory>] fatls mmc 1:1 (Device 1 : Partition 1) With this command, we will be able to list device tree files. => fatls mmc 1:1 4. Select imx8mp-evk-basler.dtb or imx8mp-evk-dual-basler.dtb and use the command editenv fdtfile.  => editenv fdtfile Output example edit: imx8mp-evk-basler.dtb 5. In edit command line put the selected device tree (*.dtb). 6. Use saveenv command to save environment and continue with the boot process. 7. Using the terminal and go to /opt/imx8-isp/bin and execute the script run.sh. $ ./run.sh -c basler_1080p60 -lm 8. Use the command gst-device-monitor-1.0 to list devices. Here you will find the path to the camera device. $ gst-device-monitor-1.0 Output example Device found: name : VIV class : Video/Source caps : video/x-raw, format=YUY2, width=[ 176, 4096, 16 ], height=[ 144, 3072, 8 ], pixel-aspect-ratio=1/1, framerate={ (fraction)30/1, (fraction)29/1, (fraction)28/1, (fraction)27/1, (fraction)26/1, (fraction)25/1, (fraction)24/1, (fraction)23/1, (fraction)22/1, (fraction)21/1, (fraction)20/1, (fraction)19/1, (fraction)18/1, (fraction)17/1, (fraction)16/1, (fraction)15/1, (fraction)14/1, (fraction)13/1, (fraction)12/1, (fraction)11/1, (fraction)10/1, (fraction)9/1, (fraction)8/1, (fraction)7/1, (fraction)6/1, (fraction)5/1, (fraction)4/1, (fraction)3/1, (fraction)2/1, (fraction)1/1 } ... properties: udev-probed = true device.bus_path = platform-vvcam-video.0 sysfs.path = /sys/devices/platform/vvcam-video.0/video4linux/video2 device.subsystem = video4linux device.product.name = VIV device.capabilities = :capture: device.api = v4l2 device.path = /dev/video2 v4l2.device.driver = viv_v4l2_device v4l2.device.card = VIV v4l2.device.bus_info = platform:viv0 v4l2.device.version = 393473 (0x00060101) v4l2.device.capabilities = 2216693761 (0x84201001) v4l2.device.device_caps = 69206017 (0x04200001) gst-launch-1.0 v4l2src device=/dev/video2 ! ... 9. Finally, use gstreamer to verify proper operation. (With this gstreamer pipeline you will see a new window with the camera output. Then, just rotate the lens to acquire the correct focus) $ gst-launch-1.0 -v v4l2src device=/dev/video2 ! "video/x-raw,format=YUY2,width=1920,height=1080" ! queue ! imxvideoconvert_g2d ! waylandsink Basic description of Gstreamer Pipeline gst-launch-1.0 -v: The option -v enables the verbose mode to get detailed information of process. v4l2src device=/dev/video2: Select input device in this case the camera is on path /dev/video3. "video/x-raw,format=YUY2,width=1920,height=1080": Received format from camera. queue: This command is a buffer between camera recording process and the following image process, this command help us to interface two process and prevent blocking where each process has different speeds, in other words, when a process A is faster than process B. imxvideoconvert_g2d: This proprietary plugin uses hardware acceleration to perform rotation, scaling, and color space conversion on video frames. waylandsink : This command creates its own window and renders the decoded frames processed previously. 10. Result     I hope this article will be helpful. Best regards, Brian.
查看全文
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
查看全文
Platform: i.MX8MP SW:Linux 5.4.70.2.3.0 On current linux BSP, PCIE driver does not support Hot-plug, customers wants to turn off PCIE device to save power, attached is guide. Remove PCIE device driver Suspend PCIE driver Turn off PCIE device power supply Turn on PCIE device power supply Resume PCIE driver Rescan PCIE device Load PCIE device driver
查看全文
PCIE IP on i.MX8MM and i.MX8MP is same, customer can follow PCIE test Application note to do compliance test, if eye diagram failed, they can fine turn corresponding regs below: iMX8MMRM.pdf IMX8MPRM.pdf GEN1:             GEN2:                 Related code in kernel Phy-fsl-imx8-pcie.c (kernel-source\drivers\phy\freescale)    3794      2020/11/4 static int imx8_pcie_phy_init(struct phy *phy) { ……          /* Configure TX drive level  */        writel(0x2d, imx8_phy->base + 0x404);          return 0; }   Thanks Lambert
查看全文
i.MX8 series contains internal HiFi4 DSP. It is targeted for Audio related signal processing. SOF (Sound Open Firmware) is open source audio DSP firmware, driver and SDK. This document introduces basic theory about IIR/FIR digital filters, how to design IIR/FIR digital filters and the Equalizer filters implementation by SOF. After that, the document also describes how HiFi4 DSP MAC engine accelerate the EQ filters calculation.
查看全文
BSP: L5.15.5_1.0.0   Platform: i.MX8MPlus EVK   1. Parameter preparation For more parameter calculation, please refer to: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M- Mini-Register-Programming-Aid-DRAM-PLL-setting/ta-p/111209  For 1866MHz LPDDR4, we need a DRAM PLL size of 933MHz. The PLL dividing parameters are: m=622,p=16,s=0, k=0.   2. Calibration and stress test with DDR Tool 2.1 Creating a test script for 1866MHz Here we copy the script from another file (e.g. 2000MHz) and modify the contents of the script.   2.2 Modify the script to adapt to 1866MHz 2.3 Download the test script After selecting the ddr script we created, click on the download button   2.4 Calibrating the stress test Set the core clock of the chip's cpu to 1.2GHz, then click the Calibration button to calibrate, then click Gen Code to generate the lpddr4_timing.c file. Set the start frequency to 1866MHz for the stress test.   2.5 Modify lpddr4_timing.c We need to modify the generated lpddr4_timing.c file to change the maximum speed to 3732MTS.   3. SPL patch After getting the correct lpddr4_timing.c file, the SPL code also needs to be modified to add support for the 933MHz DRAM PLL. diff --git a/arch/arm/mach-imx/imx8m/clock_imx8mm.c b/arch/arm/mach-imx/imx8m/clock_imx8mm.c index e39f238fdf...5622a6334e 100644 --- a/arch/arm/mach-imx/imx8m/clock_imx8mm.c +++ b/arch/arm/mach-imx/imx8m/clock_imx8mm.c @@ -55,6 +55,7 @@ static struct imx_int_pll_rate_table imx8mm_fracpll_tbl[] = { PLL_1443X_RATE(650000000U, 325, 3, 2, 0), PLL_1443X_RATE(600000000U, 300, 3, 2, 0), PLL_1443X_RATE(594000000U, 99, 1, 2, 0), + PLL_1443X_RATE(933000000U, 622, 16, 0, 0), PLL_1443X_RATE(400000000U, 400, 3, 3, 0), PLL_1443X_RATE(2660000U, 266, 3, 3, 0), PLL_1443X_RATE(167000000U, 334, 3, 4, 0), diff --git a/drivers/ddr/imx/imx8m/ddrphy_utils.c b/drivers/ddr/imx/imx8m/ddrphy_utils.c index 326b92d784..ebd005bc2b 100644 --- a/drivers/ddr/imx/imx8m/ddrphy_utils.c +++ b/drivers/ddr/imx/imx8m/ddrphy_utils.c @@ -117,6 +117,10 @@ void ddrphy_init_set_dfi_clk(unsigned int drate) dram_pll_init(MHZ(1000)); dram_disable_bypass(); break; + case 3732: + dram_pll_init(MHZ(933)); + dram_disable_bypass(); + break; case 3200: dram_pll_init(MHZ(800)); dram_disable_bypass();   4. Test results   Reference blog. DDR Tool: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467  RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352 
查看全文
Hello, here Jorge. On this post I will explain how to configure, record and play audio using an i.MX 8MIC-RPI-MX8 Board. Requirements: I.MX 8M Mini EVK Linux Binary Demo Files - i.MX 8MMini EVK (L5.15.52_2.1.0) i.MX 8MIC-RPI-MX8 Board Serial console emulator (Tera Term, Putty, etc.) Headphones/speakers The 8MIC-RPI-MX8 accessory board is designed for voice enabled application prototyping and development on the i.MX 8M family. The board plugs directly into the 40-pin expansion connector on the i.MX 8M Mini and Nano EVK’s. Some features about this board are: 8 PDM Microphones 8 monochrome LEDs 4 multi-color LEDs 2 status LEDs 4 pushbuttons Microphone Mute Switch Microphone geometry switch Connecting the i.MX 8MIC-RPI-MX8 Board. The i.MX 8MIC-RPI-MX8 Board has a 40-pin expansion connector that you can plug it directly to the EVK board. Ensure that pin 1 of the 8MIC-RPI-MX8 is aligned with pin 1 on the EVK J1001 as is showed on the next figure:  Selecting the device tree on the board. Once the pre-compiled image is flashed on the board (Flashing Linux BSP using UUU) and you connected the 8MIC-RPI-MX8 it is necessary to select the correct device tree to handle 8MIC board. On U-boot check the available .dtb files on the BSP using the next command: u-boot=> fatls mmc 2:1 And you will get the corresponding list of .dbt files:  On this case we are working with an I.MX 8M Mini EVK and the corresponding .dtb file is: imx8mm-evk-8mic-revE.dtb To select it you need to set the environment variable and save it with: u-boot=> setenv fdtfile imx8mm-evk-8mic-revE.dtb u-boot=> saveenv Doble check it using: u-boot=> printenv fdtfile   Now it is time to boot Linux using the next command: u-boot=> boot Recording audio with the i.MX 8MIC-RPI-MX8 Board. The Advanced Linux Sound Architecture (ALSA) provides audio and MIDI functionality to the Linux operating system. ALSA has the following significant features: Efficient support for all types of audio interfaces, from consumer sound cards to professional multichannel audio interfaces. Fully modularized sound drivers. SMP and thread-safe design. User space library (alsa-lib) to simplify application programming and provide higher level functionality. Support for the older Open Sound System (OSS) API, providing binary compatibility for most OSS programs. Once we are on Linux, we can check our audio codecs detected on the board using: arecord -l   Now, to record audio we need to use the ALSA arecord command to start recording with IMX8 boards, there are different options that you can check on the next link. On this case we are going to use the next: arecord -D hw:imxaudiomicfil -c8 -f s16_le -r48000 -d10 sample.wav -D: selects the device. -c: selects the number of channels on the recording. -f: selects the format. -r: selects the sample rate. -d: determinate the duration recording time in seconds. sample.wav: Is the name of the resulting audio file. Running the last command, we started to record audio. It is time to make some noise and record it!   Playing audio from IMX8 boards. Now it is time to connect our headphones or speakers to the jack.   Also, as on arecord command you can check the devices where you can play audio from the board using the next command: aplay -l And you will get all the codecs to play audio:   To play our recordings we need to use the ALSA aplay command, it is important to select the correct audio codec to hear the audio from the jack on the board: aplay -Dplughw:3,0 sample.wav -D: selects the device. sample.wav: Is the name of audio file to play   Hope this will helpful for people who wants to record audio using PDM microphones and playing audio from IMX8 boards. Best regards.
查看全文
Symptoms   Bridge mode on EQoS module will not work since Linux Kernel 5.10_2.2.0. Platforms impacted: i.MX8MP/i.MX8DXL/i.MX93   Diagnosis   When eqos module(eth1) is added to the bridge using brctl, it will first set eth1 to promiscuous mode and then set the VLAN for this bridge with a filter VID value of 1. Before adding Intel's patch, there is no problem. c89f44ff10fd net: stmmac: Add support for VLAN promiscuous mode However, when Intel's patch sets up the filter, if it finds that the promiscuous mode is turned on, it will turn off the VLAN Tag function. And it adds a judgment on whether promiscuous mode has been turned on in the function of configuring VID. Returns an error if promiscuous mode is found. Because the patch has turned off the VLAN tag function when promiscuous mode is enabled, which conflicts with continuing to configure the VID. Workaround   This patch is okay for aarch64 platform to solve this issue. diff --git a/drivers/net/ethernet/stmicro/stmmac/dwmac4_core.c b/drivers/net/ethernet/stmicro/stmmac/dwmac4_core.c index c25bfecb4a2d..2dc548b54b1c 100644 --- a/drivers/net/ethernet/stmicro/stmmac/dwmac4_core.c +++ b/drivers/net/ethernet/stmicro/stmmac/dwmac4_core.c @@ -481,12 +481,6 @@ static int dwmac4_add_hw_vlan_rx_fltr(struct net_device *dev, if (vid > 4095) return -EINVAL; - if (hw->promisc) { - netdev_err(dev, - "Adding VLAN in promisc mode not supported\n"); - return -EPERM; - } - /* Single Rx VLAN Filter */ if (hw->num_vlan == 1) { /* For single VLAN filter, VID 0 means VLAN promiscuous */ @@ -536,12 +530,6 @@ static int dwmac4_del_hw_vlan_rx_fltr(struct net_device *dev, { int i, ret = 0; - if (hw->promisc) { - netdev_err(dev, - "Deleting VLAN in promisc mode not supported\n"); - return -EPERM; - } - /* Single Rx VLAN Filter */ if (hw->num_vlan == 1) { if ((hw->vlan_filter[0] & GMAC_VLAN_TAG_VID) == vid) {  
查看全文
This article describes how to integrate NXP WiFi & BT module into i.MX platform, some debug tips, how to test, etc. Although it takes i.MX8MM as example, it is also suitable for all i.MX8 serials platform.
查看全文
On i.MX8MP EVK, image is downloaded into eMMC/SD via OTG1, if customer wants to enable USB OTG2 on i.MX8MP for uuu tool. Pls find modification as attached.
查看全文
This is a simple known-how for how to enable KASAN on L4.14.98 with i.MX8/8X and also a collection of related patches for fixing issues reported by KASAN.   Enable KASAN: It's very simple, just enable "CONFIG_KASAN" in kernel configuration. Besides this, adjusting the kernel's loading address is also required, due to KASAN (which will alloc more memory as a "tracker" for each allocation). For e.g., on imx8qxp MEK, we need to change the kernel loadaddr in uboot:     0x80280000 --> 0xE0280000 through uboot env: setenv loadaddr 0xE0280000 After this, it supposed to be working.   KASAN related patches on L4.14.98: KASAN will do detection/sanitizing for any memory allocation/access. In case of L4.14.98 on i.MX8/8X, there're several "BUG" reported by KASAN in default BSP. The attached patches are a collection for these issues.    Note: not all "BUG" reported by KASAN are really bug. Most of them are just some programming rule related problems and may not really cause memory access violation.
查看全文
On behalf of Gopise Yuan. A simple sharing for enabling some kernel options for using “lockdep”. It will be useful for detecting some deadlock (spinlock/mutex/…) issue. Validated on L4.14.x, and, found a lock violation…
查看全文
some industry customer to use i.MX8MM will use RMII to link the 100Mhz ethernet phy and wish to use our i.mx8mm output 50Mhz reference clock to external phy to save a crystal, this doc and patch explain how to support it. SW: Linux BSP 5.10.17. HW: i.MX8MM LPDDR/DDR EVK board. 中文版本为一个完整的如何支持一个100Mhz以太网PHY  
查看全文
1. Intro   This document contains instructions to run run the SAI low power audio demo on the i.MX 8M Plus EVK. Here, the  RPSMG to allows audio to be passed from the A53 cluster running Linux to the M7 core. The latter controls the on board WM8960 audio codec,  which is connected to a 3.5 mm audio jack that allow us to play music using headphones. I will show the necessary steps to make the demo work and will add some GStreamer examples to demonstrate the demo's capabilities.   TBD: update this with a nice diagram that depicts the A53 and M7 RPMSG channel. 2. Requirements   Hardware  MX 8M Plus EVK Headphones with 3.5 mm audio jack Type-C power supply for i.MX 8M Plus EVK Micro USB to USB adapter cable Software  A recent prebuilt Linux BSP image from NXP.com ( we tested this on 5.15.35 and 5.15.5 releases) Windows 10 or Ubuntu 20.04 Workstation MCUXpresso SDK for i.MX 8M Plus ( available from:  Welcome | MCUXpresso SDK Builder (nxp.com)) 3. Reference documentation for this example   MCUXpresso SDK   [1] Getting Started with MCUXpresso SDK for EVK-MIMX8MP     Available within the MCUXpresso SDK package:  \{INSTALL PATH}\SDK_X_X_X_EVK-MIMX8MP\docs    [2] SAI low power audio README file Contains instructions for the SAI Low Power Audio Demo.  Available within the MCUXpresso SDK package: \{INSTALL PATH}\SDK_X_X_X_EVK-MIMX8MP\boards\evkmimx8mp\demo_apps\sai_low_power_audio   4. Downloading a pre-built Linux BSP image for the i.MX 8M Plus   I will make use of the prebuilt Linux Image for the i.MX 8M Plus EVK for demonstrating the demo works.  At the moment of writing this time, I used the 5.15.32 release, although there are older releases like 5.10.5 that I tested and proved to work with no issues. This SAI Low Power Audio Demo shall work for other processors on the i.MX 8M family. Although specific instructions ( e.g. load address for M-core binary load) might require some adaptation. For M-core load address, please refer to the specific MCUXpresso SDK documentation for each processor. The prebuilt Linux image (5.15.32) for the i.MX 8M Plus EVK can be downloaded from here: https://www.nxp.com/webapp/Download?colCode=L5.15.32_2.0.0_MX8MP&appType=license You can download other releases from here: Embedded Linux for i.MX Applications Processors | NXP Semiconductors . Select a version and a board and select download. 5. Flashing the BSP image   If you are using an Ubuntu 20.04 workstation, I recommend you to flash the image using dd. For this, you can refer to the i.MX Linux User's Guide: Section - 4.3.2 Copying the full SD card image - https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf sudo dd if=.wic of=/dev/sdx bs=1M && sync NOTE: when using dd, ALWAYS, double check the of device that you are about to writing. Messing up with another location or partition will harm your system   If you are following this document on a Windows machine: You can use the Universal Update Utility (UUU) to flash your image on either the board's eMMC or SD card. Document named UUU.pdf shall serve as your reference guide for further instructions and flashing examples. It is available along with UUU binary here: https://github.com/NXPmicro/mfgtools/releases Two examples are shown below for your convenience:                                     SD card flash                                                 uuu -b sd_all bootloader rootfs.sdcard.bz2                                     eMMC flash                                                 uuu -b emmc_all bootloader rootfs.sdcard.bz2        uuu uuu.auto NOTE: UUU is also compatible with Ubuntu NOTE: there are other engineers who like to use BalenaEtcher for flashing their BSP images. I have tested it and works on both Ubuntu and Windows 10 machines.   6. Preparing the BSP and booting up M7 core  using U-Boot   I am writing this upon the instructions contained on the README file for the low power audio example  [2]. Instructions ready to copy and paste will follow:   Instruct U-Boot to pass to the kernel the rpmsg device tree to enable communication between the A53 cluster and the M7 one: u-boot=>setenv fdtfile imx8mp-evk-rpmsg.dtb u-boot=>saveenv Load the M7 example: u-boot=>setenv mmcargs 'setenv bootargs ${jh_clk} console=${console} root=${mmcroot} snd_pcm.max_alloc_per_card=134217728' u-boot=>saveenv Now, we need to load the M4 with the demo. Refer to [1] for further information. If running the BSP on an SD card, make sure the example binary is listed on the boot partition as follows: fatls mmc 1:1 You shall see something similar to this:             imx8mp_m7_TCM_sai_low_power_audio.bin Open the serial terminal emulator for the M7. Out of the fourth ports listed when we plug the i.MX 8M Plus serial debug cable to the PC, the M7 is typically the last one listed.   All the serial ports available to the workstation when the i.MX 8M Plus serial cable is connected to it. NOTE: you may require to install addtitional COM drivers if you are running on Windows. I like doing the previous step so I can see the result of the next commands issued in U-boot to load the M7 image. fatload mmc 1:1 0x48000000 imx8mp_m7_TCM_sai_low_power_audio.bin; cp.b 0x48000000 0x7e0000 20000; bootaux 0x7e0000 Here is an screenshot that shows how the U-Boot's response should look: U-Boot response when loading the SAI low power audio example to the Cortex M7 That should have prompted the following message on the M7 terminal: M7-core is up!   Now, let’s move to user space! u-boot=> boot 7. Testing the example using a simple GStreamer pipeline   As soon as the O.S. finishes booting. We can see that M7 terminal prompts the following: M7 is now in STOP mode; waiting for some audio to beat the room! Confirm that the WM8960 is listed as audio card as follows: cat /proc/asound/cards             Listing avaialable audio cards. WM8960 should be present. Make note of the list. The wm8960 is listed a the third sound card. This is where I like to differ a bit from [2] and I suggest a quicker test in case of not having an audio file ready. We just simply use GStreamer to play an audiotest source. Please make sure to plug in your headphones onto the board’s 3.5 mm jack before.   The following GStreamer pipeline is using the WM8960 as an audiosink.  gst-launch-1.0 audiotestsrc ! alsasink device=hw:3   NOTE: please be cautious and not put the headphones directly in your head at the first attempt. The sound can be too loud to some people. This is what you should see on the M7 side: Stop the GStreamer pipeline issuing CTRL + C. M7 shall warn you about that: NOTE: you can use the aplay command to play audio as shown on [2]. However, I consider using a testsrc is much quicker and flexible for a quick test.  8. Additional information   Feel free to go ahead and tweak the GStreamer pipeline to change audio test source properties. audiotest src. This command will let you know the available options:            gst-inspect-1.0 audiotestsrc                         NOTE: you can navigate through the displayed list using the “d”key. Press “q’’ to quit. For example:     For example, I am reproducing sound using a different setup based on the list above: gst-launch-1.0 audiotestsrc freq=4000 volume=0.8 wave=8 ! alsasink device=hw:3 9.  Errata and future updates   TBD:     Add an example on how to define the default audio card and play the audio either using gst-play or building the pipeline using filesrc Comment on the limitations of the M7 core regarding sample rate and audio formats  
查看全文
Sometimes we got CMA allocation error while there're still many free pages in CMA area.  This article analyze several cases/reason for this kind of failure.
查看全文
BSP: L5.15.5_1.0.0 Platform: i.MX8MPlus EVK Background   The function lpddr4_mr_read in BSP always return zero and this casue the customer can't use it to read MR registers in DRAM. This is a simple demo for reading MR registers. Patch Code   diff --git a/arch/arm/include/asm/arch-imx8m/ddr.h b/arch/arm/include/asm/arch-imx8m/ddr.h index 0f1e832c03..fd68996a23 100644 --- a/arch/arm/include/asm/arch-imx8m/ddr.h +++ b/arch/arm/include/asm/arch-imx8m/ddr.h @@ -721,6 +721,8 @@ int wait_ddrphy_training_complete(void); void ddrphy_init_set_dfi_clk(unsigned int drate); void ddrphy_init_read_msg_block(enum fw_type type); +unsigned int lpddr4_mr_read(unsigned int mr_rank, unsigned int mr_addr); + void update_umctl2_rank_space_setting(unsigned int pstat_num); void get_trained_CDD(unsigned int fsp); diff --git a/board/freescale/imx8mp_evk/spl.c b/board/freescale/imx8mp_evk/spl.c index 33bbbc09ac..85e40ffbbe 100644 --- a/board/freescale/imx8mp_evk/spl.c +++ b/board/freescale/imx8mp_evk/spl.c @@ -150,6 +150,40 @@ int board_fit_config_name_match(const char *name) return 0; } #endif +void lpddr4_get_info() +{ + int i = 0, attempts = 5; + + unsigned int ddr_info = 0; + unsigned int regs[] = { 5, 6, 7, 8 }; + + for(i = 0; i < ARRAY_SIZE(regs); i++){ + unsigned int data = 0; + data = lpddr4_mr_read(0xF,regs[i]); + ddr_info <<= 8; + ddr_info += (data & 0xFF); + switch (i) + { + case 0: + printf("DRAM INFO : Manufacturer ID = 0x%x",ddr_info); + if(ddr_info & 0Xff) + printf(", Micron\n"); + break; + case 1: + printf("DRAM INFO : Revision ID1 = 0x%x\n",ddr_info); + break; + case 2: + printf("DRAM INFO : Revision ID2 = 0x%x\n",ddr_info); + break; + case 3: + printf("DRAM INFO : I/O Width and Density = 0x%x\n",ddr_info); + break; + default: + break; + } + } + +} void board_init_f(ulong dummy) { @@ -187,6 +221,8 @@ void board_init_f(ulong dummy) /* DDR initialization */ spl_dram_init(); + + lpddr4_get_info(); board_init_r(NULL, 0); } diff --git a/drivers/ddr/imx/imx8m/ddrphy_utils.c b/drivers/ddr/imx/imx8m/ddrphy_utils.c index 326b92d784..f45eeaf552 100644 --- a/drivers/ddr/imx/imx8m/ddrphy_utils.c +++ b/drivers/ddr/imx/imx8m/ddrphy_utils.c @@ -194,8 +194,15 @@ unsigned int lpddr4_mr_read(unsigned int mr_rank, unsigned int mr_addr) tmp = reg32_read(DRC_PERF_MON_MRR0_DAT(0)); } while ((tmp & 0x8) == 0); tmp = reg32_read(DRC_PERF_MON_MRR1_DAT(0)); - tmp = tmp & 0xff; reg32_write(DRC_PERF_MON_MRR0_DAT(0), 0x4); + + while (tmp) { //try to find a significant byte in the word + if (tmp & 0xff) { + tmp &= 0xff; + break; + } + tmp >>= 8; + } return tmp; }     Test Result  
查看全文