i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
The document to descript change the u-boot environment variables under the Linux rootfs.  Also provide a demo on i.MX6ull evk of sdcard mirror.  Linux fw_printenv fw_setenv to access U-Boot's environment variables.pdf  --- the document fw_printenv_fw_setenv_demo_iMX6ullevk_L4.14.98_2.0.0_ga.sdcard  --- demo sdcard mirror
View full article
When working on the IOMUX settings of an i.MX processor for our design it’s always good to make use of the IOMUX Tool provided by Freescale on the Download Page of most i.MX processors. We’ll focus on the latest release of the IOMUX tool for i.MX6. The IOMUX tool provides a Graphic User Interface to easily assign internal signals to external pins/balls and resolve any potential pin conflict and muxing options for the different modules available on the i.MX processors. IOMUX Tool Download (Will request to log in) Freescale’s Boards IOMUX settings. On the IOMUX tool package you’ll find the User’s Manual and also a folder containing the muxing options for Freescale’s Reference Boards, which may be of help when working with the Reference Designs as a starting point. You may load these settings files using the file/open option. MMDC pins Since the Multi-mode DDR controller MMDC pins are not muxed these cannot be changed on the IOMUX tool. This because the memory interfaces are much more sensitive to interference and thus have dedicated pins that do not share pad with other signals. The registers are also set on the default value so it’s good to keep this in mind when working with the code provided by the IOMUX tool. Considerations when using generated code The tool can generate code to be used as reference of the IOMUX configuration but still requires manual tweaking and the header files available on the i.MX Processor’s BSP in order to be implemented in an actual application code. It’s important to review the register settings on the Register tab in order to export the desired values; otherwise the code will have the default values for the registers according to the IOMUX tool. This is especially true for the Daisy Chain settings, always manually review these. Import function limitations There is an import function available so IOMUX configuration files saved in previous versions of the IOMUX tool can be loaded on the newest version. However, this feature should be used carefully. When importing a design it’s recommended to save the imported design on the new version of the IOMUX tool as imported.xml; then opening a new configuration and saving it as new.xml and comparing register value differences to manually correct the imported.xml values. In small projects it might be recommended to manually load the IOMUX information on the new IOMUX tool version to avoid register conflicts from version to version. For more information please refer to the documentation available within the IOMUX tool package. An advanced example is also included in that document.
View full article
Question: What exactly does the DTE/DCE interface in the i.MX6's UART module do and how are RTS and CTS affected by the UARTxUFCR[DTEDCE] bit? In i.MX6 RM, revision 1: Sections 64.2.1.2.1  (CTS) and 64.2.1.2.2 (RTS) both state that CTS and RTS change direction between DCE and DTE modes.  However, sections 64.4.3.1 (RTS_B) and 64.4.3.8 (CTS_B) state they do not change functions.  Is this a documentation error, or is there a difference between CTS/RTS and CTS_B/RTS_B? It appears that some of this is covered in the IOMUX daisy chain by switching which pins are connected to CTS and RTS. Answer: Example 1: UART1 in DTE mode. RTS is an output from the UART IP block so it must be routed to a CTS pin. Therefore, the SELECT_INPUT register could only use settings 00 or 10. Example 2: UART1 in DCE mode. RTS is an input to the UART IP block so it must be routed to an RTS pin. Therefore, the SELECT_INPUT register could only be set to 01 or 11. At this point, we have assumed that the internal signals connected to the UART block do not change direction.  We believe that DCEDTE from the UART block connects into the IOMUX logic and controls the direction of the PAD.  Then, the IOMUX INPUT_SELECT mux is used to choose one of four pads to connect to the UART inputs while the IMOUX MUX_CTRL connects the output path.  Further, we assume it is an error to connect the UART input to a pad configured as an output or a UART output to a pad configured as an input. The attached shows our assumptions For the Uart IP, the CTS_B is always an output and RTS_B always an input. But the RTS_B &CTS_B IO will be swapped  when UART operates in different DTE or DCE mode.  IO port DTE mode DCE mode direction Uart IP port(internal) direction Uart IP port(internal) UART_CTS_B O CTS_B I RTS_B UART_RTS_B I RTS_B O CTS_B UART_TXD O TXD I RXD UART_RXD I RXD O TXD Regarding how to configure the IOMUX, please see the attached PDF.
View full article
Building Freescale U-boot The U-boot provided by Freescale can be downloaded in the following link: http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/ 1 - Set the cross compiler environment variables. When using Yocto, it can be made by the following command (see more details at Yocto Trainning Yocto Training - HOME ) source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi 2 - Download the source code using "git clone": git clone  http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git 3 - Create a local branch based on some remote branch. In this example, lets use branch origin/imx_v2014.04_3.14.28_1.0.0_ga cd uboot-imx git checkout -b imx_v2014.04_3.14.28_1.0.0_ga_local origin/imx_v2014.04_3.14.28_1.0.0_ga 4 - Configure the project with the board you want to build. All board are listed on file boards.cfg. Check the exactly name of the choosen board and add "_config" to build the project. In this example, lets use mx6qsabresd make mx6qsabresd_config make 5 - The binary file will be generated and will be located at project root folder. The generated file in this case will be u-boot.imx 6 - More details can be found on files doc/README.imx6 doc/README.imximage README Building Mainline U-boot The U-boot project is developed and maintained by Denx Computer Systems can be downloaded in the following link: http://git.denx.de/?p=u-boot.git;a=summary 1 - Set the cross compiler environment variables. When using Yocto, it can be made by the following command (see more details at Yocto Trainning Yocto Training - HOME ) source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi 2 - Download the source code using "git clone": git clone http://git.denx.de/u-boot.git 3 - Check the name of the board on "configs" folder. In this case lets use mx6qsabresd_config make mx6qsabresd_config make 4 - The binary file will be generated and will be located at project root folder. The generated file in this case will be u-boot.imx
View full article
I have finally been able to get multi MSI (not MSI-X) working on the i.MX6 using the Linux kernel v4.1.15 release supported by Freescale/NXP. Attached are four patches which will need to be applied. This has been tested with two different end point FPGA devices with the i.MX6 running in root complex, I can confirm that multi MSI is now working.   Freescale/NXP: Please put these patches in your supported main line so others can have native multi MSI support.   You may have to contact your board manufacturer to find where within Yocto you will need to store these patches. If just building the kernel outside of Yocto then you can directly apply them.   The four kernel (v4.1.15) files which need to be patched are: <kernel source path>/include/linux/msi.h <kernel source path>/drivers/pci/msi.c <kernel source path>/drivers/pci/host/pcie-designware.h <kernel source path>/drivers/pci/host/pcie-designware.c   Once the above patches are applied and you create a new image/build you can start using the multi MSI APIs in your driver and pci_msi_vec_count() and pci_enable_msi_range() will work; this assumes your end point device on the PCIe link is working correctly.   Hopefully this is helpful to those who need multi MSI.   This document was generated from the following discussion: SOLVED: i.MX6 and Multi MSI Working
View full article
Add SSI_ASRC_P2P support for imx6 based on Kernel 3.0.35.
View full article
The i.MX 6 D/Q/DL/S/SL Linux 3.10.53_1.1.0 GA release is now available on www.freescale.com ·         Files available           Name Description L3.10.53_1.1.0_LINUX_DOCS i.MX 6 D/Q/DL/S/SL Linux   3.10.53_1.1.0 GA BSP documentation. L3.10.53_1.1.0_iMX6QDLS_Bundle i.MX 6 D/Q/DL/S  Linux   3.10.53_1.1.0 GA BSP Binary Demo Files L3.10.53_1.1.0_iMX6SL_Bundle i.MX 6 SL  Linux   3.10.53_1.1.0 GA BSP Binary Demo Files L3.10.53_1.1.0_AACP_CODECS AAC Plus Codec for the i.MX 6 D/Q/DL/S/SL Linux 3.10.53_1.1.0   GA BSP y IMX_6_MFG_L3.10.53_1.1.0_TOOL Manufacturing Tool and Documentation for Linux   3.10.53_1.1.0 GA BSP y ·         Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board New Features ·                             Please refer to formal Release Note document for all details. Known issues For known issues and limitations please consult the release notes located in the BSP documentation package.
View full article
Host TFTP and NFS Configuration Now configure the Trivial File Transfer Protocol (TFTP) server and Networked File System (NFS) server. U-Boot will download the Linux kernel and dtb file using tftp and then the kernel will mount (via NFS) its root file system on the computer hard drive. 1. TFTP Setup   1.1.1 Prepare the TFTP Service   Get the required software if not already set up. On host for TFTP: Install TFTP on Host $ sudo apt-get install tftpd-hpa   (Note: There are a number of examples in various forums, etc, of how to automatically start the TFTP service - but not all are successful on all Linux distro's it seems! The following may work for you.)   Start the tftpd-hpa service automatically by adding a command to /etc/rc.local. $ vi /etc/rc.local   Now, just before the exit 0 line edit below command then Save and Exit. $ service tftpd-hpa start  Now, To control the TFTP service from the command line use: $ service tftpd-hpa restart    To check the status of the TFTP service from the command line use: $ service tftpd-hpa status   1.1.1 Setup the TFTP Directories Now, we have to create the directory which will contain the kernel image and the device tree blob file. $ mkdir -p /imx-boot/imx6q-sabre/tftp Then, copy the kernel image and the device tree blob file in this directory. $ cp {YOCTO_BUILD_DIR}/tmp/deploy/images/{TARGET}/zImage /imx-boot/imx6q-sabre/tftp $ cp {YOCTO_BUILD_DIR}/tmp/deploy/images/{TARGET}/<dtb file> /imx-boot/imx6q-sabre/tftp   OR we can use the default directory created by yocto {YOCTO_BUILD_DIR}/tmp/deploy/images/{TARGET}/ The tftpd-hpa service looks for requested files under /imx-boot/imx6q-sabre/tftp The default tftpd-hpa directory may vary with distribution/release, but it is specified in the configuration file: /etc/default/tfptd-hpa. We have to change this default directory with our directory   Edit default tftp directory $ vi /etc/default/tftpd-hpa   Now, change the directory defined as TFTP_DIRECTORY with your host system directory which contains kernel and device tree blob file. Using created directory TFTP_DIRECTORY=”/imx-boot/imx6q-sabre/tftp” OR Using Yocto directory path TFTP_DIRECTORY=”{YOCTO_BUILD_DIR}/tmp/deploy/images/{TARGET}” Restart the TFTP service if required $ service tftpd-hpa restart   1.2 NFS Setup 1.2.1 Prepare the NFS Service Get the required software if not already set up. On host for NFS: Install NFS on Host $ sudo apt-get install nfs-kernel-server The NFS service starts automatically. To control NFS services : $ service nfs-kernel-server restart To check the status of the NFS service from the command line : $ service nfs-kernel-server status 1.2.2 Setup the NFS Directories Now, we have to create the directory which will contain the root file system. $ mkdir -p /imx-boot/imx6q-sabre/nfs   Then, copy the rootfs in this directory. $ cp -R {YOCTO_BUILD_DIR}/tmp/work/{TARGET}-poky-linux-gnueabi/{IMAGE}/1.0-r0/rootfs/* /imx-boot/imx6q-sabre/nfs   OR we can use the default directory created by yocto. $ {YOCTO_BUILD_DIR}/tmp/work/{TARGET}-poky-linux-gnueabi/{IMAGE}/1.0-r0/rootfs 1.2.3 Update NFS Export File The NFS server requires /etc/exports to be configured correctly to access NFS filesystem directory to specific hosts. $ vi /etc/exports Then, edit below line into the opened file. <”YOUR NFS DIRECTORY”> <YOUR BOARD IP>(rw,sync,no_root_squash,no_subtree_check) Ex. If you created custom directory for NFS then, /imx-boot/imx6q-sabre/nfs <YOUR BOARD IP>(rw,sync,no_root_squash,no_subtree_check) Ex: /imx-boot/imx6q-sabre/nfs 192.168.*.*(rw,sync,no_root_squash,no_subtree_check) OR /{YOCTO_BUILD_DIR}/tmp/work/{TARGET}-poky-linux-gnueabi/{IMAGE}/1.0-r0/rootfs <YOUR BOARD IP>(rw,sync,no_root_squash,no_subtree_check)   Now, we need to restart the NFS service. $ service nfs-kernel-server restart   2 Target Setup   We need to set up the network IP address of our target. Power On the board and hit a key to stop the U-Boot from continuing. Set the below parameters, setenv serverip 192.168.0.206       //This must be your Host IP address The path where the rootfs is placed in our host has to be indicated in the U-Boot, Ex. // if you choose default folder created by YOCTO setenv nfsroot /{YOCTO_BUILD_DIR}/tmp/work/{TARGET}-poky-linux-gnueabi/{IMAGE}/1.0-r0/rootfs   OR // if you create custom directory for NFS setenv nfsroot /imx-boot/imx6q-sabre/nfs Now, we have to set kernel image name and device tree blob file name in the u-boot, setenv image < zImage name > setenv fdt_file <dtb file name on host> Now, set the bootargs for the kernel boot, setenv netargs 'setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp' Use printenv command and check loadaddr and fdt_addr environment variables variables for I.MX6Q SABRE, loadaddr=0x12000000 fdt_addr=0x18000000   Also, check netboot environment variable. It should be like below, netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi; Now, set environment variable bootcmd to boot every time from the network, setenv bootcmd run netboot Now finally save those variable in u-boot: saveenv Reset your board; it should now boot from the network: U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b (Apr 17 2018 - 17:13:43 +0530)  (..) Net:   FEC [PRIME] Normal Boot Hit any key to stop autoboot:  0   Booting from net ... Using FEC device TFTP from server 192.168.0.206; our IP address is 192.168.3.101 Filename 'zImage'. Load address: 0x12000000 Loading: #################################################################         #################################################################         #################################################################         #################################################################         #################################################################         #################################################################         ###########################################################         2.1 MiB/s done Bytes transferred = 6578216 (646028 hex) Using FEC device TFTP from server 192.168.0.206; our IP address is 192.168.3.101 Filename 'imx6q-sabresd.dtb'. Load address: 0x18000000 Loading: ####         1.8 MiB/s done Bytes transferred = 45893 (b345 hex) Kernel image @ 0x12000000 [ 0x000000 - 0x646028 ] ## Flattened Device Tree blob at 18000000   Booting using the fdt blob at 0x18000000   Using Device Tree in place at 18000000, end 1800e344 switch to ldo_bypass mode!   Starting kernel ...
View full article
           This application note shows how to get i.MX6X development resources from Freescale website. Contents           We can enter Freescale i.MX website by the follow link http://www.freescale.com/imx, and after we input it into the IE address, it will remap to the new address of http://www.freescale.com/webapp/sps/site/homepage.jsp?code=IMX_HOME&tid=vanIMX. And the website page will have all the i.MX chipsets access web link like the follows:       And if we enter the i.MX6 serials Processors web link http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=IMX6X_SERIES , we will get the page like the follows:        Which have all the i.MX6 serials processors feature lists and website links. 1       i.MX6Q/D website guide. We enter the i.MX6D/Q web link http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&webpageId=129226228141673454B24A&nodeId=018rH3ZrDRB24A&fromPage=tax its main page as follows:    The Documentation and Software&Tools items is very important to get the design resource, and the Buy/Parametrics item will have the development board and chipset order information 1.1    i.MX6Q/D Documentation      We enter the Documentation item link: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Documentation_Tab, which will have our documentation materials include the Datasheet, Errata, Application Notes, Reference manual, User guides, Fact Sheets and related supporting information. 1.1.1  i.MX6Q/D DataSheet          We have i.MX6Q/D datasheets of automotive, consumer and industrial, the datasheet will have the chipset mark number, electrical, thermal and package information. IMX6DQAEC i.MX 6Dual/6Quad Automotive and Infotainment Applications Processors IMX6DQCEC i.MX 6Dual/6Quad Applications Processors for Consumer Products IMX6DQIEC i.MX 6Dual/6Quad Applications Processors for Industrial Products 1.1.2  i.MX6Q/D Errata       Chipset Errata will show us our current version chipset bugs and rework method. IMX6DQCE Chip Errata for the i.MX 6Dual/6Quad 1.1.3  i.MX6Q/D  Application Notes AN4724 i.MX 6Dual/6Quad Product Usage Lifetime Estimates AN4629 Fast Image Processing with i.MX 6 Series AN4671 i.MX 6 Series HDMI Test Method for Eye Pattern and Electrical Characteristics AN4397      //all the i.MX6 Serial can use the same PCB, this doc descript the hardware design difference Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite AN4581 Secure Boot on i.MX50, i.MX53, and i.MX 6 Series using HABv4 AN4509   //explan the i.MX6D/Q power consumption in every working features. i.MX 6Dual/6Quad Power Consumption Measurement AN4589 Configuring USB on i.MX 6 Series Processors AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors AN4467 //explain the ddr calibration method, need check with FSL FAE for DDR test calibration tools i.MX 6 Series DDR Calibration AN4579 // explain the thermal design i.MX 6 Series Thermal Management Guidelines 1.1.4  i.MX6Q/D Chipset reference manual IMX6DQRM //i.MX6DQ reference manual for all the internal module description and registers define. i.MX 6Dual/6Quad Applications Processor Reference Manual IMX6DQ6SDLSRM   // i.MX6DQ security related reference manual, need NDA approve. Security Reference Manual for i.MX 6 1.1.5  i.MX6Q/D User guide IMX6DQ6SDLHDG //i.MX6DQ hardware design user guide, include the schematic layout check points, hardware bring up… Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications EB792 i.MX 6 Series Standardized Signal Name Map EB793 MISRA Compliance in Freescale Automotive C Language Header Files - Engineering Bulletin 1.1.6  i.MX6Q/D Fact Sheet IMX6SRSFS i.MX 6 Series of Applications Processors - Fact Sheet 1.1.7  i.MX6Q/D BSP/Codec Software Document L3.0.35_4.0.0_LINUX_DOCS   i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Documentation. Includes Release Notes, Reference Manual,... MX6 folder include the BSP release notes, reference manual, user guide and other APIs doc. L3.0.35_4.0.0_LINUX_MMDOCS   i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Multimedia Codecs Documentation. Includes CODECs Release... IMX6_JB422_100_ANDROID_DOCS   i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Documentation. Includes Release Notes, User's... 1.1.8  i.MX6Q/D InfoCTR IMX_INFOCTR //TIC support center i.MX Infocenter—Online Documentation 1.2    i.MX6Q/D  Software&Tools We enter into the Software&Tools item page: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Design_Tools_Tab 1.2.1  i.MX6Q/D  Reference Designs SABRE Platform for Smart Devices Based on the i.MX 6 Series  The Smart Application Blueprint for Rapid Engineering (SABRE) platform for smart devices allows you to hold in your hands and evaluate the full multimedia performance capabilities of i.MX 6 series applications processors based on ARM® Cortex™-A9 technology.  Targeted for any device ... Enter it: Press Buy: SABRE Board for Smart Devices Based on the i.MX 6 Series  Freescale's Smart Application Blueprint for Rapid Engineering (SABRE) board for smart devices introduces developers to quad-core processing, low-power consumption and leading-edge multimedia and graphics applications on the i.MX 6Quad ARM ® Cortex™ -A9 applications processor. The SABRE board for smart devices ... Enter it: Press Buy:   SDB board share the same PCB with SDP, but have no camera, LVDS and GPS moduel. SABRE for Automotive Infotainment Based on the i.MX 6 Series  The Smart Application Blueprint for Rapid Engineering (SABRE) for automotive infotainment offers a solid foundation for next-generation converged telematics and infotainment platform designs. Based on i.MX 6 series of applications processors, Freescale's most scalable implementation of the ARM® Cortex™-A9 CPU ... Enter it: Press Buy:    Which have the CPU board and automotive base board, And if need the automotive board LVDS display panel, we can enter the i.MX53 automotive board link to get the order name. SABRE Lite Development Kit: The SABRE Lite Development Kit includes one SABRE Lite board, one 5V power adapter, one customized serial cable, one cross serial cable (DB9-DB9), one USB cable, one net cable and one 4GByte micro SD... Format: html    Saber Lite board a mini system board which use the separate power design, which launch by 3 rd party. 1.2.2  i.MX6Q/D  PCB and Schematic i.MX6_SABRE_AI_DESIGNFILES   : Design files, including hardware schematics, layout files and BOM. Size (K): 39164 Format: zip Rev #: 1.0.2 Modified: 2/27/2013 i.MX6_SABRE_SDP_DESIGNFILES   : Design files, including hardware schematics, Gerbers, and OrCAD files.. Size (K): 11631 Format: zip Rev #: C3 Modified: 3/21/2013 iMX6_SABRE_SDB_DESIGNFILES   : Design files, including hardware schematics, Gerbers, and OrCAD files.. Size (K): 9541 Format: zip Rev #: C3 Modified: 3/21/2013 1.2.3  i.MX6Q/D  Programmers Tools IMX_6DQ_MFG_TOOL   : Tool and documentation for downloading OS images to the i.MX 6Quad and i.MX6Dual. Size (K): 69444 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 IMX_MFG_TOOL_V2_SOURCE   : Source Code for the i.MX manufacturing tool used for downloading OS images to the i.MX 6 Processors. Size (K): 955 Format: zip Rev #: 2.1.1 Modified: 12/19/2012 1.2.4  i.MX6Q/D  Software IMX_6D_Q_VIVANTE_VDK_145_TOOLS   : Set of applications for the Linux L3.0.35_4.0.0 BSP, designed to be used by graphics application developers to rapidly develop and port graphics applications. Includes applications, GPU Driver with vprofiler enabled and documentation.. Size (K): 40113 Format: zip Rev #: 1.4.5 Modified: 5/13/2013 IMX6_GPU_SDK   : i.MX6 Graphics SDK – Includes sample, demo code, and documentation for working with the i.MX6X family graphics cores. Includes OpenVG, OpenGL ES, and GAL2D reference files. Size (K): 21065 Format: gz Rev #: 1.0.0 Modified: 1/25/2013 i.MX 6Series Platform SDK   : Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license. Size (K): 29865 Format: tgz Rev #: 1.1 Modified: 2/11/2013      A non-OS i.MX6X driver test codes.  1.2.5  i.MX6Q/D  Tools IMX_CST_TOOL   : Freescale Code Signing Tool for the High Assurance Boot library. Provides software code signing support designed for use with i.MX processors that integrate the HAB library in the internal boot ROM. Size (K): 3855 Format: tgz Rev #: 2.0 Modified: 11/16/2012      Please still refer the document of i.MX6Q/D security RM and HAB application notes. IMX6_IOMUX_TOOL   : Interactive i.MX Pin Mux Tool.. Size (K): 5313 Format: zip Rev #: 3.4.0.3 Modified: 2/14/2013      Please still refer the document of i.MX6Q/D iomux table. 1.2.6  i.MX6Q/D  BSDL IMX6_DQ_BSDL   : i.MX 6Quad and i.MX 6Dual BSDL File. Size (K): 64 Format: zip Rev #: 2 Modified: 1/15/2013        A Boundary scan file for manufacture ICT test. 1.2.7  i.MX6Q/D  IBIS IMX6_DQ_IBIS   : i.MX 6Quad and i.MX 6Dual IBIS File. Size (K): 19173 Format: zip Rev #: 1 Modified: 11/9/2012       Use for signals simulation. 1.2.8  i.MX6Q/D  BSP IMX6_DQ_SABRE_AI_SD_DEMO_IMAGE   : Demo Image Flashed on the i.MX 6Quad SABRE AI SD Cards. Size (K): 1789607 Format: exe Rev #: L3.0.35_1.1.1 Modified: 4/23/2013 IMX6_DQ_SDB_SD_DEMO_IMAGE   : Demo Image Flashed on the i.MX 6Quad SDB SD Cards. Size (K): 1670416 Format: exe Rev #: R13.4.1 Modified: 4/24/2013 IMX6_DQ_SDP_SD_DEMO_IMAGE   : Demo Image Flashed on the i.MX 6Quad SDP SD Cards. Size (K): 1670892 Format: exe Rev #: R13.4.1 Modified: 4/24/2013 L3.0.35_4.0.0_DEMO_IMAGE   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Binary Demo Files. Size (K): 359441 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 IMX6_JB422_100_ANDROID_DEMO   : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Binary Demo Files. Size (K): 836432 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/8/2013 Demo image for customer to evaluate on Freescale’s board. IMX6_JB422_100_ANDROID_SOURCE   : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP, Documentation and Source Code for BSP and Codecs.. Size (K): 235533 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/9/2013 Android JB422 source codes, still have the R13.41 android source codes in the same web folder. L3.0.35_4.0.0_ER_SOURCE   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Source Code Files. Size (K): 1064236 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 Linux LTIB source codes package. L3.0.35_4.0.0_UBUNTU_RFS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux File System for the Ubuntu Images. Size (K): 820076 Format: tgz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 Ubuntu rootfs working on our linux BSP. 1.2.9  i.MX6Q/D  Software Codecs IMX6_JB422_100_AACP_CODEC   : AAC Plus Codec for i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0. Size (K): 84 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/15/2013    Android have no codec package except AACP, have include in the BSP release codes. L3.0.35_4.0.0_AACP_CODECS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux AAC Plus Codec. Size (K): 1377 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 L3.0.35_4.0.0_MM_CODECS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Multimedia Codecs Sources. Size (K): 79197 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013    Linux have MM codec package. 1.2.10              i.MX6Q/D  Updates and Patches   Which have the older patch on L3.0.35 elder version, and Android R13.4/13.4.1. 2       i.MX6DL/S website guide. We enter the i.MX6DL/S web link http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&webpageId=129226228141673454B24A&nodeId=018rH3ZrDRB24A&fromPage=tax    its main page as follows: 2.1    i.MX6DL/S Documentation http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Documentation_Tab 2.1.1  i.MX6DL/S DataSheet IMX6SDLAEC i.MX 6Solo/6DualLite Automotive and Infotainment Applications Processors IMX6SDLCEC i.MX 6Solo/6DualLite Applications Processors for Consumer Products IMX6SDLIEC i.MX 6Solo/6DualLite Applications Processors for Industrial Products 2.1.2  i.MX6DL/S Errata IMX6SDLCE Chip Errata for the i.MX 6Solo/6DualLite 2.1.3  i.MX6DL/S D  Application Notes IMX6SDLIEC i.MX 6Solo/6DualLite Applications Processors for Industrial Products AN4576 i.MX 6DualLite Power Consumption Measurement 2.1.4  i.MX6DL/S Chipset reference manual IMX6SDLRM i.MX 6Solo/6DualLite Applications Processor Reference Manual IMX6DQ6SDLSRM   Security Reference Manual for i.MX 6 2.1.5  i.MX6DL/S User Guide IMX6DQ6SDLHDG Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications EB793 MISRA Compliance in Freescale Automotive C Language Header Files - Engineering Bulletin 2.1.6  i.MX6DL/S Fact Sheet IMX6SRSFS i.MX 6 Series of Applications Processors - Fact Sheet 2.1.7  i.MX6DL/S BSP/Codec Software Document L3.0.35_4.0.0_LINUX_DOCS   i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Documentation. Includes Release Notes, Reference Manual,... L3.0.35_4.0.0_LINUX_MMDOCS   i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Multimedia Codecs Documentation. Includes CODECs Release... IMX6_JB422_100_ANDROID_DOCS   i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Documentation. Includes Release Notes, User's... 2.1.8  i.MX6DL/S InfoCTR IMX_INFOCTR i.MX Infocenter—Online Documentation 2.2    i.MX6DL/S Software&Tools http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Design_Tools_Tab 2.2.1  i.MX6DL/S Reference Designs SABRE Platform for Smart Devices Based on the i.MX 6 Series  The Smart Application Blueprint for Rapid Engineering (SABRE) platform for smart devices allows you to hold in your hands and evaluate the full multimedia performance capabilities of i.MX 6 series applications processors based on ARM® Cortex™-A9 technology.  Targeted for any device ... SABRE for Automotive Infotainment Based on the i.MX 6 Series  The Smart Application Blueprint for Rapid Engineering (SABRE) for automotive infotainment offers a solid foundation for next-generation converged telematics and infotainment platform designs. Based on i.MX 6 series of applications processors, Freescale's most scalable implementation of the ARM® Cortex™-A9 CPU ... 2.2.2  i.MX6DL/S PCB and Schematic i.MX6_SABRE_AI_DESIGNFILES   : Design files, including hardware schematics, layout files and BOM. Size (K): 39164 Format: zip Rev #: 1.0.2 Modified: 2/27/2013 I.MX_6DL_S_VIVANTE_VDK_TOOLS   : i.MX6DL and i.MX6S Vivante VDK Tools. Size (K): 39752 Format: zip Rev #: 1.4.1 Modified: 1/4/2013 i.MX 6Series Platform SDK   : Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license. Size (K): 29865 Format: tgz Rev #: 1.1 Modified: 2/11/2013 2.2.3  i.MX6DL/S Programmers Tools IMX_6DL_6S_MFG_TOOL   : Tool and documentation for downloading OS images to the i.MX 6DualLite and i.MX6Solo. Size (K): 67584 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 2.2.4  i.MX6DL/S  Software 2.2.5  i.MX6DL/S BSDL IMX6_DL_S_BSDL   : i.MX 6DualLite and i.MX 6Solo BSDL File. Size (K): 81 Format: html Rev #: 1 Modified: 11/9/2012 2.2.6  i.MX6DL/S IBIS IMX6_DL_S_IBIS   : i.MX 6DualLIte and i.MX 6Solo IBIS File. Size (K): 15450 Format: zip Rev #: 1 Modified: 11/9/2012 2.2.7  i.MX6DL/S BSP IMX6_DL_SDP_SD_DEMO_IMAGE   : Demo Image Flashed on the i.MX 6DualLiteSDP SD Cards. Size (K): 367806 Format: zip Rev #: R13.4.1 Modified: 12/10/2012 IMX6_JB422_100_ANDROID_DEMO   : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP Binary Demo Files. Size (K): 836432 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/8/2013 L3.0.35_4.0.0_DEMO_IMAGE   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Binary Demo Files. Size (K): 359441 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 IMX6_JB422_100_ANDROID_SOURCE   : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0 BSP, Documentation and Source Code for BSP and Codecs.. Size (K): 235533 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/9/2013 L3.0.35_4.0.0_ER_SOURCE   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Source Code Files. Size (K): 1064236 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 L3.0.35_4.0.0_UBUNTU_RFS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux File System for the Ubuntu Images. Size (K): 820076 Format: tgz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 2.2.8  i.MX6DL/S Software Codecs IMX6_JB422_100_AACP_CODEC   : AAC Plus Codec for i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android jb4.2.2_1.0.0. Size (K): 84 Format: gz Rev #: jb4.2.2_1.0.0 Modified: 5/15/2013 L3.0.35_4.0.0_AACP_CODECS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux AAC Plus Codec. Size (K): 1377 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 L3.0.35_4.0.0_MM_CODECS   : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux Multimedia Codecs Sources. Size (K): 79197 Format: gz Rev #: L3.0.35_4.0.0 Modified: 5/13/2013 2.2.9  i.MX6Q/D  Updates and Patches Which have the older patch on L3.0.35 elder version, and Android R13.4/13.4.1. 3       i.MX6SL website guide. http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&webpageId=129226228141673454B24A&nodeId=018rH3ZrDRB24A&fromPage=tax 3.1    i.MX6SL Documentation http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Documentation_Tab 3.1.1  i.MX6SL DataSheet IMX6SLCEC i.MX 6SoloLite Applications Processors for Consumer Products 3.1.2  i.MX6SL Errata IMX6SLCE Chip Errata for the i.MX 6SoloLite 3.1.3  i.MX6SL Application Notes AN4726 i.MX 6SoloLite Product Usage Lifetime Estimates AN4580 i.MX 6SoloLite Power Consumption Measurement 3.1.4  i.MX6SL Chipset reference manual IMX6SLRM i.MX 6SoloLite Applications Processor Reference Manual 3.1.5  i.MX6SL User guide IMX6SLHDG Hardware Development Guide for i.MX 6SoloLite Applications Processors - User Guide 3.1.6  i.MX6SL Fact  Sheet IMX6SRSFS i.MX 6 Series of Applications Processors - Fact Sheet IMX6SLEVKFS i.MX 6SoloLite Evaluation Kit - Fact Sheet 3.1.7  i.MX6SL BSP/Codec Software Document L3.0.35_2.1.0_LINUX_DOCS   i.MX 6SoloLite Linux BSP Documentation. Includes Release Notes, Reference Manual, User guide. API Documentation L3.0.35_2.1.0_LINUX_MMDOCS   i.MX 6SoloLite Linux Multimedia Codecs Documentation. Includes CODECs Release Notes and User's Guide IMX6_R13.5_ANDROID_DOCS_BUNDLE   i.MX 6 Sololite Android GA BSP Documentation. 3.1.8  i.MX6SL INFOCTR IMX_INFOCTR i.MX Infocenter—Online Documentation 3.2    i.MX6SL Software&Tools http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Design_Tools_Tab 3.2.1  i.MX6SL Reference Designs IMX6SLEVK: i.MX 6SoloLite Evaluation Kit. Freescale delivers the next installment in a line of highly-flexible, market-focused development tools with an Evaluation Kit (EVK) based on the i.MX 6SoloLite applications processor. The i.MX 6SoloLite is the first... Format: html Modified: 6/4/2013 3.2.2  i.MX6SL PCB and Schematics iMX6SL_EVK_DESIGNFILES   : Design files, including hardware schematics, Gerbers, and OrCAD files.. Size (K): 6034 Format: zip Rev #: 1 Modified: 11/12/2012 3.2.3  i.MX6SL Programmers Tools IMX_6SL_MFG_TOOL   : Tool and documentation for downloading OS images to the i.MX 6SoloLite. Size (K): 46502 Format: gz Rev #: L3.0.35_2.1.0 Modified: 5/24/2013 3.2.4  i.MX6SL Tools IMX_CST_TOOL   : Freescale Code Signing Tool for the High Assurance Boot library. Provides software code signing support designed for use with i.MX processors that integrate the HAB library in the internal boot ROM. Size (K): 3855 Format: tgz Rev #: 2.0 Modified: 11/16/2012 IMX6_IOMUX_TOOL   : Interactive i.MX Pin Mux Tool.. Size (K): 5313 Format: zip Rev #: 3.4.0.3 Modified: 2/14/2013 3.2.5  i.MX6SL Software i.MX 6Series Platform SDK   : Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code. Also includes register definition headers files, and register definitions for debuggers. BSD open source license. Size (K): 29865 Format: tgz Rev #: 1.1 Modified: 2/11/2013 3.2.6  i.MX6SL BSDL IMX6_SL_BSDL   : i.MX 6SoloLite BSDL File. Size (K): 54 Format: html Rev #: 1 Modified: 11/9/2012 3.2.7  i.MX6SL IBIS IMX6_SL_IBIS   : i.MX 6SoloLite IBIS File. Size (K): 25706 Format: zip Rev #: 1 Modified: 11/9/2012 3.2.8  i.MX6SL BSP IMX6_R13.5_ANDROID_DEMO_IMAGE   : i.MX 6Sololite GA BSP Binary Demo Files. Size (K): 372634 Format: gz Rev #: R13.5 Modified: 11/16/2012 L3.0.35_12.10.02_DEMO_IMAGE   : Linux Binary Demo Files for i.MX 6SoloLite Linux GA BSP. Size (K): 434356 Format: gz Rev #: 12.10.02 Modified: 11/9/2012 L3.0.35_2.1.0_DEMO_IMAGE   : i.MX 6SoloLite Linux Binary Demo Files. Size (K): 464844 Format: gz Rev #: L3.0.35_2.1.0. Modified: 6/4/2013 IMX6_R13.5_ANDROID_SOURCE_CODE   : i.MX 6 Sololite Android GA BSP Documentation and Source Code for BSP and Codecs.. Size (K): 100683 Format: gz Rev #: R13.5 Modified: 11/16/2012 L3.0.35_12.10.02_ER_SOURCE   : i.MX 6SoloLite Linux GA BSP 3.0.35 Source Code Files.. Size (K): 872027 Format: gz Rev #: 12.10.02 Modified: 11/9/2012 L3.0.35_12.10.02_UBUNTU_RFS   : File System for the Ubuntu Imagea for i.MX 6SoloLite Linux GA BSP. Size (K): 810816 Format: tgz Rev #: 12.10.02 Modified: 11/9/2012 L3.0.35_2.1.0_ER_SOURCE   : i.MX 6SoloLite Linux BSP Source Code Files. Size (K): 1064541 Format: gz Rev #: L3.0.35_2.1.0. Modified: 6/4/2013 3.2.9  i.MX6SL Software Codecs L3.0.35_2.1.0_AACP_CODECS   : i.MX 6SoloLite Linux AAC Plus Codec. Size (K): 1374 Format: gz Rev #: L3.0.35_2.1.0 Modified: 5/24/2013 L3.0.35_2.1.0_MM_CODECS   : i.MX 6SoloLite Linux Multimedia Codecs Sources. Size (K): 45883 Format: gz Rev #: L3.0.35_2.1.0 Modified: 5/24/2013 3.2.10              i.MX6SL Updates and Patches IMX6_R13.5_01_ANDROID_PATCHES   : Android 13.5.0-GA.01 patch release. It adds camera support (USB and CSI camera), provides some bug fixes, and includes some regular updates. The 13.5.0-GA.01 patch release is based on 13.5.0-GA.. Size (K): 186882 Format: gz Rev #: R13.5-GA.01 Modified: 1/4/2013 Which have the older patch on L3.0.35 elder version, and Android R13.5.         
View full article
本文已经发表于中国集成电路杂志2014年第七期 For English version, please check following link. Freescale i.MX6 DRAM Port Application Guide-DDR3
View full article
meta-avs-demos Yocto layer meta-avs-demos is a Yocto meta layer (complementary to the NXP BSP release for i.MX) published on CodeAurora that includes the additional required packages to support  Amazon's Alexa Voice Services SDK (AVS_SDK) applications. The build procedure is the described on the README.md of the corresponding branch. We have 2 fuctional branches now: imx-alexa-sdk: Support for Morty based i.mx releases imx7d-pico-avs-sdk_4.1.15-1.0.0: legacy support for Jethro releases The master branch is only used to collect manifest files, that used with repo init/sync commands will fetch the whole environment for the 2 special supported boards: i.MX7D Pico Pi and i.MX8M EVK. However the meta-avs-demos can be used with any i.MX board either. Recipes to include Amazon's Alexa Voice Services in your applications. The meta-avs-demos provides the required recipes to build an i.MX image with the support for running Alexa SDK. The imx-alexa-sdk branch is based on Morty and kernel 4.9.X and it supports the next builds: i.MX7D Pico Pi i.MX8M EVK Generic i.MX board For the i.MX7D Pico Pi and i.MX8M EVK there is an extended support for additional (external) Sound Cards like: TechNexion VoiceHat: 2Mic Array board with DSPConcepts SW support Synaptics Card: 2 Mic with Sensory WakeWord support The Generic i.MX is for any other regular i.MX board supported on the official NXP BSP releases. Only the default soundcard (embedded) on the board is supported. Sensory wakeword is currently only enabled for those with ARMV7 architecture. To support any external board like the VoiceHat or Synaptics is up to the user to include the additional patches/changes required. Build Instructions Follow the corresponding README file to follow the steps to build an image with Alexa SDK support README-IMX7D-PICOPI.md README-IMX8M-EVK.md README-IMX-GENERIC.md
View full article
Description by Google:      Wi-Fi scan-only mode is a new platform optimization that lets users keep Wi-Fi scan on without connecting to a Wi-Fi network, to improve location accuracy while conserving battery. Apps that depend on Wi-Fi for location services can now ask users to enable scan-only mode from Wi-Fi advanced settings. Wi-Fi scan-only mode is not dependent on device hardware and is available as part of the Android 4.3 platform. Comments by Freescale:      In order to enable wifi scan mode, we should make sure wifi driver shouldn't be removed while switching off wifi from Setting. Additionally, android4.3 has introduced one CTS test to force us to change all loadable modules into kernel built in. The reason is loadable modules are often used by rootkits and other exploits. so there will be big risk in security. OK, now let's try to keep up with the pace of AOSP.      For AR6003, we are using compat-wireless driver which accommodates all linux kernel since 2.6.We are now using olca-3.4 wifi driver but our kernel version is 3.0.35.  It is not a simple change to be directly compiled into kernel since it is lack of the basic file structure for ath6kl driver. This has been double confirmed by support guy from Atheros. More terribly, Atheros has no plan to publish new version for AR6003 but just maintain it. Yeah, my pitiful baby. Say goodbye to scan mode.      This is why this document come into being. AR6003 is our default wifi module bounded to our imx6 serial board. So formal release will lose this important feature for this limitation. Here I will give out patches to enable this feature using another wifi module-----Realtek 8723as. Ok, now let's welcome this new star. Patches description:          Patch for kernel--------Change loadable driver modules to compiled into kernel, this will let wlan0 and p2p0 interfaces still can be operated although you have switched off wifi in Setting UI.      Patch for device/fsl--------Firstly, I delete one rfkill operation in init.rc which is obsolete for BT setting. If still keep it here, it will soft block wifi interface through mac80211 rfkill. Then I clean up some setting for wifi driver module.      Patch for hardware/libhardware_legacy-------Since wifi driver is already directly built in kernel, HAL will have no need to load driver now. Refactor it and optimize it. Test it manually:          If you have one sdio rtl8723as wifi module in hand, you can test it like the following to see wifi scan mode works: Firstly, disable wifi in Setting UI. then you can check netcfg result, you will see wlan0 and p2p0 are still there, only down state: Go "advanced" menu in wifi setting,Turning on the checkbox of "Scanning always available". Check netcfg result again, Oh Oh, wlan0 and p2p0 are up: Manually "scan" through "wpa_cli" tool, you will see it works:
View full article
When to enable CONFIG_DEBUG_LL, choose the debug port and then CONFIG_EARLY_PRINTK on i.MX6, system will hang. There is no error information there as below, Uncompressing Linux... done, booting the kernel. Booting Linux on physical CPU 0x0 Initializing cgroup subsys cpu Initializing cgroup subsys cpuacct Linux version 4.1.15-00001-gd582989-dirty (jay@jay-ubuntu) (gcc version 4.9 20 150123 (prerelease) (GCC) ) #10 SMP PREEMPT Mon Jul 17 15:08:55 CST 2017 CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: Freescale i.MX6 Quad SABRE Smart Device Board bootconsole [earlycon0] enabled cma: Reserved 448 MiB at 0x2a000000 Memory policy: Data cache writealloc -------------- hang -----------------‍‍‍‍‍‍‍‍‍‍‍‍‍ The patch fix it on android n7.1.1_1.0.0, kernel: 4.1.15.
View full article
Some customer need to know how to add support RS485 mode half duplex? Here give some recommends. About i.MX6 UART to RS485 applications 1. Using RS485 mode of UART directly. On hardware, you should use UART_CTS_B to control RX & TX. On software, The link for you reference: Does UART in RS485 mode support only 9 Bit mode for i.MX6 ?  2. Sensing IO direction Automatically via hardware, don't need to tune software. For i.MX8QXP As the linux BSP for i.MX8QXP do not support RS 485 mode, so for the RS 485 using you can use the Sensing IO direction Automatically via hardware, don't need to tune software. As the above i.MX6 design.
View full article
Qt Creator can be a very good IDE in order to develop great QT applications. This IDE does not only helps with syntax highlighting, access to examples and tutorials, but also helps you to configure different toolchains Qt binary versions and target options. First download the binary installer from: For 32 bits: $ wget http://releases.qt-project.org/qtcreator/2.6.2/qt-creator-linux-x86-opensource-2.6.2.bin For 64 bits: $ wget http://releases.qt-project.org/qtcreator/2.6.2/qt-creator-linux-x86_64-opensource-2.6.2.bin execute the binary $ ./qt-creator-linux-x86_64-opensource-2.6.2.bin Follow the Installer GUI and choose a location. Default options should be OK. in my case the installation was done here: $ /home/b35153/qtcreator-2.6.2/bin Open Qt Creator (in my case from command line, use "&" to regain control of the terminal) $./qtcreator & Open Tools -> Options Choose Build & Run  on the menu of the left. and Select the Compilers Tab Here you can add the toolchain GCC compiler of your convenience. It will appear in the "Manual"  section. Now click on Qt Version Tab.  Here you can add the Qmake that you had created with your Qt installation; for example, the Qt5 installation described here: Building QT for i.MX6 It will appear in the Manual section. In my case I have Qmake for PC and Qmake for i.MX6. Now click on Kits Tab Here you can create combinations of Compilers and Qmake, and also specify where do you want the executables to go. In my case here I combined the i.MX6 toolchain and the Qmake for I.MX6 i had created. I did not set up device configuration since the sysroot is already shared to my device via NFS, but you can configure it so the files are sent via ssh to your device. And that's It! Next time you load a project you can choose which Kit you want to work on, and it will be compiled just as you need.
View full article
ccache is a C compiler cache. ccache can save a large amount of compilation time on recurring builds and builds restarted from a clean repository after make clean or git clean. It is well suited for e.g. u-boot and Linux compilation. Caching the host compiler Caching "native" builds is easily done by adding in the beginning of your $PATH a special directory, which contains links to ccache to override the usual compiler. On e.g. Debian this directory is readily available as /usr/lib/ccache, So you can do:   $ export PATH="/usr/lib/ccache:$PATH" Typical links found in this folder are:   c++ -> ../../bin/ccache   cc -> ../../bin/ccache   g++ -> ../../bin/ccache   gcc -> ../../bin/ccache etc... Caching the cross compiler Caching cross-compiled builds can be done in the same way as native builds, provided you create links of the form e.g. arm-linux-gnueabihf-gcc pointing to ccache. But there is an even more convenient way for those projects, which rely on a $CROSS_COMPILE environment variable (as is the case for e.g. u-boot and Linux). You can prefix the cross compiler with ccache there in e.g. the following way:   $ export CROSS_COMPILE="ccache arm-linux-gnueabihf-" Monitoring efficiency Now that your builds are cached, you might want to see how much is "spared" with this technique. ccache -s will tell you all sorts of statistics, such as:   cache directory                     /home/vstehle/.ccache   cache hit (direct)                 10852   cache hit (preprocessed)            3225   cache miss                         19000   called for link                    33267   called for preprocessing            9463   compile failed                         3   preprocessor error                     1   couldn't find the compiler           117   unsupported source language          921   unsupported compiler option         2167   no input file                      31681   files in cache                     51694   cache size                           1.3 Gbytes   max cache size                       4.0 Gbytes Here you see a somewhat typical 50%/50% hit/miss ratio. Enjoy! See Also ccache is usually supported natively by build systems, such as Buildroot or Yocto.
View full article
Q: how to do PCIe compliance measurement on the Sabre SDB? Phase Jitter on the PCIe reference clock had been see problem. Pin C7  "CLK1_N" and Pin D7 "CLK1_P"  were used like on the Sabre SD. During Compliance meassurments  margin of -80% and more.... was seen. Is there a known issue? Has someone done a similar compliance measurement on the Sabre SDB? A: The PCIe TX compliance tests on i.MX6 SD boards in TK's Open Lab.  Based on the internal PLL clock, i.MX6 SD boards pass the PCIe TX compliance tests. 1, please check the capacitor on NVCC_PLL_OUT, it should no less than 10uF, 22uF is better. 2, please check if the 24MHz input crystal is good enough. 50ppm is required. 3, please check the test step: 1.1     TX Test Configuration and Procedures Overview of Test Steps 1.      Integrate the patch for PCIE test to mainline, recompile the Kernel , and replace the old image of the board under test. ·         Make sure the following configuration has been set, when re-compiling the kernel image. # MX6 Options: # CONFIG_IMX_PCIE=y 2.      Correctly set up the test environment: ·         Connect the compliance load board (CLB x1/x16) revision 2.0 into the slot of DUT, and change the switch and jumpers to select x1 . ·         Connect the lane under test to oscilloscope via differential probe and matched coaxial , do remember that cable calibration should be done before test. ·         Connect the clock signal to the oscilloscope. The clock must have SSC enabled or disabled to be consistent with settings for the system during normal operation. ·         Power on the system. 3.      After I.MX6x enters Polling.Compliance , press the Toggle Button on CLB to select the output , make sure the data waveform is compliance pattern, 5.0GT/s for GEN2, 2.5GT/s for GEN1. 4.      Follow the Oscilloscope operation instruction, set it to the right mode. 5.      Capture and save at least 1 million * 200 ps of data and clock simultaneously at the sample rate of 50GS/s for GEN2, or 250,000 UI * 400 ps of data at the sample rate of 25GS/s for GEN1. 6.      Run free software Sigtest to analyze the PCIE TX signal. 7.      Customer could adjust the parameters of the PCIE_PHY by changing IOMUXC_GPR8 register settings to get the test past. a.       The default of this Register is configured as: imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN1, 0 << 0, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN2_3P5DB, 0 << 6, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_DEEMPH_GEN2_6DB, 20 << 12, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_SWING_FULL, 127 << 18, IOMUXC_GPR8); imx_pcie_clrset(IOMUXC_GPR8_TX_SWING_LOW, 127 << 25, IOMUXC_GPR8); b.      write the Register, Address: 20E_0000h base + 20h offset = 20E_0020h; command: /unit_tests/memtool -32 0x020e0020= FFFD4000 This document was generated from the following discussion: i.Mx6 PCIe compliance
View full article
Multiple-Display means video playback on multiple screens. In case playback needs to be in a unique screen, the mfw_isink element must be used and some pipelines examples can be found on this link: GStreamer iMX6 Multi-Overlay. Number of Displays Display type Kernel parameters Pipelines # Set these shells variables before running the pipelines alias gl=gst-launch SINK_1="\"mfw_v4lsink device=/dev/video17\"" SINK_2="\"mfw_v4lsink device=/dev/video18\"" SINK_3="\"mfw_v4lsink device=/dev/video20\"" media1=file:///root/media1 media2=file:///root/media2 media3=file:///root/media3 2 hdmi + lvds video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 gl playbin2 uri=$media1 video-sink=$SINK_1 playbin2 uri=$media2 video-sink=$SINK_2 2 lvds + lvds video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 gl playbin2 uri=$media1 video-sink=$SINK_1 playbin2 uri=$media2 video-sink=$SINK_2 2 lcd + lvds video=mxcfb0:dev=lcd,800x480M@55,if=RGB565 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 gl playbin2 uri=$media1 video-sink=$SINK_1 playbin2 uri=$media2 video-sink=$SINK_2 3 hdmi + lvds + lvds video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:dev=ldb,LDB-XGA,if=RGB6 video=mxcfb2:dev=ldb,LDB-XGA,if=RGB666 gl playbin2 uri=$media1 video-sink=$SINK_1 playbin2 uri=$media2 video-sink=$SINK_2 playbin2 uri=$media3 video-sink=$SINK_3
View full article
Apply this patch into the LTIB folder.
View full article