i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
This is the procedure and patch to set up Ubuntu 13.10 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0. It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-13.10-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0 $ sudo apt-get install libc6-dev-i386 $ sudo apt-get install u-boot-tools $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd $ sudo ln -s /usr/lib/x86_64-linux-gnu/librt.so   /usr/lib/librt.so C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source. tar.gz $ ./L3.0.35_4.1.0_130816_source/install      After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 13.10 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_13.10_64bit_OS.patch What the patch is doing: a) The patch modifies the following files:    dist/lfs-5.1/base_libs/base_libs.spec    dist/lfs-5.1/m4/m4.spec    dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory:    pkgs/m4-1.4.16-1383761043.patch    pkgs/m4-1.4.16-1383761043.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 m4 compilation issue: 1. https://github.com/hashdist/hashstack/commit/f6be2a58de62327d05e052d89c9aa931d4c926b3 2. https://github.com/hashdist/hashstack/issues/81 rpm-fs package failed to build issue: https://community.freescale.com/message/355771#355771 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
View full article
This is the procedure and patch to set up Ubuntu 12.04 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0.  It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-12.04.3-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install ia32-libs libc6-dev-i386 lib32z1 $ sudo apt-get install uboot-mkimage $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source.tar.gz $ ./L3.0.35_4.1.0_130816_source/install After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 12.04 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_12.04_64bit_OS.patch The patch modifies the following files: dist/lfs-5.1/base_libs/base_libs.spec dist/lfs-5.1/ncurses/ncurses.spec E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
View full article
To build Android version earlier than Lollipop from source code, you need the Sun's 1.6 SDK to be installed for ubuntu as the link Initializing a Build Environment | Android Developers. You may still cannot get the Sun's JDK  with below instruction: $ sudo add-apt-repository "deb http://archive.canonical.com/ lucid partner" $ sudo apt-get update $ sudo apt-get install sun-java6-jdk    There are below options to help install the Sun's JDK  if you cannot find a valid source through apt-get commands: $ wget --no-cookies --header "Cookie: gpw_e24=http%3A%2F%2Fwww.oracle.com%2F" http://download.oracle.com/otn-pub/java/jdk/6u45-b06/jdk-6u45-linux-x64.bin $ chmod u+x jdk-6u45-linux-x64.bin $ ./jdk-6u45-linux-x64.bin $ sudo mv jdk1.6.0_45 /opt $ sudo update-alternatives --install /usr/bin/java java /opt/java/64/jdk1.6.0_45/bin/java 1 $ sudo update-alternatives --install /usr/bin/javac javac /opt/java/64/jdk1.6.0_45/bin/javac 1 $ sudo update-alternatives --install /usr/bin/jar jar /opt/java/64/jdk1.6.0_45/bin/jar 1 # if you have already install some other version of JDK, please export the JAVA_HOME env before your android build every time $ export JAVA_HOME=/opt/jdk1.6.0_45/ #or you can directly link the java binary to the sdk version you need as below: sudo ln -s /opt/java/64/jdk1.6.0_45/bin/jar /bin/jar sudo ln -s/opt/java/64/jdk1.6.0_45/java /bin/java sudo ln -s/opt/java/64/jdk1.6.0_45/javac /bin/javac sudo ln -s/opt/java/64/jdk1.6.0_45/javah /bin/javah sudo ln -s/opt/java/64/jdk1.6.0_45/javadoc /bin/javadoc sudo ln -s/opt/java/64/jdk1.6.0_45/javaws /bin/javaws    To built the Android version Lollipop and Marshmallow from source code, you need the OpenJDK 7 to be installed for ubuntu as the link Initializing a Build Environment | Android Developers. $ sudo apt-get update $ sudo apt-get install openjdk-7-jdk You may have both openjdk7 and SUN JDK 1.6 intalled in your ubuntu to build different Android version. If you have default java SDK to be Sun's JDK 1.6, you can just use below commands to make android build system use the openjdk7 for Lollipop built $ export JAVA_HOME=/usr/lib/jvm/java-7-openjdk-amd64/ $ cd myandroid $ . ./build/envsetup.sh           //be sure to resetup the envsetup, and pick the platform to be built $ lunch
View full article
by b47504 Overview This document is intended to introduce debug tips about i.MX power management based on i.MX Android software. The following topics are involved in this document: How to debug suspend/resume issues How to do power optimization How to debug suspend/resume issues General method: Capture more PM  debug message Enable PM debug system to get more info about PM in kernel and debug interface Power management options  ---> [*] Power Management Debug Support                                     [*]   Extra PM attributes in sysfs for low-level debugging/testing Enable wakelock debug_mask to capture more message about wakelock root@android:/ # echo 15 > /sys/module/wakelock/parameters/debug_mask root@android:/ # echo 15 > /sys/module/userwakelock/parameters/debug_mask Enable earlysuspend debug_mask to capture more message about early suspend and late resume. root@sabresd_6dq:/ # echo 15 > /sys/module/earlysuspend/parameters/debug_mask Add no_console_suspend=1 to the boot option for kernel This makes the system print more useful info before entry in suspend Eg: --- a/sabresd_6dq/BoardConfig.mk +++ b/sabresd_6dq/BoardConfig.mk -BOARD_KERNEL_CMDLINE := console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale +BOARD_KERNEL_CMDLINE := console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale no_console_suspend=1 System cannot enter suspend mode Check below setting items have been disabled: §  Whether the usb cable has been removed(usb gadget will hold a wake lock) §  Setting->Display->Sleep, check whether the inactivity timeout period setting is longer than your expected time. §  Setting->System->Developer options->stay awake(stay awake not be set), check whether the option is disabled Check if all wake locks have been released(You can see which wake lock is held, and then debug into the specific module): root@sabresd_6dq:/ # cat /sys/power/wake_lock System could not resume from suspend/System crash when resume or suspend Check the PMIC_STBY_REQ signal. System use PMIC_STBY_REQ signal to notify power management IC to change voltage from standby voltage to functional voltage and vice versa. In general, pmic_stby_req pin is connected to pmic standby pin. So measure the pin to check whether the  de-assert signal is triggered. If the signal is not triggered, we may consider whether wake-up sources are correctly setup. If the signal is triggered, we may double-check whether the pmic supply power normally. And not limited to the two points, we should also double-check everything we doubt according to the system log and hardware measured waves.  Using Trace32 or ICE to locate the problem. Please view trace32 website to get more details. Track from mx6_suspend_enter in arch/arm/mach-mx6 .                Track "state" value and try to map to different the low power mode via function mxc_cpu_lp_set.                Check "mx6_suspend.S" which conduct the detailed operations in suspend: "MEM" is mapped to "dormant" mode. So goto "dormant" symbol and try to dump different operations to narrow down suspend/resume failure If this failure maybe related to DDR operation, try to dummy DDR IO relative low power operation. Using ram console to dump kernel log after reboot. Ram console will keep one kernel log copy into one certain memory space. You can use the following command to check last time kernel log, if memory power was not cut off during the reboot process. Eg(if it is the first time boot, you cannot find the /proc/last_kmsg file): root@sabresd_6dq:/ # cat /proc/last_kmsg Kernel resume back from suspend but android not This is usually introduced by the wrong key layout file Use getevent/sendevent tool to get power key scan code #getevent  Correct the Keylayout file    system/usr/keylayout/****.kl Correct the scandcode with your power key report value to Match the POWE key Suspend/Resume consume too much time: We can print the specific module name and time consume details, if the module's suspend/resume time consume more than the threshold parameter by read/write /sys/power/device_suspend_time_threshold file. By default, the parameter is setup to 0, via disabled the function. We can enable it by the following command: Eg: root@android:/ # echo 10  > /sys/power/device_suspend_time_threshold This command means that if the module's suspend/resume time consume more than 10 us, the system will print the module's detail out. If you want to know the more details how to implement it on kernel, please check kernel/power/main.c Notes: Can use the shell command to enter different system level low power modes for debug (For more details: you can check Linux_6DQ_RM.pdf): #echo mem > /sys/power/state #echo standby > /sys/power/state How to do power optimization Runtime Mode Check whether CPUFreq and  Bus_freq scale are enabled root@android:/ # cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor root@android:/ # cat /sys/devices/platform/imx_busfreq.0/enable More details about this, please refer to "Documentation/cpu-freq/ governors.txt” . Check whether the system bus is working on your expected frequency. For MX6Q: root@android:/ #  cat /sys/kernel/debug/clock/osc_clk/pll2_528_bus_main_clk/periph_clk/mmdc_ch0_axi_clk/rate Check CPU Loading and Interrupt(cat /proc/interrupts)                root@android:/ #  cat /proc/interrupts                Through this command you can check whether some module will trigger interrupt frequently.  And consider that whether we have some chances to reduce the interrupt count. Check clock tree carefully to see which clocks are not gated off  but no any modules need them. root@android:/ # powerdebug -d -c Reduce GPU frequency.GPU also offered interface to modify the frequency. According to your own product, you can reduce the gpu frequency. Default gpu3DMaxClock is set to 64 in init.rc file, we can tuning a suitable value by ourselves. diff --git a/imx6/etc/init.rc b/imx6/etc/init.rc index 8c420b5..eb11ffe 100755 --- a/imx6/etc/init.rc +++ b/imx6/etc/init.rc @@ -397,6 +397,9 @@ on boot #  Set GPU 3D minimum clock to 3/64     write /sys/module/galcore/parameters/gpu3DMinClock 3 +#  Set GPU 3D maximum clock to 64/64 +   write /sys/module/galcore/parameters/gpu3DMaxClock 64 + Suspend Mode Check whether all devices enter suspend mode or low power mode: Add debug message into devices drivers to check whether all devices driver suspend interface are called Use oscilloscope to measure the related signal (depend on specific device datasheet and custom hw design) to check whether every device enter low power mode Remove devices from the board(or rmmod the device driver) , and do hardware rework to exclude some hardware module if needed. Then we can figure out which module introduced the high consumption, and debug into the specific module. Add debug message in device drivers which may lead high power consumption, catch the waveform from these modules which may impact the high power consumption Check whether DDR enter in self-refresh mode(Please check the DDR datasheet to figure out which pin indicate self-refresh state, and check it with oscilloscope) Config GPIO PADs as output zero or input mode (depending to HW design) Cut off LDOs/DCDCs which no modules need (depending to HW design) Check all PLLs will cut off, just 32KHZ sleep clock living
View full article
Question: When working with v1.6.0.55 using the standard profile for i.MX35 the tool fails most of the time when transferring the target root file system, on v1.6.0.42 it works just fine. The tags on the internal git don’t clearly mention a tool version, but a BSP. Wwhat are the differences between v1.6.0.55 and v1.6.0.42? Or to which tag(or commit) they correspond on git? Answer: 1.6.042 commit by looking at "Apps/MfgTool.exe/docs/changelog.txt": 1ca2a16df736ac51979a67423fef6a09bed6b7e2 And 1.6.055: "06a4f9190e34297b7273fc4bb4a92737e5bc837f"
View full article
Question: To eliminate the need for pull-ups AND  pull-downs on the gpio boot override pins to save board space, does anyone know when in the boot rom that the GPIO pins are sampled and whether the internal Pull Downs are already enabled? Is this true for all the GPIO override pins? To just be able to provide an external Pull-up to specify boot options and NOT both pull-up and pull-down option. Can this be done? Answer: The pull-ups and pull-downs are active while POR_B is low (as defined in the datasheet). The pins are sampled on the 2 nd rising edge of RTC_XTALO before the rising edge of POR_B. As a caution, on-chip pull-up/downs are very weak and are primarily intended for controlling the pin (keeping it from logically wiggling) if the pin is not connected at all. If a pin is connected out to a trace, relaying on the on-chip PU/PD alone could be a little risky. Since the PU/PD is weak, it's possible to have noise coupled onto the pin. [Similar to Brett's comment above].
View full article
Notes: + Run the pipelines in the presented order + The above example streams H263 video. + the gl command is equal to 'gst-launch' (two instead of 'gst-launch'.size() chars ) + Pending work: H264 test cases and other scenarios. Scenario Shell variables and pipelines # Export always these variables on the i.MX export VSALPHA=1 export WIDTH=320 export HEIGHT=240 export SEP=20 # decoded and displayed Uni-directional: from PC to i.MX. PC is streaming 4 H.263 streams and i.MX displays all in the screen. # On i.MX (Target) gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8890 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=0 axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8891 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=0 axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8892 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8893 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT & # On PC (Source) export IP_iMX= # Place the IP address of the i.MX board gst-launch -v videotestsrc ! ffenc_h263 ! rtph263pay ! multiudpsink clients=IP_iMX:8890,IP_iMX:8891,IP_iMX:8892,$IP_iMX:8893 Uni-directional: from PC to i.MX. PC is streaming one H.264 stream and i.MX displays it on the screen # On i.MX (Target) # Make sure you set the caps correctly, specially the sprop-parameter-sets cap. The one show below is just an example and works with the source file sintel_trailer-1080p.mp4 export VSALPHA=1 GST_DEBUG=*:2 gst-launch -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, sprop-parameter-sets=(string)\"Z2QAMqw05gHgCJ+WEAAAAwAQAAADAwDxgxmg\\,aOl4TLIs\", payload=(int)96' port=8890 ! rtph264depay ! vpudec ! mfw_isink sync=false # On PC (Source) gst-launch -v filesrc location=sintel_trailer-1080p.mp4 typefind=true ! qtdemux ! rtph264pay ! multiudpsink clients=10.112.102.168:8890 Bi-directional: PC is streaming 4 H.263 streams to i.MX, iMX displays it and sends the four back to PC # On i.MX export IP_PC= # Place the IP address of the PC host machine gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8890 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=0 axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9990 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8891 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=0 axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9991 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8892 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9992 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8893 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9993 & # On PC ## Stream received from iMX export IP_iMX= # Place the IP address of the i.MX board gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9990 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9991 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9992 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9993 ! rtph263depay ! ffdec_h263 ! xvimagesink & ## Stream sent to iMX gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 !  ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8890 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8891 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8892 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8893 &
View full article
Question: How is mx6 PMIC_ON_REQ under SW control? mx6 PMIC_ON_REQ is hooked up to the PFUZE100's PWRON and Linux and our 3.0.35bsp is used. Mx6 SW control is to drive the PMIC_ON_REQ pin low.  It appears from the documentation that this pin can be controlled by either another imx6 pin OR through SW control. The issue is that the reference manual is not clear on how to do this. While doing an SR search (SR 1-877711457), it does appear the PMIC_ON_REQ is controlled by SW. Answer: In latest RM version, Figure 60-3. Chip on/off state flow diagram and Table 60-3. Power mode transitions in IMX6DQRM.pdf show two ways to make PMIC_ON_REQ go low. I'm sure in latest BSP SW method had been included. It turns out the SNVS module on the mx6s/dl is different from the mx6q/d which is again different from the mx6slx. The bottom line is that the requirements for the SNVS functionality came primarily from the Android market so many of the Linux use cases are not supported. SW control of the PMIC_ON_REQ pin is an example of this. This means that you are correct, there only 2 ways to get PMIC_ON_REQ to power up for the mx6q/d 1 -  a low on the ON/OFF pin greater than the debounce time (750ms) 2 - a wake-up/tamper event. For the mx6s/dl, there are 3 ways to get PMIC_ON_REQ to power up 1 - power-on-reset on the VSNVS  (i.e first applying VSNVS) 2 -  a low on the ON/OFF pin greater than the debounce time (750ms) 3 - a wake-up/tamper event. Note, in my case, where there is an external input that actually wakes up the system, turns on the PMIC and brings up the mx6 there is only 1 way to get PMIC_ON_REQ to go back high 1 - a low on the ON/OFF pin greater than the debounce time (750ms) As it turns out, when the VSNVS_HP section is powered (i.e VDDHIGH is applied), it gates off the wake-up timer.
View full article
Question: What exactly does the DTE/DCE interface in the i.MX6's UART module do and how are RTS and CTS affected by the UARTxUFCR[DTEDCE] bit? In i.MX6 RM, revision 1: Sections 64.2.1.2.1  (CTS) and 64.2.1.2.2 (RTS) both state that CTS and RTS change direction between DCE and DTE modes.  However, sections 64.4.3.1 (RTS_B) and 64.4.3.8 (CTS_B) state they do not change functions.  Is this a documentation error, or is there a difference between CTS/RTS and CTS_B/RTS_B? It appears that some of this is covered in the IOMUX daisy chain by switching which pins are connected to CTS and RTS. Answer: Example 1: UART1 in DTE mode. RTS is an output from the UART IP block so it must be routed to a CTS pin. Therefore, the SELECT_INPUT register could only use settings 00 or 10. Example 2: UART1 in DCE mode. RTS is an input to the UART IP block so it must be routed to an RTS pin. Therefore, the SELECT_INPUT register could only be set to 01 or 11. At this point, we have assumed that the internal signals connected to the UART block do not change direction.  We believe that DCEDTE from the UART block connects into the IOMUX logic and controls the direction of the PAD.  Then, the IOMUX INPUT_SELECT mux is used to choose one of four pads to connect to the UART inputs while the IMOUX MUX_CTRL connects the output path.  Further, we assume it is an error to connect the UART input to a pad configured as an output or a UART output to a pad configured as an input. The attached shows our assumptions For the Uart IP, the CTS_B is always an output and RTS_B always an input. But the RTS_B &CTS_B IO will be swapped  when UART operates in different DTE or DCE mode.  IO port DTE mode DCE mode direction Uart IP port(internal) direction Uart IP port(internal) UART_CTS_B O CTS_B I RTS_B UART_RTS_B I RTS_B O CTS_B UART_TXD O TXD I RXD UART_RXD I RXD O TXD Regarding how to configure the IOMUX, please see the attached PDF.
View full article
Question: In a single uImage to contain the compressed kernel and rootfs, if the uImage is greater than 16MB, the system will not boot and reports errors. Is there a size limitation on uImage?  If so, is there a work around? Answer: uImage should only contains kernel compressed. rootfs should be read through a linux partition after the kernel boots up. Regarding the uImage's size, there is no limitation. In the other hand, a single uImage with kernel and filesystem is needed; in other words, kernel (alias uImage) needs a filesystem to work, and these are two independent systems in that sense. If u-boot, kernel and filesystem are in a single device (SD Card), the filesystem must be mounted in the first partition (SD, eMMC, etc) starting somewhere > 16M/512 sectors. But in cases where: * A fast boot is needed with  very small rootfs * As a intermediate (temporal) rootfs  before switching  to the real rootfs. The usage (actually used when flashing with the MFG tool) of this intermediate system is to load heavy modules, keeping the uImage small. This mechanism is called initramfs and the uImage will contain the kernel and the this mini rootfs compressed as cpio archive. But there appears to be a 16MB limitation. See here:  http://www.isysop.com/unpacking-and-repacking-u-boot-uimage-files/ It seems to be related to alignment suggesting that 24-bit addressing is used instead of 32-bit.  I did notice Thumb mode is used, which seems odd to me.
View full article
Question: If the i.mx6’s internal real time clock is not used,  instead an external I2C device is used,  does this create a problem with using any of the i.mx6’s security features? Answer: iMX6 Secure features uses and internal real time counter (SRTC) which if enabled and reaches the maximum value it generates an interrupt informing a security violation. External RTC can't be used in security iMX6 context. I2C external RTC for applications is needed, but for security features SNVS uses the internal SRTC. Question: If I'm interpreting your comments correctly - The customers external RTC can't be used in the context of iMX6 security but can still used be used for their applications needs.  To utilize the security features of the SNVS Module (RM Chp. 60), it must use the internal SRTC.  Disabling or otherwise not implementing the requirements the SNVS module has a cascading effect on many other security features such as High-Assurance Boot (HAB) and CAAM operation.  So it seems that if the customer must have an external RTC, they should still implement the requirements of the internal SNVS/SRTC. Answer: That's the case if secure features are needed they will end up using the internal SRTC, actually I don't think is possible to be used in other scenario as is part of SNVS. Question: To better understand the implications of not having battery backup for the SNVS supply as it pertains to security, if it is normally powered all the time via either a local AC supply or POE+ and is never powered down except for service, and reboots are done with a pushbutton. Given this, can you list what types of security features cannot be implemented or will be problematic? Answer: ???
View full article
Question: How to enable touch functions on LVDS1/SabreAI base board? what should be soldered in order to connect the signals to i2c what to add in the Linux kernel (board-mx6q_sabreauto.c) BTW.: Why did we leave these disconnected? Is there any conflict on i2c? Answer: You can mount R305 and R306 to support touch on LVDS1, no code modification was needed. The only limitation is that the two LVDS's touch can't be connected to same I2C port, because they are using the same I2C address. Question: How is this working because the touch interrupt signal from LVDS1 called LCD1_TOUCH_INT_B is connected to pin21 on J44 on base board which is left floating (TP1) on CPU card P1A connector? Are both LVDS needed to work in the same time. Answer: That's the problem, the LVDS1 touch interrupt pin hasn't been connected to IMX6 CPU. Maybe you can use the SabreSD board, the two touch are ready on that board.
View full article
Question: 1)      Is WDOG2 somehow accessible from customers code in normal mode? Is it only used within the trust zone to protect against DOS attacks from normal world?) 2)      Is there any mechanism preventing changing of the watchdog registers like being able to write them only during a period after Reset? If yes, which registers are protected? Answer: WDOG1 and WDOG2 are identical the only difference is how the signals are connected. There is nothing presenting someone from using both WDOGs for non-secure purposes. There is no time window for WDOG access but there are some write-once only bits in the register, which can be written only once after reset, after that all following writes will be ignored. They are clearly described in the RM. The bits are: WDZST, WDBG, WDW, WDE, WDT, WIE, WICT, and PDE.
View full article
Question: Did we tested active PCIe components while the Cortex-A9 was in Sleep Mode (suspend to memory)? Answer: It's a known issue that PCIe can't support suspend/resume. And can't be built in kernel image if the system want suspend/resume. I think PCIe will be active while core is in sleep more. Is it different scenario? No, the pcie core is not active, it is in L2 state after suspend, and it can't resume back to L0 state when system resume is called. So, DO NOT let pcie do suspend operation right now. BTW, the tested device: * INTEL x1 1000M CT network card. * INTEL iwl wifi cards. * x1 pcie to usb3.0 card Yes, this patch had been tested on imx_3.0.35_4.0 release, and would be merged into next 3.0.35 release. TO1.2 is used. We tested the Patch against imx_3.0.35_4.0 release
View full article
Quaestion: What does exactly the RNG_TRIM after burning the SRK hash table? There is no such thing on the former i.MX HAB procedure. What would a random generator stuff bring here? Additionnally, there is the possibility to lock the SRK shadow register via an OTP bit. Is it recommeneded to lock it? if not, is it really possible to change the SRK hash value by modofying the shadow register value before performing the SRK hash key check in a HAB boot process? One last question: the PKI requires the user to enter a certificate lifetime. Does that really mean that openssl will refuse generating new signatures once the certificates lifetime is expired? Answer: 1. The intent of the of the RNG_TRIM fuses is for Freescale to essentially extendthe amount of time the RNG4 in CAAM has to generate entropy.  The longer this period the more likely it is that RNG4 will generate entropy that will pass its internal statistical tests.  The reason for the fuses is HAB (in the Closed configuration only) instantiates the RNG by default and needs some external indication on how to progran the RNG4 in CAAM to ensure the internal HW statistical tests will pass.  This was to allow the RNG to be useable by application code after execution has left the ROM.  However this requires that the RNG_TRIM fuse value be fully characterized across numerous conditions temperature, voltage etc.  This effort is still on going.  For customers performing secure boot (in Closed configuration) we recommend they follow Section 6.3 of http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf.  In this case the RNG4 can be instantiated by CAAM driver code which can be easily changed if required. 2. Yes, once the SRK hash is provisioned to the SRK_HASH field it is recommended to blow the corresponding SRK_LOCK fuse.  If the SRK_LOCK fuse is not blown then additional fuses in the SRK_HASH field can be blown.  This will cause devices in the closed configuration to fail to boot.  i.e. "bricking" the device. 3. Please see https://community.freescale.com/message/334186#334186 for the answer to your question on the certificate validity period.
View full article
Question: The description of the IOMUXC_GPR2 register is wrong. It contains exactly the same description as the LDB_CTRL register. The bits in the LDB_CTRL register work as advertised opposed to the GPR2 register. Answer: This is intentional. The LDB_CTRL description in the RM says "The register is implemented in the IOMUX Controller block (IOMUXC), as the register IOMUXC_GPR2.". And you will notice the two registers have the same address.
View full article
Question: Is SN65LVDS315 (MIPI CSI-1) compatible with our i.MX6 MIPI CSI-2 interface? CSI-2 extends CSI-1 with multiple lanes, but both standards use the same D-PHY layer. Answer: No, the i.MX6 MIPI CSI-2 interface is not compatible with CSI-1 devices. Standards that require backward compatibility to legacy standards always state that the standards are backward compatible. The CSI-2 standard does not say that. (I have a copy of the standard and I have read it specfically for that reason)  The CSI-2 standard does say that a specifically designed PHY, built to D-PHY MIPI01 specification is used for CSI-2. The PHY's used for CSI-1 and CSI-2 are different and they are not compatible. There are some processors that do have compatiblity for CSI-1 and CSI-2, but if you read closer, you will find that they have two different modes (and probably two different sets of pins): One for CSI-2 and One for CSI-2/CSI-1 legacy. It is interesting that a company would choose to inlcude a dying technology in a newer processor, but my guess is that they have a number of other CSI-1 devices they are trying to sell before they can't be used anywhere and nobody wants them. if the customer is looking for a parallel camera interface to CSI-2 converter IC, may I recommend the Toshiba TC358746 device. I have not used it specifically, but I have worked with a Toshiba rep on an HDMI to MIPI CSI-2 project that input into the i.MX6 processor. Once all the correct parameters were determined, it worked very well. Much higher data rate flow.
View full article
Question: The following contradicting information regarding the UART clock tree has been seen in the Rev. 1.0  version of the reference manual: Page 813: PLL3_PFD1 -> divide by 6 -> adjustable post divider -> UART Page 839: PLL3 -> divide by 6 -> UART In the old Rev D I found: Page 803: PLL3 -> divide by 6  ... and something about 80MHz The assumption is that correct path would be: PLL3 -> divide by 6 -> post divider -> UART. Answer: The designer said that UART _CLK_ROOT comes from PLL3 (not PLL3:PFD1) and is divided by 6 to produce 80 MHz. I'm waiting for him to confirm that the divider he mentions is CSCDR1[UART_CLK_PODF].
View full article
Question: Using Linux SDK 4.1.0, with CAAM drivers enabled, there is little noticeable difference in the performance of openssd compared to a kernel without the CAAM drivers. Tests were done using openssd. Test image AES-128 8192 byte block (M Bytes/sec) “openssl speed –evp aes-128-cbc” AES-128 8192 byte block (M Bytes/sec) With /dev/crypto “openssl speed –evp aes-128-cbc -engine cryptodev”  Ubuntu 11.04 Image 19.010 N/A Timesys 20.518 N/A SDK 4.1.0 LTIB 22.013 21.984 (errors reported) One can see that with SDK 4.1.0, performance is worse with crypto enabled.  This is probably due to the overhead of a faulty driver or incorrect implementation. The lowest number is for Ubuntu which could be attributed to the Unity GUI. Conclusion:  CAAM driver is not functional or I am using an improper testing procedure. Test Procedure: Board used is iMX6Q Sabre SDP Openssl was used for testing. Two command line commands were used, with and without the cryptodev engine. openssl speed –evp aes-128-cbc openssl speed –evp aes-128-cbc -engine cryptodev Openssl versions used in each build are slightly different: Ubuntu:              openssl 1.0.0e Timesys:              openssl  1.0.1e SDK 4.1.0:            openssl  1.0.1c Three versions of Linux were tested. Default kernel  4.0.0 with Ubuntu rootfs form image tarballs. Timesys kernel and root file system Kernel built with SDK 4.1.0 using LTIB with hardware crypto enabled Both 1 and 2 above did not have CRYPTODEV set in .config which contains the line “# CONFIG_CRYPTO_CRYPTODEV is not set” Option 3 had the line in .config as, “CONFIG_CRYPTO_CRYPTODEV=y” All three builds generate “/proc/crypto”  whose contents are attached.  A partial listing of /proc/crypto lists “caam” as a driver for all encryption methods supported.  Example printout for aes shown below: ame         : cbc(aes) driver       : cbc-aes-caam module       : kernel priority     : 3000 refcnt       : 1 selftest     : passed type         : ablkcipher async        : yes blocksize    : 16 min keysize  : 16 max keysize  : 32 ivsize       : 16 geniv        : eseqiv All three builds have “caam” and “enable_wait_mode=off” in the kernel command line in u-boot. Only option #3 contains both device file in “/dev/crypto” and an entry in “/proc/crypto” root@freescale ~$ cd / root@freescale /$ ls /proc/cr* /proc/crypto root@freescale /$ ls /dev/cr* /dev/crypto root@freescale /$ Test #1—Kernel build 4.1.0 openssl speed test without caam engine root@freescale ~$ openssl speed -evp aes-128-cbc                    Doing aes-128-cbc for 3s on 16 size blocks: 3471184 aes-128-cbc's in 2.94s Doing aes-128-cbc for 3s on 64 size blocks: 986286 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 256 size blocks: 249743 aes-128-cbc's in 2.93s Doing aes-128-cbc for 3s on 1024 size blocks: 64343 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 8192 size blocks: 7954 aes-128-cbc's in 2.96s OpenSSL 1.0.1c 10 May 2012 built on: Sat Sep 7 18:47:34 PDT 2013 options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) idea(int) blowfish(ptr) compiler: gcc -fPIC -DOPENSSL_PIC -DOPENSSL_THREADS -D_REENTRANT -DDSO_DLFCN -DHAVE_DLFCN_H -DL_ENDIAN -DTERMIO -O3 -fomit-frame-pointer -Wall The 'numbers' are in 1000s of bytes per second processed. type 16 bytes     64 bytes    256 bytes 1024 bytes   8192 bytes aes-128-cbc 18890.80k    21040.77k    21820.55k 21962.41k    22013.23k root@freescale ~$ Test #2—Timesys kernel build of openssd without /dev/crypto # openssl speed -evp aes-128-cbc Doing aes-128-cbc for 3s on 16 size blocks: 3361305 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 64 size blocks: 924423 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 256 size blocks: 236623 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 1024 size blocks: 59967 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 8192 size blocks: 7514 aes-128-cbc's in 3.00s OpenSSL 1.0.1e 11 Feb 2013 built on: Thu Sep 5 21:54:37 EDT 2013 options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) blowfish(ptr) compiler: armv7l-timesys-linux-gnueabi-gcc -fPIC -DOPENSSL_PIC -DOPENSSL_THREADS -D_REENTRANT -DDSO_DLFCN -DHAVE_DLFCN_H -I/here/workdir/factory/build_armv7l-times ys-linux-gnueabi/toolchain/usr/include -DL_ENDIAN -DTERMIO -DOPENSSL_NO_KRB5 -DOPENSSL_NO_IDEA -DOPENSSL_NO_MDC2 -DOPENSSL_NO_RC5 -Os -pipe -Wa,--noexecstack -Wall The 'numbers' are in 1000s of bytes per second processed. type 16 bytes     64 bytes    256 bytes 1024 bytes   8192 bytes aes-128-cbc 17926.96k    19721.02k    20191.83k 20468.74k    20518.23k #  Test #3—Ubuntu rootfs and kernel image root@linaro-ubuntu-desktop:/# openssl speed -evp aes-128-cbc Doing aes-128-cbc for 3s on 16 size blocks: 3030128 aes-128-cbc's in 2.98s Doing aes-128-cbc for 3s on 64 size blocks: 852897 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 256 size blocks: 220572 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 1024 size blocks: 55534 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 8192 size blocks: 6846 aes-128-cbc's in 2.95s OpenSSL 1.0.0e 6 Sep 2011 built on: Wed Oct 5 01:45:02 UTC 2011 options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) blowfish(ptr) compiler: cc -fPIC -DOPENSSL_PIC -DZLIB -DOPENSSL_THREADS -D_REENTRANT -DDSO_DLFCN -DHAVE_DLFCN_H -DL_ENDIAN -DTERMIO -O2 -Wa,--noexecstack -g -Wall The 'numbers' are in 1000s of bytes per second processed. type             16 bytes     64 bytes 256 bytes   1024 bytes   8192 bytes aes-128-cbc 16269.14k    18195.14k    18822.14k 18955.61k    19010.99k root@linaro-ubuntu-desktop:/# Test #4—SDK 4.1.0 openssl speed test with “/dev/crypto” .  Note errors. root@freescale ~$ openssl speed -evp aes-128-cbc -engine cryptodev  invalid engine "cryptodev" 716715216:error:25066067:DSO support routines:DLFCN_LOAD:could not load the shared library:dso_dlfcn.c:187:filename(/usr/lib/engines/libcryptodev.so): /usr/lib/eng ines/libcryptodev.so: cannot open shared object file: No such file or directory 716715216:error:25070067:DSO support routines:DSO_load:could not load the shared library:dso_lib.c:244: 716715216:error:260B6084:engine routines:DYNAMIC_LOAD:dso not found:eng_dyn.c:450: 716715216:error:2606A074:engine routines:ENGINE_by_id:no such engine:eng_list.c:417:id=cryptodev 716715216:error:25066067:DSO support routines:DLFCN_LOAD:could not load the shared library:dso_dlfcn.c:187:filename(libcryptodev.so): libcryptodev.so: cannot open shared object file: No such file or directory 716715216:error:25070067:DSO support routines:DSO_load:could not load the shared library:dso_lib.c:244: 716715216:error:260B6084:engine routines:DYNAMIC_LOAD:dso not found:eng_dyn.c:450: Doing aes-128-cbc for 3s on 16 size blocks: 3572980 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 64 size blocks: 966002 aes-128-cbc's in 2.94s Doing aes-128-cbc for 3s on 256 size blocks: 255307 aes-128-cbc's in 3.00s Doing aes-128-cbc for 3s on 1024 size blocks: 62967 aes-128-cbc's in 2.93s Doing aes-128-cbc for 3s on 8192 size blocks: 7890 aes-128-cbc's in 2.94s OpenSSL 1.0.1c 10 May 2012 built on: Sat Sep 7 18:47:34 PDT 2013 options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) idea(int) blowfish(ptr) compiler: gcc -fPIC -DOPENSSL_PIC -DOPENSSL_THREADS -D_REENTRANT -DDSO_DLFCN -DHAVE_DLFCN_H -DL_ENDIAN -DTERMIO -O3 -fomit-frame-pointer -Wall The 'numbers' are in 1000s of bytes per second processed. type 16 bytes     64 bytes    256 bytes 1024 bytes   8192 bytes aes-128-cbc 19055.89k    21028.61k    21786.20k 22006.21k    21984.65k root@freescale ~$ Answer: I do not know what is recent state of official Freescale BSP regarding CAAM, but to get OpenSSL working under CAAM support with reasonable acceleration  : https://community.freescale.com/message/318188#318188 The patches was used below : http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.0.35_4.0.0 Direct link to the patches: http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_3.0.35_4.0.0&id=6068d7a77b2101c172fc2f003f90b1febbf99505 http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_3.0.35_4.0.0&id=b30237c79003223c6e8035d5be183cd4f0b469f9
View full article
Question: What’s the best way to rotate a MX6 image 90 degrees, thought the IPU correct? IPU is limited to 1024x1024. Apparently we don’t support frame buffer rotation in the IPU, so we have to use some middleware. I know that Android’s surface flinger uses the GPU but do you know what we can use in Linux that uses H/W acceleration also? It looks look like X-server can rotate only when the Vivante driver is not  loaded, which means the hardware is not implementing rotations. Answer: it should be possible to split the picture into two halves and rotate them separately. Well, two halves if you can reduce the line count to 1024 … otherwise it would be 4 rotates. X11 Xrandr will be implemented on GPU sometime this year. It's in the R&D queue but as low priority. They could use GC320 low level API to rotate (if they use linux frame buffer). It implies a blit but it would be done by GC320 they will probably need to use virtualFB too. The API documentation is the BSP documentation (iMX6.2D.API.pdf) Attached a simple source using the 2D low level API. VirtualFB: https://community.freescale.com/message/289198
View full article