Q&A: Errors in the i.MX6 reference manual regarding the clock tree for the UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Q&A: Errors in the i.MX6 reference manual regarding the clock tree for the UART

Q&A: Errors in the i.MX6 reference manual regarding the clock tree for the UART

Question:
The following contradicting information regarding the UART clock tree has been seen in the Rev. 1.0  version of the reference manual:

Page 813:

PLL3_PFD1 -> divide by 6 -> adjustable post divider -> UART

Page 839:

PLL3 -> divide by 6 -> UART

In the old Rev D I found:

Page 803:

PLL3 -> divide by 6  ... and something about 80MHz

The assumption is that correct path would be:

PLL3 -> divide by 6 -> post divider -> UART.

Answer:

The designer said that UART _CLK_ROOT comes from PLL3 (not PLL3:PFD1) and is divided by 6 to produce 80 MHz.

I'm waiting for him to confirm that the divider he mentions is CSCDR1[UART_CLK_PODF].

标签 (1)
标记 (2)
无评分
版本历史
最后更新:
‎09-23-2013 01:26 AM
更新人: