NXP Tech Blog - Page 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Tech Blog - Page 10

BlackNight
NXP Employee
NXP Employee

Amazon Web Services has released a preconfigured FreeRTOS example for Armv8-M and the NXP LPCXpresso55S69 board. With the addition of board- and device-specific examples, it is even easier to start and use the Arm® TrustZone® features combined with MPU (Memory Protection Unit) on the NXP LPC55xx MCU.

Read more...

More
1 0 3,459
xiaodong_zhang
NXP Employee
NXP Employee

GmSSL是一个开源的密码工具箱,支持SM2/SM3/SM4/SM9/ZUC等国密(国家商用密码)算法、SM2国密数字证书及基于SM2证书的SSL/TLS安全通信协议,提供符合国密规范的编程接口与命令行工具,可以用于构建PKI/CA、安全通信、数据加密等符合国密标准的安全应用。GmSSL项目是OpenSSL项目的分支,并与OpenSSL保持接口兼容。因此GmSSL可以替代应用中的OpenSSL组件,并使应用自动具备基于国密的安全能力。GmSSL项目采用对商业应用友好的类BSD开源许可证,开源且可以用于闭源的商业应用。

Read more...

More
1 1 5,115
BlackNight
NXP Employee
NXP Employee

The ARM TrustZone is an optional secu=rity feature for Cortex-M33 which shall improve the security for embedded applications running on microcontroller as the NXP LPC55S69 (dual-core M33) on the LPC55S69-EVK.

Read more...

More
1 1 7,172
BlackNight
NXP Employee
NXP Employee

This article covers the NXP LPC55S69-EVK board: a dual ARM Cortex-M33 running at 100 MHz with ARM TrustZone

Read more...

More
1 0 4,863
PetrKraus
NXP Employee
NXP Employee

Comprehensive information about SDK SW components and SDK release describing YML can be found in the Yml data record guide here:

http://10.193.108.154:4000/mcu-sdk-generator/doc/Yml%20data%20record%20guide.html#add-a-middleware-y...

Example

We need to build a dependency from the eIQ component to the CMSIS DSK Library component.

Read more...

More
2 0 1,841
nxf47831
NXP Employee
NXP Employee

New features update:

  •  SDKGEN-924Support to automatically link secure and non-secure projects in Mcuxpresso IDE

        This feature supports to link trustzone projects. In MCUXpresso IDE, if you select a secure project or non-secure         project, the other trustzone paired project will be selected automatically.
        In order to enable the feature, "linked_project" need to be set for both projects.

Read more...

More
1 0 1,895
BlackNight
NXP Employee
NXP Employee

In “Tutorial: MCUXpresso SDK with Linux, Part 1: Installation and Build with Maked” I used cmake and make to build the SDK application. In this part I’m going to use the command line gdb to debug the application on the board.

Read more...

More
0 0 5,252
BlackNight
NXP Employee
NXP Employee

I admit: my work laptop machine is running a Windows 10 OS by default. But this does not prevent me running Linux in a Virtual Machine (VM). Each host platform has its benefits, and I don’t feel biased to one or the other, but I have started using Ubuntu more and more, simply because I have worked more on Embedded Linux projects. While I have used mostly Windows with Eclipse for NXP LPC, Kinetis and i.MX platforms in the past, I started using Ubuntu too from last year with the NXP MCUXpresso SDK. I did not find much documentation about this on the web, so I thought it might be a good idea to write a tutorial about it. So here we go…

Read more...

More
2 0 12.1K
Kathleen
NXP Employee
NXP Employee

The way in which people digest information is changing, as more distractions lead way to shorter attention spans and multi-tasking becomes even more important.  The new training series from NXP, i.MX RT Tech Minute, is intended to address this.  The need for technical information present in things like webinars, applications notes, white papers, etc. is important.  But what if you do not even know which topic you are interested in?  How do you know where to get started?

Read more...

More
0 0 1,852
PetrKraus
NXP Employee
NXP Employee

If you need to create of modify YML files describing SDK release and included SW components, you can get detailed information about a format of those YML files here:

https://bitbucket.sw.nxp.com/projects/MCUCORE/repos/mcu-sdk-generator/browse/doc/Yml%20data%20record...

Read more...

More
2 0 1,815
Kathleen
NXP Employee
NXP Employee

As a marketer, I never like to use the suffix “less” as it usually has a negative connotation.  “Less” means not having; without; free from something. Words like hopeless, motionless, and helpless come to mind.  So, when a system architect recently spoke to me about the products in the i.MX RT series and referred to them as being flashless, I cringed a little.

But, is being flashless such a bad thing?  Yes, it means it has no flash memory on-chip, but that is actually giving customers more - More opportunity for differentiated on-chip peripherals.  More options for selecting the perfect memory.  And more opportunity to create cost competitive solutions.

Read more...

More
0 0 1,726
tomaslestyan
NXP Employee
NXP Employee

ENG

TODO

 

CZ-SK

Vytvorenie témy

Dokument je možné vytvoriť na internej komunite dostupnej výhradne NXP zamestnancom. Po tom čo zadanie splní všetky potrebné náležitosti, bude presunuté na verejne dostupnú komunitu.

Vzor pre vytvorenie témy*.

Read more...

More
1 0 1,465
nxf47831
NXP Employee
NXP Employee

New features update:

  •  SDKGEN-865Support IAR compiler optimization strategy flag for library projects

        Compiler Optimization flags are supported for IAR application and library projects:

        1. -On / -Ol / -Om / -Oh / -Oh -Ssize / -Oh -Sspeed / -Oh -Sbalance / --no_size_contraints

Read more...

More
1 0 1,639
BlackNight
NXP Employee
NXP Employee

I really love tiny and bread board friendly boards, especially if they are very affordable and can be use with Eclipse based tools. So I was excited to see the NXP LPC845-BRK board to be available at Mouser, so I ended up ordering multiple boards right away. Why multiple? Because they only cost CHF 5.95 (around $6)!

Read more...

More
1 0 3,027
PetrKraus
NXP Employee
NXP Employee

Non-production mode (debug mode - without the production flag):

  • Returns 0 if everything is ok
  • Returns 1 if there are major cases failed, anyway the process will passed.
  • Returns 2 if there are critical cases failed, process aborts
Read more...

More
0 0 1,646
PetrKraus
NXP Employee
NXP Employee

SDK Release data tables are outputs of the SDK Generator core. These tables are actually YML files, which are inputs to next phases of the SDK generation process, like the SDK manifest generation, SDK release deployment data file generation, CMSIS pack generation and the Package Builder. The data tables are included into the SDK release superset.

Read more...

More
0 0 1,691
nxf47831
NXP Employee
NXP Employee

New features update:

  • KPSDK-26034components under components folder should be set "type". Newly added types are as following:

       Abstraction Layer: abstraction_layer ------- Extensions of SDK drivers unifying API

       Software Components: software_component ------- Pure SW components 

       Board Components: board_component ------ Drivers of on-board devices (drivers for devices on the evaluation boards)

Read more...

More
0 0 1,779
nxf47831
NXP Employee
NXP Employee

New features update:

SDKGEN-737 Support DSP project with Cadence IDE for HIFI4

  • Cadence Xtensa Xplorer, as a new toolchain, has been supported in sdk generator, and yml configure rule align with existent toolchains.
    You can generate xtensa project in two way if board supports this toolchain :
    • Add 'xtensa' toolchain in release configure yml
    • Run batch with parameter -t xtensa
Read more...

More
1 0 1,634
nxf47831
NXP Employee
NXP Employee

New features update:

  • SDKGEN-829 Support debug component and debug mode
    • The debug component will only be visible when generator is running in debug mode. User can use parameter "--debug_mode" to enter debug mode. Without --debug_mode, these components will not appear in projects/manifest/packages/cmsis pack
    • The debug component should be added into yml data record with debug_support: true
      For example, add tag in I2C component yml:
Read more...

More
1 0 1,633
lpcxpresso_supp
NXP Employee
NXP Employee

First Release v1.00 : 22nd February 2019

 

Please find attached a document detailing how to create, build and debug LPC55xx multicore applications using the LPC55S69-EVK LPCXpresso55S69 Development Board with MCUXpresso IDE v10.3.1 and MCUXpresso SDK v2.5.0

Read more...

More
1 0 7,252
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v10.3.1 (build 2233) is now available.

This is a maintenance release that builds upon the previous MCUXpresso IDE v10.3.0 release, and we recommend that all existing users download and install this new version.

Read more...

More
0 0 6,595
BlackNight
NXP Employee
NXP Employee

The LPC845-BRK is a great tiny sub-$6 breakout board featuring the LPC845M301JBD4 MCU:

  • ARM Cortex-M0+
  • 30 MHz, 64 KByte FLASH, 16 KByte SRAM
  • On-board CMSIS-DAP debug interface, works out-of-the-box with NXP MCUXpresso IDE or other 3rd party IDEs
  • 3 push buttons (user, RESET, ISP)
  • RGB LED
  • Potentiometer
Read more...

More
3 1 7,255
nxf47831
NXP Employee
NXP Employee

New features updates:

  • SDKGEN-778 Support to dump minimum merged yml information without generating all IDE projects by passing parameter “-d”

       To quickly parse SDK examples list for the special board then create CI test scope, you can get a minimum merged yaml information that dumped by SDK generator script with "-d" parameter.

Read more...

More
1 0 1,583
BlackNight
NXP Employee
NXP Employee

The following article is a step-by-step tutorial how to use the NXP MCUXpresso SDK & IDE to create a SD card bootable image on i.MX RT. It features the i.MX RT1050-EVK(B) but is with minor changes applicable to any other i.MX RT device

Read more...

More
1 0 2,883
lpcxpresso_supp
NXP Employee
NXP Employee

Updated v1.02  1st March 2019

Please find attached a document detailing various features related to using the iMXRT1060-EVK evaluation board with MCUXpresso IDE v10.3.x and SDK v2.5, including details of how to enable SWO trace on this MCU.

Updated to include a section on the MIMXRT1064 EVK.

Read more...

More
2 0 9,722
brendonslade
NXP TechSupport
NXP TechSupport

We've been working on making the flagship member of the LPC800 series more accessible to more users than ever before, and are delighted to announce the LPC845 Breakout Board is now available from our distribution partners and also direct from nxp.com! Setting a new price point for a fully featured, debug enabled platform, this board includes CMSIS-DAP compatible debug and a VCOM port in a very compact yet flexible form factor. Of course it can be used with MCUXpresso IDE, Keil, IAR and other popular tools.

Read more...

More
1 0 1,365
nxf47831
NXP Employee
NXP Employee

New features update:

  • SDKGEN-724 Set different log level for "internal" projects.

       "Internal" examples, like some library projects, are not released.  Therefore some attributes like "brief" and "version" are not required strictly. The generator has downgraded the log level from error to warning. In production mode, they won’t break down the cmd run.

Read more...

More
1 0 1,536
dishapatil14941
Contributor I

Using SDK drivers for LPC845 Breakout Board, this project measures the ambient light intensity by using LDR (Light Dependent Resistor). The voltage values from LDR are read through an ADC. The new LPC845 Breakout board has an SDK support which makes it a lot easier to interface an LDR for measuring light intensity compared to the conventional coding style. I have used the MCUXpresso IDE for modifying the pins and clock configuration settings.

Read more...

More
0 0 2,681
DishaPatil
NXP Employee
NXP Employee

The new LPC845 breakout board has 3 onboard LEDs- Red, Green, and Blue. The brightness of these LEDs can be controlled using a PWM signal by changing the duty cycle values for each of them. As this board has an SDK support, I have used the SDK drivers to implement this application. 

 

Read more...

More
0 1 4,314
DishaPatil
NXP Employee
NXP Employee

I have built an application to interface an accelerometer with the new LPC845 Breakout board using the I2C SDK driver.
The accelerometer acts as an I2C slave device to the LPC845 master device. Colors on the on-board RGB LED change according to the accelerometer position.
 
The accelerometer is a slave device in this application with slave address: 0x1D. The position of the board is determined by the x,y,z-axis values obtained from this slave device. The change in these x,y,z values detects the movement of the LPC845 Breakout board. I have assigned various patterns to the RGB LEDs for each movement along the y-axis. 
Read more...

More
0 0 3,403