SDK Release data tables

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK Release data tables

PetrKraus
NXP Employee
NXP Employee
0 0 2,210

SDK Release data tables are outputs of the SDK Generator core. These tables are actually YML files, which are inputs to next phases of the SDK generation process, like the SDK manifest generation, SDK release deployment data file generation, CMSIS pack generation and the Package Builder. The data tables are included into the SDK release superset.

Example: SDK release 9

Superset z the latest RC: https://bitbucket.sw.nxp.com/projects/MCUCORE/repos/mcu-kex/browse?at=refs%2Ftags%2FREL_2.5.0_REL9_R...

Device datatable files: ‘devices/<short_name>/<short_name>.yml’

Boafrd datatable files (boards and kits): ‘boards/<board_name>/<board_name>.yml’

Relations between boards and kits and additional information about kits: boards/board_kit_map.yml